![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _dsi_smartdma_write_mem_transfer |
| The pixel format sent on MIPI DSI data lanes. More... | |
| struct | _dsi_smartdma_handle |
| MIPI DSI transfer handle structure. More... | |
Typedefs | |
| typedef void(* | dsi_smartdma_callback_t )(MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, status_t status, void *userData) |
| MIPI DSI callback for finished transfer. More... | |
| typedef enum _dsi_smartdma_input_pixel_format | dsi_smartdma_input_pixel_format_t |
| The pixel format feed SMARTDMA. More... | |
| typedef enum _dsi_smartdma_output_pixel_format | dsi_smartdma_output_pixel_format_t |
| The pixel format sent on MIPI DSI data lanes. More... | |
| typedef struct _dsi_smartdma_write_mem_transfer | dsi_smartdma_write_mem_transfer_t |
| The pixel format sent on MIPI DSI data lanes. More... | |
Enumerations | |
| enum | _dsi_smartdma_input_pixel_format { kDSI_SMARTDMA_InputPixelFormatRGB565, kDSI_SMARTDMA_InputPixelFormatRGB888, kDSI_SMARTDMA_InputPixelFormatXRGB8888 } |
| The pixel format feed SMARTDMA. More... | |
| enum | _dsi_smartdma_output_pixel_format { kDSI_SMARTDMA_OutputPixelFormatRGB565, kDSI_SMARTDMA_OutputPixelFormatRGB888 } |
| The pixel format sent on MIPI DSI data lanes. More... | |
Driver version | |
| #define | FSL_MIPI_DSI_SMARTDMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
Transactional | |
| status_t | DSI_TransferCreateHandleSMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, dsi_smartdma_callback_t callback, void *userData) |
| Create the MIPI DSI SMARTDMA handle. More... | |
| status_t | DSI_TransferWriteMemorySMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, dsi_smartdma_write_mem_transfer_t *xfer) |
| Write display controller video memory using SMARTDMA. More... | |
| void | DSI_TransferAbortSMARTDMA (MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle) |
| Abort current APB data transfer. More... | |
| struct _dsi_smartdma_write_mem_transfer |
Data Fields | |
| dsi_smartdma_input_pixel_format_t | inputFormat |
| Input format. More... | |
| dsi_smartdma_output_pixel_format_t | outputFormat |
| Output format. More... | |
| const uint8_t * | data |
| Pointer to the data to send. More... | |
| bool | twoDimension |
| Whether to use 2-dimensional transfer. More... | |
| size_t | dataSize |
| The byte count to be write. More... | |
| size_t | minorLoop |
| SRC data transfer byte count in a minor loop, only used in 2-dimensional transfer. More... | |
| size_t | minorLoopOffset |
| SRC data byte offset added after a minor loop, only used in 2-dimensional transfer. More... | |
| size_t | majorLoop |
| SRC data transfer in a major loop of maw many minor loop is transfered, only used in 2-dimensional transfer. More... | |
| uint8_t | virtualChannel |
| Virtual channel used in the transfer, current driver always use channel 0, added for future enhancement. More... | |
| bool | disablePixelByteSwap |
| If set to true, the pixels are filled to MIPI DSI FIFO directly. More... | |
| dsi_smartdma_input_pixel_format_t _dsi_smartdma_write_mem_transfer::inputFormat |
| dsi_smartdma_output_pixel_format_t _dsi_smartdma_write_mem_transfer::outputFormat |
| const uint8_t* _dsi_smartdma_write_mem_transfer::data |
| bool _dsi_smartdma_write_mem_transfer::twoDimension |
| size_t _dsi_smartdma_write_mem_transfer::dataSize |
In 2-dimensional transfer, this parameter is ignored.
| size_t _dsi_smartdma_write_mem_transfer::minorLoop |
| size_t _dsi_smartdma_write_mem_transfer::minorLoopOffset |
| size_t _dsi_smartdma_write_mem_transfer::majorLoop |
| uint8_t _dsi_smartdma_write_mem_transfer::virtualChannel |
| bool _dsi_smartdma_write_mem_transfer::disablePixelByteSwap |
If set to false, the pixel bytes are swapped then filled to MIPI DSI FIFO. For example, when set to false and frame buffer pixel format is RGB565: LSB MSB B0 B1 B2 B3 B4 G0 G1 G2 | G3 G4 G5 R0 R1 R2 R3 R4 Then the pixel filled to DSI FIFO is: LSB MSB G3 G4 G5 R0 R1 R2 R3 R4 | B0 B1 B2 B3 B4 G0 G1 G2
| struct _dsi_smartdma_handle |
Data Fields | |
| MIPI_DSI_HOST_Type * | dsi |
| MIPI DSI peripheral. More... | |
| volatile bool | isBusy |
| MIPI DSI is busy with data transfer. More... | |
| dsi_smartdma_callback_t | callback |
| DSI callback. | |
| void * | userData |
| Callback parameter. | |
| uint32_t | smartdmaStack [16] |
| Stack for smartdma function. More... | |
| smartdma_dsi_param_t | param |
| Parameter for smartdma function. More... | |
| smartdma_dsi_2d_param_t | param2d |
| Parameter for 2-dimensional smartdma function. More... | |
| MIPI_DSI_HOST_Type* _dsi_smartdma_handle::dsi |
| volatile bool _dsi_smartdma_handle::isBusy |
| smartdma_dsi_param_t _dsi_smartdma_handle::param |
| smartdma_dsi_2d_param_t _dsi_smartdma_handle::param2d |
| uint32_t _dsi_smartdma_handle::smartdmaStack[16] |
| typedef void(* dsi_smartdma_callback_t)(MIPI_DSI_HOST_Type *base, dsi_smartdma_handle_t *handle, status_t status, void *userData) |
When transfer finished, one of these status values will be passed to the user:
| status_t DSI_TransferCreateHandleSMARTDMA | ( | MIPI_DSI_HOST_Type * | base, |
| dsi_smartdma_handle_t * | handle, | ||
| dsi_smartdma_callback_t | callback, | ||
| void * | userData | ||
| ) |
| base | MIPI DSI host peripheral base address. |
| handle | Handle pointer. |
| callback | Callback function. |
| userData | User data. |
| status_t DSI_TransferWriteMemorySMARTDMA | ( | MIPI_DSI_HOST_Type * | base, |
| dsi_smartdma_handle_t * | handle, | ||
| dsi_smartdma_write_mem_transfer_t * | xfer | ||
| ) |
Perform data transfer using SMARTDMA, when transfer finished, upper layer could be informed through callback function.
| base | MIPI DSI host peripheral base address. |
| handle | pointer to dsi_smartdma_handle_t structure which stores the transfer state. |
| xfer | Pointer to the transfer structure. |
| kStatus_Success | Data transfer started successfully. |
| kStatus_DSI_Busy | Failed to start transfer because DSI is busy with pervious transfer. |
| kStatus_DSI_NotSupported | Transfer format not supported. |
| void DSI_TransferAbortSMARTDMA | ( | MIPI_DSI_HOST_Type * | base, |
| dsi_smartdma_handle_t * | handle | ||
| ) |
| base | MIPI DSI host peripheral base address. |
| handle | pointer to dsi_smartdma_handle_t structure which stores the transfer state. |