The MCUXpresso SDK provides a peripheral driver for the General Purpose I/O (GPIO) module of MCUXpresso SDK devices.
Function groups
Initialization and deinitialization
The function GPIO_PinInit() initializes the GPIO with specified configuration.
Pin manipulation
The function GPIO_PinWrite() set output state of selected GPIO pin. The function GPIO_PinRead() read input value of selected GPIO pin.
Port manipulation
The function GPIO_PortSet() sets the output level of selected GPIO pins to the logic 1. The function GPIO_PortClear() sets the output level of selected GPIO pins to the logic 0. The function GPIO_PortToggle() reverse the output level of selected GPIO pins. The function GPIO_PortRead() read input value of selected port.
Port masking
The function GPIO_PortMaskedSet() set port mask, only pins masked by 0 will be enabled in following functions. The function GPIO_PortMaskedWrite() sets the state of selected GPIO port, only pins masked by 0 will be affected. The function GPIO_PortMaskedRead() reads the state of selected GPIO port, only pins masked by 0 are enabled for read, pins masked by 1 are read as 0.
Typical use case
Example use of GPIO API. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/gpio
|
| static void | GPIO_PortSet (GPIO_Type *base, uint32_t port, uint32_t mask) |
| | Sets the output level of the multiple GPIO pins to the logic 1. More...
|
| |
| static void | GPIO_PortClear (GPIO_Type *base, uint32_t port, uint32_t mask) |
| | Sets the output level of the multiple GPIO pins to the logic 0. More...
|
| |
| static void | GPIO_PortToggle (GPIO_Type *base, uint32_t port, uint32_t mask) |
| | Reverses current output logic of the multiple GPIO pins. More...
|
| |
|
| static void | GPIO_PinWrite (GPIO_Type *base, uint32_t port, uint32_t pin, uint8_t output) |
| | Sets the output level of the one GPIO pin to the logic 1 or 0. More...
|
| |
|
| static uint32_t | GPIO_PinRead (GPIO_Type *base, uint32_t port, uint32_t pin) |
| | Reads the current input value of the GPIO PIN. More...
|
| |
Every pin can only be configured as either output pin or input pin at a time. If configured as a input pin, then leave the outputConfig unused.
| struct _gpio_interrupt_config |
Every pin can only be configured as either output pin or input pin at a time. If configured as a input pin, then leave the outputConfig unused.
| Enumerator |
|---|
| kGPIO_DigitalInput |
Set current pin as digital input.
|
| kGPIO_DigitalOutput |
Set current pin as digital output.
|
| Enumerator |
|---|
| kGPIO_PinIntEnableLevel |
Generate Pin Interrupt on level mode.
|
| kGPIO_PinIntEnableEdge |
Generate Pin Interrupt on edge mode.
|
| Enumerator |
|---|
| kGPIO_PinIntEnableHighOrRise |
Generate Pin Interrupt on high level or rising edge.
|
| kGPIO_PinIntEnableLowOrFall |
Generate Pin Interrupt on low level or falling edge.
|
| Enumerator |
|---|
| kGPIO_InterruptA |
Set current pin as interrupt A.
|
| kGPIO_InterruptB |
Set current pin as interrupt B.
|
| void GPIO_PortInit |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port |
|
) |
| |
This function ungates the GPIO clock.
- Parameters
-
| base | GPIO peripheral base pointer. |
| port | GPIO port number. |
| void GPIO_PinInit |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
pin, |
|
|
const gpio_pin_config_t * |
config |
|
) |
| |
To initialize the GPIO, define a pin configuration, either input or output, in the user file. Then, call the GPIO_PinInit() function.
This is an example to define an input pin or output pin configuration:
* Define a digital input pin configuration,
* {
* 0,
* }
* Define a digital output pin configuration,
* {
* 0,
* }
*
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| pin | GPIO pin number |
| config | GPIO pin configuration pointer |
| static void GPIO_PinWrite |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
pin, |
|
|
uint8_t |
output |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| pin | GPIO pin number |
| output | GPIO pin output logic level.
- 0: corresponding pin output low-logic level.
- 1: corresponding pin output high-logic level.
|
| static uint32_t GPIO_PinRead |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
pin |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| pin | GPIO pin number |
- Return values
-
| GPIO | port input value
- 0: corresponding pin input low-logic level.
- 1: corresponding pin input high-logic level.
|
| static void GPIO_PortSet |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| mask | GPIO pin number macro |
| static void GPIO_PortClear |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| mask | GPIO pin number macro |
| static void GPIO_PortToggle |
( |
GPIO_Type * |
base, |
|
|
uint32_t |
port, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPIO peripheral base pointer(Typically GPIO) |
| port | GPIO port number |
| mask | GPIO pin number macro |