MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Ltc_edma_driver_aes

Overview

Macros

#define LTC_AES_DecryptCtrEDMA(base, handle, input, output, size, counter, key, keySize, counterlast, szLeft)   LTC_AES_CryptCtrEDMA(base, handle, input, output, size, counter, key, keySize, counterlast, szLeft)
 AES CTR decrypt is mapped to the AES CTR generic operation.
 
#define LTC_AES_EncryptCtrEDMA(base, handle, input, output, size, counter, key, keySize, counterlast, szLeft)   LTC_AES_CryptCtrEDMA(base, handle, input, output, size, counter, key, keySize, counterlast, szLeft)
 AES CTR encrypt is mapped to the AES CTR generic operation.
 

Functions

status_t LTC_AES_EncryptEcbEDMA (LTC_Type *base, ltc_edma_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, uint32_t size, const uint8_t *key, uint32_t keySize)
 Encrypts AES using the ECB block mode. More...
 
status_t LTC_AES_DecryptEcbEDMA (LTC_Type *base, ltc_edma_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, uint32_t size, const uint8_t *key, uint32_t keySize, ltc_aes_key_t keyType)
 Decrypts AES using ECB block mode. More...
 
status_t LTC_AES_EncryptCbcEDMA (LTC_Type *base, ltc_edma_handle_t *handle, const uint8_t *plaintext, uint8_t *ciphertext, uint32_t size, const uint8_t iv[LTC_AES_IV_SIZE], const uint8_t *key, uint32_t keySize)
 Encrypts AES using CBC block mode. More...
 
status_t LTC_AES_DecryptCbcEDMA (LTC_Type *base, ltc_edma_handle_t *handle, const uint8_t *ciphertext, uint8_t *plaintext, uint32_t size, const uint8_t iv[LTC_AES_IV_SIZE], const uint8_t *key, uint32_t keySize, ltc_aes_key_t keyType)
 Decrypts AES using CBC block mode. More...
 
status_t LTC_AES_CryptCtrEDMA (LTC_Type *base, ltc_edma_handle_t *handle, const uint8_t *input, uint8_t *output, uint32_t size, uint8_t counter[LTC_AES_BLOCK_SIZE], const uint8_t *key, uint32_t keySize, uint8_t counterlast[LTC_AES_BLOCK_SIZE], uint32_t *szLeft)
 Encrypts or decrypts AES using CTR block mode. More...
 

Function Documentation

status_t LTC_AES_EncryptEcbEDMA ( LTC_Type *  base,
ltc_edma_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
uint32_t  size,
const uint8_t *  key,
uint32_t  keySize 
)

Encrypts AES using the ECB block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_edma_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
keyInput key to use for encryption
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptEcbEDMA ( LTC_Type *  base,
ltc_edma_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
uint32_t  size,
const uint8_t *  key,
uint32_t  keySize,
ltc_aes_key_t  keyType 
)

Decrypts AES using ECB block mode.

Parameters
baseLTC peripheral base address
handlepointer to ltc_edma_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
keyInput key.
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
keyTypeInput type of the key (allows to directly load decrypt key for AES ECB decrypt operation.)
Returns
Status from decrypt operation
status_t LTC_AES_EncryptCbcEDMA ( LTC_Type *  base,
ltc_edma_handle_t *  handle,
const uint8_t *  plaintext,
uint8_t *  ciphertext,
uint32_t  size,
const uint8_t  iv[LTC_AES_IV_SIZE],
const uint8_t *  key,
uint32_t  keySize 
)
Parameters
baseLTC peripheral base address
handlepointer to ltc_edma_handle_t structure which stores the transaction state.
plaintextInput plain text to encrypt
[out]ciphertextOutput cipher text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
keyInput key to use for encryption
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
Returns
Status from encrypt operation
status_t LTC_AES_DecryptCbcEDMA ( LTC_Type *  base,
ltc_edma_handle_t *  handle,
const uint8_t *  ciphertext,
uint8_t *  plaintext,
uint32_t  size,
const uint8_t  iv[LTC_AES_IV_SIZE],
const uint8_t *  key,
uint32_t  keySize,
ltc_aes_key_t  keyType 
)
Parameters
baseLTC peripheral base address
handlepointer to ltc_edma_handle_t structure which stores the transaction state.
ciphertextInput cipher text to decrypt
[out]plaintextOutput plain text
sizeSize of input and output data in bytes. Must be multiple of 16 bytes.
ivInput initial vector to combine with the first input block.
keyInput key to use for decryption
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
keyTypeInput type of the key (allows to directly load decrypt key for AES CBC decrypt operation.)
Returns
Status from decrypt operation
status_t LTC_AES_CryptCtrEDMA ( LTC_Type *  base,
ltc_edma_handle_t *  handle,
const uint8_t *  input,
uint8_t *  output,
uint32_t  size,
uint8_t  counter[LTC_AES_BLOCK_SIZE],
const uint8_t *  key,
uint32_t  keySize,
uint8_t  counterlast[LTC_AES_BLOCK_SIZE],
uint32_t *  szLeft 
)

Encrypts or decrypts AES using CTR block mode. AES CTR mode uses only forward AES cipher and same algorithm for encryption and decryption. The only difference between encryption and decryption is that, for encryption, the input argument is plain text and the output argument is cipher text. For decryption, the input argument is cipher text and the output argument is plain text.

Parameters
baseLTC peripheral base address
handlepointer to ltc_edma_handle_t structure which stores the transaction state.
inputInput data for CTR block mode
[out]outputOutput data for CTR block mode
sizeSize of input and output data in bytes
[in,out]counterInput counter (updates on return)
keyInput key to use for forward AES cipher
keySizeSize of the input key, in bytes. Must be 16, 24, or 32.
[out]counterlastOutput cipher of last counter, for chained CTR calls. NULL can be passed if chained calls are not used.
[out]szLeftOutput number of bytes in left unused in counterlast block. NULL can be passed if chained calls are not used.
Returns
Status from encrypt operation