![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Modules | |
| ftfx adapter | |
Macros | |
| #define | FTFx_DRIVER_HAS_FLASH1_SUPPORT (0U) |
| Indicates whether the secondary flash is supported in the Flash driver. | |
FTFx configuration | |
| #define | FTFx_DRIVER_IS_FLASH_RESIDENT 1U |
| Flash driver location. More... | |
| #define | FTFx_DRIVER_IS_EXPORTED 0U |
| Flash Driver Export option. More... | |
Secondary flash configuration | |
| #define | FTFx_FLASH1_HAS_PROT_CONTROL (0U) |
| Indicates whether the secondary flash has its own protection register in flash module. More... | |
| #define | FTFx_FLASH1_HAS_XACC_CONTROL (0U) |
| Indicates whether the secondary flash has its own Execute-Only access register in flash module. More... | |
| #define FTFx_DRIVER_IS_FLASH_RESIDENT 1U |
Used for the flash resident application.
| #define FTFx_DRIVER_IS_EXPORTED 0U |
Used for the MCUXpresso SDK application.
| #define FTFx_FLASH1_HAS_PROT_CONTROL (0U) |
| #define FTFx_FLASH1_HAS_XACC_CONTROL (0U) |