MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
CAAM: Cryptographic Acceleration and Assurance Module

Overview

The MCUXpresso SDK provides the peripheral driver for the Cryptographic Acceleration and Assurance Module (CAAM) module. CAAM is a multi-functional accelerator that supports the cryptographic functions common in many security protocols. This includes AES128, AES256, DES, 3DES, SHA1, SHA224, SHA256, RSA-4096, and a random number generator with a true entropic seed. CAAM includes a DMA engine that is descriptor-based to reduce processor-accelerator interaction.

The driver comprises two sets of API functions.

In the first set, blocking APIs are provided for the selected subset of operations supported by CAAM hardware. The CAAM operations are complete, and results are made availabe for further usage, when a function returns. When called, these functions do not return until a CAAM operation is complete. These functions use main CPU for simple polling loops to determine operation complete or error status.

The CAAM job descriptor is placed on the system stack during the blocking API calls. The driver uses global variable to manage the input and output job rings. The driver uses critical section (implemented as global interrupt enable/disable) for a short time, whenever it needs to access these global variables. Therefore, the driver functions are designed to be re-entrant and as a consequence, one CPU thread can call one blocking API, such as AES Encrypt, while other CPU thread can call another blocking API, such as SHA-256 Update. The blocking functions provide typical interface to upper layer or application software.

In the second set, non-blocking variants of the first set APIs are provided. Internally, the blocking APIs are implemented as a non-blocking operation start, followed by a blocking wait (CPU polling CAAM output job ring). for an operation completion. The non-blocking functions allow upper layer to inject an application specific operation after the CAAM job start and CAAM job complete events. The RTOS event wait and RTOS event set can be an example of such an operation.

CAAM Driver Initialization and Configuration

The CAAM Job Ring interface is a software job programming interface. CAAM implements 2 Job Ring interfaces. The CAAM driver uses caam_job_ring_interface_t data type as the Job Ring interface. Job Ring interface 0 is mandatory to be configured for the CAAM driver, Job Ring interface 1 is optional.

Initialize CAAM after Power On Reset or reset cycle See the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam.

The CAAM Driver is initialized by calling the CAAM_Init() function. It enables the CAAM module clock, it configures the Job Ring interface(s) and instantiates the CAAM RNG module in normal (non-deterministic) mode. Then, it calls CAAM_RNG_GenerateSecureKey() to load the JDKEK, TDKEK, and TDSK registers and finally configures the CAAM SCFGR register.

Comments about API usage in RTOS

CAAM operations provided by this driver are re-entrant by protecting global variables (Job Ring interface) in critical section (global interrupt enable/disable by EnableGlobalIRQ() and DisableGlobalIRQ() MCUXpresso SDK APIs). If required, different RTOS threads can call CAAM driver APIs simultaneously, given that EnableGlobalIRQ() and DisableGlobalIRQ() can a create critical section.

Comments about API usage in interrupt handler

All APIs can be used from interrupt handler although execution time should be considered (interrupt latency of equal and lower priority interrupts increases).

Comments about DCACHE

CAAM driver requires any cached memory to be used with CAAM module to be set in write-trough mode, so any data in CACHE are up to date with ones in memory. This guarantee that CAAM can fetch descriptor, execute desired operation and when computation is done, it is safe to perform invalidate even over unaligned data, since all data in physical memory are up to date with ones in CACHE (so no memory corruption occurs) and finally, CPU can retrieve correct output.

CAAM Driver Examples

Simple examples

Encrypt plaintext by DES engine Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Encrypt plaintext by AES engine Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute keyed hash by AES engine (CMAC) Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute hash by MDHA engine (SHA-256) Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute modular integer exponentiation Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam Compute elliptic curve point addition Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/caam

Modules

 CAAM Blob driver
 
 CAAM Blocking APIs
 
 CAAM CRC driver
 
 CAAM Key Blankening driver
 
 CAAM Non-blocking APIs
 

Data Structures

struct  _caam_job_callback
 CAAM callback function. More...
 
struct  _caam_handle_t
 CAAM handle Specifies jobRing and optionally the user callback function. More...
 
struct  _caam_config
 CAAM configuration structure. More...
 

Typedefs

typedef struct _caam_job_callback caam_job_callback_t
 CAAM callback function. More...
 
typedef enum _caam_job_ring_t caam_job_ring_t
 CAAM job ring selection. More...
 
typedef struct _caam_handle_t caam_handle_t
 CAAM handle Specifies jobRing and optionally the user callback function. More...
 
typedef enum _caam_wait_mode caam_wait_mode_t
 CAAM driver wait mechanism.
 
typedef uint32_t caam_desc_aes_ecb_t [64]
 Memory buffer to hold CAAM descriptor for AESA ECB job.
 
typedef uint32_t caam_desc_aes_cbc_t [64]
 Memory buffer to hold CAAM descriptor for AESA CBC job.
 
typedef uint32_t caam_desc_aes_ctr_t [64]
 Memory buffer to hold CAAM descriptor for AESA CTR job.
 
typedef uint32_t caam_desc_aes_ccm_t [64]
 Memory buffer to hold CAAM descriptor for AESA CCM job.
 
typedef uint32_t caam_desc_aes_gcm_t [64]
 Memory buffer to hold CAAM descriptor for AESA GCM job.
 
typedef uint32_t caam_desc_hash_t [64]
 Memory buffer to hold CAAM descriptor for MDHA job or AESA CMAC job.
 
typedef uint32_t caam_desc_rng_t [64]
 Memory buffer to hold CAAM descriptor for RNG jobs.
 
typedef uint32_t caam_desc_cipher_des_t [64]
 Memory buffer to hold CAAM descriptor for DESA jobs.
 
typedef uint32_t caam_desc_pkha_t [64]
 Memory buffer to hold CAAM descriptor for PKHA jobs.
 
typedef uint32_t caam_desc_pkha_ecc_t [64]
 Memory buffer to hold CAAM descriptor for PKHA ECC jobs.
 
typedef uint32_t caam_desc_key_black_t [64]
 Memory buffer to hold CAAM descriptor for performing key blackening jobs.
 
typedef uint32_t caam_desc_gen_enc_blob_t [64]
 Memory buffer to hold CAAM descriptor for performing generating dek blob jobs.
 
typedef enum _caam_rng_sample_mode caam_rng_sample_mode_t
 CAAM RNG sample mode. More...
 
typedef enum _caam_rng_ring_osc_div caam_rng_ring_osc_div_t
 CAAM RNG ring oscillator divide. More...
 
typedef enum _caam_priblob caam_priblob_t
 CAAM Private Blob. More...
 
typedef struct _caam_config caam_config_t
 CAAM configuration structure. More...
 
typedef enum
_caam_ext_key_xfr_source 
caam_ext_key_xfr_source_t
 CAAM External Key Transfer command SRC (The source from which the key will be obtained)
 

Enumerations

enum  {
  kStatus_CAAM_Again = MAKE_STATUS(kStatusGroup_CAAM, 0),
  kStatus_CAAM_DataOverflow = MAKE_STATUS(kStatusGroup_CAAM, 1)
}
 CAAM status return codes. More...
 
enum  _caam_job_ring_t {
  kCAAM_JobRing0 = 0u,
  kCAAM_JobRing1 = 1u,
  kCAAM_JobRing2 = 2u,
  kCAAM_JobRing3 = 3u
}
 CAAM job ring selection. More...
 
enum  _caam_wait_mode {
  kCAAM_Blocking = 0u,
  kCAAM_Nonblocking = 1u
}
 CAAM driver wait mechanism. More...
 
enum  _caam_rng_sample_mode {
  kCAAM_RNG_SampleModeVonNeumann = 0U,
  kCAAM_RNG_SampleModeRaw = 1U,
  kCAAM_RNG_SampleModeVonNeumannRaw
}
 CAAM RNG sample mode. More...
 
enum  _caam_rng_ring_osc_div {
  kCAAM_RNG_RingOscDiv0 = 0U,
  kCAAM_RNG_RingOscDiv2 = 1U,
  kCAAM_RNG_RingOscDiv4 = 2U,
  kCAAM_RNG_RingOscDiv8 = 3U
}
 CAAM RNG ring oscillator divide. More...
 
enum  _caam_priblob {
  kCAAM_PrivSecureBootBlobs = 0U,
  kCAAM_PrivProvisioningBlobsType1 = 1U,
  kCAAM_PrivProvisioningBlobsType2 = 2U,
  kCAAM_NormalOperationBlobs = 3U
}
 CAAM Private Blob. More...
 
enum  _caam_ext_key_xfr_source {
  kCAAM_ExtKeyXfr_KeyRegisterClass1 = 1U,
  kCAAM_ExtKeyXfr_KeyRegisterClass2 = 2U,
  kCAAM_ExtKeyXfr_PkhaRamE = 3U
}
 CAAM External Key Transfer command SRC (The source from which the key will be obtained) More...
 

Functions

status_t CAAM_Init (CAAM_Type *base, const caam_config_t *config)
 Initializes the CAAM driver. More...
 
status_t CAAM_Deinit (CAAM_Type *base)
 Deinitializes the CAAM driver. More...
 
void CAAM_GetDefaultConfig (caam_config_t *config)
 Gets the default configuration structure. More...
 
status_t CAAM_Wait (CAAM_Type *base, caam_handle_t *handle, uint32_t *descriptor, caam_wait_mode_t mode)
 Wait for a CAAM job to complete. More...
 
status_t CAAM_ExternalKeyTransfer (CAAM_Type *base, caam_handle_t *handle, caam_ext_key_xfr_source_t keySource, size_t keySize)
 External Key Transfer. More...
 

Driver version

#define FSL_CAAM_DRIVER_VERSION   (MAKE_VERSION(2, 3, 2))
 CAAM driver version. More...
 

Data Structure Documentation

struct _caam_job_callback

Data Fields

void(* JobCompleted )(void *userData)
 CAAM Job complete callback.
 
struct _caam_handle_t

The user callback functions is invoked only if jobRing interrupt has been enabled by the user. By default the jobRing interrupt is disabled (default job complete test is polling CAAM output ring).

Data Fields

caam_job_callback_t callback
 Callback function.
 
void * userData
 Parameter for CAAM job complete callback.
 
struct _caam_config

Data Fields

caam_rng_sample_mode_t rngSampleMode
 RTMCTL Sample Mode. More...
 
caam_rng_ring_osc_div_t rngRingOscDiv
 RTMCTL Oscillator Divide. More...
 
bool scfgrLockTrngProgramMode
 SCFGR Lock TRNG Program Mode. More...
 
bool scfgrEnableRandomDataBuffer
 SCFGR Enable random data buffer. More...
 
bool scfgrRandomRngStateHandle0
 SCFGR Random Number Generator State Handle 0. More...
 
bool scfgrRandomDpaResistance
 SCFGR Random Differential Power Analysis Resistance. More...
 
caam_priblob_t scfgrPriblob
 SCFGR Private Blob. More...
 

Field Documentation

caam_rng_sample_mode_t _caam_config::rngSampleMode
caam_rng_ring_osc_div_t _caam_config::rngRingOscDiv
bool _caam_config::scfgrLockTrngProgramMode
bool _caam_config::scfgrEnableRandomDataBuffer
bool _caam_config::scfgrRandomRngStateHandle0
bool _caam_config::scfgrRandomDpaResistance
caam_priblob_t _caam_config::scfgrPriblob

Macro Definition Documentation

#define FSL_CAAM_DRIVER_VERSION   (MAKE_VERSION(2, 3, 2))

Version 2.3.2.

Current version: 2.3.2

Change log:

  • Version 2.0.0
    • Initial version
  • Version 2.0.1
    • Add Job Ring 2 and 3.
  • Version 2.0.2
    • Add Data and Instruction Synchronization Barrier in caam_input_ring_set_jobs_added() to make sure that the descriptor will be loaded into CAAM correctly.
  • Version 2.0.3
    • Use MACRO instead of numbers in descriptor.
    • Correct descriptor size mask.
  • Version 2.1.0
    • Add return codes check and handling.
  • Version 2.1.1
    • Add DCACHE support.
  • Version 2.1.2
    • Add data offset feature to provide support for mirrored (high-speed) memory.
  • Version 2.1.3
    • Fix MISRA-2012 issues.
  • Version 2.1.4
    • Fix MISRA-2012 issues.
  • Version 2.1.5
    • Support EXTENDED data size for all AES, HASH and RNG operations.
    • Support multiple De-Initialization/Initialization of CAAM driver within one POR event.
  • Version 2.1.6
    • Improve DCACHE handling. Requires CAAM used and cached memory set in write-trough mode.
  • Version 2.2.0
    • Added API for Blob functions and CRC
  • Version 2.2.1
    • Fixed AES-CCM decrypt failing with TAG length bigger than 8 byte.
  • Version 2.2.2
    • Modify RNG to not reseed with each request.
  • Version 2.2.3
  • Version 2.2.4
    • Fix issue where the outputSize parameter of CAAM_HASH_Finish() has impact on hash calculation.
  • Version 2.3.0
    • Add support for SHA HMAC.
  • Version 2.3.1
    • Modified function caam_aes_ccm_check_input_args() to allow payload be empty as is specified in NIST800-38C Section 5.3.
  • Version 2.3.2
    • Fix MISRA-2012 issues.

Typedef Documentation

typedef struct _caam_handle_t caam_handle_t

The user callback functions is invoked only if jobRing interrupt has been enabled by the user. By default the jobRing interrupt is disabled (default job complete test is polling CAAM output ring).

Used by caam_config_t.

Used by caam_config_t.

Used by caam_config_t.

typedef struct _caam_config caam_config_t

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_CAAM_Again 

Non-blocking function shall be called again.

kStatus_CAAM_DataOverflow 

Input data too big.

Enumerator
kCAAM_JobRing0 

CAAM Job ring 0.

kCAAM_JobRing1 

CAAM Job ring 1.

kCAAM_JobRing2 

CAAM Job ring 2.

kCAAM_JobRing3 

CAAM Job ring 3.

Enumerator
kCAAM_Blocking 

CAAM_Wait blocking mode.

kCAAM_Nonblocking 

CAAM Wait non-blocking mode.

Used by caam_config_t.

Enumerator
kCAAM_RNG_SampleModeVonNeumann 

Use von Neumann data in both Entropy shifter and Statistical Checker.

kCAAM_RNG_SampleModeRaw 

Use raw data into both Entropy shifter and Statistical Checker.

kCAAM_RNG_SampleModeVonNeumannRaw 

Use von Neumann data in Entropy shifter.

Use raw data into Statistical Checker.

Used by caam_config_t.

Enumerator
kCAAM_RNG_RingOscDiv0 

Ring oscillator with no divide.

kCAAM_RNG_RingOscDiv2 

Ring oscillator divided-by-2.

kCAAM_RNG_RingOscDiv4 

Ring oscillator divided-by-4.

kCAAM_RNG_RingOscDiv8 

Ring oscillator divided-by-8.

Used by caam_config_t.

Enumerator
kCAAM_PrivSecureBootBlobs 

Private secure boot software blobs.

kCAAM_PrivProvisioningBlobsType1 

Private Provisioning Type 1 blobs.

kCAAM_PrivProvisioningBlobsType2 

Private Provisioning Type 2 blobs.

kCAAM_NormalOperationBlobs 

Normal operation blobs.

Enumerator
kCAAM_ExtKeyXfr_KeyRegisterClass1 

The Class 1 Key Register is the source.

kCAAM_ExtKeyXfr_KeyRegisterClass2 

The Class 2 Key Register is the source.

kCAAM_ExtKeyXfr_PkhaRamE 

The PKHA E RAM is the source.

Function Documentation

status_t CAAM_Init ( CAAM_Type *  base,
const caam_config_t *  config 
)

This function initializes the CAAM driver, including CAAM's internal RNG.

Parameters
baseCAAM peripheral base address
configPointer to configuration structure.
Returns
kStatus_Success the CAAM Init has completed with zero termination status word
kStatus_Fail the CAAM Init has completed with non-zero termination status word
status_t CAAM_Deinit ( CAAM_Type *  base)

This function deinitializes the CAAM driver.

Parameters
baseCAAM peripheral base address
Returns
kStatus_Success the CAAM Deinit has completed with zero termination status word
kStatus_Fail the CAAM Deinit has completed with non-zero termination status word
void CAAM_GetDefaultConfig ( caam_config_t *  config)

This function initializes the CAAM configuration structure to a default value. The default values are as follows. caamConfig->rngSampleMode = kCAAM_RNG_SampleModeVonNeumann; caamConfig->rngRingOscDiv = kCAAM_RNG_RingOscDiv4;

Parameters
[out]configPointer to configuration structure.
status_t CAAM_Wait ( CAAM_Type *  base,
caam_handle_t *  handle,
uint32_t *  descriptor,
caam_wait_mode_t  mode 
)

This function polls CAAM output ring for a specific job.

The CAAM job ring is specified by the jobRing field in the caam_handle_t structure. The job to be waited is specified by it's descriptor address.

This function has two modes, determined by the mode argument. In blocking mode, the function polls the specified jobRing until the descriptor is available in the CAAM output job ring. In non-blocking mode, it polls the output ring once and returns status immediately.

The function can be called from multiple threads or interrupt service routines, as internally it uses global critical section (global interrupt disable enable) to protect it's operation against concurrent accesses. The global interrupt is disabled only when the descriptor is found in the output ring, for a very short time, to remove the descriptor from the output ring safely.

Parameters
baseCAAM peripheral base address
handleData structure with CAAM jobRing used for this request
descriptor
modeBlocking and non-blocking mode. Zero is blocking. Non-zero is non-blocking.
Returns
kStatus_Success the CAAM job has completed with zero job termination status word
kStatus_Fail the CAAM job has completed with non-zero job termination status word
kStatus_Again In non-blocking mode, the job is not ready in the CAAM Output Ring
status_t CAAM_ExternalKeyTransfer ( CAAM_Type *  base,
caam_handle_t *  handle,
caam_ext_key_xfr_source_t  keySource,
size_t  keySize 
)

This function loads the given key source to an CAAM external destination via a private interface, such as Inline Encryption Engine IEE Private Key bus.

The CAAM job ring is specified by the jobRing field in the caam_handle_t structure.

This function is blocking.

Parameters
baseCAAM peripheral base address
handleData structure with CAAM jobRing used for this request.
keySourceThe source from which the key will be obtained.
keySizeSize of the key in bytes.
Returns
kStatus_Success the CAAM job has completed with zero job termination status word
kStatus_Fail the CAAM job has completed with non-zero job termination status word