|  | MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    NXP Semiconductors | 
| Data Structures | |
| struct | i2s_dma_handle_t | 
| i2s dma handle  More... | |
| Typedefs | |
| typedef void(* | i2s_dma_transfer_callback_t )(I2S_Type *base, i2s_dma_handle_t *handle, status_t completionStatus, void *userData) | 
| Callback function invoked from DMA API on completion.  More... | |
| Driver version | |
| #define | FSL_I2S_DMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 3)) | 
| I2S DMA driver version 2.3.3.  More... | |
| DMA API | |
| void | I2S_TxTransferCreateHandleDMA (I2S_Type *base, i2s_dma_handle_t *handle, dma_handle_t *dmaHandle, i2s_dma_transfer_callback_t callback, void *userData) | 
| Initializes handle for transfer of audio data.  More... | |
| status_t | I2S_TxTransferSendDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t transfer) | 
| Begins or queue sending of the given data.  More... | |
| void | I2S_TransferAbortDMA (I2S_Type *base, i2s_dma_handle_t *handle) | 
| Aborts transfer of data.  More... | |
| void | I2S_RxTransferCreateHandleDMA (I2S_Type *base, i2s_dma_handle_t *handle, dma_handle_t *dmaHandle, i2s_dma_transfer_callback_t callback, void *userData) | 
| Initializes handle for reception of audio data.  More... | |
| status_t | I2S_RxTransferReceiveDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t transfer) | 
| Begins or queue reception of data into given buffer.  More... | |
| void | I2S_DMACallback (dma_handle_t *handle, void *userData, bool transferDone, uint32_t tcds) | 
| Invoked from DMA interrupt handler.  More... | |
| void | I2S_TransferInstallLoopDMADescriptorMemory (i2s_dma_handle_t *handle, void *dmaDescriptorAddr, size_t dmaDescriptorNum) | 
| Install DMA descriptor memory for loop transfer only.  More... | |
| status_t | I2S_TransferSendLoopDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t *xfer, uint32_t loopTransferCount) | 
| Send link transfer data using DMA.  More... | |
| status_t | I2S_TransferReceiveLoopDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t *xfer, uint32_t loopTransferCount) | 
| Receive link transfer data using DMA.  More... | |
| struct _i2s_dma_handle | 
Members not to be accessed / modified outside of the driver.
| Data Fields | |
| uint32_t | state | 
| Internal state of I2S DMA transfer. | |
| uint8_t | bytesPerFrame | 
| bytes per frame | |
| i2s_dma_transfer_callback_t | completionCallback | 
| Callback function pointer. | |
| void * | userData | 
| Application data passed to callback. | |
| dma_handle_t * | dmaHandle | 
| DMA handle. | |
| volatile i2s_transfer_t | i2sQueue [I2S_NUM_BUFFERS] | 
| Transfer queue storing transfer buffers. | |
| volatile uint8_t | queueUser | 
| Queue index where user's next transfer will be stored. | |
| volatile uint8_t | queueDriver | 
| Queue index of buffer actually used by the driver. | |
| dma_descriptor_t * | i2sLoopDMADescriptor | 
| descriptor pool pointer | |
| size_t | i2sLoopDMADescriptorNum | 
| number of descriptor in descriptors pool | |
| #define FSL_I2S_DMA_DRIVER_VERSION (MAKE_VERSION(2, 3, 3)) | 
| typedef void(* i2s_dma_transfer_callback_t)(I2S_Type *base, i2s_dma_handle_t *handle, status_t completionStatus, void *userData) | 
| base | I2S base pointer. | 
| handle | pointer to I2S transaction. | 
| completionStatus | status of the transaction. | 
| userData | optional pointer to user arguments data. | 
| void I2S_TxTransferCreateHandleDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| dma_handle_t * | dmaHandle, | ||
| i2s_dma_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| dmaHandle | pointer to dma handle structure. | 
| callback | function to be called back when transfer is done or fails. | 
| userData | pointer to data passed to callback. | 
| status_t I2S_TxTransferSendDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| transfer | data buffer. | 
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with unsent buffers. | 
| void I2S_TransferAbortDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| void I2S_RxTransferCreateHandleDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| dma_handle_t * | dmaHandle, | ||
| i2s_dma_transfer_callback_t | callback, | ||
| void * | userData | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| dmaHandle | pointer to dma handle structure. | 
| callback | function to be called back when transfer is done or fails. | 
| userData | pointer to data passed to callback. | 
| status_t I2S_RxTransferReceiveDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| i2s_transfer_t | transfer | ||
| ) | 
| base | I2S base pointer. | 
| handle | pointer to handle structure. | 
| transfer | data buffer. | 
| kStatus_Success | |
| kStatus_I2S_Busy | if all queue slots are occupied with buffers which are not full. | 
| void I2S_DMACallback | ( | dma_handle_t * | handle, | 
| void * | userData, | ||
| bool | transferDone, | ||
| uint32_t | tcds | ||
| ) | 
| handle | pointer to DMA handle structure. | 
| userData | argument for user callback. | 
| transferDone | if transfer was done. | 
| tcds | 
| void I2S_TransferInstallLoopDMADescriptorMemory | ( | i2s_dma_handle_t * | handle, | 
| void * | dmaDescriptorAddr, | ||
| size_t | dmaDescriptorNum | ||
| ) | 
This function used to register DMA descriptor memory for the i2s loop dma transfer.
It must be callbed before I2S_TransferSendLoopDMA/I2S_TransferReceiveLoopDMA and after I2S_RxTransferCreateHandleDMA/I2S_TxTransferCreateHandleDMA.
User should be take care about the address of DMA descriptor pool which required align with 16BYTE at least.
| handle | Pointer to i2s DMA transfer handle. | 
| dmaDescriptorAddr | DMA descriptor start address. | 
| dmaDescriptorNum | DMA descriptor number. | 
| status_t I2S_TransferSendLoopDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| i2s_transfer_t * | xfer, | ||
| uint32_t | loopTransferCount | ||
| ) | 
This function receives data using DMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
This function support loop transfer, such as A->B->...->A, the loop transfer chain will be converted into a chain of descriptor and submit to dma. Application must be aware of that the more counts of the loop transfer, then more DMA descriptor memory required, user can use function I2S_InstallDMADescriptorMemory to register the dma descriptor memory.
As the DMA support maximum 1024 transfer count, so application must be aware of that this transfer function support maximum 1024 samples in each transfer, otherwise assert error or error status will be returned. Once the loop transfer start, application can use function I2S_TransferAbortDMA to stop the loop transfer.
| base | I2S peripheral base address. | 
| handle | Pointer to usart_dma_handle_t structure. | 
| xfer | I2S DMA transfer structure. See i2s_transfer_t. | 
| loopTransferCount | loop count | 
| kStatus_Success | 
| status_t I2S_TransferReceiveLoopDMA | ( | I2S_Type * | base, | 
| i2s_dma_handle_t * | handle, | ||
| i2s_transfer_t * | xfer, | ||
| uint32_t | loopTransferCount | ||
| ) | 
This function receives data using DMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.
This function support loop transfer, such as A->B->...->A, the loop transfer chain will be converted into a chain of descriptor and submit to dma. Application must be aware of that the more counts of the loop transfer, then more DMA descriptor memory required, user can use function I2S_InstallDMADescriptorMemory to register the dma descriptor memory.
As the DMA support maximum 1024 transfer count, so application must be aware of that this transfer function support maximum 1024 samples in each transfer, otherwise assert error or error status will be returned. Once the loop transfer start, application can use function I2S_TransferAbortDMA to stop the loop transfer.
| base | I2S peripheral base address. | 
| handle | Pointer to usart_dma_handle_t structure. | 
| xfer | I2S DMA transfer structure. See i2s_transfer_t. | 
| loopTransferCount | loop count | 
| kStatus_Success |