MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

Files

file  fsl_clock.h
 

Data Structures

struct  pll_config_t
 PLL configuration structure. More...
 
struct  pll_setup_t
 PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More...
 
struct  usb_pll_setup_t
 PLL setup structure This structure can be used to pre-build a USB PLL setup configuration at run-time and quickly set the usb PLL to the configuration. More...
 

Macros

#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0
 Configure whether driver controls clock. More...
 
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U
 User-defined the size of cache for CLOCK_PllGetConfig() function. More...
 
#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define ROM_CLOCKS
 Clock ip name array for ROM. More...
 
#define SRAM_CLOCKS
 Clock ip name array for SRAM. More...
 
#define FLASH_CLOCKS
 Clock ip name array for FLASH. More...
 
#define FMC_CLOCKS
 Clock ip name array for FMC. More...
 
#define EEPROM_CLOCKS
 Clock ip name array for EEPROM. More...
 
#define SPIFI_CLOCKS
 Clock ip name array for SPIFI. More...
 
#define INPUTMUX_CLOCKS
 Clock ip name array for INPUTMUX. More...
 
#define IOCON_CLOCKS
 Clock ip name array for IOCON. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define PINT_CLOCKS
 Clock ip name array for PINT. More...
 
#define GINT_CLOCKS
 Clock ip name array for GINT. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define RTC_CLOCKS
 Clock ip name array for RTC. More...
 
#define ADC0_CLOCKS
 Clock ip name array for ADC0. More...
 
#define MRT_CLOCKS
 Clock ip name array for MRT. More...
 
#define RIT_CLOCKS
 Clock ip name array for RIT. More...
 
#define SCT_CLOCKS
 Clock ip name array for SCT0. More...
 
#define MCAN_CLOCKS
 Clock ip name array for MCAN. More...
 
#define UTICK_CLOCKS
 Clock ip name array for UTICK. More...
 
#define FLEXCOMM_CLOCKS
 Clock ip name array for FLEXCOMM. More...
 
#define LPUART_CLOCKS
 Clock ip name array for LPUART. More...
 
#define BI2C_CLOCKS
 Clock ip name array for BI2C. More...
 
#define LPSI_CLOCKS
 Clock ip name array for LSPI. More...
 
#define FLEXI2S_CLOCKS
 Clock ip name array for FLEXI2S. More...
 
#define DMIC_CLOCKS
 Clock ip name array for DMIC. More...
 
#define CTIMER_CLOCKS
 Clock ip name array for CT32B. More...
 
#define LCD_CLOCKS
 Clock ip name array for LCD. More...
 
#define SDIO_CLOCKS
 Clock ip name array for SDIO. More...
 
#define USBRAM_CLOCKS
 Clock ip name array for USBRAM. More...
 
#define EMC_CLOCKS
 Clock ip name array for EMC. More...
 
#define ETH_CLOCKS
 Clock ip name array for ETH. More...
 
#define AES_CLOCKS
 Clock ip name array for AES. More...
 
#define OTP_CLOCKS
 Clock ip name array for OTP. More...
 
#define RNG_CLOCKS
 Clock ip name array for RNG. More...
 
#define USBHMR0_CLOCKS
 Clock ip name array for USBHMR0. More...
 
#define USBHSL0_CLOCKS
 Clock ip name array for USBHSL0. More...
 
#define SHA0_CLOCKS
 Clock ip name array for SHA0. More...
 
#define SMARTCARD_CLOCKS
 Clock ip name array for SMARTCARD. More...
 
#define USBD_CLOCKS
 Clock ip name array for USBD. More...
 
#define USBH_CLOCKS
 Clock ip name array for USBH. More...
 
#define CLK_GATE_REG_OFFSET_SHIFT   8U
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
#define CLK_ATTACH_ID(mux, sel, pos)   ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U))
 Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More...
 
#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)
 PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More...
 
#define PLL_CONFIGFLAG_FORCENOFRACT   (1U << 2U)
 Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or \ SS hardware.
 
#define PLL_SETUPFLAG_POWERUP   (1U << 0U)
 PLL setup structure flags for 'flags' field These flags control how the PLL setup function sets up the PLL. More...
 
#define PLL_SETUPFLAG_WAITLOCK   (1U << 1U)
 Setup will wait for PLL lock, implies the PLL will be pwoered on.
 
#define PLL_SETUPFLAG_ADGVOLT   (1U << 2U)
 Optimize system voltage for the new PLL rate.
 

Enumerations

enum  clock_ip_name_t {
  kCLOCK_IpInvalid = 0U,
  kCLOCK_Rom = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 1),
  kCLOCK_Sram1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 3),
  kCLOCK_Sram2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 4),
  kCLOCK_Sram3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 5),
  kCLOCK_Spifi = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 10),
  kCLOCK_InputMux = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 11),
  kCLOCK_Iocon = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 13),
  kCLOCK_Gpio0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 14),
  kCLOCK_Gpio1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 15),
  kCLOCK_Gpio2 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 16),
  kCLOCK_Gpio3 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 17),
  kCLOCK_Pint = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 18),
  kCLOCK_Gint = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 19),
  kCLOCK_Dma = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 20),
  kCLOCK_Crc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 21),
  kCLOCK_Wwdt = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 22),
  kCLOCK_Rtc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 23),
  kCLOCK_Adc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 27),
  kCLOCK_Mrt = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 0),
  kCLOCK_Rit = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 1),
  kCLOCK_Sct0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 2),
  kCLOCK_Mcan0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 7),
  kCLOCK_Mcan1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 8),
  kCLOCK_Utick = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 10),
  kCLOCK_FlexComm0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11),
  kCLOCK_FlexComm1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12),
  kCLOCK_FlexComm2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13),
  kCLOCK_FlexComm3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14),
  kCLOCK_FlexComm4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15),
  kCLOCK_FlexComm5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16),
  kCLOCK_FlexComm6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17),
  kCLOCK_FlexComm7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18),
  kCLOCK_MinUart0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11),
  kCLOCK_MinUart1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12),
  kCLOCK_MinUart2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13),
  kCLOCK_MinUart3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14),
  kCLOCK_MinUart4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15),
  kCLOCK_MinUart5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16),
  kCLOCK_MinUart6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17),
  kCLOCK_MinUart7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18),
  kCLOCK_LSpi0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11),
  kCLOCK_LSpi1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12),
  kCLOCK_LSpi2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13),
  kCLOCK_LSpi3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14),
  kCLOCK_LSpi4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15),
  kCLOCK_LSpi5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16),
  kCLOCK_LSpi6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17),
  kCLOCK_LSpi7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18),
  kCLOCK_BI2c0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11),
  kCLOCK_BI2c1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12),
  kCLOCK_BI2c2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13),
  kCLOCK_BI2c3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14),
  kCLOCK_BI2c4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15),
  kCLOCK_BI2c5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16),
  kCLOCK_BI2c6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17),
  kCLOCK_BI2c7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18),
  kCLOCK_FlexI2s0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11),
  kCLOCK_FlexI2s1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12),
  kCLOCK_FlexI2s2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13),
  kCLOCK_FlexI2s3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14),
  kCLOCK_FlexI2s4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15),
  kCLOCK_FlexI2s5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16),
  kCLOCK_FlexI2s6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17),
  kCLOCK_FlexI2s7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18),
  kCLOCK_DMic = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 19),
  kCLOCK_Ct32b2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 22),
  kCLOCK_Usbd0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 25),
  kCLOCK_Ct32b0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 26),
  kCLOCK_Ct32b1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 27),
  kCLOCK_BodyBias0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 29),
  kCLOCK_EzhArchB0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 31),
  kCLOCK_Lcd = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 2),
  kCLOCK_Sdio = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 3),
  kCLOCK_Usbh1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 4),
  kCLOCK_Usbd1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 5),
  kCLOCK_UsbRam1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 6),
  kCLOCK_Emc = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 7),
  kCLOCK_Eth = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 8),
  kCLOCK_Gpio4 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 9),
  kCLOCK_Gpio5 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 10),
  kCLOCK_Aes = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 11),
  kCLOCK_Otp = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 12),
  kCLOCK_Rng = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 13),
  kCLOCK_FlexComm8 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14),
  kCLOCK_FlexComm9 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15),
  kCLOCK_MinUart8 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14),
  kCLOCK_MinUart9 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15),
  kCLOCK_LSpi8 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14),
  kCLOCK_LSpi9 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15),
  kCLOCK_BI2c8 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14),
  kCLOCK_BI2c9 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15),
  kCLOCK_FlexI2s8 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 14),
  kCLOCK_FlexI2s9 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 15),
  kCLOCK_Usbhmr0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 16),
  kCLOCK_Usbhsl0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 17),
  kCLOCK_Sha0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 18),
  kCLOCK_SmartCard0 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 19),
  kCLOCK_SmartCard1 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 20),
  kCLOCK_FlexComm10 = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 21),
  kCLOCK_Puf = CLK_GATE_DEFINE(AHB_CLK_CTRL2, 23),
  kCLOCK_Ct32b3 = CLK_GATE_DEFINE(ASYNC_CLK_CTRL0, 13),
  kCLOCK_Ct32b4 = CLK_GATE_DEFINE(ASYNC_CLK_CTRL0, 14)
}
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  clock_name_t {
  kCLOCK_CoreSysClk,
  kCLOCK_BusClk,
  kCLOCK_ClockOut,
  kCLOCK_FroHf,
  kCLOCK_UsbPll,
  kCLOCK_Mclk,
  kCLOCK_Fro12M,
  kCLOCK_ExtClk,
  kCLOCK_PllOut,
  kCLOCK_UsbClk,
  kCLOCK_WdtOsc,
  kCLOCK_Frg,
  kCLOCK_AsyncApbClk
}
 Clock name used to get clock frequency. More...
 
enum  async_clock_src_t {
  kCLOCK_AsyncMainClk = 0,
  kCLOCK_AsyncFro12Mhz,
  kCLOCK_AsyncAudioPllClk,
  kCLOCK_AsyncI2cClkFc6
}
 Clock source selections for the asynchronous APB clock. More...
 
enum  clock_attach_id_t {
  kSYSTICK_DIV_CLK_to_SYSTICKCLK = MUX_A(CM_STICKCLKSEL, 0),
  kWDT_OSC_to_SYSTICKCLK = MUX_A(CM_STICKCLKSEL, 1),
  kOSC32K_to_SYSTICKCLK = MUX_A(CM_STICKCLKSEL, 2),
  kFRO12M_to_SYSTICKCLK = MUX_A(CM_STICKCLKSEL, 3),
  kNONE_to_SYSTICKCLK = MUX_A(CM_STICKCLKSEL, 7),
  kFRO12M_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 0, 0),
  kEXT_CLK_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 1) | MUX_B(CM_MAINCLKSELB, 0, 0),
  kWDT_OSC_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 2) | MUX_B(CM_MAINCLKSELB, 0, 0),
  kFRO_HF_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 3) | MUX_B(CM_MAINCLKSELB, 0, 0),
  kSYS_PLL_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 2, 0),
  kOSC32K_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 3, 0),
  kMAIN_CLK_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 0),
  kEXT_CLK_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 1),
  kWDT_OSC_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 2),
  kFRO_HF_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 3),
  kSYS_PLL_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 4),
  kUSB_PLL_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 5),
  kAUDIO_PLL_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 6),
  kOSC32K_OSC_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 7),
  kFRO12M_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 0),
  kEXT_CLK_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 1),
  kWDT_OSC_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 2),
  kOSC32K_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 3),
  kNONE_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 7),
  kFRO12M_to_AUDIO_PLL = MUX_A(CM_AUDPLLCLKSEL, 0),
  kEXT_CLK_to_AUDIO_PLL = MUX_A(CM_AUDPLLCLKSEL, 1),
  kNONE_to_AUDIO_PLL = MUX_A(CM_AUDPLLCLKSEL, 7),
  kMAIN_CLK_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 0),
  kSYS_PLL_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 1),
  kUSB_PLL_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 2),
  kFRO_HF_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 3),
  kAUDIO_PLL_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 4),
  kNONE_to_SPIFI_CLK = MUX_A(CM_SPIFICLKSEL, 7),
  kFRO_HF_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 0),
  kSYS_PLL_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 1),
  kUSB_PLL_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 2),
  kAUDIO_PLL_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 3),
  kNONE_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 7),
  kFRO_HF_to_USB0_CLK = MUX_A(CM_USB0CLKSEL, 0),
  kSYS_PLL_to_USB0_CLK = MUX_A(CM_USB0CLKSEL, 1),
  kUSB_PLL_to_USB0_CLK = MUX_A(CM_USB0CLKSEL, 2),
  kNONE_to_USB0_CLK = MUX_A(CM_USB0CLKSEL, 7),
  kFRO_HF_to_USB1_CLK = MUX_A(CM_USB1CLKSEL, 0),
  kSYS_PLL_to_USB1_CLK = MUX_A(CM_USB1CLKSEL, 1),
  kUSB_PLL_to_USB1_CLK = MUX_A(CM_USB1CLKSEL, 2),
  kNONE_to_USB1_CLK = MUX_A(CM_USB1CLKSEL, 7),
  kFRO12M_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 0),
  kFRO_HF_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 1),
  kAUDIO_PLL_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 2),
  kMCLK_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 3),
  kFRG_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 4),
  kNONE_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 7),
  kFRO12M_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 0),
  kFRO_HF_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 1),
  kAUDIO_PLL_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 2),
  kMCLK_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 3),
  kFRG_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 4),
  kNONE_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 7),
  kFRO12M_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 0),
  kFRO_HF_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 1),
  kAUDIO_PLL_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 2),
  kMCLK_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 3),
  kFRG_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 4),
  kNONE_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 7),
  kFRO12M_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 0),
  kFRO_HF_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 1),
  kAUDIO_PLL_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 2),
  kMCLK_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 3),
  kFRG_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 4),
  kNONE_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 7),
  kFRO12M_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 0),
  kFRO_HF_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 1),
  kAUDIO_PLL_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 2),
  kMCLK_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 3),
  kFRG_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 4),
  kNONE_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 7),
  kFRO12M_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 0),
  kFRO_HF_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 1),
  kAUDIO_PLL_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 2),
  kMCLK_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 3),
  kFRG_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 4),
  kNONE_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 7),
  kFRO12M_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 0),
  kFRO_HF_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 1),
  kAUDIO_PLL_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 2),
  kMCLK_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 3),
  kFRG_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 4),
  kNONE_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 7),
  kFRO12M_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 0),
  kFRO_HF_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 1),
  kAUDIO_PLL_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 2),
  kMCLK_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 3),
  kFRG_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 4),
  kNONE_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 7),
  kFRO12M_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 0),
  kFRO_HF_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 1),
  kAUDIO_PLL_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 2),
  kMCLK_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 3),
  kFRG_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 4),
  kNONE_to_FLEXCOMM8 = MUX_A(CM_FXCOMCLKSEL8, 7),
  kFRO12M_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 0),
  kFRO_HF_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 1),
  kAUDIO_PLL_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 2),
  kMCLK_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 3),
  kFRG_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 4),
  kNONE_to_FLEXCOMM9 = MUX_A(CM_FXCOMCLKSEL9, 7),
  kMAIN_CLK_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 0),
  kSYS_PLL_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 1),
  kUSB_PLL_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 2),
  kFRO_HF_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 3),
  kAUDIO_PLL_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 4),
  kNONE_to_FLEXCOMM10 = MUX_A(CM_FXCOMCLKSEL10, 7),
  kFRO_HF_to_MCLK = MUX_A(CM_MCLKCLKSEL, 0),
  kAUDIO_PLL_to_MCLK = MUX_A(CM_MCLKCLKSEL, 1),
  kNONE_to_MCLK = MUX_A(CM_MCLKCLKSEL, 7),
  kMAIN_CLK_to_FRG = MUX_A(CM_FRGCLKSEL, 0),
  kSYS_PLL_to_FRG = MUX_A(CM_FRGCLKSEL, 1),
  kFRO12M_to_FRG = MUX_A(CM_FRGCLKSEL, 2),
  kFRO_HF_to_FRG = MUX_A(CM_FRGCLKSEL, 3),
  kNONE_to_FRG = MUX_A(CM_FRGCLKSEL, 7),
  kFRO12M_to_DMIC = MUX_A(CM_DMICCLKSEL, 0),
  kFRO_HF_DIV_to_DMIC = MUX_A(CM_DMICCLKSEL, 1),
  kAUDIO_PLL_to_DMIC = MUX_A(CM_DMICCLKSEL, 2),
  kMCLK_to_DMIC = MUX_A(CM_DMICCLKSEL, 3),
  kMAIN_CLK_to_DMIC = MUX_A(CM_DMICCLKSEL, 4),
  kWDT_OSC_to_DMIC = MUX_A(CM_DMICCLKSEL, 5),
  kNONE_to_DMIC = MUX_A(CM_DMICCLKSEL, 7),
  kMAIN_CLK_to_SCT_CLK = MUX_A(CM_SCTCLKSEL, 0),
  kSYS_PLL_to_SCT_CLK = MUX_A(CM_SCTCLKSEL, 1),
  kFRO_HF_to_SCT_CLK = MUX_A(CM_SCTCLKSEL, 2),
  kAUDIO_PLL_to_SCT_CLK = MUX_A(CM_SCTCLKSEL, 3),
  kNONE_to_SCT_CLK = MUX_A(CM_SCTCLKSEL, 7),
  kMAIN_CLK_to_LCD_CLK = MUX_A(CM_LCDCLKSEL, 0),
  kLCDCLKIN_to_LCD_CLK = MUX_A(CM_LCDCLKSEL, 1),
  kFRO_HF_to_LCD_CLK = MUX_A(CM_LCDCLKSEL, 2),
  kNONE_to_LCD_CLK = MUX_A(CM_LCDCLKSEL, 3),
  kMAIN_CLK_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 0),
  kSYS_PLL_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 1),
  kUSB_PLL_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 2),
  kFRO_HF_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 3),
  kAUDIO_PLL_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 4),
  kNONE_to_SDIO_CLK = MUX_A(CM_SDIOCLKSEL, 7),
  kMAIN_CLK_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 0),
  kFRO12M_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 1),
  kAUDIO_PLL_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 2),
  kI2C_CLK_FC6_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 3),
  kNONE_to_NONE = (int)0x80000000U
}
 The enumerator of clock attach Id. More...
 
enum  clock_div_name_t {
  kCLOCK_DivSystickClk = 0,
  kCLOCK_DivArmTrClkDiv = 1,
  kCLOCK_DivCan0Clk = 2,
  kCLOCK_DivCan1Clk = 3,
  kCLOCK_DivSmartCard0Clk = 4,
  kCLOCK_DivSmartCard1Clk = 5,
  kCLOCK_DivAhbClk = 32,
  kCLOCK_DivClkOut = 33,
  kCLOCK_DivFrohfClk = 34,
  kCLOCK_DivSpifiClk = 36,
  kCLOCK_DivAdcAsyncClk = 37,
  kCLOCK_DivUsb0Clk = 38,
  kCLOCK_DivUsb1Clk = 39,
  kCLOCK_DivFrg = 40,
  kCLOCK_DivDmicClk = 42,
  kCLOCK_DivMClk = 43,
  kCLOCK_DivLcdClk = 44,
  kCLOCK_DivSctClk = 45,
  kCLOCK_DivEmcClk = 46,
  kCLOCK_DivSdioClk = 47
}
 Clock dividers. More...
 
enum  pll_error_t {
  kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
  kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1),
  kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2),
  kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3),
  kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4),
  kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5),
  kStatus_PLL_CCOTooLow = MAKE_STATUS(kStatusGroup_Generic, 6),
  kStatus_PLL_CCOTooHigh = MAKE_STATUS(kStatusGroup_Generic, 7)
}
 PLL status definitions. More...
 
enum  clock_usb_src_t {
  kCLOCK_UsbSrcFro = (uint32_t)kCLOCK_FroHf,
  kCLOCK_UsbSrcSystemPll = (uint32_t)kCLOCK_PllOut,
  kCLOCK_UsbSrcMainClock = (uint32_t)kCLOCK_CoreSysClk,
  kCLOCK_UsbSrcUsbPll = (uint32_t)kCLOCK_UsbPll,
  kCLOCK_UsbSrcNone
}
 USB clock source definition. More...
 
enum  usb_pll_psel
 USB PDEL Divider. More...
 

Functions

void CLOCK_SetupFROClocking (uint32_t froFreq)
 Initialize the Core clock to given frequency (12, 48 or 96 MHz), this API is implememnt in ROM code. Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. Usage: CLOCK_SetupFROClocking(frequency), (frequency must be one of 12, 48 or 96 MHz) Note: Need to make sure ROM and OTP has power(PDRUNCFG0[17,29]= 0U) before calling this API since this API is implemented in ROM code and the FROHF TRIM value is stored in OTP. More...
 
void CLOCK_AttachClk (clock_attach_id_t connection)
 Configure the clock selection muxes. More...
 
clock_attach_id_t CLOCK_GetClockAttachId (clock_attach_id_t attachId)
 Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More...
 
void CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset)
 Setup peripheral clock dividers. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetFro12MFreq (void)
 Return Frequency of FRO 12MHz. More...
 
uint32_t CLOCK_GetClockOutClkFreq (void)
 Return Frequency of ClockOut. More...
 
uint32_t CLOCK_GetSpifiClkFreq (void)
 Return Frequency of Spifi Clock. More...
 
uint32_t CLOCK_GetAdcClkFreq (void)
 Return Frequency of Adc Clock. More...
 
uint32_t CLOCK_GetMCanClkFreq (uint32_t MCanSel)
 brief Return Frequency of MCAN Clock param MCanSel : 0U: MCAN0; 1U: MCAN1 return Frequency of MCAN Clock
 
uint32_t CLOCK_GetUsb0ClkFreq (void)
 Return Frequency of Usb0 Clock. More...
 
uint32_t CLOCK_GetUsb1ClkFreq (void)
 Return Frequency of Usb1 Clock. More...
 
uint32_t CLOCK_GetMclkClkFreq (void)
 Return Frequency of MClk Clock. More...
 
uint32_t CLOCK_GetSctClkFreq (void)
 Return Frequency of SCTimer Clock. More...
 
uint32_t CLOCK_GetSdioClkFreq (void)
 Return Frequency of SDIO Clock. More...
 
uint32_t CLOCK_GetLcdClkFreq (void)
 Return Frequency of LCD Clock. More...
 
uint32_t CLOCK_GetLcdClkIn (void)
 Return Frequency of LCD CLKIN Clock. More...
 
uint32_t CLOCK_GetExtClkFreq (void)
 Return Frequency of External Clock. More...
 
uint32_t CLOCK_GetWdtOscFreq (void)
 Return Frequency of Watchdog Oscillator. More...
 
uint32_t CLOCK_GetFroHfFreq (void)
 Return Frequency of High-Freq output of FRO. More...
 
uint32_t CLOCK_GetFrgClkFreq (void)
 Return Frequency of frg. More...
 
uint32_t CLOCK_GetDmicClkFreq (void)
 Return Frequency of dmic. More...
 
uint32_t CLOCK_SetFRGClock (uint32_t freq)
 Set FRG Clk. More...
 
uint32_t CLOCK_GetPllOutFreq (void)
 Return Frequency of PLL. More...
 
uint32_t CLOCK_GetUsbPllOutFreq (void)
 Return Frequency of USB PLL. More...
 
uint32_t CLOCK_GetAudioPllOutFreq (void)
 Return Frequency of AUDIO PLL. More...
 
uint32_t CLOCK_GetOsc32KFreq (void)
 Return Frequency of 32kHz osc. More...
 
uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of Core System. More...
 
uint32_t CLOCK_GetI2SMClkFreq (void)
 Return Frequency of I2S MCLK Clock. More...
 
uint32_t CLOCK_GetFlexCommClkFreq (uint32_t id)
 Return Frequency of Flexcomm functional Clock. More...
 
uint32_t CLOCK_GetFRGInputClock (void)
 return FRG Clk More...
 
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc (void)
 Return Asynchronous APB Clock source. More...
 
uint32_t CLOCK_GetAsyncApbClkFreq (void)
 Return Frequency of Asynchronous APB Clock. More...
 
__STATIC_INLINE uint32_t CLOCK_GetEmcClkFreq (void)
 Return EMC source. More...
 
uint32_t CLOCK_GetAudioPLLInClockRate (void)
 Return Audio PLL input clock rate. More...
 
uint32_t CLOCK_GetSystemPLLInClockRate (void)
 Return System PLL input clock rate. More...
 
uint32_t CLOCK_GetSystemPLLOutClockRate (bool recompute)
 Return System PLL output clock rate. More...
 
uint32_t CLOCK_GetAudioPLLOutClockRate (bool recompute)
 Return System AUDIO PLL output clock rate. More...
 
uint32_t CLOCK_GetUsbPLLOutClockRate (bool recompute)
 Return System USB PLL output clock rate. More...
 
__STATIC_INLINE void CLOCK_SetBypassPLL (bool bypass)
 Enables and disables PLL bypass mode. More...
 
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked (void)
 Check if PLL is locked or not. More...
 
__STATIC_INLINE bool CLOCK_IsUsbPLLLocked (void)
 Check if USB PLL is locked or not. More...
 
__STATIC_INLINE bool CLOCK_IsAudioPLLLocked (void)
 Check if AUDIO PLL is locked or not. More...
 
__STATIC_INLINE void CLOCK_Enable_SysOsc (bool enable)
 Enables and disables SYS OSC. More...
 
void CLOCK_SetStoredPLLClockRate (uint32_t rate)
 Store the current PLL rate. More...
 
void CLOCK_SetStoredAudioPLLClockRate (uint32_t rate)
 Store the current AUDIO PLL rate. More...
 
uint32_t CLOCK_GetSystemPLLOutFromSetup (pll_setup_t *pSetup)
 Return System PLL output clock rate from setup structure. More...
 
uint32_t CLOCK_GetAudioPLLOutFromSetup (pll_setup_t *pSetup)
 Return System AUDIO PLL output clock rate from setup structure. More...
 
uint32_t CLOCK_GetAudioPLLOutFromFractSetup (pll_setup_t *pSetup)
 Return System AUDIO PLL output clock rate from audio fractioanl setup structure. More...
 
uint32_t CLOCK_GetUsbPLLOutFromSetup (const usb_pll_setup_t *pSetup)
 Return System USB PLL output clock rate from setup structure. More...
 
pll_error_t CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup)
 Set PLL output based on the passed PLL setup data. More...
 
pll_error_t CLOCK_SetupAudioPLLData (pll_config_t *pControl, pll_setup_t *pSetup)
 Set AUDIO PLL output based on the passed AUDIO PLL setup data. More...
 
pll_error_t CLOCK_SetupSystemPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetupAudioPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg)
 Set AUDIO PLL output from AUDIOPLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetupAudioPLLPrecFract (pll_setup_t *pSetup, uint32_t flagcfg)
 Set AUDIO PLL output from AUDIOPLL setup structure using the Audio Fractional divider register(precise frequency) More...
 
pll_error_t CLOCK_SetPLLFreq (const pll_setup_t *pSetup)
 Set PLL output from PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetAudioPLLFreq (const pll_setup_t *pSetup)
 Set Audio PLL output from Audio PLL setup structure (precise frequency) More...
 
pll_error_t CLOCK_SetUsbPLLFreq (const usb_pll_setup_t *pSetup)
 Set USB PLL output from USB PLL setup structure (precise frequency) More...
 
void CLOCK_SetupSystemPLLMult (uint32_t multiply_by, uint32_t input_freq)
 Set PLL output based on the multiplier and input frequency. More...
 
static void CLOCK_DisableUsbDevicefs0Clock (clock_ip_name_t clk)
 Disable USB clock. More...
 
bool CLOCK_EnableUsbfs0DeviceClock (clock_usb_src_t src, uint32_t freq)
 Enable USB Device FS clock. More...
 
bool CLOCK_EnableUsbfs0HostClock (clock_usb_src_t src, uint32_t freq)
 Enable USB HOST FS clock. More...
 
void CLOCK_SetStoredUsbPLLClockRate (uint32_t rate)
 Set the current Usb PLL Rate.
 
bool CLOCK_EnableUsbhs0DeviceClock (clock_usb_src_t src, uint32_t freq)
 Enable USB Device HS clock. More...
 
bool CLOCK_EnableUsbhs0HostClock (clock_usb_src_t src, uint32_t freq)
 Enable USB HOST HS clock. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 3, 3))
 CLOCK driver version 2.3.3. More...
 

Data Structure Documentation

struct pll_config_t

This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.

Data Fields

uint32_t desiredRate
 Desired PLL rate in Hz.
 
uint32_t inputRate
 PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set.
 
uint32_t flags
 PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions.
 
struct pll_setup_t

It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.

Data Fields

uint32_t pllctrl
 PLL control register SYSPLLCTRL.
 
uint32_t pllndec
 PLL NDEC register SYSPLLNDEC.
 
uint32_t pllpdec
 PLL PDEC register SYSPLLPDEC.
 
uint32_t pllmdec
 PLL MDEC registers SYSPLLPDEC.
 
uint32_t pllRate
 Acutal PLL rate.
 
uint32_t audpllfrac
 only aduio PLL has this function
 
uint32_t flags
 PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions.
 
struct usb_pll_setup_t

It can be populated with the USB PLL setup function. If powering up or waiting for USB PLL lock, the PLL input clock source should be configured prior to USB PLL setup.

Data Fields

uint8_t msel
 USB PLL control register msel:1U-256U.
 
uint8_t psel
 USB PLL control register psel:only support inter 1U 2U 4U 8U.
 
uint8_t nsel
 USB PLL control register nsel:only suppoet inter 1U 2U 3U 4U.
 
bool direct
 USB PLL CCO output control.
 
bool bypass
 USB PLL inout clock bypass control.
 
bool fbsel
 USB PLL ineter mode and non-integer mode control.
 
uint32_t inputRate
 USB PLL input rate.
 

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 3, 3))
#define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL   0

When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.

Note
All drivers share this feature switcher. If it is set to 1, application should handle clock enable and disable for all drivers.
#define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT   2U

Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.

#define ADC_CLOCKS
Value:
{ \
}
Clock gate name: Adc0.
Definition: fsl_clock.h:341
#define ROM_CLOCKS
Value:
{ \
}
Clock gate name: Rom.
Definition: fsl_clock.h:307
#define SRAM_CLOCKS
Value:
{ \
}
Clock gate name: Sram2.
Definition: fsl_clock.h:311
Clock gate name: Sram3.
Definition: fsl_clock.h:313
Clock gate name: Sram1.
Definition: fsl_clock.h:309
#define FLASH_CLOCKS
Value:
{ \
kCLOCK_Flash \
}
#define FMC_CLOCKS
Value:
{ \
kCLOCK_Fmc \
}
#define EEPROM_CLOCKS
Value:
{ \
kCLOCK_Eeprom \
}
#define SPIFI_CLOCKS
Value:
{ \
}
Clock gate name: Spifi.
Definition: fsl_clock.h:315
#define INPUTMUX_CLOCKS
Value:
{ \
}
Clock gate name: InputMux.
Definition: fsl_clock.h:317
#define IOCON_CLOCKS
Value:
{ \
}
Clock gate name: Iocon.
Definition: fsl_clock.h:319
#define GPIO_CLOCKS
Value:
{ \
}
Clock gate name: Gpio1.
Definition: fsl_clock.h:323
Clock gate name: Gpio3.
Definition: fsl_clock.h:327
Clock gate name: Gpio5.
Definition: fsl_clock.h:465
Clock gate name: Gpio0.
Definition: fsl_clock.h:321
Clock gate name: Gpio2.
Definition: fsl_clock.h:325
Clock gate name: Gpio4.
Definition: fsl_clock.h:463
#define PINT_CLOCKS
Value:
{ \
}
Clock gate name: Pint.
Definition: fsl_clock.h:329
#define GINT_CLOCKS
Value:
{ \
}
Clock gate name: Gint.
Definition: fsl_clock.h:331
#define DMA_CLOCKS
Value:
{ \
}
Clock gate name: Dma.
Definition: fsl_clock.h:333
#define CRC_CLOCKS
Value:
{ \
}
Clock gate name: Crc.
Definition: fsl_clock.h:335
#define WWDT_CLOCKS
Value:
{ \
}
Clock gate name: Wwdt.
Definition: fsl_clock.h:337
#define RTC_CLOCKS
Value:
{ \
}
Clock gate name: Rtc.
Definition: fsl_clock.h:339
#define ADC0_CLOCKS
Value:
{ \
}
Clock gate name: Adc0.
Definition: fsl_clock.h:341
#define MRT_CLOCKS
Value:
{ \
}
Clock gate name: Mrt.
Definition: fsl_clock.h:343
#define RIT_CLOCKS
Value:
{ \
}
Clock gate name: Rit.
Definition: fsl_clock.h:345
#define SCT_CLOCKS
Value:
{ \
}
Clock gate name: Sct0.
Definition: fsl_clock.h:347
#define MCAN_CLOCKS
Value:
{ \
}
Clock gate name: Mcan1.
Definition: fsl_clock.h:351
Clock gate name: Mcan0.
Definition: fsl_clock.h:349
#define UTICK_CLOCKS
Value:
{ \
}
Clock gate name: Utick.
Definition: fsl_clock.h:353
#define FLEXCOMM_CLOCKS
Value:
{ \
}
Clock gate name: FlexComm10.
Definition: fsl_clock.h:503
Clock gate name: FlexComm5.
Definition: fsl_clock.h:365
Clock gate name: FlexComm7.
Definition: fsl_clock.h:369
Clock gate name: FlexComm0.
Definition: fsl_clock.h:355
Clock gate name: FlexComm9.
Definition: fsl_clock.h:475
Clock gate name: FlexComm6.
Definition: fsl_clock.h:367
Clock gate name: FlexComm8.
Definition: fsl_clock.h:473
Clock gate name: FlexComm3.
Definition: fsl_clock.h:361
Clock gate name: FlexComm1.
Definition: fsl_clock.h:357
Clock gate name: FlexComm2.
Definition: fsl_clock.h:359
Clock gate name: FlexComm4.
Definition: fsl_clock.h:363
#define LPUART_CLOCKS
Value:
{ \
}
Clock gate name: MinUart9.
Definition: fsl_clock.h:479
Clock gate name: MinUart5.
Definition: fsl_clock.h:381
Clock gate name: MinUart6.
Definition: fsl_clock.h:383
Clock gate name: MinUart0.
Definition: fsl_clock.h:371
Clock gate name: MinUart1.
Definition: fsl_clock.h:373
Clock gate name: MinUart7.
Definition: fsl_clock.h:385
Clock gate name: MinUart2.
Definition: fsl_clock.h:375
Clock gate name: MinUart4.
Definition: fsl_clock.h:379
Clock gate name: MinUart8.
Definition: fsl_clock.h:477
Clock gate name: MinUart3.
Definition: fsl_clock.h:377
#define BI2C_CLOCKS
Value:
{ \
}
Clock gate name: BI2c3.
Definition: fsl_clock.h:409
Clock gate name: BI2c0.
Definition: fsl_clock.h:403
Clock gate name: BI2c8.
Definition: fsl_clock.h:485
Clock gate name: BI2c6.
Definition: fsl_clock.h:415
Clock gate name: BI2c7.
Definition: fsl_clock.h:417
Clock gate name: BI2c5.
Definition: fsl_clock.h:413
Clock gate name: BI2c9.
Definition: fsl_clock.h:487
Clock gate name: BI2c1.
Definition: fsl_clock.h:405
Clock gate name: BI2c2.
Definition: fsl_clock.h:407
Clock gate name: BI2c4.
Definition: fsl_clock.h:411
#define LPSI_CLOCKS
Value:
{ \
}
Clock gate name: LSpi8.
Definition: fsl_clock.h:481
Clock gate name: LSpi7.
Definition: fsl_clock.h:401
Clock gate name: LSpi2.
Definition: fsl_clock.h:391
Clock gate name: LSpi0.
Definition: fsl_clock.h:387
Clock gate name: LSpi4.
Definition: fsl_clock.h:395
Clock gate name: LSpi1.
Definition: fsl_clock.h:389
Clock gate name: LSpi9.
Definition: fsl_clock.h:483
Clock gate name: LSpi6.
Definition: fsl_clock.h:399
Clock gate name: LSpi3.
Definition: fsl_clock.h:393
Clock gate name: LSpi5.
Definition: fsl_clock.h:397
#define FLEXI2S_CLOCKS
Value:
{ \
}
Clock gate name: FlexI2s8.
Definition: fsl_clock.h:489
Clock gate name: FlexI2s9.
Definition: fsl_clock.h:491
Clock gate name: FlexI2s4.
Definition: fsl_clock.h:427
Clock gate name: FlexI2s3.
Definition: fsl_clock.h:425
Clock gate name: FlexI2s5.
Definition: fsl_clock.h:429
Clock gate name: FlexI2s1.
Definition: fsl_clock.h:421
Clock gate name: FlexI2s6.
Definition: fsl_clock.h:431
Clock gate name: FlexI2s0.
Definition: fsl_clock.h:419
Clock gate name: FlexI2s7.
Definition: fsl_clock.h:433
Clock gate name: FlexI2s2.
Definition: fsl_clock.h:423
#define DMIC_CLOCKS
Value:
{ \
}
Clock gate name: DMic.
Definition: fsl_clock.h:435
#define CTIMER_CLOCKS
Value:
{ \
}
Clock gate name: Ct32b1.
Definition: fsl_clock.h:443
Clock gate name: Ct32b0.
Definition: fsl_clock.h:441
Clock gate name: Ct32b3.
Definition: fsl_clock.h:507
Clock gate name: Ct32b4.
Definition: fsl_clock.h:509
Clock gate name: Ct32b2.
Definition: fsl_clock.h:437
#define LCD_CLOCKS
Value:
{ \
}
Clock gate name: Lcd.
Definition: fsl_clock.h:449
#define SDIO_CLOCKS
Value:
{ \
}
Clock gate name: Sdio.
Definition: fsl_clock.h:451
#define USBRAM_CLOCKS
Value:
{ \
}
Clock gate name: UsbRam1.
Definition: fsl_clock.h:457
#define EMC_CLOCKS
Value:
{ \
}
Clock gate name: Emc.
Definition: fsl_clock.h:459
#define ETH_CLOCKS
Value:
{ \
}
Clock gate name: Eth.
Definition: fsl_clock.h:461
#define AES_CLOCKS
Value:
{ \
}
Clock gate name: Aes.
Definition: fsl_clock.h:467
#define OTP_CLOCKS
Value:
{ \
}
Clock gate name: Otp.
Definition: fsl_clock.h:469
#define RNG_CLOCKS
Value:
{ \
}
Clock gate name: Rng.
Definition: fsl_clock.h:471
#define USBHMR0_CLOCKS
Value:
{ \
}
Clock gate name: Usbhmr0.
Definition: fsl_clock.h:493
#define USBHSL0_CLOCKS
Value:
{ \
}
Clock gate name: Usbhsl0.
Definition: fsl_clock.h:495
#define SHA0_CLOCKS
Value:
{ \
}
Clock gate name: Sha0.
Definition: fsl_clock.h:497
#define SMARTCARD_CLOCKS
Value:
{ \
}
Clock gate name: SmartCard0.
Definition: fsl_clock.h:499
Clock gate name: SmartCard1.
Definition: fsl_clock.h:501
#define USBD_CLOCKS
Value:
{ \
}
Clock gate name: Usbd0.
Definition: fsl_clock.h:439
Clock gate name: Usbh1.
Definition: fsl_clock.h:453
Clock gate name: Usbd1.
Definition: fsl_clock.h:455
#define USBH_CLOCKS
Value:
{ \
}
Clock gate name: Usbh1.
Definition: fsl_clock.h:453
#define CLK_GATE_REG_OFFSET_SHIFT   8U
#define CLK_ATTACH_ID (   mux,
  sel,
  pos 
)    ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U))

[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*

#define PLL_CONFIGFLAG_USEINRATE   (1U << 0U)


When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.

When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup

#define PLL_SETUPFLAG_POWERUP   (1U << 0U)

Setup will power on the PLL after setup

Enumeration Type Documentation

Enumerator
kCLOCK_IpInvalid 

Invalid Ip Name.

kCLOCK_Rom 

Clock gate name: Rom.

kCLOCK_Sram1 

Clock gate name: Sram1.

kCLOCK_Sram2 

Clock gate name: Sram2.

kCLOCK_Sram3 

Clock gate name: Sram3.

kCLOCK_Spifi 

Clock gate name: Spifi.

kCLOCK_InputMux 

Clock gate name: InputMux.

kCLOCK_Iocon 

Clock gate name: Iocon.

kCLOCK_Gpio0 

Clock gate name: Gpio0.

kCLOCK_Gpio1 

Clock gate name: Gpio1.

kCLOCK_Gpio2 

Clock gate name: Gpio2.

kCLOCK_Gpio3 

Clock gate name: Gpio3.

kCLOCK_Pint 

Clock gate name: Pint.

kCLOCK_Gint 

Clock gate name: Gint.

kCLOCK_Dma 

Clock gate name: Dma.

kCLOCK_Crc 

Clock gate name: Crc.

kCLOCK_Wwdt 

Clock gate name: Wwdt.

kCLOCK_Rtc 

Clock gate name: Rtc.

kCLOCK_Adc0 

Clock gate name: Adc0.

kCLOCK_Mrt 

Clock gate name: Mrt.

kCLOCK_Rit 

Clock gate name: Rit.

kCLOCK_Sct0 

Clock gate name: Sct0.

kCLOCK_Mcan0 

Clock gate name: Mcan0.

kCLOCK_Mcan1 

Clock gate name: Mcan1.

kCLOCK_Utick 

Clock gate name: Utick.

kCLOCK_FlexComm0 

Clock gate name: FlexComm0.

kCLOCK_FlexComm1 

Clock gate name: FlexComm1.

kCLOCK_FlexComm2 

Clock gate name: FlexComm2.

kCLOCK_FlexComm3 

Clock gate name: FlexComm3.

kCLOCK_FlexComm4 

Clock gate name: FlexComm4.

kCLOCK_FlexComm5 

Clock gate name: FlexComm5.

kCLOCK_FlexComm6 

Clock gate name: FlexComm6.

kCLOCK_FlexComm7 

Clock gate name: FlexComm7.

kCLOCK_MinUart0 

Clock gate name: MinUart0.

kCLOCK_MinUart1 

Clock gate name: MinUart1.

kCLOCK_MinUart2 

Clock gate name: MinUart2.

kCLOCK_MinUart3 

Clock gate name: MinUart3.

kCLOCK_MinUart4 

Clock gate name: MinUart4.

kCLOCK_MinUart5 

Clock gate name: MinUart5.

kCLOCK_MinUart6 

Clock gate name: MinUart6.

kCLOCK_MinUart7 

Clock gate name: MinUart7.

kCLOCK_LSpi0 

Clock gate name: LSpi0.

kCLOCK_LSpi1 

Clock gate name: LSpi1.

kCLOCK_LSpi2 

Clock gate name: LSpi2.

kCLOCK_LSpi3 

Clock gate name: LSpi3.

kCLOCK_LSpi4 

Clock gate name: LSpi4.

kCLOCK_LSpi5 

Clock gate name: LSpi5.

kCLOCK_LSpi6 

Clock gate name: LSpi6.

kCLOCK_LSpi7 

Clock gate name: LSpi7.

kCLOCK_BI2c0 

Clock gate name: BI2c0.

kCLOCK_BI2c1 

Clock gate name: BI2c1.

kCLOCK_BI2c2 

Clock gate name: BI2c2.

kCLOCK_BI2c3 

Clock gate name: BI2c3.

kCLOCK_BI2c4 

Clock gate name: BI2c4.

kCLOCK_BI2c5 

Clock gate name: BI2c5.

kCLOCK_BI2c6 

Clock gate name: BI2c6.

kCLOCK_BI2c7 

Clock gate name: BI2c7.

kCLOCK_FlexI2s0 

Clock gate name: FlexI2s0.

kCLOCK_FlexI2s1 

Clock gate name: FlexI2s1.

kCLOCK_FlexI2s2 

Clock gate name: FlexI2s2.

kCLOCK_FlexI2s3 

Clock gate name: FlexI2s3.

kCLOCK_FlexI2s4 

Clock gate name: FlexI2s4.

kCLOCK_FlexI2s5 

Clock gate name: FlexI2s5.

kCLOCK_FlexI2s6 

Clock gate name: FlexI2s6.

kCLOCK_FlexI2s7 

Clock gate name: FlexI2s7.

kCLOCK_DMic 

Clock gate name: DMic.

kCLOCK_Ct32b2 

Clock gate name: Ct32b2.

kCLOCK_Usbd0 

Clock gate name: Usbd0.

kCLOCK_Ct32b0 

Clock gate name: Ct32b0.

kCLOCK_Ct32b1 

Clock gate name: Ct32b1.

kCLOCK_BodyBias0 

Clock gate name: BodyBias0.

kCLOCK_EzhArchB0 

Clock gate name: EzhArchB0.

kCLOCK_Lcd 

Clock gate name: Lcd.

kCLOCK_Sdio 

Clock gate name: Sdio.

kCLOCK_Usbh1 

Clock gate name: Usbh1.

kCLOCK_Usbd1 

Clock gate name: Usbd1.

kCLOCK_UsbRam1 

Clock gate name: UsbRam1.

kCLOCK_Emc 

Clock gate name: Emc.

kCLOCK_Eth 

Clock gate name: Eth.

kCLOCK_Gpio4 

Clock gate name: Gpio4.

kCLOCK_Gpio5 

Clock gate name: Gpio5.

kCLOCK_Aes 

Clock gate name: Aes.

kCLOCK_Otp 

Clock gate name: Otp.

kCLOCK_Rng 

Clock gate name: Rng.

kCLOCK_FlexComm8 

Clock gate name: FlexComm8.

kCLOCK_FlexComm9 

Clock gate name: FlexComm9.

kCLOCK_MinUart8 

Clock gate name: MinUart8.

kCLOCK_MinUart9 

Clock gate name: MinUart9.

kCLOCK_LSpi8 

Clock gate name: LSpi8.

kCLOCK_LSpi9 

Clock gate name: LSpi9.

kCLOCK_BI2c8 

Clock gate name: BI2c8.

kCLOCK_BI2c9 

Clock gate name: BI2c9.

kCLOCK_FlexI2s8 

Clock gate name: FlexI2s8.

kCLOCK_FlexI2s9 

Clock gate name: FlexI2s9.

kCLOCK_Usbhmr0 

Clock gate name: Usbhmr0.

kCLOCK_Usbhsl0 

Clock gate name: Usbhsl0.

kCLOCK_Sha0 

Clock gate name: Sha0.

kCLOCK_SmartCard0 

Clock gate name: SmartCard0.

kCLOCK_SmartCard1 

Clock gate name: SmartCard1.

kCLOCK_FlexComm10 

Clock gate name: FlexComm10.

kCLOCK_Puf 

Clock gate name: Puf.

kCLOCK_Ct32b3 

Clock gate name: Ct32b3.

kCLOCK_Ct32b4 

Clock gate name: Ct32b4.

Enumerator
kCLOCK_CoreSysClk 

Core/system clock (aka MAIN_CLK)

kCLOCK_BusClk 

Bus clock (AHB clock)

kCLOCK_ClockOut 

CLOCKOUT.

kCLOCK_FroHf 

FRO48/96.

kCLOCK_UsbPll 

USB1 PLL.

kCLOCK_Mclk 

MCLK.

kCLOCK_Fro12M 

FRO12M.

kCLOCK_ExtClk 

External Clock.

kCLOCK_PllOut 

PLL Output.

kCLOCK_UsbClk 

USB input.

kCLOCK_WdtOsc 

Watchdog Oscillator.

kCLOCK_Frg 

Frg Clock.

kCLOCK_AsyncApbClk 

Async APB clock.

Enumerator
kCLOCK_AsyncMainClk 

Main System clock.

kCLOCK_AsyncFro12Mhz 

12MHz FRO

kCLOCK_AsyncAudioPllClk 

Async Audio PLL clock.

kCLOCK_AsyncI2cClkFc6 

Async I2C clock.

Enumerator
kSYSTICK_DIV_CLK_to_SYSTICKCLK 

Attach SYSTICK_DIV_CLK to SYSTICKCLK.

kWDT_OSC_to_SYSTICKCLK 

Attach WDT_OSC to SYSTICKCLK.

kOSC32K_to_SYSTICKCLK 

Attach OSC32K to SYSTICKCLK.

kFRO12M_to_SYSTICKCLK 

Attach FRO12M to SYSTICKCLK.

kNONE_to_SYSTICKCLK 

Attach NONE to SYSTICKCLK.

kFRO12M_to_MAIN_CLK 

Attach FRO12M to MAIN_CLK.

kEXT_CLK_to_MAIN_CLK 

Attach EXT_CLK to MAIN_CLK.

kWDT_OSC_to_MAIN_CLK 

Attach WDT_OSC to MAIN_CLK.

kFRO_HF_to_MAIN_CLK 

Attach FRO_HF to MAIN_CLK.

kSYS_PLL_to_MAIN_CLK 

Attach SYS_PLL to MAIN_CLK.

kOSC32K_to_MAIN_CLK 

Attach OSC32K to MAIN_CLK.

kMAIN_CLK_to_CLKOUT 

Attach MAIN_CLK to CLKOUT.

kEXT_CLK_to_CLKOUT 

Attach EXT_CLK to CLKOUT.

kWDT_OSC_to_CLKOUT 

Attach WDT_OSC to CLKOUT.

kFRO_HF_to_CLKOUT 

Attach FRO_HF to CLKOUT.

kSYS_PLL_to_CLKOUT 

Attach SYS_PLL to CLKOUT.

kUSB_PLL_to_CLKOUT 

Attach USB_PLL to CLKOUT.

kAUDIO_PLL_to_CLKOUT 

Attach AUDIO_PLL to CLKOUT.

kOSC32K_OSC_to_CLKOUT 

Attach OSC32K_OSC to CLKOUT.

kFRO12M_to_SYS_PLL 

Attach FRO12M to SYS_PLL.

kEXT_CLK_to_SYS_PLL 

Attach EXT_CLK to SYS_PLL.

kWDT_OSC_to_SYS_PLL 

Attach WDT_OSC to SYS_PLL.

kOSC32K_to_SYS_PLL 

Attach OSC32K to SYS_PLL.

kNONE_to_SYS_PLL 

Attach NONE to SYS_PLL.

kFRO12M_to_AUDIO_PLL 

Attach FRO12M to AUDIO_PLL.

kEXT_CLK_to_AUDIO_PLL 

Attach EXT_CLK to AUDIO_PLL.

kNONE_to_AUDIO_PLL 

Attach NONE to AUDIO_PLL.

kMAIN_CLK_to_SPIFI_CLK 

Attach MAIN_CLK to SPIFI_CLK.

kSYS_PLL_to_SPIFI_CLK 

Attach SYS_PLL to SPIFI_CLK.

kUSB_PLL_to_SPIFI_CLK 

Attach USB_PLL to SPIFI_CLK.

kFRO_HF_to_SPIFI_CLK 

Attach FRO_HF to SPIFI_CLK.

kAUDIO_PLL_to_SPIFI_CLK 

Attach AUDIO_PLL to SPIFI_CLK.

kNONE_to_SPIFI_CLK 

Attach NONE to SPIFI_CLK.

kFRO_HF_to_ADC_CLK 

Attach FRO_HF to ADC_CLK.

kSYS_PLL_to_ADC_CLK 

Attach SYS_PLL to ADC_CLK.

kUSB_PLL_to_ADC_CLK 

Attach USB_PLL to ADC_CLK.

kAUDIO_PLL_to_ADC_CLK 

Attach AUDIO_PLL to ADC_CLK.

kNONE_to_ADC_CLK 

Attach NONE to ADC_CLK.

kFRO_HF_to_USB0_CLK 

Attach FRO_HF to USB0_CLK.

kSYS_PLL_to_USB0_CLK 

Attach SYS_PLL to USB0_CLK.

kUSB_PLL_to_USB0_CLK 

Attach USB_PLL to USB0_CLK.

kNONE_to_USB0_CLK 

Attach NONE to USB0_CLK.

kFRO_HF_to_USB1_CLK 

Attach FRO_HF to USB1_CLK.

kSYS_PLL_to_USB1_CLK 

Attach SYS_PLL to USB1_CLK.

kUSB_PLL_to_USB1_CLK 

Attach USB_PLL to USB1_CLK.

kNONE_to_USB1_CLK 

Attach NONE to USB1_CLK.

kFRO12M_to_FLEXCOMM0 

Attach FRO12M to FLEXCOMM0.

kFRO_HF_to_FLEXCOMM0 

Attach FRO_HF to FLEXCOMM0.

kAUDIO_PLL_to_FLEXCOMM0 

Attach AUDIO_PLL to FLEXCOMM0.

kMCLK_to_FLEXCOMM0 

Attach MCLK to FLEXCOMM0.

kFRG_to_FLEXCOMM0 

Attach FRG to FLEXCOMM0.

kNONE_to_FLEXCOMM0 

Attach NONE to FLEXCOMM0.

kFRO12M_to_FLEXCOMM1 

Attach FRO12M to FLEXCOMM1.

kFRO_HF_to_FLEXCOMM1 

Attach FRO_HF to FLEXCOMM1.

kAUDIO_PLL_to_FLEXCOMM1 

Attach AUDIO_PLL to FLEXCOMM1.

kMCLK_to_FLEXCOMM1 

Attach MCLK to FLEXCOMM1.

kFRG_to_FLEXCOMM1 

Attach FRG to FLEXCOMM1.

kNONE_to_FLEXCOMM1 

Attach NONE to FLEXCOMM1.

kFRO12M_to_FLEXCOMM2 

Attach FRO12M to FLEXCOMM2.

kFRO_HF_to_FLEXCOMM2 

Attach FRO_HF to FLEXCOMM2.

kAUDIO_PLL_to_FLEXCOMM2 

Attach AUDIO_PLL to FLEXCOMM2.

kMCLK_to_FLEXCOMM2 

Attach MCLK to FLEXCOMM2.

kFRG_to_FLEXCOMM2 

Attach FRG to FLEXCOMM2.

kNONE_to_FLEXCOMM2 

Attach NONE to FLEXCOMM2.

kFRO12M_to_FLEXCOMM3 

Attach FRO12M to FLEXCOMM3.

kFRO_HF_to_FLEXCOMM3 

Attach FRO_HF to FLEXCOMM3.

kAUDIO_PLL_to_FLEXCOMM3 

Attach AUDIO_PLL to FLEXCOMM3.

kMCLK_to_FLEXCOMM3 

Attach MCLK to FLEXCOMM3.

kFRG_to_FLEXCOMM3 

Attach FRG to FLEXCOMM3.

kNONE_to_FLEXCOMM3 

Attach NONE to FLEXCOMM3.

kFRO12M_to_FLEXCOMM4 

Attach FRO12M to FLEXCOMM4.

kFRO_HF_to_FLEXCOMM4 

Attach FRO_HF to FLEXCOMM4.

kAUDIO_PLL_to_FLEXCOMM4 

Attach AUDIO_PLL to FLEXCOMM4.

kMCLK_to_FLEXCOMM4 

Attach MCLK to FLEXCOMM4.

kFRG_to_FLEXCOMM4 

Attach FRG to FLEXCOMM4.

kNONE_to_FLEXCOMM4 

Attach NONE to FLEXCOMM4.

kFRO12M_to_FLEXCOMM5 

Attach FRO12M to FLEXCOMM5.

kFRO_HF_to_FLEXCOMM5 

Attach FRO_HF to FLEXCOMM5.

kAUDIO_PLL_to_FLEXCOMM5 

Attach AUDIO_PLL to FLEXCOMM5.

kMCLK_to_FLEXCOMM5 

Attach MCLK to FLEXCOMM5.

kFRG_to_FLEXCOMM5 

Attach FRG to FLEXCOMM5.

kNONE_to_FLEXCOMM5 

Attach NONE to FLEXCOMM5.

kFRO12M_to_FLEXCOMM6 

Attach FRO12M to FLEXCOMM6.

kFRO_HF_to_FLEXCOMM6 

Attach FRO_HF to FLEXCOMM6.

kAUDIO_PLL_to_FLEXCOMM6 

Attach AUDIO_PLL to FLEXCOMM6.

kMCLK_to_FLEXCOMM6 

Attach MCLK to FLEXCOMM6.

kFRG_to_FLEXCOMM6 

Attach FRG to FLEXCOMM6.

kNONE_to_FLEXCOMM6 

Attach NONE to FLEXCOMM6.

kFRO12M_to_FLEXCOMM7 

Attach FRO12M to FLEXCOMM7.

kFRO_HF_to_FLEXCOMM7 

Attach FRO_HF to FLEXCOMM7.

kAUDIO_PLL_to_FLEXCOMM7 

Attach AUDIO_PLL to FLEXCOMM7.

kMCLK_to_FLEXCOMM7 

Attach MCLK to FLEXCOMM7.

kFRG_to_FLEXCOMM7 

Attach FRG to FLEXCOMM7.

kNONE_to_FLEXCOMM7 

Attach NONE to FLEXCOMM7.

kFRO12M_to_FLEXCOMM8 

Attach FRO12M to FLEXCOMM8.

kFRO_HF_to_FLEXCOMM8 

Attach FRO_HF to FLEXCOMM8.

kAUDIO_PLL_to_FLEXCOMM8 

Attach AUDIO_PLL to FLEXCOMM8.

kMCLK_to_FLEXCOMM8 

Attach MCLK to FLEXCOMM8.

kFRG_to_FLEXCOMM8 

Attach FRG to FLEXCOMM8.

kNONE_to_FLEXCOMM8 

Attach NONE to FLEXCOMM8.

kFRO12M_to_FLEXCOMM9 

Attach FRO12M to FLEXCOMM9.

kFRO_HF_to_FLEXCOMM9 

Attach FRO_HF to FLEXCOMM9.

kAUDIO_PLL_to_FLEXCOMM9 

Attach AUDIO_PLL to FLEXCOMM9.

kMCLK_to_FLEXCOMM9 

Attach MCLK to FLEXCOMM9.

kFRG_to_FLEXCOMM9 

Attach FRG to FLEXCOMM9.

kNONE_to_FLEXCOMM9 

Attach NONE to FLEXCOMM9.

kMAIN_CLK_to_FLEXCOMM10 

Attach MAIN_CLK to FLEXCOMM10.

kSYS_PLL_to_FLEXCOMM10 

Attach SYS_PLL to FLEXCOMM10.

kUSB_PLL_to_FLEXCOMM10 

Attach USB_PLL to FLEXCOMM10.

kFRO_HF_to_FLEXCOMM10 

Attach FRO_HF to FLEXCOMM10.

kAUDIO_PLL_to_FLEXCOMM10 

Attach AUDIO_PLL to FLEXCOMM10.

kNONE_to_FLEXCOMM10 

Attach NONE to FLEXCOMM10.

kFRO_HF_to_MCLK 

Attach FRO_HF to MCLK.

kAUDIO_PLL_to_MCLK 

Attach AUDIO_PLL to MCLK.

kNONE_to_MCLK 

Attach NONE to MCLK.

kMAIN_CLK_to_FRG 

Attach MAIN_CLK to FRG.

kSYS_PLL_to_FRG 

Attach SYS_PLL to FRG.

kFRO12M_to_FRG 

Attach FRO12M to FRG.

kFRO_HF_to_FRG 

Attach FRO_HF to FRG.

kNONE_to_FRG 

Attach NONE to FRG.

kFRO12M_to_DMIC 

Attach FRO12M to DMIC.

kFRO_HF_DIV_to_DMIC 

Attach FRO_HF_DIV to DMIC.

kAUDIO_PLL_to_DMIC 

Attach AUDIO_PLL to DMIC.

kMCLK_to_DMIC 

Attach MCLK to DMIC.

kMAIN_CLK_to_DMIC 

Attach MAIN_CLK to DMIC.

kWDT_OSC_to_DMIC 

Attach WDT_OSC to DMIC.

kNONE_to_DMIC 

Attach NONE to DMIC.

kMAIN_CLK_to_SCT_CLK 

Attach MAIN_CLK to SCT_CLK.

kSYS_PLL_to_SCT_CLK 

Attach SYS_PLL to SCT_CLK.

kFRO_HF_to_SCT_CLK 

Attach FRO_HF to SCT_CLK.

kAUDIO_PLL_to_SCT_CLK 

Attach AUDIO_PLL to SCT_CLK.

kNONE_to_SCT_CLK 

Attach NONE to SCT_CLK.

kMAIN_CLK_to_LCD_CLK 

Attach MAIN_CLK to LCD_CLK.

kLCDCLKIN_to_LCD_CLK 

Attach LCDCLKIN to LCD_CLK.

kFRO_HF_to_LCD_CLK 

Attach FRO_HF to LCD_CLK.

kNONE_to_LCD_CLK 

Attach NONE to LCD_CLK.

kMAIN_CLK_to_SDIO_CLK 

Attach MAIN_CLK to SDIO_CLK.

kSYS_PLL_to_SDIO_CLK 

Attach SYS_PLL to SDIO_CLK.

kUSB_PLL_to_SDIO_CLK 

Attach USB_PLL to SDIO_CLK.

kFRO_HF_to_SDIO_CLK 

Attach FRO_HF to SDIO_CLK.

kAUDIO_PLL_to_SDIO_CLK 

Attach AUDIO_PLL to SDIO_CLK.

kNONE_to_SDIO_CLK 

Attach NONE to SDIO_CLK.

kMAIN_CLK_to_ASYNC_APB 

Attach MAIN_CLK to ASYNC_APB.

kFRO12M_to_ASYNC_APB 

Attach FRO12M to ASYNC_APB.

kAUDIO_PLL_to_ASYNC_APB 

Attach AUDIO_PLL to ASYNC_APB.

kI2C_CLK_FC6_to_ASYNC_APB 

Attach I2C_CLK_FC6 to ASYNC_APB.

kNONE_to_NONE 

Attach NONE to NONE.

Enumerator
kCLOCK_DivSystickClk 

Systick Clock Divider.

kCLOCK_DivArmTrClkDiv 

Arm Tr Clk Div Divider.

kCLOCK_DivCan0Clk 

Can0 Clock Divider.

kCLOCK_DivCan1Clk 

Can1 Clock Divider.

kCLOCK_DivSmartCard0Clk 

Smart Card0 Clock Divider.

kCLOCK_DivSmartCard1Clk 

Smart Card1 Clock Divider.

kCLOCK_DivAhbClk 

Ahb Clock Divider.

kCLOCK_DivClkOut 

Clk Out Divider.

kCLOCK_DivFrohfClk 

Frohf Clock Divider.

kCLOCK_DivSpifiClk 

Spifi Clock Divider.

kCLOCK_DivAdcAsyncClk 

Adc Async Clock Divider.

kCLOCK_DivUsb0Clk 

Usb0 Clock Divider.

kCLOCK_DivUsb1Clk 

Usb1 Clock Divider.

kCLOCK_DivFrg 

Frg Divider.

kCLOCK_DivDmicClk 

Dmic Clock Divider.

kCLOCK_DivMClk 

Main Clock Divider.

kCLOCK_DivLcdClk 

Lcd Clock Divider.

kCLOCK_DivSctClk 

Sct Clock Divider.

kCLOCK_DivEmcClk 

Emc Clock Divider.

kCLOCK_DivSdioClk 

Sdio clock divider.

Enumerator
kStatus_PLL_Success 

PLL operation was successful.

kStatus_PLL_OutputTooLow 

PLL output rate request was too low.

kStatus_PLL_OutputTooHigh 

PLL output rate request was too high.

kStatus_PLL_InputTooLow 

PLL input rate is too low.

kStatus_PLL_InputTooHigh 

PLL input rate is too high.

kStatus_PLL_OutsideIntLimit 

Requested output rate isn't possible.

kStatus_PLL_CCOTooLow 

Requested CCO rate isn't possible.

kStatus_PLL_CCOTooHigh 

Requested CCO rate isn't possible.

Enumerator
kCLOCK_UsbSrcFro 

Use FRO 96 or 48 MHz.

kCLOCK_UsbSrcSystemPll 

Use System PLL output.

kCLOCK_UsbSrcMainClock 

Use Main clock.

kCLOCK_UsbSrcUsbPll 

Use USB PLL clock.

kCLOCK_UsbSrcNone 

Use None, this may be selected in order to reduce power when no output is needed.

Function Documentation

void CLOCK_SetupFROClocking ( uint32_t  froFreq)
Parameters
froFreqtarget fro frequency.
Returns
Nothing
void CLOCK_AttachClk ( clock_attach_id_t  connection)
Parameters
connection: Clock to be configured.
Returns
Nothing
clock_attach_id_t CLOCK_GetClockAttachId ( clock_attach_id_t  attachId)
Parameters
attachId: Clock attach id to get.
Returns
Clock source value.
void CLOCK_SetClkDiv ( clock_div_name_t  div_name,
uint32_t  divided_by_value,
bool  reset 
)
Parameters
div_name: Clock divider name
divided_by_value,:Value to be divided
reset: Whether to reset the divider counter.
Returns
Nothing
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetFro12MFreq ( void  )
Returns
Frequency of FRO 12MHz
uint32_t CLOCK_GetClockOutClkFreq ( void  )
Returns
Frequency of ClockOut
uint32_t CLOCK_GetSpifiClkFreq ( void  )
Returns
Frequency of Spifi.
uint32_t CLOCK_GetAdcClkFreq ( void  )
Returns
Frequency of Adc Clock.
uint32_t CLOCK_GetUsb0ClkFreq ( void  )
Returns
Frequency of Usb0 Clock.
uint32_t CLOCK_GetUsb1ClkFreq ( void  )
Returns
Frequency of Usb1 Clock.
uint32_t CLOCK_GetMclkClkFreq ( void  )
Returns
Frequency of MClk Clock.
uint32_t CLOCK_GetSctClkFreq ( void  )
Returns
Frequency of SCTimer Clock.
uint32_t CLOCK_GetSdioClkFreq ( void  )
Returns
Frequency of SDIO Clock.
uint32_t CLOCK_GetLcdClkFreq ( void  )
Returns
Frequency of LCD Clock.
uint32_t CLOCK_GetLcdClkIn ( void  )
Returns
Frequency of LCD CLKIN Clock.
uint32_t CLOCK_GetExtClkFreq ( void  )
Returns
Frequency of External Clock. If no external clock is used returns 0.
uint32_t CLOCK_GetWdtOscFreq ( void  )
Returns
Frequency of Watchdog Oscillator
uint32_t CLOCK_GetFroHfFreq ( void  )
Returns
Frequency of High-Freq output of FRO
uint32_t CLOCK_GetFrgClkFreq ( void  )
Returns
Frequency of FRG
uint32_t CLOCK_GetDmicClkFreq ( void  )
Returns
Frequency of DMIC
uint32_t CLOCK_SetFRGClock ( uint32_t  freq)
Returns
1: if set FRG CLK successfully. 0: if set FRG CLK fail.
uint32_t CLOCK_GetPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetUsbPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetAudioPllOutFreq ( void  )
Returns
Frequency of PLL
uint32_t CLOCK_GetOsc32KFreq ( void  )
Returns
Frequency of 32kHz osc
uint32_t CLOCK_GetCoreSysClkFreq ( void  )
Returns
Frequency of Core System
uint32_t CLOCK_GetI2SMClkFreq ( void  )
Returns
Frequency of I2S MCLK Clock
uint32_t CLOCK_GetFlexCommClkFreq ( uint32_t  id)
Returns
Frequency of Flexcomm functional Clock
uint32_t CLOCK_GetFRGInputClock ( void  )
Returns
Frequency of FRG CLK.
__STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc ( void  )
Returns
Asynchronous APB CLock source
uint32_t CLOCK_GetAsyncApbClkFreq ( void  )
Returns
Frequency of Asynchronous APB Clock Clock
__STATIC_INLINE uint32_t CLOCK_GetEmcClkFreq ( void  )
Returns
EMC source
uint32_t CLOCK_GetAudioPLLInClockRate ( void  )
Returns
Audio PLL input clock rate
uint32_t CLOCK_GetSystemPLLInClockRate ( void  )
Returns
System PLL input clock rate
uint32_t CLOCK_GetSystemPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a PLL rate recomputation if true
Returns
System PLL output clock rate
Note
The PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
uint32_t CLOCK_GetAudioPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a AUDIO PLL rate recomputation if true
Returns
System AUDIO PLL output clock rate
Note
The AUDIO PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
uint32_t CLOCK_GetUsbPLLOutClockRate ( bool  recompute)
Parameters
recompute: Forces a USB PLL rate recomputation if true
Returns
System USB PLL output clock rate
Note
The USB PLL rate is cached in the driver in a variable as the rate computation function can take some time to perform. It is recommended to use 'false' with the 'recompute' parameter.
__STATIC_INLINE void CLOCK_SetBypassPLL ( bool  bypass)

bypass : true to bypass PLL (PLL output = PLL input, false to disable bypass

Returns
System PLL output clock rate
__STATIC_INLINE bool CLOCK_IsSystemPLLLocked ( void  )
Returns
true if the PLL is locked, false if not locked
__STATIC_INLINE bool CLOCK_IsUsbPLLLocked ( void  )
Returns
true if the USB PLL is locked, false if not locked
__STATIC_INLINE bool CLOCK_IsAudioPLLLocked ( void  )
Returns
true if the AUDIO PLL is locked, false if not locked
__STATIC_INLINE void CLOCK_Enable_SysOsc ( bool  enable)

enable : true to enable SYS OSC, false to disable SYS OSC

void CLOCK_SetStoredPLLClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL
Returns
Nothing
void CLOCK_SetStoredAudioPLLClockRate ( uint32_t  rate)
Parameters
rate,:Current rate of the PLL
Returns
Nothing
uint32_t CLOCK_GetSystemPLLOutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetAudioPLLOutFromSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetAudioPLLOutFromFractSetup ( pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
uint32_t CLOCK_GetUsbPLLOutFromSetup ( const usb_pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to a PLL setup structure
Returns
System PLL output clock rate the setup structure will generate
pll_error_t CLOCK_SetupPLLData ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupAudioPLLData ( pll_config_t *  pControl,
pll_setup_t *  pSetup 
)
Parameters
pControl: Pointer to populated PLL control structure to generate setup with
pSetup: Pointer to PLL setup structure to be filled
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
Actual frequency for setup may vary from the desired frequency based on the accuracy of input clocks, rounding, non-fractional PLL mode, etc.
pll_error_t CLOCK_SetupSystemPLLPrec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetupAudioPLLPrec ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the AUDIO PLL, wait for PLL lock, and adjust system voltages to the new AUDIOPLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the AUDIO PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetupAudioPLLPrecFract ( pll_setup_t *  pSetup,
uint32_t  flagcfg 
)
Parameters
pSetup: Pointer to populated PLL setup structure
flagcfg: Flag configuration for PLL config structure
Returns
PLL_ERROR_SUCCESS on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the AUDIO PLL, wait for PLL lock, and adjust system voltages to the new AUDIOPLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the AUDIO PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetPLLFreq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or PLL setup error code
Note
This function will power off the PLL, setup the PLL with the new setup data, and then optionally powerup the PLL, wait for PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetAudioPLLFreq ( const pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated PLL setup structure
Returns
kStatus_PLL_Success on success, or Audio PLL setup error code
Note
This function will power off the PLL, setup the Audio PLL with the new setup data, and then optionally powerup the PLL, wait for Audio PLL lock, and adjust system voltages to the new PLL rate. The function will not alter any source clocks (ie, main systen clock) that may use the Audio PLL, so these should be setup prior to and after exiting the function.
pll_error_t CLOCK_SetUsbPLLFreq ( const usb_pll_setup_t *  pSetup)
Parameters
pSetup: Pointer to populated USB PLL setup structure
Returns
kStatus_PLL_Success on success, or USB PLL setup error code
Note
This function will power off the USB PLL, setup the PLL with the new setup data, and then optionally powerup the USB PLL, wait for USB PLL lock, and adjust system voltages to the new USB PLL rate. The function will not alter any source clocks (ie, usb pll clock) that may use the USB PLL, so these should be setup prior to and after exiting the function.
void CLOCK_SetupSystemPLLMult ( uint32_t  multiply_by,
uint32_t  input_freq 
)
Parameters
multiply_by: multiplier
input_freq: Clock input frequency of the PLL
Returns
Nothing
Note
Unlike the Chip_Clock_SetupSystemPLLPrec() function, this function does not disable or enable PLL power, wait for PLL lock, or adjust system voltages. These must be done in the application. The function will not alter any source clocks (ie, main systen clock) that may use the PLL, so these should be setup prior to and after exiting the function.
static void CLOCK_DisableUsbDevicefs0Clock ( clock_ip_name_t  clk)
inlinestatic

Disable USB clock.

bool CLOCK_EnableUsbfs0DeviceClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB Device Full Speed clock.
bool CLOCK_EnableUsbfs0HostClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB HOST Full Speed clock.
bool CLOCK_EnableUsbhs0DeviceClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB Device High Speed clock.
bool CLOCK_EnableUsbhs0HostClock ( clock_usb_src_t  src,
uint32_t  freq 
)
Parameters
src: clock source
freq,:clock frequency Enable USB HOST High Speed clock.