![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides a peripheral driver for the SHA module in MCUXpresso SDK devices.
The driver provides blocking synchronous APIs. The SHA operations are complete (and results are made availabe for further usage) when a function returns. When called, these functions do not return until an SHA operation is complete. These functions use main CPU for simple polling loops to determine operation complete or error status and data movements. The driver functions are not re-entrant. These functions provide typical interface to upper layer or application software.
Clock to the SHA module has to be enabled before using the driver API.
SHA operations provided by this driver are not re-entrant. Therefore, the application software should ensure the SHA module operation is not requested from different tasks or interrupt service routines while an operation is in progress.
Typical use case Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sha
Modules | |
| Sha_algorithm_level_api | |
Files | |
| file | fsl_sha.h |
Data Structures | |
| struct | sha_ctx_t |
| Storage type used to save hash context. More... | |
Macros | |
| #define | SHA_CTX_SIZE 22U |
| SHA Context size. More... | |
Typedefs | |
| typedef void(* | sha_callback_t )(SHA_Type *base, sha_ctx_t *ctx, status_t status, void *userData) |
| background hash callback function. More... | |
Enumerations | |
| enum | sha_algo_t { kSHA_Sha1, kSHA_Sha256 } |
| Supported cryptographic block cipher functions for HASH creation. More... | |
Driver version | |
| #define | FSL_SHA_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
| Defines LPC SHA driver version 2.3.2. More... | |
| struct sha_ctx_t |
| #define FSL_SHA_DRIVER_VERSION (MAKE_VERSION(2, 3, 2)) |
Current version: 2.3.2
Change log:
| #define SHA_CTX_SIZE 22U |
| enum sha_algo_t |