MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Serial Manager

Overview

This chapter describes the programming interface of the serial manager component.

The serial manager component provides a series of APIs to operate different serial port types. The port types it supports are UART, USB CDC and SWO.

Modules

 Serial Port SWO
 
 Serial Port Uart
 

Data Structures

struct  _serial_manager_config
 serial manager config structure More...
 
struct  _serial_manager_callback_message
 Callback message structure. More...
 

Macros

#define SERIAL_MANAGER_NON_BLOCKING_MODE   (1U)
 Enable or disable serial manager non-blocking mode (1 - enable, 0 - disable)
 
#define SERIAL_MANAGER_RING_BUFFER_FLOWCONTROL   (0U)
 Enable or ring buffer flow control (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_UART   (0U)
 Enable or disable uart port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_UART_DMA   (0U)
 Enable or disable uart dma port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_USBCDC   (0U)
 Enable or disable USB CDC port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_SWO   (0U)
 Enable or disable SWO port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_VIRTUAL   (0U)
 Enable or disable USB CDC virtual port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_RPMSG   (0U)
 Enable or disable rPMSG port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_SPI_MASTER   (0U)
 Enable or disable SPI Master port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_SPI_SLAVE   (0U)
 Enable or disable SPI Slave port (1 - enable, 0 - disable)
 
#define SERIAL_PORT_TYPE_BLE_WU   (0U)
 Enable or disable BLE WU port (1 - enable, 0 - disable)
 
#define SERIAL_MANAGER_WRITE_TIME_DELAY_DEFAULT_VALUE   (1U)
 Set the default delay time in ms used by SerialManager_WriteTimeDelay(). More...
 
#define SERIAL_MANAGER_READ_TIME_DELAY_DEFAULT_VALUE   (1U)
 Set the default delay time in ms used by SerialManager_ReadTimeDelay(). More...
 
#define SERIAL_MANAGER_TASK_HANDLE_RX_AVAILABLE_NOTIFY   (0U)
 Enable or disable SerialManager_Task() handle RX data available notify.
 
#define SERIAL_MANAGER_WRITE_HANDLE_SIZE   (44U)
 Set serial manager write handle size.
 
#define SERIAL_MANAGER_USE_COMMON_TASK   (0U)
 SERIAL_PORT_UART_HANDLE_SIZE/SERIAL_PORT_USB_CDC_HANDLE_SIZE + serial manager dedicated size. More...
 
#define SERIAL_MANAGER_HANDLE_SIZE   (SERIAL_MANAGER_HANDLE_SIZE_TEMP + 124U)
 Definition of serial manager handle size. More...
 
#define SERIAL_MANAGER_HANDLE_DEFINE(name)   uint32_t name[((SERIAL_MANAGER_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]
 Defines the serial manager handle. More...
 
#define SERIAL_MANAGER_WRITE_HANDLE_DEFINE(name)   uint32_t name[((SERIAL_MANAGER_WRITE_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]
 Defines the serial manager write handle. More...
 
#define SERIAL_MANAGER_READ_HANDLE_DEFINE(name)   uint32_t name[((SERIAL_MANAGER_READ_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]
 Defines the serial manager read handle. More...
 
#define SERIAL_MANAGER_TASK_PRIORITY   (2U)
 Macro to set serial manager task priority. More...
 
#define SERIAL_MANAGER_TASK_STACK_SIZE   (1000U)
 Macro to set serial manager task stack size. More...
 

Typedefs

typedef void * serial_handle_t
 The handle of the serial manager module.
 
typedef void * serial_write_handle_t
 The write handle of the serial manager module.
 
typedef void * serial_read_handle_t
 The read handle of the serial manager module.
 
typedef enum _serial_port_type serial_port_type_t
 serial port type
 
typedef enum _serial_manager_type serial_manager_type_t
 serial manager type
 
typedef struct
_serial_manager_config 
serial_manager_config_t
 serial manager config structure
 
typedef enum _serial_manager_status serial_manager_status_t
 serial manager error code
 
typedef struct
_serial_manager_callback_message 
serial_manager_callback_message_t
 Callback message structure.
 
typedef void(* serial_manager_callback_t )(void *callbackParam, serial_manager_callback_message_t *message, serial_manager_status_t status)
 serial manager callback function
 
typedef int32_t(* serial_manager_lowpower_critical_callback_t )(int32_t power_mode)
 serial manager Lowpower Critical callback function
 

Enumerations

enum  _serial_port_type {
  kSerialPort_None = 0U,
  kSerialPort_Uart = 1U,
  kSerialPort_UsbCdc,
  kSerialPort_Swo,
  kSerialPort_Virtual,
  kSerialPort_Rpmsg,
  kSerialPort_UartDma,
  kSerialPort_SpiMaster,
  kSerialPort_SpiSlave,
  kSerialPort_BleWu
}
 serial port type More...
 
enum  _serial_manager_type {
  kSerialManager_NonBlocking = 0x0U,
  kSerialManager_Blocking = 0x8F41U
}
 serial manager type More...
 
enum  _serial_manager_status {
  kStatus_SerialManager_Success = kStatus_Success,
  kStatus_SerialManager_Error = MAKE_STATUS(kStatusGroup_SERIALMANAGER, 1),
  kStatus_SerialManager_Busy = MAKE_STATUS(kStatusGroup_SERIALMANAGER, 2),
  kStatus_SerialManager_Notify = MAKE_STATUS(kStatusGroup_SERIALMANAGER, 3),
  kStatus_SerialManager_Canceled,
  kStatus_SerialManager_HandleConflict = MAKE_STATUS(kStatusGroup_SERIALMANAGER, 5),
  kStatus_SerialManager_RingBufferOverflow,
  kStatus_SerialManager_NotConnected = MAKE_STATUS(kStatusGroup_SERIALMANAGER, 7)
}
 serial manager error code More...
 

Functions

serial_manager_status_t SerialManager_Init (serial_handle_t serialHandle, const serial_manager_config_t *serialConfig)
 Initializes a serial manager module with the serial manager handle and the user configuration structure. More...
 
serial_manager_status_t SerialManager_Deinit (serial_handle_t serialHandle)
 De-initializes the serial manager module instance. More...
 
serial_manager_status_t SerialManager_OpenWriteHandle (serial_handle_t serialHandle, serial_write_handle_t writeHandle)
 Opens a writing handle for the serial manager module. More...
 
serial_manager_status_t SerialManager_CloseWriteHandle (serial_write_handle_t writeHandle)
 Closes a writing handle for the serial manager module. More...
 
serial_manager_status_t SerialManager_OpenReadHandle (serial_handle_t serialHandle, serial_read_handle_t readHandle)
 Opens a reading handle for the serial manager module. More...
 
serial_manager_status_t SerialManager_CloseReadHandle (serial_read_handle_t readHandle)
 Closes a reading for the serial manager module. More...
 
serial_manager_status_t SerialManager_WriteBlocking (serial_write_handle_t writeHandle, uint8_t *buffer, uint32_t length)
 Transmits data with the blocking mode. More...
 
serial_manager_status_t SerialManager_ReadBlocking (serial_read_handle_t readHandle, uint8_t *buffer, uint32_t length)
 Reads data with the blocking mode. More...
 
serial_manager_status_t SerialManager_WriteNonBlocking (serial_write_handle_t writeHandle, uint8_t *buffer, uint32_t length)
 Transmits data with the non-blocking mode. More...
 
serial_manager_status_t SerialManager_ReadNonBlocking (serial_read_handle_t readHandle, uint8_t *buffer, uint32_t length)
 Reads data with the non-blocking mode. More...
 
serial_manager_status_t SerialManager_TryRead (serial_read_handle_t readHandle, uint8_t *buffer, uint32_t length, uint32_t *receivedLength)
 Tries to read data. More...
 
serial_manager_status_t SerialManager_CancelWriting (serial_write_handle_t writeHandle)
 Cancels unfinished send transmission. More...
 
serial_manager_status_t SerialManager_CancelReading (serial_read_handle_t readHandle)
 Cancels unfinished receive transmission. More...
 
serial_manager_status_t SerialManager_InstallTxCallback (serial_write_handle_t writeHandle, serial_manager_callback_t callback, void *callbackParam)
 Installs a TX callback and callback parameter. More...
 
serial_manager_status_t SerialManager_InstallRxCallback (serial_read_handle_t readHandle, serial_manager_callback_t callback, void *callbackParam)
 Installs a RX callback and callback parameter. More...
 
static bool SerialManager_needPollingIsr (void)
 Check if need polling ISR. More...
 
serial_manager_status_t SerialManager_EnterLowpower (serial_handle_t serialHandle)
 Prepares to enter low power consumption. More...
 
serial_manager_status_t SerialManager_ExitLowpower (serial_handle_t serialHandle)
 Restores from low power consumption. More...
 
void SerialManager_SetLowpowerCriticalCb (const serial_manager_lowpower_critical_CBs_t *pfCallback)
 This function performs initialization of the callbacks structure used to disable lowpower when serial manager is active. More...
 

Data Structure Documentation

struct _serial_manager_config

Data Fields

uint8_t * ringBuffer
 Ring buffer address, it is used to buffer data received by the hardware. More...
 
uint32_t ringBufferSize
 The size of the ring buffer.
 
serial_port_type_t type
 Serial port type.
 
serial_manager_type_t blockType
 Serial manager port type.
 
void * portConfig
 Serial port configuration.
 

Field Documentation

uint8_t* _serial_manager_config::ringBuffer

Besides, the memory space cannot be free during the lifetime of the serial manager module.

struct _serial_manager_callback_message

Data Fields

uint8_t * buffer
 Transferred buffer.
 
uint32_t length
 Transferred data length.
 

Macro Definition Documentation

#define SERIAL_MANAGER_WRITE_TIME_DELAY_DEFAULT_VALUE   (1U)
#define SERIAL_MANAGER_READ_TIME_DELAY_DEFAULT_VALUE   (1U)
#define SERIAL_MANAGER_USE_COMMON_TASK   (0U)

Macro to determine whether use common task.

#define SERIAL_MANAGER_HANDLE_SIZE   (SERIAL_MANAGER_HANDLE_SIZE_TEMP + 124U)
#define SERIAL_MANAGER_HANDLE_DEFINE (   name)    uint32_t name[((SERIAL_MANAGER_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]

This macro is used to define a 4 byte aligned serial manager handle. Then use "(serial_handle_t)name" to get the serial manager handle.

The macro should be global and could be optional. You could also define serial manager handle by yourself.

This is an example,

* SERIAL_MANAGER_HANDLE_DEFINE(serialManagerHandle);
*
Parameters
nameThe name string of the serial manager handle.
#define SERIAL_MANAGER_WRITE_HANDLE_DEFINE (   name)    uint32_t name[((SERIAL_MANAGER_WRITE_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]

This macro is used to define a 4 byte aligned serial manager write handle. Then use "(serial_write_handle_t)name" to get the serial manager write handle.

The macro should be global and could be optional. You could also define serial manager write handle by yourself.

This is an example,

* SERIAL_MANAGER_WRITE_HANDLE_DEFINE(serialManagerwriteHandle);
*
Parameters
nameThe name string of the serial manager write handle.
#define SERIAL_MANAGER_READ_HANDLE_DEFINE (   name)    uint32_t name[((SERIAL_MANAGER_READ_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))]

This macro is used to define a 4 byte aligned serial manager read handle. Then use "(serial_read_handle_t)name" to get the serial manager read handle.

The macro should be global and could be optional. You could also define serial manager read handle by yourself.

This is an example,

* SERIAL_MANAGER_READ_HANDLE_DEFINE(serialManagerReadHandle);
*
Parameters
nameThe name string of the serial manager read handle.
#define SERIAL_MANAGER_TASK_PRIORITY   (2U)
#define SERIAL_MANAGER_TASK_STACK_SIZE   (1000U)

Enumeration Type Documentation

Enumerator
kSerialPort_None 

Serial port is none.

kSerialPort_Uart 

Serial port UART.

kSerialPort_UsbCdc 

Serial port USB CDC.

kSerialPort_Swo 

Serial port SWO.

kSerialPort_Virtual 

Serial port Virtual.

kSerialPort_Rpmsg 

Serial port RPMSG.

kSerialPort_UartDma 

Serial port UART DMA.

kSerialPort_SpiMaster 

Serial port SPIMASTER.

kSerialPort_SpiSlave 

Serial port SPISLAVE.

kSerialPort_BleWu 

Serial port BLE WU.

Enumerator
kSerialManager_NonBlocking 

None blocking handle.

kSerialManager_Blocking 

Blocking handle.

Enumerator
kStatus_SerialManager_Success 

Success.

kStatus_SerialManager_Error 

Failed.

kStatus_SerialManager_Busy 

Busy.

kStatus_SerialManager_Notify 

Ring buffer is not empty.

kStatus_SerialManager_Canceled 

the non-blocking request is canceled

kStatus_SerialManager_HandleConflict 

The handle is opened.

kStatus_SerialManager_RingBufferOverflow 

The ring buffer is overflowed.

kStatus_SerialManager_NotConnected 

The host is not connected.

Function Documentation

serial_manager_status_t SerialManager_Init ( serial_handle_t  serialHandle,
const serial_manager_config_t *  serialConfig 
)

This function configures the Serial Manager module with user-defined settings. The user can configure the configuration structure. The parameter serialHandle is a pointer to point to a memory space of size SERIAL_MANAGER_HANDLE_SIZE allocated by the caller. The Serial Manager module supports three types of serial port, UART (includes UART, USART, LPSCI, LPUART, etc), USB CDC and swo. Please refer to serial_port_type_t for serial port setting. These three types can be set by using serial_manager_config_t.

Example below shows how to use this API to configure the Serial Manager. For UART,

* #define SERIAL_MANAGER_RING_BUFFER_SIZE (256U)
* static SERIAL_MANAGER_HANDLE_DEFINE(s_serialHandle);
* static uint8_t s_ringBuffer[SERIAL_MANAGER_RING_BUFFER_SIZE];
*
* serial_port_uart_config_t uartConfig;
* config.ringBuffer = &s_ringBuffer[0];
* config.ringBufferSize = SERIAL_MANAGER_RING_BUFFER_SIZE;
* uartConfig.instance = 0;
* uartConfig.clockRate = 24000000;
* uartConfig.baudRate = 115200;
* uartConfig.parityMode = kSerialManager_UartParityDisabled;
* uartConfig.stopBitCount = kSerialManager_UartOneStopBit;
* uartConfig.enableRx = 1;
* uartConfig.enableTx = 1;
* uartConfig.enableRxRTS = 0;
* uartConfig.enableTxCTS = 0;
* config.portConfig = &uartConfig;
* SerialManager_Init((serial_handle_t)s_serialHandle, &config);
*

For USB CDC,

* #define SERIAL_MANAGER_RING_BUFFER_SIZE (256U)
* static SERIAL_MANAGER_HANDLE_DEFINE(s_serialHandle);
* static uint8_t s_ringBuffer[SERIAL_MANAGER_RING_BUFFER_SIZE];
*
* serial_port_usb_cdc_config_t usbCdcConfig;
* config.ringBuffer = &s_ringBuffer[0];
* config.ringBufferSize = SERIAL_MANAGER_RING_BUFFER_SIZE;
* usbCdcConfig.controllerIndex = kSerialManager_UsbControllerKhci0;
* config.portConfig = &usbCdcConfig;
* SerialManager_Init((serial_handle_t)s_serialHandle, &config);
*

Example below shows how to use this API to configure the Serial Manager task configuration. For example if user need do specfical configuration(s_os_thread_def_serialmanager)for the serial mananger task,

* #define SERIAL_MANAGER_RING_BUFFER_SIZE (256U)
* static SERIAL_MANAGER_HANDLE_DEFINE(s_serialHandle);
* static uint8_t s_ringBuffer[SERIAL_MANAGER_RING_BUFFER_SIZE];
* const osa_task_def_t s_os_thread_def_serialmanager = {
* .tpriority = 4,
* .instances = 1,
* .stacksize = 2048,
* };
* serial_port_uart_config_t uartConfig;
* config.ringBuffer = &s_ringBuffer[0];
* config.ringBufferSize = SERIAL_MANAGER_RING_BUFFER_SIZE;
* config.serialTaskConfig = (osa_task_def_t *)&s_os_thread_def_serialmanager,
* uartConfig.instance = 0;
* uartConfig.clockRate = 24000000;
* uartConfig.baudRate = 115200;
* uartConfig.parityMode = kSerialManager_UartParityDisabled;
* uartConfig.stopBitCount = kSerialManager_UartOneStopBit;
* uartConfig.enableRx = 1;
* uartConfig.enableTx = 1;
* uartConfig.enableRxRTS = 0;
* uartConfig.enableTxCTS = 0;
* config.portConfig = &uartConfig;
* SerialManager_Init((serial_handle_t)s_serialHandle, &config);
*
Parameters
serialHandlePointer to point to a memory space of size SERIAL_MANAGER_HANDLE_SIZE allocated by the caller. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: SERIAL_MANAGER_HANDLE_DEFINE(serialHandle); or uint32_t serialHandle[((SERIAL_MANAGER_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))];
serialConfigPointer to user-defined configuration structure.
Return values
kStatus_SerialManager_ErrorAn error occurred.
kStatus_SerialManager_SuccessThe Serial Manager module initialization succeed.
serial_manager_status_t SerialManager_Deinit ( serial_handle_t  serialHandle)

This function de-initializes the serial manager module instance. If the opened writing or reading handle is not closed, the function will return kStatus_SerialManager_Busy.

Parameters
serialHandleThe serial manager module handle pointer.
Return values
kStatus_SerialManager_SuccessThe serial manager de-initialization succeed.
kStatus_SerialManager_BusyOpened reading or writing handle is not closed.
serial_manager_status_t SerialManager_OpenWriteHandle ( serial_handle_t  serialHandle,
serial_write_handle_t  writeHandle 
)

This function Opens a writing handle for the serial manager module. If the serial manager needs to be used in different tasks, the task should open a dedicated write handle for itself by calling SerialManager_OpenWriteHandle. Since there can only one buffer for transmission for the writing handle at the same time, multiple writing handles need to be opened when the multiple transmission is needed for a task.

Parameters
serialHandleThe serial manager module handle pointer. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices.
writeHandleThe serial manager module writing handle pointer. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: SERIAL_MANAGER_WRITE_HANDLE_DEFINE(writeHandle); or uint32_t writeHandle[((SERIAL_MANAGER_WRITE_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))];
Return values
kStatus_SerialManager_ErrorAn error occurred.
kStatus_SerialManager_HandleConflictThe writing handle was opened.
kStatus_SerialManager_SuccessThe writing handle is opened.

Example below shows how to use this API to write data. For task 1,

* static SERIAL_MANAGER_WRITE_HANDLE_DEFINE(s_serialWriteHandle1);
* static uint8_t s_nonBlockingWelcome1[] = "This is non-blocking writing log for task1!\r\n";
* Task1_SerialManagerTxCallback,
* s_serialWriteHandle1);
* s_nonBlockingWelcome1,
* sizeof(s_nonBlockingWelcome1) - 1U);
*

For task 2,

* static SERIAL_MANAGER_WRITE_HANDLE_DEFINE(s_serialWriteHandle2);
* static uint8_t s_nonBlockingWelcome2[] = "This is non-blocking writing log for task2!\r\n";
* Task2_SerialManagerTxCallback,
* s_serialWriteHandle2);
* s_nonBlockingWelcome2,
* sizeof(s_nonBlockingWelcome2) - 1U);
*
serial_manager_status_t SerialManager_CloseWriteHandle ( serial_write_handle_t  writeHandle)

This function Closes a writing handle for the serial manager module.

Parameters
writeHandleThe serial manager module writing handle pointer.
Return values
kStatus_SerialManager_SuccessThe writing handle is closed.
serial_manager_status_t SerialManager_OpenReadHandle ( serial_handle_t  serialHandle,
serial_read_handle_t  readHandle 
)

This function Opens a reading handle for the serial manager module. The reading handle can not be opened multiple at the same time. The error code kStatus_SerialManager_Busy would be returned when the previous reading handle is not closed. And there can only be one buffer for receiving for the reading handle at the same time.

Parameters
serialHandleThe serial manager module handle pointer. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices.
readHandleThe serial manager module reading handle pointer. The handle should be 4 byte aligned, because unaligned access doesn't be supported on some devices. You can define the handle in the following two ways: SERIAL_MANAGER_READ_HANDLE_DEFINE(readHandle); or uint32_t readHandle[((SERIAL_MANAGER_READ_HANDLE_SIZE + sizeof(uint32_t) - 1U) / sizeof(uint32_t))];
Return values
kStatus_SerialManager_ErrorAn error occurred.
kStatus_SerialManager_SuccessThe reading handle is opened.
kStatus_SerialManager_BusyPrevious reading handle is not closed.

Example below shows how to use this API to read data.

* static SERIAL_MANAGER_READ_HANDLE_DEFINE(s_serialReadHandle);
* static uint8_t s_nonBlockingBuffer[64];
* APP_SerialManagerRxCallback,
* s_serialReadHandle);
* s_nonBlockingBuffer,
* sizeof(s_nonBlockingBuffer));
*
serial_manager_status_t SerialManager_CloseReadHandle ( serial_read_handle_t  readHandle)

This function Closes a reading for the serial manager module.

Parameters
readHandleThe serial manager module reading handle pointer.
Return values
kStatus_SerialManager_SuccessThe reading handle is closed.
serial_manager_status_t SerialManager_WriteBlocking ( serial_write_handle_t  writeHandle,
uint8_t *  buffer,
uint32_t  length 
)

This is a blocking function, which polls the sending queue, waits for the sending queue to be empty. This function sends data using an interrupt method. The interrupt of the hardware could not be disabled. And There can only one buffer for transmission for the writing handle at the same time.

Note
The function SerialManager_WriteBlocking and the function SerialManager_WriteNonBlocking cannot be used at the same time. And, the function SerialManager_CancelWriting cannot be used to abort the transmission of this function.
Parameters
writeHandleThe serial manager module handle pointer.
bufferStart address of the data to write.
lengthLength of the data to write.
Return values
kStatus_SerialManager_SuccessSuccessfully sent all data.
kStatus_SerialManager_BusyPrevious transmission still not finished; data not all sent yet.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_ReadBlocking ( serial_read_handle_t  readHandle,
uint8_t *  buffer,
uint32_t  length 
)

This is a blocking function, which polls the receiving buffer, waits for the receiving buffer to be full. This function receives data using an interrupt method. The interrupt of the hardware could not be disabled. And There can only one buffer for receiving for the reading handle at the same time.

Note
The function SerialManager_ReadBlocking and the function SerialManager_ReadNonBlocking cannot be used at the same time. And, the function SerialManager_CancelReading cannot be used to abort the transmission of this function.
Parameters
readHandleThe serial manager module handle pointer.
bufferStart address of the data to store the received data.
lengthThe length of the data to be received.
Return values
kStatus_SerialManager_SuccessSuccessfully received all data.
kStatus_SerialManager_BusyPrevious transmission still not finished; data not all received yet.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_WriteNonBlocking ( serial_write_handle_t  writeHandle,
uint8_t *  buffer,
uint32_t  length 
)

This is a non-blocking function, which returns directly without waiting for all data to be sent. When all data is sent, the module notifies the upper layer through a TX callback function and passes the status parameter kStatus_SerialManager_Success. This function sends data using an interrupt method. The interrupt of the hardware could not be disabled. And There can only one buffer for transmission for the writing handle at the same time.

Note
The function SerialManager_WriteBlocking and the function SerialManager_WriteNonBlocking cannot be used at the same time. And, the TX callback is mandatory before the function could be used.
Parameters
writeHandleThe serial manager module handle pointer.
bufferStart address of the data to write.
lengthLength of the data to write.
Return values
kStatus_SerialManager_SuccessSuccessfully sent all data.
kStatus_SerialManager_BusyPrevious transmission still not finished; data not all sent yet.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_ReadNonBlocking ( serial_read_handle_t  readHandle,
uint8_t *  buffer,
uint32_t  length 
)

This is a non-blocking function, which returns directly without waiting for all data to be received. When all data is received, the module driver notifies the upper layer through a RX callback function and passes the status parameter kStatus_SerialManager_Success. This function receives data using an interrupt method. The interrupt of the hardware could not be disabled. And There can only one buffer for receiving for the reading handle at the same time.

Note
The function SerialManager_ReadBlocking and the function SerialManager_ReadNonBlocking cannot be used at the same time. And, the RX callback is mandatory before the function could be used.
Parameters
readHandleThe serial manager module handle pointer.
bufferStart address of the data to store the received data.
lengthThe length of the data to be received.
Return values
kStatus_SerialManager_SuccessSuccessfully received all data.
kStatus_SerialManager_BusyPrevious transmission still not finished; data not all received yet.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_TryRead ( serial_read_handle_t  readHandle,
uint8_t *  buffer,
uint32_t  length,
uint32_t *  receivedLength 
)

The function tries to read data from internal ring buffer. If the ring buffer is not empty, the data will be copied from ring buffer to up layer buffer. The copied length is the minimum of the ring buffer and up layer length. After the data is copied, the actual data length is passed by the parameter length. And There can only one buffer for receiving for the reading handle at the same time.

Parameters
readHandleThe serial manager module handle pointer.
bufferStart address of the data to store the received data.
lengthThe length of the data to be received.
receivedLengthLength received from the ring buffer directly.
Return values
kStatus_SerialManager_SuccessSuccessfully received all data.
kStatus_SerialManager_BusyPrevious transmission still not finished; data not all received yet.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_CancelWriting ( serial_write_handle_t  writeHandle)

The function cancels unfinished send transmission. When the transfer is canceled, the module notifies the upper layer through a TX callback function and passes the status parameter kStatus_SerialManager_Canceled.

Note
The function SerialManager_CancelWriting cannot be used to abort the transmission of the function SerialManager_WriteBlocking.
Parameters
writeHandleThe serial manager module handle pointer.
Return values
kStatus_SerialManager_SuccessGet successfully abort the sending.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_CancelReading ( serial_read_handle_t  readHandle)

The function cancels unfinished receive transmission. When the transfer is canceled, the module notifies the upper layer through a RX callback function and passes the status parameter kStatus_SerialManager_Canceled.

Note
The function SerialManager_CancelReading cannot be used to abort the transmission of the function SerialManager_ReadBlocking.
Parameters
readHandleThe serial manager module handle pointer.
Return values
kStatus_SerialManager_SuccessGet successfully abort the receiving.
kStatus_SerialManager_ErrorAn error occurred.
serial_manager_status_t SerialManager_InstallTxCallback ( serial_write_handle_t  writeHandle,
serial_manager_callback_t  callback,
void *  callbackParam 
)

This function is used to install the TX callback and callback parameter for the serial manager module. When any status of TX transmission changed, the driver will notify the upper layer by the installed callback function. And the status is also passed as status parameter when the callback is called.

Parameters
writeHandleThe serial manager module handle pointer.
callbackThe callback function.
callbackParamThe parameter of the callback function.
Return values
kStatus_SerialManager_SuccessSuccessfully install the callback.
serial_manager_status_t SerialManager_InstallRxCallback ( serial_read_handle_t  readHandle,
serial_manager_callback_t  callback,
void *  callbackParam 
)

This function is used to install the RX callback and callback parameter for the serial manager module. When any status of RX transmission changed, the driver will notify the upper layer by the installed callback function. And the status is also passed as status parameter when the callback is called.

Parameters
readHandleThe serial manager module handle pointer.
callbackThe callback function.
callbackParamThe parameter of the callback function.
Return values
kStatus_SerialManager_SuccessSuccessfully install the callback.
static bool SerialManager_needPollingIsr ( void  )
inlinestatic

This function is used to check if need polling ISR.

Return values
TRUEif need polling.
serial_manager_status_t SerialManager_EnterLowpower ( serial_handle_t  serialHandle)

This function is used to prepare to enter low power consumption.

Parameters
serialHandleThe serial manager module handle pointer.
Return values
kStatus_SerialManager_SuccessSuccessful operation.
serial_manager_status_t SerialManager_ExitLowpower ( serial_handle_t  serialHandle)

This function is used to restore from low power consumption.

Parameters
serialHandleThe serial manager module handle pointer.
Return values
kStatus_SerialManager_SuccessSuccessful operation.
void SerialManager_SetLowpowerCriticalCb ( const serial_manager_lowpower_critical_CBs_t *  pfCallback)
Parameters
pfCallbackPointer to the function structure used to allow/disable lowpower.