![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _spdif_edma_transfer |
| SPDIF transfer structure. More... | |
| struct | _spdif_edma_handle |
| SPDIF DMA transfer handle, users should not touch the content of the handle. More... | |
Typedefs | |
| typedef void(* | spdif_edma_callback_t )(SPDIF_Type *base, spdif_edma_handle_t *handle, status_t status, void *userData) |
| SPDIF eDMA transfer callback function for finish and error. | |
| typedef struct _spdif_edma_transfer | spdif_edma_transfer_t |
| SPDIF transfer structure. | |
Driver version | |
| #define | FSL_SPDIF_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 8)) |
| Version 2.0.8. | |
eDMA Transactional | |
| void | SPDIF_TransferTxCreateHandleEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_callback_t callback, void *userData, edma_handle_t *dmaLeftHandle, edma_handle_t *dmaRightHandle) |
| Initializes the SPDIF eDMA handle. More... | |
| void | SPDIF_TransferRxCreateHandleEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_callback_t callback, void *userData, edma_handle_t *dmaLeftHandle, edma_handle_t *dmaRightHandle) |
| Initializes the SPDIF Rx eDMA handle. More... | |
| status_t | SPDIF_TransferSendEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_transfer_t *xfer) |
| Performs a non-blocking SPDIF transfer using DMA. More... | |
| status_t | SPDIF_TransferReceiveEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, spdif_edma_transfer_t *xfer) |
| Performs a non-blocking SPDIF receive using eDMA. More... | |
| void | SPDIF_TransferAbortSendEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle) |
| Aborts a SPDIF transfer using eDMA. More... | |
| void | SPDIF_TransferAbortReceiveEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle) |
| Aborts a SPDIF receive using eDMA. More... | |
| status_t | SPDIF_TransferGetSendCountEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, size_t *count) |
| Gets byte count sent by SPDIF. More... | |
| status_t | SPDIF_TransferGetReceiveCountEDMA (SPDIF_Type *base, spdif_edma_handle_t *handle, size_t *count) |
| Gets byte count received by SPDIF. More... | |
| struct _spdif_edma_transfer |
Data Fields | |
| uint8_t * | leftData |
| Data start address to transfer. More... | |
| uint8_t * | rightData |
| Data start address to transfer. More... | |
| size_t | dataSize |
| Transfer size. More... | |
| uint8_t* _spdif_edma_transfer::leftData |
| uint8_t* _spdif_edma_transfer::rightData |
| size_t _spdif_edma_transfer::dataSize |
| struct _spdif_edma_handle |
Data Fields | |
| edma_handle_t * | dmaLeftHandle |
| DMA handler for SPDIF left channel. | |
| edma_handle_t * | dmaRightHandle |
| DMA handler for SPDIF right channel. | |
| uint8_t | nbytes |
| eDMA minor byte transfer count initially configured. More... | |
| uint8_t | count |
| The transfer data count in a DMA request. | |
| uint32_t | state |
| Internal state for SPDIF eDMA transfer. | |
| spdif_edma_callback_t | callback |
| Callback for users while transfer finish or error occurs. | |
| void * | userData |
| User callback parameter. | |
| edma_tcd_t | leftTcd [SPDIF_XFER_QUEUE_SIZE+1U] |
| TCD pool for eDMA transfer. More... | |
| edma_tcd_t | rightTcd [SPDIF_XFER_QUEUE_SIZE+1U] |
| TCD pool for eDMA transfer. More... | |
| spdif_edma_transfer_t | spdifQueue [SPDIF_XFER_QUEUE_SIZE] |
| Transfer queue storing queued transfer. More... | |
| size_t | transferSize [SPDIF_XFER_QUEUE_SIZE] |
| Data bytes need to transfer, left and right are the same, so use one. | |
| volatile uint8_t | queueUser |
| Index for user to queue transfer. More... | |
| volatile uint8_t | queueDriver |
| Index for driver to get the transfer data and size. | |
| uint8_t _spdif_edma_handle::nbytes |
| edma_tcd_t _spdif_edma_handle::leftTcd[SPDIF_XFER_QUEUE_SIZE+1U] |
| edma_tcd_t _spdif_edma_handle::rightTcd[SPDIF_XFER_QUEUE_SIZE+1U] |
| spdif_edma_transfer_t _spdif_edma_handle::spdifQueue[SPDIF_XFER_QUEUE_SIZE] |
| volatile uint8_t _spdif_edma_handle::queueUser |
| void SPDIF_TransferTxCreateHandleEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaLeftHandle, | ||
| edma_handle_t * | dmaRightHandle | ||
| ) |
This function initializes the SPDIF master DMA handle, which can be used for other SPDIF master transactional APIs. Usually, for a specified SPDIF instance, call this API once to get the initialized handle.
| base | SPDIF base pointer. |
| handle | SPDIF eDMA handle pointer. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaLeftHandle | eDMA handle pointer for left channel, this handle shall be static allocated by users. |
| dmaRightHandle | eDMA handle pointer for right channel, this handle shall be static allocated by users. |
| void SPDIF_TransferRxCreateHandleEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | dmaLeftHandle, | ||
| edma_handle_t * | dmaRightHandle | ||
| ) |
This function initializes the SPDIF slave DMA handle, which can be used for other SPDIF master transactional APIs. Usually, for a specified SPDIF instance, call this API once to get the initialized handle.
| base | SPDIF base pointer. |
| handle | SPDIF eDMA handle pointer. |
| callback | Pointer to user callback function. |
| userData | User parameter passed to the callback function. |
| dmaLeftHandle | eDMA handle pointer for left channel, this handle shall be static allocated by users. |
| dmaRightHandle | eDMA handle pointer for right channel, this handle shall be static allocated by users. |
| status_t SPDIF_TransferSendEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_transfer_t * | xfer | ||
| ) |
| base | SPDIF base pointer. |
| handle | SPDIF eDMA handle pointer. |
| xfer | Pointer to the DMA transfer structure. |
| kStatus_Success | Start a SPDIF eDMA send successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_TxBusy | SPDIF is busy sending data. |
| status_t SPDIF_TransferReceiveEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| spdif_edma_transfer_t * | xfer | ||
| ) |
| base | SPDIF base pointer |
| handle | SPDIF eDMA handle pointer. |
| xfer | Pointer to DMA transfer structure. |
| kStatus_Success | Start a SPDIF eDMA receive successfully. |
| kStatus_InvalidArgument | The input argument is invalid. |
| kStatus_RxBusy | SPDIF is busy receiving data. |
| void SPDIF_TransferAbortSendEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle | ||
| ) |
| base | SPDIF base pointer. |
| handle | SPDIF eDMA handle pointer. |
| void SPDIF_TransferAbortReceiveEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle | ||
| ) |
| base | SPDIF base pointer |
| handle | SPDIF eDMA handle pointer. |
| status_t SPDIF_TransferGetSendCountEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SPDIF base pointer. |
| handle | SPDIF eDMA handle pointer. |
| count | Bytes count sent by SPDIF. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |
| status_t SPDIF_TransferGetReceiveCountEDMA | ( | SPDIF_Type * | base, |
| spdif_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | SPDIF base pointer |
| handle | SPDIF eDMA handle pointer. |
| count | Bytes count received by SPDIF. |
| kStatus_Success | Succeed get the transfer count. |
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. |