The MCUXpresso SDK provides a peripheral driver for the Direct Memory Access Multiplexer (DMAMUX) of MCUXpresso SDK devices.
Typical use case
DMAMUX Operation
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dmamux 
      
        
          | void DMAMUX_Init  | 
          ( | 
          DMAMUX_Type *  | 
          base | ) | 
           | 
        
      
 
This function ungates the DMAMUX clock.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
  
   
 
 
      
        
          | void DMAMUX_Deinit  | 
          ( | 
          DMAMUX_Type *  | 
          base | ) | 
           | 
        
      
 
This function gates the DMAMUX clock.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_EnableChannel  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function enables the DMAMUX channel.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_DisableChannel  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function disables the DMAMUX channel.
- Note
 - The user must disable the DMAMUX channel before configuring it. 
 
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_SetSource  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel,  | 
         
        
           | 
           | 
          int32_t  | 
          source  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
    | source | Channel source, which is used to trigger the DMA transfer.User need to use the dma_request_source_t type as the input parameter.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_EnablePeriodTrigger  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function enables the DMAMUX period trigger feature.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_DisablePeriodTrigger  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function disables the DMAMUX period trigger.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
  
   
 
 
  
  
      
        
          | static void DMAMUX_EnableAlwaysOn  | 
          ( | 
          DMAMUX_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint32_t  | 
          channel,  | 
         
        
           | 
           | 
          bool  | 
          enable  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
This function enables the DMAMUX channel always ON feature.
- Parameters
 - 
  
    | base | DMAMUX peripheral base address.  | 
    | channel | DMAMUX channel number.  | 
    | enable | Switcher of the always ON feature. "true" means enabled, "false" means disabled.  |