The MCUXpresso SDK provides a peripheral driver for I2S function using Flexible I/O module of MCUXpresso SDK devices.
The FlexIO I2S driver includes functional APIs and transactional APIs.
Functional APIs are feature/property target low level APIs.
Functional APIs can be used for FlexIO I2S initialization/configuration/operation for optimization/customization purpose. Using the functional API requires the knowledge of the FlexIO I2S peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. FlexIO I2S functional operation groups provide the functional APIs set.
Transactional APIs are transaction target high level APIs. The transactional APIs can be used to enable the peripheral and also in the application if the code size and performance of transactional APIs can satisfy requirements. If the code size and performance are critical requirements, see the transactional API implementation and write custom code. All transactional APIs use the sai_handle_t as the first parameter. Initialize the handle by calling the FlexIO_I2S_TransferTxCreateHandle() or FlexIO_I2S_TransferRxCreateHandle() API.
Transactional APIs support asynchronous transfer. This means that the functions FLEXIO_I2S_TransferSendNonBlocking() and FLEXIO_I2S_TransferReceiveNonBlocking() set up an interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_FLEXIO_I2S_TxIdle and kStatus_FLEXIO_I2S_RxIdle status.
Typical use case
FlexIO I2S send/receive using an interrupt method
volatile bool txFinished;
volatile bool rxFinished;
const uint8_t sendData[] = [......];
{
    userData = userData;
    if (kStatus_FLEXIO_I2S_TxIdle == status)
    {
        txFinished = true;
    }
}
void main(void)
{
    
    FLEXIO_I2S_TxGetDefaultConfig(&user_config);
    FLEXIO_I2S_TxInit(FLEXIO I2S0, &user_config);
    
    FLEXIO_I2S_TransferTxSetTransferFormat(FLEXIO I2S0, &g_saiHandle, mclkSource, mclk);
    
    sendXfer.
dataSize = 
sizeof(sendData)/
sizeof(sendData[0]);
 
    txFinished = false;
    
    
    while (!txFinished)
    {
    }
    
}
 
FLEXIO_I2S send/receive using a DMA method
dma_handle_t g_saiTxDmaHandle;
dma_handle_t g_saiRxDmaHandle;
volatile bool txFinished;
uint8_t sendData[] = ...;
{
    userData = userData;
    if (kStatus_FLEXIO_I2S_TxIdle == status)
    {
        txFinished = true;
    }
}
void main(void)
{
    
    FLEXIO_I2S_TxGetDefaultConfig(&user_config);
    FLEXIO_I2S_TxInit(FLEXIO I2S0, &user_config);
    
    DMAMUX_SetSource(DMAMUX0, FLEXIO_I2S_TX_DMA_CHANNEL, FLEXIO_I2S_TX_DMA_REQUEST);
 
    DMA_Init(DMA0);
    
    DMA_TransferTxCreateHandle(&g_saiTxDmaHandle, DMA0, FLEXIO_I2S_TX_DMA_CHANNEL);
    FLEXIO_I2S_TransferTxCreateHandleDMA(FLEXIO I2S0, &g_saiTxDmaHandle, FLEXIO_I2S_UserCallback, NULL);
    
    sendXfer.
dataSize = 
sizeof(sendData)/
sizeof(sendData[0]);
 
    txFinished = false;
    
    FLEXIO_I2S_TransferSendDMA(&g_saiHandle, &sendXfer);
    
    while (!txFinished)
    {
    }
    
}
  
 | 
| enum   | {  
  kStatus_FLEXIO_I2S_Idle = MAKE_STATUS(kStatusGroup_FLEXIO_I2S, 0), 
 
  kStatus_FLEXIO_I2S_TxBusy = MAKE_STATUS(kStatusGroup_FLEXIO_I2S, 1), 
 
  kStatus_FLEXIO_I2S_RxBusy = MAKE_STATUS(kStatusGroup_FLEXIO_I2S, 2), 
 
  kStatus_FLEXIO_I2S_Error = MAKE_STATUS(kStatusGroup_FLEXIO_I2S, 3), 
 
  kStatus_FLEXIO_I2S_QueueFull = MAKE_STATUS(kStatusGroup_FLEXIO_I2S, 4), 
 
  kStatus_FLEXIO_I2S_Timeout
 
 } | 
|   | FlexIO I2S transfer status.  More...
  | 
|   | 
| enum   | _flexio_i2s_master_slave {  
  kFLEXIO_I2S_Master = 0x0U, 
 
  kFLEXIO_I2S_Slave = 0x1U
 
 } | 
|   | Master or slave mode.  More...
  | 
|   | 
| enum   | {  
  kFLEXIO_I2S_TxDataRegEmptyInterruptEnable = 0x1U, 
 
  kFLEXIO_I2S_RxDataRegFullInterruptEnable = 0x2U
 
 } | 
|   | _flexio_i2s_interrupt_enable Define FlexIO FlexIO I2S interrupt mask.  More...
  | 
|   | 
| enum   | {  
  kFLEXIO_I2S_TxDataRegEmptyFlag = 0x1U, 
 
  kFLEXIO_I2S_RxDataRegFullFlag = 0x2U
 
 } | 
|   | _flexio_i2s_status_flags Define FlexIO FlexIO I2S status mask.  More...
  | 
|   | 
| enum   | _flexio_i2s_sample_rate {  
  kFLEXIO_I2S_SampleRate8KHz = 8000U, 
 
  kFLEXIO_I2S_SampleRate11025Hz = 11025U, 
 
  kFLEXIO_I2S_SampleRate12KHz = 12000U, 
 
  kFLEXIO_I2S_SampleRate16KHz = 16000U, 
 
  kFLEXIO_I2S_SampleRate22050Hz = 22050U, 
 
  kFLEXIO_I2S_SampleRate24KHz = 24000U, 
 
  kFLEXIO_I2S_SampleRate32KHz = 32000U, 
 
  kFLEXIO_I2S_SampleRate44100Hz = 44100U, 
 
  kFLEXIO_I2S_SampleRate48KHz = 48000U, 
 
  kFLEXIO_I2S_SampleRate96KHz = 96000U
 
 } | 
|   | Audio sample rate.  More...
  | 
|   | 
| enum   | _flexio_i2s_word_width {  
  kFLEXIO_I2S_WordWidth8bits = 8U, 
 
  kFLEXIO_I2S_WordWidth16bits = 16U, 
 
  kFLEXIO_I2S_WordWidth24bits = 24U, 
 
  kFLEXIO_I2S_WordWidth32bits = 32U
 
 } | 
|   | Audio word width.  More...
  | 
|   | 
 | 
| void  | FLEXIO_I2S_MasterSetFormat (FLEXIO_I2S_Type *base, flexio_i2s_format_t *format, uint32_t srcClock_Hz) | 
|   | Configures the FlexIO I2S audio format in master mode.  More...
  | 
|   | 
| void  | FLEXIO_I2S_SlaveSetFormat (FLEXIO_I2S_Type *base, flexio_i2s_format_t *format) | 
|   | Configures the FlexIO I2S audio format in slave mode.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_WriteBlocking (FLEXIO_I2S_Type *base, uint8_t bitWidth, uint8_t *txData, size_t size) | 
|   | Sends data using a blocking method.  More...
  | 
|   | 
| static void  | FLEXIO_I2S_WriteData (FLEXIO_I2S_Type *base, uint8_t bitWidth, uint32_t data) | 
|   | Writes data into a data register.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_ReadBlocking (FLEXIO_I2S_Type *base, uint8_t bitWidth, uint8_t *rxData, size_t size) | 
|   | Receives a piece of data using a blocking method.  More...
  | 
|   | 
| static uint32_t  | FLEXIO_I2S_ReadData (FLEXIO_I2S_Type *base) | 
|   | Reads a data from the data register.  More...
  | 
|   | 
 | 
| void  | FLEXIO_I2S_TransferTxCreateHandle (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, flexio_i2s_callback_t callback, void *userData) | 
|   | Initializes the FlexIO I2S handle.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferSetFormat (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, flexio_i2s_format_t *format, uint32_t srcClock_Hz) | 
|   | Configures the FlexIO I2S audio format.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferRxCreateHandle (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, flexio_i2s_callback_t callback, void *userData) | 
|   | Initializes the FlexIO I2S receive handle.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_TransferSendNonBlocking (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, flexio_i2s_transfer_t *xfer) | 
|   | Performs an interrupt non-blocking send transfer on FlexIO I2S.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_TransferReceiveNonBlocking (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, flexio_i2s_transfer_t *xfer) | 
|   | Performs an interrupt non-blocking receive transfer on FlexIO I2S.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferAbortSend (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle) | 
|   | Aborts the current send.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferAbortReceive (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle) | 
|   | Aborts the current receive.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_TransferGetSendCount (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, size_t *count) | 
|   | Gets the remaining bytes to be sent.  More...
  | 
|   | 
| status_t  | FLEXIO_I2S_TransferGetReceiveCount (FLEXIO_I2S_Type *base, flexio_i2s_handle_t *handle, size_t *count) | 
|   | Gets the remaining bytes to be received.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferTxHandleIRQ (void *i2sBase, void *i2sHandle) | 
|   | Tx interrupt handler.  More...
  | 
|   | 
| void  | FLEXIO_I2S_TransferRxHandleIRQ (void *i2sBase, void *i2sHandle) | 
|   | Rx interrupt handler.  More...
  | 
|   | 
      
        
          | struct _flexio_i2s_config | 
        
      
 
 
      
        
          | struct _flexio_i2s_format | 
        
      
 
Data Fields | 
| 
uint8_t  | bitWidth | 
|   | Bit width of audio data, always 8/16/24/32 bits. 
  | 
|   | 
| 
uint32_t  | sampleRate_Hz | 
|   | Sample rate of the audio data. 
  | 
|   | 
 
 
      
        
          | struct _flexio_i2s_transfer | 
        
      
 
Data Fields | 
| 
uint8_t *  | data | 
|   | Data buffer start pointer. 
  | 
|   | 
| size_t  | dataSize | 
|   | Bytes to be transferred.  More...
  | 
|   | 
      
        
          | size_t _flexio_i2s_transfer::dataSize | 
        
      
 
 
 
 
      
        
          | struct _flexio_i2s_handle | 
        
      
 
 
      
        
          | #define FSL_FLEXIO_I2S_DRIVER_VERSION   (MAKE_VERSION(2, 2, 0)) | 
        
      
 
 
      
        
          | #define I2S_RETRY_TIMES   0U /* Define to zero means keep waiting until the flag is assert/deassert. */ | 
        
      
 
 
      
        
          | #define FLEXIO_I2S_XFER_QUEUE_SIZE   (4U) | 
        
      
 
 
| Enumerator | 
|---|
| kStatus_FLEXIO_I2S_Idle  | 
 FlexIO I2S is in idle state.  
 | 
| kStatus_FLEXIO_I2S_TxBusy  | 
 FlexIO I2S Tx is busy.  
 | 
| kStatus_FLEXIO_I2S_RxBusy  | 
 FlexIO I2S Tx is busy.  
 | 
| kStatus_FLEXIO_I2S_Error  | 
 FlexIO I2S error occurred.  
 | 
| kStatus_FLEXIO_I2S_QueueFull  | 
 FlexIO I2S transfer queue is full.  
 | 
| kStatus_FLEXIO_I2S_Timeout  | 
 FlexIO I2S timeout polling status flags.  
 | 
 
 
| Enumerator | 
|---|
| kFLEXIO_I2S_Master  | 
 Master mode.  
 | 
| kFLEXIO_I2S_Slave  | 
 Slave mode.  
 | 
 
 
| Enumerator | 
|---|
| kFLEXIO_I2S_TxDataRegEmptyInterruptEnable  | 
 Transmit buffer empty interrupt enable.  
 | 
| kFLEXIO_I2S_RxDataRegFullInterruptEnable  | 
 Receive buffer full interrupt enable.  
 | 
 
 
| Enumerator | 
|---|
| kFLEXIO_I2S_TxDataRegEmptyFlag  | 
 Transmit buffer empty flag.  
 | 
| kFLEXIO_I2S_RxDataRegFullFlag  | 
 Receive buffer full flag.  
 | 
 
 
| Enumerator | 
|---|
| kFLEXIO_I2S_SampleRate8KHz  | 
 Sample rate 8000Hz.  
 | 
| kFLEXIO_I2S_SampleRate11025Hz  | 
 Sample rate 11025Hz.  
 | 
| kFLEXIO_I2S_SampleRate12KHz  | 
 Sample rate 12000Hz.  
 | 
| kFLEXIO_I2S_SampleRate16KHz  | 
 Sample rate 16000Hz.  
 | 
| kFLEXIO_I2S_SampleRate22050Hz  | 
 Sample rate 22050Hz.  
 | 
| kFLEXIO_I2S_SampleRate24KHz  | 
 Sample rate 24000Hz.  
 | 
| kFLEXIO_I2S_SampleRate32KHz  | 
 Sample rate 32000Hz.  
 | 
| kFLEXIO_I2S_SampleRate44100Hz  | 
 Sample rate 44100Hz.  
 | 
| kFLEXIO_I2S_SampleRate48KHz  | 
 Sample rate 48000Hz.  
 | 
| kFLEXIO_I2S_SampleRate96KHz  | 
 Sample rate 96000Hz.  
 | 
 
 
| Enumerator | 
|---|
| kFLEXIO_I2S_WordWidth8bits  | 
 Audio data width 8 bits.  
 | 
| kFLEXIO_I2S_WordWidth16bits  | 
 Audio data width 16 bits.  
 | 
| kFLEXIO_I2S_WordWidth24bits  | 
 Audio data width 24 bits.  
 | 
| kFLEXIO_I2S_WordWidth32bits  | 
 Audio data width 32 bits.  
 | 
 
 
This API configures FlexIO pins and shifter to I2S and configures the FlexIO I2S with a configuration structure. The configuration structure can be filled by the user, or be set with default values by FLEXIO_I2S_GetDefaultConfig().
- Note
 - This API should be called at the beginning of the application to use the FlexIO I2S driver. Otherwise, any access to the FlexIO I2S module can cause hard fault because the clock is not enabled.
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
    | config | FlexIO I2S configure structure.  | 
  
   
 
 
The purpose of this API is to get the configuration structure initialized for use in FLEXIO_I2S_Init(). Users may use the initialized structure unchanged in FLEXIO_I2S_Init() or modify some fields of the structure before calling FLEXIO_I2S_Init().
- Parameters
 - 
  
    | config | pointer to master configuration structure  | 
  
   
 
 
Calling this API resets the FlexIO I2S shifter and timer config. After calling this API, call the FLEXO_I2S_Init to use the FlexIO I2S module.
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
  
   
 
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type  | 
    | enable | True to enable, false dose not have any effect.  | 
  
   
 
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
  
   
- Returns
 - Status flag, which are ORed by the enumerators in the _flexio_i2s_status_flags. 
 
 
 
This function enables the FlexIO UART interrupt.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
    | mask | interrupt source  | 
  
   
 
 
      
        
          | void FLEXIO_I2S_DisableInterrupts  | 
          ( | 
          FLEXIO_I2S_Type *  | 
          base,  | 
        
        
           | 
           | 
          uint32_t  | 
          mask  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function enables the FlexIO UART interrupt.
- Parameters
 - 
  
    | base | pointer to FLEXIO_I2S_Type structure  | 
    | mask | interrupt source  | 
  
   
 
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
    | enable | True means enable DMA, false means disable DMA.  | 
  
   
 
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
    | enable | True means enable DMA, false means disable DMA.  | 
  
   
 
 
  
  
      
        
          | static uint32_t FLEXIO_I2S_TxGetDataRegisterAddress  | 
          ( | 
          FLEXIO_I2S_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
This function returns the I2S data register address, mainly used by DMA/eDMA.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
  
   
- Returns
 - FlexIO i2s send data register address. 
 
 
 
  
  
      
        
          | static uint32_t FLEXIO_I2S_RxGetDataRegisterAddress  | 
          ( | 
          FLEXIO_I2S_Type *  | 
          base | ) | 
           | 
         
       
   | 
  
inlinestatic   | 
  
 
This function returns the I2S data register address, mainly used by DMA/eDMA.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
  
   
- Returns
 - FlexIO i2s receive data register address. 
 
 
 
Audio format can be changed in run-time of FlexIO I2S. This function configures the sample rate and audio data format to be transferred.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
    | format | Pointer to FlexIO I2S audio data format structure.  | 
    | srcClock_Hz | I2S master clock source frequency in Hz.  | 
  
   
 
 
Audio format can be changed in run-time of FlexIO I2S. This function configures the sample rate and audio data format to be transferred.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
    | format | Pointer to FlexIO I2S audio data format structure.  | 
  
   
 
 
- Note
 - This function blocks via polling until data is ready to be sent.
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer.  | 
    | bitWidth | How many bits in a audio word, usually 8/16/24/32 bits.  | 
    | txData | Pointer to the data to be written.  | 
    | size | Bytes to be written.  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Successfully write data.  | 
    | kStatus_FLEXIO_I2C_Timeout | Timeout polling status flags.  | 
  
   
 
 
  
  
      
        
          | static void FLEXIO_I2S_WriteData  | 
          ( | 
          FLEXIO_I2S_Type *  | 
          base,  | 
         
        
           | 
           | 
          uint8_t  | 
          bitWidth,  | 
         
        
           | 
           | 
          uint32_t  | 
          data  | 
         
        
           | 
          ) | 
           |  | 
         
       
   | 
  
inlinestatic   | 
  
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer.  | 
    | bitWidth | How many bits in a audio word, usually 8/16/24/32 bits.  | 
    | data | Data to be written.  | 
  
   
 
 
- Note
 - This function blocks via polling until data is ready to be sent.
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
    | bitWidth | How many bits in a audio word, usually 8/16/24/32 bits.  | 
    | rxData | Pointer to the data to be read.  | 
    | size | Bytes to be read.  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Successfully read data.  | 
    | kStatus_FLEXIO_I2C_Timeout | Timeout polling status flags.  | 
  
   
 
 
- Parameters
 - 
  
    | base | FlexIO I2S base pointer  | 
  
   
- Returns
 - Data read from data register. 
 
 
 
This function initializes the FlexIO I2S handle which can be used for other FlexIO I2S transactional APIs. Call this API once to get the initialized handle.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure  | 
    | handle | Pointer to flexio_i2s_handle_t structure to store the transfer state.  | 
    | callback | FlexIO I2S callback function, which is called while finished a block.  | 
    | userData | User parameter for the FlexIO I2S callback.  | 
  
   
 
 
Audio format can be changed at run-time of FlexIO I2S. This function configures the sample rate and audio data format to be transferred.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | FlexIO I2S handle pointer.  | 
    | format | Pointer to audio data format structure.  | 
    | srcClock_Hz | FlexIO I2S bit clock source frequency in Hz. This parameter should be 0 while in slave mode.  | 
  
   
 
 
This function initializes the FlexIO I2S handle which can be used for other FlexIO I2S transactional APIs. Call this API once to get the initialized handle.
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure to store the transfer state.  | 
    | callback | FlexIO I2S callback function, which is called while finished a block.  | 
    | userData | User parameter for the FlexIO I2S callback.  | 
  
   
 
 
- Note
 - The API returns immediately after transfer initiates. Call FLEXIO_I2S_GetRemainingBytes to poll the transfer status and check whether the transfer is finished. If the return status is 0, the transfer is finished.
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
    | xfer | Pointer to flexio_i2s_transfer_t structure  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Successfully start the data transmission.  | 
    | kStatus_FLEXIO_I2S_TxBusy | Previous transmission still not finished, data not all written to TX register yet.  | 
    | kStatus_InvalidArgument | The input parameter is invalid.  | 
  
   
 
 
- Note
 - The API returns immediately after transfer initiates. Call FLEXIO_I2S_GetRemainingBytes to poll the transfer status to check whether the transfer is finished. If the return status is 0, the transfer is finished.
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
    | xfer | Pointer to flexio_i2s_transfer_t structure  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Successfully start the data receive.  | 
    | kStatus_FLEXIO_I2S_RxBusy | Previous receive still not finished.  | 
    | kStatus_InvalidArgument | The input parameter is invalid.  | 
  
   
 
 
- Note
 - This API can be called at any time when interrupt non-blocking transfer initiates to abort the transfer in a early time.
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
  
   
 
 
- Note
 - This API can be called at any time when interrupt non-blocking transfer initiates to abort the transfer in a early time.
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
  
   
 
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
    | count | Bytes sent.  | 
  
   
- Return values
 - 
  
    | kStatus_Success | Succeed get the transfer count.  | 
    | kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress.  | 
  
   
 
 
- Parameters
 - 
  
    | base | Pointer to FLEXIO_I2S_Type structure.  | 
    | handle | Pointer to flexio_i2s_handle_t structure which stores the transfer state  | 
    | count | Bytes recieved.  | 
  
   
- Returns
 - count Bytes received. 
 
- Return values
 - 
  
    | kStatus_Success | Succeed get the transfer count.  | 
    | kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress.  | 
  
   
 
 
      
        
          | void FLEXIO_I2S_TransferTxHandleIRQ  | 
          ( | 
          void *  | 
          i2sBase,  | 
        
        
           | 
           | 
          void *  | 
          i2sHandle  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | i2sBase | Pointer to FLEXIO_I2S_Type structure.  | 
    | i2sHandle | Pointer to flexio_i2s_handle_t structure  | 
  
   
 
 
      
        
          | void FLEXIO_I2S_TransferRxHandleIRQ  | 
          ( | 
          void *  | 
          i2sBase,  | 
        
        
           | 
           | 
          void *  | 
          i2sHandle  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
- Parameters
 - 
  
    | i2sBase | Pointer to FLEXIO_I2S_Type structure.  | 
    | i2sHandle | Pointer to flexio_i2s_handle_t structure.  |