![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| struct | sai_edma_handle | 
| SAI DMA transfer handle, users should not touch the content of the handle.  More... | |
Typedefs | |
| typedef void(* | sai_edma_callback_t )(I2S_Type *base, sai_edma_handle_t *handle, status_t status, void *userData) | 
| SAI eDMA transfer callback function for finish and error.  | |
| typedef enum _sai_edma_interleave | sai_edma_interleave_t | 
| sai interleave type  | |
Enumerations | |
| enum | _sai_edma_interleave {  kSAI_EDMAInterleavePerChannelSample, kSAI_EDMAInterleavePerChannelBlock }  | 
| sai interleave type  More... | |
Driver version | |
| #define | FSL_SAI_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 7, 1)) | 
| Version 2.7.1.  | |
eDMA Transactional | |
| void | SAI_TransferTxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *txDmaHandle) | 
| Initializes the SAI eDMA handle.  More... | |
| void | SAI_TransferRxCreateHandleEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_edma_callback_t callback, void *userData, edma_handle_t *rxDmaHandle) | 
| Initializes the SAI Rx eDMA handle.  More... | |
| void | SAI_TransferSetInterleaveType (sai_edma_handle_t *handle, sai_edma_interleave_t interleaveType) | 
| Initializes the SAI interleave type.  More... | |
| void | SAI_TransferTxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) | 
| Configures the SAI Tx.  More... | |
| void | SAI_TransferRxSetConfigEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transceiver_t *saiConfig) | 
| Configures the SAI Rx.  More... | |
| status_t | SAI_TransferSendEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI transfer using DMA.  More... | |
| status_t | SAI_TransferReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer) | 
| Performs a non-blocking SAI receive using eDMA.  More... | |
| status_t | SAI_TransferSendLoopEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer, uint32_t loopTransferCount) | 
| Performs a non-blocking SAI loop transfer using eDMA.  More... | |
| status_t | SAI_TransferReceiveLoopEDMA (I2S_Type *base, sai_edma_handle_t *handle, sai_transfer_t *xfer, uint32_t loopTransferCount) | 
| Performs a non-blocking SAI loop transfer using eDMA.  More... | |
| void | SAI_TransferTerminateSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Terminate all SAI send.  More... | |
| void | SAI_TransferTerminateReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Terminate all SAI receive.  More... | |
| void | SAI_TransferAbortSendEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Aborts a SAI transfer using eDMA.  More... | |
| void | SAI_TransferAbortReceiveEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Aborts a SAI receive using eDMA.  More... | |
| status_t | SAI_TransferGetSendCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) | 
| Gets byte count sent by SAI.  More... | |
| status_t | SAI_TransferGetReceiveCountEDMA (I2S_Type *base, sai_edma_handle_t *handle, size_t *count) | 
| Gets byte count received by SAI.  More... | |
| uint32_t | SAI_TransferGetValidTransferSlotsEDMA (I2S_Type *base, sai_edma_handle_t *handle) | 
| Gets valid transfer slot.  More... | |
| struct sai_edma_handle | 
Data Fields | |
| edma_handle_t * | dmaHandle | 
| DMA handler for SAI send.  | |
| uint8_t | nbytes | 
| eDMA minor byte transfer count initially configured.  More... | |
| uint8_t | bytesPerFrame | 
| Bytes in a frame.  | |
| uint8_t | channelMask | 
| Enabled channel mask value, reference _sai_channel_mask.  | |
| uint8_t | channelNums | 
| total enabled channel nums  | |
| uint8_t | channel | 
| Which data channel.  | |
| uint8_t | count | 
| The transfer data count in a DMA request.  | |
| uint32_t | state | 
| Internal state for SAI eDMA transfer.  | |
| sai_edma_callback_t | callback | 
| Callback for users while transfer finish or error occurs.  | |
| void * | userData | 
| User callback parameter.  | |
| uint8_t | tcd [(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] | 
| TCD pool for eDMA transfer.  More... | |
| sai_transfer_t | saiQueue [SAI_XFER_QUEUE_SIZE] | 
| Transfer queue storing queued transfer.  More... | |
| size_t | transferSize [SAI_XFER_QUEUE_SIZE] | 
| Data bytes need to transfer.  | |
| sai_edma_interleave_t | interleaveType | 
| Transfer interleave type.  | |
| volatile uint8_t | queueUser | 
| Index for user to queue transfer.  More... | |
| volatile uint8_t | queueDriver | 
| Index for driver to get the transfer data and size.  | |
| uint8_t sai_edma_handle::nbytes | 
| uint8_t sai_edma_handle::tcd[(SAI_XFER_QUEUE_SIZE+1U)*sizeof(edma_tcd_t)] | 
| sai_transfer_t sai_edma_handle::saiQueue[SAI_XFER_QUEUE_SIZE] | 
| volatile uint8_t sai_edma_handle::queueUser | 
| enum _sai_edma_interleave | 
| void SAI_TransferTxCreateHandleEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | txDmaHandle | ||
| ) | 
This function initializes the SAI master DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| txDmaHandle | eDMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferRxCreateHandleEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_edma_callback_t | callback, | ||
| void * | userData, | ||
| edma_handle_t * | rxDmaHandle | ||
| ) | 
This function initializes the SAI slave DMA handle, which can be used for other SAI master transactional APIs. Usually, for a specified SAI instance, call this API once to get the initialized handle.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| callback | Pointer to user callback function. | 
| userData | User parameter passed to the callback function. | 
| rxDmaHandle | eDMA handle pointer, this handle shall be static allocated by users. | 
| void SAI_TransferSetInterleaveType | ( | sai_edma_handle_t * | handle, | 
| sai_edma_interleave_t | interleaveType | ||
| ) | 
This function initializes the SAI DMA handle member interleaveType, it shall be called only when application would like to use type kSAI_EDMAInterleavePerChannelBlock, since the default interleaveType is kSAI_EDMAInterleavePerChannelSample always
| handle | SAI eDMA handle pointer. | 
| interleaveType | Multi channel interleave type. | 
| void SAI_TransferTxSetConfigEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| saiConfig | sai configurations. | 
| void SAI_TransferRxSetConfigEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transceiver_t * | saiConfig | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| saiConfig | sai configurations. | 
| status_t SAI_TransferSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
This function support multi channel transfer,
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to the DMA transfer structure. | 
| kStatus_Success | Start a SAI eDMA send successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_TxBusy | SAI is busy sending data. | 
| status_t SAI_TransferReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer | ||
| ) | 
This function support multi channel transfer,
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to DMA transfer structure. | 
| kStatus_Success | Start a SAI eDMA receive successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| kStatus_RxBusy | SAI is busy receiving data. | 
| status_t SAI_TransferSendLoopEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer, | ||
| uint32_t | loopTransferCount | ||
| ) | 
Once the loop transfer start, application can use function SAI_TransferAbortSendEDMA to stop the loop transfer.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to the DMA transfer structure, should be a array with elements counts >=1(loopTransferCount). | 
| loopTransferCount | the counts of xfer array. | 
| kStatus_Success | Start a SAI eDMA send successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| status_t SAI_TransferReceiveLoopEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| sai_transfer_t * | xfer, | ||
| uint32_t | loopTransferCount | ||
| ) | 
Once the loop transfer start, application can use function SAI_TransferAbortReceiveEDMA to stop the loop transfer.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| xfer | Pointer to the DMA transfer structure, should be a array with elements counts >=1(loopTransferCount). | 
| loopTransferCount | the counts of xfer array. | 
| kStatus_Success | Start a SAI eDMA receive successfully. | 
| kStatus_InvalidArgument | The input argument is invalid. | 
| void SAI_TransferTerminateSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortSendEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferTerminateReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortReceiveEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferAbortSendEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateSendEDMA.
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| void SAI_TransferAbortReceiveEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function only aborts the current transfer slots, the other transfer slots' information still kept in the handler. If users want to terminate all transfer slots, just call SAI_TransferTerminateReceiveEDMA.
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| status_t SAI_TransferGetSendCountEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer. | 
| handle | SAI eDMA handle pointer. | 
| count | Bytes count sent by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. | 
| status_t SAI_TransferGetReceiveCountEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle, | ||
| size_t * | count | ||
| ) | 
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| count | Bytes count received by SAI. | 
| kStatus_Success | Succeed get the transfer count. | 
| kStatus_NoTransferInProgress | There is no non-blocking transaction in progress. | 
| uint32_t SAI_TransferGetValidTransferSlotsEDMA | ( | I2S_Type * | base, | 
| sai_edma_handle_t * | handle | ||
| ) | 
This function can be used to query the valid transfer request slot that the application can submit. It should be called in the critical section, that means the application could call it in the corresponding callback function or disable IRQ before calling it in the application, otherwise, the returned value may not correct.
| base | SAI base pointer | 
| handle | SAI eDMA handle pointer. | 
| valid | slot count that application submit. |