![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The I2C_EDMA module provide a method for I2C transfer operation based on EDMA.
Data Structures | |
| struct | _i2c_master_edma_transfer_handle |
| I2C master eDMA transfer structure. More... | |
Typedefs | |
| typedef struct _i2c_master_edma_transfer_handle | i2c_master_edma_transfer_handle_t |
| Retry times for waiting flag. More... | |
| typedef void(* | i2c_master_edma_transfer_callback_t )(i2c_master_edma_transfer_handle_t *handle) |
| I2C master eDMA transfer callback typedef. More... | |
Driver version | |
| #define | FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| I2C EDMA driver version. More... | |
I2C Block eDMA Transfer Operation | |
| void | I2C_MasterCreateEDMAHandle (I2C_Type *base, i2c_master_edma_transfer_handle_t *psHandle, i2c_master_edma_transfer_callback_t pfCallback, void *pUserData, DMA_Type *edmaBase, edma_channel_t eEdmaChannel) |
| Initializes the I2C handle which is used in transactional functions. More... | |
| status_t | I2C_MasterTransferEDMA (i2c_master_edma_transfer_handle_t *psHandle, i2c_master_transfer_t *psTransfer) |
| Performs a master eDMA non-blocking transfer on the I2C bus. More... | |
| status_t | I2C_MasterTransferGetCountEDMA (i2c_master_edma_transfer_handle_t *psHandle, uint16_t *pu16Count) |
| Gets a master transfer status during the eDMA non-blocking transfer. More... | |
| void | I2C_MasterTransferAbortEDMA (i2c_master_edma_transfer_handle_t *psHandle) |
| Aborts a master eDMA non-blocking transfer early. More... | |
| struct _i2c_master_edma_transfer_handle |
This struct address should be sizeof(edma_channel_tcd_t) aligned.
Data Fields | |
| edma_channel_tcd_t | sTcd |
| TCD for EDMA transfer. More... | |
| I2C_Type * | base |
| I2C base pointer to the I2C instance that assigned to this handle. More... | |
| i2c_master_transfer_t | sTransfer |
| I2C master transfer structure. More... | |
| uint16_t | u16TransferSize |
| Total bytes to be transferred. More... | |
| uint8_t | u8State |
| I2C master transfer status. More... | |
| edma_handle_t | sEdmaHandle |
| The eDMA handler used. More... | |
| status_t | completionStatus |
| I2C master transfer complete status, indicating how the transfer ends. More... | |
| i2c_master_edma_transfer_callback_t | pfCallback |
| A callback function called after the eDMA transfer is finished. More... | |
| void * | pUserData |
User configurable pointer to any data, function, structure etc that user wish to use in the callback | |
| edma_channel_tcd_t _i2c_master_edma_transfer_handle::sTcd |
| I2C_Type* _i2c_master_edma_transfer_handle::base |
| i2c_master_transfer_t _i2c_master_edma_transfer_handle::sTransfer |
| uint16_t _i2c_master_edma_transfer_handle::u16TransferSize |
| uint8_t _i2c_master_edma_transfer_handle::u8State |
| edma_handle_t _i2c_master_edma_transfer_handle::sEdmaHandle |
| status_t _i2c_master_edma_transfer_handle::completionStatus |
| i2c_master_edma_transfer_callback_t _i2c_master_edma_transfer_handle::pfCallback |
| #define FSL_I2C_EDMA_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
I2C master eDMA handle typedef.
| typedef void(* i2c_master_edma_transfer_callback_t)(i2c_master_edma_transfer_handle_t *handle) |
| void I2C_MasterCreateEDMAHandle | ( | I2C_Type * | base, |
| i2c_master_edma_transfer_handle_t * | psHandle, | ||
| i2c_master_edma_transfer_callback_t | pfCallback, | ||
| void * | pUserData, | ||
| DMA_Type * | edmaBase, | ||
| edma_channel_t | eEdmaChannel | ||
| ) |
| base | I2C peripheral base address. |
| psHandle | A pointer to the i2c_master_edma_transfer_handle_t structure. |
| pfCallback | A pointer to the user callback function. |
| pUserData | A user parameter passed to the callback function. |
| edmaBase | Edma base address. |
| eEdmaChannel | eDMA channel for master transfer. |
| status_t I2C_MasterTransferEDMA | ( | i2c_master_edma_transfer_handle_t * | psHandle, |
| i2c_master_transfer_t * | psTransfer | ||
| ) |
| psHandle | A pointer to the i2c_master_edma_transfer_handle_t structure. |
| psTransfer | A pointer to the transfer structure of i2c_master_transfer_t. |
| kStatus_Success | Successfully completed the data transmission. |
| kStatus_I2C_Busy | A previous transmission is still not finished. |
| kStatus_I2C_Timeout | Transfer error, waits for a signal timeout. |
| kStatus_I2C_ArbitrationLost | Transfer error, arbitration lost. |
| kStataus_I2C_Nak | Transfer error, receive NAK during transfer. |
| status_t I2C_MasterTransferGetCountEDMA | ( | i2c_master_edma_transfer_handle_t * | psHandle, |
| uint16_t * | pu16Count | ||
| ) |
| psHandle | A pointer to the i2c_master_edma_transfer_handle_t structure. |
| pu16Count | A number of bytes transferred by the non-blocking transaction. |
| void I2C_MasterTransferAbortEDMA | ( | i2c_master_edma_transfer_handle_t * | psHandle | ) |
| psHandle | A pointer to the i2c_master_edma_transfer_handle_t structure. |