The MCUXpresso SDK provides a peripheral driver for the General Power Controller (GPC) module of MCUXpresso SDK devices.
API functions are provided to configure the system about working in dedicated power mode. There are mainly about enabling the power for memory, enabling the wakeup sources for STOP modes, and power up/down operations for various peripherals.
|
|
typedef struct _gpc_lpm_config | gpc_lpm_config_t |
| | configuration for enter DSM mode
|
| |
|
| enum | _gpc_lpm_mode {
kGPC_RunMode = 0U,
kGPC_WaitMode = 1U,
kGPC_StopMode = 2U
} |
| | GPC LPM mode definition. More...
|
| |
| enum | _gpc_pgc_ack_sel {
kGPC_DummyPGCPowerUpAck = GPC_PGC_ACK_SEL_DUMMY_PGC_PUP_ACK_MASK,
kGPC_VirtualPGCPowerUpAck = GPC_PGC_ACK_SEL_VIRTUAL_PGC_PUP_ACK_MASK,
kGPC_DummyPGCPowerDownAck = GPC_PGC_ACK_SEL_DUMMY_PGC_PDN_ACK_MASK,
kGPC_VirtualPGCPowerDownAck = GPC_PGC_ACK_SEL_VIRTUAL_PGC_PDN_ACK_MASK,
kGPC_NocPGCPowerUpAck = GPC_PGC_ACK_SEL_NOC_PGC_PUP_ACK,
kGPC_NocPGCPowerDownAck = GPC_PGC_ACK_SEL_NOC_PGC_PDN_ACK
} |
| | PGC ack signal selection. More...
|
| |
| enum | _gpc_standby_count {
kGPC_StandbyCounter4CkilClk = 0U,
kGPC_StandbyCounter8CkilClk = 1U,
kGPC_StandbyCounter16CkilClk = 2U,
kGPC_StandbyCounter32CkilClk = 3U,
kGPC_StandbyCounter64CkilClk = 4U,
kGPC_StandbyCounter128CkilClk = 5U,
kGPC_StandbyCounter256CkilClk = 6U,
kGPC_StandbyCounter512CkilClk = 7U
} |
| | Standby counter which GPC will wait between PMIC_STBY_REQ negation and assertion of PMIC_READY. More...
|
| |
|
| static void | GPC_AllowIRQs (GPC_Type *base) |
| | Allow all the IRQ/Events within the charge of GPC. More...
|
| |
| static void | GPC_DisallowIRQs (GPC_Type *base) |
| | Disallow all the IRQ/Events within the charge of GPC. More...
|
| |
| static uint32_t | GPC_GetLpmMode (GPC_Type *base) |
| | Get current LPM mode. More...
|
| |
| void | GPC_EnableIRQ (GPC_Type *base, uint32_t irqId) |
| | Enable the IRQ. More...
|
| |
| void | GPC_DisableIRQ (GPC_Type *base, uint32_t irqId) |
| | Disable the IRQ. More...
|
| |
| bool | GPC_GetIRQStatusFlag (GPC_Type *base, uint32_t irqId) |
| | Get the IRQ/Event flag. More...
|
| |
| static void | GPC_DsmTriggerMask (GPC_Type *base, bool enable) |
| | Mask the DSM trigger. More...
|
| |
| static void | GPC_WFIMask (GPC_Type *base, bool enable) |
| | Mask the WFI. More...
|
| |
| static void | GPC_SelectPGCAckSignal (GPC_Type *base, uint32_t mask) |
| | Select the PGC ACK signal. More...
|
| |
| static void | GPC_PowerDownRequestMask (GPC_Type *base, bool enable) |
| | Power down request to virtual PGC mask or not. More...
|
| |
| static void | GPC_PGCMapping (GPC_Type *base, uint32_t mask) |
| | PGC CPU Mapping. More...
|
| |
| static void | GPC_TimeSlotConfigureForPUS (GPC_Type *base, uint8_t slotIndex, uint32_t value) |
| | Time slot configure. More...
|
| |
| void | GPC_EnterWaitMode (GPC_Type *base, gpc_lpm_config_t *config) |
| | Enter WAIT mode. More...
|
| |
| void | GPC_EnterStopMode (GPC_Type *base, gpc_lpm_config_t *config) |
| | Enter STOP mode. More...
|
| |
| void | GPC_Init (GPC_Type *base, uint32_t powerUpSlot, uint32_t powerDownSlot) |
| | GPC init function. More...
|
| |
| Enumerator |
|---|
| kGPC_RunMode |
run mode
|
| kGPC_WaitMode |
wait mode
|
| kGPC_StopMode |
stop mode
|
| Enumerator |
|---|
| kGPC_DummyPGCPowerUpAck |
dummy power up ack signal
|
| kGPC_VirtualPGCPowerUpAck |
virtual pgc power up ack signal
|
| kGPC_DummyPGCPowerDownAck |
dummy power down ack signal
|
| kGPC_VirtualPGCPowerDownAck |
virtual pgc power down ack signal
|
| kGPC_NocPGCPowerUpAck |
NOC power up ack signal.
|
| kGPC_NocPGCPowerDownAck |
NOC power.
|
| Enumerator |
|---|
| kGPC_StandbyCounter4CkilClk |
4 ckil clocks
|
| kGPC_StandbyCounter8CkilClk |
8 ckil clocks
|
| kGPC_StandbyCounter16CkilClk |
16 ckil clocks
|
| kGPC_StandbyCounter32CkilClk |
32 ckil clocks
|
| kGPC_StandbyCounter64CkilClk |
64 ckil clocks
|
| kGPC_StandbyCounter128CkilClk |
128 ckil clocks
|
| kGPC_StandbyCounter256CkilClk |
256 ckil clocks
|
| kGPC_StandbyCounter512CkilClk |
512 ckil clocks
|
| static void GPC_AllowIRQs |
( |
GPC_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| static void GPC_DisallowIRQs |
( |
GPC_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| static uint32_t GPC_GetLpmMode |
( |
GPC_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
- Return values
-
| lpm | mode, reference _gpc_lpm_mode |
| void GPC_EnableIRQ |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be enabled, available range is 0-127,reference SOC headerfile IRQn_Type. |
| void GPC_DisableIRQ |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be disabled, available range is 0-127,reference SOC headerfile IRQn_Type. |
| bool GPC_GetIRQStatusFlag |
( |
GPC_Type * |
base, |
|
|
uint32_t |
irqId |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| irqId | ID number of IRQ to be enabled, available range is 0-127,reference SOC headerfile IRQn_Type. |
- Returns
- Indicated IRQ/Event is asserted or not.
| static void GPC_DsmTriggerMask |
( |
GPC_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| enable | true to enable mask, false to disable mask. |
| static void GPC_WFIMask |
( |
GPC_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| enable | true to enable mask, false to disable mask. |
| static void GPC_SelectPGCAckSignal |
( |
GPC_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| mask | reference _gpc_pgc_ack_sel. |
| static void GPC_PowerDownRequestMask |
( |
GPC_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| enable | true to mask, false to not mask. |
| static void GPC_PGCMapping |
( |
GPC_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| mask | mask value reference PGC CPU mapping definition. |
| static void GPC_TimeSlotConfigureForPUS |
( |
GPC_Type * |
base, |
|
|
uint8_t |
slotIndex, |
|
|
uint32_t |
value |
|
) |
| |
|
inlinestatic |
- Parameters
-
| base | GPC peripheral base address. |
| slotIndex | time slot index. |
| value | value to be configured |
- Parameters
-
| base | GPC peripheral base address. |
| config | lpm mode configurations. |
- Parameters
-
| base | GPC peripheral base address. |
| config | lpm mode configurations. |
| void GPC_Init |
( |
GPC_Type * |
base, |
|
|
uint32_t |
powerUpSlot, |
|
|
uint32_t |
powerDownSlot |
|
) |
| |
- Parameters
-
| base | GPC peripheral base address. |
| powerUpSlot | power up slot number. |
| powerDownSlot | power down slot number. |