The MCUXpresso SDK provides a driver for the SEMA4 module of MCUXpresso SDK devices.
|
| void | SEMA4_Init (SEMA4_Type *base) |
| | Initializes the SEMA4 module. More...
|
| |
| void | SEMA4_Deinit (SEMA4_Type *base) |
| | De-initializes the SEMA4 module. More...
|
| |
| status_t | SEMA4_TryLock (SEMA4_Type *base, uint8_t gateNum, uint8_t procNum) |
| | Tries to lock the SEMA4 gate. More...
|
| |
| void | SEMA4_Lock (SEMA4_Type *base, uint8_t gateNum, uint8_t procNum) |
| | Locks the SEMA4 gate. More...
|
| |
| static void | SEMA4_Unlock (SEMA4_Type *base, uint8_t gateNum) |
| | Unlocks the SEMA4 gate. More...
|
| |
| static int32_t | SEMA4_GetLockProc (SEMA4_Type *base, uint8_t gateNum) |
| | Gets the status of the SEMA4 gate. More...
|
| |
| status_t | SEMA4_ResetGate (SEMA4_Type *base, uint8_t gateNum) |
| | Resets the SEMA4 gate to an unlocked status. More...
|
| |
| static status_t | SEMA4_ResetAllGates (SEMA4_Type *base) |
| | Resets all SEMA4 gates to an unlocked status. More...
|
| |
| static void | SEMA4_EnableGateNotifyInterrupt (SEMA4_Type *base, uint8_t procNum, uint32_t mask) |
| | Enable the gate notification interrupt. More...
|
| |
| static void | SEMA4_DisableGateNotifyInterrupt (SEMA4_Type *base, uint8_t procNum, uint32_t mask) |
| | Disable the gate notification interrupt. More...
|
| |
| static uint32_t | SEMA4_GetGateNotifyStatus (SEMA4_Type *base, uint8_t procNum) |
| | Get the gate notification flags. More...
|
| |
| status_t | SEMA4_ResetGateNotify (SEMA4_Type *base, uint8_t gateNum) |
| | Resets the SEMA4 gate IRQ notification. More...
|
| |
| static status_t | SEMA4_ResetAllGateNotify (SEMA4_Type *base) |
| | Resets all SEMA4 gates IRQ notification. More...
|
| |
| #define SEMA4_GATE_NUM_RESET_ALL (64U) |
| void SEMA4_Init |
( |
SEMA4_Type * |
base | ) |
|
This function initializes the SEMA4 module. It only enables the clock but does not reset the gates because the module might be used by other processors at the same time. To reset the gates, call either SEMA4_ResetGate or SEMA4_ResetAllGates function.
- Parameters
-
| base | SEMA4 peripheral base address. |
| void SEMA4_Deinit |
( |
SEMA4_Type * |
base | ) |
|
This function de-initializes the SEMA4 module. It only disables the clock.
- Parameters
-
| base | SEMA4 peripheral base address. |
| status_t SEMA4_TryLock |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum, |
|
|
uint8_t |
procNum |
|
) |
| |
This function tries to lock the specific SEMA4 gate. If the gate has been locked by another processor, this function returns an error code.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number to lock. |
| procNum | Current processor number. |
- Return values
-
| kStatus_Success | Lock the sema4 gate successfully. |
| kStatus_Fail | Sema4 gate has been locked by another processor. |
| void SEMA4_Lock |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum, |
|
|
uint8_t |
procNum |
|
) |
| |
This function locks the specific SEMA4 gate. If the gate has been locked by other processors, this function waits until it is unlocked and then lock it.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number to lock. |
| procNum | Current processor number. |
| static void SEMA4_Unlock |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum |
|
) |
| |
|
inlinestatic |
This function unlocks the specific SEMA4 gate. It only writes unlock value to the SEMA4 gate register. However, it does not check whether the SEMA4 gate is locked by the current processor or not. As a result, if the SEMA4 gate is not locked by the current processor, this function has no effect.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number to unlock. |
| static int32_t SEMA4_GetLockProc |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum |
|
) |
| |
|
inlinestatic |
This function checks the lock status of a specific SEMA4 gate.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number. |
- Returns
- Return -1 if the gate is unlocked, otherwise return the processor number which has locked the gate.
| status_t SEMA4_ResetGate |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum |
|
) |
| |
This function resets a SEMA4 gate to an unlocked status.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number. |
- Return values
-
| kStatus_Success | SEMA4 gate is reset successfully. |
| kStatus_Fail | Some other reset process is ongoing. |
| static status_t SEMA4_ResetAllGates |
( |
SEMA4_Type * |
base | ) |
|
|
inlinestatic |
This function resets all SEMA4 gate to an unlocked status.
- Parameters
-
| base | SEMA4 peripheral base address. |
- Return values
-
| kStatus_Success | SEMA4 is reset successfully. |
| kStatus_Fail | Some other reset process is ongoing. |
| static void SEMA4_EnableGateNotifyInterrupt |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
procNum, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
Gate notification provides such feature, when core tried to lock the gate and failed, it could get notification when the gate is idle.
- Parameters
-
| base | SEMA4 peripheral base address. |
| procNum | Current processor number. |
| mask | OR'ed value of the gate index, for example: (1<<0) | (1<<1) means gate 0 and gate 1. |
| static void SEMA4_DisableGateNotifyInterrupt |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
procNum, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
Gate notification provides such feature, when core tried to lock the gate and failed, it could get notification when the gate is idle.
- Parameters
-
| base | SEMA4 peripheral base address. |
| procNum | Current processor number. |
| mask | OR'ed value of the gate index, for example: (1<<0) | (1<<1) means gate 0 and gate 1. |
| static uint32_t SEMA4_GetGateNotifyStatus |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
procNum |
|
) |
| |
|
inlinestatic |
Gate notification provides such feature, when core tried to lock the gate and failed, it could get notification when the gate is idle. The status flags are cleared automatically when the gate is locked by current core or locked again before the other core.
- Parameters
-
| base | SEMA4 peripheral base address. |
| procNum | Current processor number. |
- Returns
- OR'ed value of the gate index, for example: (1<<0) | (1<<1) means gate 0 and gate 1 flags are pending.
| status_t SEMA4_ResetGateNotify |
( |
SEMA4_Type * |
base, |
|
|
uint8_t |
gateNum |
|
) |
| |
This function resets a SEMA4 gate IRQ notification.
- Parameters
-
| base | SEMA4 peripheral base address. |
| gateNum | Gate number. |
- Return values
-
| kStatus_Success | Reset successfully. |
| kStatus_Fail | Some other reset process is ongoing. |
| static status_t SEMA4_ResetAllGateNotify |
( |
SEMA4_Type * |
base | ) |
|
|
inlinestatic |
This function resets all SEMA4 gate IRQ notifications.
- Parameters
-
| base | SEMA4 peripheral base address. |
- Return values
-
| kStatus_Success | Reset successfully. |
| kStatus_Fail | Some other reset process is ongoing. |