MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
eLCDIF: Enhanced LCD Interface

Overview

The MCUXpresso SDK provides a peripheral driver for the Enhanced LCD Interface(eLCDIF)

The Enhanced LCD Interface supports MPU mode, VSYNC mode, RGB mode (or DOTCLK mode), and DVI mode. The current eLCDIF driver only supports RGB mode.

Typical use case

Frame buffer update

The function ELCDIF_SetNextBufferAddr sets the next frame to show to eLCDIF, the eLCDIF loads the new frame and sets the interrupt kELCDIF_CurFrameDone. If no new frame is set, the old one is displayed.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/elcdif

Alpha surface

The alpha surface can be enabled to add an extra overlay on the normal display buffer. In this example, the alpha surface is enabled, and the alpha value is updated after every frame loaded to eLCDIF.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/elcdif

Data Structures

struct  _elcdif_pixel_format_reg
 The register value when using different pixel format. More...
 
struct  _elcdif_rgb_mode_config
 eLCDIF configure structure for RGB mode (DOTCLK mode). More...
 
struct  _elcdif_as_buffer_config
 eLCDIF alpha surface buffer configuration. More...
 
struct  _elcdif_as_blend_config
 eLCDIF alpha surface blending configuration. More...
 

Typedefs

typedef enum _elcdif_pixel_format elcdif_pixel_format_t
 The pixel format. More...
 
typedef enum _elcdif_lcd_data_bus elcdif_lcd_data_bus_t
 The LCD data bus type. More...
 
typedef struct
_elcdif_pixel_format_reg 
elcdif_pixel_format_reg_t
 The register value when using different pixel format. More...
 
typedef struct
_elcdif_rgb_mode_config 
elcdif_rgb_mode_config_t
 eLCDIF configure structure for RGB mode (DOTCLK mode).
 
typedef enum
_elcdif_as_pixel_format 
elcdif_as_pixel_format_t
 eLCDIF alpha surface pixel format.
 
typedef struct
_elcdif_as_buffer_config 
elcdif_as_buffer_config_t
 eLCDIF alpha surface buffer configuration.
 
typedef enum _elcdif_alpha_mode elcdif_alpha_mode_t
 eLCDIF alpha mode during blending.
 
typedef enum _elcdif_rop_mode elcdif_rop_mode_t
 eLCDIF ROP mode during blending. More...
 
typedef struct
_elcdif_as_blend_config 
elcdif_as_blend_config_t
 eLCDIF alpha surface blending configuration.
 
typedef enum _elcdif_lut elcdif_lut_t
 eLCDIF LUT More...
 

Enumerations

enum  _elcdif_polarity_flags {
  kELCDIF_VsyncActiveLow = 0U,
  kELCDIF_HsyncActiveLow = 0U,
  kELCDIF_DataEnableActiveLow = 0U,
  kELCDIF_DriveDataOnFallingClkEdge = 0U,
  kELCDIF_VsyncActiveHigh = LCDIF_VDCTRL0_VSYNC_POL_MASK,
  kELCDIF_HsyncActiveHigh = LCDIF_VDCTRL0_HSYNC_POL_MASK,
  kELCDIF_DataEnableActiveHigh = LCDIF_VDCTRL0_ENABLE_POL_MASK,
  kELCDIF_DriveDataOnRisingClkEdge = LCDIF_VDCTRL0_DOTCLK_POL_MASK
}
 eLCDIF signal polarity flags More...
 
enum  _elcdif_interrupt_enable {
  kELCDIF_BusMasterErrorInterruptEnable = LCDIF_CTRL1_BM_ERROR_IRQ_EN_MASK,
  kELCDIF_TxFifoOverflowInterruptEnable = LCDIF_CTRL1_OVERFLOW_IRQ_EN_MASK,
  kELCDIF_TxFifoUnderflowInterruptEnable = LCDIF_CTRL1_UNDERFLOW_IRQ_EN_MASK,
  kELCDIF_CurFrameDoneInterruptEnable,
  kELCDIF_VsyncEdgeInterruptEnable
}
 The eLCDIF interrupts to enable. More...
 
enum  _elcdif_interrupt_flags {
  kELCDIF_BusMasterError = LCDIF_CTRL1_BM_ERROR_IRQ_MASK,
  kELCDIF_TxFifoOverflow = LCDIF_CTRL1_OVERFLOW_IRQ_MASK,
  kELCDIF_TxFifoUnderflow = LCDIF_CTRL1_UNDERFLOW_IRQ_MASK,
  kELCDIF_CurFrameDone,
  kELCDIF_VsyncEdge = LCDIF_CTRL1_VSYNC_EDGE_IRQ_MASK
}
 The eLCDIF interrupt status flags. More...
 
enum  _elcdif_status_flags {
  kELCDIF_LFifoFull = LCDIF_STAT_LFIFO_FULL_MASK,
  kELCDIF_LFifoEmpty = LCDIF_STAT_LFIFO_EMPTY_MASK,
  kELCDIF_TxFifoFull = LCDIF_STAT_TXFIFO_FULL_MASK,
  kELCDIF_TxFifoEmpty = LCDIF_STAT_TXFIFO_EMPTY_MASK
}
 eLCDIF status flags More...
 
enum  _elcdif_pixel_format {
  kELCDIF_PixelFormatRAW8 = 0,
  kELCDIF_PixelFormatRGB565 = 1,
  kELCDIF_PixelFormatRGB666 = 2,
  kELCDIF_PixelFormatXRGB8888 = 3,
  kELCDIF_PixelFormatRGB888 = 4
}
 The pixel format. More...
 
enum  _elcdif_lcd_data_bus {
  kELCDIF_DataBus8Bit = LCDIF_CTRL_LCD_DATABUS_WIDTH(1),
  kELCDIF_DataBus16Bit = LCDIF_CTRL_LCD_DATABUS_WIDTH(0),
  kELCDIF_DataBus18Bit = LCDIF_CTRL_LCD_DATABUS_WIDTH(2),
  kELCDIF_DataBus24Bit = LCDIF_CTRL_LCD_DATABUS_WIDTH(3)
}
 The LCD data bus type. More...
 
enum  _elcdif_as_pixel_format {
  kELCDIF_AsPixelFormatARGB8888 = 0x0,
  kELCDIF_AsPixelFormatRGB888 = 0x4,
  kELCDIF_AsPixelFormatARGB1555 = 0x8,
  kELCDIF_AsPixelFormatARGB4444 = 0x9,
  kELCDIF_AsPixelFormatRGB555 = 0xC,
  kELCDIF_AsPixelFormatRGB444 = 0xD,
  kELCDIF_AsPixelFormatRGB565 = 0xE
}
 eLCDIF alpha surface pixel format. More...
 
enum  _elcdif_alpha_mode {
  kELCDIF_AlphaEmbedded,
  kELCDIF_AlphaOverride,
  kELCDIF_AlphaMultiply,
  kELCDIF_AlphaRop
}
 eLCDIF alpha mode during blending. More...
 
enum  _elcdif_rop_mode {
  kELCDIF_RopMaskAs = 0x0,
  kELCDIF_RopMaskNotAs = 0x1,
  kELCDIF_RopMaskAsNot = 0x2,
  kELCDIF_RopMergeAs = 0x3,
  kELCDIF_RopMergeNotAs = 0x4,
  kELCDIF_RopMergeAsNot = 0x5,
  kELCDIF_RopNotCopyAs = 0x6,
  kELCDIF_RopNot = 0x7,
  kELCDIF_RopNotMaskAs = 0x8,
  kELCDIF_RopNotMergeAs = 0x9,
  kELCDIF_RopXorAs = 0xA,
  kELCDIF_RopNotXorAs = 0xB
}
 eLCDIF ROP mode during blending. More...
 
enum  _elcdif_lut {
  kELCDIF_Lut0 = 0,
  kELCDIF_Lut1
}
 eLCDIF LUT More...
 

Driver version

#define FSL_ELCDIF_DRIVER_VERSION   (MAKE_VERSION(2, 0, 7))
 eLCDIF driver version
 

eLCDIF initialization and de-initialization

void ELCDIF_RgbModeInit (LCDIF_Type *base, const elcdif_rgb_mode_config_t *config)
 Initializes the eLCDIF to work in RGB mode (DOTCLK mode). More...
 
void ELCDIF_RgbModeGetDefaultConfig (elcdif_rgb_mode_config_t *config)
 Gets the eLCDIF default configuration structure for RGB (DOTCLK) mode. More...
 
void ELCDIF_Deinit (LCDIF_Type *base)
 Deinitializes the eLCDIF peripheral. More...
 

Module operation

void ELCDIF_RgbModeSetPixelFormat (LCDIF_Type *base, elcdif_pixel_format_t pixelFormat)
 Set the pixel format in RGB (DOTCLK) mode. More...
 
static void ELCDIF_RgbModeStart (LCDIF_Type *base)
 Start to display in RGB (DOTCLK) mode. More...
 
void ELCDIF_RgbModeStop (LCDIF_Type *base)
 Stop display in RGB (DOTCLK) mode and wait until finished. More...
 
static void ELCDIF_SetNextBufferAddr (LCDIF_Type *base, uint32_t bufferAddr)
 Set the next frame buffer address to display. More...
 
void ELCDIF_Reset (LCDIF_Type *base)
 Reset the eLCDIF peripheral. More...
 

Status

static uint32_t ELCDIF_GetCrcValue (const LCDIF_Type *base)
 Get the CRC value of the frame sent out. More...
 
static uint32_t ELCDIF_GetBusMasterErrorAddr (const LCDIF_Type *base)
 Get the bus master error virtual address. More...
 
static uint32_t ELCDIF_GetStatus (const LCDIF_Type *base)
 Get the eLCDIF status. More...
 
static uint32_t ELCDIF_GetLFifoCount (const LCDIF_Type *base)
 Get current count in Latency buffer (LFIFO). More...
 

Interrupts

static void ELCDIF_EnableInterrupts (LCDIF_Type *base, uint32_t mask)
 Enables eLCDIF interrupt requests. More...
 
static void ELCDIF_DisableInterrupts (LCDIF_Type *base, uint32_t mask)
 Disables eLCDIF interrupt requests. More...
 
static uint32_t ELCDIF_GetInterruptStatus (const LCDIF_Type *base)
 Get eLCDIF interrupt peding status. More...
 
static void ELCDIF_ClearInterruptStatus (LCDIF_Type *base, uint32_t mask)
 Clear eLCDIF interrupt peding status. More...
 

LUT

The Lookup Table (LUT) is used to expand the 8 bits pixel to 24 bits pixel before output to external displayer.

There are two 256x24 bits LUT memory in LCDIF, the LSB of frame buffer address determins which memory to use.

static void ELCDIF_EnableLut (LCDIF_Type *base, bool enable)
 Enable or disable the LUT. More...
 
status_t ELCDIF_UpdateLut (LCDIF_Type *base, elcdif_lut_t lut, uint16_t startIndex, const uint32_t *lutData, uint16_t count)
 Load the LUT value. More...
 

Data Structure Documentation

struct _elcdif_pixel_format_reg

These register bits control the pixel format:

  • CTRL[DATA_FORMAT_24_BIT]
  • CTRL[DATA_FORMAT_18_BIT]
  • CTRL[DATA_FORMAT_16_BIT]
  • CTRL[WORD_LENGTH]
  • CTRL1[BYTE_PACKING_FORMAT]

Data Fields

uint32_t regCtrl
 Value of register CTRL. More...
 
uint32_t regCtrl1
 Value of register CTRL1. More...
 

Field Documentation

uint32_t _elcdif_pixel_format_reg::regCtrl
uint32_t _elcdif_pixel_format_reg::regCtrl1
struct _elcdif_rgb_mode_config

Data Fields

uint16_t panelWidth
 Display panel width, pixels per line. More...
 
uint16_t panelHeight
 Display panel height, how many lines per panel. More...
 
uint8_t hsw
 HSYNC pulse width. More...
 
uint8_t hfp
 Horizontal front porch. More...
 
uint8_t hbp
 Horizontal back porch. More...
 
uint8_t vsw
 VSYNC pulse width. More...
 
uint8_t vfp
 Vrtical front porch. More...
 
uint8_t vbp
 Vertical back porch. More...
 
uint32_t polarityFlags
 OR'ed value of _elcdif_polarity_flags, used to contol the signal polarity. More...
 
uint32_t bufferAddr
 Frame buffer address. More...
 
elcdif_pixel_format_t pixelFormat
 Pixel format. More...
 
elcdif_lcd_data_bus_t dataBus
 LCD data bus. More...
 

Field Documentation

uint16_t _elcdif_rgb_mode_config::panelWidth
uint16_t _elcdif_rgb_mode_config::panelHeight
uint8_t _elcdif_rgb_mode_config::hsw
uint8_t _elcdif_rgb_mode_config::hfp
uint8_t _elcdif_rgb_mode_config::hbp
uint8_t _elcdif_rgb_mode_config::vsw
uint8_t _elcdif_rgb_mode_config::vfp
uint8_t _elcdif_rgb_mode_config::vbp
uint32_t _elcdif_rgb_mode_config::polarityFlags
uint32_t _elcdif_rgb_mode_config::bufferAddr
elcdif_pixel_format_t _elcdif_rgb_mode_config::pixelFormat
elcdif_lcd_data_bus_t _elcdif_rgb_mode_config::dataBus
struct _elcdif_as_buffer_config

Data Fields

uint32_t bufferAddr
 Buffer address. More...
 
elcdif_as_pixel_format_t pixelFormat
 Pixel format. More...
 

Field Documentation

uint32_t _elcdif_as_buffer_config::bufferAddr
elcdif_as_pixel_format_t _elcdif_as_buffer_config::pixelFormat
struct _elcdif_as_blend_config

Data Fields

uint8_t alpha
 User defined alpha value, only used when alphaMode is kELCDIF_AlphaOverride or kELCDIF_AlphaRop. More...
 
bool invertAlpha
 Set true to invert the alpha. More...
 
elcdif_alpha_mode_t alphaMode
 Alpha mode. More...
 
elcdif_rop_mode_t ropMode
 ROP mode, only valid when alphaMode is kELCDIF_AlphaRop. More...
 

Field Documentation

uint8_t _elcdif_as_blend_config::alpha
bool _elcdif_as_blend_config::invertAlpha
elcdif_alpha_mode_t _elcdif_as_blend_config::alphaMode
elcdif_rop_mode_t _elcdif_as_blend_config::ropMode

Typedef Documentation

This enumerator should be defined together with the array s_pixelFormatReg. To support new pixel format, enhance this enumerator and s_pixelFormatReg.

These register bits control the pixel format:

  • CTRL[DATA_FORMAT_24_BIT]
  • CTRL[DATA_FORMAT_18_BIT]
  • CTRL[DATA_FORMAT_16_BIT]
  • CTRL[WORD_LENGTH]
  • CTRL1[BYTE_PACKING_FORMAT]

Explanation:

  • AS: Alpha surface
  • PS: Process surface
  • nAS: Alpha surface NOT value
  • nPS: Process surface NOT value
typedef enum _elcdif_lut elcdif_lut_t

The Lookup Table (LUT) is used to expand the 8 bits pixel to 24 bits pixel before output to external displayer.

There are two 256x24 bits LUT memory in LCDIF, the LSB of frame buffer address determins which memory to use.

Enumeration Type Documentation

Enumerator
kELCDIF_VsyncActiveLow 

VSYNC active low.

kELCDIF_HsyncActiveLow 

HSYNC active low.

kELCDIF_DataEnableActiveLow 

Data enable line active low.

kELCDIF_DriveDataOnFallingClkEdge 

Drive data on falling clock edge, capture data on rising clock edge.

kELCDIF_VsyncActiveHigh 

VSYNC active high.

kELCDIF_HsyncActiveHigh 

HSYNC active high.

kELCDIF_DataEnableActiveHigh 

Data enable line active high.

kELCDIF_DriveDataOnRisingClkEdge 

Drive data on falling clock edge, capture data on rising clock edge.

Enumerator
kELCDIF_BusMasterErrorInterruptEnable 

Bus master error interrupt.

kELCDIF_TxFifoOverflowInterruptEnable 

TXFIFO overflow interrupt.

kELCDIF_TxFifoUnderflowInterruptEnable 

TXFIFO underflow interrupt.

kELCDIF_CurFrameDoneInterruptEnable 

Interrupt when hardware enters vertical blanking state.

kELCDIF_VsyncEdgeInterruptEnable 

Interrupt when hardware encounters VSYNC edge.

Enumerator
kELCDIF_BusMasterError 

Bus master error interrupt.

kELCDIF_TxFifoOverflow 

TXFIFO overflow interrupt.

kELCDIF_TxFifoUnderflow 

TXFIFO underflow interrupt.

kELCDIF_CurFrameDone 

Interrupt when hardware enters vertical blanking state.

kELCDIF_VsyncEdge 

Interrupt when hardware encounters VSYNC edge.

Enumerator
kELCDIF_LFifoFull 

LFIFO full.

kELCDIF_LFifoEmpty 

LFIFO empty.

kELCDIF_TxFifoFull 

TXFIFO full.

kELCDIF_TxFifoEmpty 

TXFIFO empty.

This enumerator should be defined together with the array s_pixelFormatReg. To support new pixel format, enhance this enumerator and s_pixelFormatReg.

Enumerator
kELCDIF_PixelFormatRAW8 

RAW 8 bit, four data use 32 bits.

kELCDIF_PixelFormatRGB565 

RGB565, two pixel use 32 bits.

kELCDIF_PixelFormatRGB666 

RGB666 unpacked, one pixel uses 32 bits, high byte unused, upper 2 bits of other bytes unused.

kELCDIF_PixelFormatXRGB8888 

XRGB8888 unpacked, one pixel uses 32 bits, high byte unused.

kELCDIF_PixelFormatRGB888 

RGB888 packed, one pixel uses 24 bits.

Enumerator
kELCDIF_DataBus8Bit 

8-bit data bus.

kELCDIF_DataBus16Bit 

16-bit data bus, support RGB565.

kELCDIF_DataBus18Bit 

18-bit data bus, support RGB666.

kELCDIF_DataBus24Bit 

24-bit data bus, support RGB888.

Enumerator
kELCDIF_AsPixelFormatARGB8888 

32-bit pixels with alpha.

kELCDIF_AsPixelFormatRGB888 

32-bit pixels without alpha (unpacked 24-bit format)

kELCDIF_AsPixelFormatARGB1555 

16-bit pixels with alpha.

kELCDIF_AsPixelFormatARGB4444 

16-bit pixels with alpha.

kELCDIF_AsPixelFormatRGB555 

16-bit pixels without alpha.

kELCDIF_AsPixelFormatRGB444 

16-bit pixels without alpha.

kELCDIF_AsPixelFormatRGB565 

16-bit pixels without alpha.

Enumerator
kELCDIF_AlphaEmbedded 

The alpha surface pixel alpha value will be used for blend.

kELCDIF_AlphaOverride 

The user defined alpha value will be used for blend directly.

kELCDIF_AlphaMultiply 

The alpha surface pixel alpha value scaled the user defined alpha value will be used for blend, for example, pixel alpha set set to 200, user defined alpha set to 100, then the reault alpha is 200 * 100 / 255.

kELCDIF_AlphaRop 

Raster operation.

Explanation:

  • AS: Alpha surface
  • PS: Process surface
  • nAS: Alpha surface NOT value
  • nPS: Process surface NOT value
Enumerator
kELCDIF_RopMaskAs 

AS AND PS.

kELCDIF_RopMaskNotAs 

nAS AND PS.

kELCDIF_RopMaskAsNot 

AS AND nPS.

kELCDIF_RopMergeAs 

AS OR PS.

kELCDIF_RopMergeNotAs 

nAS OR PS.

kELCDIF_RopMergeAsNot 

AS OR nPS.

kELCDIF_RopNotCopyAs 

nAS.

kELCDIF_RopNot 

nPS.

kELCDIF_RopNotMaskAs 

AS NAND PS.

kELCDIF_RopNotMergeAs 

AS NOR PS.

kELCDIF_RopXorAs 

AS XOR PS.

kELCDIF_RopNotXorAs 

AS XNOR PS.

The Lookup Table (LUT) is used to expand the 8 bits pixel to 24 bits pixel before output to external displayer.

There are two 256x24 bits LUT memory in LCDIF, the LSB of frame buffer address determins which memory to use.

Enumerator
kELCDIF_Lut0 

LUT 0.

kELCDIF_Lut1 

LUT 1.

Function Documentation

void ELCDIF_RgbModeInit ( LCDIF_Type *  base,
const elcdif_rgb_mode_config_t config 
)

This function ungates the eLCDIF clock and configures the eLCDIF peripheral according to the configuration structure.

Parameters
baseeLCDIF peripheral base address.
configPointer to the configuration structure.
void ELCDIF_RgbModeGetDefaultConfig ( elcdif_rgb_mode_config_t config)

This function sets the configuration structure to default values. The default configuration is set to the following values.

config->panelWidth = 480U;
config->panelHeight = 272U;
config->hsw = 41;
config->hfp = 4;
config->hbp = 8;
config->vsw = 10;
config->vfp = 4;
config->vbp = 2;
config->polarityFlags = kELCDIF_VsyncActiveLow |
config->bufferAddr = 0U;
config->pixelFormat = kELCDIF_PixelFormatRGB888;
config->dataBus = kELCDIF_DataBus24Bit;
Parameters
configPointer to the eLCDIF configuration structure.
void ELCDIF_Deinit ( LCDIF_Type *  base)
Parameters
baseeLCDIF peripheral base address.
void ELCDIF_RgbModeSetPixelFormat ( LCDIF_Type *  base,
elcdif_pixel_format_t  pixelFormat 
)
Parameters
baseeLCDIF peripheral base address.
pixelFormatThe pixel format.
static void ELCDIF_RgbModeStart ( LCDIF_Type *  base)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
void ELCDIF_RgbModeStop ( LCDIF_Type *  base)
Parameters
baseeLCDIF peripheral base address.
static void ELCDIF_SetNextBufferAddr ( LCDIF_Type *  base,
uint32_t  bufferAddr 
)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
bufferAddrThe frame buffer address to set.
void ELCDIF_Reset ( LCDIF_Type *  base)
Parameters
baseeLCDIF peripheral base address.
static uint32_t ELCDIF_GetCrcValue ( const LCDIF_Type *  base)
inlinestatic

When a frame is sent complete (the interrupt kELCDIF_CurFrameDone assert), this function can be used to get the CRC value of the frame sent.

Parameters
baseeLCDIF peripheral base address.
Returns
The CRC value.
Note
The CRC value is dependent on the LCD_DATABUS_WIDTH.
static uint32_t ELCDIF_GetBusMasterErrorAddr ( const LCDIF_Type *  base)
inlinestatic

When bus master error occurs (the interrupt kELCDIF_BusMasterError assert), this function can get the virtual address at which the AXI master received an error response from the slave.

Parameters
baseeLCDIF peripheral base address.
Returns
The error virtual address.
static uint32_t ELCDIF_GetStatus ( const LCDIF_Type *  base)
inlinestatic

The status flags are returned as a mask value, application could check the corresponding bit. Example:

uint32_t statusFlags;
statusFlags = ELCDIF_GetStatus(LCDIF);
if (kELCDIF_LFifoFull & statusFlags)
{
}
if (kELCDIF_TxFifoEmpty & statusFlags)
{
}
Parameters
baseeLCDIF peripheral base address.
Returns
The mask value of status flags, it is OR'ed value of _elcdif_status_flags.
static uint32_t ELCDIF_GetLFifoCount ( const LCDIF_Type *  base)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
Returns
The LFIFO current count
static void ELCDIF_EnableInterrupts ( LCDIF_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
maskinterrupt source, OR'ed value of _elcdif_interrupt_enable.
static void ELCDIF_DisableInterrupts ( LCDIF_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
maskinterrupt source, OR'ed value of _elcdif_interrupt_enable.
static uint32_t ELCDIF_GetInterruptStatus ( const LCDIF_Type *  base)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
Returns
Interrupt pending status, OR'ed value of _elcdif_interrupt_flags.
static void ELCDIF_ClearInterruptStatus ( LCDIF_Type *  base,
uint32_t  mask 
)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
maskof the flags to clear, OR'ed value of _elcdif_interrupt_flags.
static void ELCDIF_EnableLut ( LCDIF_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseeLCDIF peripheral base address.
enableTrue to enable, false to disable.
status_t ELCDIF_UpdateLut ( LCDIF_Type *  base,
elcdif_lut_t  lut,
uint16_t  startIndex,
const uint32_t *  lutData,
uint16_t  count 
)

This function loads the LUT value to the specific LUT memory, user can specify the start entry index.

Parameters
baseeLCDIF peripheral base address.
lutWhich LUT to load.
startIndexThe start index of the LUT entry to update.
lutDataThe LUT data to load.
countCount of lutData.
Return values
kStatus_SuccessInitialization success.
kStatus_InvalidArgumentWrong argument.