MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
MMAU: Memory Mapped Arithmetic Unit

Overview

The MCUXpresso SDK provides a peripheral driver for the Memory Mapped Arithmetic Unit (MMAU) block of MCUXpresso SDK devices.

The Memory Mapped Arithmetic Unit (MMAU) provides acceleration to a set of math operations, including signed/unsigned multiplication and accumulation, division and root-square, and so on.

Function groups

MMAU Initialization

To initialize the MMAU driver, call the MMAU_EnableDMA(MMAU, true) and MMAU_EnableSupervisorOnly(MMAU, false) functions. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mmau

MMAU Interrupts

MMAU supports three interrupts: Accumulation Overflow (Q), Divide/Multiply Overflow (V) and Divide-by-Zero (DZ). These interrupts were definition at mmau_flag_t structure. The MMAU driver supports enable/disable the interrupts, get/clear the interrupt flags.

For example: Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mmau

MMAU Instruction flags

The MMAU driver provides four instruction flags: Accumulation Overflow (Q), Divide or Multiply Overflow (V), Divide-by-Zero (DZ) and Signed calculation result is negative (N). These flags were updated after each calculation. MMAU driver contains get and set functions to access instruction flags. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mmau

MMAU Operators

The MMAU driver supports multiply, divide and square root functions. Each kind of function supports Unsigned Integer, Signed Integer (except square root) and Fractional Number as operator.

Typical use case and example

This example demonstrates the SIN calculation. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/mmau

Typedefs

typedef enum _mmau_interrupt_enable mmau_interrupt_enable_t
 MMAU interrupt configuration structure, default settings all disabled. More...
 
typedef enum _mmau_interrupt_flag mmau_interrupt_flag_t
 MMAU interrupt and instruction flags.
 
typedef enum _mmau_instruction_flag mmau_instruction_flag_t
 MMAU interrupt and instruction flags.
 

Enumerations

enum  _mmau_interrupt_enable {
  kMMAU_AccumOverflowInterruptEnable = (MMAU_CSR_QIE_MASK),
  kMMAU_OverflowInterruptEnable = (MMAU_CSR_VIE_MASK),
  kMMAU_DivideByZeroInterruptEnable = (MMAU_CSR_DZIE_MASK)
}
 MMAU interrupt configuration structure, default settings all disabled. More...
 
enum  _mmau_interrupt_flag {
  kMMAU_AccumOverflowInterruptFlag = (MMAU_CSR_QIF_MASK),
  kMMAU_OverflowInterruptFlag = (MMAU_CSR_VIF_MASK),
  kMMAU_DivideByZeroInterruptFlag = (MMAU_CSR_DZIF_MASK)
}
 MMAU interrupt and instruction flags. More...
 
enum  _mmau_instruction_flag {
  kMMAU_AccumOverflowInstructionFlag = (MMAU_CSR_Q_MASK),
  kMMAU_OverflowInstructionFlag = (MMAU_CSR_V_MASK),
  kMMAU_DivideByZeroInstructionFlag = (MMAU_CSR_DZ_MASK),
  kMMAU_NegativeInstructionFlag = (MMAU_CSR_N_MASK)
}
 MMAU interrupt and instruction flags. More...
 

Functions

static uint32_t MMAU_GetHwRevCmd (MMAU_Type *base)
 Gets hardware revision level. More...
 

Driver version

#define FSL_MMAU_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 Version 2.0.1.
 

Registers decorated load/store addresses

#define MMAU__X0   0xF0004000UL
 Accumulator register X0.
 
#define MMAU__X1   0xF0004004UL
 Accumulator register X1.
 
#define MMAU__X2   0xF0004008UL
 Accumulator register X2.
 
#define MMAU__X3   0xF000400CUL
 Accumulator register X3.
 
#define MMAU__A0   0xF0004010UL
 Accumulator register A0.
 
#define MMAU__A1   0xF0004014UL
 Accumulator register A1.
 
#define MMAU__A10   0xF0004010UL
 Accumulator register pair A10.
 

Unsigned integer instructions decorated load/store addresses

#define MMAU__REGRW   0xF0004000UL
 Registers RW.
 
#define MMAU__UMUL   0xF0004020UL
 A10=X2*X3.
 
#define MMAU__UMULD   0xF0004040UL
 A10=X21*X3.
 
#define MMAU__UMULDA   0xF0004060UL
 A10=A10*X3.
 
#define MMAU__UMAC   0xF00040A0UL
 A10=X2*X3+A10.
 
#define MMAU__UMACD   0xF00040C0UL
 A10=X21*X3+A10.
 
#define MMAU__UMACDA   0xF00040E0UL
 A10=A10*X3+X21.
 
#define MMAU__UDIV   0xF0004120UL
 X21/X3=A10.
 
#define MMAU__UDIVD   0xF0004140UL
 A10=X2/X3.
 
#define MMAU__UDIVDA   0xF0004160UL
 A10=X21/X3.
 
#define MMAU__UDIVDD   0xF0004180UL
 A10=A10/X3.
 
#define MMAU__UDIVDDA   0xF00041A0UL
 A10=A10/X32.
 
#define MMAU__USQR   0xF0004220UL
 A10=SQR(X3)
 
#define MMAU__USQRD   0xF0004240UL
 A10=SQR(X32)
 
#define MMAU__USQRDA   0xF0004260UL
 A10=SQR(A10)
 

Signed fractional instructions decorated load/store addresses

#define MMAU__QSQR   0xF00042A0UL
 A10=SQR(X3)
 
#define MMAU__QSQRD   0xF00042C0UL
 A10=SQR(X32)
 
#define MMAU__QSQRDA   0xF00042E0UL
 A10=SQR(A10)
 
#define MMAU__QDIV   0xF0004320UL
 A10=X2/X3.
 
#define MMAU__QDIVD   0xF0004340UL
 A10=X21/X3.
 
#define MMAU__QDIVDA   0xF0004360UL
 A10=A10/X3.
 
#define MMAU__QMUL   0xF0004420UL
 A10=X2*X3.
 
#define MMAU__QMULD   0xF0004440UL
 A10=X21*X3.
 
#define MMAU__QMULDA   0xF0004460UL
 A10=A10*X3.
 
#define MMAU__QMAC   0xF00044A0UL
 A10=X2*X3+A10.
 
#define MMAU__QMACD   0xF00044C0UL
 A10=X21*X3+A10.
 
#define MMAU__QMACDA   0xF00044E0UL
 A10=A10*X3+X21.
 

Signed integer instructions decorated load/store addresses

#define MMAU__SMUL   0xF0004620UL
 A10=X2*X3.
 
#define MMAU__SMULD   0xF0004640UL
 A10=X21*X3.
 
#define MMAU__SMULDA   0xF0004660UL
 A10=A10*X3.
 
#define MMAU__SMAC   0xF00046A0UL
 A10=X2*X3+A10.
 
#define MMAU__SMACD   0xF00046C0UL
 A10=X21*X3+A10.
 
#define MMAU__SMACDA   0xF00046E0UL
 A10=A10*X3+X21.
 
#define MMAU__SDIV   0xF0004720UL
 A10=X2/X3.
 
#define MMAU__SDIVD   0xF0004740UL
 A10=X21/X3.
 
#define MMAU__SDIVDA   0xF0004760UL
 A10=A10/X3.
 
#define MMAU__SDIVDD   0xF0004780UL
 A10=X10/X32.
 
#define MMAU__SDIVDDA   0xF00047A0UL
 A10=A10/X32.
 

Auxiliary decorated load/store addresses

#define MMAU__SAT   0xF0004800UL
 Saturation.
 

Fractional Data Type

typedef short int frac16_t
 Q0.15 fractional.
 
typedef long frac24_t
 Q8.23 fractional.
 
typedef long frac32_t
 Q0.31 fractional.
 
typedef long long frac48_t
 Q16.47 fractional.
 
typedef long long frac64_t
 Q0.63 fractional.
 

MMAU Configure

static void MMAU_EnableDMA (MMAU_Type *base, bool enable)
 Enable DMA for MMAU module. More...
 
static void MMAU_EnableSupervisorOnly (MMAU_Type *base, bool enable)
 Enable supervisor only for MMAU module. More...
 
void MMAU_Reset (MMAU_Type *base)
 Set control/status register into reset state. More...
 

MMAU Interrupt

static void MMAU_EnableInterrupts (MMAU_Type *base, uint32_t mask)
 Enable MMAU interrupts. More...
 
static void MMAU_DisableInterrupts (MMAU_Type *base, uint32_t mask)
 Disable MMAU interrupts. More...
 
static uint32_t MMAU_GetEnabledInterrupts (MMAU_Type *base)
 Gets enabled interrupts. More...
 
static uint32_t MMAU_GetInterruptFlags (MMAU_Type *base)
 Get interrupt flags. More...
 
void MMAU_ClearInterruptFlags (MMAU_Type *base, uint32_t mask)
 Clears interrupt flags. More...
 

MMAU Instruction flag

static uint32_t MMAU_GetInstructionFlags (MMAU_Type *base)
 Gets the instruction flags. More...
 
void MMAU_SetInstructionFlags (MMAU_Type *base, uint32_t mask)
 Sets the instruction flags. More...
 
void MMAU_ClearInstructionFlags (MMAU_Type *base, uint32_t mask)
 Clears instruction flags. More...
 

Unsigned Integer Operands

static void MMAU_ulda_d (register uint64_t dval)
 Load A10 accumulator register of the MMAU by 64-bit unsigned value. More...
 
static uint64_t MMAU_d_umul_ll (register uint32_t lval1, register uint32_t lval2)
 Multiply two 32-bit unsigned values returning a 64-bit unsigned product. More...
 
static uint64_t MMAU_d_umul_dl (register uint64_t dval, register uint32_t lval)
 Multiply 64-bit unsigned value with 32-bit unsigned value returning a 64-bit unsigned product. More...
 
static uint64_t MMAU_d_umuls_dl (register uint64_t dval, register uint32_t lval)
 Saturating multiply 64-bit unsigned value with 32-bit unsigned value returning saturated 64-bit unsigned product. More...
 
static uint64_t MMAU_d_umula_l (register uint32_t lval)
 Multiply 32-bit unsigned value with 64-bit unsigned value stored in the A10 register of the MMAU returning a 64-bit unsigned product. More...
 
static uint64_t MMAU_d_umulas_l (register uint32_t lval)
 Saturating multiply 32-bit unsigned value with 64-bit unsigned value stored in the A10 register of the MMAU returning saturated 64-bit unsigned product. More...
 
static uint64_t MMAU_d_umac_ll (register uint32_t lval1, register uint32_t lval2)
 Multiply two 32-bit unsigned values and add product with value stored in the A10 register of the MMAU returning a 64-bit unsigned A10 register value. More...
 
static uint64_t MMAU_d_umacs_ll (register uint32_t lval1, register uint32_t lval2)
 Saturating multiply two 32-bit unsigned values and add product with value stored in the A10 register of the MMAU returning a 64-bit unsigned A10 register value. More...
 
static uint64_t MMAU_d_umac_dl (register uint64_t dval, register uint32_t lval)
 Multiply 64-bit unsigned value with 32-bit unsigned value and add product with value stored in the A10 register of the MMAU returning a 64-bit unsigned A10 register value. More...
 
static uint64_t MMAU_d_umacs_dl (register uint64_t dval, register uint32_t lval)
 Saturating multiply 64-bit unsigned value with 32-bit unsigned value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit unsigned A10 register value. More...
 
static uint64_t MMAU_d_umaca_dl (register uint64_t dval, register uint32_t lval)
 Multiply 32-bit unsigned value by value stored in the A10 register of the MMAU and add product with 64-bit unsigned value returning a 64-bit unsigned A10 register value. More...
 
static uint64_t MMAU_d_umacas_dl (register uint64_t dval, register uint32_t lval)
 Saturating multiply 32-bit unsigned value by value stored in the A10 register of the MMAU and add product with 64-bit unsigned value returning a saturated 64-bit unsigned A10 register value. More...
 
static uint32_t MMAU_l_udiv_ll (register uint32_t lnum, register uint32_t lden)
 Divide two 32-bit unsigned values returning a 32-bit unsigned quotient. More...
 
static uint64_t MMAU_d_udiv_dl (register uint64_t dnum, register uint32_t lden)
 Divide 64-bit unsigned value by 32-bit unsigned value returning a 64-bit unsigned quotient. More...
 
static uint64_t MMAU_d_udiv_dd (register uint64_t dnum, register uint64_t dden)
 Divide two 64-bit unsigned values returning a 64-bit unsigned quotient. More...
 
static uint64_t MMAU_d_udiva_l (register uint32_t lden1)
 Divide 32-bit unsigned value stored in the A10 register of the MMAU by 32-bit unsigned value returning a 64-bit unsigned quotient. More...
 
static uint64_t MMAU_d_udiva_d (register uint64_t dden1)
 Divide 64-bit unsigned value stored in the A10 register of the MMAU by 64-bit unsigned value returning a 64-bit unsigned quotient. More...
 
static uint32_t MMAU_l_usqr_l (register uint32_t lrad)
 Compute and return a 32-bit unsigned square root of the 32-bit unsigned radicand. More...
 
static uint32_t MMAU_l_usqr_d (register uint64_t drad)
 Compute and return a 32-bit unsigned square root of the 64-bit unsigned radicand. More...
 
static uint16_t MMAU_s_usqr_l (register uint32_t lrad)
 Compute and return a 16-bit unsigned square root of the 32-bit unsigned radicand. More...
 
static uint32_t MMAU_l_usqra (void)
 Compute and return a 32-bit unsigned square root of the radicand stored in the A10 register of the MMAU. More...
 

Signed Integer Operands

static void MMAU_slda_d (register int64_t dval)
 Load A10 accumulator register of the MMAU by 64-bit integer value. More...
 
static int64_t MMAU_d_smul_ll (register int32_t lval1, register int32_t lval2)
 Multiply two 32-bit integer values returning a 64-bit integer product. More...
 
static int64_t MMAU_d_smul_dl (register int64_t dval, register int32_t lval)
 Multiply 64-bit integer value with 32-bit integer value returning a 64-bit integer product. More...
 
static int64_t MMAU_d_smuls_dl (register int64_t dval, register int32_t lval)
 Saturating multiply 64-bit integer value with 32-bit integer value returning saturated 64-bit integer product. More...
 
static int64_t MMAU_d_smula_l (register int32_t lval)
 Multiply 32-bit integer value with 64-bit integer value stored in the A10 register of the MMAU returning a 64-bit integer product. More...
 
static int64_t MMAU_d_smulas_l (register int32_t lval)
 Saturating multiply 32-bit integer value with 64-bit integer value stored in the A10 register of the MMAU returning saturated 64-bit integer product. More...
 
static int64_t MMAU_d_smac_ll (register int32_t lval1, register int32_t lval2)
 Multiply two 32-bit integer values and add product with value stored in the A10 register of the MMAU returning a 64-bit integer A10 register value. More...
 
static int64_t MMAU_d_smacs_ll (register int32_t lval1, register int32_t lval2)
 Saturating multiply two 32-bit integer values and add product with value stored in the A10 register of the MMAU returning a 64-bit integer A10 register value. More...
 
static int64_t MMAU_d_smac_dl (register int64_t dval, register int32_t lval)
 Multiply 64-bit integer value with 32-bit integer value and add product with value stored in the A10 register of the MMAU returning a 64-bit integer A10 register value. More...
 
static int64_t MMAU_d_smacs_dl (register int64_t dval, register int32_t lval)
 Saturating multiply 64-bit integer value with 32-bit integer value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit integer A10 register value. More...
 
static int64_t MMAU_d_smaca_dl (register int64_t dval, register int32_t lval)
 Multiply 32-bit integer value by value stored in the A10 register of the MMAU and add product with 64-bit integer value returning a 64-bit integer A10 register value. More...
 
static int64_t MMAU_d_smacas_dl (register int64_t dval, register int32_t lval)
 Saturating multiply 32-bit integer value by value stored in the A10 register of the MMAU and add product with 64-bit integer value returning a saturated 64-bit integer A10 register value. More...
 
static int32_t MMAU_l_sdiv_ll (register int32_t lnum, register int32_t lden)
 Divide two 32-bit integer values returning a 32-bit integer quotient. More...
 
static int32_t MMAU_l_sdivs_ll (register int32_t lnum, register int32_t lden)
 Divide two 32-bit integer values returning a 32-bit integer quotient. More...
 
static int64_t MMAU_d_sdiv_dl (register int64_t dnum, register int32_t lden)
 Divide 64-bit integer value by 32-bit integer value returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdivs_dl (register int64_t dnum, register int32_t lden)
 Divide 64-bit integer value by 32-bit integer value returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdiv_dd (register int64_t dnum, register int64_t dden)
 Divide two 64-bit integer values returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdivs_dd (register int64_t dnum, register int64_t dden)
 Divide two 64-bit integer values returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdiva_l (register int32_t lden1)
 Divide 32-bit integer value stored in the A10 register of the MMAU by 32-bit integer value returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdivas_l (register int32_t lden1)
 Divide 32-bit integer value stored in the A10 register of the MMAU by 32-bit integer value returning saturated 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdiva_d (register int64_t dden1)
 Divide 64-bit integer value stored in the A10 register of the MMAU by 64-bit integer value returning a 64-bit integer quotient. More...
 
static int64_t MMAU_d_sdivas_d (register int64_t dden1)
 Divide 64-bit integer value stored in the A10 register of the MMAU by 64-bit integer value returning saturated 64-bit integer quotient. More...
 

Fractional Operands

static void MMAU_lda_d (register frac64_t dval)
 Load A10 accumulator register of the MMAU by 64-bit fractional value. More...
 
static frac32_t MMAU_l_mul_ll (register frac32_t lval1, register frac32_t lval2)
 Multiply two 32-bit fractional values returning a 32-bit fractional product. More...
 
static frac32_t MMAU_l_muls_ll (register frac32_t lval1, register frac32_t lval2)
 Saturating multiply two 32-bit fractional values returning saturated 32-bit fractional product. More...
 
static frac64_t MMAU_d_mul_ll (register frac32_t lval1, register frac32_t lval2)
 Multiply two 32-bit fractional values returning a 64-bit fractional product. More...
 
static frac64_t MMAU_d_muls_ll (register frac32_t lval1, register frac32_t lval2)
 Saturating multiply two 32-bit fractional values returning saturated 64-bit fractional product. More...
 
static frac64_t MMAU_d_mul_dl (register frac64_t dval, register frac32_t lval)
 Multiply 64-bit fractional value with 32-bit fractional value returning a 64-bit fractional product. More...
 
static frac64_t MMAU_d_muls_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 64-bit fractional value with 32-bit fractional value returning saturated 64-bit fractional product. More...
 
static frac64_t MMAU_d_mula_l (register frac32_t lval)
 Multiply 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning a 64-bit fractional product. More...
 
static frac64_t MMAU_d_mulas_l (register frac32_t lval)
 Saturating multiply 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning saturated 64-bit fractional product. More...
 
static frac32_t MMAU_l_mul_dl (register frac64_t dval, register frac32_t lval)
 Multiply 64-bit fractional value with 32-bit fractional value returning a 32-bit fractional product. More...
 
static frac32_t MMAU_l_muls_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 64-bit fractional value with 32-bit fractional value returning saturated 32-bit fractional product. More...
 
static frac32_t MMAU_l_mula_l (register frac32_t lval)
 Multiply 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning a 32-bit fractional product. More...
 
static frac32_t MMAU_l_mulas_l (register frac32_t lval)
 Saturating multiply 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning saturated 32-bit fractional product. More...
 
static frac64_t MMAU_d_mac_ll (register frac32_t lval1, register frac32_t lval2)
 Multiply two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 64-bit fractional A10 register value. More...
 
static frac64_t MMAU_d_macs_ll (register frac32_t lval1, register frac32_t lval2)
 Saturating multiply two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 64-bit fractional A10 register value. More...
 
static frac64_t MMAU_d_mac_dl (register frac64_t dval, register frac32_t lval)
 Multiply 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning a 64-bit fractional A10 register value. More...
 
static frac64_t MMAU_d_macs_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit fractional A10 register value. More...
 
static frac64_t MMAU_d_maca_dl (register frac64_t dval, register frac32_t lval)
 Multiply 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a 64-bit fractional A10 register value. More...
 
static frac64_t MMAU_d_macas_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a saturated 64-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_mac_ll (register frac32_t lval1, register frac32_t lval2)
 Multiply two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_macs_ll (register frac32_t lval1, register frac32_t lval2)
 Saturating multiply two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_mac_dl (register frac64_t dval, register frac32_t lval)
 Multiply 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning a 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_macs_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning saturated 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_maca_dl (register frac64_t dval, register frac32_t lval)
 Multiply 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_macas_dl (register frac64_t dval, register frac32_t lval)
 Saturating multiply 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a saturated 32-bit fractional A10 register value. More...
 
static frac32_t MMAU_l_div_ll (register frac32_t lnum, register frac32_t lden)
 Divide two 32-bit fractional values returning a 32-bit fractional quotient. More...
 
static frac32_t MMAU_l_divs_ll (register frac32_t lnum, register frac32_t lden)
 Divide two 32-bit fractional values returning a 32-bit fractional quotient. More...
 
static frac32_t MMAU_l_divas_l (register frac32_t lden)
 Divide 64-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning saturated 32-bit fractional quotient. More...
 
static frac64_t MMAU_d_div_dl (register frac64_t dnum, register frac32_t lden)
 Divide 64-bit fractional value by 32-bit fractional value returning a 64-bit fractional quotient. More...
 
static frac64_t MMAU_d_divs_dl (register frac64_t dnum, register frac32_t lden)
 Divide 64-bit fractional value by 32-bit fractional value returning a 64-bit fractional quotient. More...
 
static frac64_t MMAU_d_diva_l (register frac32_t lden1)
 Divide 32-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a 64-bit fractional quotient. More...
 
static frac64_t MMAU_d_divas_l (register frac32_t lden1)
 Divide 32-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning saturated 64-bit fractional quotient. More...
 
static frac32_t MMAU_l_diva_l (register frac32_t lden)
 Divide 64-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a 32-bit fractional quotient. More...
 
static frac32_t MMAU_l_sqr_l (register frac32_t lrad)
 Compute and return a 32-bit fractional square root of the 32-bit fractional radicand. More...
 
static frac32_t MMAU_l_sqr_d (register frac64_t drad)
 Compute and return a 32-bit fractional square root of the 64-bit fractional radicand. More...
 
static frac32_t MMAU_l_sqra (void)
 Compute and return a 32-bit fractional square root of the radicand stored in the A10 register of the MMAU. More...
 

Typedef Documentation

This structure contains the settings for all of the MMAU interrupt configurations.

Enumeration Type Documentation

This structure contains the settings for all of the MMAU interrupt configurations.

Enumerator
kMMAU_AccumOverflowInterruptEnable 

Accumulation Overflow Enable.

kMMAU_OverflowInterruptEnable 

Multiply or Divide overflow Enable.

kMMAU_DivideByZeroInterruptEnable 

Divide by Zero Enable.

Enumerator
kMMAU_AccumOverflowInterruptFlag 

Accumulation Overflow Interrupt Flag.

kMMAU_OverflowInterruptFlag 

Multiply or Divide overflow Interrupt Flag.

kMMAU_DivideByZeroInterruptFlag 

Divide by Zero Interrupt Flag.

Enumerator
kMMAU_AccumOverflowInstructionFlag 

Accumulation Overflow.

kMMAU_OverflowInstructionFlag 

Multiply or Divide overflow.

kMMAU_DivideByZeroInstructionFlag 

Divide by Zero.

kMMAU_NegativeInstructionFlag 

Signed calculation result is negative.

Function Documentation

static void MMAU_EnableDMA ( MMAU_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseMMAU peripheral address.
enableMode of DMA access
  • true Enable DMA access
  • false Disable DMA access
static void MMAU_EnableSupervisorOnly ( MMAU_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseMMAU peripheral address.
enableMode of MMAU module can be access
  • true MMAU registers can only be access in Supervisor Mode.
  • false MMAU registers can be access in both User Mode or Supervisor Mode.
void MMAU_Reset ( MMAU_Type *  base)

This function sets control/status register to a known state. This state is defined in Reference Manual, which is power on reset value. This function must execute in a Supervisor Mode

Parameters
baseMMAU peripheral address.
static void MMAU_EnableInterrupts ( MMAU_Type *  base,
uint32_t  mask 
)
inlinestatic

This function enables the interrupts related to the mask. Example:

Parameters
baseMMAU peripheral address.
maskMask of the interrupt enable to be written (kMMAU_AccumOverflowInterruptEnable|kMMAU_OverflowInterruptEnable|kMMAU_DivideByZeroInterruptEnable).
static void MMAU_DisableInterrupts ( MMAU_Type *  base,
uint32_t  mask 
)
inlinestatic

This function disables the interrupt related to the mask. Example:

Parameters
baseMMAU peripheral address.
maskMask of the interrupt enable to be written (kMMAU_AccumOverflowInterruptEnable|kMMAU_OverflowInterruptEnable|kMMAU_DivideByZeroInterruptEnable).
static uint32_t MMAU_GetEnabledInterrupts ( MMAU_Type *  base)
inlinestatic

This function gets all interrupt values. Example:

uint32_t flags = 0;
...
{
...
}
Parameters
baseMMAU peripheral address.
Returns
Combination of enabled interrupt
static uint32_t MMAU_GetInterruptFlags ( MMAU_Type *  base)
inlinestatic

This function gets interrupt flags.

Parameters
baseMMAU peripheral address.
Returns
the mask of these interrupt flag bits.
void MMAU_ClearInterruptFlags ( MMAU_Type *  base,
uint32_t  mask 
)

This function clears the interrupt flags. Example, if you want to clear Overflow and DivideByZero interrupt flags:

Parameters
baseMMAU peripheral address.
maskMask of the asserted interrupt flags (kMMAU_AccumOverflowInterruptFlag|kMMAU_OverflowInterruptFlag|kMMAU_DivideByZeroInterruptFlag).
static uint32_t MMAU_GetInstructionFlags ( MMAU_Type *  base)
inlinestatic

This function gets the instruction flag. Instruction flags are updated by the MMAU after computation of each instruction. Example:

uint32_t flags;
...
{
...
}
Parameters
baseMMAU peripheral address.
Returns
Combination of all instruction flags.
void MMAU_SetInstructionFlags ( MMAU_Type *  base,
uint32_t  mask 
)

This function sets the instruction flags. Example:

Parameters
baseMMAU peripheral address.
maskMask of the instruction flags to be written

(kMMAU_AccumOverflowInstructionFlag|kMMAU_OverflowInstructionFlag|kMMAU_DivideByZeroInstructionFlag|kMMAU_NegativeInstructionFlag).

void MMAU_ClearInstructionFlags ( MMAU_Type *  base,
uint32_t  mask 
)

This function clears the instruction flags. Example, if you want to clear Overflow and DivideByZero instruction flags:

Parameters
baseMMAU peripheral address.
maskMask of the asserted instruction flags

(kMMAU_AccumOverflowInstructionFlag|kMMAU_OverflowInstructionFlag|kMMAU_DivideByZeroInstructionFlag|kMMAU_NegativeInstructionFlag).

static uint32_t MMAU_GetHwRevCmd ( MMAU_Type *  base)
inlinestatic

This function gets the hardware revision level of the MMAU. It returns HDR field of the control/status register.

Parameters
baseMMAU peripheral address.
Returns
uint32_t hardware revision level.
static void MMAU_ulda_d ( register uint64_t  dval)
inlinestatic

The ulda_d function loads A10 accumulator register of the MMAU by 64-bit unsigned value.

Parameters
dvaluint64_t unsigned load value.
static uint64_t MMAU_d_umul_ll ( register uint32_t  lval1,
register uint32_t  lval2 
)
inlinestatic

The MMAU_d_umul_ll function multiplies two 32-bit unsigned values returning a 64-bit unsigned product.

Parameters
lval1uint32_t unsigned value.
lval2uint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umul_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umul_dl function multiplies 64-bit unsigned value with 32-bit unsigned value returning a 64-bit unsigned product.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umuls_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umuls_dl function multiplies 64-bit unsigned value with 32-bit unsigned value returning saturated 64-bit unsigned product.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umula_l ( register uint32_t  lval)
inlinestatic

The MMAU_d_umula_l function multiplies 32-bit unsigned value with 64-bit unsigned value stored in the A10 register of the MMAU returning a 64-bit unsigned product.

Parameters
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umulas_l ( register uint32_t  lval)
inlinestatic

The MMAU_d_umulas_l function multiplies 32-bit unsigned value with 64-bit unsigned value stored in the A10 register of the MMAU returning saturated 64-bit unsigned product.

Parameters
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umac_ll ( register uint32_t  lval1,
register uint32_t  lval2 
)
inlinestatic

The MMAU_d_umac_ll function multiplies two 32-bit unsigned values and add product with value stored in the A10 register of the MMAU returning a 64-bit unsigned A10 register value.

Parameters
lval1uint32_t unsigned value.
lval2uint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umacs_ll ( register uint32_t  lval1,
register uint32_t  lval2 
)
inlinestatic

The MMAU_d_umacs_ll function multiplies two 32-bit unsigned values and add product with value stored in the A10 register of the MMAU returning saturated 64-bit unsigned A10 register value.

Parameters
lval1uint32_t unsigned value.
lval2uint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umac_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umac_dl function multiplies 64-bit unsigned value with 32-bit unsigned value and add product with value stored in the A10 register of the MMAU returning a 64-bit unsigned A10 register value.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umacs_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umacs_dl function multiplies 64-bit unsigned value with 32-bit unsigned value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit unsigned A10 register value.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umaca_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umaca_dl function multiplies 32-bit unsigned value by value stored in the A10 register of the MMAU and add product with 64-bit unsigned value returning a 64-bit unsigned A10 register value.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_umacas_dl ( register uint64_t  dval,
register uint32_t  lval 
)
inlinestatic

The MMAU_d_umacas_dl function multiplies 32-bit unsigned value by value stored in the A10 register of the MMAU and add product with 64-bit unsigned value returning saturated 64-bit unsigned A10 register value.

Parameters
dvaluint64_t unsigned value.
lvaluint32_t unsigned value.
Returns
uint64_t unsigned value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static uint32_t MMAU_l_udiv_ll ( register uint32_t  lnum,
register uint32_t  lden 
)
inlinestatic

The MMAU_l_udiv_ll function divides two 32-bit unsigned values returning a 32-bit unsigned quotient.

Parameters
lnumuint32_t unsigned divisor value.
ldenuint32_t unsigned dividend value.
Returns
uint32_t unsigned quotient value.
Note
Quotient is stored in A0 register of the MMAU for next computation.
static uint64_t MMAU_d_udiv_dl ( register uint64_t  dnum,
register uint32_t  lden 
)
inlinestatic

The MMAU_d_udiv_dl function divides 64-bit unsigned value by 32-bit unsigned value returning a 64-bit unsigned quotient.

Parameters
dnumuint64_t unsigned divisor value.
ldenuint32_t unsigned dividend value.
Returns
uint64_t unsigned quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_udiv_dd ( register uint64_t  dnum,
register uint64_t  dden 
)
inlinestatic

The MMAU_d_udiv_dd function divides two 64-bit unsigned values returning a 64-bit unsigned quotient.

Parameters
dnumuint64_t unsigned divisor value.
ddenuint64_t unsigned dividend value.
Returns
uint64_t unsigned quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_udiva_l ( register uint32_t  lden1)
inlinestatic

The MMAU_d_udiva_l function divides 64-bit unsigned value stored in the A10 register of the MMAU by 32-bit unsigned value returning a 64-bit unsigned quotient.

Parameters
lden1uint32_t unsigned dividend value.
Returns
uint64_t unsigned quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static uint64_t MMAU_d_udiva_d ( register uint64_t  dden1)
inlinestatic

The MMAU_d_udiva_d function divides 64-bit unsigned value stored in the A10 register of the MMAU by 64-bit unsigned value returning a 64-bit unsigned quotient.

Parameters
dden1uint64_t unsigned dividend value.
Returns
uint64_t unsigned quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static uint32_t MMAU_l_usqr_l ( register uint32_t  lrad)
inlinestatic

The MMAU_l_usqr_l function computes and returns a 32-bit unsigned square root of the 32-bit unsigned radicand.

Parameters
lraduint32_t unsigned radicand.
Returns
uint32_t unsigned square root.
Note
Quotient is stored in A0 register of the MMAU for next computation.
static uint32_t MMAU_l_usqr_d ( register uint64_t  drad)
inlinestatic

The MMAU_l_usqr_d function computes and returns a 32-bit unsigned square root of the 64-bit unsigned radicand.

Parameters
draduint64_t unsigned radicand.
Returns
uint32_t unsigned square root.
Note
Quotient is stored in A0 register of the MMAU for next computation.
static uint16_t MMAU_s_usqr_l ( register uint32_t  lrad)
inlinestatic

The MMAU_s_usqr_l function computes and returns a 16-bit unsigned square root of the 32-bit unsigned radicand.

Parameters
lraduint32 unsigned radicand.
Returns
uint16 unsigned square root.
Note
Square root is stored in A0 register of the MMAU for next computation.
static uint32_t MMAU_l_usqra ( void  )
inlinestatic

The MMAU_l_usqra function computes and returns a 32-bit unsigned square root of the radicand stored in the A10 register of the MMAU.

Returns
uint32_t unsigned square root.
Note
Quotient is stored in A0 register of the MMAU for next computation.
static void MMAU_slda_d ( register int64_t  dval)
inlinestatic

The MMAU_slda_d function loads A10 accumulator register of the MMAU by 64-bit integer value.

Parameters
dvalint64_t integer value.
static int64_t MMAU_d_smul_ll ( register int32_t  lval1,
register int32_t  lval2 
)
inlinestatic

The MMAU_d_smul_ll function multiplies two 32-bit integer values returning a 64-bit integer product.

Parameters
lval1int32_t integer value.
lval2int32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smul_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smul_dl function multiplies 64-bit integer value with 32-bit integer value returning a 64-bit integer product.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smuls_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smuls_dl function multiplies 64-bit integer value with 32-bit integer value returning saturated 64-bit integer product.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smula_l ( register int32_t  lval)
inlinestatic

The MMAU_d_smula_l function multiplies 32-bit integer value with 64-bit integer value stored in the A10 register of the MMAU returning a 64-bit integer product.

Parameters
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smulas_l ( register int32_t  lval)
inlinestatic

The MMAU_d_smulas_l function multiplies 32-bit integer value with 64-bit integer value stored in the A10 register of the MMAU returning saturated 64-bit integer product.

Parameters
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smac_ll ( register int32_t  lval1,
register int32_t  lval2 
)
inlinestatic

The MMAU_d_smac_ll function multiplies two 32-bit integer values and add product with value stored in the A10 register of the MMAU returning a 64-bit integer A10 register value.

Parameters
lval1int32_t integer value.
lval2int32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smacs_ll ( register int32_t  lval1,
register int32_t  lval2 
)
inlinestatic

The MMAU_d_smacs_ll function multiplies two 32-bit integer values and add product with value stored in the A10 register of the MMAU returning saturated 64-bit integer A10 register value.

Parameters
lval1int32_t integer value.
lval2int32_t integer value.
Returns
int64_t integer value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smac_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smac_dl function multiplies 64-bit integer value with 32-bit integer value and add product with value stored in the A10 register of the MMAU returning a 64-bit integer A10 register value.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smacs_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smacs_dl function multiplies 64-bit integer value with 32-bit integer value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit integer A10 register value.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static int64_t MMAU_d_smaca_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smaca_dl function multiplies 32-bit integer value by value stored in the A10 register of the MMAU and add product with 64-bit integer value returning a 64-bit integer A10 register value.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_smacas_dl ( register int64_t  dval,
register int32_t  lval 
)
inlinestatic

The MMAU_d_smacas_dl function multiplies 32-bit integer value by value stored in the A10 register of the MMAU and add product with 64-bit integer value returning saturated 64-bit integer A10 register value.

Parameters
dvalint64_t integer value.
lvalint32_t integer value.
Returns
int64_t integer value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static int32_t MMAU_l_sdiv_ll ( register int32_t  lnum,
register int32_t  lden 
)
inlinestatic

The MMAU_l_sdiv_ll function divides two 32-bit integer values returning a 32-bit integer quotient.

Parameters
lnumint32_t integer divisor value.
ldenint32_t integer dividend value.
Returns
int32_t integer quotient value.
Note
Quotient is stored in A0 register of the MMAU for next computation.
static int32_t MMAU_l_sdivs_ll ( register int32_t  lnum,
register int32_t  lden 
)
inlinestatic

The MMAU_l_sdivs_ll function divides two 32-bit integer values returning a 32-bit integer quotient.

Parameters
lnumint32_t integer divisor value.
ldenint32_t integer dividend value.
Returns
int32_t integer quotient value.
Note
Saturated quotient is stored in A0 register of the MMAU for next computation.
static int64_t MMAU_d_sdiv_dl ( register int64_t  dnum,
register int32_t  lden 
)
inlinestatic

The MMAU_d_sdiv_dl function divides 64-bit integer value by 32-bit integer value returning a 64-bit integer quotient.

Parameters
dnumint64_t integer divisor value.
ldenint32_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdivs_dl ( register int64_t  dnum,
register int32_t  lden 
)
inlinestatic

The MMAU_d_sdivs_dl function divides 64-bit integer value by 32-bit integer value returning a 64-bit integer quotient.

Parameters
dnumint64_t integer divisor value.
ldenint32_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdiv_dd ( register int64_t  dnum,
register int64_t  dden 
)
inlinestatic

The MMAU_d_sdiv_dd function divides two 64-bit integer values returning a 64-bit integer quotient.

Parameters
dnumint64_t integer divisor value.
ddenint64_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdivs_dd ( register int64_t  dnum,
register int64_t  dden 
)
inlinestatic

The MMAU_d_sdivs_dd function divides two 64-bit integer values returning a 64-bit integer quotient.

Parameters
dnumint64_t integer divisor value.
ddenint64_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdiva_l ( register int32_t  lden1)
inlinestatic

The MMAU_d_sdiva_l function divides 32-bit integer value stored in the A10 register of the MMAU by 32-bit integer value returning a 64-bit integer quotient.

Parameters
lden1int32_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdivas_l ( register int32_t  lden1)
inlinestatic

The MMAU_d_sdivas_l function divides 32-bit integer value stored in the A10 register of the MMAU by 32-bit integer value returning a saturated 64-bit integer quotient.

Parameters
lden1int32_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdiva_d ( register int64_t  dden1)
inlinestatic

The MMAU_d_sdiva_d function divides 64-bit integer value stored in the A10 register of the MMAU by 64-bit integer value returning a 64-bit integer quotient.

Parameters
dden1int64_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static int64_t MMAU_d_sdivas_d ( register int64_t  dden1)
inlinestatic

The MMAU_d_sdivas_d function divides 64-bit integer value stored in the A10 register of the MMAU by 64-bit integer value returning a saturated 64-bit integer quotient.

Parameters
dden1int64_t integer dividend value.
Returns
int64_t integer quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation.
static void MMAU_lda_d ( register frac64_t  dval)
inlinestatic

The MMAU_lda_d function loads A10 accumulator register of the MMAU by 64-bit fractional value.

Parameters
dvalfrac64_t fractional value.
static frac32_t MMAU_l_mul_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_l_mul_ll function multiplies two 32-bit fractional values returning a 32-bit fractional product.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_muls_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_l_muls_ll function multiplies two 32-bit fractional values returning saturated 32-bit fractional product.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_mul_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_d_mul_ll function multiplies two 32-bit fractional values returning a 64-bit fractional product.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_muls_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_d_muls_ll function multiplies two 32-bit fractional values returning saturated 64-bit fractional product.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac64_t MMAU_d_mul_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_mul_dl function multiplies 64-bit fractional value with 32-bit fractional value returning a 64-bit fractional product.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_muls_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_muls_dl function multiplies 64-bit fractional value with 32-bit fractional value returning saturated 64-bit fractional product.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac64_t MMAU_d_mula_l ( register frac32_t  lval)
inlinestatic

The MMAU_d_mula_l function multiplies 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning a 64-bit fractional product.

Parameters
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_mulas_l ( register frac32_t  lval)
inlinestatic

The MMAU_d_mulas_l function multiplies 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning saturated 64-bit fractional product.

Parameters
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac32_t MMAU_l_mul_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_mul_dl function multiplies 64-bit fractional value with 32-bit fractional value returning a 32-bit fractional product.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_muls_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_muls_dl function multiplies 64-bit fractional value with 32-bit fractional value returning saturated 32-bit fractional product.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_mula_l ( register frac32_t  lval)
inlinestatic

The MMAU_l_mula_l function multiplies 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning a 32-bit fractional product.

Parameters
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_mulas_l ( register frac32_t  lval)
inlinestatic

The MMAU_l_mulas_l function multiplies 32-bit fractional value with 64-bit fractional value stored in the A10 register of the MMAU returning saturated 32-bit fractional product.

Parameters
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_mac_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_d_mac_ll function multiplies two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 64-bit fractional A10 register value.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_macs_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_d_macs_ll function multiplies two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning saturated 64-bit fractional A10 register value.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac64_t MMAU_d_mac_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_mac_dl function multiplies 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning a 64-bit fractional A10 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_macs_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_macs_dl function multiplies 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning saturated 64-bit fractional A10 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac64_t MMAU_d_maca_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_maca_dl function multiplies 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a 64-bit fractional A10 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_macas_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_d_macas_dl function multiplies 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning saturated 64-bit fractional A10 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac64_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac32_t MMAU_l_mac_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_l_mac_ll function multiplies two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning a 32-bit fractional A1 register value.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_macs_ll ( register frac32_t  lval1,
register frac32_t  lval2 
)
inlinestatic

The MMAU_l_macs_ll function multiplies two 32-bit fractional values and add product with value stored in the A10 register of the MMAU returning saturated 32-bit fractional A1 register value.

Parameters
lval1frac32_t fractional value.
lval2frac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_mac_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_mac_dl function multiplies 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning a 32-bit fractional A1 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_macs_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_macs_dl function multiplies 64-bit fractional value with 32-bit fractional value and add product with value stored in the A10 register of the MMAU returning saturated 32-bit fractional A1 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_maca_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_maca_dl function multiplies 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning a 32-bit fractional A1 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_macas_dl ( register frac64_t  dval,
register frac32_t  lval 
)
inlinestatic

The MMAU_l_macas_dl function multiplies 32-bit fractional value by value stored in the A10 register of the MMAU and add product with 64-bit fractional value returning saturated 32-bit fractional A1 register value.

Parameters
dvalfrac64_t fractional value.
lvalfrac32_t fractional value.
Returns
frac32_t fractional value after multiply.
Note
Saturated product is stored in A10 register of the MMAU for next computation.
static frac32_t MMAU_l_div_ll ( register frac32_t  lnum,
register frac32_t  lden 
)
inlinestatic

The MMAU_l_div_ll function divides two 32-bit fractional values returning a 32-bit fractional quotient.

Parameters
lnumfrac32_t fractional divisor value.
ldenfrac32_t fractional dividend value.
Returns
frac32_t fractional quotient value.
Note
Quotient is stored in A1 register of the MMAU for next computation.
static frac32_t MMAU_l_divs_ll ( register frac32_t  lnum,
register frac32_t  lden 
)
inlinestatic

The MMAU_l_divs_ll function divides two 32-bit fractional values returning a 32-bit fractional quotient.

Parameters
lnumfrac32_t fractional divisor value.
ldenfrac32_t fractional dividend value.
Returns
frac32_t fractional quotient value.
Note
Saturated quotient is stored in A1 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac32_t MMAU_l_divas_l ( register frac32_t  lden)
inlinestatic

The MMAU_l_divas_l function divides 64-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a saturated 32-bit fractional quotient.

Parameters
ldenfrac32_t fractional dividend value.
Returns
frac32_t fractional quotient value.
Note
Saturated quotient is stored in A1 register of the MMAU for next computation.
static frac64_t MMAU_d_div_dl ( register frac64_t  dnum,
register frac32_t  lden 
)
inlinestatic

The MMAU_d_div_dl function divides 64-bit fractional value by 32-bit fractional value returning a 64-bit fractional quotient.

Parameters
dnumfrac64_t fractional divisor value.
ldenfrac32_t fractional dividend value.
Returns
frac64_t fractional quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_divs_dl ( register frac64_t  dnum,
register frac32_t  lden 
)
inlinestatic

The MMAU_d_divs_dl function divides 64-bit fractional value by 32-bit fractional value returning a 64-bit fractional quotient.

Parameters
dnumfrac64_t fractional divisor value.
ldenfrac32_t fractional dividend value.
Returns
frac64_t fractional quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac64_t MMAU_d_diva_l ( register frac32_t  lden1)
inlinestatic

The MMAU_d_diva_l function divides 32-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a 64-bit fractional quotient.

Parameters
lden1frac32_t fractional dividend value.
Returns
frac64_t fractional quotient value.
Note
Quotient is stored in A10 register of the MMAU for next computation.
static frac64_t MMAU_d_divas_l ( register frac32_t  lden1)
inlinestatic

The MMAU_d_divas_l function divides 32-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a saturated 64-bit fractional quotient.

Parameters
lden1frac32_t fractional dividend value.
Returns
frac64_t fractional quotient value.
Note
Saturated quotient is stored in A10 register of the MMAU for next computation. If saturation occurs, the instruction sets the accumulation overflow (Q) and multiply or divide overflow (V) flags to 1 in the CSR. Otherwise, it clears the Q and V flags.
static frac32_t MMAU_l_diva_l ( register frac32_t  lden)
inlinestatic

The MMAU_l_diva_l function divides 64-bit fractional value stored in the A10 register of the MMAU by 32-bit fractional value returning a 32-bit fractional quotient.

Parameters
ldenfrac32_t fractional dividend value.
Returns
frac32_t fractional quotient value.
Note
Quotient is stored in A1 register of the MMAU for next computation.
static frac32_t MMAU_l_sqr_l ( register frac32_t  lrad)
inlinestatic

The MMAU_l_sqr_l function computes and returns a 32-bit fractional square root of the 32-bit fractional radicand.

Parameters
lradfrac32_t fractional radicand.
Returns
frac32_t fractional square root.
Note
Square root is stored in A1 register of the MMAU for next computation.
static frac32_t MMAU_l_sqr_d ( register frac64_t  drad)
inlinestatic

The MMAU_l_sqr_d function computes and returns a 32-bit fractional square root of the 64-bit fractional radicand.

Parameters
dradfrac64_t fractional radicand.
Returns
frac32_t fractional square root.
Note
Quotient is stored in A1 register of the MMAU for next computation.
static frac32_t MMAU_l_sqra ( void  )
inlinestatic

The MMAU_l_sqra function computes and returns a 32-bit fractional square root of the radicand stored in the A10 register of the MMAU.

Returns
frac32_t fractional square root.
Note
Quotient is stored in A1 register of the MMAU for next computation.