MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Clock Driver

Overview

The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.

The clock driver supports:

The MCUXpresso SDK provides a peripheral clock driver for the SYSCON module of MCUXpresso SDK devices.

Function description

Clock driver provides these functions:

SYSCON Clock frequency functions

SYSCON clock module provides clocks, such as MCLKCLK, ADCCLK, DMICCLK, MCGFLLCLK, FXCOMCLK, WDTOSC, RTCOSC, USBCLK, and SYSPLL. The functions CLOCK_EnableClock() and CLOCK_DisableClock() enables and disables the various clocks. CLOCK_SetupFROClocking() initializes the FRO to 12 MHz, 48 MHz, or 96 MHz frequency. CLOCK_SetupPLLData(), CLOCK_SetupSystemPLLPrec(), and CLOCK_SetPLLFreq() functions are used to setup the PLL. The SYSCON clock driver provides functions to get the frequency of these clocks, such as CLOCK_GetFreq(), CLOCK_GetFro12MFreq(), CLOCK_GetExtClkFreq(), CLOCK_GetWdtOscFreq(), CLOCK_GetFroHfFreq(), CLOCK_GetPllOutFreq(), CLOCK_GetOsc32KFreq(), CLOCK_GetCoreSysClkFreq(), CLOCK_GetI2SMClkFreq(), CLOCK_GetFlexCommClkFreq, and CLOCK_GetAsyncApbClkFreq.

SYSCON clock Selection Muxes

The SYSCON clock driver provides the function to configure the clock selected. The function CLOCK_AttachClk() is implemented for this. The function selects the clock source for a particular peripheral like MAINCLK, DMIC, FLEXCOMM, USB, ADC, and PLL.

SYSCON clock dividers

The SYSCON clock module provides the function to setup the peripheral clock dividers. The function CLOCK_SetClkDiv() configures the CLKDIV registers for various periperals like USB, DMIC, I2S, SYSTICK, AHB, ADC, and also CLKOUT and TRACE functions.

SYSCON flash wait states

The SYSCON clock driver provides the function CLOCK_SetFLASHAccessCyclesForFreq() that configures FLASHCFG register with a selected FLASHTIM value.

Typical use case

POWER_DisablePD(kPDRUNCFG_PD_FRO_EN); /*!< Ensure FRO is on so that we can switch to its 12MHz mode temporarily 

Files

file  fsl_clock.h
 

Data Structures

struct  _clock_sys_pll
 PLL configuration structure. More...
 

Macros

#define ADC_CLOCKS
 Clock ip name array for ADC. More...
 
#define ACMP_CLOCKS
 Clock ip name array for ACMP. More...
 
#define SWM_CLOCKS
 Clock ip name array for SWM. More...
 
#define ROM_CLOCKS
 Clock ip name array for ROM. More...
 
#define SRAM_CLOCKS
 Clock ip name array for SRAM. More...
 
#define IOCON_CLOCKS
 Clock ip name array for IOCON. More...
 
#define GPIO_CLOCKS
 Clock ip name array for GPIO. More...
 
#define GPIO_INT_CLOCKS
 Clock ip name array for GPIO_INT. More...
 
#define DMA_CLOCKS
 Clock ip name array for DMA. More...
 
#define CRC_CLOCKS
 Clock ip name array for CRC. More...
 
#define WWDT_CLOCKS
 Clock ip name array for WWDT. More...
 
#define SCT_CLOCKS
 Clock ip name array for SCT0. More...
 
#define I2C_CLOCKS
 Clock ip name array for I2C. More...
 
#define USART_CLOCKS
 Clock ip name array for I2C. More...
 
#define SPI_CLOCKS
 Clock ip name array for SPI. More...
 
#define MTB_CLOCKS
 Clock ip name array for MTB. More...
 
#define MRT_CLOCKS
 Clock ip name array for MRT. More...
 
#define WKT_CLOCKS
 Clock ip name array for WKT. More...
 
#define CLK_GATE_DEFINE(reg, bit)   ((((reg)&0xFFU) << 8U) | ((bit)&0xFFU))
 Internal used Clock definition only. More...
 

Typedefs

typedef enum _clock_ip_name clock_ip_name_t
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
typedef enum _clock_name clock_name_t
 Clock name used to get clock frequency. More...
 
typedef enum _clock_select clock_select_t
 Clock Mux Switches CLK_MUX_DEFINE(reg, mux) reg is used to define the mux register mux is used to define the mux value. More...
 
typedef enum _clock_divider clock_divider_t
 Clock divider.
 
typedef enum _clock_wdt_analog_freq clock_wdt_analog_freq_t
 watch dog analog output frequency
 
typedef enum _clock_sys_pll_src clock_sys_pll_src
 PLL clock definition. More...
 
typedef enum _clock_main_clk_src clock_main_clk_src_t
 Main clock source definition.
 
typedef struct _clock_sys_pll clock_sys_pll_t
 PLL configuration structure.
 

Enumerations

enum  _clock_ip_name {
  kCLOCK_Sys = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 0U),
  kCLOCK_Rom = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 1U),
  kCLOCK_Ram0_1 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 2U),
  kCLOCK_Flashreg = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 3U),
  kCLOCK_Flash = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 4U),
  kCLOCK_I2c0 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 5U),
  kCLOCK_Gpio0 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 6U),
  kCLOCK_Swm = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 7U),
  kCLOCK_Sct = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 8U),
  kCLOCK_Wkt = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 9U),
  kCLOCK_Mrt = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 10U),
  kCLOCK_Spi0 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 11U),
  kCLOCK_Spi1 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 12U),
  kCLOCK_Crc = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 13U),
  kCLOCK_Uart0 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 14U),
  kCLOCK_Uart1 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 15U),
  kCLOCK_Uart2 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 16U),
  kCLOCK_Wwdt = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 17U),
  kCLOCK_Iocon = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 18U),
  kCLOCK_Acmp = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 19U),
  kCLOCK_I2c1 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 21U),
  kCLOCK_I2c2 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 22U),
  kCLOCK_I2c3 = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 23U),
  kCLOCK_Adc = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 24U),
  kCLOCK_Mtb = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 26U),
  kCLOCK_Dma = CLK_GATE_DEFINE(SYS_AHB_CLK_CTRL, 29U)
}
 Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More...
 
enum  _clock_name {
  kCLOCK_CoreSysClk,
  kCLOCK_MainClk,
  kCLOCK_SysOsc,
  kCLOCK_Irc,
  kCLOCK_ExtClk,
  kCLOCK_PllOut,
  kCLOCK_Pllin,
  kCLOCK_WdtOsc
}
 Clock name used to get clock frequency. More...
 
enum  _clock_select {
  kSYSPLL_From_Irc = CLK_MUX_DEFINE(SYSPLLCLKSEL, 0U),
  kSYSPLL_From_SysOsc = CLK_MUX_DEFINE(SYSPLLCLKSEL, 1U),
  kSYSPLL_From_ExtClk = CLK_MUX_DEFINE(SYSPLLCLKSEL, 3U),
  kMAINCLK_From_Irc = CLK_MUX_DEFINE(MAINCLKSEL, 0U),
  kMAINCLK_From_SysPllIn = CLK_MUX_DEFINE(MAINCLKSEL, 1U),
  kMAINCLK_From_WdtOsc = CLK_MUX_DEFINE(MAINCLKSEL, 2U),
  kMAINCLK_From_SysPll = CLK_MUX_DEFINE(MAINCLKSEL, 3U),
  kCLKOUT_From_Irc = CLK_MUX_DEFINE(CLKOUTSEL, 0U),
  kCLKOUT_From_SysOsc = CLK_MUX_DEFINE(CLKOUTSEL, 1U),
  kCLKOUT_From_WdtOsc = CLK_MUX_DEFINE(CLKOUTSEL, 2U),
  kCLKOUT_From_MainClk = CLK_MUX_DEFINE(CLKOUTSEL, 3U)
}
 Clock Mux Switches CLK_MUX_DEFINE(reg, mux) reg is used to define the mux register mux is used to define the mux value. More...
 
enum  _clock_divider {
  kCLOCK_DivUsartClk = CLK_DIV_DEFINE(UARTCLKDIV),
  kCLOCK_DivClkOut = CLK_DIV_DEFINE(CLKOUTDIV),
  kCLOCK_DivUartFrg = CLK_DIV_DEFINE(UARTFRGDIV),
  kCLOCK_IOCONCLKDiv6 = CLK_DIV_DEFINE(IOCONCLKDIV6),
  kCLOCK_IOCONCLKDiv5 = CLK_DIV_DEFINE(IOCONCLKDIV5),
  kCLOCK_IOCONCLKDiv4 = CLK_DIV_DEFINE(IOCONCLKDIV4),
  kCLOCK_IOCONCLKDiv3 = CLK_DIV_DEFINE(IOCONCLKDIV3),
  kCLOCK_IOCONCLKDiv2 = CLK_DIV_DEFINE(IOCONCLKDIV2),
  kCLOCK_IOCONCLKDiv1 = CLK_DIV_DEFINE(IOCONCLKDIV1),
  kCLOCK_IOCONCLKDiv0 = CLK_DIV_DEFINE(IOCONCLKDIV0)
}
 Clock divider. More...
 
enum  _clock_wdt_analog_freq {
  kCLOCK_WdtAnaFreq0HZ = CLK_WDT_OSC_DEFINE(0U, 0U),
  kCLOCK_WdtAnaFreq600KHZ = CLK_WDT_OSC_DEFINE(600000U, 1U),
  kCLOCK_WdtAnaFreq1050KHZ = CLK_WDT_OSC_DEFINE(1050000U, 2u),
  kCLOCK_WdtAnaFreq1400KHZ = CLK_WDT_OSC_DEFINE(1400000U, 3U),
  kCLOCK_WdtAnaFreq1750KHZ = CLK_WDT_OSC_DEFINE(1750000U, 4U),
  kCLOCK_WdtAnaFreq2100KHZ = CLK_WDT_OSC_DEFINE(2100000U, 5U),
  kCLOCK_WdtAnaFreq2400KHZ = CLK_WDT_OSC_DEFINE(2400000U, 6U),
  kCLOCK_WdtAnaFreq2700KHZ = CLK_WDT_OSC_DEFINE(2700000U, 7U),
  kCLOCK_WdtAnaFreq3000KHZ = CLK_WDT_OSC_DEFINE(3000000U, 8U),
  kCLOCK_WdtAnaFreq3250KHZ = CLK_WDT_OSC_DEFINE(3250000U, 9U),
  kCLOCK_WdtAnaFreq3500KHZ = CLK_WDT_OSC_DEFINE(3500000U, 10U),
  kCLOCK_WdtAnaFreq3750KHZ = CLK_WDT_OSC_DEFINE(3750000U, 11U),
  kCLOCK_WdtAnaFreq4000KHZ = CLK_WDT_OSC_DEFINE(4000000U, 12U),
  kCLOCK_WdtAnaFreq4200KHZ = CLK_WDT_OSC_DEFINE(4200000U, 13U),
  kCLOCK_WdtAnaFreq4400KHZ = CLK_WDT_OSC_DEFINE(4400000U, 14U),
  kCLOCK_WdtAnaFreq4600KHZ = CLK_WDT_OSC_DEFINE(4600000U, 15U)
}
 watch dog analog output frequency More...
 
enum  _clock_sys_pll_src {
  kCLOCK_SysPllSrcIrc = 0U,
  kCLOCK_SysPllSrcSysosc = 1U,
  kCLOCK_SysPllSrcExtClk = 3U
}
 PLL clock definition. More...
 
enum  _clock_main_clk_src {
  kCLOCK_MainClkSrcIrc = CLK_MAIN_CLK_MUX_DEFINE(0U, 0U),
  kCLOCK_MainClkSrcSysPllin = CLK_MAIN_CLK_MUX_DEFINE(1U, 0U),
  kCLOCK_MainClkSrcWdtOsc = CLK_MAIN_CLK_MUX_DEFINE(2U, 0U),
  kCLOCK_MainClkSrcSysPll = CLK_MAIN_CLK_MUX_DEFINE(3U, 0U)
}
 Main clock source definition. More...
 

Variables

volatile uint32_t g_Wdt_Osc_Freq
 watchdog oscilltor clock frequency. More...
 
volatile uint32_t g_Ext_Clk_Freq
 external clock frequency. More...
 

Driver version

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 4, 4))
 CLOCK driver version 2.4.4. More...
 

Clock gate, mux, and divider.

static void CLOCK_EnableClock (clock_ip_name_t clk)
 
static void CLOCK_DisableClock (clock_ip_name_t clk)
 
static void CLOCK_Select (clock_select_t sel)
 
static void CLOCK_SetClkDivider (clock_divider_t name, uint32_t value)
 
static uint32_t CLOCK_GetClkDivider (clock_divider_t name)
 
static void CLOCK_SetCoreSysClkDiv (uint32_t value)
 
void CLOCK_SetMainClkSrc (clock_main_clk_src_t src)
 Set main clock reference source. More...
 
static void CLOCK_SetFRGClkMul (uint32_t mul)
 

Get frequency

uint32_t CLOCK_GetMainClkFreq (void)
 Return Frequency of Main Clock. More...
 
static uint32_t CLOCK_GetCoreSysClkFreq (void)
 Return Frequency of core. More...
 
uint32_t CLOCK_GetClockOutClkFreq (void)
 Return Frequency of ClockOut. More...
 
uint32_t CLOCK_GetIrcFreq (void)
 Return Frequency of IRC. More...
 
uint32_t CLOCK_GetSysOscFreq (void)
 Return Frequency of SYSOSC. More...
 
uint32_t CLOCK_GetUartClkFreq (void)
 Get UART0 frequency. More...
 
uint32_t CLOCK_GetUart0ClkFreq (void)
 Get UART0 frequency. More...
 
uint32_t CLOCK_GetUart1ClkFreq (void)
 Get UART1 frequency. More...
 
uint32_t CLOCK_GetUart2ClkFreq (void)
 Get UART2 frequency. More...
 
uint32_t CLOCK_GetFreq (clock_name_t clockName)
 Return Frequency of selected clock. More...
 
uint32_t CLOCK_GetSystemPLLInClockRate (void)
 Return System PLL input clock rate. More...
 
static uint32_t CLOCK_GetSystemPLLFreq (void)
 Return Frequency of System PLL. More...
 
static uint32_t CLOCK_GetWdtOscFreq (void)
 Get watch dog OSC frequency. More...
 
static uint32_t CLOCK_GetExtClkFreq (void)
 Get external clock frequency. More...
 

PLL operations

void CLOCK_InitSystemPll (const clock_sys_pll_t *config)
 System PLL initialize. More...
 
static void CLOCK_DenitSystemPll (void)
 System PLL Deinitialize. More...
 

External/internal oscillator clock operations

void CLOCK_InitExtClkin (uint32_t clkInFreq)
 Init external CLK IN, select the CLKIN as the external clock source. More...
 
void CLOCK_InitSysOsc (uint32_t oscFreq)
 Init SYS OSC. More...
 
void CLOCK_InitXtalin (uint32_t xtalInFreq)
 XTALIN init function system oscillator is bypassed, sys_osc_clk is fed driectly from the XTALIN. More...
 
static void CLOCK_DeinitSysOsc (void)
 Deinit SYS OSC.
 
void CLOCK_InitWdtOsc (clock_wdt_analog_freq_t wdtOscFreq, uint32_t wdtOscDiv)
 Init watch dog OSC Any setting of the FREQSEL bits will yield a Fclkana value within 40% of the listed frequency value. More...
 
static void CLOCK_DeinitWdtOsc (void)
 Deinit watch dog OSC.
 
bool CLOCK_SetUARTFRGClkFreq (uint32_t freq)
 Set UARTFRG. More...
 
void CLOCK_UpdateClkOUTsrc (void)
 updates the clock source of the CLKOUT
 
static void CLOCK_SetUARTFRGMULT (uint32_t mul)
 Set UARTFRGMULT. More...
 

Data Structure Documentation

struct _clock_sys_pll

Data Fields

uint32_t targetFreq
 System pll fclk output frequency, the output frequency should be lower than 100MHZ.
 
clock_sys_pll_src src
 System pll clock source.
 

Macro Definition Documentation

#define FSL_CLOCK_DRIVER_VERSION   (MAKE_VERSION(2, 4, 4))
#define ADC_CLOCKS
Value:
{ \
}
Clock gate name: Adc.
Definition: fsl_clock.h:187
#define ACMP_CLOCKS
Value:
{ \
}
Clock gate name: Acmp.
Definition: fsl_clock.h:183
#define SWM_CLOCKS
Value:
{ \
}
Clock gate name: Swm.
Definition: fsl_clock.h:171
#define ROM_CLOCKS
Value:
{ \
}
Clock gate name: Rom.
Definition: fsl_clock.h:165
#define SRAM_CLOCKS
Value:
{ \
}
Clock gate name: Ram0_1.
Definition: fsl_clock.h:166
#define IOCON_CLOCKS
Value:
{ \
}
Clock gate name: Iocon.
Definition: fsl_clock.h:182
#define GPIO_CLOCKS
Value:
{ \
}
Clock gate name: Gpio0.
Definition: fsl_clock.h:170
#define GPIO_INT_CLOCKS
Value:
{ \
kCLOCK_GpioInt, \
}
#define DMA_CLOCKS
Value:
{ \
}
Clock gate name: Dma.
Definition: fsl_clock.h:189
#define CRC_CLOCKS
Value:
{ \
}
Clock gate name: Crc.
Definition: fsl_clock.h:177
#define WWDT_CLOCKS
Value:
{ \
}
Clock gate name: Wwdt.
Definition: fsl_clock.h:181
#define SCT_CLOCKS
Value:
{ \
}
Clock gate name: Sct.
Definition: fsl_clock.h:172
#define I2C_CLOCKS
Value:
{ \
}
Clock gate name: I2c1.
Definition: fsl_clock.h:184
Clock gate name: I2c3.
Definition: fsl_clock.h:186
Clock gate name: I2c2.
Definition: fsl_clock.h:185
Clock gate name: I2c0.
Definition: fsl_clock.h:169
#define USART_CLOCKS
Value:
{ \
}
Clock gate name: Uart0.
Definition: fsl_clock.h:178
Clock gate name: Uart1.
Definition: fsl_clock.h:179
Clock gate name: Uart2.
Definition: fsl_clock.h:180
#define SPI_CLOCKS
Value:
{ \
}
Clock gate name: Spi1.
Definition: fsl_clock.h:176
Clock gate name: Spi0.
Definition: fsl_clock.h:175
#define MTB_CLOCKS
Value:
{ \
}
Clock gate name: Mtb.
Definition: fsl_clock.h:188
#define MRT_CLOCKS
Value:
{ \
}
Clock gate name: Mrt.
Definition: fsl_clock.h:174
#define WKT_CLOCKS
Value:
{ \
}
Clock gate name: Wkt.
Definition: fsl_clock.h:173
#define CLK_GATE_DEFINE (   reg,
  bit 
)    ((((reg)&0xFFU) << 8U) | ((bit)&0xFFU))

Typedef Documentation

typedef enum _clock_name clock_name_t

Enumeration Type Documentation

Enumerator
kCLOCK_Sys 

Clock gate name: Sys.

kCLOCK_Rom 

Clock gate name: Rom.

kCLOCK_Ram0_1 

Clock gate name: Ram0_1.

kCLOCK_Flashreg 

Clock gate name: Flashreg.

kCLOCK_Flash 

Clock gate name: Flash.

kCLOCK_I2c0 

Clock gate name: I2c0.

kCLOCK_Gpio0 

Clock gate name: Gpio0.

kCLOCK_Swm 

Clock gate name: Swm.

kCLOCK_Sct 

Clock gate name: Sct.

kCLOCK_Wkt 

Clock gate name: Wkt.

kCLOCK_Mrt 

Clock gate name: Mrt.

kCLOCK_Spi0 

Clock gate name: Spi0.

kCLOCK_Spi1 

Clock gate name: Spi1.

kCLOCK_Crc 

Clock gate name: Crc.

kCLOCK_Uart0 

Clock gate name: Uart0.

kCLOCK_Uart1 

Clock gate name: Uart1.

kCLOCK_Uart2 

Clock gate name: Uart2.

kCLOCK_Wwdt 

Clock gate name: Wwdt.

kCLOCK_Iocon 

Clock gate name: Iocon.

kCLOCK_Acmp 

Clock gate name: Acmp.

kCLOCK_I2c1 

Clock gate name: I2c1.

kCLOCK_I2c2 

Clock gate name: I2c2.

kCLOCK_I2c3 

Clock gate name: I2c3.

kCLOCK_Adc 

Clock gate name: Adc.

kCLOCK_Mtb 

Clock gate name: Mtb.

kCLOCK_Dma 

Clock gate name: Dma.

Enumerator
kCLOCK_CoreSysClk 

Cpu/AHB/AHB matrix/Memories,etc.

kCLOCK_MainClk 

Main clock.

kCLOCK_SysOsc 

Crystal Oscillator.

kCLOCK_Irc 

IRC12M.

kCLOCK_ExtClk 

External Clock.

kCLOCK_PllOut 

PLL Output.

kCLOCK_Pllin 

PLL Input.

kCLOCK_WdtOsc 

Watchdog Oscillator.

Enumerator
kSYSPLL_From_Irc 

Mux SYSPLL from Irc.

kSYSPLL_From_SysOsc 

Mux SYSPLL from SysOsc.

kSYSPLL_From_ExtClk 

Mux SYSPLL from ExtClk.

kMAINCLK_From_Irc 

Mux MAINCLK from Irc.

kMAINCLK_From_SysPllIn 

Mux MAINCLK from SysPllIn.

kMAINCLK_From_WdtOsc 

Mux MAINCLK from WdtOsc.

kMAINCLK_From_SysPll 

Mux MAINCLK from SysPll.

kCLKOUT_From_Irc 

Mux CLKOUT from Irc.

kCLKOUT_From_SysOsc 

Mux CLKOUT from SysOsc.

kCLKOUT_From_WdtOsc 

Mux CLKOUT from WdtOsc.

kCLKOUT_From_MainClk 

Mux clock out from Main clock.

Enumerator
kCLOCK_DivUsartClk 

Usart Clock Divider.

kCLOCK_DivClkOut 

Clk Out Divider.

kCLOCK_DivUartFrg 

Uart Frg Divider.

kCLOCK_IOCONCLKDiv6 

IOCON Clock Div6 Divider.

kCLOCK_IOCONCLKDiv5 

IOCON Clock Div5 Divider.

kCLOCK_IOCONCLKDiv4 

IOCON Clock Div4 Divider.

kCLOCK_IOCONCLKDiv3 

IOCON Clock Div3 Divider.

kCLOCK_IOCONCLKDiv2 

IOCON Clock Div2 Divider.

kCLOCK_IOCONCLKDiv1 

IOCON Clock Div1 Divider.

kCLOCK_IOCONCLKDiv0 

IOCON Clock Div0 Divider.

Enumerator
kCLOCK_WdtAnaFreq0HZ 

Watch dog analog output frequency is 0HZ.

kCLOCK_WdtAnaFreq600KHZ 

Watch dog analog output frequency is 600KHZ.

kCLOCK_WdtAnaFreq1050KHZ 

Watch dog analog output frequency is 1050KHZ.

kCLOCK_WdtAnaFreq1400KHZ 

Watch dog analog output frequency is 1400KHZ.

kCLOCK_WdtAnaFreq1750KHZ 

Watch dog analog output frequency is 1750KHZ.

kCLOCK_WdtAnaFreq2100KHZ 

Watch dog analog output frequency is 2100KHZ.

kCLOCK_WdtAnaFreq2400KHZ 

Watch dog analog output frequency is 2400KHZ.

kCLOCK_WdtAnaFreq2700KHZ 

Watch dog analog output frequency is 2700KHZ.

kCLOCK_WdtAnaFreq3000KHZ 

Watch dog analog output frequency is 3000KHZ.

kCLOCK_WdtAnaFreq3250KHZ 

Watch dog analog output frequency is 3250KHZ.

kCLOCK_WdtAnaFreq3500KHZ 

Watch dog analog output frequency is 3500KHZ.

kCLOCK_WdtAnaFreq3750KHZ 

Watch dog analog output frequency is 3750KHZ.

kCLOCK_WdtAnaFreq4000KHZ 

Watch dog analog output frequency is 4000KHZ.

kCLOCK_WdtAnaFreq4200KHZ 

Watch dog analog output frequency is 4200KHZ.

kCLOCK_WdtAnaFreq4400KHZ 

Watch dog analog output frequency is 4400KHZ.

kCLOCK_WdtAnaFreq4600KHZ 

Watch dog analog output frequency is 4600KHZ.

Enumerator
kCLOCK_SysPllSrcIrc 

system pll source from FRO

kCLOCK_SysPllSrcSysosc 

system pll source from system osc

kCLOCK_SysPllSrcExtClk 

system pll source from ext clkin

Enumerator
kCLOCK_MainClkSrcIrc 

main clock source from FRO

kCLOCK_MainClkSrcSysPllin 

main clock source from pll input

kCLOCK_MainClkSrcWdtOsc 

main clock source from watchdog oscillator

kCLOCK_MainClkSrcSysPll 

main clock source from system pll

Function Documentation

void CLOCK_SetMainClkSrc ( clock_main_clk_src_t  src)
Parameters
srcRefer to clock_main_clk_src_t to set the main clock source.
uint32_t CLOCK_GetMainClkFreq ( void  )
Returns
Frequency of Main Clock.
static uint32_t CLOCK_GetCoreSysClkFreq ( void  )
inlinestatic
Returns
Frequency of core.
uint32_t CLOCK_GetClockOutClkFreq ( void  )
Returns
Frequency of ClockOut
uint32_t CLOCK_GetIrcFreq ( void  )
Returns
Frequency of IRC
uint32_t CLOCK_GetSysOscFreq ( void  )
Returns
Frequency of SYSOSC
uint32_t CLOCK_GetUartClkFreq ( void  )
Return values
UART0frequency value.
uint32_t CLOCK_GetUart0ClkFreq ( void  )
Return values
UART0frequency value.
uint32_t CLOCK_GetUart1ClkFreq ( void  )
Return values
UART1frequency value.
uint32_t CLOCK_GetUart2ClkFreq ( void  )
Return values
UART2frequency value.
uint32_t CLOCK_GetFreq ( clock_name_t  clockName)
Returns
Frequency of selected clock
uint32_t CLOCK_GetSystemPLLInClockRate ( void  )
Returns
System PLL input clock rate
static uint32_t CLOCK_GetSystemPLLFreq ( void  )
inlinestatic
Returns
Frequency of PLL
static uint32_t CLOCK_GetWdtOscFreq ( void  )
inlinestatic
Return values
watchdog OSC frequency value.
static uint32_t CLOCK_GetExtClkFreq ( void  )
inlinestatic
Return values
externalclock frequency value.
void CLOCK_InitSystemPll ( const clock_sys_pll_t *  config)
Parameters
configSystem PLL configurations.
static void CLOCK_DenitSystemPll ( void  )
inlinestatic
void CLOCK_InitExtClkin ( uint32_t  clkInFreq)
Parameters
clkInFreqexternal clock in frequency.
void CLOCK_InitSysOsc ( uint32_t  oscFreq)
Parameters
oscFreqoscillator frequency value.
void CLOCK_InitXtalin ( uint32_t  xtalInFreq)
Parameters
xtalInFreqXTALIN frequency value
Returns
Frequency of PLL
void CLOCK_InitWdtOsc ( clock_wdt_analog_freq_t  wdtOscFreq,
uint32_t  wdtOscDiv 
)

The watchdog oscillator is the clock source with the lowest power consumption. If accurate timing is required, use the FRO or system oscillator. The frequency of the watchdog oscillator is undefined after reset. The watchdog oscillator frequency must be programmed by writing to the WDTOSCCTRL register before using the watchdog oscillator. Watchdog osc output frequency = wdtOscFreq / wdtOscDiv, should in range 9.3KHZ to 2.3MHZ.

Parameters
wdtOscFreqwatch dog analog part output frequency, reference _wdt_analog_output_freq.
wdtOscDivwatch dog analog part output frequency divider, shoule be a value >= 2U and multiple of 2
bool CLOCK_SetUARTFRGClkFreq ( uint32_t  freq)
Deprecated:
Do not use this function. Refer to CLOCK_SetFRGClkMul().
Parameters
freqUART clock src.
static void CLOCK_SetUARTFRGMULT ( uint32_t  mul)
inlinestatic
Parameters
mulUARTFRGMULT.

Variable Documentation

volatile uint32_t g_Wdt_Osc_Freq

This variable is used to store the watchdog oscillator frequency which is set by CLOCK_InitWdtOsc, and it is returned by CLOCK_GetWdtOscFreq.

volatile uint32_t g_Ext_Clk_Freq

This variable is used to store the external clock frequency which is include external oscillator clock and external clk in clock frequency value, it is set by CLOCK_InitExtClkin when CLK IN is used as external clock or by CLOCK_InitSysOsc when external oscillator is used as external clock ,and it is returned by CLOCK_GetExtClkFreq.