![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The codec common driver provides a codec control abstraction interface.
Data Structures | |
| struct | _codec_config |
| Initialize structure of the codec. More... | |
| struct | _codec_capability |
| codec capability More... | |
| struct | _codec_handle |
| Codec handle definition. More... | |
Macros | |
| #define | CODEC_VOLUME_MAX_VALUE (100U) |
| codec maximum volume range | |
Typedefs | |
| typedef enum _codec_audio_protocol | codec_audio_protocol_t |
| AUDIO format definition. More... | |
| typedef enum _codec_module | codec_module_t |
| audio codec module | |
| typedef enum _codec_module_ctrl_cmd | codec_module_ctrl_cmd_t |
| audio codec module control cmd | |
| typedef struct _codec_handle | codec_handle_t |
| codec handle declaration | |
| typedef struct _codec_config | codec_config_t |
| Initialize structure of the codec. | |
| typedef struct _codec_capability | codec_capability_t |
| codec capability | |
Functions | |
| status_t | CODEC_Init (codec_handle_t *handle, codec_config_t *config) |
| Codec initilization. More... | |
| status_t | CODEC_Deinit (codec_handle_t *handle) |
| Codec de-initilization. More... | |
| status_t | CODEC_SetFormat (codec_handle_t *handle, uint32_t mclk, uint32_t sampleRate, uint32_t bitWidth) |
| set audio data format. More... | |
| status_t | CODEC_ModuleControl (codec_handle_t *handle, codec_module_ctrl_cmd_t cmd, uint32_t data) |
| codec module control. More... | |
| status_t | CODEC_SetVolume (codec_handle_t *handle, uint32_t channel, uint32_t volume) |
| set audio codec pl volume. More... | |
| status_t | CODEC_SetMute (codec_handle_t *handle, uint32_t channel, bool mute) |
| set audio codec module mute. More... | |
| status_t | CODEC_SetPower (codec_handle_t *handle, codec_module_t module, bool powerOn) |
| set audio codec power. More... | |
| status_t | CODEC_SetRecord (codec_handle_t *handle, uint32_t recordSource) |
| codec set record source. More... | |
| status_t | CODEC_SetRecordChannel (codec_handle_t *handle, uint32_t leftRecordChannel, uint32_t rightRecordChannel) |
| codec set record channel. More... | |
| status_t | CODEC_SetPlay (codec_handle_t *handle, uint32_t playSource) |
| codec set play source. More... | |
Driver version | |
| #define | FSL_CODEC_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| CLOCK driver version 2.3.1. More... | |
| struct _codec_config |
Data Fields | |
| uint32_t | codecDevType |
| codec type | |
| void * | codecDevConfig |
| Codec device specific configuration. | |
| struct _codec_capability |
Data Fields | |
| uint32_t | codecModuleCapability |
| codec module capability | |
| uint32_t | codecPlayCapability |
| codec play capability | |
| uint32_t | codecRecordCapability |
| codec record capability | |
| uint32_t | codecVolumeCapability |
| codec volume capability | |
| struct _codec_handle |
Data Fields | |
| codec_config_t * | codecConfig |
| codec configuration function pointer | |
| const codec_capability_t * | codecCapability |
| codec capability | |
| uint8_t | codecDevHandle [HAL_CODEC_HANDLER_SIZE] |
| codec device handle | |
| #define FSL_CODEC_DRIVER_VERSION (MAKE_VERSION(2, 3, 1)) |
| typedef enum _codec_audio_protocol codec_audio_protocol_t |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| enum _codec_module |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| status_t CODEC_Init | ( | codec_handle_t * | handle, |
| codec_config_t * | config | ||
| ) |
| handle | codec handle. |
| config | codec configurations. |
| status_t CODEC_Deinit | ( | codec_handle_t * | handle | ) |
| handle | codec handle. |
| status_t CODEC_SetFormat | ( | codec_handle_t * | handle, |
| uint32_t | mclk, | ||
| uint32_t | sampleRate, | ||
| uint32_t | bitWidth | ||
| ) |
| handle | codec handle. |
| mclk | master clock frequency in HZ. |
| sampleRate | sample rate in HZ. |
| bitWidth | bit width. |
| status_t CODEC_ModuleControl | ( | codec_handle_t * | handle, |
| codec_module_ctrl_cmd_t | cmd, | ||
| uint32_t | data | ||
| ) |
This function is used for codec module control, support switch digital interface cmd, can be expand to support codec module specific feature.
| handle | codec handle. |
| cmd | module control cmd, reference _codec_module_ctrl_cmd. |
| data | value to write, when cmd is kCODEC_ModuleRecordSourceChannel, the data should be a value combine of channel and source, please reference macro CODEC_MODULE_RECORD_SOURCE_CHANNEL(source, LP, LN, RP, RN), reference codec specific driver for detail configurations. |
| status_t CODEC_SetVolume | ( | codec_handle_t * | handle, |
| uint32_t | channel, | ||
| uint32_t | volume | ||
| ) |
| handle | codec handle. |
| channel | audio codec volume channel, can be a value or combine value of _codec_volume_capability or _codec_play_channel. |
| volume | volume value, support 0 ~ 100, 0 is mute, 100 is the maximum volume value. |
| status_t CODEC_SetMute | ( | codec_handle_t * | handle, |
| uint32_t | channel, | ||
| bool | mute | ||
| ) |
| handle | codec handle. |
| channel | audio codec volume channel, can be a value or combine value of _codec_volume_capability or _codec_play_channel. |
| mute | true is mute, false is unmute. |
| status_t CODEC_SetPower | ( | codec_handle_t * | handle, |
| codec_module_t | module, | ||
| bool | powerOn | ||
| ) |
| handle | codec handle. |
| module | audio codec module. |
| powerOn | true is power on, false is power down. |
| status_t CODEC_SetRecord | ( | codec_handle_t * | handle, |
| uint32_t | recordSource | ||
| ) |
| handle | codec handle. |
| recordSource | audio codec record source, can be a value or combine value of _codec_record_source. |
| status_t CODEC_SetRecordChannel | ( | codec_handle_t * | handle, |
| uint32_t | leftRecordChannel, | ||
| uint32_t | rightRecordChannel | ||
| ) |
| handle | codec handle. |
| leftRecordChannel | audio codec record channel, reference _codec_record_channel, can be a value combine of member in _codec_record_channel. |
| rightRecordChannel | audio codec record channel, reference _codec_record_channel, can be a value combine of member in _codec_record_channel. |
| status_t CODEC_SetPlay | ( | codec_handle_t * | handle, |
| uint32_t | playSource | ||
| ) |
| handle | codec handle. |
| playSource | audio codec play source, can be a value or combine value of _codec_play_source. |