![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _nboot_secure_counter |
| Data structure holding secure counter value used by nboot library. More... | |
| struct | _nboot_context |
| NBOOT context type. More... | |
| struct | _nboot_rot_auth_parms |
| NBOOT type for the root of trust parameters. More... | |
| struct | _nboot_sb3_load_manifest_parms |
| manifest loading parameters More... | |
| struct | _nboot_img_auth_ecdsa_parms |
| Data structure holding input arguments to POR secure boot (authentication) algorithm. More... | |
| struct | _nboot_cmac_authenticate_parms |
| Data structure holding input arguments for CMAC authentication. More... | |
Macros | |
| #define | NXPCLHASH_WA_SIZE_MAX (128U + 64U) |
| Define the max workarea size required for this component. | |
| #define | NXPCLCSS_HASH_RTF_OUTPUT_SIZE_HAL ((size_t)32U) |
| Size of RTF appendix to hash output buffer, in bytes. | |
| #define | kNBOOT_RootKeyUsage_DebugCA_ImageCA_FwCA_ImageKey_FwKey (0x0U) |
| NBOOT type for the root key usage. More... | |
| #define | kNBOOT_RootKey_Enabled (0xAAU) |
| NBOOT type for the root key revocation. More... | |
| #define | kNBOOT_RootKey_Ecdsa_P256 (0x0000FE01U) |
| NBOOT type specifying the elliptic curve to be used. More... | |
| #define | nboot_lc_nxpBlank (0xFFFF0000U) |
| Enumeration for SoC Lifecycle. More... | |
Typedefs | |
| typedef uint32_t | nboot_status_t |
| Type for nboot status codes. | |
| typedef uint64_t | nboot_status_protected_t |
| Type for nboot protected status codes. | |
|
typedef struct _nboot_secure_counter | nboot_secure_counter_t |
| Data structure holding secure counter value used by nboot library. | |
| typedef struct _nboot_context | nboot_context_t |
| NBOOT context type. More... | |
| typedef struct _nboot_rot_auth_parms | nboot_rot_auth_parms_t |
| NBOOT type for the root of trust parameters. More... | |
| typedef struct _nboot_sb3_load_manifest_parms | nboot_sb3_load_manifest_parms_t |
| manifest loading parameters More... | |
| typedef struct _nboot_img_auth_ecdsa_parms | nboot_img_auth_ecdsa_parms_t |
| Data structure holding input arguments to POR secure boot (authentication) algorithm. More... | |
|
typedef struct _nboot_cmac_authenticate_parms | nboot_img_authenticate_cmac_parms_t |
| Data structure holding input arguments for CMAC authentication. | |
| typedef enum _nboot_bool | nboot_bool_t |
| Boolean type for the NBOOT functions. More... | |
Enumerations | |
| enum | { kStatus_NBOOT_Success = 0x5A5A5A5AU, kStatus_NBOOT_Fail = 0x5A5AA5A5U, kStatus_NBOOT_InvalidArgument = 0x5A5AA5F0U, kStatus_NBOOT_RequestTimeout = 0x5A5AA5E1U, kStatus_NBOOT_KeyNotLoaded = 0x5A5AA5E2U, kStatus_NBOOT_AuthFail = 0x5A5AA5E4U, kStatus_NBOOT_OperationNotAvaialable = 0x5A5AA5E5U, kStatus_NBOOT_KeyNotAvailable = 0x5A5AA5E6U, kStatus_NBOOT_IvCounterOverflow = 0x5A5AA5E7U, kStatus_NBOOT_SelftestFail = 0x5A5AA5E8U, kStatus_NBOOT_InvalidDataFormat = 0x5A5AA5E9U, kStatus_NBOOT_IskCertUserDataTooBig, kStatus_NBOOT_IskCertSignatureOffsetTooSmall, kStatus_NBOOT_MemcpyFail = 0x5A5A845AU } |
| nboot status codes. More... | |
| enum | _nboot_bool { kNBOOT_TRUE = 0x3C5AC33CU, kNBOOT_TRUE256 = 0x3C5AC35AU, kNBOOT_TRUE384 = 0x3C5AC3A5U, kNBOOT_FALSE = 0x5AA55AA5U } |
| Boolean type for the NBOOT functions. More... | |
Functions | |
| status_t | NBOOT_GenerateRandom (uint8_t *output, size_t outputByteLen) |
| This API function is used to generate random number with specified length. More... | |
| nboot_status_t | NBOOT_ContextInit (nboot_context_t *context) |
| The function is used for initializing of the nboot context data structure. More... | |
| nboot_status_t | NBOOT_ContextDeinit (nboot_context_t *context) |
| The function is used to deinitialize nboot context data structure. More... | |
| nboot_status_protected_t | NBOOT_Sb3LoadManifest (nboot_context_t *context, uint32_t *manifest, nboot_sb3_load_manifest_parms_t *params) |
| Verify NBOOT SB3.1 manifest (header message) More... | |
| nboot_status_protected_t | NBOOT_Sb3LoadBlock (nboot_context_t *context, uint32_t *block) |
| Verify NBOOT SB3.1 block. More... | |
| nboot_status_protected_t | NBOOT_ImgAuthenticateEcdsa (nboot_context_t *context, uint8_t imageStartAddress[], nboot_bool_t *isSignatureVerified, nboot_img_auth_ecdsa_parms_t *parms) |
| This function authenticates image with asymmetric cryptography. More... | |
| nboot_status_protected_t | NBOOT_ImgAuthenticateCmac (nboot_context_t *context, uint8_t imageStartAddress[], nboot_bool_t *isSignatureVerified, nboot_img_authenticate_cmac_parms_t *parms) |
| This function calculates the CMAC over the given image and compares it to the expected value. More... | |
| struct _nboot_secure_counter |
| struct _nboot_context |
This type defines the NBOOT context
Data Fields | |
| uint32_t | totalBlocks |
| holds number of SB3 blocks. More... | |
| uint32_t | processData |
| flag, initialized by nboot_sb3_load_header(). More... | |
| uint32_t | timeout |
| timeout value for css operation. More... | |
| uint32_t | keyinfo [NBOOT_KEYINFO_WORDLEN] |
| data for NBOOT key management. More... | |
| uint32_t | context [NBOOT_CONTEXT_WORDLEN] |
| work area for NBOOT lib. More... | |
| uint32_t | uuid [4] |
| holds UUID value from NMPA | |
| uint32_t | prngReadyFlag |
| flag, used by nboot_rng_generate_lq_random() to determine whether CSS is ready to generate rnd number | |
| uint32_t | oemShareValidFlag |
| flag, used during TP to determine whether valid oemShare was set by nboot_tp_isp_gen_oem_master_share() | |
| uint32_t | oemShare [4] |
| buffer to store OEM_SHARE computed by nxpCLTrustProv_nboot_isp_gen_oem_master_share() | |
| nboot_secure_counter_t | secureCounter |
| Secure counter used by nboot. | |
| uint32_t _nboot_context::totalBlocks |
Initialized by nboot_sb3_load_header().
| uint32_t _nboot_context::processData |
SB3 related flag set by NBOOT in case the nboot_sb3_load_block() provides plain data to output buffer (for processing by ROM SB3 loader
| uint32_t _nboot_context::timeout |
In case it is 0, infinite wait is performed
| uint32_t _nboot_context::keyinfo[NBOOT_KEYINFO_WORDLEN] |
| uint32_t _nboot_context::context[NBOOT_CONTEXT_WORDLEN] |
| struct _nboot_rot_auth_parms |
This type defines the NBOOT root of trust parameters
Data Fields | |
| nboot_root_key_revocation_t | soc_rootKeyRevocation [NBOOT_ROOT_CERT_COUNT] |
| Provided by caller based on NVM information in CFPA: ROTKH_REVOKE. | |
| uint32_t | soc_imageKeyRevocation |
| Provided by caller based on NVM information in CFPA: IMAGE_KEY_REVOKE. | |
| uint32_t | soc_rkh [12] |
| Provided by caller based on NVM information in CMPA: ROTKH (hash of hashes) More... | |
| uint32_t | soc_numberOfRootKeys |
| unsigned int, between minimum = 1 and maximum = 4; | |
| nboot_root_key_usage_t | soc_rootKeyUsage [NBOOT_ROOT_CERT_COUNT] |
| CMPA. | |
| nboot_root_key_type_and_length_t | soc_rootKeyTypeAndLength |
| static selection between ECDSA P-256 or ECDSA P-384 based root keys | |
| uint32_t _nboot_rot_auth_parms::soc_rkh[12] |
In case of kNBOOT_RootKey_Ecdsa_P384, sock_rkh[0..11] are used In case of kNBOOT_RootKey_Ecdsa_P256, sock_rkh[0..7] are used
| struct _nboot_sb3_load_manifest_parms |
This type defines the NBOOT SB3.1 manifest loading parameters
Data Fields | |
| nboot_rot_auth_parms_t | soc_RoTNVM |
| trusted information originated from CFPA and NMPA | |
| uint32_t | soc_trustedFirmwareVersion |
| Provided by caller based on NVM information in CFPA: Secure_FW_Version. | |
| struct _nboot_img_auth_ecdsa_parms |
Shall be read from SoC trusted NVM or SoC fuses.
Data Fields | |
| nboot_rot_auth_parms_t | soc_RoTNVM |
| trusted information originated from CFPA and NMPA | |
| uint32_t | soc_trustedFirmwareVersion |
| Provided by caller based on NVM information in CFPA: Secure_FW_Version. | |
| struct _nboot_cmac_authenticate_parms |
Data Fields | |
| uint32_t | expectedMAC [4] |
| expected MAC result | |
| #define kNBOOT_RootKeyUsage_DebugCA_ImageCA_FwCA_ImageKey_FwKey (0x0U) |
This type defines the NBOOT root key usage; any other value means the root key is not valid (treat as if revoked).
| #define kNBOOT_RootKey_Enabled (0xAAU) |
This type defines the NBOOT root key revocation; any other value means the root key is revoked.
| #define kNBOOT_RootKey_Ecdsa_P256 (0x0000FE01U) |
This type defines the elliptic curve type and length
| #define nboot_lc_nxpBlank (0xFFFF0000U) |
| typedef struct _nboot_context nboot_context_t |
This type defines the NBOOT context
| typedef struct _nboot_rot_auth_parms nboot_rot_auth_parms_t |
This type defines the NBOOT root of trust parameters
| typedef struct _nboot_sb3_load_manifest_parms nboot_sb3_load_manifest_parms_t |
This type defines the NBOOT SB3.1 manifest loading parameters
| typedef struct _nboot_img_auth_ecdsa_parms nboot_img_auth_ecdsa_parms_t |
Shall be read from SoC trusted NVM or SoC fuses.
| typedef enum _nboot_bool nboot_bool_t |
This type defines boolean values used by NBOOT functions that are not easily disturbed by Fault Attacks
| anonymous enum |
| enum _nboot_bool |
This type defines boolean values used by NBOOT functions that are not easily disturbed by Fault Attacks
| status_t NBOOT_GenerateRandom | ( | uint8_t * | output, |
| size_t | outputByteLen | ||
| ) |
| output | Pointer to random number buffer |
| outputByteLen | length of generated random number in bytes. Length has to be in range <1, 2^16> |
| kStatus_NBOOT_InvalidArgument | Invalid input parameters (Input pointers points to NULL or length is invalid) |
| kStatus_NBOOT_Success | Operation successfully finished |
| kStatus_NBOOT_Fail | Error occured during operation |
| nboot_status_t NBOOT_ContextInit | ( | nboot_context_t * | context | ) |
It should be called prior to any other calls of nboot API.
| context | Pointer to nboot_context_t structure. |
| kStatus_NBOOT_Success | Operation successfully finished |
| kStatus_NBOOT_Fail | Error occured during operation |
| nboot_status_t NBOOT_ContextDeinit | ( | nboot_context_t * | context | ) |
Its contents are overwritten with random data so that any sensitive data does not remain in memory.
| context | Pointer to nboot_context_t structure. |
| kStatus_NBOOT_Success | Operation successfully finished |
| kStatus_NBOOT_Fail | Error occured during operation |
| nboot_status_protected_t NBOOT_Sb3LoadManifest | ( | nboot_context_t * | context, |
| uint32_t * | manifest, | ||
| nboot_sb3_load_manifest_parms_t * | params | ||
| ) |
This function verifies the NBOOT SB3.1 manifest (header message), initializes the context and loads keys into the CSS key store so that they can be used by nboot_sb3_load_block function. The NBOOT context has to be initialized by the function nboot_context_init before calling this function. Please note that this API is intended to be used only by users who needs to split FW update process (loading of SB3.1 file) to partial steps to customize whole operation. For regular SB3.1 processing, please use API described in chapter SBloader APIs.
| context | Pointer to nboot_context_t structure. |
| manifest | Pointer to the input manifest buffer |
| params | additional input parameters. Please refer to nboot_sb3_load_manifest_parms_t definition for details. |
| kStatus_NBOOT_Success | Operation successfully finished |
| kStatus_NBOOT_Fail | Error occured during operation |
| nboot_status_protected_t NBOOT_Sb3LoadBlock | ( | nboot_context_t * | context, |
| uint32_t * | block | ||
| ) |
This function verifies and decrypts an NBOOT SB3.1 block. Decryption is performed in-place. The NBOOT context has to be initialized by the function nboot_context_init before calling this function. Please note that this API is intended to be used only by users who needs to split FW update process (loading of SB3.1 file) to partial steps to customize whole operation. For regular SB3.1 processing, please use API described in chapter SBloader APIs.
| context | Pointer to nboot_context_t structure. |
| block | Pointer to the input SB3.1 data block |
| kStatus_NBOOT_Success | successfully finished |
| kStatus_NBOOT_Fail | occured during operation |
| nboot_status_protected_t NBOOT_ImgAuthenticateEcdsa | ( | nboot_context_t * | context, |
| uint8_t | imageStartAddress[], | ||
| nboot_bool_t * | isSignatureVerified, | ||
| nboot_img_auth_ecdsa_parms_t * | parms | ||
| ) |
The NBOOT context has to be initialized by the function nboot_context_init before calling this function.
| context | Pointer to nboot_context_t structure. |
| imageStartAddress | Pointer to start of the image in memory. |
| isSignatureVerified | Pointer to memory holding function call result. After the function returns, the value will be set to kNBOOT_TRUE when the image is authentic. Any other value means the authentication does not pass. |
| parms | Pointer to a data structure in trusted memory, holding input parameters for the algorithm. The data structure shall be correctly filled before the function call. |
| kStatus_NBOOT_Success | Operation successfully finished |
| kStatus_NBOOT_Fail | Returned in all other cases. Doesn't always mean invalid image, it could also mean transient error caused by short time environmental conditions. |
| nboot_status_protected_t NBOOT_ImgAuthenticateCmac | ( | nboot_context_t * | context, |
| uint8_t | imageStartAddress[], | ||
| nboot_bool_t * | isSignatureVerified, | ||
| nboot_img_authenticate_cmac_parms_t * | parms | ||
| ) |
To be more resistant against SPA, it is recommended that imageStartAddress is word aligned. The NBOOT context has to be initialized by the nboot_context_init() before calling this function.
| context | Pointer to nboot_context_t structure. |
| imageStartAddress | Pointer to start of the image in memory. |
| isSignatureVerified | Pointer to memory holding function call result. After the function returns, the value will be set to |
| parms | Pointer to a data structure in trusted memory, holding the reference MAC. The data structure shall be correctly filled before the function call. |
| kStatus_NBOOT_Success | |
| kStatus_NBOOT_Fail |