MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
INPUTMUX: Input Multiplexing Driver

Overview

The MCUXpresso SDK provides a driver for the Input multiplexing (INPUTMUX).
It configures the inputs to the pin interrupt block, DMA trigger, and frequency measure function. Once configured, the clock is not needed for the inputmux.

Input Multiplexing Driver operation

INPUTMUX_AttachSignal function configures the specified input

Typical use case

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/inputmux

Files

file  fsl_inputmux.h
 
file  fsl_inputmux_connections.h
 

Functions

void INPUTMUX_Init (INPUTMUX_Type *base)
 Initialize INPUTMUX peripheral. More...
 
void INPUTMUX_AttachSignal (INPUTMUX_Type *base, uint32_t index, inputmux_connection_t connection)
 Attaches a signal. More...
 
void INPUTMUX_EnableSignal (INPUTMUX_Type *base, inputmux_signal_t signal, bool enable)
 Enable/disable a signal. More...
 
void INPUTMUX_Deinit (INPUTMUX_Type *base)
 Deinitialize INPUTMUX peripheral. More...
 

Input multiplexing connections

enum  _inputmux_connection_t {
  kINPUTMUX_SctGpioInAToSct0 = 0U + (SCT0_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToSct0 = 58U + (SCT0_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer0Captsel = 48U + (TIMER0CAPTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer0Trigger = 48U + (TIMER0TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer1Captsel = 48U + (TIMER1CAPTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer1Trigger = 48U + (TIMER1TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer2Captsel = 48U + (TIMER2CAPTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer2Trigger = 48U + (TIMER2TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_GpioPort1Pin31ToPintsel = 63U + (PINTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToDma0 = 52U + (DMA0_ITRIG_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutTrigoutToTriginChannels = 52U + (DMA0_OTRIG_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_Aoi1Out2ToFreqmeasRef = 9u + (FREQMEAS_REF_REG << PMUX_SHIFT) ,
  kINPUTMUX_Aoi1Out2ToFreqmeasTarget = 9u + (FREQMEAS_TARGET_REG << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer3Captsel = 48U + (TIMER3CAPTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer3Trigger = 48U + (TIMER3TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToTimer4Captsel = 48U + (TIMER4CAPTSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_GpioPort0Pin31ToPintSecsel = 31U + (PINTSECSEL0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToDma1 = 24U + (DMA1_ITRIG_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma1I3c0TxTrigoutToTriginChannels = 13U + (DMA1_OTRIG_INMUX0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToHscmp0Trigger = 37U + (HSCMP0_TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToAdc0Trigger = 52U + (ADC0_TRIG0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToAdc1Trigger = 52U + (ADC1_TRIG0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToDac0Trigger = 28U + (DAC0_TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToDac1Trigger = 28U + (DAC1_TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToDac2Trigger = 28U + (DAC2_TRIGIN << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc0Trigger = 54U + (ENC0TRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc0Home = 54U + (ENC0HOME << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc0Index = 54U + (ENC0INDEX << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc0Phaseb = 54U + (ENC0PHASEB << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc0Phasea = 54U + (ENC0PHASEA << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc1Trigger = 54U + (ENC1TRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc1Home = 54U + (ENC1HOME << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc1Index = 54U + (ENC1INDEX << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc1Phaseb = 54U + (ENC1PHASEB << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToEnc1Phasea = 54U + (ENC1PHASEA << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm0ExtSyncTrigger = 54U + (PWM0_EXTSYNC0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm0ExtATrigger = 54U + (PWM0_EXTA0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm0ExtForceTrigger = 54U + (PWM0_EXTFORCETRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm0FaultTrigger = 54U + (PWM0_FAULT0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm0ExtClkTrigger = 54U + (PWM0_EXTCLKTRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm1ExtSyncTrigger = 54U + (PWM1_EXTSYNC0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm1ExtATrigger = 54U + (PWM1_EXTA0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm1ExtForceTrigger = 54U + (PWM1_EXTFORCETRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm1FaultTrigger = 54U + (PWM1_FAULT0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToPwm1ExtClkTrigger = 54U + (PWM1_EXTCLKTRIG << PMUX_SHIFT) ,
  kINPUTMUX_Dma1Trigout2ToAoi0InTrigger = 60U + (AOI0_IN0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma1Trigout2ToAoi1InTrigger = 60U + (AOI1_IN0 << PMUX_SHIFT) ,
  kINPUTMUX_TmprOutToAoiExtTrigger = 24U + (AOI_EXT_TRIG0 << PMUX_SHIFT) ,
  kINPUTMUX_Dma0Trigout2ToHscmp1Trigger = 37U + (HSCMP1_TRIGIN << PMUX_SHIFT)
}
 INPUTMUX connections type. More...
 
enum  _inputmux_signal_t {
  kINPUTMUX_FlexSpiRxToDmac0Ch0RequestEna = 0U + (DMA0_REQ_EN0_ID << ENA_SHIFT) ,
  kINPUTMUX_Aoi0Out3ToDmac0Ch31RequestEna = 31U + (DMA0_REQ_EN0_ID << ENA_SHIFT) ,
  kINPUTMUX_TmprOutToDmac0Ch52RequestEna = 20U + (DMA0_REQ_EN1_ID << ENA_SHIFT) ,
  kINPUTMUX_I3c0TxToDmac1Ch13RequestEna = 13U + (DMA1_REQ_EN_ID << ENA_SHIFT) ,
  kINPUTMUX_Dmac0InputTriggerAoi0Out3Ena = 31U + (DMA0_ITRIG_EN0_ID << ENA_SHIFT) ,
  kINPUTMUX_Dmac0InputTriggerTmprOutEna = 20U + (DMA0_ITRIG_EN1_ID << ENA_SHIFT)
}
 INPUTMUX signal enable/disable type. More...
 
typedef enum _inputmux_connection_t inputmux_connection_t
 INPUTMUX connections type.
 
typedef enum _inputmux_signal_t inputmux_signal_t
 INPUTMUX signal enable/disable type.
 
#define SCT0_INMUX0   0x00U
 Periphinmux IDs.
 
#define TIMER0CAPTSEL0   0x20U
 
#define TIMER0TRIGIN   0x30U
 
#define TIMER1CAPTSEL0   0x40U
 
#define TIMER1TRIGIN   0x50U
 
#define TIMER2CAPTSEL0   0x60U
 
#define TIMER2TRIGIN   0x70U
 
#define PINTSEL_PMUX_ID   0xC0U
 
#define PINTSEL0   0xC0U
 
#define DMA0_ITRIG_INMUX0   0xE0U
 
#define DMA0_OTRIG_INMUX0   0x160U
 
#define FREQMEAS_REF_REG   0x180U
 
#define FREQMEAS_TARGET_REG   0x184U
 
#define TIMER3CAPTSEL0   0x1A0U
 
#define TIMER3TRIGIN   0x1B0U
 
#define TIMER4CAPTSEL0   0x1C0U
 
#define TIMER4TRIGIN   0x1D0U
 
#define PINTSECSEL0   0x1E0U
 
#define DMA1_ITRIG_INMUX0   0x200U
 
#define DMA1_OTRIG_INMUX0   0x240U
 
#define HSCMP0_TRIGIN   0x260U
 
#define ADC0_TRIG0   0x280U
 
#define ADC1_TRIG0   0x2C0U
 
#define DAC0_TRIGIN   0x300U
 
#define DAC1_TRIGIN   0x320U
 
#define DAC2_TRIGIN   0x340U
 
#define ENC0TRIG   0x360U
 
#define ENC0HOME   0x364U
 
#define ENC0INDEX   0x368U
 
#define ENC0PHASEB   0x36CU
 
#define ENC0PHASEA   0x370U
 
#define ENC1TRIG   0x380U
 
#define ENC1HOME   0x384U
 
#define ENC1INDEX   0x388U
 
#define ENC1PHASEB   0x38CU
 
#define ENC1PHASEA   0x390U
 
#define PWM0_EXTSYNC0   0x3A0U
 
#define PWM0_EXTA0   0x3B0U
 
#define PWM0_EXTFORCETRIG   0x3C0U
 
#define PWM0_FAULT0   0x3C4U
 
#define PWM1_EXTSYNC0   0x3E0U
 
#define PWM1_EXTA0   0x3F0U
 
#define PWM1_EXTFORCETRIG   0x400U
 
#define PWM1_FAULT0   0x404U
 
#define PWM0_EXTCLKTRIG   0x420U
 
#define PWM1_EXTCLKTRIG   0x424U
 
#define AOI0_IN0   0x440U
 
#define AOI1_IN0   0x480U
 
#define AOI_EXT_TRIG0   0x4C0U
 
#define HSCMP1_TRIGIN   0x4E0U
 
#define HSCMP2_TRIGIN   0x500U
 
#define DMA0_ITRIG_INMUX_32   0x520U
 
#define DMA0_REQ_EN0_ID   0x740U
 
#define DMA0_REQ_EN1_ID   0x744U
 
#define DMA1_REQ_EN_ID   0x760U
 
#define DMA0_ITRIG_EN0_ID   0x780U
 
#define DMA0_ITRIG_EN1_ID   0x784U
 
#define DMA1_ITRIG_EN_ID   0x7A0U
 
#define ENA_SHIFT   8U
 
#define PMUX_SHIFT   20U
 

Driver version

#define FSL_INPUTMUX_DRIVER_VERSION   (MAKE_VERSION(2, 0, 7))
 Group interrupt driver version for SDK.
 

Enumeration Type Documentation

Enumerator
kINPUTMUX_SctGpioInAToSct0 

SCT0 INMUX.

kINPUTMUX_TmprOutToSct0 

TIMER0 CAPTSEL.

kINPUTMUX_TmprOutToTimer0Captsel 

TIMER0 Trigger.

kINPUTMUX_TmprOutToTimer0Trigger 

TIMER1 CAPTSEL.

kINPUTMUX_TmprOutToTimer1Captsel 

TIMER1 Trigger.

kINPUTMUX_TmprOutToTimer1Trigger 

TIMER2 CAPTSEL.

kINPUTMUX_TmprOutToTimer2Captsel 

TIMER2 Trigger.

kINPUTMUX_TmprOutToTimer2Trigger 

Pin interrupt select.

kINPUTMUX_GpioPort1Pin31ToPintsel 

DMA0 Input trigger.

kINPUTMUX_TmprOutToDma0 

DMA0 output trigger.

kINPUTMUX_TmprOutTrigoutToTriginChannels 

Selection for frequency measurement reference clock.

kINPUTMUX_Aoi1Out2ToFreqmeasRef 

Selection for frequency measurement target clock.

kINPUTMUX_Aoi1Out2ToFreqmeasTarget 

TIMER3 CAPTSEL.

kINPUTMUX_TmprOutToTimer3Captsel 

TIMER3 Trigger.

kINPUTMUX_TmprOutToTimer3Trigger 

Timer4 CAPTSEL.

kINPUTMUX_TmprOutToTimer4Captsel 

TIMER4 Trigger.

kINPUTMUX_GpioPort0Pin31ToPintSecsel 

DMA1 Input trigger.

kINPUTMUX_TmprOutToDma1 

DMA1 output trigger.

kINPUTMUX_Dma1I3c0TxTrigoutToTriginChannels 

HSCMP0 trigger.

kINPUTMUX_Dma0Trigout2ToHscmp0Trigger 

ADC0 trigger.

kINPUTMUX_Dma0Trigout2ToAdc0Trigger 

ADC1 trigger.

kINPUTMUX_Dma0Trigout2ToAdc1Trigger 

DAC0 trigger.

kINPUTMUX_Dma0Trigout2ToDac0Trigger 

DAC1 trigger.

kINPUTMUX_Dma0Trigout2ToDac1Trigger 

DAC2 trigger.

kINPUTMUX_Dma0Trigout2ToDac2Trigger 

ENC0 TRIG.

kINPUTMUX_Dma0Trigout2ToEnc0Trigger 

ENC0 HOME.

kINPUTMUX_Dma0Trigout2ToEnc0Home 

ENC0 INDEX.

kINPUTMUX_Dma0Trigout2ToEnc0Index 

ENC0 PHASEB.

kINPUTMUX_Dma0Trigout2ToEnc0Phaseb 

ENC0 PHASEA.

kINPUTMUX_Dma0Trigout2ToEnc0Phasea 

ENC1 TRIG.

kINPUTMUX_Dma0Trigout2ToEnc1Trigger 

ENC1 HOME.

kINPUTMUX_Dma0Trigout2ToEnc1Home 

ENC1 INDEX.

kINPUTMUX_Dma0Trigout2ToEnc1Index 

ENC1 PHASEB.

kINPUTMUX_Dma0Trigout2ToEnc1Phaseb 

ENC1 PHASEA.

kINPUTMUX_Dma0Trigout2ToEnc1Phasea 

PWM0 external synchronization trigger.

kINPUTMUX_Dma0Trigout2ToPwm0ExtSyncTrigger 

PWM0 input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm0ExtATrigger 

PWM0 external force trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm0ExtForceTrigger 

PWM0 fault input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm0FaultTrigger 

PWM0 extclk input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm0ExtClkTrigger 

PWM1 external synchronization trigger.

kINPUTMUX_Dma0Trigout2ToPwm1ExtSyncTrigger 

PWM1 input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm1ExtATrigger 

PWM1 external force trigger connections.

kINPUTMUX_Dma0Trigout2ToPwm1ExtForceTrigger 

PWM1 fault input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm1FaultTrigger 

PWM1 extclk input trigger connections trigger.

kINPUTMUX_Dma0Trigout2ToPwm1ExtClkTrigger 

AOI0 trigger.

kINPUTMUX_Dma1Trigout2ToAoi0InTrigger 

AOI1 trigger.

kINPUTMUX_Dma1Trigout2ToAoi1InTrigger 

AOI External trigger.

kINPUTMUX_TmprOutToAoiExtTrigger 

HSCMP1 trigger.

kINPUTMUX_Dma0Trigout2ToHscmp1Trigger 

HSCMP2 trigger.

Enumerator
kINPUTMUX_FlexSpiRxToDmac0Ch0RequestEna 

DMA0 REQ(DMA0_REQEN0) signal.

kINPUTMUX_Aoi0Out3ToDmac0Ch31RequestEna 

DMA0 REQ(DMA0_REQEN0) signal.

kINPUTMUX_TmprOutToDmac0Ch52RequestEna 

DMA1 REQ(DMA1_REQEN) signal.

kINPUTMUX_I3c0TxToDmac1Ch13RequestEna 

DMA0 input trigger(DMA0_ITRIGEN0) source enable.

kINPUTMUX_Dmac0InputTriggerAoi0Out3Ena 

DMA0 input trigger(DMA0_ITRIGEN1) source enable.

kINPUTMUX_Dmac0InputTriggerTmprOutEna 

DMA1 input trigger(DMA1_ITRIGEN) source enable.

Function Documentation

void INPUTMUX_Init ( INPUTMUX_Type *  base)

This function enables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.
void INPUTMUX_AttachSignal ( INPUTMUX_Type *  base,
uint32_t  index,
inputmux_connection_t  connection 
)

This function attaches multiplexed signals from INPUTMUX to target signals. For example, to attach GPIO PORT0 Pin 5 to PINT peripheral, do the following:

* INPUTMUX_AttachSignal(INPUTMUX, 2, kINPUTMUX_GpioPort0Pin5ToPintsel);
*

In this example, INTMUX has 8 registers for PINT, PINT_SEL0~PINT_SEL7. With parameter index specified as 2, this function configures register PINT_SEL2.

Parameters
baseBase address of the INPUTMUX peripheral.
indexThe serial number of destination register in the group of INPUTMUX registers with same name.
connectionApplies signal from source signals collection to target signal.
Return values
None.
void INPUTMUX_EnableSignal ( INPUTMUX_Type *  base,
inputmux_signal_t  signal,
bool  enable 
)

This function gates the INPUTPMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
signalEnable signal register id and bit offset.
enableSelects enable or disable.
Return values
None.
void INPUTMUX_Deinit ( INPUTMUX_Type *  base)

This function disables the INPUTMUX clock.

Parameters
baseBase address of the INPUTMUX peripheral.
Return values
None.