The MCUXpresso SDK provides a driver for the In Application Programming (IAP). 
It provides a set of functions to call the on-chip in application programming interface. User code executing from on-chip RAM can call these function to read information like part id, read and write flash, read and write ffr. 
In Application Programming operation
FLASH_Init() Initializes the global flash properties structure members
FLASH_Erase() Erases the flash sectors encompassed by parameters passed into function
FLASH_Program() Programs flash with data at locations passed in through parameters
FLASH_VerifyErase() Verifies an erasure of the desired flash area hase been erased
FLASH_VerifyProgram() Verifies programming of the desired flash area hase been programed
FLASH_GetProperty() Returns the desired flash property.
FFR_Init() Generic APIs for FFR
FFR_Deinit() Generic APIs for FFR
FFR_CustomerPagesInit() APIs to access CFPA pages
FFR_InfieldPageWrite() APIs to access CFPA pages
FFR_GetCustomerInfieldData() APIs to access CMPA pages
FFR_GetCustomerData() Read data stored in 'Customer Factory CFG Page'
FFR_KeystoreWrite() Read data stored in 'Customer Factory CFG Page'
FFR_KeystoreGetAC() Read data stored in 'Customer Factory CFG Page'
FFR_KeystoreGetKC() Read data stored in 'Customer Factory CFG Page'
FFR_GetUUID() Read data stored in 'NXP Manufacuring Programmed CFG Page'
FFR_GetManufactureData() Read data stored in 'NXP Manufacuring Programmed CFG Page'
kb_init() Initialize ROM API for a given operation
kb_deinit() Cleans up the ROM API context
kb_execute() Perform the operation configured during init
skboot_authenticate() Authenticate entry function with ARENA allocator init
HASH_IRQHandler() Interface for image authentication API
kb_init() Initialize ROM API for a given operation
kb_deinit() Cleans up the ROM API context
kb_execute() Perform the operation configured during init
skboot_authenticate() Authenticate entry function with ARENA allocator init
HASH_IRQHandler() Interface for image authentication API
Typical use case
IAP Basic Operations
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/iap1 
 | 
| enum   | flash_property_tag_t {  
  kFLASH_PropertyPflashSectorSize = 0x00U, 
 
  kFLASH_PropertyPflashTotalSize = 0x01U, 
 
  kFLASH_PropertyPflashBlockSize = 0x02U, 
 
  kFLASH_PropertyPflashBlockCount = 0x03U, 
 
  kFLASH_PropertyPflashBlockBaseAddr = 0x04U, 
 
  kFLASH_PropertyPflashPageSize = 0x30U, 
 
  kFLASH_PropertyPflashSystemFreq = 0x31U, 
 
  kFLASH_PropertyFfrSectorSize = 0x40U, 
 
  kFLASH_PropertyFfrTotalSize = 0x41U, 
 
  kFLASH_PropertyFfrBlockBaseAddr = 0x42U, 
 
  kFLASH_PropertyFfrPageSize = 0x43U
 
 } | 
|   | Enumeration for various flash properties.  More...
  | 
|   | 
| enum   | _flash_max_erase_page_value { kFLASH_MaxPagesToErase = 100U
 } | 
|   | Enumeration for flash max pages to erase.  More...
  | 
|   | 
| enum   | _flash_alignment_property {  
  kFLASH_AlignementUnitVerifyErase = 4, 
 
  kFLASH_AlignementUnitProgram = 512, 
 
  kFLASH_AlignementUnitSingleWordRead = 16
 
 } | 
|   | Enumeration for flash alignment property.  More...
  | 
|   | 
| enum   | _flash_read_ecc_option { , kFLASH_ReadWithEccOff = 1
 } | 
|   | Enumeration for flash read ecc option.  More...
  | 
|   | 
| enum   | _flash_read_margin_option {  
  kFLASH_ReadMarginNormal = 0, 
 
  kFLASH_ReadMarginVsProgram = 1, 
 
  kFLASH_ReadMarginVsErase = 2, 
 
  kFLASH_ReadMarginIllegalBitCombination = 3
 
 } | 
|   | Enumeration for flash read margin option.  More...
  | 
|   | 
| enum   | _flash_read_dmacc_option {  
  kFLASH_ReadDmaccDisabled = 0, 
 
  kFLASH_ReadDmaccEnabled = 1
 
 } | 
|   | Enumeration for flash read dmacc option.  More...
  | 
|   | 
| enum   | _flash_ramp_control_option {  
  kFLASH_RampControlDivisionFactorReserved = 0, 
 
  kFLASH_RampControlDivisionFactor256 = 1, 
 
  kFLASH_RampControlDivisionFactor128 = 2, 
 
  kFLASH_RampControlDivisionFactor64 = 3
 
 } | 
|   | Enumeration for flash ramp control option.  More...
  | 
|   | 
 | 
| enum   | _flash_status {  
  kStatus_FLASH_Success = MAKE_STATUS(kStatusGroupGeneric, 0), 
 
  kStatus_FLASH_InvalidArgument = MAKE_STATUS(kStatusGroupGeneric, 4), 
 
  kStatus_FLASH_SizeError = MAKE_STATUS(kStatusGroupFlashDriver, 0), 
 
  kStatus_FLASH_AlignmentError, 
 
  kStatus_FLASH_AddressError = MAKE_STATUS(kStatusGroupFlashDriver, 2), 
 
  kStatus_FLASH_AccessError, 
 
  kStatus_FLASH_ProtectionViolation, 
 
  kStatus_FLASH_CommandFailure, 
 
  kStatus_FLASH_UnknownProperty = MAKE_STATUS(kStatusGroupFlashDriver, 6), 
 
  kStatus_FLASH_EraseKeyError = MAKE_STATUS(kStatusGroupFlashDriver, 7), 
 
  kStatus_FLASH_RegionExecuteOnly, 
 
  kStatus_FLASH_ExecuteInRamFunctionNotReady, 
 
  kStatus_FLASH_CommandNotSupported = MAKE_STATUS(kStatusGroupFlashDriver, 11), 
 
  kStatus_FLASH_ReadOnlyProperty = MAKE_STATUS(kStatusGroupFlashDriver, 12), 
 
  kStatus_FLASH_InvalidPropertyValue, 
 
  kStatus_FLASH_InvalidSpeculationOption, 
 
  kStatus_FLASH_EccError, 
 
  kStatus_FLASH_CompareError, 
 
  kStatus_FLASH_RegulationLoss = MAKE_STATUS(kStatusGroupFlashDriver, 0x12), 
 
  kStatus_FLASH_InvalidWaitStateCycles, 
 
  kStatus_FLASH_OutOfDateCfpaPage, 
 
  kStatus_FLASH_BlankIfrPageData = MAKE_STATUS(kStatusGroupFlashDriver, 0x21), 
 
  kStatus_FLASH_EncryptedRegionsEraseNotDoneAtOnce, 
 
  kStatus_FLASH_ProgramVerificationNotAllowed, 
 
  kStatus_FLASH_HashCheckError, 
 
  kStatus_FLASH_SealedFfrRegion = MAKE_STATUS(kStatusGroupFlashDriver, 0x25), 
 
  kStatus_FLASH_FfrRegionWriteBroken, 
 
  kStatus_FLASH_NmpaAccessNotAllowed, 
 
  kStatus_FLASH_CmpaCfgDirectEraseNotAllowed, 
 
  kStatus_FLASH_FfrBankIsLocked = MAKE_STATUS(kStatusGroupFlashDriver, 0x29), 
 
  kStatus_FLASH_EraseFrequencyError, 
 
  kStatus_FLASH_ProgramFrequencyError
 
 } | 
|   | Flash driver status codes.  More...
  | 
|   | 
| #define  | kStatusGroupGeneric   0 | 
|   | Flash driver status group.  More...
  | 
|   | 
| 
#define  | kStatusGroupFlashDriver   1 | 
|   | 
| #define  | MAKE_STATUS(group, code)   ((((group)*100) + (code))) | 
|   | Constructs a status code value from a group and a code number.  More...
  | 
|   | 
      
        
          | struct flash_mode_config_t | 
        
      
 
 
      
        
          | struct flash_ffr_config_t | 
        
      
 
 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs. 
 
      
        
          | uint32_t flash_config_t::PFlashTotalSize | 
        
      
 
 
      
        
          | uint32_t flash_config_t::PFlashBlockCount | 
        
      
 
 
      
        
          | uint32_t flash_config_t::PFlashPageSize | 
        
      
 
 
      
        
          | uint32_t flash_config_t::PFlashSectorSize | 
        
      
 
 
 
 
      
        
          | #define MAKE_VERSION | 
          ( | 
            | 
          major,  | 
        
        
           | 
           | 
            | 
          minor,  | 
        
        
           | 
           | 
            | 
          bugfix  | 
        
        
           | 
          ) | 
           |    (((major) << 16) | ((minor) << 8) | (bugfix)) | 
        
      
 
 
      
        
          | #define FSL_FEATURE_FLASH_IP_IS_C040HD_ATFC   (1) | 
        
      
 
 
      
        
          | #define kStatusGroupGeneric   0 | 
        
      
 
 
      
        
          | #define MAKE_STATUS | 
          ( | 
            | 
          group,  | 
        
        
           | 
           | 
            | 
          code  | 
        
        
           | 
          ) | 
           |    ((((group)*100) + (code))) | 
        
      
 
 
      
        
          | #define FOUR_CHAR_CODE | 
          ( | 
            | 
          a,  | 
        
        
           | 
           | 
            | 
          b,  | 
        
        
           | 
           | 
            | 
          c,  | 
        
        
           | 
           | 
            | 
          d  | 
        
        
           | 
          ) | 
           |    (((d) << 24) | ((c) << 16) | ((b) << 8) | ((a))) | 
        
      
 
 
| Enumerator | 
|---|
| kFLASH_DriverVersionName  | 
 Flash driver version name.  
 | 
| kFLASH_DriverVersionMajor  | 
 Major flash driver version.  
 | 
| kFLASH_DriverVersionMinor  | 
 Minor flash driver version.  
 | 
| kFLASH_DriverVersionBugfix  | 
 Bugfix for flash driver version.  
 | 
 
 
| Enumerator | 
|---|
| kStatus_FLASH_Success  | 
 API is executed successfully.  
 | 
| kStatus_FLASH_InvalidArgument  | 
 Invalid argument.  
 | 
| kStatus_FLASH_SizeError  | 
 Error size.  
 | 
| kStatus_FLASH_AlignmentError  | 
 Parameter is not aligned with the specified baseline.  
 | 
| kStatus_FLASH_AddressError  | 
 Address is out of range.  
 | 
| kStatus_FLASH_AccessError  | 
 Invalid instruction codes and out-of bound addresses.  
 | 
| kStatus_FLASH_ProtectionViolation  | 
 The program/erase operation is requested to execute on protected areas.  
 | 
| kStatus_FLASH_CommandFailure  | 
 Run-time error during command execution.  
 | 
| kStatus_FLASH_UnknownProperty  | 
 Unknown property.  
 | 
| kStatus_FLASH_EraseKeyError  | 
 API erase key is invalid.  
 | 
| kStatus_FLASH_RegionExecuteOnly  | 
 The current region is execute-only.  
 | 
| kStatus_FLASH_ExecuteInRamFunctionNotReady  | 
 Execute-in-RAM function is not available.  
 | 
| kStatus_FLASH_CommandNotSupported  | 
 Flash API is not supported.  
 | 
| kStatus_FLASH_ReadOnlyProperty  | 
 The flash property is read-only.  
 | 
| kStatus_FLASH_InvalidPropertyValue  | 
 The flash property value is out of range.  
 | 
| kStatus_FLASH_InvalidSpeculationOption  | 
 The option of flash prefetch speculation is invalid.  
 | 
| kStatus_FLASH_EccError  | 
 A correctable or uncorrectable error during command execution.  
 | 
| kStatus_FLASH_CompareError  | 
 Destination and source memory contents do not match.  
 | 
| kStatus_FLASH_RegulationLoss  | 
 A loss of regulation during read.  
 | 
| kStatus_FLASH_InvalidWaitStateCycles  | 
 The wait state cycle set to r/w mode is invalid.  
 | 
| kStatus_FLASH_OutOfDateCfpaPage  | 
 CFPA page version is out of date.  
 | 
| kStatus_FLASH_BlankIfrPageData  | 
 Blank page cannnot be read.  
 | 
| kStatus_FLASH_EncryptedRegionsEraseNotDoneAtOnce  | 
 Encrypted flash subregions are not erased at once.  
 | 
| kStatus_FLASH_ProgramVerificationNotAllowed  | 
 Program verification is not allowed when the encryption is enabled.  
 | 
| kStatus_FLASH_HashCheckError  | 
 Hash check of page data is failed.  
 | 
| kStatus_FLASH_SealedFfrRegion  | 
 The FFR region is sealed.  
 | 
| kStatus_FLASH_FfrRegionWriteBroken  | 
 The FFR Spec region is not allowed to be written discontinuously.  
 | 
| kStatus_FLASH_NmpaAccessNotAllowed  | 
 The NMPA region is not allowed to be read/written/erased.  
 | 
| kStatus_FLASH_CmpaCfgDirectEraseNotAllowed  | 
 The CMPA Cfg region is not allowed to be erased directly.  
 | 
| kStatus_FLASH_FfrBankIsLocked  | 
 The FFR bank region is locked.  
 | 
| kStatus_FLASH_EraseFrequencyError  | 
 Core frequency is over 100MHZ.  
 | 
| kStatus_FLASH_ProgramFrequencyError  | 
 Core frequency is over 100MHZ.  
 | 
 
 
- Note
 - The resulting value is built with a byte order such that the string being readable in expected order when viewed in a hex editor, if the value is treated as a 32-bit little endian value. 
 
| Enumerator | 
|---|
| kFLASH_ApiEraseKey  | 
 Key value used to validate all flash erase APIs.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_PropertyPflashSectorSize  | 
 Pflash sector size property.  
 | 
| kFLASH_PropertyPflashTotalSize  | 
 Pflash total size property.  
 | 
| kFLASH_PropertyPflashBlockSize  | 
 Pflash block size property.  
 | 
| kFLASH_PropertyPflashBlockCount  | 
 Pflash block count property.  
 | 
| kFLASH_PropertyPflashBlockBaseAddr  | 
 Pflash block base address property.  
 | 
| kFLASH_PropertyPflashPageSize  | 
 Pflash page size property.  
 | 
| kFLASH_PropertyPflashSystemFreq  | 
 System Frequency System Frequency.  
 | 
| kFLASH_PropertyFfrSectorSize  | 
 FFR sector size property.  
 | 
| kFLASH_PropertyFfrTotalSize  | 
 FFR total size property.  
 | 
| kFLASH_PropertyFfrBlockBaseAddr  | 
 FFR block base address property.  
 | 
| kFLASH_PropertyFfrPageSize  | 
 FFR page size property.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_MaxPagesToErase  | 
 The max value in pages to erase.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_AlignementUnitVerifyErase  | 
 The alignment unit in bytes used for verify erase operation.  
 | 
| kFLASH_AlignementUnitProgram  | 
 The alignment unit in bytes used for program operation.  
 | 
| kFLASH_AlignementUnitSingleWordRead  | 
 The alignment unit in bytes used for verify program operation.  
The alignment unit in bytes used for SingleWordRead command.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_ReadWithEccOff  | 
 ECC is on.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_ReadMarginNormal  | 
 Normal read.  
 | 
| kFLASH_ReadMarginVsProgram  | 
 Margin vs.  
program  
 | 
| kFLASH_ReadMarginVsErase  | 
 Margin vs.  
erase  
 | 
| kFLASH_ReadMarginIllegalBitCombination  | 
 Illegal bit combination.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_ReadDmaccDisabled  | 
 Memory word.  
 | 
| kFLASH_ReadDmaccEnabled  | 
 DMACC word.  
 | 
 
 
| Enumerator | 
|---|
| kFLASH_RampControlDivisionFactorReserved  | 
 Reserved.  
 | 
| kFLASH_RampControlDivisionFactor256  | 
 clk48mhz / 256 = 187.5KHz  
 | 
| kFLASH_RampControlDivisionFactor128  | 
 clk48mhz / 128 = 375KHz  
 | 
| kFLASH_RampControlDivisionFactor64  | 
 clk48mhz / 64 = 750KHz  
 | 
 
 
This function checks and initializes the Flash module for the other Flash APIs.
- Parameters
 - 
  
    | config | Pointer to the storage for the driver runtime state. | 
  
   
- Return values
 - 
  
  
 
 
 
This function erases the appropriate number of flash sectors based on the desired start address and length.
- Parameters
 - 
  
    | config | The pointer to the storage for the driver runtime state.  | 
    | start | The start address of the desired flash memory to be erased. The start address need to be 512bytes-aligned.  | 
    | lengthInBytes | The length, given in bytes (not words or long-words) to be erased. Must be 512bytes-aligned.  | 
    | key | The value used to validate all flash erase APIs. | 
  
   
- Return values
 - 
  
  
 
 
 
      
        
          | status_t FLASH_Program  | 
          ( | 
          flash_config_t *  | 
          config,  | 
        
        
           | 
           | 
          uint32_t  | 
          start,  | 
        
        
           | 
           | 
          const uint8_t *  | 
          src,  | 
        
        
           | 
           | 
          uint32_t  | 
          lengthInBytes  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
- Parameters
 - 
  
    | config | A pointer to the storage for the driver runtime state.  | 
    | start | The start address of the desired flash memory to be programmed. Must be 512bytes-aligned.  | 
    | src | A pointer to the source buffer of data that is to be programmed into the flash.  | 
    | lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be 512bytes-aligned. | 
  
   
- Return values
 - 
  
  
 
 
 
This function read the flash memory from a given flash area as determined by the start address and the length.
- Parameters
 - 
  
    | config | A pointer to the storage for the driver runtime state.  | 
    | start | The start address of the desired flash memory to be read.  | 
    | dest | A pointer to the dest buffer of data that is to be read from the flash.  | 
    | lengthInBytes | The length, given in bytes (not words or long-words), to be read. | 
  
   
- Return values
 - 
  
  
 
 
 
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased to the specified read margin level.
- Parameters
 - 
  
    | config | A pointer to the storage for the driver runtime state.  | 
    | start | The start address of the desired flash memory to be verified. The start address need to be 512bytes-aligned.  | 
    | lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be 512bytes-aligned. | 
  
   
- Return values
 - 
  
  
 
 
 
      
        
          | status_t FLASH_VerifyProgram  | 
          ( | 
          flash_config_t *  | 
          config,  | 
        
        
           | 
           | 
          uint32_t  | 
          start,  | 
        
        
           | 
           | 
          uint32_t  | 
          lengthInBytes,  | 
        
        
           | 
           | 
          const uint8_t *  | 
          expectedData,  | 
        
        
           | 
           | 
          uint32_t *  | 
          failedAddress,  | 
        
        
           | 
           | 
          uint32_t *  | 
          failedData  | 
        
        
           | 
          ) | 
           |  | 
        
      
 
This function verifies the data programed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
- Parameters
 - 
  
    | config | A pointer to the storage for the driver runtime state.  | 
    | start | The start address of the desired flash memory to be verified. need be 512bytes-aligned.  | 
    | lengthInBytes | The length, given in bytes (not words or long-words), to be verified. need be 512bytes-aligned.  | 
    | expectedData | A pointer to the expected data that is to be verified against.  | 
    | failedAddress | A pointer to the returned failing address.  | 
    | failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. | 
  
   
- Return values
 - 
  
  
 
 
 
- Parameters
 - 
  
    | config | A pointer to the storage for the driver runtime state.  | 
    | whichProperty | The desired property from the list of properties in enum flash_property_tag_t  | 
    | value | A pointer to the value returned for the desired flash property. | 
  
   
- Return values
 - 
  
  
 
 
 
      
        
          | void BOOTLOADER_UserEntry  | 
          ( | 
          void *  | 
          arg | ) | 
           | 
        
      
 
- Parameters
 - 
  
    | arg | Indicates API prototype fields definition. Refer to the above user_app_boot_invoke_option_t structure  |