MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
I2C: Inter-Integrated Circuit Driver

Overview

This document consists of sections titled with Driver Overview, Data Structures, Enumerations, Functions, etc., each with an overview list and detailed documentation. It is recommended to read the Driver Overview first for it includes a comprehensive description of the peripheral, driver and driver changes. Other sections give detailed information for APIs, enums, macros, etc., for your further reference.

Modules

 I2C Peripheral and Driver Overview
 Content including 1) peripheral features, work logic and work method; 2) driver design logic and use method; 3) typical use case.
 
 The Driver Change Log
 The current I2C driver version is 2.0.1.
 

Data Structures

struct  _i2c_master_config
 I2C master configuration structure. More...
 
struct  _i2c_slave_config
 I2C slave configuration structure. More...
 
struct  _i2c_config
 I2C configuration structure. More...
 
struct  _i2c_master_transfer
 I2C master transfer configuration structure. More...
 
struct  _i2c_master_transfer_handle
 I2C master transfer handle. More...
 
struct  _i2c_slave_transfer
 I2C slave transfer configuration structure. More...
 
struct  _i2c_slave_transfer_handle
 I2C slave transfer handle. More...
 

Macros

#define I2C_RETRY_TIMES   0U /* Default defines to zero, driver keeps checking status flag untill it changes. */
 Retry times when checking status flags. More...
 
#define I2C_SMBUS_ENABLE   0U /* Default defines to zero, driver uses simple I2C transfer. */
 Control whether to use SMBus featues. More...
 
#define I2C_MASTER_FACK_CONTROL   0U /* Default defines to zero means master will send ack automatically. */
 Control whether to enable FACK for master read operation in non SMBus tranfer. More...
 

Typedefs

typedef struct _i2c_master_config i2c_master_config_t
 I2C master configuration structure. More...
 
typedef enum
_i2c_slave_address_mode 
i2c_slave_address_mode_t
 Slave addressing mode, address match or range address match. More...
 
typedef struct _i2c_slave_config i2c_slave_config_t
 I2C slave configuration structure. More...
 
typedef struct _i2c_config i2c_config_t
 I2C configuration structure. More...
 
typedef enum _i2c_data_direction i2c_data_direction_t
 Peripheral data direction. More...
 
typedef enum
_i2c_master_transfer_direction 
i2c_master_transfer_direction_t
 Master transfer direction. More...
 
typedef struct _i2c_master_transfer i2c_master_transfer_t
 I2C master transfer configuration structure. More...
 
typedef struct
_i2c_master_transfer_handle 
i2c_master_transfer_handle_t
 Forward declaration of the I2C master transfer handle structure. More...
 
typedef void(* i2c_master_transfer_callback_t )(i2c_master_transfer_handle_t *psHandle)
 I2C master transfer callback function definition. More...
 
typedef enum
_i2c_slave_transfer_event 
i2c_slave_transfer_event_t
 Set of slave transfer events. More...
 
typedef struct _i2c_slave_transfer i2c_slave_transfer_t
 I2C slave transfer configuration structure. More...
 
typedef struct
_i2c_slave_transfer_handle 
i2c_slave_transfer_handle_t
 Forward declaration of the I2C slave transfer handle structure. More...
 
typedef void(* i2c_slave_transfer_callback_t )(i2c_slave_transfer_handle_t *psHandle)
 I2C slave transfer callback function definition. More...
 

Enumerations

enum  {
  kStatus_I2C_Busy = MAKE_STATUS(kStatusGroup_I2C, 0),
  kStatus_I2C_Idle = MAKE_STATUS(kStatusGroup_I2C, 1),
  kStatus_I2C_Nak = MAKE_STATUS(kStatusGroup_I2C, 2),
  kStatus_I2C_ArbitrationLost = MAKE_STATUS(kStatusGroup_I2C, 3),
  kStatus_I2C_Timeout,
  kStatus_I2C_Addr_Nak = MAKE_STATUS(kStatusGroup_I2C, 5),
  kStatus_I2C_Pec_Error = MAKE_STATUS(kStatusGroup_I2C, 6)
}
 I2C API status codes, used by bus operation APIs and transactional APIs as return value to indicate the bus's current status as the API's execution result, or used in the callback to indicate transfer results. More...
 
enum  _i2c_status_flags {
  kI2C_ReceiveNakFlag = I2C_S_RXAK_MASK,
  kI2C_InterruptPendingFlag = I2C_S_IICIF_MASK,
  kI2C_SlaveTransmitFlag = I2C_S_SRW_MASK,
  kI2C_RangeAddressMatchInterruptFlag,
  kI2C_ArbitrationLostInterruptFlag = I2C_S_ARBL_MASK,
  kI2C_BusBusyFlag = I2C_S_BUSY_MASK,
  kI2C_AddressAsSlaveInterruptFlag,
  kI2C_ByteTransferCompleteInterruptFlag = I2C_S_TCF_MASK,
  kI2C_StopDetectInterruptFlag = I2C_FLT_STOPF_MASK << 8,
  kI2C_StartDetectInterruptFlag = I2C_FLT_STARTF_MASK << 8,
  kI2C_SclLowTimeoutFlag = I2C_SMB_SLTF_MASK << 8,
  kI2C_BusIdleFlag = I2C_SMB_SHTF1_MASK << 8,
  kI2C_SdaLowTimeoutInterruptFlag,
  kI2C_StatusAllFlags
}
 I2C hardware status flags. More...
 
enum  _i2c_interrupt_enable {
  kI2C_GlobalInterruptEnable = I2C_C1_IICIE_MASK,
  kI2C_StartStopDetectInterruptEnable = I2C_FLT_SSIE_MASK,
  kI2C_SdaLowTimeoutInterruptEnable = I2C_SMB_SHTF2IE_MASK
}
 I2C interrupt enable/disable source. More...
 
enum  _i2c_slave_address_mode {
  kI2C_AddressMatch = 0x0U,
  kI2C_AddressRangeMatch = 0X1U,
  kI2C_AddressMatch10bit = 0X2U
}
 Slave addressing mode, address match or range address match. More...
 
enum  _i2c_data_direction {
  kI2C_Read = 0x0U,
  kI2C_Write = 0x1U
}
 Peripheral data direction. More...
 
enum  _i2c_master_transfer_control_flags {
  kI2C_TransferStartStopFlag = 0x0U,
  kI2C_TransferNoStartFlag = 0x1U,
  kI2C_TransferRepeatedStartFlag = 0x2U,
  kI2C_TransferNoStopFlag = 0x4U
}
 I2C master transfer control flags. More...
 
enum  _i2c_master_transfer_direction {
  kI2C_MasterTransmit = 0x0U,
  kI2C_MasterReceive = 0x1U
}
 Master transfer direction. More...
 
enum  _i2c_slave_transfer_event {
  kI2C_SlaveAddressMatchEvent,
  kI2C_SlaveOutofTransmitDataEvent = 0x02U,
  kI2C_SlaveOutofReceiveSpaceEvent,
  kI2C_SlaveStartEvent = 0x08U,
  kI2C_SlaveCompletionEvent,
  kI2C_SlaveGenaralcallEvent = 0x20U,
  kI2C_SlaveAllEvents
}
 Set of slave transfer events. More...
 

Functions

uint32_t I2C_GetInstance (I2C_Type *base)
 Gets instance number for I2C module. More...
 

Driver version

#define FSL_I2C_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 I2C driver version. More...
 

Module Init/Deinit Sub-group

void I2C_MasterGetDefaultConfig (i2c_master_config_t *psMasterConfig, uint32_t u32SrcClockHz)
 Sets the I2C master configuration structure to default values. More...
 
void I2C_MasterInit (I2C_Type *base, const i2c_master_config_t *psMasterConfig)
 Initializes the I2C peripheral to operate as master. More...
 
void I2C_MasterDeinit (I2C_Type *base)
 De-initializes the I2C peripheral. More...
 
void I2C_SlaveGetDefaultConfig (i2c_slave_config_t *psSlaveConfig, uint16_t u16PrimaryAddress, uint32_t u32SrcClockHz)
 Sets the I2C slave configuration structure to default values. More...
 
void I2C_SlaveInit (I2C_Type *base, const i2c_slave_config_t *psSlaveConfig)
 Initializes the I2C peripheral to operate as slave. More...
 
static void I2C_SlaveDeinit (I2C_Type *base)
 De-initializes the I2C peripheral. More...
 
void I2C_GetDefaultConfig (i2c_config_t *psConfig, uint16_t u16PrimaryAddress, uint32_t u32SrcClockHz)
 Sets the I2C configuration structure to default values. More...
 
void I2C_Init (I2C_Type *base, const i2c_config_t *psConfig)
 Initializes the I2C peripheral. More...
 
static void I2C_Deinit (I2C_Type *base)
 De-initializes the I2C peripheral. More...
 

Hardware Status Flags Sub-group

uint16_t I2C_MasterGetStatusFlags (I2C_Type *base)
 Gets the I2C master hardware status flags. More...
 
static void I2C_MasterClearStatusFlags (I2C_Type *base, uint16_t u16StatusFlags)
 Clears the I2C master status flags. More...
 
static uint16_t I2C_SlaveGetStatusFlags (I2C_Type *base)
 Gets the I2C slave hardware status flags. More...
 
static void I2C_SlaveClearStatusFlags (I2C_Type *base, uint16_t u16StatusFlags)
 Clears the I2C slave status flags. More...
 

Interrupt Sub-group

void I2C_EnableInterrupts (I2C_Type *base, uint8_t u8Interrupts)
 Enables I2C interrupt source. More...
 
void I2C_DisableInterrupts (I2C_Type *base, uint8_t u8Interrupts)
 Disables I2C interrupt source. More...
 
uint8_t I2C_GetEnabledInterrupts (I2C_Type *base)
 Get all the enabled interrupt sources. More...
 

Common Peripheral Configuration Sub-group

static bool I2C_IsMaster (I2C_Type *base)
 Returns whether the I2C module is in master mode. More...
 
static void I2C_Reset (I2C_Type *base)
 Sets the I2C register value to reset value. More...
 
static void I2C_Enable (I2C_Type *base, bool bEnable)
 Enables or disables the I2C peripheral operation. More...
 
static void I2C_EnableFastAck (I2C_Type *base, bool bEnable)
 Enables/Disables fast NACK/ACK feature. More...
 
static void I2C_EnableHighDrive (I2C_Type *base, bool bEnable)
 Enables/Disables high drive. More...
 
static void I2C_EnableStopHold (I2C_Type *base, bool bEnable)
 Enables/Disables double buffer. More...
 
static void I2C_SetTransferDirection (I2C_Type *base, i2c_data_direction_t eDataDirection)
 Sets I2C module data direction. More...
 
void I2C_SetSclTimeoutValue (I2C_Type *base, uint16_t u16SclTimout_Ms, uint32_t u32SrcClockHz)
 brief Sets the I2C SCL timeout value. More...
 
void I2C_SetGlitchFilter (I2C_Type *base, uint16_t u16GlitchFilter_Ns, uint32_t u32SrcClockHz)
 brief Sets the I2C master glitch filter width. More...
 
static void I2C_EnableDMA (I2C_Type *base, bool bEnable)
 Enables/disables the I2C DMA request. More...
 
static uint32_t I2C_GetDataRegAddr (I2C_Type *base)
 Gets the I2C data register address. More...
 

Slave Peripheral Configuration Sub-group

static void I2C_SlaveEnableAlertResponse (I2C_Type *base, bool bEnable)
 Enables/Disables alert response. More...
 
static void I2C_SlaveEnableSecondaryAddress (I2C_Type *base, bool bEnable)
 Enables/Disables secondary address. More...
 
static void I2C_SlaveEnableGeneralCall (I2C_Type *base, bool bEnable)
 Enables/Disables general call. More...
 
static void I2C_SlaveEnableWakeUp (I2C_Type *base, bool bEnable)
 Enables/Disables slave low power wakeup. More...
 
void I2C_SlaveSetAddressingMode (I2C_Type *base, i2c_slave_address_mode_t eAddressingMode, uint16_t u16Address, uint8_t u8MaxAddress)
 Configure the slave addressing mode. More...
 

Master Peripheral Configuration Sub-group

void I2C_MasterSetBaudRate (I2C_Type *base, uint32_t u32BaudRateBps, uint32_t u32SrcClockHz)
 Sets the I2C master transfer baud rate. More...
 

Common Bus Operation Sub-Group

static uint8_t I2C_ReadByte (I2C_Type *base)
 Reads one byte from data register directly. More...
 
static void I2C_WriteByte (I2C_Type *base, uint8_t u8Data)
 Writes one byte to the data register directly. More...
 
static void I2C_SendAck (I2C_Type *base, bool bIsAck)
 Sends an acknowledge/non-acknowledge signal to the bus on the following receiving byte if SMB[FACK] is cleared, or on the current receiving byte if SMB[FACK] is set. More...
 

Master Bus Operation Sub-Group

status_t I2C_MasterStart (I2C_Type *base, uint8_t u8Address, i2c_master_transfer_direction_t eDirection)
 Sends a START signal on the I2C bus then the 7-bit slave address with transmit/receive bit. More...
 
status_t I2C_MasterRepeatedStart (I2C_Type *base, uint8_t u8Address, i2c_master_transfer_direction_t eDirection)
 Sends a repeated START signal, then the 7-bit slave address with transmit/receive bit to I2C bus. More...
 
status_t I2C_MasterStop (I2C_Type *base)
 Sends a STOP signal on the I2C bus. More...
 
status_t I2C_MasterWriteBlocking (I2C_Type *base, const uint8_t *pu8Data, uint16_t txSize, bool bSendStop)
 Sends a piece of data to I2C bus in master mode in blocking way. More...
 
status_t I2C_MasterReadBlocking (I2C_Type *base, uint8_t *pu8RxBuff, uint16_t rxSize, bool bSendStop)
 Receives a piece of data from I2C bus in master mode in blocking way. More...
 

Slave Bus Operation Sub-Group

status_t I2C_SlaveWriteBlocking (I2C_Type *base, const uint8_t *pu8TxBuff, uint16_t txSize)
 Sends a piece of data to I2C bus in slave mode in blocking way. More...
 
status_t I2C_SlaveReadBlocking (I2C_Type *base, uint8_t *pu8RxBuff, uint16_t rxSize)
 Receives a piece of data from I2C bus in slave mode in blocking way. More...
 

Master Transfer Sub-group

status_t I2C_MasterTransferBlocking (I2C_Type *base, i2c_master_transfer_t *psTransferConfig)
 Performs a master polling transfer on the I2C bus. More...
 
void I2C_MasterTransferCreateHandle (I2C_Type *base, i2c_master_transfer_handle_t *psHandle, i2c_master_transfer_callback_t pfCallback, void *pUserData)
 Initializes the I2C master transfer in interrupt way. More...
 
status_t I2C_MasterTransferNonBlocking (i2c_master_transfer_handle_t *psHandle, i2c_master_transfer_t *psTransferConfig)
 Initiates a master transfer on the I2C bus in interrupt way. More...
 
status_t I2C_MasterTransferGetCount (i2c_master_transfer_handle_t *psHandle, uint16_t *count)
 Gets the master transfer count and status during a interrupt transfer. More...
 
status_t I2C_MasterTransferAbort (i2c_master_transfer_handle_t *psHandle)
 Aborts an in-process transfer in interrupt way. More...
 

Slave Transfer Sub-group

void I2C_SlaveTransferCreateHandle (I2C_Type *base, i2c_slave_transfer_handle_t *psHandle, i2c_slave_transfer_callback_t pfCallback, void *pUserData)
 Initializes the I2C slave transfer in interrupt way. More...
 
status_t I2C_SlaveTransferNonBlocking (i2c_slave_transfer_handle_t *psHandle, i2c_slave_transfer_t *psTransferConfig)
 Sets I2C slave ready to process bus events. More...
 
status_t I2C_SlaveTransferGetCount (i2c_slave_transfer_handle_t *psHandle, uint16_t *count)
 Gets how many bytes slave have transferred in curent data buffer. More...
 
void I2C_SlaveTransferAbort (i2c_slave_transfer_handle_t *psHandle)
 Aborts the slave transfer. More...
 

Data Structure Documentation

struct _i2c_master_config

This structure includes all the master operation needed features, user can configure these features one by one manually, or call I2C_MasterGetDefaultConfig to set the structure to default value. Then, call I2C_MasterInit to initialize I2C module. After initialization, the I2C module can only operate as master. To deinitialize I2C, call I2C_MasterDeinit.

Data Fields

bool bEnableModule
 Enable the I2C peripheral during initialization. More...
 
bool bEnableStopHold
 Control the stop hold enable. More...
 
uint8_t u8GlitchFilterWidth
 Control the width of the glitch filter. More...
 
uint8_t u8Interrupts
 Mask of the interrupts to be enabled in the init function. More...
 
uint32_t u32BaudRateBps
 Baud rate value in bits-per-second. More...
 
uint32_t u32SrcClockHz
 The clock source frequency for I2C module. More...
 

Field Documentation

bool _i2c_master_config::bEnableModule
bool _i2c_master_config::bEnableStopHold

I2C_FLT_SHEN

uint8_t _i2c_master_config::u8GlitchFilterWidth

I2C_FLT_FLT

uint8_t _i2c_master_config::u8Interrupts
uint32_t _i2c_master_config::u32BaudRateBps

I2C_F_MULT, I2C_F_ICR

uint32_t _i2c_master_config::u32SrcClockHz
struct _i2c_slave_config

This structure includes all the slave operation needed features, user can configure these features one by one manually, or call I2C_SlaveGetDefaultConfig to set the structure to default value. Then, call I2C_SlaveInit to initialize I2C module. After initialization, the I2C module can only operate as slave. To deinitialize I2C, call I2C_SlaveDeinit.

Data Fields

bool bEnableModule
 Enable the I2C peripheral during initialization. More...
 
bool bEnableStopHold
 Control the stop hold enable. More...
 
uint8_t u8GlitchFilterWidth
 Control the width of the glitch filter. More...
 
bool bEnableWakeUp
 Enable/disable waking up MCU from low-power mode. More...
 
bool bEnableGeneralCall
 Enable the general call addressing mode, not affected by address length. More...
 
i2c_slave_address_mode_t eAddressingMode
 Addressing mode chosen from i2c_slave_address_mode_t. More...
 
uint16_t bitsPrimaryAddress: 10
 Primary Slave address. More...
 
uint16_t bitsMaxAddress: 7
 The maximum boundary of slave address used in a range address match addressing. More...
 
uint8_t u8Interrupts
 Mask of the interrupts to be enabled in the init function. More...
 
uint32_t u32SclStopHoldTime_ns
 
 the delay from the rising edge of SCL (I2C clock) to the rising edge of SDA

(I2C data) while SCL is high (stop condition), SDA hold time and SCL start hold time are also configured according to the SCL stop hold time. More...

 
uint32_t u32SrcClockHz
 The clock source frequency for I2C module. More...
 

Field Documentation

bool _i2c_slave_config::bEnableModule
bool _i2c_slave_config::bEnableStopHold

I2C_FLT_SHEN

uint8_t _i2c_slave_config::u8GlitchFilterWidth

I2C_FLT_FLT

bool _i2c_slave_config::bEnableWakeUp

I2C_C1_WUEN

bool _i2c_slave_config::bEnableGeneralCall

General call address is 0x00. I2C_C2_GCAEN

i2c_slave_address_mode_t _i2c_slave_config::eAddressingMode

I2C_C2_ADEXT I2C_C2_RMEN

uint16_t _i2c_slave_config::bitsPrimaryAddress

I2C_A1_AD[7] I2C_C2_AD[3]

uint16_t _i2c_slave_config::bitsMaxAddress

In range address match, address greater than primary address and less than or equal to upper address is marked as matched. I2C_RA_RAD[7]

uint8_t _i2c_slave_config::u8Interrupts
uint32_t _i2c_slave_config::u32SclStopHoldTime_ns
uint32_t _i2c_slave_config::u32SrcClockHz
struct _i2c_config

This structure includes all I2C features, user can configure user can configure these features one by one manually, or call I2C_GetDefaultConfig to set the structure to default value. Then, call I2C_Init to initialize I2C module. To deinitialize I2C, call I2C_Deinit.

Data Fields

bool bEnableModule
 Enable the I2C peripheral during initialization. More...
 
bool bEnableStopHold
 Control the stop hold enable. More...
 
uint8_t u8GlitchFilterWidth
 Control the width of the glitch filter. More...
 
bool bEnableWakeUp
 Enable/disable waking up MCU from low-power mode. More...
 
bool bEnableGeneralCall
 Enable the general call addressing mode, not affected by address length. More...
 
i2c_slave_address_mode_t eAddressingMode
 Addressing mode chosen from i2c_slave_address_mode_t. More...
 
uint16_t bitsPrimaryAddress: 10
 Primary Slave address. More...
 
uint16_t bitsMaxAddress: 7
 The maximum boundary of slave address used in a range address match addressing. More...
 
uint8_t u8Interrupts
 Mask of the interrupts to be enabled in the init function. More...
 
uint32_t u32BaudRateBps
 Baud rate value in bits-per-second. More...
 
uint32_t u32SrcClockHz
 The clock source frequency for I2C module. More...
 

Field Documentation

bool _i2c_config::bEnableModule
bool _i2c_config::bEnableStopHold

I2C_FLT_SHEN

uint8_t _i2c_config::u8GlitchFilterWidth

I2C_FLT_FLT

bool _i2c_config::bEnableWakeUp

I2C_C1_WUEN

bool _i2c_config::bEnableGeneralCall

General call address is 0x00. I2C_C2_GCAEN

i2c_slave_address_mode_t _i2c_config::eAddressingMode

I2C_C2_ADEXT I2C_C2_RMEN

uint16_t _i2c_config::bitsPrimaryAddress

I2C_A1_AD[7] I2C_C2_AD[3]

uint16_t _i2c_config::bitsMaxAddress

In range address match, address greater than primary address and less than or equal to upper address is marked as matched. I2C_RA_RAD[7]

uint8_t _i2c_config::u8Interrupts
uint32_t _i2c_config::u32BaudRateBps

I2C_F_MULT, I2C_F_ICR

uint32_t _i2c_config::u32SrcClockHz
struct _i2c_master_transfer

This structure definition includes all the user configurable features, that are used to control single I2C transfer of master mode, in polling way or in interrupt way.

Data Fields

uint8_t u8ControlFlagMask
 
      The transfer flag which controls the transfer start/stop signal, refer @ref

_i2c_master_transfer_flags. More...

 
uint8_t u8SlaveAddress
 7-bit slave address. More...
 
i2c_master_transfer_direction_t eDirection
 Transfer direction, kI2C_MasterTransmit or kI2C_MasterReceive. More...
 
uint8_t * pu8Command
 Pointer to command code. More...
 
uint8_t u8CommandSize
 Size of the command code, max value 4. More...
 
uint8_t *volatile pu8Data
 Pointer to the send/receive data buffer. More...
 
volatile uint16_t u16DataSize
 Transfer size. More...
 

Field Documentation

uint8_t _i2c_master_transfer::u8ControlFlagMask
uint8_t _i2c_master_transfer::u8SlaveAddress
i2c_master_transfer_direction_t _i2c_master_transfer::eDirection
uint8_t* _i2c_master_transfer::pu8Command
uint8_t _i2c_master_transfer::u8CommandSize
uint8_t* volatile _i2c_master_transfer::pu8Data
volatile uint16_t _i2c_master_transfer::u16DataSize
struct _i2c_master_transfer_handle
Note
If user wants to use the transactional API to transfer data in interrupt way in master mode, one I2C instance should and can only be allocated one master handle.
The handle is maintained by I2C driver internally, which means the transfer state is retained and user shall not modify its state u8State in application level. If user only wish to use transactional APIs without understanding its machanism, it is not necessary to understand these members.

Data Fields

I2C_Type * base
 I2C base pointer to the I2C instance that assigned to this handle. More...
 
i2c_master_transfer_t sTransfer
 I2C master transfer structure. More...
 
uint16_t u16TransferSize
 Total bytes to be transferred. More...
 
uint8_t u8State
 A transfer state maintained during transfer. More...
 
i2c_master_transfer_callback_t pfCompletionCallback
 Callback function invoked when the transfer is finished. More...
 
status_t completionStatus
 I2C master transfer complete status, indicating how the transfer ends. More...
 
void * pUserData
 User configurable pointer to any data, function, structure etc that user wish to use in the callback.
 

Field Documentation

I2C_Type* _i2c_master_transfer_handle::base
i2c_master_transfer_t _i2c_master_transfer_handle::sTransfer
uint16_t _i2c_master_transfer_handle::u16TransferSize
uint8_t _i2c_master_transfer_handle::u8State
i2c_master_transfer_callback_t _i2c_master_transfer_handle::pfCompletionCallback
status_t _i2c_master_transfer_handle::completionStatus
struct _i2c_slave_transfer

Covers slave transfer data buffer pointer, data size and the events user want driver to alert.

Note
Unlike master who controls the transfer flow, slave has to monitor any bus event and change its configuration accordingly. So this slave transfer configuration structure is also used as second parameter of callback, for user to change the transfer configuration in the callback. The read-only member eEvent shows which event occured that causes the callback being invoked.

Data Fields

uint8_t u8EventMask
 Mask of the events. More...
 
uint8_t *volatile pu8Data
 Pointer to the buffer of data to send, or to store received data. More...
 
volatile uint16_t u16DataSize
 Transfer size. More...
 
i2c_slave_transfer_event_t eEvent
 The event that caused the callback being invoked. More...
 

Field Documentation

uint8_t _i2c_slave_transfer::u8EventMask

When these enents occur during transfer driver will alert user using callback.

uint8_t* volatile _i2c_slave_transfer::pu8Data
volatile uint16_t _i2c_slave_transfer::u16DataSize
i2c_slave_transfer_event_t _i2c_slave_transfer::eEvent

Read-only.

struct _i2c_slave_transfer_handle
Note
If user wants to use the transactional API to transfer data in slave mode, one I2C instance should and can only be allocated one handle.
The handle is maintained by I2C driver internally, which means the transfer state is retained and user shall not modify its state u8State in application level. If user only wish to use transactional APIs without understanding its machanism, it is not necessary to understand these members.

Data Fields

I2C_Type * base
 I2C base pointer to the I2C instance that assigned to this handle. More...
 
i2c_slave_transfer_t sTransfer
 I2C slave transfer structure. More...
 
uint16_t u16TransferredCount
 The number of bytes actually transferred for curent data buffer. More...
 
uint8_t u8State
 A transfer state maintained during transfer. More...
 
i2c_slave_transfer_callback_t pfCallback
 Callback function invoked at the transfer event. More...
 
status_t completionStatus
 
                            I2C slave transfer complete status, indicating how the transfer ends, such as

kStatus_I2C_Nak indicates the slave was nacked by master before all the data was sent. More...

 
void * pUserData
 User configurable pointer to any data, function, structure etc that user wish to use in the callback. More...
 

Field Documentation

I2C_Type* _i2c_slave_transfer_handle::base
i2c_slave_transfer_t _i2c_slave_transfer_handle::sTransfer
uint16_t _i2c_slave_transfer_handle::u16TransferredCount
uint8_t _i2c_slave_transfer_handle::u8State
i2c_slave_transfer_callback_t _i2c_slave_transfer_handle::pfCallback
status_t _i2c_slave_transfer_handle::completionStatus

This parameter is only useful when eEvent is kI2C_SlaveCompletionEvent.

void* _i2c_slave_transfer_handle::pUserData

Macro Definition Documentation

#define FSL_I2C_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
#define I2C_RETRY_TIMES   0U /* Default defines to zero, driver keeps checking status flag untill it changes. */
#define I2C_SMBUS_ENABLE   0U /* Default defines to zero, driver uses simple I2C transfer. */
#define I2C_MASTER_FACK_CONTROL   0U /* Default defines to zero means master will send ack automatically. */

This is used to lower transfer speed by clock stretch for MCU with FSL_FEATURE_I2C_HAS_DOUBLE_BUFFERING supported and enabled.

Typedef Documentation

This structure includes all the master operation needed features, user can configure these features one by one manually, or call I2C_MasterGetDefaultConfig to set the structure to default value. Then, call I2C_MasterInit to initialize I2C module. After initialization, the I2C module can only operate as master. To deinitialize I2C, call I2C_MasterDeinit.

This structure includes all the slave operation needed features, user can configure these features one by one manually, or call I2C_SlaveGetDefaultConfig to set the structure to default value. Then, call I2C_SlaveInit to initialize I2C module. After initialization, the I2C module can only operate as slave. To deinitialize I2C, call I2C_SlaveDeinit.

typedef struct _i2c_config i2c_config_t

This structure includes all I2C features, user can configure user can configure these features one by one manually, or call I2C_GetDefaultConfig to set the structure to default value. Then, call I2C_Init to initialize I2C module. To deinitialize I2C, call I2C_Deinit.

This structure definition includes all the user configurable features, that are used to control single I2C transfer of master mode, in polling way or in interrupt way.

typedef void(* i2c_master_transfer_callback_t)(i2c_master_transfer_handle_t *psHandle)

Defines the interface of user callback function used in master interrupt transfer. The callback function shall be defined and declared in application level by user. Before starting master transfer by calling I2C_MasterTransferNonBlocking, call I2C_MasterTransferCreateHandle to install the user callback. When master transfer ends successfully or failed due to any event like arbitration lost or nacked by slave, user callback will be invoked by driver. And then user can decide what to do next in the callback according to its parameter completionStatus which indicates how the transfer ends.

Parameters
psHandleI2C transfer handle, which contains the information of base pointer, completionStatus and user data.

This enumeration lists all the protocol level events that may happen during slave transfer. They can be used for two related purposes:

  1. User can select certain events and combined them by OR operation to form a mask, and use the mask to configure slave transfer configuration stucture i2c_slave_transfer_t::u8EventMask. If any of these selected events happens, driver will alert user by invoking callback.
  2. When slave callback is invoked, user has to know which specific event occured. Callback uses slave transfer configuration structure i2c_slave_transfer_t as 2nd parameter, its member i2c_slave_transfer_t::eEvent shows which event just happened.

Covers slave transfer data buffer pointer, data size and the events user want driver to alert.

Note
Unlike master who controls the transfer flow, slave has to monitor any bus event and change its configuration accordingly. So this slave transfer configuration structure is also used as second parameter of callback, for user to change the transfer configuration in the callback. The read-only member eEvent shows which event occured that causes the callback being invoked.
typedef void(* i2c_slave_transfer_callback_t)(i2c_slave_transfer_handle_t *psHandle)

Defines the interface of slave user callback function. The callback function shall be defined and declared in application level by user. Before calling I2C_SlaveTransferNonBlocking to let I2C slave ready to process bus events, call I2C_SlaveTransferCreateHandle first to install the user callback to slave handle. When I2C slave meets user selected events, callback will be invoked and user can decide the following steps in the callback. All the events that can trigger callback are listed in i2c_slave_transfer_event_t.

Parameters
psHandleI2C transfer handle, which contains the information of base pointer, completionStatus transfer data, data length and user data.

Enumeration Type Documentation

anonymous enum
Enumerator
kStatus_I2C_Busy 

I2C bus is busy.

kStatus_I2C_Idle 

I2C Bus is idle.

kStatus_I2C_Nak 

I2C detected NACK on bus.

When in SMBus mode, this means the receiver nacks transmitter before PEC byte.

kStatus_I2C_ArbitrationLost 

I2C lost arbitration during addressing.

kStatus_I2C_Timeout 

Timeout happens when waiting for status flags to change.

kStatus_I2C_Addr_Nak 

NACK was detected during the address probe.

kStatus_I2C_Pec_Error 

Detected NACK for the PEC byte in transmit, or the received PEC does not match with the calculated CRC.

These enumerations can be ORed together to form bit masks. The masks can be used as parameter by I2C_MasterClearStatusFlags and I2C_SlaveClearStatusFlags, or as return value by I2C_MasterGetStatusFlags and I2C_SlaveGetStatusFlags.

Enumerator
kI2C_ReceiveNakFlag 

I2C reveived none ack flag.

kI2C_InterruptPendingFlag 

I2C interrupt pending flag.

Byte transfer complete, address match, arbitration lost, start/stop detection and SMBus timeout can all cause this status bit to set. This flag can be cleared.

kI2C_SlaveTransmitFlag 

I2C slave write/read status flag.

kI2C_RangeAddressMatchInterruptFlag 

Received address is within address range.

This flag can be cleared.

kI2C_ArbitrationLostInterruptFlag 

This flag can be cleared.

kI2C_BusBusyFlag 

I2C bus busy flag.

kI2C_AddressAsSlaveInterruptFlag 

Addressed as slave, including general call, alert response, primary/secondary address and range address match.

This flag can be cleared.

kI2C_ByteTransferCompleteInterruptFlag 

I2C trasfer complete flag.

kI2C_StopDetectInterruptFlag 

This flag can be cleared.

kI2C_StartDetectInterruptFlag 

This flag can be cleared.

kI2C_SclLowTimeoutFlag 

I2C SCL signal low timeout flag.

This flag can be cleared.

kI2C_BusIdleFlag 

I2C SCL and SDA both high timeout flag indicating bus idle.

kI2C_SdaLowTimeoutInterruptFlag 

I2C SDA signal low timeout flag.

This flag can be cleared.

kI2C_StatusAllFlags 

All flags which are clearable.

These enumerations can be ORed together to form bit masks. The masks can be used as parameter by I2C_EnableInterrupts, I2C_DisableInterrupts, or as return value by I2C_GetEnabledInterrupts.

Enumerator
kI2C_GlobalInterruptEnable 

I2C global interrupt.

kI2C_StartStopDetectInterruptEnable 

I2C start&stop detect interrupt.

kI2C_SdaLowTimeoutInterruptEnable 

I2C SDA low timeout interrupt.

Enumerator
kI2C_AddressMatch 

7-bit addressing mode.

kI2C_AddressRangeMatch 

Range address match addressing mode.

kI2C_AddressMatch10bit 

10-bit addressing mode.

Enumerator
kI2C_Read 

I2C read data from bus.

kI2C_Write 

I2C write data to bus.

These flags can be ORed together to form bit mask. The mask is used to configure master transfer's start/stop condition in i2c_master_transfer_t::u8ControlFlagMask.

Enumerator
kI2C_TransferStartStopFlag 

A transfer starts with a start signal, stops with a stop signal.

kI2C_TransferNoStartFlag 

A transfer starts without a start signal, only support write only or write+read with no start flag, do not support read only with no start flag.

kI2C_TransferRepeatedStartFlag 

A transfer starts with a repeated start signal.

kI2C_TransferNoStopFlag 

A transfer ends without a stop signal.

Enumerator
kI2C_MasterTransmit 

Master transmits data to slave.

kI2C_MasterReceive 

Master receives data from slave.

This enumeration lists all the protocol level events that may happen during slave transfer. They can be used for two related purposes:

  1. User can select certain events and combined them by OR operation to form a mask, and use the mask to configure slave transfer configuration stucture i2c_slave_transfer_t::u8EventMask. If any of these selected events happens, driver will alert user by invoking callback.
  2. When slave callback is invoked, user has to know which specific event occured. Callback uses slave transfer configuration structure i2c_slave_transfer_t as 2nd parameter, its member i2c_slave_transfer_t::eEvent shows which event just happened.
Enumerator
kI2C_SlaveAddressMatchEvent 

Slave detects general call or alert response address, or primary/secondary/range address is matched after a start or repeated start.

kI2C_SlaveOutofTransmitDataEvent 

Slave runs out of data to transmit, request a new data buffer.

kI2C_SlaveOutofReceiveSpaceEvent 

Slave runs out of space to store received data, request a new data buffer.

kI2C_SlaveStartEvent 

A start/repeated start was detected.

kI2C_SlaveCompletionEvent 

Slave detects a stop signal, or slave is nacked by master during master-receive, or slave has finished transmit/receive previously configured amount of data.

kI2C_SlaveGenaralcallEvent 

Received the general call address after a start or repeated start.

kI2C_SlaveAllEvents 

A bit mask of all available events.

Function Documentation

void I2C_MasterGetDefaultConfig ( i2c_master_config_t *  psMasterConfig,
uint32_t  u32SrcClockHz 
)

The purpose of this API is to initialize the configuration structure to default value for I2C_MasterInit to use. Use the unchanged structure in I2C_MasterInit or modify the structure before calling I2C_MasterInit. This is an example:

* I2C_MasterGetDefaultConfig(&config, 12000000U);
* config.u32BaudRateBps = 100000;
* I2C_MasterInit(I2C0, &config);
*
Parameters
psMasterConfigPointer to the master configuration structure.
u32SrcClockHzThe clock source frequency for I2C module.
void I2C_MasterInit ( I2C_Type *  base,
const i2c_master_config_t *  psMasterConfig 
)

This API initialize the I2C module for master operation, including the feature configuration of high drive capacity, doubble buffer, glitch filter, SCL timeout value, stop hold off enable and transfer baudrate. User can also configure whether to enable the module in the function.

Note
If FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL is enbaled by user, the init function will not ungate I2C clock source before initialization, to avoid hardfault, user has to manually enable ungate the clock source before calling the API

The configuration structure can be filled manully or be set with default values by calling I2C_MasterGetDefaultConfig. This is an example.

* I2C_MasterGetDefaultConfig(&config, 12000000U);
* I2C_MasterInit(I2C0, &config);
*
Parameters
baseI2C base pointer
psMasterConfigPointer to the master configuration structure
void I2C_MasterDeinit ( I2C_Type *  base)

Call this API to disable the I2C module.

Parameters
baseI2C base pointer
void I2C_SlaveGetDefaultConfig ( i2c_slave_config_t *  psSlaveConfig,
uint16_t  u16PrimaryAddress,
uint32_t  u32SrcClockHz 
)

The purpose of this API is to initialize the configuration structure for I2C_SlaveInit to use. Use the unchanged initialized structure in I2C_SlaveInit or modify the structure before calling I2C_SlaveInit. This is an example.

* I2C_SlaveGetDefaultConfig(&config, 0x23U, 12000000U);
*
Parameters
psSlaveConfigPointer to the slave configuration structure.
u16PrimaryAddressFor 7-bit address low 7-bit is used, for 10-bit address low 10-bit is used.
u32SrcClockHzThe clock source frequency for I2C module.
void I2C_SlaveInit ( I2C_Type *  base,
const i2c_slave_config_t *  psSlaveConfig 
)

This API initialize the I2C module for slave operation, including the feature configuration of high drive capacity, doubble buffer, glitch filter, SCL timeout value, stop hold off enable, addressing mode, alert response/general call minitoring, auto baudrate control, low power mode wake up, SCL/SDA setup and hold time. User can also configure whether to enable the module in the function.

Note
If FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL is enbaled by user, the init function will not ungate I2C clock source before initialization, to avoid hardfault, user has to manually enable ungate the clock source before calling the API

The configuration structure can be filled manully or be set with default values by calling I2C_SlaveGetDefaultConfig. This is an example.

* I2C_SlaveGetDefaultConfig(&sConfig, 12000000U);
* sConfig.u8PrimaryAddress = 0x2AU;
* I2C_SlaveInit(I2C0, &sConfig);
*
Parameters
baseI2C base pointer
psSlaveConfigPointer to the slave configuration structure
static void I2C_SlaveDeinit ( I2C_Type *  base)
inlinestatic

Call this API to disable the I2C module.

Parameters
baseI2C base pointer
void I2C_GetDefaultConfig ( i2c_config_t *  psConfig,
uint16_t  u16PrimaryAddress,
uint32_t  u32SrcClockHz 
)

The purpose of this API is to initialize the configuration structure for I2C_Init to use. Use the unchanged initialized structure in I2C_Init or modify the structure before calling I2C_Init. This is an example.

* i2c_config_t config;
* I2C_GetDefaultConfig(&config, 0x23U, 12000000U);
*
Parameters
psConfigPointer to the slave configuration structure.
u16PrimaryAddressFor 7-bit address low 7-bit is used, for 10-bit address low 10-bit is used.
u32SrcClockHzThe clock source frequency for I2C module.
void I2C_Init ( I2C_Type *  base,
const i2c_config_t *  psConfig 
)

This API initialize the I2C module, including the feature configuration of high drive capacity, doubble buffer, glitch filter, SCL timeout value, stop hold off enable, addressing mode, alert response/general call minitoring, auto baudrate control, low power mode wake up and baudrate. User can also configure whether to enable the module in the function.

Note
If FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL is enbaled by user, the init function will not ungate I2C clock source before initialization, to avoid hardfault, user has to manually enable ungate the clock source before calling the API

The configuration structure can be filled manully or be set with default values by calling I2C_GetDefaultConfig. This is an example.

* i2c_config_t sConfig;
* I2C_GetDefaultConfig(&sConfig, 0x23U, 12000000U);
* I2C_Init(I2C0, &sConfig);
*
Parameters
baseI2C base pointer
psConfigPointer to the I2C configuration structure
static void I2C_Deinit ( I2C_Type *  base)
inlinestatic

Call this API to disable the I2C module.

Parameters
baseI2C base pointer
uint16_t I2C_MasterGetStatusFlags ( I2C_Type *  base)
Parameters
baseI2C base pointer
Returns
the mask of status flags, can be a single flag or several flags in _i2c_status_flags ORed together.
static void I2C_MasterClearStatusFlags ( I2C_Type *  base,
uint16_t  u16StatusFlags 
)
inlinestatic
Parameters
baseI2C base pointer
u16StatusFlagsThe status flag mask, can be a single flag or several flags in _i2c_status_flags ORed together. These flags among _i2c_status_flags can be cleared:
  • kI2C_StartDetectInterruptFlag (only supported on certain SoCs)
  • kI2C_StopDetectInterruptFlag (only supported on certain SoCs)
  • kI2C_ArbitrationLostInterruptFlag
  • kI2C_InterruptPendingFlag
  • kI2C_RangeAddressMatchInterruptFlag
  • kI2C_AddressAsSlaveInterruptFlag
  • kI2C_SclLowTimeoutFlag
  • kI2C_SdaLowTimeoutInterruptFlag
static uint16_t I2C_SlaveGetStatusFlags ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
the mask of status flags, can be a single flag or several flags in _i2c_status_flags ORed together.
static void I2C_SlaveClearStatusFlags ( I2C_Type *  base,
uint16_t  u16StatusFlags 
)
inlinestatic
Parameters
baseI2C base pointer
u16StatusFlagsThe status flag mask, can be a single flag or several flags in _i2c_status_flags ORed together. These flags among _i2c_status_flags can be cleared:
  • kI2C_StartDetectInterruptFlag (only supported on certain SoCs)
  • kI2C_StopDetectInterruptFlag (only supported on certain SoCs)
  • kI2C_ArbitrationLostInterruptFlag
  • kI2C_InterruptPendingFlag
  • kI2C_RangeAddressMatchInterruptFlag
  • kI2C_AddressAsSlaveInterruptFlag
  • kI2C_SclLowTimeoutFlag
  • kI2C_SdaLowTimeoutInterruptFlag
void I2C_EnableInterrupts ( I2C_Type *  base,
uint8_t  u8Interrupts 
)
Note
Before enabling kI2C_GlobalInterruptEnable, check kI2C_RangeAddressMatchInterruptFlag and kI2C_AddressAsSlaveInterruptFlag first, because any write operation on C1 will clear these 2 bits.
Parameters
baseI2C base pointer
u8InterruptsThe interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together.
void I2C_DisableInterrupts ( I2C_Type *  base,
uint8_t  u8Interrupts 
)
Note
Before disabling kI2C_GlobalInterruptEnable, check kI2C_RangeAddressMatchInterruptFlag and kI2C_AddressAsSlaveInterruptFlag first, because any write operation on C1 will clear these 2 bits.
Parameters
baseI2C base pointer
u8InterruptsThe interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together.
uint8_t I2C_GetEnabledInterrupts ( I2C_Type *  base)
Parameters
baseI2C base pointer
Returns
The interrupt source mask, can be a single source or several sources in _i2c_interrupt_enable ORed together.
static bool I2C_IsMaster ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
True for master mode, false for slave mode.
static void I2C_Reset ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
static void I2C_Enable ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnablePass true to enable and false to disable the module.
static void I2C_EnableFastAck ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic

When enbled, writing 0/1 to TXAK generates an ACK/NACK after receiving a data byte, when disabled, writing 0/1 to TXAK generates an ACK/NACK on the following receiving data byte.

Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_EnableHighDrive ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_EnableStopHold ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_SetTransferDirection ( I2C_Type *  base,
i2c_data_direction_t  eDataDirection 
)
inlinestatic
Parameters
baseI2C base pointer
eDataDirectionkI2C_Write to write data to bus, kI2C_Read to read data from bua
void I2C_SetSclTimeoutValue ( I2C_Type *  base,
uint16_t  u16SclTimout_Ms,
uint32_t  u32SrcClockHz 
)

After the I2C module is initialized, user can call this function to change the timeout value.

param base I2C base pointer. param u16SclTimout_Ms The SCL timeout value in ms. param u32SrcClockHz I2C peripheral clock frequency in Hz

void I2C_SetGlitchFilter ( I2C_Type *  base,
uint16_t  u16GlitchFilter_Ns,
uint32_t  u32SrcClockHz 
)

After the I2C module is initialized as master, user can call this function to change the glitch filter width.

param base I2C base pointer. param u16GlitchFilter_Ns The GLitch filter length in nano seconds. param u32SrcClockHz I2C peripheral clock frequency in Hz

static void I2C_EnableDMA ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnabletrue to enable, false to disable
static uint32_t I2C_GetDataRegAddr ( I2C_Type *  base)
inlinestatic

This API is used to provide the transfer address for I2C DMA transfer.

Parameters
baseI2C base pointer
Returns
data register address
static void I2C_SlaveEnableAlertResponse ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic

When enbled, I2C slave will monitor the bus line, and when alert response address is received address match status flag will be set.

Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_SlaveEnableSecondaryAddress ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_SlaveEnableGeneralCall ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
static void I2C_SlaveEnableWakeUp ( I2C_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseI2C base pointer
bEnableTrue to enable, false to disable.
void I2C_SlaveSetAddressingMode ( I2C_Type *  base,
i2c_slave_address_mode_t  eAddressingMode,
uint16_t  u16Address,
uint8_t  u8MaxAddress 
)

After the I2C module is initialized as slave, user can call this function to change the configuration of slave addressing mode.

Parameters
baseI2C base pointer.
eAddressingModeThe slave addressing mode, single address or range address.
u16AddressI2C slave address. For 7-bit address low 7-bit is used, for 10-bit address low 10-bit is used.
u8MaxAddressThe maximum boundary of slave address used in a range address match.
void I2C_MasterSetBaudRate ( I2C_Type *  base,
uint32_t  u32BaudRateBps,
uint32_t  u32SrcClockHz 
)

After the I2C module is initialized as master, user can call this function to change the transfer baud rate.

Parameters
baseI2C base pointer.
u32BaudRateBpsthe baud rate value in bits-per-second.
u32SrcClockHzI2C peripheral clock frequency in Hz
static uint8_t I2C_ReadByte ( I2C_Type *  base)
inlinestatic
Parameters
baseI2C base pointer
Returns
The data read from data register.
static void I2C_WriteByte ( I2C_Type *  base,
uint8_t  u8Data 
)
inlinestatic
Parameters
baseI2C base pointer
u8DataThe byte to write.
static void I2C_SendAck ( I2C_Type *  base,
bool  bIsAck 
)
inlinestatic
Parameters
baseI2C base pointer
bIsAckTrue to send ACK signal, false to send NACK signal
status_t I2C_MasterStart ( I2C_Type *  base,
uint8_t  u8Address,
i2c_master_transfer_direction_t  eDirection 
)

This function is used to initiate a new transfer in master mode, by sending a START signal, then the slave address with transmit/receive bit to I2C bus.

Note
The return value of this API only indicates whether the start signal is sent to bus, user has to check kI2C_ArbitrationLostInterruptFlag and kI2C_ReceiveNakFlag using I2C_MasterClearStatusFlags to see if valid slave device is avaliable or the aribitration is lost.
Parameters
baseI2C base pointer
u8Address7-bit slave device address.
eDirectionMaster transfer directions(transmit/receive).
Return values
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
kStatus_SuccessSuccessfully send the start signal.
kStatus_I2C_BusyCurrent bus is busy.
status_t I2C_MasterRepeatedStart ( I2C_Type *  base,
uint8_t  u8Address,
i2c_master_transfer_direction_t  eDirection 
)
Parameters
baseI2C peripheral base pointer
u8Address7-bit slave device address.
eDirectionMaster transfer directions(transmit/receive).
Return values
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
kStatus_SuccessSuccessfully send the start signal.
kStatus_I2C_BusyCurrent bus is busy but not occupied by current I2C master.
status_t I2C_MasterStop ( I2C_Type *  base)
Parameters
baseI2C base pointer
Return values
kStatus_SuccessSuccessfully send the stop signal.
kStatus_I2C_TimeoutSend stop signal failed, timeout.
status_t I2C_MasterWriteBlocking ( I2C_Type *  base,
const uint8_t *  pu8Data,
uint16_t  txSize,
bool  bSendStop 
)

Call this function when using I2C as master to send certain bytes of data to bus when start signal is already sent. User can specify whether to send a stop siganl after the data. This function uses the blocking way, which means it does not return until all the data is sent to bus and stop signal is successfully issued(if user configures the stop signal).

Parameters
baseI2C base pointer.
pu8DataThe pointer to the data to be transmitted.
txSizeThe length in bytes of the data to be transmitted.
bSendStopWhether to send stop signal after the data transfer.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_ArbitrationLostTransfer error, arbitration lost.
kStatus_I2C_NakTransfer error, receive NAK during transfer.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
status_t I2C_MasterReadBlocking ( I2C_Type *  base,
uint8_t *  pu8RxBuff,
uint16_t  rxSize,
bool  bSendStop 
)

Call this function when using I2C as master to receive certain bytes of data from bus when start signal is already sent. User can specify whether to send a stop siganl after the data. This function uses the blocking way, which means it does not return until all the data has been received and stop signal is successfully issued(if user configures the stop signal).

Note
If user configures to send stop signal after the data, this function stops the bus before reading the final byte from data register. Without stopping the bus prior to the final read, the bus will issue another read, resulting in garbage data being read into the data register.
Parameters
baseI2C base pointer.
pu8RxBuffThe pointer to the data to store the received data.
rxSizeThe length in bytes of the data to be received.
bSendStopWhether to send stop signal after the data transfer.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_TimeoutSend stop signal failed, timeout.
status_t I2C_SlaveWriteBlocking ( I2C_Type *  base,
const uint8_t *  pu8TxBuff,
uint16_t  txSize 
)

Call this funtion to let I2C slave poll register status until it is addressed, then slave sends txSize of data to bus until all the data has been sent to bus or untill it is nacked.

Parameters
baseI2C base pointer.
pu8TxBuffThe pointer to the data to be transferred.
txSizeThe length in bytes of the data to be transferred.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_ArbitrationLostTransfer error, arbitration lost.
kStatus_I2C_NakTransfer error, receive NAK during transfer.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
status_t I2C_SlaveReadBlocking ( I2C_Type *  base,
uint8_t *  pu8RxBuff,
uint16_t  rxSize 
)

Call this funtion to let I2C slave poll register status until it is addressed, then slave receives rxSize of data until all the data has been received.

Parameters
baseI2C base pointer.
pu8RxBuffThe pointer to the data to store the received data.
rxSizeThe length in bytes of the data to be received.
Return values
kStatus_SuccessSuccessfully complete data receive.
kStatus_I2C_TimeoutWait status flag timeout.
status_t I2C_MasterTransferBlocking ( I2C_Type *  base,
i2c_master_transfer_t *  psTransferConfig 
)
Note
The API does not return until the transfer succeeds or fails due to arbitration lost or receiving a NAK.
Parameters
baseI2C peripheral base address.
psTransferConfigPointer to the transfer configuration structure.
Return values
kStatus_SuccessSuccessfully complete the data transmission.
kStatus_I2C_BusyPrevious transmission still not finished.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flagsto change.
kStatus_I2C_ArbitrationLostTransfer error, arbitration lost.
kStatus_I2C_NakTransfer error, receive NAK during transfer.
void I2C_MasterTransferCreateHandle ( I2C_Type *  base,
i2c_master_transfer_handle_t *  psHandle,
i2c_master_transfer_callback_t  pfCallback,
void *  pUserData 
)

This function is responsible for initializig master transfer psHandle, installing user callback, registering master IRQ handling function and opening global interrupt.

Parameters
baseI2C base pointer.
psHandlepointer to i2c_master_transfer_handle_t structure to store the transfer state.
pfCallbackpointer to user callback function.
pUserDataUser configurable pointer to any data, function, structure etc that user wish to use in the callback
status_t I2C_MasterTransferNonBlocking ( i2c_master_transfer_handle_t *  psHandle,
i2c_master_transfer_t *  psTransferConfig 
)
Note
Transfer in interrupt way is non-blocking which means this API returns immediately after transfer initiates. User can call I2C_MasterTransferGetCount to get the count of data that master has transmitted/received and check transfer status. If the return status is kStatus_NoTransferInProgress, the transfer is finished. Also if user installs a user callback when calling I2C_MasterTransferCreateHandle before, the callback will be invoked when transfer finishes.
Parameters
psHandlepointer to i2c_master_transfer_handle_t structure which stores the transfer state.
psTransferConfigPointer to the transfer configuration structure.
Return values
kStatus_SuccessSuccessfully start the data transmission.
kStatus_I2C_BusyPrevious transmission still not finished.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flagsto change.
status_t I2C_MasterTransferGetCount ( i2c_master_transfer_handle_t *  psHandle,
uint16_t *  count 
)
Parameters
psHandlepointer to i2c_master_transfer_handle_t structure which stores the transfer state.
countPointer to number of bytes transferred so far by the non-blocking transaction.
Return values
kStatus_InvalidArgumentcount is Invalid.
kStatus_NoTransferInProgressCurent no transfer is in progress.
kStatus_SuccessSuccessfully obtained the count.
status_t I2C_MasterTransferAbort ( i2c_master_transfer_handle_t *  psHandle)
Note
This API can be called at any time after a transfer of interrupt way initiates and before it finishes to abort the transfer early.
Parameters
psHandlepointer to i2c_master_transfer_handle_t structure which stores the transfer state
Return values
kStatus_I2C_BusyMaster lost arbitration, bus is in use by other master.
kStatus_I2C_TimeoutTransfer error, timeout happens when waiting for status flags to change.
kStatus_SuccessSuccessfully abort the transfer.
void I2C_SlaveTransferCreateHandle ( I2C_Type *  base,
i2c_slave_transfer_handle_t *  psHandle,
i2c_slave_transfer_callback_t  pfCallback,
void *  pUserData 
)

This function is responsible for initializig slave transfer handle, installing user callback, registering slave IRQ handling function and opening global interrupt.

Parameters
baseI2C base pointer.
psHandlepointer to i2c_slave_transfer_handle_t structure to store the transfer state.
pfCallbackpointer to user callback function.
pUserDataUser configurable pointer to any data, function, structure etc that user wish to use in the callback
status_t I2C_SlaveTransferNonBlocking ( i2c_slave_transfer_handle_t *  psHandle,
i2c_slave_transfer_t *  psTransferConfig 
)

Call this API to let I2C start monitoring bus events driven by I2C master on bus. When user specified event occurs, callback will be invoked passes event information to the callback.

Note
When kI2C_SlaveOutofTransmitDataEvent and kI2C_SlaveOutofReceiveSpaceEvent occured, slave callback will always be revoked regardless which events user choose to enable. This means user need not configure them in the psTransferConfig. If user wants to enable all the events, use kI2C_SlaveAllEvents for convenience.
Parameters
psHandlePointer to i2c_slave_transfer_handle_t structure which stores the transfer state.
psTransferConfigI2C transfer configuration.
Return values
kStatus_SuccessI2C slave set to standby state successfully and ready to process events.
kStatus_I2C_BusyI2C slave has already been started on this handle.
status_t I2C_SlaveTransferGetCount ( i2c_slave_transfer_handle_t *  psHandle,
uint16_t *  count 
)
Parameters
psHandlepointer to i2c_slave_transfer_handle_t structure.
countNumber of bytes slave have transferred after the last start/repeated start.
Return values
kStatus_InvalidArgumentcount is Invalid.
kStatus_NoTransferInProgressCurent no transfer is in progress.
kStatus_SuccessSuccessfully obtained the count.
void I2C_SlaveTransferAbort ( i2c_slave_transfer_handle_t *  psHandle)
Note
This API can be called at any time to stop slave for handling further bus events.
Parameters
psHandlepointer to i2c_slave_transfer_handle_t structure which stores the transfer state.
uint32_t I2C_GetInstance ( I2C_Type *  base)
Parameters
baseI2C base pointer.
Return values
Thenumber of the instance.