MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages

Overview

This section describes the programming interface of the DSPI peripheral driver. The DSPI driver configures DSPI module and provides functional and transactional interfaces to build the DSPI application.

Data Structures

struct  _dspi_master_edma_handle
 DSPI master eDMA transfer handle structure used for the transactional API. More...
 
struct  _dspi_slave_edma_handle
 DSPI slave eDMA transfer handle structure used for the transactional API. More...
 

Macros

#define DSPI_EDMA_MAX_TRANSFER_SIZE(base, width)
 DSPI EDMA max transfer data size calculate. More...
 

Typedefs

typedef struct
_dspi_master_edma_handle 
dspi_master_edma_handle_t
 Forward declaration of the DSPI eDMA master handle typedefs.
 
typedef struct
_dspi_slave_edma_handle 
dspi_slave_edma_handle_t
 Forward declaration of the DSPI eDMA slave handle typedefs.
 
typedef void(* dspi_master_edma_transfer_callback_t )(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData)
 Completion callback function pointer type. More...
 
typedef void(* dspi_slave_edma_transfer_callback_t )(SPI_Type *base, dspi_slave_edma_handle_t *handle, status_t status, void *userData)
 Completion callback function pointer type. More...
 

Driver version

#define FSL_DSPI_EDMA_DRIVER_VERSION   (MAKE_VERSION(2, 2, 6))
 DSPI EDMA driver version 2.2.6.
 

Transactional APIs

void DSPI_MasterTransferCreateHandleEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, dspi_master_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToIntermediaryHandle, edma_handle_t *edmaIntermediaryToTxRegHandle)
 Initializes the DSPI master eDMA handle. More...
 
status_t DSPI_MasterTransferEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, dspi_transfer_t *transfer)
 DSPI master transfer data using eDMA. More...
 
status_t DSPI_MasterHalfDuplexTransferEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, dspi_half_duplex_transfer_t *xfer)
 Transfers a block of data using a eDMA method. More...
 
void DSPI_MasterTransferAbortEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle)
 DSPI master aborts a transfer which is using eDMA. More...
 
status_t DSPI_MasterTransferGetCountEDMA (SPI_Type *base, dspi_master_edma_handle_t *handle, size_t *count)
 Gets the master eDMA transfer count. More...
 
void DSPI_SlaveTransferCreateHandleEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, dspi_slave_edma_transfer_callback_t callback, void *userData, edma_handle_t *edmaRxRegToRxDataHandle, edma_handle_t *edmaTxDataToTxRegHandle)
 Initializes the DSPI slave eDMA handle. More...
 
status_t DSPI_SlaveTransferEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, dspi_transfer_t *transfer)
 DSPI slave transfer data using eDMA. More...
 
void DSPI_SlaveTransferAbortEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle)
 DSPI slave aborts a transfer which is using eDMA. More...
 
status_t DSPI_SlaveTransferGetCountEDMA (SPI_Type *base, dspi_slave_edma_handle_t *handle, size_t *count)
 Gets the slave eDMA transfer count. More...
 

Data Structure Documentation

struct _dspi_master_edma_handle

Data Fields

uint32_t bitsPerFrame
 The desired number of bits per frame. More...
 
volatile uint32_t command
 The desired data command. More...
 
volatile uint32_t lastCommand
 The desired last data command. More...
 
uint8_t fifoSize
 FIFO dataSize. More...
 
volatile bool isPcsActiveAfterTransfer
 Indicates whether the PCS signal keeps active after the last frame transfer. More...
 
uint8_t nbytes
 eDMA minor byte transfer count initially configured. More...
 
volatile uint8_t state
 DSPI transfer state, see _dspi_transfer_state. More...
 
const uint8_t *volatile txData
 Send buffer. More...
 
uint8_t *volatile rxData
 Receive buffer. More...
 
volatile size_t remainingSendByteCount
 A number of bytes remaining to send. More...
 
volatile size_t remainingReceiveByteCount
 A number of bytes remaining to receive. More...
 
size_t totalByteCount
 A number of transfer bytes.
 
uint32_t rxBuffIfNull
 Used if there is not rxData for DMA purpose. More...
 
uint32_t txBuffIfNull
 Used if there is not txData for DMA purpose. More...
 
dspi_master_edma_transfer_callback_t callback
 Completion callback. More...
 
void * userData
 Callback user data. More...
 
edma_handle_t * edmaRxRegToRxDataHandle
 edma_handle_t handle point used for RxReg to RxData buff
 
edma_handle_t * edmaTxDataToIntermediaryHandle
 edma_handle_t handle point used for TxData to Intermediary
 
edma_handle_t * edmaIntermediaryToTxRegHandle
 edma_handle_t handle point used for Intermediary to TxReg
 
edma_tcd_t dspiSoftwareTCD [2]
 SoftwareTCD , internal used.
 

Field Documentation

uint32_t _dspi_master_edma_handle::bitsPerFrame
volatile uint32_t _dspi_master_edma_handle::command
volatile uint32_t _dspi_master_edma_handle::lastCommand
uint8_t _dspi_master_edma_handle::fifoSize
volatile bool _dspi_master_edma_handle::isPcsActiveAfterTransfer
uint8_t _dspi_master_edma_handle::nbytes
volatile uint8_t _dspi_master_edma_handle::state
const uint8_t* volatile _dspi_master_edma_handle::txData
uint8_t* volatile _dspi_master_edma_handle::rxData
volatile size_t _dspi_master_edma_handle::remainingSendByteCount
volatile size_t _dspi_master_edma_handle::remainingReceiveByteCount
uint32_t _dspi_master_edma_handle::rxBuffIfNull
uint32_t _dspi_master_edma_handle::txBuffIfNull
dspi_master_edma_transfer_callback_t _dspi_master_edma_handle::callback
void* _dspi_master_edma_handle::userData
struct _dspi_slave_edma_handle

Data Fields

uint32_t bitsPerFrame
 The desired number of bits per frame. More...
 
const uint8_t *volatile txData
 Send buffer. More...
 
uint8_t *volatile rxData
 Receive buffer. More...
 
volatile size_t remainingSendByteCount
 A number of bytes remaining to send. More...
 
volatile size_t remainingReceiveByteCount
 A number of bytes remaining to receive. More...
 
size_t totalByteCount
 A number of transfer bytes.
 
uint32_t rxBuffIfNull
 Used if there is not rxData for DMA purpose. More...
 
uint32_t txBuffIfNull
 Used if there is not txData for DMA purpose. More...
 
uint32_t txLastData
 Used if there is an extra byte when 16bits per frame for DMA purpose. More...
 
uint8_t nbytes
 eDMA minor byte transfer count initially configured. More...
 
volatile uint8_t state
 DSPI transfer state. More...
 
dspi_slave_edma_transfer_callback_t callback
 Completion callback. More...
 
void * userData
 Callback user data. More...
 
edma_handle_t * edmaRxRegToRxDataHandle
 edma_handle_t handle point used for RxReg to RxData buff
 
edma_handle_t * edmaTxDataToTxRegHandle
 edma_handle_t handle point used for TxData to TxReg
 

Field Documentation

uint32_t _dspi_slave_edma_handle::bitsPerFrame
const uint8_t* volatile _dspi_slave_edma_handle::txData
uint8_t* volatile _dspi_slave_edma_handle::rxData
volatile size_t _dspi_slave_edma_handle::remainingSendByteCount
volatile size_t _dspi_slave_edma_handle::remainingReceiveByteCount
uint32_t _dspi_slave_edma_handle::rxBuffIfNull
uint32_t _dspi_slave_edma_handle::txBuffIfNull
uint32_t _dspi_slave_edma_handle::txLastData
uint8_t _dspi_slave_edma_handle::nbytes
volatile uint8_t _dspi_slave_edma_handle::state
dspi_slave_edma_transfer_callback_t _dspi_slave_edma_handle::callback
void* _dspi_slave_edma_handle::userData

Macro Definition Documentation

#define DSPI_EDMA_MAX_TRANSFER_SIZE (   base,
  width 
)
Value:
((1 == FSL_FEATURE_DSPI_HAS_SEPARATE_DMA_RX_TX_REQn(base)) ? ((width > 8U) ? 65534U : 32767U) : \
((width > 8U) ? 1022U : 511U))
Parameters
baseDSPI peripheral base address.
widthTransfer width

Typedef Documentation

typedef void(* dspi_master_edma_transfer_callback_t)(SPI_Type *base, dspi_master_edma_handle_t *handle, status_t status, void *userData)
Parameters
baseDSPI peripheral base address.
handleA pointer to the handle for the DSPI master.
statusSuccess or error code describing whether the transfer completed.
userDataAn arbitrary pointer-dataSized value passed from the application.
typedef void(* dspi_slave_edma_transfer_callback_t)(SPI_Type *base, dspi_slave_edma_handle_t *handle, status_t status, void *userData)
Parameters
baseDSPI peripheral base address.
handleA pointer to the handle for the DSPI slave.
statusSuccess or error code describing whether the transfer completed.
userDataAn arbitrary pointer-dataSized value passed from the application.

Function Documentation

void DSPI_MasterTransferCreateHandleEDMA ( SPI_Type *  base,
dspi_master_edma_handle_t *  handle,
dspi_master_edma_transfer_callback_t  callback,
void *  userData,
edma_handle_t *  edmaRxRegToRxDataHandle,
edma_handle_t *  edmaTxDataToIntermediaryHandle,
edma_handle_t *  edmaIntermediaryToTxRegHandle 
)

This function initializes the DSPI eDMA handle which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.

Note
DSPI eDMA has separated (RX and TX as two sources) or shared (RX and TX are the same source) DMA request source.
  • For the separated DMA request source, enable and set the RX DMAMUX source for edmaRxRegToRxDataHandle and TX DMAMUX source for edmaIntermediaryToTxRegHandle.
  • For the shared DMA request source, enable and set the RX/RX DMAMUX source for the edmaRxRegToRxDataHandle.
Parameters
baseDSPI peripheral base address.
handleDSPI handle pointer to _dspi_master_edma_handle.
callbackDSPI callback.
userDataA callback function parameter.
edmaRxRegToRxDataHandleedmaRxRegToRxDataHandle pointer to edma_handle_t.
edmaTxDataToIntermediaryHandleedmaTxDataToIntermediaryHandle pointer to edma_handle_t.
edmaIntermediaryToTxRegHandleedmaIntermediaryToTxRegHandle pointer to edma_handle_t.
status_t DSPI_MasterTransferEDMA ( SPI_Type *  base,
dspi_master_edma_handle_t *  handle,
dspi_transfer_t *  transfer 
)

This function transfers data using eDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.

Note
The max transfer size of each transfer depends on whether the instance's Tx/Rx shares the same DMA request. If FSL_FEATURE_DSPI_HAS_SEPARATE_DMA_RX_TX_REQn(x) is true, then the max transfer size is 32767 datawidth of data, otherwise is 511.
Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_master_edma_handle structure which stores the transfer state.
transferA pointer to the dspi_transfer_t structure.
Returns
status of status_t.
status_t DSPI_MasterHalfDuplexTransferEDMA ( SPI_Type *  base,
dspi_master_edma_handle_t *  handle,
dspi_half_duplex_transfer_t *  xfer 
)

This function transfers data using eDNA, the transfer mechanism is half-duplex. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called.

Parameters
baseDSPI base pointer
handleA pointer to the _dspi_master_edma_handle structure which stores the transfer state.
xferA pointer to the dspi_half_duplex_transfer_t structure.
Returns
status of status_t.
void DSPI_MasterTransferAbortEDMA ( SPI_Type *  base,
dspi_master_edma_handle_t *  handle 
)

This function aborts a transfer which is using eDMA.

Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_master_edma_handle structure which stores the transfer state.
status_t DSPI_MasterTransferGetCountEDMA ( SPI_Type *  base,
dspi_master_edma_handle_t *  handle,
size_t *  count 
)

This function gets the master eDMA transfer count.

Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_master_edma_handle structure which stores the transfer state.
countA number of bytes transferred by the non-blocking transaction.
Returns
status of status_t.
void DSPI_SlaveTransferCreateHandleEDMA ( SPI_Type *  base,
dspi_slave_edma_handle_t *  handle,
dspi_slave_edma_transfer_callback_t  callback,
void *  userData,
edma_handle_t *  edmaRxRegToRxDataHandle,
edma_handle_t *  edmaTxDataToTxRegHandle 
)

This function initializes the DSPI eDMA handle which can be used for other DSPI transactional APIs. Usually, for a specified DSPI instance, call this API once to get the initialized handle.

Note
DSPI eDMA has separated (RN and TX in 2 sources) or shared (RX and TX are the same source) DMA request source.
  • For the separated DMA request source, enable and set the RX DMAMUX source for edmaRxRegToRxDataHandle and TX DMAMUX source for edmaTxDataToTxRegHandle.
  • For the shared DMA request source, enable and set the RX/RX DMAMUX source for the edmaRxRegToRxDataHandle.
Parameters
baseDSPI peripheral base address.
handleDSPI handle pointer to _dspi_slave_edma_handle.
callbackDSPI callback.
userDataA callback function parameter.
edmaRxRegToRxDataHandleedmaRxRegToRxDataHandle pointer to edma_handle_t.
edmaTxDataToTxRegHandleedmaTxDataToTxRegHandle pointer to edma_handle_t.
status_t DSPI_SlaveTransferEDMA ( SPI_Type *  base,
dspi_slave_edma_handle_t *  handle,
dspi_transfer_t *  transfer 
)

This function transfers data using eDMA. This is a non-blocking function, which returns right away. When all data is transferred, the callback function is called. Note that the slave eDMA transfer doesn't support transfer_size is 1 when the bitsPerFrame is greater than eight.

Note
The max transfer size of each transfer depends on whether the instance's Tx/Rx shares the same DMA request. If FSL_FEATURE_DSPI_HAS_SEPARATE_DMA_RX_TX_REQn(x) is true, then the max transfer size is 32767 datawidth of data, otherwise is 511.
Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_slave_edma_handle structure which stores the transfer state.
transferA pointer to the dspi_transfer_t structure.
Returns
status of status_t.
void DSPI_SlaveTransferAbortEDMA ( SPI_Type *  base,
dspi_slave_edma_handle_t *  handle 
)

This function aborts a transfer which is using eDMA.

Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_slave_edma_handle structure which stores the transfer state.
status_t DSPI_SlaveTransferGetCountEDMA ( SPI_Type *  base,
dspi_slave_edma_handle_t *  handle,
size_t *  count 
)

This function gets the slave eDMA transfer count.

Parameters
baseDSPI peripheral base address.
handleA pointer to the _dspi_slave_edma_handle structure which stores the transfer state.
countA number of bytes transferred so far by the non-blocking transaction.
Returns
status of status_t.