MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
I2s_dma_driver

Overview

Data Structures

struct  _i2s_dma_handle
 i2s dma handle More...
 

Typedefs

typedef struct _i2s_dma_handle i2s_dma_handle_t
 Members not to be accessed / modified outside of the driver. More...
 
typedef void(* i2s_dma_transfer_callback_t )(I2S_Type *base, i2s_dma_handle_t *handle, status_t completionStatus, void *userData)
 Callback function invoked from DMA API on completion. More...
 

Driver version

#define FSL_I2S_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 3))
 I2S DMA driver version 2.3.3. More...
 

DMA API

void I2S_TxTransferCreateHandleDMA (I2S_Type *base, i2s_dma_handle_t *handle, dma_handle_t *dmaHandle, i2s_dma_transfer_callback_t callback, void *userData)
 Initializes handle for transfer of audio data. More...
 
status_t I2S_TxTransferSendDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t transfer)
 Begins or queue sending of the given data. More...
 
void I2S_TransferAbortDMA (I2S_Type *base, i2s_dma_handle_t *handle)
 Aborts transfer of data. More...
 
void I2S_RxTransferCreateHandleDMA (I2S_Type *base, i2s_dma_handle_t *handle, dma_handle_t *dmaHandle, i2s_dma_transfer_callback_t callback, void *userData)
 Initializes handle for reception of audio data. More...
 
status_t I2S_RxTransferReceiveDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t transfer)
 Begins or queue reception of data into given buffer. More...
 
void I2S_DMACallback (dma_handle_t *handle, void *userData, bool transferDone, uint32_t tcds)
 Invoked from DMA interrupt handler. More...
 
void I2S_TransferInstallLoopDMADescriptorMemory (i2s_dma_handle_t *handle, void *dmaDescriptorAddr, size_t dmaDescriptorNum)
 Install DMA descriptor memory for loop transfer only. More...
 
status_t I2S_TransferSendLoopDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t *xfer, uint32_t loopTransferCount)
 Send link transfer data using DMA. More...
 
status_t I2S_TransferReceiveLoopDMA (I2S_Type *base, i2s_dma_handle_t *handle, i2s_transfer_t *xfer, uint32_t loopTransferCount)
 Receive link transfer data using DMA. More...
 

Data Structure Documentation

struct _i2s_dma_handle

Data Fields

uint32_t state
 Internal state of I2S DMA transfer.
 
uint8_t bytesPerFrame
 bytes per frame
 
i2s_dma_transfer_callback_t completionCallback
 Callback function pointer.
 
void * userData
 Application data passed to callback.
 
dma_handle_t * dmaHandle
 DMA handle.
 
volatile i2s_transfer_t i2sQueue [I2S_NUM_BUFFERS]
 Transfer queue storing transfer buffers.
 
volatile uint8_t queueUser
 Queue index where user's next transfer will be stored.
 
volatile uint8_t queueDriver
 Queue index of buffer actually used by the driver.
 
dma_descriptor_t * i2sLoopDMADescriptor
 descriptor pool pointer
 
size_t i2sLoopDMADescriptorNum
 number of descriptor in descriptors pool
 

Macro Definition Documentation

#define FSL_I2S_DMA_DRIVER_VERSION   (MAKE_VERSION(2, 3, 3))

Typedef Documentation

typedef void(* i2s_dma_transfer_callback_t)(I2S_Type *base, i2s_dma_handle_t *handle, status_t completionStatus, void *userData)
Parameters
baseI2S base pointer.
handlepointer to I2S transaction.
completionStatusstatus of the transaction.
userDataoptional pointer to user arguments data.

Function Documentation

void I2S_TxTransferCreateHandleDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
dma_handle_t *  dmaHandle,
i2s_dma_transfer_callback_t  callback,
void *  userData 
)
Parameters
baseI2S base pointer.
handlepointer to handle structure.
dmaHandlepointer to dma handle structure.
callbackfunction to be called back when transfer is done or fails.
userDatapointer to data passed to callback.
status_t I2S_TxTransferSendDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
i2s_transfer_t  transfer 
)
Parameters
baseI2S base pointer.
handlepointer to handle structure.
transferdata buffer.
Return values
kStatus_Success
kStatus_I2S_Busyif all queue slots are occupied with unsent buffers.
void I2S_TransferAbortDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle 
)
Parameters
baseI2S base pointer.
handlepointer to handle structure.
void I2S_RxTransferCreateHandleDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
dma_handle_t *  dmaHandle,
i2s_dma_transfer_callback_t  callback,
void *  userData 
)
Parameters
baseI2S base pointer.
handlepointer to handle structure.
dmaHandlepointer to dma handle structure.
callbackfunction to be called back when transfer is done or fails.
userDatapointer to data passed to callback.
status_t I2S_RxTransferReceiveDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
i2s_transfer_t  transfer 
)
Parameters
baseI2S base pointer.
handlepointer to handle structure.
transferdata buffer.
Return values
kStatus_Success
kStatus_I2S_Busyif all queue slots are occupied with buffers which are not full.
void I2S_DMACallback ( dma_handle_t *  handle,
void *  userData,
bool  transferDone,
uint32_t  tcds 
)
Parameters
handlepointer to DMA handle structure.
userDataargument for user callback.
transferDoneif transfer was done.
tcds
void I2S_TransferInstallLoopDMADescriptorMemory ( i2s_dma_handle_t *  handle,
void *  dmaDescriptorAddr,
size_t  dmaDescriptorNum 
)

This function used to register DMA descriptor memory for the i2s loop dma transfer.

It must be callbed before I2S_TransferSendLoopDMA/I2S_TransferReceiveLoopDMA and after I2S_RxTransferCreateHandleDMA/I2S_TxTransferCreateHandleDMA.

User should be take care about the address of DMA descriptor pool which required align with 16BYTE at least.

Parameters
handlePointer to i2s DMA transfer handle.
dmaDescriptorAddrDMA descriptor start address.
dmaDescriptorNumDMA descriptor number.
status_t I2S_TransferSendLoopDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
i2s_transfer_t *  xfer,
uint32_t  loopTransferCount 
)

This function receives data using DMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.

This function support loop transfer, such as A->B->...->A, the loop transfer chain will be converted into a chain of descriptor and submit to dma. Application must be aware of that the more counts of the loop transfer, then more DMA descriptor memory required, user can use function I2S_InstallDMADescriptorMemory to register the dma descriptor memory.

As the DMA support maximum 1024 transfer count, so application must be aware of that this transfer function support maximum 1024 samples in each transfer, otherwise assert error or error status will be returned. Once the loop transfer start, application can use function I2S_TransferAbortDMA to stop the loop transfer.

Parameters
baseI2S peripheral base address.
handlePointer to usart_dma_handle_t structure.
xferI2S DMA transfer structure. See i2s_transfer_t.
loopTransferCountloop count
Return values
kStatus_Success
status_t I2S_TransferReceiveLoopDMA ( I2S_Type *  base,
i2s_dma_handle_t *  handle,
i2s_transfer_t *  xfer,
uint32_t  loopTransferCount 
)

This function receives data using DMA. This is a non-blocking function, which returns right away. When all data is received, the receive callback function is called.

This function support loop transfer, such as A->B->...->A, the loop transfer chain will be converted into a chain of descriptor and submit to dma. Application must be aware of that the more counts of the loop transfer, then more DMA descriptor memory required, user can use function I2S_InstallDMADescriptorMemory to register the dma descriptor memory.

As the DMA support maximum 1024 transfer count, so application must be aware of that this transfer function support maximum 1024 samples in each transfer, otherwise assert error or error status will be returned. Once the loop transfer start, application can use function I2S_TransferAbortDMA to stop the loop transfer.

Parameters
baseI2S peripheral base address.
handlePointer to usart_dma_handle_t structure.
xferI2S DMA transfer structure. See i2s_transfer_t.
loopTransferCountloop count
Return values
kStatus_Success