MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power Driver

Overview

Power driver provides APIs to control peripherals power and control the system power mode.

Macros

#define WAKEUP_SYS   (1UL << 0) /*!< [SLEEP, DEEP SLEEP ] */ /* WWDT0_IRQ and BOD_IRQ*/
 Low Power Modes Wake up sources.
 
#define WAKEUP_SDMA0   (1UL << 1)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_GLOBALINT0   (1UL << 2)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_GLOBALINT1   (1UL << 3)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_GPIO_INT0_0   (1UL << 4)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_1   (1UL << 5)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_2   (1UL << 6)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_3   (1UL << 7)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_UTICK   (1UL << 8)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_MRT   (1UL << 9)
 [SLEEP, ]
 
#define WAKEUP_CTIMER0   (1UL << 10)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER1   (1UL << 11)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SCT   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_CTIMER3   (1UL << 13)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM0   (1UL << 14)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM1   (1UL << 15)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM2   (1UL << 16)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM3   (1UL << 17)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_FLEXCOMM4   (1UL << 18)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM5   (1UL << 19)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM6   (1UL << 20)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_FLEXCOMM7   (1UL << 21)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_ADC0   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_ADC1   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_ACMP   (1UL << 24)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_DMIC   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_HWVAD   (1UL << 26)
 [SLEEP, DEEP SLEEP, ]
 
#define WAKEUP_USB0_NEEDCLK   (1UL << 27)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_USB0   (1UL << 28)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_RTC_ALARM_WAKEUP   (1UL << 29)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_EZH_ARCH_B   (1UL << 30)
 [SLEEP, ]
 
#define WAKEUP_WAKEUP_MAILBOX   (1UL << 31)
 [SLEEP, DEEP SLEEP, ]
 
#define WAKEUP_GPIO_INT0_4   (1UL << 0)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_5   (1UL << 1)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_6   (1UL << 2)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_GPIO_INT0_7   (1UL << 3)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER2   (1UL << 4)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CTIMER4   (1UL << 5)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_OS_EVENT_TIMER   (1UL << 6)
 [SLEEP, DEEP SLEEP, POWER DOWN, DEEP POWER DOWN]
 
#define WAKEUP_FLEXSPI   (1UL << 7)
 [SLEEP, ]
 
#define WAKEUP_CAN0_0   (1UL << 11)
 [SLEEP, ]
 
#define WAKEUP_CAN0_1   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_SPIFILTER   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_SEC_HYPERVISOR_CALL   (1UL << 17)
 [SLEEP, ]
 
#define WAKEUP_SEC_GPIO_INT0_0   (1UL << 18)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_GPIO_INT0_1   (1UL << 19)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_SEC_VIO   (1UL << 21)
 [SLEEP, ]
 
#define WAKEUP_CSS_IRQ0   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_PKC   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_PUF   (1UL << 24)
 [SLEEP, ]
 
#define WAKEUP_PQ   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_SDMA1   (1UL << 26)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_LSPI_HS   (1UL << 27)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_CODE_WDG   (1UL << 28)
 [SLEEP, ]
 
#define WAKEUP_I3C   (1UL << 30)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_NEUTRON   (1UL << 0)
 [SLEEP, ]
 
#define WAKEUP_CSS_IRQ1   (1UL << 1)
 [SLEEP, ]
 
#define WAKEUP_DAC0   (1UL << 10)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_DAC1   (1UL << 11)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_DAC2   (1UL << 12)
 [SLEEP, DEEP SLEEP ]
 
#define WAKEUP_HS_COMP0   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_HS_COMP1   (1UL << 14)
 [SLEEP, ]
 
#define WAKEUP_HS_COMP2   (1UL << 15)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_CAPTURE   (1UL << 16)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_FAULT   (1UL << 17)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD_ERROR   (1UL << 18)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE0   (1UL << 19)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD0   (1UL << 20)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE1   (1UL << 21)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD1   (1UL << 22)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE2   (1UL << 23)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD2   (1UL << 24)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_COMPARE3   (1UL << 25)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM0_RELOAD3   (1UL << 26)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_CAPTURE   (1UL << 27)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_FAULT   (1UL << 28)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD_ERROR   (1UL << 29)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE0   (1UL << 30)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD0   (1UL << 31)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE1   (1UL << 0)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD1   (1UL << 1)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE2   (1UL << 2)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD2   (1UL << 3)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_COMPARE3   (1UL << 4)
 [SLEEP, ]
 
#define WAKEUP_FLEXPWM1_RELOAD3   (1UL << 5)
 [SLEEP, ]
 
#define WAKEUP_ENC0_COMPARE   (1UL << 6)
 [SLEEP, ]
 
#define WAKEUP_ENC0_HOME   (1UL << 7)
 [SLEEP, ]
 
#define WAKEUP_ENC0_WDG   (1UL << 8)
 [SLEEP, ]
 
#define WAKEUP_ENC0_IDX   (1UL << 9)
 [SLEEP, ]
 
#define WAKEUP_ENC1_COMPARE   (1UL << 10)
 [SLEEP, ]
 
#define WAKEUP_ENC1_HOME   (1UL << 11)
 [SLEEP, ]
 
#define WAKEUP_ENC1_WDG   (1UL << 12)
 [SLEEP, ]
 
#define WAKEUP_ENC1_IDX   (1UL << 13)
 [SLEEP, ]
 
#define WAKEUP_ITRC   (1UL << 14)
 [SLEEP, DEEP SLEEP, POWER DOWN ]
 
#define WAKEUP_CF_DSP24L_IRQ0   (1UL << 15)
 [SLEEP, ]
 
#define WAKEUP_CF_DSP24L_IRQ1   (1UL << 16)
 [SLEEP, ]
 
#define WAKEUP_FTM0   (1UL << 17)
 [SLEEP, ]
 
#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)
 Sleep Postpone (DEEP-SLEEP) More...
 
#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)
 Wake for Flexcomms. More...
 
#define LOWPOWER_HWWAKE_DMIC   (1UL << 2)
 Wake for DMIC. More...
 
#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)
 Wake for DMA0. More...
 
#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)
 Wake for DMA1. More...
 
#define LOWPOWER_HWWAKE_DAC   (1UL << 6)
 Wake for DAC0, DAC1, DAC2. More...
 
#define LOWPOWER_HWWAKE_ENABLE_FRO192M   (1UL << 31)
 Need to be set if FRO192M is disable - via PDCTRL0 - in Deep Sleep mode and any of \ LOWPOWER_HWWAKE_PERIPHERALS, LOWPOWER_HWWAKE_SDMA0, LOWPOWER_HWWAKE_SDMA1 or LOWPOWER_HWWAKE_DAC is \ set.
 
#define LOWPOWER_CPURETCTRL_ENA_DISABLE   0
 CPU State retention (POWER-DOWN) More...
 
#define LOWPOWER_CPURETCTRL_ENA_ENABLE   1
 In POWER DOWN mode, CPU Retention is enabled.
 
#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0
 Wake up I/O sources (DEEP POWER-DOWN) More...
 
#define LOWPOWER_WAKEUPIOSRC_PIO1_INDEX   2
 Pin P0(28)
 
#define LOWPOWER_WAKEUPIOSRC_PIO2_INDEX   4
 Pin P1(18)
 
#define LOWPOWER_WAKEUPIOSRC_PIO3_INDEX   6
 Pin P1(30)
 
#define LOWPOWER_WAKEUPIOSRC_PIO4_INDEX   8
 Pin P0(26)
 
#define LOWPOWER_WAKEUPIOSRC_DISABLE   0UL
 Wake up is disable.
 
#define LOWPOWER_WAKEUPIOSRC_RISING   1UL
 Wake up on rising edge.
 
#define LOWPOWER_WAKEUPIOSRC_FALLING   2UL
 Wake up on falling edge.
 
#define LOWPOWER_WAKEUPIOSRC_RISING_FALLING   3UL
 Wake up on both rising or falling edges.
 
#define LOWPOWER_WAKEUPIOSRC_PIO0MODE_INDEX   10
 Pin P1( 1)
 
#define LOWPOWER_WAKEUPIOSRC_PIO1MODE_INDEX   12
 Pin P0(28)
 
#define LOWPOWER_WAKEUPIOSRC_PIO2MODE_INDEX   14
 Pin P1(18)
 
#define LOWPOWER_WAKEUPIOSRC_PIO3MODE_INDEX   16
 Pin P1(30)
 
#define LOWPOWER_WAKEUPIOSRC_PIO4MODE_INDEX   18
 Pin P0(26)
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PLAIN   0
 Wake up Pad is plain input.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PULLDOWN   1
 Wake up Pad is pull-down.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_PULLUP   2
 Wake up Pad is pull-up.
 
#define LOWPOWER_WAKEUPIOSRC_IO_MODE_REPEATER   3
 Wake up Pad is in repeater.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX   20
 Wake-up I/O 0 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX   21
 Wake-up I/O 1 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX   22
 Wake-up I/O 2 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX   23
 Wake-up I/O 3 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_INDEX   24
 Wake-up I/O 4 pull-up/down disable/enable control index.
 
#define LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO4_DISABLEPULLUPDOWN_INDEX)
 Wake-up I/O 4 pull-up/down disable/enable mask.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX   25
 Wake-up I/O 0 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX   26
 Wake-up I/O 1 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX   27
 Wake-up I/O 2 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX   28
 Wake-up I/O 3 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_INDEX   29
 Wake-up I/O 4 pull-up/down configuration index.
 
#define LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO0_PULLUPDOWN_INDEX)
 Wake-up I/O 0 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO1_PULLUPDOWN_INDEX)
 Wake-up I/O 1 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO2_PULLUPDOWN_INDEX)
 Wake-up I/O 2 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO3_PULLUPDOWN_INDEX)
 Wake-up I/O 3 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_MASK   (1UL << LOWPOWER_WAKEUPIO_PIO4_PULLUPDOWN_INDEX)
 Wake-up I/O 4 pull-up/down mask.
 
#define LOWPOWER_WAKEUPIO_PULLDOWN   0
 Select pull-down.
 
#define LOWPOWER_WAKEUPIO_PULLUP   1
 Select pull-up.
 
#define LOWPOWER_WAKEUPIO_CFG_SRC_IOCON   0
 Wake-up pins configuration (in/out, pull up/down plain input ...) is coming from IOCON (valid for \ DEEP-SLEEP and POWER-DOWN)
 
#define LOWPOWER_WAKEUPIO_CFG_SRC_PMC   1
 Wake-up pins configuration (in/out, pull up/down plain input ...) is coming from PMC and set up via \ the second parameter (wakeup_io_ctrl) of POWER_SetWakeUpPins API (valid for DEEP-SLEEP and POWER-DOWN)
 

Typedefs

typedef enum _power_mode_config power_mode_cfg_t
 Low Power Modes configuration.
 
typedef enum _power_reset_cause power_reset_cause_t
 Device Reset Causes.
 
typedef enum _power_boot_mode power_boot_mode_t
 Device Boot Modes.
 
typedef enum _power_wakeup_pin_t power_wakeup_pin_t
 Device wake up pins events.
 
typedef enum _power_pd_bit pd_bit_t
 analog components power modes control during low power modes
 
typedef enum _power_sram_bit power_sram_bit_t
 SRAM instances bit masks.
 
typedef enum _power_sram_index power_sram_index_t
 SRAM instances indexes.
 
typedef enum _power_sram_pwr_mode power_sram_pwr_mode_t
 SRAM Power Mode.
 
typedef enum
_power_bod_vddmain_level 
power_bod_vddmain_level_t
 BOD VDDMAIN level.
 
typedef enum _power_bod_core_level power_bod_core_level_t
 BOD core level.
 
typedef enum _power_bod_hyst power_bod_hyst_t
 BODs (VDDMAIN & Core) Hysteresis control.
 
typedef enum _power_core_pwr_source power_core_pwr_source_t
 Core Power Source.
 
typedef enum _power_core_pwr_state power_core_pwr_state_t
 Core Regulators Power State.
 
typedef enum _power_status power_status_t
 Generic Power Library APIs Status codes.
 

Enumerations

enum  _power_mode_config
 Low Power Modes configuration.
 
enum  _power_reset_cause {
  kRESET_CAUSE_POR = 0UL,
  kRESET_CAUSE_PADRESET = 1UL,
  kRESET_CAUSE_BODRESET = 2UL,
  kRESET_CAUSE_ARMSYSTEMRESET = 3UL,
  kRESET_CAUSE_WDTRESET = 4UL,
  kRESET_CAUSE_SWRRESET = 5UL,
  kRESET_CAUSE_CDOGRESET = 6UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO = 7UL,
  kRESET_CAUSE_DPDRESET_RTC = 8UL,
  kRESET_CAUSE_DPDRESET_OSTIMER = 9UL,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER,
  kRESET_CAUSE_DPDRESET_RTC_OSTIMER,
  kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER = 13UL,
  kRESET_CAUSE_NOT_RELEVANT,
  kRESET_CAUSE_NOT_DETERMINISTIC = 15UL
}
 Device Reset Causes. More...
 
enum  _power_boot_mode {
  kBOOT_MODE_POWER_UP,
  kBOOT_MODE_LP_DEEP_SLEEP = 1UL,
  kBOOT_MODE_LP_POWER_DOWN = 2UL,
  kBOOT_MODE_LP_DEEP_POWER_DOWN = 4UL
}
 Device Boot Modes. More...
 
enum  _power_wakeup_pin_t {
  kWAKEUP_PIN_NONE = 0UL,
  kWAKEUP_PIN_0 = (1UL << 0),
  kWAKEUP_PIN_1 = (1UL << 1),
  kWAKEUP_PIN_2 = (1UL << 2),
  kWAKEUP_PIN_3 = (1UL << 3),
  kWAKEUP_PIN_4 = (1UL << 4),
  kWAKEUP_PIN_MULTIPLE = 0x1FUL
}
 Device wake up pins events. More...
 
enum  _power_pd_bit
 analog components power modes control during low power modes
 
enum  _power_sram_bit {
  kPOWER_SRAM_RAM_X0 = (1UL << 0),
  kPOWER_SRAM_RAM_00 = (1UL << 1),
  kPOWER_SRAM_RAM_01 = (1UL << 2),
  kPOWER_SRAM_RAM_02 = (1UL << 3),
  kPOWER_SRAM_RAM_03 = (1UL << 4),
  kPOWER_SRAM_RAM_10 = (1UL << 5),
  kPOWER_SRAM_RAM_20 = (1UL << 6),
  kPOWER_SRAM_RAM_30 = (1UL << 7),
  kPOWER_SRAM_RAM_40 = (1UL << 8),
  kPOWER_SRAM_RAM_41 = (1UL << 9),
  kPOWER_SRAM_RAM_42 = (1UL << 10),
  kPOWER_SRAM_RAM_43 = (1UL << 11),
  kPOWER_SRAM_FLASHCACHE = (1UL << 12),
  kPOWER_SRAM_FLEXSPICACHE = (1UL << 13),
  kPOWER_SRAM_FLEXSPIH2PREG = (1UL << 14),
  kPOWER_SRAM_DSLP_MASK = 0x7FFFUL,
  kPOWER_SRAM_PDWN_MASK = 0xFFFUL,
  kPOWER_SRAM_DPWD_MASK = 0xF3FUL
}
 SRAM instances bit masks. More...
 
enum  _power_sram_index {
  kPOWER_SRAM_IDX_RAM_X0 = 0UL,
  kPOWER_SRAM_IDX_RAM_00 = 1UL,
  kPOWER_SRAM_IDX_RAM_01 = 2UL,
  kPOWER_SRAM_IDX_RAM_02 = 3UL,
  kPOWER_SRAM_IDX_RAM_03 = 4UL,
  kPOWER_SRAM_IDX_RAM_10 = 5UL,
  kPOWER_SRAM_IDX_RAM_20 = 6UL,
  kPOWER_SRAM_IDX_RAM_30 = 7UL,
  kPOWER_SRAM_IDX_RAM_40 = 8UL,
  kPOWER_SRAM_IDX_RAM_41 = 9UL,
  kPOWER_SRAM_IDX_RAM_42 = 10UL,
  kPOWER_SRAM_IDX_RAM_43 = 11UL,
  kPOWER_SRAM_IDX_FLASHCACHE = 12UL,
  kPOWER_SRAM_IDX_FLEXSPICACHE = 13UL,
  kPOWER_SRAM_IDX_FLEXSPIH2PREG = 14UL
}
 SRAM instances indexes. More...
 
enum  _power_sram_pwr_mode {
  kPOWER_SRAMPwrActive = 0U,
  kPOWER_SRAMPwrLightSleep = 1U,
  kPOWER_SRAMPwrDeepSleep = 2U,
  kPOWER_SRAMPwrShutDown = 3U
}
 SRAM Power Mode. More...
 
enum  _power_bod_vddmain_level {
  kPOWER_BodVddmainLevel1000mv = 0,
  kPOWER_BodVddmainLevel1100mv = 1,
  kPOWER_BodVddmainLevel1200mv = 2,
  kPOWER_BodVddmainLevel1300mv = 3,
  kPOWER_BodVddmainLevel1400mv = 4,
  kPOWER_BodVddmainLevel1500mv = 5,
  kPOWER_BodVddmainLevel1600mv = 6,
  kPOWER_BodVddmainLevel1650mv = 7,
  kPOWER_BodVddmainLevel1700mv = 8,
  kPOWER_BodVddmainLevel1750mv = 9,
  kPOWER_BodVddmainLevel1800mv = 10,
  kPOWER_BodVddmainLevel1900mv = 11,
  kPOWER_BodVddmainLevel2000mv = 12,
  kPOWER_BodVddmainLevel2100mv = 13,
  kPOWER_BodVddmainLevel2200mv = 14,
  kPOWER_BodVddmainLevel2300mv = 15,
  kPOWER_BodVddmainLevel2400mv = 16,
  kPOWER_BodVddmainLevel2500mv = 17,
  kPOWER_BodVddmainLevel2600mv = 18,
  kPOWER_BodVddmainLevel2700mv = 19,
  kPOWER_BodVddmainLevel2800mv = 20,
  kPOWER_BodVddmainLevel2900mv = 21,
  kPOWER_BodVddmainLevel3000mv = 22,
  kPOWER_BodVddmainLevel3100mv = 23,
  kPOWER_BodVddmainLevel3200mv = 24,
  kPOWER_BodVddmainLevel3300mv = 25
}
 BOD VDDMAIN level. More...
 
enum  _power_bod_core_level {
  kPOWER_BodCoreLevel0A600mv = 0,
  kPOWER_BodCoreLevel0A650mv = 1,
  kPOWER_BodCoreLevel0A700mv = 2,
  kPOWER_BodCoreLevel0A750mv = 3,
  kPOWER_BodCoreLevel0A800mv = 4,
  kPOWER_BodCoreLevel0A850mv = 5,
  kPOWER_BodCoreLevel0A900mv = 6,
  kPOWER_BodCoreLevel0A950mv = 7,
  kPOWER_BodCoreLevel1B929mv = 5,
  kPOWER_BodCoreLevel1B984mv = 6,
  kPOWER_BodCoreLevel1B1038mv = 7
}
 BOD core level. More...
 
enum  _power_bod_hyst {
  kPOWER_BodHystLevel25mv = 0U,
  kPOWER_BodHystLevel50mv = 1U,
  kPOWER_BodHystLevel75mv = 2U,
  kPOWER_BodHystLevel100mv = 3U
}
 BODs (VDDMAIN & Core) Hysteresis control. More...
 
enum  _power_core_pwr_source {
  kPOWER_CoreSrcDCDC = 0U,
  kPOWER_CoreSrcLDOCoreHP = 1U,
  kPOWER_CoreSrcLDOCoreLP = 2U,
  kPOWER_CoreSrcExternal = 3U
}
 Core Power Source. More...
 
enum  _power_core_pwr_state {
  kPOWER_CorePwrDisable = 0U,
  kPOWER_CorePwrEnable = 1U
}
 Core Regulators Power State. More...
 
enum  _power_status {
  kPOWER_Status_Success = 0U,
  kPOWER_Status_Fail = 1U
}
 Generic Power Library APIs Status codes. More...
 

Functions

static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Syscon. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Syscon. More...
 
power_status_t POWER_PowerInit (void)
 SoC Power Management Controller initialization. More...
 
power_status_t POWER_SetCorePowerSource (power_core_pwr_source_t pwr_source)
 Selects the core logic supply source. More...
 
power_core_pwr_source_t POWER_GetCorePowerSource (void)
 Returns the current core logic supply source. More...
 
power_status_t POWER_CorePowerSourceControl (power_core_pwr_source_t pwr_source, power_core_pwr_state_t pwr_state)
 Allows to control the state (enabled or disabled) of the core logic internal regulators (DCDC, LDO_CORE) More...
 
power_status_t POWER_SRAMPowerModeControl (power_sram_bit_t sram_inst, power_sram_pwr_mode_t pwr_mode)
 Allows to configure SRAM instances (low) power modes when the part is in ACTIVE mode. More...
 
power_sram_pwr_mode_t POWER_GetSRAMPowerMode (power_sram_index_t sram_index)
 
void POWER_EnterSleep (void)
 Configures and enters in SLEEP low power mode. More...
 
void POWER_EnterDeepSleep (uint32_t exclude_from_pd[2], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[4], uint32_t hardware_wake_ctrl)
 Configures and enters in DEEP-SLEEP low power mode. More...
 
void POWER_EnterPowerDown (uint32_t exclude_from_pd[1], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[4], uint32_t cpu_retention_addr)
 Configures and enters in POWERDOWN low power mode. More...
 
void POWER_EnterDeepPowerDown (uint32_t exclude_from_pd[1], uint32_t sram_retention_ctrl, uint32_t wakeup_interrupts[2], uint32_t wakeup_io_ctrl)
 Configures and enters in DEEPPOWERDOWN low power mode. More...
 
void POWER_SetWakeUpPins (uint32_t wakeup_io_cfg_src, uint32_t wakeup_io_ctrl)
 Configures the 5 wake-up pins to wake up the part in DEEP-SLEEP and POWER-DOWN low power modes. More...
 
void POWER_GetWakeUpCause (power_reset_cause_t *reset_cause, power_boot_mode_t *boot_mode, power_wakeup_pin_t *wakeup_pin_cause)
 Return some key information related to the device reset causes / wake-up sources, for all power modes. More...
 
void POWER_SetVoltageForFreq (uint32_t system_freq_hz)
 Configures the device internal power control settings. More...
 

Driver version

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
 power driver version 2.0.1. More...
 

Macro Definition Documentation

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 0, 1))
#define LOWPOWER_HWWAKE_FORCED   (1UL << 0)

Force peripheral clocking to stay on during deep-sleep mode.

#define LOWPOWER_HWWAKE_PERIPHERALS   (1UL << 1)

Any Flexcomm FIFO reaching the level specified by its own TXLVL will cause \ peripheral clocking to wake up temporarily while the related status is asserted

#define LOWPOWER_HWWAKE_DMIC   (1UL << 2)

DMIC being busy will cause peripheral clocking to remain running until DMIC \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS

#define LOWPOWER_HWWAKE_SDMA0   (1UL << 3)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS or LOWPOWER_HWWAKE_DAC

#define LOWPOWER_HWWAKE_SDMA1   (1UL << 5)

DMA0 being busy will cause peripheral clocking to remain running until DMA \ completes. Used in conjonction with LOWPOWER_HWWAKE_PERIPHERALS or LOWPOWER_HWWAKE_DAC

#define LOWPOWER_HWWAKE_DAC   (1UL << 6)

Any DAC0/1/2 FIFO reaching the level specified by the configuration \ will generate an asynchronous SDMA0 request, and SDMA0 will wake up the bus \ clock temporarily to transfer data to DAC0/1/2.

#define LOWPOWER_CPURETCTRL_ENA_DISABLE   0

In POWER DOWN mode, CPU Retention is disabled

#define LOWPOWER_WAKEUPIOSRC_PIO0_INDEX   0

Pin P1( 1)

Enumeration Type Documentation

Enumerator
kRESET_CAUSE_POR 

Power On Reset.

kRESET_CAUSE_PADRESET 

Hardware Pin Reset.

kRESET_CAUSE_BODRESET 

Brown-out Detector reset (either BODVBAT or BODCORE)

kRESET_CAUSE_ARMSYSTEMRESET 

ARM System Reset.

kRESET_CAUSE_WDTRESET 

Watchdog Timer Reset.

kRESET_CAUSE_SWRRESET 

Software Reset.

kRESET_CAUSE_CDOGRESET 

Code Watchdog Reset.

kRESET_CAUSE_DPDRESET_WAKEUPIO 

Any of the 5 wake-up pins.

kRESET_CAUSE_DPDRESET_RTC 

Real Time Clock (RTC)

kRESET_CAUSE_DPDRESET_OSTIMER 

OS Event Timer (OSTIMER)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC 

Any of the 5 wake-up pins and RTC (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_WAKEUPIO_OSTIMER 

Any of the 5 wake-up pins and OSTIMER (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_RTC_OSTIMER 

Real Time Clock or OS Event Timer (the 2 events occured within 1 nano-second of each other)

kRESET_CAUSE_DPDRESET_WAKEUPIO_RTC_OSTIMER 

Any of the 5 wake-up pins or RTC or OS Event Timer (the 3 events occured within 1 nano-second of each other)

kRESET_CAUSE_NOT_RELEVANT 

No reset cause (for example, this code is used when waking up from DEEP-SLEEP low power mode)

kRESET_CAUSE_NOT_DETERMINISTIC 

Unknown Reset Cause.

Should be treated like "Hardware Pin Reset" from an application point of view.

Enumerator
kBOOT_MODE_POWER_UP 

All non Low Power Mode wake up (Power On Reset, Pin Reset, BoD Reset, ARM System Reset ...

)

kBOOT_MODE_LP_DEEP_SLEEP 

Wake up from DEEP-SLEEP Low Power mode.

kBOOT_MODE_LP_POWER_DOWN 

Wake up from POWER-DOWN Low Power mode.

kBOOT_MODE_LP_DEEP_POWER_DOWN 

Wake up from DEEP-POWER-DOWN Low Power mode.

Enumerator
kWAKEUP_PIN_NONE 

No wake up pin event.

kWAKEUP_PIN_0 

Wake up pin 0 event.

kWAKEUP_PIN_1 

Wake up pin 1 event.

kWAKEUP_PIN_2 

Wake up pin 2 event.

kWAKEUP_PIN_3 

Wake up pin 3 event.

kWAKEUP_PIN_4 

Wake up pin 4 event.

kWAKEUP_PIN_MULTIPLE 

More than 1 wake up pins events occured (within 1 nano-second of each other)

Enumerator
kPOWER_SRAM_RAM_X0 

RAM_X0.

kPOWER_SRAM_RAM_00 

RAM_00.

kPOWER_SRAM_RAM_01 

RAM_01.

kPOWER_SRAM_RAM_02 

RAM_02.

kPOWER_SRAM_RAM_03 

RAM_03.

kPOWER_SRAM_RAM_10 

RAM_10.

kPOWER_SRAM_RAM_20 

RAM_20.

kPOWER_SRAM_RAM_30 

RAM_30.

kPOWER_SRAM_RAM_40 

RAM_40.

kPOWER_SRAM_RAM_41 

RAM_41.

kPOWER_SRAM_RAM_42 

RAM_42.

kPOWER_SRAM_RAM_43 

RAM_43.

kPOWER_SRAM_FLASHCACHE 

Reserved.

Flash Cache SRAM instance

kPOWER_SRAM_FLEXSPICACHE 

Reserved.

FlexSPI Cache SRAM instance

kPOWER_SRAM_FLEXSPIH2PREG 

Reserved.

FlexSPI Dual Port Register Files instances

kPOWER_SRAM_DSLP_MASK 

Reserved.

DEEP-SLEEP SRAM instances

kPOWER_SRAM_PDWN_MASK 

Reserved.

POWER-DOWN SRAM instances

kPOWER_SRAM_DPWD_MASK 

Reserved.

DEEP-POWER-DOWN SRAM instances (RAM_20 & RAM_30 excluded).

Enumerator
kPOWER_SRAM_IDX_RAM_X0 

RAM_X0.

kPOWER_SRAM_IDX_RAM_00 

RAM_00.

kPOWER_SRAM_IDX_RAM_01 

RAM_01.

kPOWER_SRAM_IDX_RAM_02 

RAM_02.

kPOWER_SRAM_IDX_RAM_03 

RAM_03.

kPOWER_SRAM_IDX_RAM_10 

RAM_10.

kPOWER_SRAM_IDX_RAM_20 

RAM_20.

kPOWER_SRAM_IDX_RAM_30 

RAM_30.

kPOWER_SRAM_IDX_RAM_40 

RAM_40.

kPOWER_SRAM_IDX_RAM_41 

RAM_41.

kPOWER_SRAM_IDX_RAM_42 

RAM_42.

kPOWER_SRAM_IDX_RAM_43 

RAM_43.

kPOWER_SRAM_IDX_FLASHCACHE 

Reserved.

Flash Cache SRAM instance

kPOWER_SRAM_IDX_FLEXSPICACHE 

Reserved.

FlexSPI Cache SRAM instance

kPOWER_SRAM_IDX_FLEXSPIH2PREG 

Reserved.

FlexSPI Dual Port Register Files instances

Enumerator
kPOWER_SRAMPwrActive 

Active.

kPOWER_SRAMPwrLightSleep 

RESERVED, DO NOT USE (Light Sleep)

kPOWER_SRAMPwrDeepSleep 

Deep Sleep : SRAM content retained.

kPOWER_SRAMPwrShutDown 

Shutdown: SRAM content lost.

Enumerator
kPOWER_BodVddmainLevel1000mv 

VDDMAIN Brown out detector level 1V.

kPOWER_BodVddmainLevel1100mv 

VDDMAIN Brown out detector level 1.1V.

kPOWER_BodVddmainLevel1200mv 

VDDMAIN Brown out detector level 1.2V.

kPOWER_BodVddmainLevel1300mv 

VDDMAIN Brown out detector level 1.3V.

kPOWER_BodVddmainLevel1400mv 

VDDMAIN Brown out detector level 1.4V.

kPOWER_BodVddmainLevel1500mv 

VDDMAIN Brown out detector level 1.5V.

kPOWER_BodVddmainLevel1600mv 

VDDMAIN Brown out detector level 1.6V.

kPOWER_BodVddmainLevel1650mv 

VDDMAIN Brown out detector level 1.65V.

kPOWER_BodVddmainLevel1700mv 

VDDMAIN Brown out detector level 1.7V.

kPOWER_BodVddmainLevel1750mv 

VDDMAIN Brown out detector level 1.75V.

kPOWER_BodVddmainLevel1800mv 

VDDMAIN Brown out detector level 1.8V.

kPOWER_BodVddmainLevel1900mv 

VDDMAIN Brown out detector level 1.9V.

kPOWER_BodVddmainLevel2000mv 

VDDMAIN Brown out detector level 2V.

kPOWER_BodVddmainLevel2100mv 

VDDMAIN Brown out detector level 2.1V.

kPOWER_BodVddmainLevel2200mv 

VDDMAIN Brown out detector level 2.2V.

kPOWER_BodVddmainLevel2300mv 

VDDMAIN Brown out detector level 2.3V.

kPOWER_BodVddmainLevel2400mv 

VDDMAIN Brown out detector level 2.4V.

kPOWER_BodVddmainLevel2500mv 

VDDMAIN Brown out detector level 2.5V.

kPOWER_BodVddmainLevel2600mv 

VDDMAIN Brown out detector level 2.6V.

kPOWER_BodVddmainLevel2700mv 

VDDMAIN Brown out detector level 2.7V.

kPOWER_BodVddmainLevel2800mv 

VDDMAIN Brown out detector level 2.80 V.

kPOWER_BodVddmainLevel2900mv 

VDDMAIN Brown out detector level 2.9V.

kPOWER_BodVddmainLevel3000mv 

VDDMAIN Brown out detector level 3.0V.

kPOWER_BodVddmainLevel3100mv 

VDDMAIN Brown out detector level 3.1V.

kPOWER_BodVddmainLevel3200mv 

VDDMAIN Brown out detector level 3.2V.

kPOWER_BodVddmainLevel3300mv 

VDDMAIN Brown out detector level 3.3V.

Enumerator
kPOWER_BodCoreLevel0A600mv 

core Brown out detector level 600mV for 0A

kPOWER_BodCoreLevel0A650mv 

core Brown out detector level 650mV for 0A

kPOWER_BodCoreLevel0A700mv 

core Brown out detector level 700mV for 0A

kPOWER_BodCoreLevel0A750mv 

core Brown out detector level 750mV for 0A

kPOWER_BodCoreLevel0A800mv 

core Brown out detector level 800mV for 0A

kPOWER_BodCoreLevel0A850mv 

core Brown out detector level 850mV for 0A

kPOWER_BodCoreLevel0A900mv 

core Brown out detector level 900mV for 0A

kPOWER_BodCoreLevel0A950mv 

core Brown out detector level 950mV for 0A

kPOWER_BodCoreLevel1B929mv 

core Brown out detector level 929mV for 1B

kPOWER_BodCoreLevel1B984mv 

core Brown out detector level 984mV for 1B

kPOWER_BodCoreLevel1B1038mv 

core Brown out detector level 1038mV for 1B

Enumerator
kPOWER_BodHystLevel25mv 

BOD Hysteresis control level 25mv.

kPOWER_BodHystLevel50mv 

BOD Hysteresis control level 50mv.

kPOWER_BodHystLevel75mv 

BOD Hysteresis control level 75mv.

kPOWER_BodHystLevel100mv 

BOD Hysteresis control level 100mv.

Enumerator
kPOWER_CoreSrcDCDC 

DCDC.

kPOWER_CoreSrcLDOCoreHP 

LDO Core High Power Mode.

kPOWER_CoreSrcLDOCoreLP 

LDO Core Low Power Mode (DO NOT USE : Reserved for test purposes)

kPOWER_CoreSrcExternal 

External (DO NOT USE : Reserved for test purposes)

Enumerator
kPOWER_CorePwrDisable 

Disable.

kPOWER_CorePwrEnable 

Enable.

Enumerator
kPOWER_Status_Success 

OK.

kPOWER_Status_Fail 

Generic error code.

Function Documentation

static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
Returns
none
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
Returns
none
power_status_t POWER_PowerInit ( void  )
Returns
power_status_t
power_status_t POWER_SetCorePowerSource ( power_core_pwr_source_t  pwr_source)
Parameters
pwr_source: Defines which regulator will be used to power the part core logic (internally)
Returns
power_status_t
power_core_pwr_source_t POWER_GetCorePowerSource ( void  )
Returns
power_core_pwr_source_t
power_status_t POWER_CorePowerSourceControl ( power_core_pwr_source_t  pwr_source,
power_core_pwr_state_t  pwr_state 
)
Parameters
pwr_source: Defines which regulator will be enabled or disabled
pwr_state: Defines the state of the internal regulator indicated by pwr_source
Returns
power_status_t
power_status_t POWER_SRAMPowerModeControl ( power_sram_bit_t  sram_inst,
power_sram_pwr_mode_t  pwr_mode 
)
Parameters
sram_inst: Defines the SRAM instance(s) to be configured.
pwr_mode: Defines the SRAM low power mode to be applied to all SRAM instances given by sram_inst
Returns
power_status_t
power_sram_pwr_mode_t POWER_GetSRAMPowerMode ( power_sram_index_t  sram_index)
Parameters
sram_index: SRAM instances indexes
Returns
power_sram_pwr_mode_t
void POWER_EnterSleep ( void  )
Returns
Nothing
void POWER_EnterDeepSleep ( uint32_t  exclude_from_pd[2],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[4],
uint32_t  hardware_wake_ctrl 
)
Parameters
exclude_from_pd,:Defines which analog peripherals shall NOT be powered down (it is a 2 x 32-bit vectors, aligned with "pd_bit_t" definition)
sram_retention_ctrl,:Defines which SRAM instances will be put in "retention" mode during deep-sleep (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:Defines which peripheral interrupts can be a wake-up source during deep-sleep (it is a 4 x 32-bit vectors, aligned with "WAKEUP_" definition)
hardware_wake_ctrl,:configure DMA services during deep-sleep without waking up entire device (see "LOWPOWER_HWWAKE_*" definition).
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU & System CLock frequency is switched to FRO12MHz and is NOT restored back by the API.
void POWER_EnterPowerDown ( uint32_t  exclude_from_pd[1],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[4],
uint32_t  cpu_retention_addr 
)
Parameters
exclude_from_pd,:Defines which analog peripherals shall NOT be powered down (it is a 1 x 32-bit vector, aligned with "pd_bit_t" definition)
sram_retention_ctrl,:Defines which SRAM instances will be put in "retention" mode during power-down (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:Defines which peripheral interrupts can be a wake-up source during power-down (it is a 2 x 32-bit vectors, aligned with "WAKEUP_" definition)
cpu_retention_addr,:Must be:
  • Word aligned (address ending by 0x0, 0x4, 0x8 and 0xC).
  • Between 0x2000_0000 and 0x2000_09FC (inside RAM_00) or
  • Between 0x2000_1000 and 0x2000_19FC (inside RAM_01) or
  • Between 0x2000_2000 and 0x2000_29FC (inside RAM_02) or
  • Between 0x2000_3000 and 0x2000_39FC (inside RAM_03)
  • The CPU state will be stored in SRAM from "cpu_retention_addr" to "cpu_retention_addr + 1540". Therefore, any data present in this area before calling the function will be lost.
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU0 & System Clock frequency is switched to FRO12MHz and is NOT restored back by the API.
      2 - It is the responsability of the user to make sure that SRAM instance containing the application
          software stack and variables WILL BE preserved during low power (via parameter "sram_retention_ctrl")
void POWER_EnterDeepPowerDown ( uint32_t  exclude_from_pd[1],
uint32_t  sram_retention_ctrl,
uint32_t  wakeup_interrupts[2],
uint32_t  wakeup_io_ctrl 
)
Parameters
exclude_from_pd,:Defines which analog peripherals shall NOT be powered down (it is a 1 x 32-bit vector, aligned with "pd_bit_t" definition)
sram_retention_ctrl,:Defines which SRAM instances will be put in "retention" mode during deep power-down (aligned with "power_sram_bit_t" definition)
wakeup_interrupts,:Defines which peripheral interrupts can be a wake-up source during deep power-down (it is a 2 x 32-bit vectors, aligned with "WAKEUP_" definition)
wakeup_io_ctrl,:configure the 5 wake-up pins that can wake-up the part from deep power-down mode (see "LOWPOWER_WAKEUPIOSRC_*" definition)
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - CPU0 & System Clock frequency is switched to FRO12MHz and is NOT restored back by the API.
      2 - The HARD FAULT handler should execute from SRAM. (The Hard fault handler should initiate a full chip
reset)
void POWER_SetWakeUpPins ( uint32_t  wakeup_io_cfg_src,
uint32_t  wakeup_io_ctrl 
)
Parameters
wakeup_io_cfg_src: for all wake-up pins : indicates if the config is from IOCON (0) or from PMC (1).
wakeup_io_ctrl,:the 5 wake-up pins configurations (see "LOWPOWER_WAKEUPIOSRC_*" definition)
Returns
Nothing
     !!! IMPORTANT NOTES :
      1 - To be called just before POWER_EnterDeepSleep() or POWER_EnterPowerDown().
void POWER_GetWakeUpCause ( power_reset_cause_t *  reset_cause,
power_boot_mode_t *  boot_mode,
power_wakeup_pin_t *  wakeup_pin_cause 
)
Parameters
reset_cause: the device reset cause, according to the definition of power_reset_cause_t type.
boot_mode: the device boot mode, according to the definition of power_boot_mode_t type.
wakeup_pin_cause,:the wake-up pin sources, according to the definition of power_wakeup_pin_t type.
Returns
Nothing
void POWER_SetVoltageForFreq ( uint32_t  system_freq_hz)
Parameters
system_freq_hz,:operating frequency required (in Hertz).
Returns
Nothing
     prepare on-chip power regulators (DC-DC Converter / Core and Always-on
     Low Drop-Out regulators)  to deliver the amount of power needed for the
     requested performance level, as defined by the CPU operating frequency.