MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PRINCE: PRINCE bus crypto engine

Overview

The MCUXpresso SDK provides a peripheral driver for the PRINCE bus crypto engine module of MCUXpresso SDK devices.

..

This example code shows how to use the PRINCE driver.

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/prince

Typedefs

typedef enum _skboot_status skboot_status_t
 Secure status enumeration. More...
 
typedef enum _secure_bool secure_bool_t
 Secure boolean enumeration. More...
 
typedef enum _prince_region prince_region_t
 Prince region. More...
 
typedef enum _prince_lock prince_lock_t
 Prince lock. More...
 
typedef enum _prince_flags prince_flags_t
 Prince flag. More...
 

Enumerations

enum  _skboot_status {
  kStatus_SKBOOT_Success = 0x5ac3c35au,
  kStatus_SKBOOT_Fail = 0xc35ac35au,
  kStatus_SKBOOT_InvalidArgument = 0xc35a5ac3u,
  kStatus_SKBOOT_KeyStoreMarkerInvalid = 0xc3c35a5au
}
 Secure status enumeration. More...
 
enum  _secure_bool {
  kSECURE_TRUE = 0xc33cc33cU,
  kSECURE_FALSE = 0x5aa55aa5U
}
 Secure boolean enumeration. More...
 
enum  _prince_region {
  kPRINCE_Region0 = 0U,
  kPRINCE_Region1 = 1U,
  kPRINCE_Region2 = 2U
}
 Prince region. More...
 
enum  _prince_lock {
  kPRINCE_Region0Lock = 1U,
  kPRINCE_Region1Lock = 2U,
  kPRINCE_Region2Lock = 4U,
  kPRINCE_MaskLock = 256U
}
 Prince lock. More...
 
enum  _prince_flags {
  kPRINCE_Flag_None = 0U,
  kPRINCE_Flag_EraseCheck = 1U,
  kPRINCE_Flag_WriteCheck = 2U
}
 Prince flag. More...
 

Functions

static void PRINCE_EncryptEnable (PRINCE_Type *base)
 Enable data encryption. More...
 
static void PRINCE_EncryptDisable (PRINCE_Type *base)
 Disable data encryption. More...
 
static bool PRINCE_IsEncryptEnable (PRINCE_Type *base)
 Is Enable data encryption. More...
 
static void PRINCE_SetMask (PRINCE_Type *base, uint64_t mask)
 Sets PRINCE data mask. More...
 
static void PRINCE_SetLock (PRINCE_Type *base, uint32_t lock)
 Locks access for specified region registers or data mask register. More...
 
status_t PRINCE_GenNewIV (prince_region_t region, uint8_t *iv_code, bool store, flash_config_t *flash_context)
 Generate new IV code. More...
 
status_t PRINCE_LoadIV (prince_region_t region, uint8_t *iv_code)
 Load IV code. More...
 
status_t PRINCE_SetEncryptForAddressRange (prince_region_t region, uint32_t start_address, uint32_t length, flash_config_t *flash_context, bool regenerate_iv)
 Allow encryption/decryption for specified address range. More...
 
status_t PRINCE_GetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t *sr_enable)
 Gets the PRINCE Sub-Region Enable register. More...
 
status_t PRINCE_GetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t *region_base_addr)
 Gets the PRINCE region base address register. More...
 
status_t PRINCE_SetRegionIV (PRINCE_Type *base, prince_region_t region, const uint8_t iv[8])
 Sets the PRINCE region IV. More...
 
status_t PRINCE_SetRegionBaseAddress (PRINCE_Type *base, prince_region_t region, uint32_t region_base_addr)
 Sets the PRINCE region base address. More...
 
status_t PRINCE_SetRegionSREnable (PRINCE_Type *base, prince_region_t region, uint32_t sr_enable)
 Sets the PRINCE Sub-Region Enable register. More...
 
status_t PRINCE_FlashEraseWithChecker (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key)
 Erases the flash sectors encompassed by parameters passed into function. More...
 
status_t PRINCE_FlashProgramWithChecker (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes)
 Programs flash with data at locations passed in through parameters. More...
 

Driver version

#define FSL_PRINCE_DRIVER_VERSION   (MAKE_VERSION(2, 6, 0))
 PRINCE driver version 2.6.0. More...
 

Macro Definition Documentation

#define FSL_PRINCE_DRIVER_VERSION   (MAKE_VERSION(2, 6, 0))

Current version: 2.6.0

Change log:

  • Version 2.0.0
    • Initial version.
  • Version 2.1.0
    • Update for the A1 rev. of LPC55Sxx serie.
  • Version 2.2.0
    • Add runtime checking of the A0 and A1 rev. of LPC55Sxx serie to support both silicone revisions.
  • Version 2.3.0
    • Add support for LPC55S1x and LPC55S2x series
  • Version 2.3.0
    • Fix MISRA-2012 issues.
  • Version 2.3.1
    • Add support for LPC55S0x series
  • Version 2.3.2
    • Fix documentation of enumeration. Extend PRINCE example.
  • Version 2.4.0
    • Add support for LPC55S3x series
  • Version 2.5.0
    • Add PRINCE_Config() and PRINCE_Reconfig() features.
  • Version 2.5.1
    • Fix build error due to renamed symbols
  • Version 2.6.0
    • Renamed CSS to ELS

Typedef Documentation

Enumeration Type Documentation

Enumerator
kStatus_SKBOOT_Success 

PRINCE Success.

kStatus_SKBOOT_Fail 

PRINCE Fail.

kStatus_SKBOOT_InvalidArgument 

PRINCE Invalid argument.

kStatus_SKBOOT_KeyStoreMarkerInvalid 

PRINCE Invalid marker.

Enumerator
kSECURE_TRUE 

PRINCE true.

kSECURE_FALSE 

PRINCE false.

Enumerator
kPRINCE_Region0 

PRINCE region 0.

kPRINCE_Region1 

PRINCE region 1.

kPRINCE_Region2 

PRINCE region 2.

Enumerator
kPRINCE_Region0Lock 

PRINCE region 0 lock.

kPRINCE_Region1Lock 

PRINCE region 1 lock.

kPRINCE_Region2Lock 

PRINCE region 2 lock.

kPRINCE_MaskLock 

PRINCE mask register lock.

Enumerator
kPRINCE_Flag_None 

PRINCE Flag None.

kPRINCE_Flag_EraseCheck 

PRINCE Flag Erase check.

kPRINCE_Flag_WriteCheck 

PRINCE Flag Write check.

Function Documentation

static void PRINCE_EncryptEnable ( PRINCE_Type *  base)
inlinestatic

This function enables PRINCE on-the-fly data encryption.

Parameters
basePRINCE peripheral address.
static void PRINCE_EncryptDisable ( PRINCE_Type *  base)
inlinestatic

This function disables PRINCE on-the-fly data encryption.

Parameters
basePRINCE peripheral address.
static bool PRINCE_IsEncryptEnable ( PRINCE_Type *  base)
inlinestatic

This function test if PRINCE on-the-fly data encryption is enabled.

Parameters
basePRINCE peripheral address.
Returns
true if enabled, false if not
static void PRINCE_SetMask ( PRINCE_Type *  base,
uint64_t  mask 
)
inlinestatic

This function sets the PRINCE mask that is used to mask decrypted data.

Parameters
basePRINCE peripheral address.
mask64-bit data mask value.
static void PRINCE_SetLock ( PRINCE_Type *  base,
uint32_t  lock 
)
inlinestatic

This function sets lock on specified region registers or mask register.

Parameters
basePRINCE peripheral address.
lockregisters to lock. This is a logical OR of members of the enumeration prince_lock_t
status_t PRINCE_GenNewIV ( prince_region_t  region,
uint8_t *  iv_code,
bool  store,
flash_config_t *  flash_context 
)

This function generates new IV code and stores it into the persistent memory. Ensure about 800 bytes free space on the stack when calling this routine with the store parameter set to true!

Parameters
regionPRINCE region index.
iv_codeIV code pointer used for storing the newly generated 52 bytes long IV code.
storeflag to allow storing the newly generated IV code into the persistent memory (FFR).
flash_contextpointer to the flash driver context structure.
Returns
kStatus_Success upon success
kStatus_Fail otherwise, kStatus_Fail is also returned if the key code for the particular PRINCE region is not present in the keystore (though new IV code has been provided)
status_t PRINCE_LoadIV ( prince_region_t  region,
uint8_t *  iv_code 
)

This function enables IV code loading into the PRINCE bus encryption engine.

Parameters
regionPRINCE region index.
iv_codeIV code pointer used for passing the IV code.
Returns
kStatus_Success upon success
kStatus_Fail otherwise
status_t PRINCE_SetEncryptForAddressRange ( prince_region_t  region,
uint32_t  start_address,
uint32_t  length,
flash_config_t *  flash_context,
bool  regenerate_iv 
)

This function sets the encryption/decryption for specified address range. The SR mask value for the selected Prince region is calculated from provided start_address and length parameters. This calculated value is OR'ed with the actual SR mask value and stored into the PRINCE SR_ENABLE register and also into the persistent memory (FFR) to be used after the device reset. It is possible to define several nonadjacent encrypted areas within one Prince region when calling this function repeatedly. If the length parameter is set to 0, the SR mask value is set to 0 and thus the encryption/decryption for the whole selected Prince region is disabled. Ensure about 800 bytes free space on the stack when calling this routine!

Parameters
regionPRINCE region index.
start_addressstart address of the area to be encrypted/decrypted.
lengthlength of the area to be encrypted/decrypted.
flash_contextpointer to the flash driver context structure.
regenerate_ivflag to allow IV code regenerating, storing into the persistent memory (FFR) and loading into the PRINCE engine
Returns
kStatus_Success upon success
kStatus_Fail otherwise
status_t PRINCE_GetRegionSREnable ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t *  sr_enable 
)

This function gets PRINCE SR_ENABLE register.

Parameters
basePRINCE peripheral address.
regionPRINCE region index.
sr_enableSub-Region Enable register pointer.
Returns
kStatus_Success upon success
kStatus_InvalidArgument
status_t PRINCE_GetRegionBaseAddress ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t *  region_base_addr 
)

This function gets PRINCE BASE_ADDR register.

Parameters
basePRINCE peripheral address.
regionPRINCE region index.
region_base_addrRegion base address pointer.
Returns
kStatus_Success upon success
kStatus_InvalidArgument
status_t PRINCE_SetRegionIV ( PRINCE_Type *  base,
prince_region_t  region,
const uint8_t  iv[8] 
)

This function sets specified AES IV for the given region.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
iv64-bit AES IV in little-endian byte order.
status_t PRINCE_SetRegionBaseAddress ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t  region_base_addr 
)

This function configures PRINCE region base address.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
region_base_addrBase Address for region.
status_t PRINCE_SetRegionSREnable ( PRINCE_Type *  base,
prince_region_t  region,
uint32_t  sr_enable 
)

This function configures PRINCE SR_ENABLE register.

Parameters
basePRINCE peripheral address.
regionSelection of the PRINCE region to be configured.
sr_enableSub-Region Enable register value.
status_t PRINCE_FlashEraseWithChecker ( flash_config_t *  config,
uint32_t  start,
uint32_t  lengthInBytes,
uint32_t  key 
)

This function erases the appropriate number of flash sectors based on the desired start address and length. It deals with the flash erase function complenentary to the standard erase API of the IAP1 driver. This implementation additionally checks if the whole encrypted PRINCE subregions are erased at once to avoid secrets revealing. The checker implementation is limited to one contiguous PRINCE-controlled memory area.

Parameters
configThe pointer to the flash driver context structure.
startThe start address of the desired flash memory to be erased. The start address needs to be prince-sburegion-aligned.
lengthInBytesThe length, given in bytes (not words or long-words) to be erased. Must be prince-sburegion-size-aligned.
keyThe value used to validate all flash erase APIs.
Returns
kStatus_FLASH_Success API was executed successfully.
kStatus_FLASH_InvalidArgument An invalid argument is provided.
kStatus_FLASH_AlignmentError The parameter is not aligned with the specified baseline.
kStatus_FLASH_AddressError The address is out of range.
kStatus_FLASH_EraseKeyError The API erase key is invalid.
kStatus_FLASH_CommandFailure Run-time error during the command execution.
kStatus_FLASH_CommandNotSupported Flash API is not supported.
kStatus_FLASH_EccError A correctable or uncorrectable error during command execution.
kStatus_FLASH_EncryptedRegionsEraseNotDoneAtOnce Encrypted flash subregions are not erased at once.
status_t PRINCE_FlashProgramWithChecker ( flash_config_t *  config,
uint32_t  start,
uint8_t *  src,
uint32_t  lengthInBytes 
)

This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length. It deals with the flash program function complenentary to the standard program API of the IAP1 driver. This implementation additionally checks if the whole PRINCE subregions are programmed at once to avoid secrets revealing. The checker implementation is limited to one contiguous PRINCE-controlled memory area.

Parameters
configThe pointer to the flash driver context structure.
startThe start address of the desired flash memory to be programmed. Must be prince-sburegion-aligned.
srcA pointer to the source buffer of data that is to be programmed into the flash.
lengthInBytesThe length, given in bytes (not words or long-words), to be programmed. Must be prince-sburegion-size-aligned.
Returns
kStatus_FLASH_Success API was executed successfully.
kStatus_FLASH_InvalidArgument An invalid argument is provided.
kStatus_FLASH_AlignmentError Parameter is not aligned with the specified baseline.
kStatus_FLASH_AddressError Address is out of range.
kStatus_FLASH_AccessError Invalid instruction codes and out-of bounds addresses.
kStatus_FLASH_CommandFailure Run-time error during the command execution.
kStatus_FLASH_CommandFailure Run-time error during the command execution.
kStatus_FLASH_CommandNotSupported Flash API is not supported.
kStatus_FLASH_EccError A correctable or uncorrectable error during command execution.
kStatus_FLASH_SizeError Encrypted flash subregions are not programmed at once.