The MCUXpresso SDK provides a driver for the Real Time Clock (RTC) of MCUXpresso SDK devices.
Function groups
The RTC driver supports operating the module as a time counter.
Initialization and deinitialization
The function RTC_Init() initializes the RTC with specified configurations. The function RTC_GetDefaultConfig() gets the default configurations.
The function RTC_Deinit() disables the RTC timer and disables the module clock.
Set & Get Datetime
The function RTC_SetDatetime() sets the timer period in seconds. Users pass in the details in date & time format by using the below data structure.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/rtc The function RTC_GetDatetime() reads the current timer value in seconds, converts it to date & time format and stores it into a datetime structure passed in by the user.
Set & Get Alarm
The function RTC_SetAlarm() sets the alarm time period in seconds. Users pass in the details in date & time format by using the datetime data structure.
The function RTC_GetAlarm() reads the alarm time in seconds, converts it to date & time format and stores it into a datetime structure passed in by the user.
Start & Stop timer
The function RTC_StartTimer() starts the RTC time counter.
The function RTC_StopTimer() stops the RTC time counter.
Status
Provides functions to get and clear the RTC status.
Interrupt
Provides functions to enable/disable RTC interrupts and get current enabled interrupts.
RTC Oscillator
Some SoC's allow control of the RTC oscillator through the RTC module.
The function RTC_SetOscCapLoad() allows the user to modify the capacitor load configuration of the RTC oscillator.
Monotonic Counter
Some SoC's have a 64-bit Monotonic counter available in the RTC module.
The function RTC_SetMonotonicCounter() writes a 64-bit to the counter.
The function RTC_GetMonotonicCounter() reads the monotonic counter and returns the 64-bit counter value to the user.
The function RTC_IncrementMonotonicCounter() increments the Monotonic Counter by one.
Typical use case
RTC tick example
Example to set the RTC current time and trigger an alarm. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/rtc
|
enum | rtc_interrupt_enable_t {
kRTC_TimeInvalidInterruptEnable = (1U << 0U),
kRTC_TimeOverflowInterruptEnable = (1U << 1U),
kRTC_AlarmInterruptEnable = (1U << 2U),
kRTC_SecondsInterruptEnable = (1U << 3U),
kRTC_MonotonicOverflowInterruptEnable = (1U << 4U)
} |
| List of RTC interrupts. More...
|
|
enum | rtc_status_flags_t {
kRTC_TimeInvalidFlag = (1U << 0U),
kRTC_TimeOverflowFlag = (1U << 1U),
kRTC_AlarmFlag = (1U << 2U),
kRTC_MonotonicOverflowFlag = (1U << 3U)
} |
| List of RTC flags. More...
|
|
enum | rtc_osc_cap_load_t {
kRTC_Capacitor_2p = RTC_CR_SC2P_MASK,
kRTC_Capacitor_4p = RTC_CR_SC4P_MASK,
kRTC_Capacitor_8p = RTC_CR_SC8P_MASK,
kRTC_Capacitor_16p = RTC_CR_SC16P_MASK
} |
| List of RTC Oscillator capacitor load settings. More...
|
|
uint16_t rtc_datetime_t::year |
uint8_t rtc_datetime_t::month |
uint8_t rtc_datetime_t::day |
uint8_t rtc_datetime_t::hour |
uint8_t rtc_datetime_t::minute |
uint8_t rtc_datetime_t::second |
This structure holds the configuration settings for the RTC peripheral. To initialize this structure to reasonable defaults, call the RTC_GetDefaultConfig() function and pass a pointer to your config structure instance.
The config struct can be made const so it resides in flash
Data Fields |
bool | wakeupSelect |
| true: Wakeup pin outputs the 32 KHz clock; false:Wakeup pin used to wakeup the chip
|
|
bool | updateMode |
| true: Registers can be written even when locked under certain conditions, false: No writes allowed when registers are locked
|
|
bool | supervisorAccess |
| true: Non-supervisor accesses are allowed; false: Non-supervisor accesses are not supported
|
|
uint32_t | compensationInterval |
| Compensation interval that is written to the CIR field in RTC TCR Register.
|
|
uint32_t | compensationTime |
| Compensation time that is written to the TCR field in RTC TCR Register.
|
|
Enumerator |
---|
kRTC_TimeInvalidInterruptEnable |
Time invalid interrupt.
|
kRTC_TimeOverflowInterruptEnable |
Time overflow interrupt.
|
kRTC_AlarmInterruptEnable |
Alarm interrupt.
|
kRTC_SecondsInterruptEnable |
Seconds interrupt.
|
kRTC_MonotonicOverflowInterruptEnable |
Monotonic Overflow Interrupt Enable.
|
Enumerator |
---|
kRTC_TimeInvalidFlag |
Time invalid flag.
|
kRTC_TimeOverflowFlag |
Time overflow flag.
|
kRTC_AlarmFlag |
Alarm flag.
|
kRTC_MonotonicOverflowFlag |
Monotonic Overflow Flag.
|
Enumerator |
---|
kRTC_Capacitor_2p |
2 pF capacitor load
|
kRTC_Capacitor_4p |
4 pF capacitor load
|
kRTC_Capacitor_8p |
8 pF capacitor load
|
kRTC_Capacitor_16p |
16 pF capacitor load
|
void RTC_Init |
( |
RTC_Type * |
base, |
|
|
const rtc_config_t * |
config |
|
) |
| |
This function issues a software reset if the timer invalid flag is set.
- Note
- This API should be called at the beginning of the application using the RTC driver.
- Parameters
-
base | RTC peripheral base address |
config | Pointer to the user's RTC configuration structure. |
static void RTC_Deinit |
( |
RTC_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
base | RTC peripheral base address |
The default values are as follows.
* config->wakeupSelect = false;
* config->updateMode = false;
* config->supervisorAccess = false;
* config->compensationInterval = 0;
* config->compensationTime = 0;
*
- Parameters
-
config | Pointer to the user's RTC configuration structure. |
status_t RTC_SetDatetime |
( |
RTC_Type * |
base, |
|
|
const rtc_datetime_t * |
datetime |
|
) |
| |
The RTC counter must be stopped prior to calling this function because writes to the RTC seconds register fail if the RTC counter is running.
- Parameters
-
base | RTC peripheral base address |
datetime | Pointer to the structure where the date and time details are stored. |
- Returns
- kStatus_Success: Success in setting the time and starting the RTC kStatus_InvalidArgument: Error because the datetime format is incorrect
- Parameters
-
base | RTC peripheral base address |
datetime | Pointer to the structure where the date and time details are stored. |
status_t RTC_SetAlarm |
( |
RTC_Type * |
base, |
|
|
const rtc_datetime_t * |
alarmTime |
|
) |
| |
The function checks whether the specified alarm time is greater than the present time. If not, the function does not set the alarm and returns an error.
- Parameters
-
base | RTC peripheral base address |
alarmTime | Pointer to the structure where the alarm time is stored. |
- Returns
- kStatus_Success: success in setting the RTC alarm kStatus_InvalidArgument: Error because the alarm datetime format is incorrect kStatus_Fail: Error because the alarm time has already passed
- Parameters
-
base | RTC peripheral base address |
datetime | Pointer to the structure where the alarm date and time details are stored. |
void RTC_EnableInterrupts |
( |
RTC_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
base | RTC peripheral base address |
mask | The interrupts to enable. This is a logical OR of members of the enumeration rtc_interrupt_enable_t |
void RTC_DisableInterrupts |
( |
RTC_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
base | RTC peripheral base address |
mask | The interrupts to enable. This is a logical OR of members of the enumeration rtc_interrupt_enable_t |
uint32_t RTC_GetEnabledInterrupts |
( |
RTC_Type * |
base | ) |
|
- Parameters
-
base | RTC peripheral base address |
- Returns
- The enabled interrupts. This is the logical OR of members of the enumeration rtc_interrupt_enable_t
uint32_t RTC_GetStatusFlags |
( |
RTC_Type * |
base | ) |
|
- Parameters
-
base | RTC peripheral base address |
- Returns
- The status flags. This is the logical OR of members of the enumeration rtc_status_flags_t
void RTC_ClearStatusFlags |
( |
RTC_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
- Parameters
-
base | RTC peripheral base address |
mask | The status flags to clear. This is a logical OR of members of the enumeration rtc_status_flags_t |
static void RTC_SetClockSource |
( |
RTC_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
base | RTC peripheral base address |
- Note
- After setting this bit, wait the oscillator startup time before enabling the time counter to allow the 32.768 kHz clock time to stabilize.
static void RTC_StartTimer |
( |
RTC_Type * |
base | ) |
|
|
inlinestatic |
After calling this function, the timer counter increments once a second provided SR[TOF] or SR[TIF] are not set.
- Parameters
-
base | RTC peripheral base address |
static void RTC_StopTimer |
( |
RTC_Type * |
base | ) |
|
|
inlinestatic |
RTC's seconds register can be written to only when the timer is stopped.
- Parameters
-
base | RTC peripheral base address |
static void RTC_SetOscCapLoad |
( |
RTC_Type * |
base, |
|
|
uint32_t |
capLoad |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | RTC peripheral base address |
capLoad | Oscillator loads to enable. This is a logical OR of members of the enumeration rtc_osc_cap_load_t |
static void RTC_Reset |
( |
RTC_Type * |
base | ) |
|
|
inlinestatic |
This resets all RTC registers except for the SWR bit and the RTC_WAR and RTC_RAR registers. The SWR bit is cleared by software explicitly clearing it.
- Parameters
-
base | RTC peripheral base address |
void RTC_GetMonotonicCounter |
( |
RTC_Type * |
base, |
|
|
uint64_t * |
counter |
|
) |
| |
- Parameters
-
base | RTC peripheral base address |
counter | Pointer to variable where the value is stored. |
void RTC_SetMonotonicCounter |
( |
RTC_Type * |
base, |
|
|
uint64_t |
counter |
|
) |
| |
The Monotonic Overflow Flag in RTC_SR is cleared due to the API.
- Parameters
-
base | RTC peripheral base address |
counter | Counter value |
status_t RTC_IncrementMonotonicCounter |
( |
RTC_Type * |
base | ) |
|
Increments the Monotonic Counter (registers RTC_MCLR and RTC_MCHR accordingly) by setting the monotonic counter enable (MER[MCE]) and then writing to the RTC_MCLR register. A write to the monotonic counter low that causes it to overflow also increments the monotonic counter high.
- Parameters
-
base | RTC peripheral base address |
- Returns
- kStatus_Success: success kStatus_Fail: error occurred, either time invalid or monotonic overflow flag was found