The MCUXpresso SDK provides a peripheral driver for the Serial Audio Interface (SAI) module of MCUXpresso SDK devices.
SAI driver includes functional APIs and transactional APIs.
Functional APIs target low-level APIs. Functional APIs can be used for SAI initialization, configuration and operation, and for optimization and customization purposes. Using the functional API requires the knowledge of the SAI peripheral and how to organize functional APIs to meet the application requirements. All functional API use the peripheral base address as the first parameter. SAI functional operation groups provide the functional API set.
Transactional APIs target high-level APIs. Transactional APIs can be used to enable the peripheral and in the application if the code size and performance of transactional APIs satisfy the requirements. If the code size and performance are a critical requirement, see the transactional API implementation and write a custom code. All transactional APIs use the sai_handle_t as the first parameter. Initialize the handle by calling the SAI_TransferTxCreateHandle() or SAI_TransferRxCreateHandle() API.
Transactional APIs support asynchronous transfer. This means that the functions SAI_TransferSendNonBlocking() and SAI_TransfferReceiveNonBlocking() set up the interrupt for data transfer. When the transfer completes, the upper layer is notified through a callback function with the kStatus_SAI_TxIdle and kStatus_SAI_RxIdle status.
Typical use case
SAI Send/receive using an interrupt method
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sai
SAI Send/receive using a DMA method
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/sai
|
typedef void(* | sai_transfer_callback_t )(I2S_Type *base, sai_handle_t *handle, status_t status, void *userData) |
| SAI transfer callback prototype.
|
|
|
enum | _sai_status_t {
kStatus_SAI_TxBusy = MAKE_STATUS(kStatusGroup_SAI, 0),
kStatus_SAI_RxBusy = MAKE_STATUS(kStatusGroup_SAI, 1),
kStatus_SAI_TxError = MAKE_STATUS(kStatusGroup_SAI, 2),
kStatus_SAI_RxError = MAKE_STATUS(kStatusGroup_SAI, 3),
kStatus_SAI_QueueFull = MAKE_STATUS(kStatusGroup_SAI, 4),
kStatus_SAI_TxIdle = MAKE_STATUS(kStatusGroup_SAI, 5),
kStatus_SAI_RxIdle = MAKE_STATUS(kStatusGroup_SAI, 6)
} |
| SAI return status. More...
|
|
enum | sai_protocol_t {
kSAI_BusLeftJustified = 0x0U,
kSAI_BusRightJustified,
kSAI_BusI2S,
kSAI_BusPCMA,
kSAI_BusPCMB
} |
| Define the SAI bus type. More...
|
|
enum | sai_master_slave_t {
kSAI_Master = 0x0U,
kSAI_Slave = 0x1U
} |
| Master or slave mode. More...
|
|
enum | sai_mono_stereo_t {
kSAI_Stereo = 0x0U,
kSAI_MonoRight,
kSAI_MonoLeft
} |
| Mono or stereo audio format. More...
|
|
enum | sai_sync_mode_t {
kSAI_ModeAsync = 0x0U,
kSAI_ModeSync,
kSAI_ModeSyncWithOtherTx,
kSAI_ModeSyncWithOtherRx
} |
| Synchronous or asynchronous mode. More...
|
|
enum | sai_mclk_source_t {
kSAI_MclkSourceSysclk = 0x0U,
kSAI_MclkSourceSelect1,
kSAI_MclkSourceSelect2,
kSAI_MclkSourceSelect3
} |
| Mater clock source. More...
|
|
enum | sai_bclk_source_t {
kSAI_BclkSourceBusclk = 0x0U,
kSAI_BclkSourceMclkDiv,
kSAI_BclkSourceOtherSai0,
kSAI_BclkSourceOtherSai1
} |
| Bit clock source. More...
|
|
enum | _sai_interrupt_enable_t {
kSAI_WordStartInterruptEnable,
kSAI_SyncErrorInterruptEnable = I2S_TCSR_SEIE_MASK,
kSAI_FIFOWarningInterruptEnable = I2S_TCSR_FWIE_MASK,
kSAI_FIFOErrorInterruptEnable = I2S_TCSR_FEIE_MASK,
kSAI_FIFORequestInterruptEnable = I2S_TCSR_FRIE_MASK
} |
| The SAI interrupt enable flag. More...
|
|
enum | _sai_dma_enable_t {
kSAI_FIFOWarningDMAEnable = I2S_TCSR_FWDE_MASK,
kSAI_FIFORequestDMAEnable = I2S_TCSR_FRDE_MASK
} |
| The DMA request sources. More...
|
|
enum | _sai_flags {
kSAI_WordStartFlag = I2S_TCSR_WSF_MASK,
kSAI_SyncErrorFlag = I2S_TCSR_SEF_MASK,
kSAI_FIFOErrorFlag = I2S_TCSR_FEF_MASK,
kSAI_FIFORequestFlag = I2S_TCSR_FRF_MASK,
kSAI_FIFOWarningFlag = I2S_TCSR_FWF_MASK
} |
| The SAI status flag. More...
|
|
enum | sai_reset_type_t {
kSAI_ResetTypeSoftware = I2S_TCSR_SR_MASK,
kSAI_ResetTypeFIFO = I2S_TCSR_FR_MASK,
kSAI_ResetAll = I2S_TCSR_SR_MASK | I2S_TCSR_FR_MASK
} |
| The reset type. More...
|
|
enum | sai_sample_rate_t {
kSAI_SampleRate8KHz = 8000U,
kSAI_SampleRate11025Hz = 11025U,
kSAI_SampleRate12KHz = 12000U,
kSAI_SampleRate16KHz = 16000U,
kSAI_SampleRate22050Hz = 22050U,
kSAI_SampleRate24KHz = 24000U,
kSAI_SampleRate32KHz = 32000U,
kSAI_SampleRate44100Hz = 44100U,
kSAI_SampleRate48KHz = 48000U,
kSAI_SampleRate96KHz = 96000U
} |
| Audio sample rate. More...
|
|
enum | sai_word_width_t {
kSAI_WordWidth8bits = 8U,
kSAI_WordWidth16bits = 16U,
kSAI_WordWidth24bits = 24U,
kSAI_WordWidth32bits = 32U
} |
| Audio word width. More...
|
|
|
void | SAI_TxSetFormat (I2S_Type *base, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Tx audio format. More...
|
|
void | SAI_RxSetFormat (I2S_Type *base, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Rx audio format. More...
|
|
void | SAI_WriteBlocking (I2S_Type *base, uint32_t channel, uint32_t bitWidth, uint8_t *buffer, uint32_t size) |
| Sends data using a blocking method. More...
|
|
static void | SAI_WriteData (I2S_Type *base, uint32_t channel, uint32_t data) |
| Writes data into SAI FIFO. More...
|
|
void | SAI_ReadBlocking (I2S_Type *base, uint32_t channel, uint32_t bitWidth, uint8_t *buffer, uint32_t size) |
| Receives data using a blocking method. More...
|
|
static uint32_t | SAI_ReadData (I2S_Type *base, uint32_t channel) |
| Reads data from the SAI FIFO. More...
|
|
|
void | SAI_TransferTxCreateHandle (I2S_Type *base, sai_handle_t *handle, sai_transfer_callback_t callback, void *userData) |
| Initializes the SAI Tx handle. More...
|
|
void | SAI_TransferRxCreateHandle (I2S_Type *base, sai_handle_t *handle, sai_transfer_callback_t callback, void *userData) |
| Initializes the SAI Rx handle. More...
|
|
status_t | SAI_TransferTxSetFormat (I2S_Type *base, sai_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Tx audio format. More...
|
|
status_t | SAI_TransferRxSetFormat (I2S_Type *base, sai_handle_t *handle, sai_transfer_format_t *format, uint32_t mclkSourceClockHz, uint32_t bclkSourceClockHz) |
| Configures the SAI Rx audio format. More...
|
|
status_t | SAI_TransferSendNonBlocking (I2S_Type *base, sai_handle_t *handle, sai_transfer_t *xfer) |
| Performs an interrupt non-blocking send transfer on SAI. More...
|
|
status_t | SAI_TransferReceiveNonBlocking (I2S_Type *base, sai_handle_t *handle, sai_transfer_t *xfer) |
| Performs an interrupt non-blocking receive transfer on SAI. More...
|
|
status_t | SAI_TransferGetSendCount (I2S_Type *base, sai_handle_t *handle, size_t *count) |
| Gets a set byte count. More...
|
|
status_t | SAI_TransferGetReceiveCount (I2S_Type *base, sai_handle_t *handle, size_t *count) |
| Gets a received byte count. More...
|
|
void | SAI_TransferAbortSend (I2S_Type *base, sai_handle_t *handle) |
| Aborts the current send. More...
|
|
void | SAI_TransferAbortReceive (I2S_Type *base, sai_handle_t *handle) |
| Aborts the the current IRQ receive. More...
|
|
void | SAI_TransferTerminateSend (I2S_Type *base, sai_handle_t *handle) |
| Terminate all SAI send. More...
|
|
void | SAI_TransferTerminateReceive (I2S_Type *base, sai_handle_t *handle) |
| Terminate all SAI receive. More...
|
|
void | SAI_TransferTxHandleIRQ (I2S_Type *base, sai_handle_t *handle) |
| Tx interrupt handler. More...
|
|
void | SAI_TransferRxHandleIRQ (I2S_Type *base, sai_handle_t *handle) |
| Tx interrupt handler. More...
|
|
struct sai_transfer_format_t |
uint8_t sai_transfer_format_t::channel |
bool sai_transfer_format_t::isFrameSyncCompact |
uint8_t* sai_transfer_t::data |
size_t sai_transfer_t::dataSize |
#define SAI_XFER_QUEUE_SIZE (4) |
Enumerator |
---|
kStatus_SAI_TxBusy |
SAI Tx is busy.
|
kStatus_SAI_RxBusy |
SAI Rx is busy.
|
kStatus_SAI_TxError |
SAI Tx FIFO error.
|
kStatus_SAI_RxError |
SAI Rx FIFO error.
|
kStatus_SAI_QueueFull |
SAI transfer queue is full.
|
kStatus_SAI_TxIdle |
SAI Tx is idle.
|
kStatus_SAI_RxIdle |
SAI Rx is idle.
|
Enumerator |
---|
kSAI_BusLeftJustified |
Uses left justified format.
|
kSAI_BusRightJustified |
Uses right justified format.
|
kSAI_BusI2S |
Uses I2S format.
|
kSAI_BusPCMA |
Uses I2S PCM A format.
|
kSAI_BusPCMB |
Uses I2S PCM B format.
|
Enumerator |
---|
kSAI_Master |
Master mode.
|
kSAI_Slave |
Slave mode.
|
Enumerator |
---|
kSAI_Stereo |
Stereo sound.
|
kSAI_MonoRight |
Only Right channel have sound.
|
kSAI_MonoLeft |
Only left channel have sound.
|
Enumerator |
---|
kSAI_ModeAsync |
Asynchronous mode.
|
kSAI_ModeSync |
Synchronous mode (with receiver or transmit)
|
kSAI_ModeSyncWithOtherTx |
Synchronous with another SAI transmit.
|
kSAI_ModeSyncWithOtherRx |
Synchronous with another SAI receiver.
|
Enumerator |
---|
kSAI_MclkSourceSysclk |
Master clock from the system clock.
|
kSAI_MclkSourceSelect1 |
Master clock from source 1.
|
kSAI_MclkSourceSelect2 |
Master clock from source 2.
|
kSAI_MclkSourceSelect3 |
Master clock from source 3.
|
Enumerator |
---|
kSAI_BclkSourceBusclk |
Bit clock using bus clock.
|
kSAI_BclkSourceMclkDiv |
Bit clock using master clock divider.
|
kSAI_BclkSourceOtherSai0 |
Bit clock from other SAI device.
|
kSAI_BclkSourceOtherSai1 |
Bit clock from other SAI device.
|
Enumerator |
---|
kSAI_WordStartInterruptEnable |
Word start flag, means the first word in a frame detected.
|
kSAI_SyncErrorInterruptEnable |
Sync error flag, means the sync error is detected.
|
kSAI_FIFOWarningInterruptEnable |
FIFO warning flag, means the FIFO is empty.
|
kSAI_FIFOErrorInterruptEnable |
FIFO error flag.
|
kSAI_FIFORequestInterruptEnable |
FIFO request, means reached watermark.
|
Enumerator |
---|
kSAI_FIFOWarningDMAEnable |
FIFO warning caused by the DMA request.
|
kSAI_FIFORequestDMAEnable |
FIFO request caused by the DMA request.
|
Enumerator |
---|
kSAI_WordStartFlag |
Word start flag, means the first word in a frame detected.
|
kSAI_SyncErrorFlag |
Sync error flag, means the sync error is detected.
|
kSAI_FIFOErrorFlag |
FIFO error flag.
|
kSAI_FIFORequestFlag |
FIFO request flag.
|
kSAI_FIFOWarningFlag |
FIFO warning flag.
|
Enumerator |
---|
kSAI_ResetTypeSoftware |
Software reset, reset the logic state.
|
kSAI_ResetTypeFIFO |
FIFO reset, reset the FIFO read and write pointer.
|
kSAI_ResetAll |
All reset.
|
Enumerator |
---|
kSAI_SampleRate8KHz |
Sample rate 8000 Hz.
|
kSAI_SampleRate11025Hz |
Sample rate 11025 Hz.
|
kSAI_SampleRate12KHz |
Sample rate 12000 Hz.
|
kSAI_SampleRate16KHz |
Sample rate 16000 Hz.
|
kSAI_SampleRate22050Hz |
Sample rate 22050 Hz.
|
kSAI_SampleRate24KHz |
Sample rate 24000 Hz.
|
kSAI_SampleRate32KHz |
Sample rate 32000 Hz.
|
kSAI_SampleRate44100Hz |
Sample rate 44100 Hz.
|
kSAI_SampleRate48KHz |
Sample rate 48000 Hz.
|
kSAI_SampleRate96KHz |
Sample rate 96000 Hz.
|
Enumerator |
---|
kSAI_WordWidth8bits |
Audio data width 8 bits.
|
kSAI_WordWidth16bits |
Audio data width 16 bits.
|
kSAI_WordWidth24bits |
Audio data width 24 bits.
|
kSAI_WordWidth32bits |
Audio data width 32 bits.
|
void SAI_TxInit |
( |
I2S_Type * |
base, |
|
|
const sai_config_t * |
config |
|
) |
| |
Ungates the SAI clock, resets the module, and configures SAI Tx with a configuration structure. The configuration structure can be custom filled or set with default values by SAI_TxGetDefaultConfig().
- Note
- This API should be called at the beginning of the application to use the SAI driver. Otherwise, accessing the SAIM module can cause a hard fault because the clock is not enabled.
- Parameters
-
base | SAI base pointer |
config | SAI configuration structure. |
void SAI_RxInit |
( |
I2S_Type * |
base, |
|
|
const sai_config_t * |
config |
|
) |
| |
Ungates the SAI clock, resets the module, and configures the SAI Rx with a configuration structure. The configuration structure can be custom filled or set with default values by SAI_RxGetDefaultConfig().
- Note
- This API should be called at the beginning of the application to use the SAI driver. Otherwise, accessing the SAI module can cause a hard fault because the clock is not enabled.
- Parameters
-
base | SAI base pointer |
config | SAI configuration structure. |
This API initializes the configuration structure for use in SAI_TxConfig(). The initialized structure can remain unchanged in SAI_TxConfig(), or it can be modified before calling SAI_TxConfig(). This is an example.
- Parameters
-
config | pointer to master configuration structure |
This API initializes the configuration structure for use in SAI_RxConfig(). The initialized structure can remain unchanged in SAI_RxConfig() or it can be modified before calling SAI_RxConfig(). This is an example.
- Parameters
-
config | pointer to master configuration structure |
void SAI_Deinit |
( |
I2S_Type * |
base | ) |
|
This API gates the SAI clock. The SAI module can't operate unless SAI_TxInit or SAI_RxInit is called to enable the clock.
- Parameters
-
void SAI_TxReset |
( |
I2S_Type * |
base | ) |
|
This function enables the software reset and FIFO reset of SAI Tx. After reset, clear the reset bit.
- Parameters
-
void SAI_RxReset |
( |
I2S_Type * |
base | ) |
|
This function enables the software reset and FIFO reset of SAI Rx. After reset, clear the reset bit.
- Parameters
-
void SAI_TxEnable |
( |
I2S_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
- Parameters
-
base | SAI base pointer |
enable | True means enable SAI Tx, false means disable. |
void SAI_RxEnable |
( |
I2S_Type * |
base, |
|
|
bool |
enable |
|
) |
| |
- Parameters
-
base | SAI base pointer |
enable | True means enable SAI Rx, false means disable. |
static uint32_t SAI_TxGetStatusFlag |
( |
I2S_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
- Returns
- SAI Tx status flag value. Use the Status Mask to get the status value needed.
static void SAI_TxClearStatusFlags |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | State mask. It can be a combination of the following source if defined:
- kSAI_WordStartFlag
- kSAI_SyncErrorFlag
- kSAI_FIFOErrorFlag
|
static uint32_t SAI_RxGetStatusFlag |
( |
I2S_Type * |
base | ) |
|
|
inlinestatic |
- Parameters
-
- Returns
- SAI Rx status flag value. Use the Status Mask to get the status value needed.
static void SAI_RxClearStatusFlags |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | State mask. It can be a combination of the following sources if defined.
- kSAI_WordStartFlag
- kSAI_SyncErrorFlag
- kSAI_FIFOErrorFlag
|
FIFO reset means clear all the data in the FIFO, and make the FIFO pointer both to 0. Software reset means claer the Tx internal logic, including the bit clock, frame count etc. But software reset will not clear any configuration registers like TCR1~TCR5. This function will also clear all the error flags such as FIFO error, sync error etc.
- Parameters
-
base | SAI base pointer |
type | Reset type, FIFO reset or software reset |
FIFO reset means clear all the data in the FIFO, and make the FIFO pointer both to 0. Software reset means claer the Rx internal logic, including the bit clock, frame count etc. But software reset will not clear any configuration registers like RCR1~RCR5. This function will also clear all the error flags such as FIFO error, sync error etc.
- Parameters
-
base | SAI base pointer |
type | Reset type, FIFO reset or software reset |
void SAI_TxSetChannelFIFOMask |
( |
I2S_Type * |
base, |
|
|
uint8_t |
mask |
|
) |
| |
- Parameters
-
base | SAI base pointer |
mask | Channel enable mask, 0 means all channel FIFO disabled, 1 means channel 0 enabled, 3 means both channel 0 and channel 1 enabled. |
void SAI_RxSetChannelFIFOMask |
( |
I2S_Type * |
base, |
|
|
uint8_t |
mask |
|
) |
| |
- Parameters
-
base | SAI base pointer |
mask | Channel enable mask, 0 means all channel FIFO disabled, 1 means channel 0 enabled, 3 means both channel 0 and channel 1 enabled. |
static void SAI_TxEnableInterrupts |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | interrupt source The parameter can be a combination of the following sources if defined.
- kSAI_WordStartInterruptEnable
- kSAI_SyncErrorInterruptEnable
- kSAI_FIFOWarningInterruptEnable
- kSAI_FIFORequestInterruptEnable
- kSAI_FIFOErrorInterruptEnable
|
static void SAI_RxEnableInterrupts |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | interrupt source The parameter can be a combination of the following sources if defined.
- kSAI_WordStartInterruptEnable
- kSAI_SyncErrorInterruptEnable
- kSAI_FIFOWarningInterruptEnable
- kSAI_FIFORequestInterruptEnable
- kSAI_FIFOErrorInterruptEnable
|
static void SAI_TxDisableInterrupts |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | interrupt source The parameter can be a combination of the following sources if defined.
- kSAI_WordStartInterruptEnable
- kSAI_SyncErrorInterruptEnable
- kSAI_FIFOWarningInterruptEnable
- kSAI_FIFORequestInterruptEnable
- kSAI_FIFOErrorInterruptEnable
|
static void SAI_RxDisableInterrupts |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | interrupt source The parameter can be a combination of the following sources if defined.
- kSAI_WordStartInterruptEnable
- kSAI_SyncErrorInterruptEnable
- kSAI_FIFOWarningInterruptEnable
- kSAI_FIFORequestInterruptEnable
- kSAI_FIFOErrorInterruptEnable
|
static void SAI_TxEnableDMA |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | DMA source The parameter can be combination of the following sources if defined.
- kSAI_FIFOWarningDMAEnable
- kSAI_FIFORequestDMAEnable
|
enable | True means enable DMA, false means disable DMA. |
static void SAI_RxEnableDMA |
( |
I2S_Type * |
base, |
|
|
uint32_t |
mask, |
|
|
bool |
enable |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer |
mask | DMA source The parameter can be a combination of the following sources if defined.
- kSAI_FIFOWarningDMAEnable
- kSAI_FIFORequestDMAEnable
|
enable | True means enable DMA, false means disable DMA. |
static uint32_t SAI_TxGetDataRegisterAddress |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel |
|
) |
| |
|
inlinestatic |
This API is used to provide a transfer address for the SAI DMA transfer configuration.
- Parameters
-
base | SAI base pointer. |
channel | Which data channel used. |
- Returns
- data register address.
static uint32_t SAI_RxGetDataRegisterAddress |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel |
|
) |
| |
|
inlinestatic |
This API is used to provide a transfer address for the SAI DMA transfer configuration.
- Parameters
-
base | SAI base pointer. |
channel | Which data channel used. |
- Returns
- data register address.
void SAI_TxSetFormat |
( |
I2S_Type * |
base, |
|
|
sai_transfer_format_t * |
format, |
|
|
uint32_t |
mclkSourceClockHz, |
|
|
uint32_t |
bclkSourceClockHz |
|
) |
| |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred.
- Parameters
-
base | SAI base pointer. |
format | Pointer to the SAI audio data format structure. |
mclkSourceClockHz | SAI master clock source frequency in Hz. |
bclkSourceClockHz | SAI bit clock source frequency in Hz. If the bit clock source is a master clock, this value should equal the masterClockHz. |
void SAI_RxSetFormat |
( |
I2S_Type * |
base, |
|
|
sai_transfer_format_t * |
format, |
|
|
uint32_t |
mclkSourceClockHz, |
|
|
uint32_t |
bclkSourceClockHz |
|
) |
| |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred.
- Parameters
-
base | SAI base pointer. |
format | Pointer to the SAI audio data format structure. |
mclkSourceClockHz | SAI master clock source frequency in Hz. |
bclkSourceClockHz | SAI bit clock source frequency in Hz. If the bit clock source is a master clock, this value should equal the masterClockHz. |
void SAI_WriteBlocking |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel, |
|
|
uint32_t |
bitWidth, |
|
|
uint8_t * |
buffer, |
|
|
uint32_t |
size |
|
) |
| |
- Note
- This function blocks by polling until data is ready to be sent.
- Parameters
-
base | SAI base pointer. |
channel | Data channel used. |
bitWidth | How many bits in an audio word; usually 8/16/24/32 bits. |
buffer | Pointer to the data to be written. |
size | Bytes to be written. |
static void SAI_WriteData |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel, |
|
|
uint32_t |
data |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer. |
channel | Data channel used. |
data | Data needs to be written. |
void SAI_ReadBlocking |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel, |
|
|
uint32_t |
bitWidth, |
|
|
uint8_t * |
buffer, |
|
|
uint32_t |
size |
|
) |
| |
- Note
- This function blocks by polling until data is ready to be sent.
- Parameters
-
base | SAI base pointer. |
channel | Data channel used. |
bitWidth | How many bits in an audio word; usually 8/16/24/32 bits. |
buffer | Pointer to the data to be read. |
size | Bytes to be read. |
static uint32_t SAI_ReadData |
( |
I2S_Type * |
base, |
|
|
uint32_t |
channel |
|
) |
| |
|
inlinestatic |
- Parameters
-
base | SAI base pointer. |
channel | Data channel used. |
- Returns
- Data in SAI FIFO.
void SAI_TransferTxCreateHandle |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_callback_t |
callback, |
|
|
void * |
userData |
|
) |
| |
This function initializes the Tx handle for the SAI Tx transactional APIs. Call this function once to get the handle initialized.
- Parameters
-
base | SAI base pointer |
handle | SAI handle pointer. |
callback | Pointer to the user callback function. |
userData | User parameter passed to the callback function |
void SAI_TransferRxCreateHandle |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_callback_t |
callback, |
|
|
void * |
userData |
|
) |
| |
This function initializes the Rx handle for the SAI Rx transactional APIs. Call this function once to get the handle initialized.
- Parameters
-
base | SAI base pointer. |
handle | SAI handle pointer. |
callback | Pointer to the user callback function. |
userData | User parameter passed to the callback function. |
status_t SAI_TransferTxSetFormat |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_format_t * |
format, |
|
|
uint32_t |
mclkSourceClockHz, |
|
|
uint32_t |
bclkSourceClockHz |
|
) |
| |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred.
- Parameters
-
base | SAI base pointer. |
handle | SAI handle pointer. |
format | Pointer to the SAI audio data format structure. |
mclkSourceClockHz | SAI master clock source frequency in Hz. |
bclkSourceClockHz | SAI bit clock source frequency in Hz. If a bit clock source is a master clock, this value should equal the masterClockHz in format. |
- Returns
- Status of this function. Return value is the status_t.
status_t SAI_TransferRxSetFormat |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_format_t * |
format, |
|
|
uint32_t |
mclkSourceClockHz, |
|
|
uint32_t |
bclkSourceClockHz |
|
) |
| |
The audio format can be changed at run-time. This function configures the sample rate and audio data format to be transferred.
- Parameters
-
base | SAI base pointer. |
handle | SAI handle pointer. |
format | Pointer to the SAI audio data format structure. |
mclkSourceClockHz | SAI master clock source frequency in Hz. |
bclkSourceClockHz | SAI bit clock source frequency in Hz. If a bit clock source is a master clock, this value should equal the masterClockHz in format. |
- Returns
- Status of this function. Return value is one of status_t.
status_t SAI_TransferSendNonBlocking |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_t * |
xfer |
|
) |
| |
- Note
- This API returns immediately after the transfer initiates. Call the SAI_TxGetTransferStatusIRQ to poll the transfer status and check whether the transfer is finished. If the return status is not kStatus_SAI_Busy, the transfer is finished.
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
xfer | Pointer to the sai_transfer_t structure. |
- Return values
-
kStatus_Success | Successfully started the data receive. |
kStatus_SAI_TxBusy | Previous receive still not finished. |
kStatus_InvalidArgument | The input parameter is invalid. |
status_t SAI_TransferReceiveNonBlocking |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
sai_transfer_t * |
xfer |
|
) |
| |
- Note
- This API returns immediately after the transfer initiates. Call the SAI_RxGetTransferStatusIRQ to poll the transfer status and check whether the transfer is finished. If the return status is not kStatus_SAI_Busy, the transfer is finished.
- Parameters
-
base | SAI base pointer |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
xfer | Pointer to the sai_transfer_t structure. |
- Return values
-
kStatus_Success | Successfully started the data receive. |
kStatus_SAI_RxBusy | Previous receive still not finished. |
kStatus_InvalidArgument | The input parameter is invalid. |
status_t SAI_TransferGetSendCount |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
size_t * |
count |
|
) |
| |
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
count | Bytes count sent. |
- Return values
-
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
status_t SAI_TransferGetReceiveCount |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle, |
|
|
size_t * |
count |
|
) |
| |
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
count | Bytes count received. |
- Return values
-
kStatus_Success | Succeed get the transfer count. |
kStatus_NoTransferInProgress | There is not a non-blocking transaction currently in progress. |
void SAI_TransferAbortSend |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
- Note
- This API can be called any time when an interrupt non-blocking transfer initiates to abort the transfer early.
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
void SAI_TransferAbortReceive |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
- Note
- This API can be called when an interrupt non-blocking transfer initiates to abort the transfer early.
- Parameters
-
base | SAI base pointer |
handle | Pointer to the sai_handle_t structure which stores the transfer state. |
void SAI_TransferTerminateSend |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortSend.
- Parameters
-
base | SAI base pointer. |
handle | SAI eDMA handle pointer. |
void SAI_TransferTerminateReceive |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
This function will clear all transfer slots buffered in the sai queue. If users only want to abort the current transfer slot, please call SAI_TransferAbortReceive.
- Parameters
-
base | SAI base pointer. |
handle | SAI eDMA handle pointer. |
void SAI_TransferTxHandleIRQ |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure. |
void SAI_TransferRxHandleIRQ |
( |
I2S_Type * |
base, |
|
|
sai_handle_t * |
handle |
|
) |
| |
- Parameters
-
base | SAI base pointer. |
handle | Pointer to the sai_handle_t structure. |