![]() |
MCUXpresso SDK API Reference Manual
Rev. 0
NXP Semiconductors
|
Data Structures | |
| struct | rtos_smartcard_context_t |
| Runtime RTOS Smart card driver context. More... | |
Macros | |
| #define | RTOS_SMARTCARD_COMPLETE 0x1u |
| Smart card RTOS transfer complete flag. | |
| #define | RTOS_SMARTCARD_TIMEOUT 0x2u |
| Smart card RTOS transfer time-out flag. | |
| #define | SMARTCARD_Control(base, context, control, param) SMARTCARD_UART_Control(base, context, control, 0) |
| Common Smart card driver API defines. More... | |
| #define | SMARTCARD_Transfer(base, context, xfer) SMARTCARD_UART_TransferNonBlocking(base, context, xfer) |
| Common Smart card API macro. | |
| #define | SMARTCARD_AbortTransfer(base, context) SMARTCARD_UART_AbortTransfer(base, context) |
| Common Smart card API macro. | |
| #define | SMARTCARD_Init(base, context, sourceClockHz) SMARTCARD_UART_Init(base, context, sourceClockHz) |
| Common Smart card API macro. | |
| #define | SMARTCARD_Deinit(base) SMARTCARD_UART_Deinit(base) |
| Common Smart card API macro. | |
| #define | SMARTCARD_GetTransferRemainingBytes(base, context) SMARTCARD_UART_GetTransferRemainingBytes(base, context) |
| Common Smart card API macro. | |
| #define | SMARTCARD_GetDefaultConfig(cardParams) SMARTCARD_UART_GetDefaultConfig(cardParams) |
| Common Smart card API macro. | |
Functions | |
| int | SMARTCARD_RTOS_Init (void *base, rtos_smartcard_context_t *ctx, uint32_t sourceClockHz) |
| Initializes a Smart card (EMVSIM/UART) peripheral for Smart card/ISO-7816 operation. More... | |
| int | SMARTCARD_RTOS_Deinit (rtos_smartcard_context_t *ctx) |
| This function disables the Smart card (EMVSIM/UART) interrupts, disables the transmitter and receiver, and flushes the FIFOs (for modules that support FIFOs) and gates Smart card clock in SIM. More... | |
| int | SMARTCARD_RTOS_Transfer (rtos_smartcard_context_t *ctx, smartcard_xfer_t *xfer) |
| Transfers data using interrupts. More... | |
| int | SMARTCARD_RTOS_AbortTransfer (rtos_smartcard_context_t *ctx) |
| Terminates an asynchronous EMVSIM transfer early. More... | |
| int | SMARTCARD_RTOS_WaitForXevent (rtos_smartcard_context_t *ctx) |
| Waits until the transfer is finished. More... | |
| int | SMARTCARD_RTOS_Control (rtos_smartcard_context_t *ctx, smartcard_control_t control, uint32_t param) |
| Controls the Smart card module per different user requests. More... | |
| int | SMARTCARD_RTOS_PHY_Control (rtos_smartcard_context_t *ctx, smartcard_interface_control_t control, uint32_t param) |
| Controls the Smart card module as per different user request. More... | |
| int | SMARTCARD_RTOS_PHY_Activate (rtos_smartcard_context_t *ctx, smartcard_reset_type_t resetType) |
| Activates the Smart card interface. More... | |
| int | SMARTCARD_RTOS_PHY_Deactivate (rtos_smartcard_context_t *ctx) |
| Deactivates the Smart card interface. More... | |
| struct rtos_smartcard_context_t |
Data Fields | |
| SemaphoreHandle_t | x_sem |
| RTOS unique access assurance object. | |
| SemaphoreHandle_t | x_event |
| RTOS synchronization object. | |
| smartcard_context_t | x_context |
| transactional layer state | |
| #define SMARTCARD_Control | ( | base, | |
| context, | |||
| control, | |||
| param | |||
| ) | SMARTCARD_UART_Control(base, context, control, 0) |
Common Smart card API macro
| int SMARTCARD_RTOS_Init | ( | void * | base, |
| rtos_smartcard_context_t * | ctx, | ||
| uint32_t | sourceClockHz | ||
| ) |
Also initialize Smart card PHY interface.
This function ungates the Smart card clock, initializes the module to EMV default settings, configures the IRQ state structure, and enables the module-level interrupt to the core. Initializes RTOS synchronization objects and context.
| base | The Smart card peripheral base address. |
| ctx | The Smart card RTOS structure. |
| sourceClockHz | Smart card clock generation module source clock. |
| int SMARTCARD_RTOS_Deinit | ( | rtos_smartcard_context_t * | ctx | ) |
It also deactivates Smart card PHY interface, stops Smart card clocks, and frees all synchronization objects allocated in the RTOS Smart card context.
| ctx | The Smart card RTOS state. |
| int SMARTCARD_RTOS_Transfer | ( | rtos_smartcard_context_t * | ctx, |
| smartcard_xfer_t * | xfer | ||
| ) |
A blocking (also known as synchronous) function means that the function returns after the transfer is done. User can cancel this transfer by calling the function AbortTransfer.
| ctx | A pointer to the RTOS Smart card driver context. |
| xfer | Smart card transfer structure. |
| int SMARTCARD_RTOS_AbortTransfer | ( | rtos_smartcard_context_t * | ctx | ) |
During an async EMVSIM transfer, the user can terminate the transfer early if the transfer is still in progress.
| ctx | A pointer to the RTOS Smart card driver context. |
| int SMARTCARD_RTOS_WaitForXevent | ( | rtos_smartcard_context_t * | ctx | ) |
Task waits on a transfer finish event. Don't initialize the transfer. Instead, wait for a transfer callback. This function can be used while waiting on an initial TS character.
| ctx | A pointer to the RTOS Smart card driver context. |
| int SMARTCARD_RTOS_Control | ( | rtos_smartcard_context_t * | ctx, |
| smartcard_control_t | control, | ||
| uint32_t | param | ||
| ) |
| ctx | The Smart card RTOS context pointer. |
| control | Control type. |
| param | Integer value to control the command. |
| int SMARTCARD_RTOS_PHY_Control | ( | rtos_smartcard_context_t * | ctx, |
| smartcard_interface_control_t | control, | ||
| uint32_t | param | ||
| ) |
| ctx | The Smart card RTOS context pointer. |
| control | Control type |
| param | Integer value to control the command. |
| int SMARTCARD_RTOS_PHY_Activate | ( | rtos_smartcard_context_t * | ctx, |
| smartcard_reset_type_t | resetType | ||
| ) |
| ctx | The Smart card RTOS driver context structure. |
| resetType | type of reset to be performed, possible values = kSmartcardColdReset, kSmartcardWarmReset |
| int SMARTCARD_RTOS_PHY_Deactivate | ( | rtos_smartcard_context_t * | ctx | ) |
| ctx | The Smart card RTOS driver context structure. |