MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Power Driver

Overview

Power driver provides APIs to control peripherals power and control the system power mode.

Macros

#define PMUC_PCON_RESERVED_MASK   ((0xf << 4) | (0x6 << 8) | 0xfffff000u)
 PMU PCON reserved mask, used to clear reserved field which should not write 1.
 

Typedefs

typedef enum _power_gen_reg power_gen_reg_t
 pmu general purpose register index
 
typedef enum _power_bod_reset_level power_bod_reset_level_t
 BOD reset level, if VDD below reset level value, the reset will be asserted.
 
typedef enum
_power_bod_interrupt_level 
power_bod_interrupt_level_t
 BOD interrupt level, if VDD below interrupt level value, the BOD interrupt will be asserted.
 

Enumerations

enum  _power_wakeup
 Deep sleep and power down mode wake up configurations.
 
enum  _power_dpd_wakeup_pin
 Deep power down mode wake up pins.
 
enum  _power_deep_sleep_active
 Deep sleep/power down mode active part.
 
enum  _power_gen_reg {
  kPmu_GenReg0 = 0U,
  kPmu_GenReg1 = 1U,
  kPmu_GenReg2 = 2U,
  kPmu_GenReg3 = 3U,
  kPmu_GenReg4 = 4U
}
 pmu general purpose register index More...
 
enum  _power_bod_reset_level { kBod_ResetLevel0 = 0U }
 BOD reset level, if VDD below reset level value, the reset will be asserted. More...
 
enum  _power_bod_interrupt_level {
  kBod_InterruptLevelReserved = 0U,
  kBod_InterruptLevel1,
  kBod_InterruptLevel2,
  kBod_InterruptLevel3
}
 BOD interrupt level, if VDD below interrupt level value, the BOD interrupt will be asserted. More...
 

Driver version

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))
 power driver version 2.1.0. More...
 

SYSCON Power Configuration

static void POWER_EnablePD (pd_bit_t en)
 API to enable PDRUNCFG bit in the Syscon. More...
 
static void POWER_DisablePD (pd_bit_t en)
 API to disable PDRUNCFG bit in the Syscon. More...
 

ARM core Power Configuration

static void POWER_EnableDeepSleep (void)
 API to enable deep sleep bit in the ARM Core. More...
 
static void POWER_DisableDeepSleep (void)
 API to disable deep sleep bit in the ARM Core. More...
 

PMU functionality

void POWER_EnterSleep (void)
 API to enter sleep power mode. More...
 
void POWER_EnterDeepSleep (uint32_t activePart)
 API to enter deep sleep power mode. More...
 
void POWER_EnterPowerDown (uint32_t activePart)
 API to enter power down mode. More...
 
void POWER_EnterDeepPowerDownMode (void)
 API to enter deep power down mode. More...
 
static uint32_t POWER_GetSleepModeFlag (void)
 API to get sleep mode flag. More...
 
static void POWER_ClrSleepModeFlag (void)
 API to clear sleep mode flag.
 
static uint32_t POWER_GetDeepPowerDownModeFlag (void)
 API to get deep power down mode flag. More...
 
static void POWER_ClrDeepPowerDownModeFlag (void)
 API to clear deep power down mode flag.
 
static void POWER_ClrWakeupPinFlag (void)
 API to clear wake up pin status flag.
 
static void POWER_EnableNonDpd (bool enable)
 API to enable non deep power down mode. More...
 
static void POWER_EnableLPO (bool enable)
 API to enable LPO. More...
 
static void POWER_WakeUpConfig (uint32_t mask, bool powerDown)
 API to config wakeup configurations for deep sleep mode and power down mode. More...
 
static void POWER_DeepSleepConfig (uint32_t mask, bool powerDown)
 API to config active part for deep sleep mode and power down mode. More...
 

API to enable wake up pin for deep power down mode

Parameters
wakeup_pinwake up pin for which to enable.reference _power_dpd_wakeup_pin.
Returns
none
static void POWER_DeepPowerDownWakeupSourceSelect (uint32_t wakeup_pin)
 
static void POWER_SetRetainData (power_gen_reg_t index, uint32_t data)
 API to retore data to general purpose register which can be retain during deep power down mode. More...
 
static uint32_t POWER_GetRetainData (power_gen_reg_t index)
 API to get data from general purpose register which retain during deep power down mode. More...
 
static void POWER_SetBodLevel (power_bod_reset_level_t resetLevel, power_bod_interrupt_level_t interruptLevel, bool enable)
 Set Bod interrupt level and reset level. More...
 

Macro Definition Documentation

#define FSL_POWER_DRIVER_VERSION   (MAKE_VERSION(2, 1, 0))

Enumeration Type Documentation

Enumerator
kPmu_GenReg0 

general purpose register0

kPmu_GenReg1 

general purpose register1

kPmu_GenReg2 

general purpose register2

kPmu_GenReg3 

general purpose register3

kPmu_GenReg4 

general purpose reguster4

Enumerator
kBod_ResetLevel0 

BOD Reset Level0: 1.51V.

Enumerator
kBod_InterruptLevelReserved 

BOD interrupt level reserved.

kBod_InterruptLevel1 

BOD interrupt level1: 2.24V.

kBod_InterruptLevel2 

BOD interrupt level2: 2.52V.

kBod_InterruptLevel3 

BOD interrupt level3: 2.81V.

Function Documentation

static void POWER_EnablePD ( pd_bit_t  en)
inlinestatic

Note that enabling the bit powers down the peripheral

Parameters
enperipheral for which to enable the PDRUNCFG bit
Returns
none
static void POWER_DisablePD ( pd_bit_t  en)
inlinestatic

Note that disabling the bit powers up the peripheral

Parameters
enperipheral for which to disable the PDRUNCFG bit
Returns
none
static void POWER_EnableDeepSleep ( void  )
inlinestatic
Returns
none
static void POWER_DisableDeepSleep ( void  )
inlinestatic
Returns
none
void POWER_EnterSleep ( void  )
Returns
none
void POWER_EnterDeepSleep ( uint32_t  activePart)
Parameters
activePart,:should be a single or combine value of _power_deep_sleep_active .
Returns
none
void POWER_EnterPowerDown ( uint32_t  activePart)
Parameters
activePart,:should be a single or combine value of _power_deep_sleep_active .
Returns
none
void POWER_EnterDeepPowerDownMode ( void  )
Returns
none
static uint32_t POWER_GetSleepModeFlag ( void  )
inlinestatic
Returns
sleep mode flag: 0 is active mode, 1 is sleep mode entered.
static uint32_t POWER_GetDeepPowerDownModeFlag ( void  )
inlinestatic
Returns
sleep mode flag: 0 not deep power down, 1 is deep power down mode entered.
static void POWER_EnableNonDpd ( bool  enable)
inlinestatic
Parameters
enable,:true is enable non deep power down, otherwise disable.
static void POWER_EnableLPO ( bool  enable)
inlinestatic
Parameters
enable,:true to enable LPO, false to disable LPO.
static void POWER_WakeUpConfig ( uint32_t  mask,
bool  powerDown 
)
inlinestatic
Parameters
mask,:wake up configurations for deep sleep mode and power down mode, reference _power_wakeup.
powerDown,:true is power down the mask part, false is powered part.
static void POWER_DeepSleepConfig ( uint32_t  mask,
bool  powerDown 
)
inlinestatic
Parameters
mask,:active part configurations for deep sleep mode and power down mode, reference _power_deep_sleep_active.
powerDown,:true is power down the mask part, false is powered part.
static void POWER_SetRetainData ( power_gen_reg_t  index,
uint32_t  data 
)
inlinestatic
Parameters
index,:general purpose data register index.
data,:data to restore.
static uint32_t POWER_GetRetainData ( power_gen_reg_t  index)
inlinestatic
Parameters
index,:general purpose data register index.
Returns
data stored in the general purpose register.
static void POWER_SetBodLevel ( power_bod_reset_level_t  resetLevel,
power_bod_interrupt_level_t  interruptLevel,
bool  enable 
)
inlinestatic
Parameters
resetLevelBOD reset threshold level, please refer to power_bod_reset_level_t.
interruptLevelBOD interrupt threshold level, please refer to power_bod_interrupt_level_t.
enableUsed to enable/disable the BOD interrupt and BOD reset.