![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _dcdc_config |
| Configuration for DCDC. More... | |
| struct | _dcdc_min_power_config |
| Configuration for min power setting. More... | |
| struct | _dcdc_detection_config |
| Configuration for DCDC detection. More... | |
| struct | _dcdc_loop_control_config |
| Configuration for the loop control. More... | |
| struct | _dcdc_internal_regulator_config |
| Configuration for DCDC internal regulator. More... | |
| struct | _dcdc_low_power_config |
| Configuration for DCDC low power. More... | |
| struct | _dcdc_setpoint_config |
| DCDC configuration in set point mode. More... | |
Macros | |
| #define | FSL_DCDC_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
| DCDC driver version. More... | |
| #define | STANDBY_MODE_VDD1P0_TARGET_VOLTAGE |
| The array of VDD1P0 target voltage in standby mode. More... | |
| #define | STANDBY_MODE_VDD1P8_TARGET_VOLTAGE |
| The array of VDD1P8 target voltage in standby mode. More... | |
| #define | BUCK_MODE_VDD1P0_TARGET_VOLTAGE |
| The array of VDD1P0 target voltage in buck mode. More... | |
| #define | BUCK_MODE_VDD1P8_TARGET_VOLTAGE |
| The array of VDD1P8 target voltage in buck mode. More... | |
Typedefs | |
| typedef enum _dcdc_control_mode | dcdc_control_mode_t |
| DCDC control mode, including setpoint control mode and static control mode. | |
| typedef enum _dcdc_trim_input_mode | dcdc_trim_input_mode_t |
| DCDC trim input mode, including sample trim input and hold trim input. | |
|
typedef enum _dcdc_standby_mode_1P0_target_vol | dcdc_standby_mode_1P0_target_vol_t |
| The enumeration VDD1P0's target voltage value in standby mode. | |
|
typedef enum _dcdc_standby_mode_1P8_target_vol | dcdc_standby_mode_1P8_target_vol_t |
| The enumeration VDD1P8's target voltage value in standby mode. | |
|
typedef enum _dcdc_buck_mode_1P0_target_vol | dcdc_buck_mode_1P0_target_vol_t |
| The enumeration VDD1P0's target voltage value in buck mode. | |
|
typedef enum _dcdc_buck_mode_1P8_target_vol | dcdc_buck_mode_1P8_target_vol_t |
| The enumeration VDD1P8's target voltage value in buck mode. | |
|
typedef enum _dcdc_comparator_current_bias | dcdc_comparator_current_bias_t |
| The current bias of low power comparator. | |
|
typedef enum _dcdc_peak_current_threshold | dcdc_peak_current_threshold_t |
| The threshold if peak current detection. | |
| typedef enum _dcdc_clock_source | dcdc_clock_source_t |
| Oscillator clock option. | |
|
typedef enum _dcdc_voltage_output_sel | dcdc_voltage_output_sel_t |
| Voltage output option. | |
| typedef struct _dcdc_config | dcdc_config_t |
| Configuration for DCDC. | |
|
typedef struct _dcdc_min_power_config | dcdc_min_power_config_t |
| Configuration for min power setting. | |
|
typedef struct _dcdc_detection_config | dcdc_detection_config_t |
| Configuration for DCDC detection. | |
|
typedef struct _dcdc_loop_control_config | dcdc_loop_control_config_t |
| Configuration for the loop control. | |
|
typedef struct _dcdc_internal_regulator_config | dcdc_internal_regulator_config_t |
| Configuration for DCDC internal regulator. | |
|
typedef struct _dcdc_low_power_config | dcdc_low_power_config_t |
| Configuration for DCDC low power. | |
|
typedef struct _dcdc_setpoint_config | dcdc_setpoint_config_t |
| DCDC configuration in set point mode. | |
Initialization and De-initialization Interfaces | |
| void | DCDC_Init (DCDC_Type *base, const dcdc_config_t *config) |
| Initializes the basic resource of DCDC module, such as control mode, etc. More... | |
| void | DCDC_Deinit (DCDC_Type *base) |
| De-initializes the DCDC module. More... | |
| void | DCDC_GetDefaultConfig (dcdc_config_t *config) |
| Gets the default setting for DCDC, such as control mode, etc. More... | |
Power Mode Related Interfaces | |
| static void | DCDC_EnterLowPowerModeViaStandbyRequest (DCDC_Type *base, bool enable) |
| Makes the DCDC enter into low power mode for GPC standby request or not. More... | |
| static void | DCDC_EnterLowPowerMode (DCDC_Type *base, bool enable) |
| Makes DCDC enter into low power mode or not, before entering low power mode must disable stepping for VDD1P8 and VDD1P0. More... | |
| static void | DCDC_EnterStandbyMode (DCDC_Type *base, bool enable) |
| Makes DCDC enter into standby mode or not. More... | |
Outputs' Target Voltage Related Interfaces | |
| static void | DCDC_SetVDD1P0StandbyModeTargetVoltage (DCDC_Type *base, dcdc_standby_mode_1P0_target_vol_t targetVoltage) |
| Sets the target value(ranges from 0.625V to 1.4V) of VDD1P0 in standby mode, 25mV each step. More... | |
| static uint16_t | DCDC_GetVDD1P0StandbyModeTargetVoltage (DCDC_Type *base) |
| Gets the target value of VDD1P0 in standby mode, the result takes "mV" as the unit. More... | |
| static void | DCDC_SetVDD1P8StandbyModeTargetVoltage (DCDC_Type *base, dcdc_standby_mode_1P8_target_vol_t targetVoltage) |
| Sets the target value(ranges from 1.525V to 2.3V) of VDD1P8 in standby mode, 25mV each step. More... | |
| static uint16_t | DCDC_GetVDD1P8StandbyModeTargetVoltage (DCDC_Type *base) |
| Gets the target value of VDD1P8 in standby mode, the result takes "mV" as the unit. More... | |
| static void | DCDC_SetVDD1P0BuckModeTargetVoltage (DCDC_Type *base, dcdc_buck_mode_1P0_target_vol_t targetVoltage) |
| Sets the target value(ranges from 0.6V to 1.375V) of VDD1P0 in buck mode, 25mV each step. More... | |
| static uint16_t | DCDC_GetVDD1P0BuckModeTargetVoltage (DCDC_Type *base) |
| Gets the target value of VDD1P0 in buck mode, the result takes "mV" as the unit. More... | |
| static void | DCDC_SetVDD1P8BuckModeTargetVoltage (DCDC_Type *base, dcdc_buck_mode_1P8_target_vol_t targetVoltage) |
| Sets the target value(ranges from 1.5V to 2.275V) of VDD1P8 in buck mode, 25mV each step. More... | |
| static uint16_t | DCDC_GetVDD1P8BuckModeTargetVoltage (DCDC_Type *base) |
| Gets the target value of VDD1P8 in buck mode, the result takes "mV" as the unit. More... | |
| static void | DCDC_EnableVDD1P0TargetVoltageStepping (DCDC_Type *base, bool enable) |
| Enables/Disables stepping for VDD1P0, before entering low power modes the stepping for VDD1P0 must be disabled. More... | |
| static void | DCDC_EnableVDD1P8TargetVoltageStepping (DCDC_Type *base, bool enable) |
| Enables/Disables stepping for VDD1P8, before entering low power modes the stepping for VDD1P8 must be disabled. More... | |
Detection Related Inferfaces | |
| void | DCDC_GetDefaultDetectionConfig (dcdc_detection_config_t *config) |
| Gets the default setting for detection configuration. More... | |
| void | DCDC_SetDetectionConfig (DCDC_Type *base, const dcdc_detection_config_t *config) |
| Configures the DCDC detection. More... | |
DCDC Miscellaneous Inferfaces | |
| static void | DCDC_EnableOutputRangeComparator (DCDC_Type *base, bool enable) |
| Enables/Disables the output range comparator. More... | |
| void | DCDC_SetClockSource (DCDC_Type *base, dcdc_clock_source_t clockSource) |
| Configures the DCDC clock source. More... | |
| void | DCDC_GetDefaultLowPowerConfig (dcdc_low_power_config_t *config) |
| Gets the default setting for low power configuration. More... | |
| void | DCDC_SetLowPowerConfig (DCDC_Type *base, const dcdc_low_power_config_t *config) |
| Configures the DCDC low power. More... | |
| static void | DCDC_SetBandgapVoltageTrimValue (DCDC_Type *base, uint32_t trimValue) |
| Sets the bangap trim value(0~31) to trim bandgap voltage. More... | |
| void | DCDC_GetDefaultLoopControlConfig (dcdc_loop_control_config_t *config) |
| Gets the default setting for loop control configuration. More... | |
| void | DCDC_SetLoopControlConfig (DCDC_Type *base, const dcdc_loop_control_config_t *config) |
| Configures the DCDC loop control. More... | |
| void | DCDC_SetMinPowerConfig (DCDC_Type *base, const dcdc_min_power_config_t *config) |
| Configures for the min power. More... | |
| static void | DCDC_SetLPComparatorBiasValue (DCDC_Type *base, dcdc_comparator_current_bias_t biasValue) |
| Sets the current bias of low power comparator. More... | |
| void | DCDC_SetInternalRegulatorConfig (DCDC_Type *base, const dcdc_internal_regulator_config_t *config) |
| Configures the DCDC internal regulator. More... | |
| static void | DCDC_EnableAdjustDelay (DCDC_Type *base, bool enable) |
| Adjusts delay to reduce ground noise. More... | |
| static void | DCDC_EnableImproveTransition (DCDC_Type *base, bool enable) |
| Enables/Disables to improve the transition from heavy load to light load. More... | |
Setpoint Control Related Interfaces | |
| void | DCDC_SetPointInit (DCDC_Type *base, const dcdc_setpoint_config_t *config) |
| Initializes DCDC module when the control mode selected as setpoint mode. More... | |
| static void | DCDC_SetPointDeinit (DCDC_Type *base, uint32_t setpointMap) |
| Disable DCDC module when the control mode selected as setpoint mode. More... | |
DCDC Status Related Interfaces | |
| static uint32_t | DCDC_GetStatusFlags (DCDC_Type *base) |
| Get DCDC status flags. More... | |
Application Guideline Interfaces | |
| void | DCDC_BootIntoDCM (DCDC_Type *base) |
| Boots DCDC into DCM(discontinous conduction mode). More... | |
| void | DCDC_BootIntoCCM (DCDC_Type *base) |
| Boots DCDC into CCM(continous conduction mode). More... | |
| struct _dcdc_config |
Data Fields | |
| dcdc_control_mode_t | controlMode |
| DCDC control mode. More... | |
| dcdc_trim_input_mode_t | trimInputMode |
| Hold trim input. More... | |
| bool | enableDcdcTimeout |
| Enable internal count for DCDC_OK timeout. More... | |
| bool | enableSwitchingConverterOutput |
| Enable the VDDIO switching converter output. More... | |
| dcdc_control_mode_t _dcdc_config::controlMode |
| dcdc_trim_input_mode_t _dcdc_config::trimInputMode |
| bool _dcdc_config::enableDcdcTimeout |
| bool _dcdc_config::enableSwitchingConverterOutput |
| struct _dcdc_min_power_config |
Data Fields | |
| bool | enableUseHalfFreqForContinuous |
| Set DCDC clock to half frequency for the continuous mode. More... | |
| bool | enableUseHalfFetForContinuous |
| Use half switch FET for the continuous mode. More... | |
| bool | enableUseDoubleFetForContinuous |
| Use double switch FET for the continuous mode. More... | |
| bool | enableUseHalfFetForPulsed |
| Use half switch FET for the Pulsed mode. More... | |
| bool | enableUseDoubleFetForPulsed |
| Use double switch FET for the Pulsed mode. More... | |
| bool | enableUseHalfFreqForPulsed |
| Set DCDC clock to half frequency for the Pulsed mode. More... | |
| bool _dcdc_min_power_config::enableUseHalfFreqForContinuous |
| bool _dcdc_min_power_config::enableUseHalfFetForContinuous |
| bool _dcdc_min_power_config::enableUseDoubleFetForContinuous |
| bool _dcdc_min_power_config::enableUseHalfFetForPulsed |
| bool _dcdc_min_power_config::enableUseDoubleFetForPulsed |
| bool _dcdc_min_power_config::enableUseHalfFreqForPulsed |
| struct _dcdc_detection_config |
Data Fields | |
| bool | enableXtalokDetection |
| Enable xtalok detection circuit. More... | |
| bool | powerDownOverVoltageVdd1P8Detection |
| Power down over-voltage detection comparator for VDD1P8. More... | |
| bool | powerDownOverVoltageVdd1P0Detection |
| Power down over-voltage detection comparator for VDD1P0. More... | |
| bool | powerDownLowVoltageDetection |
| Power down low-voltage detection comparator. More... | |
| bool | powerDownOverCurrentDetection |
| Power down over-current detection. More... | |
| bool | powerDownPeakCurrentDetection |
| Power down peak-current detection. More... | |
| bool | powerDownZeroCrossDetection |
| Power down the zero cross detection function for discontinuous conductor mode. More... | |
| dcdc_peak_current_threshold_t | PeakCurrentThreshold |
| The threshold of peak current detection. More... | |
| bool _dcdc_detection_config::enableXtalokDetection |
| bool _dcdc_detection_config::powerDownOverVoltageVdd1P8Detection |
| bool _dcdc_detection_config::powerDownOverVoltageVdd1P0Detection |
| bool _dcdc_detection_config::powerDownLowVoltageDetection |
| bool _dcdc_detection_config::powerDownOverCurrentDetection |
| bool _dcdc_detection_config::powerDownPeakCurrentDetection |
| bool _dcdc_detection_config::powerDownZeroCrossDetection |
| dcdc_peak_current_threshold_t _dcdc_detection_config::PeakCurrentThreshold |
| struct _dcdc_loop_control_config |
Data Fields | |
| bool | enableCommonHysteresis |
| Enable hysteresis in switching converter common mode analog comparators. More... | |
| bool | enableCommonThresholdDetection |
| Increase the threshold detection for common mode analog comparator. More... | |
| bool | enableDifferentialHysteresis |
| Enable hysteresis in switching converter differential mode analog comparators. More... | |
| bool | enableDifferentialThresholdDetection |
| Increase the threshold detection for differential mode analog comparators. More... | |
| bool | enableInvertHysteresisSign |
| Invert the sign of the hysteresis in DC-DC analog comparators. More... | |
| bool | enableRCThresholdDetection |
| Increase the threshold detection for RC scale circuit. More... | |
| uint32_t | enableRCScaleCircuit |
| Available range is 0~7. More... | |
| uint32_t | complementFeedForwardStep |
| Available range is 0~7. More... | |
| uint32_t | controlParameterMagnitude |
| Available range is 0~15. More... | |
| uint32_t | integralProportionalRatio |
| Available range is 0~3.Ratio of integral control parameter to proportional control parameter in the switching DC-DC converter, and can be used to optimize efficiency and loop response. More... | |
| bool | enableDiffHysteresis |
| Enable hysteresis in switching converter differential mode analog comparators. More... | |
| bool | enableDiffHysteresisThresh |
| This field act the same rule as enableDiffHysteresis. More... | |
| bool | enableCommonHysteresisThresh |
| This field act the same rule as enableCommonHysteresis. More... | |
| bool _dcdc_loop_control_config::enableCommonHysteresis |
This feature will improve transient supply ripple and efficiency.
This feature improves transient supply ripple and efficiency.
| bool _dcdc_loop_control_config::enableCommonThresholdDetection |
| bool _dcdc_loop_control_config::enableDifferentialHysteresis |
This feature will improve transient supply ripple and efficiency.
| bool _dcdc_loop_control_config::enableDifferentialThresholdDetection |
| bool _dcdc_loop_control_config::enableInvertHysteresisSign |
| bool _dcdc_loop_control_config::enableRCThresholdDetection |
| uint32_t _dcdc_loop_control_config::enableRCScaleCircuit |
Enable analog circuit of DC-DC converter to respond faster under transient load conditions.
| uint32_t _dcdc_loop_control_config::complementFeedForwardStep |
Two's complement feed forward step in duty cycle in the switching DC-DC converter. Each time this field makes a transition from 0x0, the loop filter of the DC-DC converter is stepped once by a value proportional to the change. This can be used to force a certain control loop behavior, such as improving response under known heavy load transients.
| uint32_t _dcdc_loop_control_config::controlParameterMagnitude |
Magnitude of proportional control parameter in the switching DC-DC converter control loop.
| uint32_t _dcdc_loop_control_config::integralProportionalRatio |
| bool _dcdc_loop_control_config::enableDiffHysteresis |
This feature improves transient supply ripple and efficiency.
| bool _dcdc_loop_control_config::enableDiffHysteresisThresh |
However, if this field is enabled along with the enableDiffHysteresis, the Hysteresis wuold be doubled.
| bool _dcdc_loop_control_config::enableCommonHysteresisThresh |
However, if this field is enabled along with the enableCommonHysteresis, the Hysteresis wuold be doubled.
| struct _dcdc_internal_regulator_config |
Data Fields | |
| uint32_t | feedbackPoint |
| Available range is 0~3. More... | |
| uint32_t _dcdc_internal_regulator_config::feedbackPoint |
Select the feedback point of the internal regulator.
| struct _dcdc_low_power_config |
Configuration for the low power.
Data Fields | |
| bool | enableAdjustHystereticValue |
| Adjust hysteretic value in low power from 12.5mV to 25mV. More... | |
| dcdc_work_mode_t | workModeInVLPRW |
| Select the behavior of DCDC in device VLPR and VLPW low power modes. More... | |
| dcdc_work_mode_t | workModeInVLPS |
| Select the behavior of DCDC in device VLPS low power modes. More... | |
| bool | enableHysteresisVoltageSense |
| Enable hysteresis in low power voltage sense. More... | |
| bool | enableAdjustHystereticValueSense |
| Adjust hysteretic value in low power voltage sense. More... | |
| bool | enableHystersisComparator |
| Enable hysteresis in low power comparator. More... | |
| bool | enableAdjustHystereticValueComparator |
| Adjust hysteretic value in low power comparator. More... | |
| dcdc_hysteretic_threshold_offset_value_t | hystereticUpperThresholdValue |
| Configure the hysteretic upper threshold value in low power mode. More... | |
| dcdc_hysteretic_threshold_offset_value_t | hystereticLowerThresholdValue |
| Configure the hysteretic lower threshold value in low power mode. More... | |
| bool | enableDiffComparators |
| Enable low power differential comparators, to sense lower supply in pulsed mode. More... | |
| bool _dcdc_low_power_config::enableAdjustHystereticValue |
| dcdc_work_mode_t _dcdc_low_power_config::workModeInVLPRW |
| dcdc_work_mode_t _dcdc_low_power_config::workModeInVLPS |
| bool _dcdc_low_power_config::enableHysteresisVoltageSense |
| bool _dcdc_low_power_config::enableAdjustHystereticValueSense |
| bool _dcdc_low_power_config::enableHystersisComparator |
| bool _dcdc_low_power_config::enableAdjustHystereticValueComparator |
| dcdc_hysteretic_threshold_offset_value_t _dcdc_low_power_config::hystereticUpperThresholdValue |
| dcdc_hysteretic_threshold_offset_value_t _dcdc_low_power_config::hystereticLowerThresholdValue |
| bool _dcdc_low_power_config::enableDiffComparators |
| struct _dcdc_setpoint_config |
Data Fields | |
| uint32_t | enableDCDCMap |
| The setpoint map that enable the DCDC module. More... | |
| uint32_t | enableDigLogicMap |
| The setpoint map that enable the DCDC dig logic. More... | |
| uint32_t | lowpowerMap |
| The setpoint map that enable the DCDC Low powermode. More... | |
| uint32_t | standbyMap |
| The setpoint map that enable the DCDC standby mode. More... | |
| uint32_t | standbyLowpowerMap |
| The setpoint map that enable the DCDC low power mode, when the related setpoint is in standby mode. More... | |
| dcdc_buck_mode_1P8_target_vol_t * | buckVDD1P8TargetVoltage |
| Point to the array that store the target voltage level of VDD1P8 in buck mode, please refer to dcdc_buck_mode_1P8_target_vol_t. More... | |
| dcdc_buck_mode_1P0_target_vol_t * | buckVDD1P0TargetVoltage |
| Point to the array that store the target voltage level of VDD1P0 in buck mode, please refer to dcdc_buck_mode_1P0_target_vol_t. More... | |
| dcdc_standby_mode_1P8_target_vol_t * | standbyVDD1P8TargetVoltage |
Point to the array that store the target voltage level of VDD1P8 in standby mode, please refer to dcdc_standby_mode_1P8_target_vol_t. More... | |
| dcdc_standby_mode_1P0_target_vol_t * | standbyVDD1P0TargetVoltage |
Point to the array that store the target voltage level of VDD1P0 in standby mode, please refer to dcdc_standby_mode_1P0_target_vol_t. More... | |
| uint32_t _dcdc_setpoint_config::enableDCDCMap |
Should be the OR'ed value of _dcdc_setpoint_map.
| uint32_t _dcdc_setpoint_config::enableDigLogicMap |
Should be the OR'ed value of _dcdc_setpoint_map.
| uint32_t _dcdc_setpoint_config::lowpowerMap |
Should be the OR'ed value of _dcdc_setpoint_map.
| uint32_t _dcdc_setpoint_config::standbyMap |
Should be the OR'ed value of _dcdc_setpoint_map.
| uint32_t _dcdc_setpoint_config::standbyLowpowerMap |
Please refer to _dcdc_setpoint_map.
| dcdc_buck_mode_1P8_target_vol_t* _dcdc_setpoint_config::buckVDD1P8TargetVoltage |
Note that the pointed array must have 16 elements.
| dcdc_buck_mode_1P0_target_vol_t* _dcdc_setpoint_config::buckVDD1P0TargetVoltage |
Note that the pointed array must have 16 elements.
| dcdc_standby_mode_1P8_target_vol_t* _dcdc_setpoint_config::standbyVDD1P8TargetVoltage |
Note that the pointed array must have 16 elements.
| dcdc_standby_mode_1P0_target_vol_t* _dcdc_setpoint_config::standbyVDD1P0TargetVoltage |
Note that the pointed array must have 16 elements.
| #define FSL_DCDC_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
Version 2.1.2.
| #define STANDBY_MODE_VDD1P0_TARGET_VOLTAGE |
| #define STANDBY_MODE_VDD1P8_TARGET_VOLTAGE |
| #define BUCK_MODE_VDD1P0_TARGET_VOLTAGE |
| #define BUCK_MODE_VDD1P8_TARGET_VOLTAGE |
| enum _dcdc_status_flags |
| enum _dcdc_setpoint_map |
| enum _dcdc_control_mode |
| enum _dcdc_clock_source |
| void DCDC_Init | ( | DCDC_Type * | base, |
| const dcdc_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to the dcdc_config_t structure. |
| void DCDC_Deinit | ( | DCDC_Type * | base | ) |
| base | DCDC peripheral base address. |
| void DCDC_GetDefaultConfig | ( | dcdc_config_t * | config | ) |
This function initializes the user configuration structure to a default value. The default values are:
| config | Pointer to configuration structure. See to dcdc_config_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Used to control the behavior.
|
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Used to control the behavior.
|
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Used to control the behavior.
|
|
inlinestatic |
| base | DCDC peripheral base address. |
| targetVoltage | The target value of VDD1P0 in standby mode, see dcdc_standby_mode_1P0_target_vol_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| targetVoltage | The target value of VDD1P8 in standby mode, see dcdc_standby_mode_1P8_target_vol_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| targetVoltage | The target value of VDD1P0 in buck mode, see dcdc_buck_mode_1P0_target_vol_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| targetVoltage | The target value of VDD1P8 in buck mode, see dcdc_buck_mode_1P8_target_vol_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Used to control the behavior.
|
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Used to control the behavior.
|
| void DCDC_GetDefaultDetectionConfig | ( | dcdc_detection_config_t * | config | ) |
The default configuration are set according to responding registers' setting when powered on. They are:
| config | Pointer to configuration structure. See to dcdc_detection_config_t. |
| void DCDC_SetDetectionConfig | ( | DCDC_Type * | base, |
| const dcdc_detection_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to configuration structure. See to dcdc_detection_config_t. |
|
inlinestatic |
The output range comparator is disabled by default.
| base | DCDC peripheral base address. |
| enable | Enable the feature or not.
|
| void DCDC_SetClockSource | ( | DCDC_Type * | base, |
| dcdc_clock_source_t | clockSource | ||
| ) |
| base | DCDC peripheral base address. |
| clockSource | Clock source for DCDC. See to dcdc_clock_source_t. |
| void DCDC_GetDefaultLowPowerConfig | ( | dcdc_low_power_config_t * | config | ) |
The default configuration are set according to responding registers' setting when powered on. They are:
| config | Pointer to configuration structure. See to dcdc_low_power_config_t. |
| void DCDC_SetLowPowerConfig | ( | DCDC_Type * | base, |
| const dcdc_low_power_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to configuration structure. See to dcdc_low_power_config_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| trimValue | The bangap trim value. Available range is 0U-31U. |
| void DCDC_GetDefaultLoopControlConfig | ( | dcdc_loop_control_config_t * | config | ) |
The default configuration are set according to responding registers' setting when powered on. They are:
| config | Pointer to configuration structure. See to dcdc_loop_control_config_t. |
| void DCDC_SetLoopControlConfig | ( | DCDC_Type * | base, |
| const dcdc_loop_control_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to configuration structure. See to dcdc_loop_control_config_t. |
| void DCDC_SetMinPowerConfig | ( | DCDC_Type * | base, |
| const dcdc_min_power_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to configuration structure. See to dcdc_min_power_config_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| biasValue | The current bias of low power comparator. Refer to dcdc_comparator_current_bias_t. |
| void DCDC_SetInternalRegulatorConfig | ( | DCDC_Type * | base, |
| const dcdc_internal_regulator_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | Pointer to configuration structure. See to dcdc_internal_regulator_config_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Enable the feature or not. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| enable | Enable the feature or not. |
| void DCDC_SetPointInit | ( | DCDC_Type * | base, |
| const dcdc_setpoint_config_t * | config | ||
| ) |
| base | DCDC peripheral base address. |
| config | The pointer to the structure dcdc_setpoint_config_t. |
|
inlinestatic |
| base | DCDC peripheral base address. |
| setpointMap | The map of the setpoint to disable the DCDC module, Should be the OR'ed value of _dcdc_setpoint_map. |
|
inlinestatic |
| base | peripheral base address. |
| void DCDC_BootIntoDCM | ( | DCDC_Type * | base | ) |
| base | DCDC peripheral base address. |
| void DCDC_BootIntoCCM | ( | DCDC_Type * | base | ) |
| base | DCDC peripheral base address. |