![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | _src_setpoint_authentication |
| The structure of setpoint authentication. More... | |
| struct | _src_domain_mode_authentication |
| The stucture of domain mode authentication. More... | |
Typedefs | |
| typedef enum _src_core_name | src_core_name_t |
| System core. | |
|
typedef enum _src_boot_fuse_selection | src_boot_fuse_selection_t |
| The enumeration of the boot fuse selection. | |
|
typedef enum _src_global_system_reset_source | src_global_system_reset_source_t |
| The enumeration of global system reset sources. | |
|
typedef enum _src_global_system_reset_mode | src_global_system_reset_mode_t |
| The enumeration of global system reset mode. | |
| typedef enum _src_reset_slice_name | src_reset_slice_name_t |
| The enumeration of the slice name. | |
|
typedef enum _src_general_purpose_register_index | src_general_purpose_register_index_t |
| The index of each general purpose register. | |
|
typedef struct _src_setpoint_authentication | src_setpoint_authentication_t |
| The structure of setpoint authentication. | |
|
typedef struct _src_domain_mode_authentication | src_domain_mode_authentication_t |
| The stucture of domain mode authentication. | |
| typedef enum _src_slice_reset_state | src_slice_reset_state_t |
| The enumeration of the reset state of each slice. | |
Driver version | |
| #define | FSL_SRC_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| SRC driver version 2.1.1. More... | |
Core Reset release | |
| void | SRC_ReleaseCoreReset (SRC_Type *base, src_core_name_t coreName) |
| Releases related core reset operation. More... | |
Latched Boot Arguments Related Interfaces | |
| static uint32_t | SRC_GetBootConfig (SRC_Type *base) |
| Gets Boot configuration. More... | |
| static uint8_t | SRC_GetBootMode (SRC_Type *base) |
| Gets the latched state of the BOOT_MODE1 and BOOT_MODE0 signals. More... | |
| static src_boot_fuse_selection_t | SRC_GetBootFuseSelection (SRC_Type *base) |
| Gets the state of the BT_FUSE_SEL fuse. More... | |
| static uint8_t | SRC_GetSECConfigFuseState (SRC_Type *base) |
| Gets the state of the SECCONFIG[1] fuse. More... | |
Global System Related Interfaces | |
| void | SRC_SetGlobalSystemResetMode (SRC_Type *base, src_global_system_reset_source_t resetSource, src_global_system_reset_mode_t resetMode) |
| Sets the reset mode of global system reset source. More... | |
| static uint32_t | SRC_GetResetStatusFlags (SRC_Type *base) |
| Gets global system reset status flags. More... | |
| static void | SRC_ClearGlobalSystemResetStatus (SRC_Type *base, uint32_t mask) |
| Clears the status of global reset. More... | |
Slice Software Reset Related Interfaces | |
| void | SRC_AssertSliceSoftwareReset (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Asserts software reset for the selected slice. More... | |
Slice Low-Power Mode Transition Related Interfaces | |
| static void | SRC_AllowUserModeAccess (SRC_Type *base, src_reset_slice_name_t sliceName, bool enable) |
| Allows/disallows user mode access. More... | |
| static void | SRC_AllowNonSecureModeAccess (SRC_Type *base, src_reset_slice_name_t sliceName, bool enable) |
| Allows/disallows non secure mode access. More... | |
| static void | SRC_LockAccessSetting (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Locks the setting of user mode access and non secure mode access. More... | |
| static void | SRC_SetDomainIdWhiteList (SRC_Type *base, src_reset_slice_name_t sliceName, uint8_t domainId) |
| Sets the domain ID white list for the selected slice. More... | |
| static void | SRC_LockDomainIdWhiteList (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Locks the value of white list. More... | |
| static void | SRC_SetAssignList (SRC_Type *base, src_reset_slice_name_t sliceName, uint32_t assignList) |
| Sets the value of assign list. More... | |
| static void | SRC_LockAssignList (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Locks the value of assign list. More... | |
| static void | SRC_EnableSetPointTransferReset (SRC_Type *base, src_reset_slice_name_t sliceName, bool enable) |
| Enable/disable setpoint transfer reset. More... | |
| static void | SRC_EnableDomainModeTransferReset (SRC_Type *base, src_reset_slice_name_t sliceName, bool enable) |
| Enable/disable domain mode transfer reset. More... | |
| void | SRC_SetSliceSetPointConfig (SRC_Type *base, src_reset_slice_name_t sliceName, uint32_t setpointConfig) |
| Sets setpoint configuration for the selected reset slice. More... | |
| void | SRC_SetSliceDomainModeConfig (SRC_Type *base, src_reset_slice_name_t sliceName, uint32_t domainConfig) |
| Sets domain mode configuration for the selected reset slice. More... | |
| void | SRC_LockSliceMode (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Locks the value of SETPOINT_MODE and DOMAIN_MODE for the selected reset slice. More... | |
Get/Clear Slice Reset Status Flags | |
| static uint32_t | SRC_GetSliceResetStatusFlags (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Gets the reset status flags of the selected slice. More... | |
| static void | SRC_ClearSliceResetStatusFlags (SRC_Type *base, src_reset_slice_name_t sliceName, uint32_t mask) |
| Clears the reset status flags of the selected slice. More... | |
Get Slice Reset State | |
| src_slice_reset_state_t | SRC_GetSliceResetState (SRC_Type *base, src_reset_slice_name_t sliceName) |
| Gets the reset state of the selected slice. More... | |
General Purpose Registers Related Interfaces | |
| static void | SRC_SetGeneralPurposeRegister (SRC_Type *base, src_general_purpose_register_index_t index, uint32_t value) |
| Sets value to general purpose registers. More... | |
| static uint32_t | SRC_GetGeneralPurposeRegister (SRC_Type *base, src_general_purpose_register_index_t index) |
| Gets the value from general purpose registers. More... | |
| struct _src_setpoint_authentication |
Data Fields | |
| bool | enableSetpointTranferReset |
| Control whether reset slice is in setpoint mode. More... | |
| uint32_t | whiteList |
| Select the core to access set point control register. More... | |
| bool | lockWhiteList |
| Control whether lock the value in white list. | |
| bool | lockSetting |
| Control whether lock the setpoint access setting. More... | |
| bool | allowNonSecureModeAccess |
| Allow both secure and non-secure modes to config setpoint. More... | |
| bool | allowUserModeAccess |
| Allow both privilege and user modes to config setpoint. More... | |
| bool _src_setpoint_authentication::enableSetpointTranferReset |
| uint32_t _src_setpoint_authentication::whiteList |
The logic OR'ed value of src_core_name_t enumeration.
| bool _src_setpoint_authentication::lockSetting |
| bool _src_setpoint_authentication::allowNonSecureModeAccess |
| bool _src_setpoint_authentication::allowUserModeAccess |
| struct _src_domain_mode_authentication |
Data Fields | |
| bool | enableDomainModeTransferReset |
| Control whether reset slice is in domaim mode. More... | |
| uint32_t | assignList |
| Select the core that reset of slice would be subject to the selected core status transition. More... | |
| bool | lockAssignList |
| Control whether lock the value in Assign list. More... | |
| bool _src_domain_mode_authentication::enableDomainModeTransferReset |
| uint32_t _src_domain_mode_authentication::assignList |
The logic OR'ed value of src_core_name_t enumeration.
| bool _src_domain_mode_authentication::lockAssignList |
| #define FSL_SRC_DRIVER_VERSION (MAKE_VERSION(2, 1, 1)) |
| enum _src_core_name |
| void SRC_ReleaseCoreReset | ( | SRC_Type * | base, |
| src_core_name_t | coreName | ||
| ) |
The core reset will be held until the boot core to release it.
| base | SRC peripheral base address. |
| coreName | The name of the reset core to be released. |
|
inlinestatic |
| base | SRC peripheral base address. |
|
inlinestatic |
| base | SRC peripheral base address. |
|
inlinestatic |
| base | SRC peripheral base address. |
|
inlinestatic |
| base | SRC peripheral base address. |
| void SRC_SetGlobalSystemResetMode | ( | SRC_Type * | base, |
| src_global_system_reset_source_t | resetSource, | ||
| src_global_system_reset_mode_t | resetMode | ||
| ) |
This function sets the selected mode of the input global system reset sources.
| base | SRC peripheral base address. |
| resetSource | The global system reset source. See src_global_system_reset_source_t for more details. |
| resetMode | The reset mode of each reset source. See src_global_system_reset_mode_t for more details. |
|
inlinestatic |
| base | SRC peripheral base address. |
|
inlinestatic |
| base | SRC peripheral base address. |
| mask | The reset status flag to be cleared. See _src_global_system_reset_status_flags for more details. |
| void SRC_AssertSliceSoftwareReset | ( | SRC_Type * | base, |
| src_reset_slice_name_t | sliceName | ||
| ) |
| base | SRC peripheral base address. |
| sliceName | The slice to be reset. See src_reset_slice_name_t for more details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| enable | Used to control user mode access.
|
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| enable | Used to control non secure mode access.
|
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| domainId | The core to access registers, should be the OR'ed value of src_core_name_t. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| assignList | Cores that subject to corresponding core status transition, should be the OR'ed value of src_core_name_t. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| enable | User to control setpoint transfer reset.
|
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice name to set, please refer to src_reset_slice_name_t for details. |
| enable | User to control domain mode reset.
|
| void SRC_SetSliceSetPointConfig | ( | SRC_Type * | base, |
| src_reset_slice_name_t | sliceName, | ||
| uint32_t | setpointConfig | ||
| ) |
| base | SRC peripheral base address. |
| sliceName | The selected reset slice. See src_reset_slice_name_t for more details. |
| setpointConfig | The logic OR'ed value of _src_setpoint_selection enumeration, when the system in the selected setpoint slice reset will be asserted. |
| void SRC_SetSliceDomainModeConfig | ( | SRC_Type * | base, |
| src_reset_slice_name_t | sliceName, | ||
| uint32_t | domainConfig | ||
| ) |
| base | SRC peripheral base address. |
| sliceName | The selected reset slice. See src_reset_slice_name_t for more details. |
| domainConfig | The logic OR'ed value of _src_domain_mode_selection enumerations. |
| void SRC_LockSliceMode | ( | SRC_Type * | base, |
| src_reset_slice_name_t | sliceName | ||
| ) |
| base | SRC peripheral base address. |
| sliceName | The selected reset slice. See src_reset_slice_name_t for more details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The slice to be reset. See src_reset_slice_name_t for more details. |
|
inlinestatic |
| base | SRC peripheral base address. |
| sliceName | The selected slice. See src_reset_slice_name_t for more details. |
| mask | The reset status flags to be cleared. Please refer to _src_slice_reset_source for more details. |
| src_slice_reset_state_t SRC_GetSliceResetState | ( | SRC_Type * | base, |
| src_reset_slice_name_t | sliceName | ||
| ) |
| base | SRC peripheral base address. |
| sliceName | The selected slice. See src_reset_slice_name_t for more details. |
| kSRC_SliceResetInProcess | The reset is in process. |
| kSRC_SliceResetFinished | The reset is finished. |
|
inlinestatic |
| base | SRC peripheral base address. |
| index | The index of GPRx register array. Please refer to src_general_purpose_register_index_t. |
| value | Setting value for GPRx register. |
|
inlinestatic |
| base | SRC peripheral base address. |
| index | The index of GPRx register array. Please refer to src_general_purpose_register_index_t. |