![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
The clock driver supports:
Files | |
| file | fsl_clock.h |
Data Structures | |
| struct | _pll_config |
| PLL configuration structure. More... | |
| struct | _pll_setup |
| PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More... | |
Macros | |
| #define | CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT 2U |
| User-defined the size of cache for CLOCK_PllGetConfig() function. More... | |
| #define | FLEXCOMM_CLOCKS |
| Clock ip name array for FLEXCOMM. More... | |
| #define | LPUART_CLOCKS |
| Clock ip name array for LPUART. More... | |
| #define | BI2C_CLOCKS |
| Clock ip name array for BI2C. More... | |
| #define | LPSI_CLOCKS |
| Clock ip name array for LSPI. More... | |
| #define | FLEXI2S_CLOCKS |
| Clock ip name array for FLEXI2S. More... | |
| #define | UTICK_CLOCKS |
| Clock ip name array for UTICK. More... | |
| #define | DMA_CLOCKS |
| Clock ip name array for DMA. More... | |
| #define | CTIMER_CLOCKS |
| Clock ip name array for CT32B. More... | |
| #define | GPIO_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | ADC_CLOCKS |
| Clock ip name array for ADC. More... | |
| #define | MRT_CLOCKS |
| Clock ip name array for MRT. More... | |
| #define | SCT_CLOCKS |
| Clock ip name array for MRT. More... | |
| #define | RTC_CLOCKS |
| Clock ip name array for RTC. More... | |
| #define | WWDT_CLOCKS |
| Clock ip name array for WWDT. More... | |
| #define | CRC_CLOCKS |
| Clock ip name array for CRC. More... | |
| #define | USBD_CLOCKS |
| Clock ip name array for USBD. More... | |
| #define | GINT_CLOCKS |
| Clock ip name array for GINT. More... | |
| #define | CLK_GATE_REG_OFFSET_SHIFT 8U |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| #define | CLK_ATTACH_ID(mux, sel, pos) ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U)) |
| Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More... | |
| #define | PLL_CONFIGFLAG_USEINRATE (1U << 0U) |
| PLL configuration structure flags for 'flags' field These flags control how the PLL configuration function sets up the PLL setup structure. More... | |
| #define | PLL_CONFIGFLAG_FORCENOFRACT (1U << 2U) |
| Force non-fractional output mode, PLL output will not use the fractional, automatic bandwidth, or \ SS hardware. | |
| #define | PLL_SETUPFLAG_POWERUP (1U << 0U) |
| PLL setup structure flags for 'flags' field These flags control how the PLL setup function sets up the PLL. More... | |
| #define | PLL_SETUPFLAG_WAITLOCK (1U << 1U) |
| Setup will wait for PLL lock, implies the PLL will be pwoered on. | |
| #define | PLL_SETUPFLAG_ADGVOLT (1U << 2U) |
| Optimize system voltage for the new PLL rate. | |
| #define | PLL_SETUPFLAG_USEFEEDBACKDIV2 (1U << 3U) |
| Use feedback divider by 2 in divider path. | |
Typedefs | |
| typedef enum _clock_ip_name | clock_ip_name_t |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| typedef enum _clock_name | clock_name_t |
| Clock name used to get clock frequency. More... | |
| typedef enum _async_clock_src | async_clock_src_t |
| Clock source selections for the asynchronous APB clock. | |
| typedef enum _clock_attach_id | clock_attach_id_t |
| The enumerator of clock attach Id. | |
| typedef enum _clock_div_name | clock_div_name_t |
| Clock dividers. More... | |
| typedef enum _clock_flashtim | clock_flashtim_t |
| FLASH Access time definitions. | |
| typedef enum _ss_progmodfm | ss_progmodfm_t |
| PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the SYSPLLSSCTRL1 register in the UM. | |
| typedef enum _ss_progmoddp | ss_progmoddp_t |
| PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the SYSPLLSSCTRL1 register in the UM. | |
| typedef enum _ss_modwvctrl | ss_modwvctrl_t |
| PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the SYSPLLSSCTRL1 register in the UM. More... | |
| typedef struct _pll_config | pll_config_t |
| PLL configuration structure. More... | |
| typedef struct _pll_setup | pll_setup_t |
| PLL setup structure This structure can be used to pre-build a PLL setup configuration at run-time and quickly set the PLL to the configuration. More... | |
| typedef enum _pll_error | pll_error_t |
| PLL status definitions. | |
| typedef enum _clock_usb_src | clock_usb_src_t |
| USB clock source definition. More... | |
Enumerations | |
| enum | _clock_ip_name { kCLOCK_IpInvalid = 0U, kCLOCK_Rom = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 1), kCLOCK_Flash = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 7), kCLOCK_Fmc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 8), kCLOCK_InputMux = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 11), kCLOCK_Iocon = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 13), kCLOCK_Gpio0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 14), kCLOCK_Gpio1 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 15), kCLOCK_Pint = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 18), kCLOCK_Gint = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 19), kCLOCK_Dma = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 20), kCLOCK_Crc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 21), kCLOCK_Wwdt = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 22), kCLOCK_Rtc = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 23), kCLOCK_Adc0 = CLK_GATE_DEFINE(AHB_CLK_CTRL0, 27), kCLOCK_Mrt = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 0), kCLOCK_Sct0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 2), kCLOCK_Utick = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 10), kCLOCK_FlexComm0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_FlexComm1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_FlexComm2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_FlexComm3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_FlexComm4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_FlexComm5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_FlexComm6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_FlexComm7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_MinUart0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_MinUart1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_MinUart2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_MinUart3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_MinUart4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_MinUart5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_MinUart6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_MinUart7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_LSpi0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_LSpi1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_LSpi2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_LSpi3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_LSpi4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_LSpi5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_LSpi6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_LSpi7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_BI2c0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_BI2c1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_BI2c2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_BI2c3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_BI2c4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_BI2c5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_BI2c6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_BI2c7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_FlexI2s0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 11), kCLOCK_FlexI2s1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 12), kCLOCK_FlexI2s2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 13), kCLOCK_FlexI2s3 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 14), kCLOCK_FlexI2s4 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 15), kCLOCK_FlexI2s5 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 16), kCLOCK_FlexI2s6 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 17), kCLOCK_FlexI2s7 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 18), kCLOCK_Ct32b2 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 22), kCLOCK_Usbd0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 25), kCLOCK_Ctimer0 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 26), kCLOCK_Ctimer1 = CLK_GATE_DEFINE(AHB_CLK_CTRL1, 27), kCLOCK_Ctimer3 = CLK_GATE_DEFINE(ASYNC_CLK_CTRL0, 13) } |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| enum | _clock_name { kCLOCK_CoreSysClk, kCLOCK_BusClk, kCLOCK_ClockOut, kCLOCK_FroHf, kCLOCK_Fro12M, kCLOCK_ExtClk, kCLOCK_PllOut, kCLOCK_WdtOsc, kCLOCK_Frg, kCLOCK_AsyncApbClk, kCLOCK_FlexI2S } |
| Clock name used to get clock frequency. More... | |
| enum | _async_clock_src { kCLOCK_AsyncMainClk = 0, kCLOCK_AsyncFro12Mhz } |
| Clock source selections for the asynchronous APB clock. More... | |
| enum | _clock_attach_id { kFRO12M_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 0, 0), kEXT_CLK_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 1) | MUX_B(CM_MAINCLKSELB, 0, 0), kWDT_OSC_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 2) | MUX_B(CM_MAINCLKSELB, 0, 0), kFRO_HF_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 3) | MUX_B(CM_MAINCLKSELB, 0, 0), kSYS_PLL_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 2, 0), kOSC32K_to_MAIN_CLK = MUX_A(CM_MAINCLKSELA, 0) | MUX_B(CM_MAINCLKSELB, 3, 0), kFRO12M_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 0), kEXT_CLK_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 1), kWDT_OSC_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 2), kOSC32K_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 3), kNONE_to_SYS_PLL = MUX_A(CM_SYSPLLCLKSEL, 7), kMAIN_CLK_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 0), kFRO12M_to_ASYNC_APB = MUX_A(CM_ASYNCAPB, 1), kMAIN_CLK_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 0), kSYS_PLL_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 1), kFRO_HF_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 2), kNONE_to_ADC_CLK = MUX_A(CM_ADCASYNCCLKSEL, 7), kFRO12M_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 0), kFRO_HF_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 1), kSYS_PLL_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 2), kMCLK_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 3), kFRG_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 4), kNONE_to_FLEXCOMM0 = MUX_A(CM_FXCOMCLKSEL0, 7), kFRO12M_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 0), kFRO_HF_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 1), kSYS_PLL_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 2), kMCLK_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 3), kFRG_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 4), kNONE_to_FLEXCOMM1 = MUX_A(CM_FXCOMCLKSEL1, 7), kFRO12M_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 0), kFRO_HF_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 1), kSYS_PLL_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 2), kMCLK_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 3), kFRG_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 4), kNONE_to_FLEXCOMM2 = MUX_A(CM_FXCOMCLKSEL2, 7), kFRO12M_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 0), kFRO_HF_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 1), kSYS_PLL_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 2), kMCLK_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 3), kFRG_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 4), kNONE_to_FLEXCOMM3 = MUX_A(CM_FXCOMCLKSEL3, 7), kFRO12M_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 0), kFRO_HF_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 1), kSYS_PLL_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 2), kMCLK_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 3), kFRG_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 4), kNONE_to_FLEXCOMM4 = MUX_A(CM_FXCOMCLKSEL4, 7), kFRO12M_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 0), kFRO_HF_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 1), kSYS_PLL_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 2), kMCLK_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 3), kFRG_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 4), kNONE_to_FLEXCOMM5 = MUX_A(CM_FXCOMCLKSEL5, 7), kFRO12M_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 0), kFRO_HF_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 1), kSYS_PLL_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 2), kMCLK_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 3), kFRG_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 4), kNONE_to_FLEXCOMM6 = MUX_A(CM_FXCOMCLKSEL6, 7), kFRO12M_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 0), kFRO_HF_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 1), kSYS_PLL_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 2), kMCLK_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 3), kFRG_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 4), kNONE_to_FLEXCOMM7 = MUX_A(CM_FXCOMCLKSEL7, 7), kMAIN_CLK_to_FRG = MUX_A(CM_FRGCLKSEL, 0), kSYS_PLL_to_FRG = MUX_A(CM_FRGCLKSEL, 1), kFRO12M_to_FRG = MUX_A(CM_FRGCLKSEL, 2), kFRO_HF_to_FRG = MUX_A(CM_FRGCLKSEL, 3), kNONE_to_FRG = MUX_A(CM_FRGCLKSEL, 7), kFRO_HF_to_MCLK = MUX_A(CM_FXI2S0MCLKCLKSEL, 0), kSYS_PLL_to_MCLK = MUX_A(CM_FXI2S0MCLKCLKSEL, 1), kMAIN_CLK_to_MCLK = MUX_A(CM_FXI2S0MCLKCLKSEL, 2), kNONE_to_MCLK = MUX_A(CM_FXI2S0MCLKCLKSEL, 7), kFRO_HF_to_USB_CLK = MUX_A(CM_USBCLKSEL, 0), kSYS_PLL_to_USB_CLK = MUX_A(CM_USBCLKSEL, 1), kMAIN_CLK_to_USB_CLK = MUX_A(CM_USBCLKSEL, 2), kNONE_to_USB_CLK = MUX_A(CM_USBCLKSEL, 7), kMAIN_CLK_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 0), kEXT_CLK_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 1), kWDT_OSC_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 2), kFRO_HF_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 3), kSYS_PLL_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 4), kFRO12M_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 5), kOSC32K_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 6), kNONE_to_CLKOUT = MUX_A(CM_CLKOUTCLKSELA, 7), kNONE_to_NONE = (int)0x80000000U } |
| The enumerator of clock attach Id. More... | |
| enum | _clock_div_name { kCLOCK_DivSystickClk = 0, kCLOCK_DivTraceClk = 1, kCLOCK_DivAhbClk = 32, kCLOCK_DivClkOut = 33, kCLOCK_DivAdcAsyncClk = 37, kCLOCK_DivUsbClk = 38, kCLOCK_DivFrg = 40, kCLOCK_DivFxI2s0MClk = 43 } |
| Clock dividers. More... | |
| enum | _clock_flashtim { kCLOCK_Flash1Cycle = 0, kCLOCK_Flash2Cycle, kCLOCK_Flash3Cycle, kCLOCK_Flash4Cycle, kCLOCK_Flash5Cycle, kCLOCK_Flash6Cycle, kCLOCK_Flash7Cycle } |
| FLASH Access time definitions. More... | |
| enum | _ss_progmodfm { kSS_MF_512 = (0 << 20), kSS_MF_384 = (1 << 20), kSS_MF_256 = (2 << 20), kSS_MF_128 = (3 << 20), kSS_MF_64 = (4 << 20), kSS_MF_32 = (5 << 20), kSS_MF_24 = (6 << 20), kSS_MF_16 = (7 << 20) } |
| PLL Spread Spectrum (SS) Programmable modulation frequency See (MF) field in the SYSPLLSSCTRL1 register in the UM. More... | |
| enum | _ss_progmoddp { kSS_MR_K0 = (0 << 23), kSS_MR_K1 = (1 << 23), kSS_MR_K1_5 = (2 << 23), kSS_MR_K2 = (3 << 23), kSS_MR_K3 = (4 << 23), kSS_MR_K4 = (5 << 23), kSS_MR_K6 = (6 << 23), kSS_MR_K8 = (7 << 23) } |
| PLL Spread Spectrum (SS) Programmable frequency modulation depth See (MR) field in the SYSPLLSSCTRL1 register in the UM. More... | |
| enum | _ss_modwvctrl { kSS_MC_NOC = (0 << 26), kSS_MC_RECC = (2 << 26), kSS_MC_MAXC = (3 << 26) } |
| PLL Spread Spectrum (SS) Modulation waveform control See (MC) field in the SYSPLLSSCTRL1 register in the UM. More... | |
| enum | _pll_error { kStatus_PLL_Success = MAKE_STATUS(kStatusGroup_Generic, 0), kStatus_PLL_OutputTooLow = MAKE_STATUS(kStatusGroup_Generic, 1), kStatus_PLL_OutputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 2), kStatus_PLL_InputTooLow = MAKE_STATUS(kStatusGroup_Generic, 3), kStatus_PLL_InputTooHigh = MAKE_STATUS(kStatusGroup_Generic, 4), kStatus_PLL_OutsideIntLimit = MAKE_STATUS(kStatusGroup_Generic, 5) } |
| PLL status definitions. More... | |
| enum | _clock_usb_src { kCLOCK_UsbSrcFro = (uint32_t)kCLOCK_FroHf, kCLOCK_UsbSrcSystemPll = (uint32_t)kCLOCK_PllOut, kCLOCK_UsbSrcMainClock = (uint32_t)kCLOCK_CoreSysClk, kCLOCK_UsbSrcNone } |
| USB clock source definition. More... | |
Functions | |
| static void | CLOCK_SetFLASHAccessCycles (clock_flashtim_t clks) |
| Set FLASH memory access time in clocks. More... | |
| status_t | CLOCK_SetupFROClocking (uint32_t iFreq) |
| Initialize the Core clock to given frequency (12, 48 or 96 MHz). Turns on FRO and uses default CCO, if freq is 12000000, then high speed output is off, else high speed output is enabled. More... | |
| void | CLOCK_AttachClk (clock_attach_id_t connection) |
| Configure the clock selection muxes. More... | |
| clock_attach_id_t | CLOCK_GetClockAttachId (clock_attach_id_t attachId) |
| Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More... | |
| void | CLOCK_SetClkDiv (clock_div_name_t div_name, uint32_t divided_by_value, bool reset) |
| Setup peripheral clock dividers. More... | |
| void | CLOCK_SetFLASHAccessCyclesForFreq (uint32_t iFreq) |
| Set the flash wait states for the input freuqency. More... | |
| uint32_t | CLOCK_GetFreq (clock_name_t clockName) |
| Return Frequency of selected clock. More... | |
| uint32_t | CLOCK_GetFRGInputClock (void) |
| Return Input frequency for the Fractional baud rate generator. More... | |
| uint32_t | CLOCK_SetFRGClock (uint32_t freq) |
| Set output of the Fractional baud rate generator. More... | |
| uint32_t | CLOCK_GetFro12MFreq (void) |
| Return Frequency of FRO 12MHz. More... | |
| uint32_t | CLOCK_GetExtClkFreq (void) |
| Return Frequency of External Clock. More... | |
| uint32_t | CLOCK_GetWdtOscFreq (void) |
| Return Frequency of Watchdog Oscillator. More... | |
| uint32_t | CLOCK_GetFroHfFreq (void) |
| Return Frequency of High-Freq output of FRO. More... | |
| uint32_t | CLOCK_GetPllOutFreq (void) |
| Return Frequency of PLL. More... | |
| uint32_t | CLOCK_GetOsc32KFreq (void) |
| Return Frequency of 32kHz osc. More... | |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| Return Frequency of Core System. More... | |
| uint32_t | CLOCK_GetI2SMClkFreq (void) |
| Return Frequency of I2S MCLK Clock. More... | |
| uint32_t | CLOCK_GetFlexCommClkFreq (uint32_t id) |
| Return Frequency of Flexcomm functional Clock. More... | |
| uint32_t | CLOCK_GetUsbClkFreq (void) |
| brief Return Frequency of Usb Clock return Frequency of Usb Clock. | |
| uint32_t | CLOCK_GetAdcClkFreq (void) |
| Return Frequency of Adc Clock. More... | |
| uint32_t | CLOCK_GetClockOutClkFreq (void) |
| Return Frequency of ClockOut. More... | |
| __STATIC_INLINE async_clock_src_t | CLOCK_GetAsyncApbClkSrc (void) |
| Return Asynchronous APB Clock source. More... | |
| uint32_t | CLOCK_GetAsyncApbClkFreq (void) |
| Return Frequency of Asynchronous APB Clock. More... | |
| uint32_t | CLOCK_GetSystemPLLInClockRate (void) |
| Return System PLL input clock rate. More... | |
| uint32_t | CLOCK_GetSystemPLLOutClockRate (bool recompute) |
| Return System PLL output clock rate. More... | |
| __STATIC_INLINE void | CLOCK_SetBypassPLL (bool bypass) |
| Enables and disables PLL bypass mode. More... | |
| __STATIC_INLINE bool | CLOCK_IsSystemPLLLocked (void) |
| Check if PLL is locked or not. More... | |
| void | CLOCK_SetStoredPLLClockRate (uint32_t rate) |
| Store the current PLL rate. More... | |
| uint32_t | CLOCK_GetSystemPLLOutFromSetup (pll_setup_t *pSetup) |
| Return System PLL output clock rate from setup structure. More... | |
| pll_error_t | CLOCK_SetupPLLData (pll_config_t *pControl, pll_setup_t *pSetup) |
| Set PLL output based on the passed PLL setup data. More... | |
| pll_error_t | CLOCK_SetupSystemPLLPrec (pll_setup_t *pSetup, uint32_t flagcfg) |
| Set PLL output from PLL setup structure (precise frequency) More... | |
| pll_error_t | CLOCK_SetPLLFreq (const pll_setup_t *pSetup) |
| Set PLL output from PLL setup structure (precise frequency) More... | |
| void | CLOCK_SetupSystemPLLMult (uint32_t multiply_by, uint32_t input_freq) |
| Set PLL output based on the multiplier and input frequency. More... | |
| static void | CLOCK_DisableUsbfs0Clock (void) |
| Disable USB FS clock. More... | |
Driver version | |
| #define | FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(2, 4, 2)) |
| CLOCK driver version 2.4.2. More... | |
| struct _pll_config |
This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.
Data Fields | |
| uint32_t | desiredRate |
| Desired PLL rate in Hz. | |
| uint32_t | inputRate |
| PLL input clock in Hz, only used if PLL_CONFIGFLAG_USEINRATE flag is set. | |
| uint32_t | flags |
| PLL configuration flags, Or'ed value of PLL_CONFIGFLAG_* definitions. | |
| ss_progmodfm_t | ss_mf |
| SS Programmable modulation frequency, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| ss_progmoddp_t | ss_mr |
| SS Programmable frequency modulation depth, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| ss_modwvctrl_t | ss_mc |
| SS Modulation waveform control, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag. | |
| bool | mfDither |
| false for fixed modulation frequency or true for dithering, only applicable when not using PLL_CONFIGFLAG_FORCENOFRACT flag | |
| struct _pll_setup |
It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.
Data Fields | |
| uint32_t | syspllctrl |
| PLL control register SYSPLLCTRL. | |
| uint32_t | syspllndec |
| PLL NDEC register SYSPLLNDEC. | |
| uint32_t | syspllpdec |
| PLL PDEC register SYSPLLPDEC. | |
| uint32_t | syspllssctrl [2] |
| PLL SSCTL registers SYSPLLSSCTRL. | |
| uint32_t | pllRate |
| Acutal PLL rate. | |
| uint32_t | flags |
| PLL setup flags, Or'ed value of PLL_SETUPFLAG_* definitions. | |
| #define FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(2, 4, 2)) |
| #define CLOCK_USR_CFG_PLL_CONFIG_CACHE_COUNT 2U |
Once define this MACRO to be non-zero value, CLOCK_PllGetConfig() function would cache the recent calulation and accelerate the execution to get the right settings.
| #define FLEXCOMM_CLOCKS |
| #define LPUART_CLOCKS |
| #define BI2C_CLOCKS |
| #define LPSI_CLOCKS |
| #define FLEXI2S_CLOCKS |
| #define UTICK_CLOCKS |
| #define DMA_CLOCKS |
| #define CTIMER_CLOCKS |
| #define GPIO_CLOCKS |
| #define ADC_CLOCKS |
| #define MRT_CLOCKS |
| #define SCT_CLOCKS |
| #define RTC_CLOCKS |
| #define WWDT_CLOCKS |
| #define CRC_CLOCKS |
| #define USBD_CLOCKS |
| #define GINT_CLOCKS |
GINT0 & GINT1 share same slot
| #define CLK_GATE_REG_OFFSET_SHIFT 8U |
| #define CLK_ATTACH_ID | ( | mux, | |
| sel, | |||
| pos | |||
| ) | ((((uint32_t)(mux) << 0U) | (((uint32_t)(sel) + 1U) & 0xFU) << 8U) << ((pos)*12U)) |
[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*
| #define PLL_CONFIGFLAG_USEINRATE (1U << 0U) |
When the PLL_CONFIGFLAG_USEINRATE flag is selected, the 'InputRate' field in the configuration structure must be assigned with the expected PLL frequency. If the PLL_CONFIGFLAG_USEINRATE is not used, 'InputRate' is ignored in the configuration function and the driver will determine the PLL rate from the currently selected PLL source. This flag might be used to configure the PLL input clock more accurately when using the WDT oscillator or a more dyanmic CLKIN source.
When the PLL_CONFIGFLAG_FORCENOFRACT flag is selected, the PLL hardware for the automatic bandwidth selection, Spread Spectrum (SS) support, and fractional M-divider are not used.
Flag to use InputRate in PLL configuration structure for setup
| #define PLL_SETUPFLAG_POWERUP (1U << 0U) |
Setup will power on the PLL after setup
| typedef enum _clock_ip_name clock_ip_name_t |
| typedef enum _clock_name clock_name_t |
| typedef enum _clock_div_name clock_div_name_t |
| typedef enum _ss_modwvctrl ss_modwvctrl_t |
Compensation for low pass filtering of the PLL to get a triangular modulation at the output of the PLL, giving a flat frequency spectrum.
| typedef struct _pll_config pll_config_t |
This structure can be used to configure the settings for a PLL setup structure. Fill in the desired configuration for the PLL and call the PLL setup function to fill in a PLL setup structure.
| typedef struct _pll_setup pll_setup_t |
It can be populated with the PLL setup function. If powering up or waiting for PLL lock, the PLL input clock source should be configured prior to PLL setup.
| typedef enum _clock_usb_src clock_usb_src_t |
| enum _clock_ip_name |
| enum _clock_name |
| enum _async_clock_src |
| enum _clock_attach_id |
| enum _clock_div_name |
| enum _clock_flashtim |
| enum _ss_progmodfm |
| enum _ss_progmoddp |
| enum _ss_modwvctrl |
| enum _pll_error |
| enum _clock_usb_src |
|
inlinestatic |
| clks | : Clock cycles for FLASH access |
| status_t CLOCK_SetupFROClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be one of CLK_FRO_12MHZ or CLK_FRO_48MHZ or CLK_FRO_96MHZ) |
| void CLOCK_AttachClk | ( | clock_attach_id_t | connection | ) |
| connection | : Clock to be configured. |
| clock_attach_id_t CLOCK_GetClockAttachId | ( | clock_attach_id_t | attachId | ) |
| attachId | : Clock attach id to get. |
| void CLOCK_SetClkDiv | ( | clock_div_name_t | div_name, |
| uint32_t | divided_by_value, | ||
| bool | reset | ||
| ) |
| div_name | : Clock divider name |
| divided_by_value,: | Value to be divided |
| reset | : Whether to reset the divider counter. |
| void CLOCK_SetFLASHAccessCyclesForFreq | ( | uint32_t | iFreq | ) |
| iFreq | : Input frequency |
| uint32_t CLOCK_GetFreq | ( | clock_name_t | clockName | ) |
| uint32_t CLOCK_GetFRGInputClock | ( | void | ) |
| uint32_t CLOCK_SetFRGClock | ( | uint32_t | freq | ) |
| freq | : Desired output frequency |
| uint32_t CLOCK_GetFro12MFreq | ( | void | ) |
| uint32_t CLOCK_GetExtClkFreq | ( | void | ) |
| uint32_t CLOCK_GetWdtOscFreq | ( | void | ) |
| uint32_t CLOCK_GetFroHfFreq | ( | void | ) |
| uint32_t CLOCK_GetPllOutFreq | ( | void | ) |
| uint32_t CLOCK_GetOsc32KFreq | ( | void | ) |
| uint32_t CLOCK_GetCoreSysClkFreq | ( | void | ) |
| uint32_t CLOCK_GetI2SMClkFreq | ( | void | ) |
| uint32_t CLOCK_GetFlexCommClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetAdcClkFreq | ( | void | ) |
| uint32_t CLOCK_GetClockOutClkFreq | ( | void | ) |
| __STATIC_INLINE async_clock_src_t CLOCK_GetAsyncApbClkSrc | ( | void | ) |
| uint32_t CLOCK_GetAsyncApbClkFreq | ( | void | ) |
| uint32_t CLOCK_GetSystemPLLInClockRate | ( | void | ) |
| uint32_t CLOCK_GetSystemPLLOutClockRate | ( | bool | recompute | ) |
| recompute | : Forces a PLL rate recomputation if true |
| __STATIC_INLINE void CLOCK_SetBypassPLL | ( | bool | bypass | ) |
bypass : true to bypass PLL (PLL output = PLL input, false to disable bypass
| __STATIC_INLINE bool CLOCK_IsSystemPLLLocked | ( | void | ) |
| void CLOCK_SetStoredPLLClockRate | ( | uint32_t | rate | ) |
| rate,: | Current rate of the PLL |
| uint32_t CLOCK_GetSystemPLLOutFromSetup | ( | pll_setup_t * | pSetup | ) |
| pSetup | : Pointer to a PLL setup structure |
| pll_error_t CLOCK_SetupPLLData | ( | pll_config_t * | pControl, |
| pll_setup_t * | pSetup | ||
| ) |
| pControl | : Pointer to populated PLL control structure to generate setup with |
| pSetup | : Pointer to PLL setup structure to be filled |
| pll_error_t CLOCK_SetupSystemPLLPrec | ( | pll_setup_t * | pSetup, |
| uint32_t | flagcfg | ||
| ) |
| pSetup | : Pointer to populated PLL setup structure |
| flagcfg | : Flag configuration for PLL config structure |
| pll_error_t CLOCK_SetPLLFreq | ( | const pll_setup_t * | pSetup | ) |
| pSetup | : Pointer to populated PLL setup structure |
| void CLOCK_SetupSystemPLLMult | ( | uint32_t | multiply_by, |
| uint32_t | input_freq | ||
| ) |
| multiply_by | : multiplier |
| input_freq | : Clock input frequency of the PLL |
|
inlinestatic |
Disable USB FS clock.