![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
The clock driver supports:
Files | |
| file | fsl_clock.h |
Data Structures | |
| struct | firc_trim_config_t |
| firc trim configuration. More... | |
| struct | sirc_trim_config_t |
| sirc trim configuration. More... | |
Macros | |
| #define | FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0U |
| Configure whether driver controls clock. More... | |
| #define | CLK_GATE_REG_OFFSET(value) (((uint32_t)(value)) >> 16U) |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| #define | AOI_CLOCKS |
| Clock ip name array for AOI. More... | |
| #define | CRC_CLOCKS |
| Clock ip name array for CRC. More... | |
| #define | CTIMER_CLOCKS |
| Clock ip name array for CTIMER. More... | |
| #define | DMA_CLOCKS |
| Clock ip name array for DMA. More... | |
| #define | EDMA_CLOCKS |
| Clock gate name array for EDMA. More... | |
| #define | ERM_CLOCKS |
| Clock ip name array for ERM. More... | |
| #define | EIM_CLOCKS |
| Clock ip name array for EIM. More... | |
| #define | FREQME_CLOCKS |
| Clock ip name array for FREQME. More... | |
| #define | GPIO_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | I3C_CLOCKS |
| Clock ip name array for I3C. | |
| #define | INPUTMUX_CLOCKS |
| Clock ip name array for INPUTMUX. More... | |
| #define | LPCMP_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | LPADC_CLOCKS |
| Clock ip name array for LPADC. More... | |
| #define | LPUART_CLOCKS |
| Clock ip name array for LPUART. More... | |
| #define | LPI2C_CLOCKS |
| Clock ip name array for LPI2C. More... | |
| #define | LPSPI_CLOCKS |
| Clock ip name array for LSPI. More... | |
| #define | MTR_CLOCKS |
| Clock ip name array for MTR. More... | |
| #define | OSTIMER_CLOCKS |
| Clock ip name array for OSTIMER. More... | |
| #define | PWM_CLOCKS |
| Clock ip name array for PWM. More... | |
| #define | QDC_CLOCKS |
| Clock ip name array for QDC. More... | |
| #define | UTICK_CLOCKS |
| Clock ip name array for UTICK. More... | |
| #define | WWDT_CLOCKS |
| Clock ip name array for WWDT. More... | |
| #define | BUS_CLK kCLOCK_BusClk |
| Peripherals clock source definition. More... | |
| #define | CLK_ATTACH_REG_OFFSET(value) (((uint32_t)(value)) >> 16U) |
| Clock Mux Switches The encoding is as follows each connection identified is 32bits wide while 24bits are valuable starting from LSB upwards. More... | |
Enumerations | |
| enum | clock_ip_name_t { kCLOCK_GateINPUTMUX0 = (0x00000U | (0U)), kCLOCK_InputMux = (0x00000U | (0U)), kCLOCK_GateI3C0 = (0x00000U | (1U)), kCLOCK_GateCTIMER0 = (0x00000U | (2U)), kCLOCK_GateCTIMER1 = (0x00000U | (3U)), kCLOCK_GateCTIMER2 = (0x00000U | (4U)), kCLOCK_GateFREQME = (0x00000U | (5U)), kCLOCK_GateUTICK0 = (0x00000U | (6U)), kCLOCK_GateWWDT0 = (0x00000U | (7U)), kCLOCK_GateDMA = (0x00000U | (8U)), kCLOCK_GateAOI0 = (0x00000U | (9U)), kCLOCK_GateCRC = (0x00000U | (10U)), kCLOCK_Crc0 = (0x00000U | (10U)), kCLOCK_GateEIM = (0x00000U | (11U)), kCLOCK_GateERM = (0x00000U | (12U)), kCLOCK_GateLPI2C0 = (0x00000U | (16U)), kCLOCK_GateLPSPI0 = (0x00000U | (17U)), kCLOCK_GateLPSPI1 = (0x00000U | (18U)), kCLOCK_GateLPUART0 = (0x00000U | (19U)), kCLOCK_GateLPUART1 = (0x00000U | (20U)), kCLOCK_GateLPUART2 = (0x00000U | (21U)), kCLOCK_GateUSB0 = (0x00000U | (22U)), kCLOCK_GateQDC0 = (0x00000U | (23U)), kCLOCK_GateFLEXPWM0 = (0x00000U | (24U)), kCLOCK_GateOSTIMER0 = (0x00000U | (25U)), kCLOCK_GateADC0 = (0x00000U | (26U)), kCLOCK_GateCMP0 = (0x00000U | (27U)), kCLOCK_GateCMP1 = (0x00000U | (28U)), kCLOCK_GatePORT0 = (0x00000U | (29U)), kCLOCK_GatePORT1 = (0x00000U | (30U)), kCLOCK_GatePORT2 = (0x00000U | (31U)), kCLOCK_GatePORT3 = ((0x10U << 16U) | (0U)), kCLOCK_GateATX0 = ((0x10U << 16U) | (1U)), kCLOCK_GateMTR = ((0x10U << 16U) | (2U)), kCLOCK_GateTCU = ((0x10U << 16U) | (3U)), kCLOCK_GateEZRAMC_RAMA = ((0x10U << 16U) | (4U)), kCLOCK_GateGPIO0 = ((0x10U << 16U) | (5U)), kCLOCK_GateGPIO1 = ((0x10U << 16U) | (6U)), kCLOCK_GateGPIO2 = ((0x10U << 16U) | (7U)), kCLOCK_GateGPIO3 = ((0x10U << 16U) | (8U)), kCLOCK_GateROMCP = ((0x10U << 16U) | (9U)), kCLOCK_GatePWMSM0 = ((REG_PWM0SUBCTL << 16U) | (0U)), kCLOCK_GatePWMSM1 = ((REG_PWM0SUBCTL << 16U) | (1U)), kCLOCK_GatePWMSM2 = ((REG_PWM0SUBCTL << 16U) | (2U)), kCLOCK_GateNotAvail = (0xFFFFFFFFU) } |
| Clock gate name used for CLOCK_EnableClock/CLOCK_DisableClock. More... | |
| enum | clock_name_t { kCLOCK_MainClk, kCLOCK_CoreSysClk, kCLOCK_SYSTEM_CLK, kCLOCK_BusClk, kCLOCK_ExtClk, kCLOCK_FroHf, kCLOCK_FroHfDiv, kCLOCK_Clk48M, kCLOCK_Fro12M, kCLOCK_Clk1M, kCLOCK_Fro16K, kCLOCK_Clk16K0, kCLOCK_Clk16K1, kCLOCK_SLOW_CLK } |
| Clock name used to get clock frequency. More... | |
| enum | clock_select_name_t { kCLOCK_SelI3C0_FCLK = (0x0A0U), kCLOCK_SelCTIMER0 = (0x0A8U), kCLOCK_SelCTIMER1 = (0x0B0U), kCLOCK_SelCTIMER2 = (0x0B8U), kCLOCK_SelLPI2C0 = (0x0C8U), kCLOCK_SelLPSPI0 = (0x0D0U), kCLOCK_SelLPSPI1 = (0x0D8U), kCLOCK_SelLPUART0 = (0x0E0U), kCLOCK_SelLPUART1 = (0x0E8U), kCLOCK_SelLPUART2 = (0x0F0U), kCLOCK_SelUSB0 = (0x0F8U), kCLOCK_SelLPTMR0 = (0x100U), kCLOCK_SelOSTIMER0 = (0x108U), kCLOCK_SelADC0 = (0x110U), kCLOCK_SelCMP0_RR = (0x120U), kCLOCK_SelCMP1_RR = (0x130U), kCLOCK_SelTRACE = (0x138U), kCLOCK_SelCLKOUT = (0x140U), kCLOCK_SelSYSTICK = (0x148U), kCLOCK_SelSCGSCS = (0x200U), kCLOCK_SelMax = (0x200U) } |
| Clock name used to get clock frequency. More... | |
| enum | clock_attach_id_t { kCLK_IN_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 1U), kFRO12M_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 2U), kFRO_HF_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 3U), kCLK_16K_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 4U), kNONE_to_MAIN_CLK = CLK_ATTACH_MUX(kCLOCK_SelSCGSCS, 7U), kFRO12M_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 0U), kFRO_HF_DIV_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 2U), kCLK_IN_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 3U), kCLK_1M_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 5U), kNONE_to_I3C0FCLK = CLK_ATTACH_MUX(kCLOCK_SelI3C0_FCLK, 7U), kFRO12M_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 0U), kFRO_HF_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 1U), kCLK_IN_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 3U), kCLK_16K_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 4U), kCLK_1M_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 5U), kNONE_to_CTIMER0 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER0, 7U), kFRO12M_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 0U), kFRO_HF_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 1U), kCLK_IN_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 3U), kCLK_16K_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 4U), kCLK_1M_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 5U), kNONE_to_CTIMER1 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER1, 7U), kFRO12M_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 0U), kFRO_HF_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 1U), kCLK_IN_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 3U), kCLK_16K_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 4U), kCLK_1M_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 5U), kNONE_to_CTIMER2 = CLK_ATTACH_MUX(kCLOCK_SelCTIMER2, 7U), kFRO12M_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 0U), kFRO_HF_DIV_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 2U), kCLK_IN_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 3U), kCLK_1M_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 5U), kNONE_to_LPI2C0 = CLK_ATTACH_MUX(kCLOCK_SelLPI2C0, 7U), kFRO12M_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 0U), kFRO_HF_DIV_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 2U), kCLK_IN_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 3U), kCLK_1M_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 5U), kNONE_to_LPSPI0 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI0, 7U), kFRO12M_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 0U), kFRO_HF_DIV_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 2U), kCLK_IN_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 3U), kCLK_1M_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 5U), kNONE_to_LPSPI1 = CLK_ATTACH_MUX(kCLOCK_SelLPSPI1, 7U), kFRO12M_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 0U), kFRO_HF_DIV_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 2U), kCLK_IN_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 3U), kCLK_16K_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 4U), kCLK_1M_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 5U), kNONE_to_LPUART0 = CLK_ATTACH_MUX(kCLOCK_SelLPUART0, 7U), kFRO12M_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 0U), kFRO_HF_DIV_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 2U), kCLK_IN_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 3U), kCLK_16K_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 4U), kCLK_1M_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 5U), kNONE_to_LPUART1 = CLK_ATTACH_MUX(kCLOCK_SelLPUART1, 7U), kFRO12M_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 0U), kFRO_HF_DIV_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 2U), kCLK_IN_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 3U), kCLK_16K_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 4U), kCLK_1M_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 5U), kNONE_to_LPUART2 = CLK_ATTACH_MUX(kCLOCK_SelLPUART2, 7U), kCLK_48M_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 1U), kCLK_IN_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 2U), kNONE_to_USB0 = CLK_ATTACH_MUX(kCLOCK_SelUSB0, 3U), kFRO12M_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 0U), kFRO_HF_DIV_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 2U), kCLK_IN_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 3U), kCLK_1M_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 5U), kNONE_to_LPTMR0 = CLK_ATTACH_MUX(kCLOCK_SelLPTMR0, 7U), kCLK_16K_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 0U), kCLK_1M_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 2U), kNONE_to_OSTIMER = CLK_ATTACH_MUX(kCLOCK_SelOSTIMER0, 3U), kFRO12M_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 0U), kFRO_HF_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 1U), kCLK_IN_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 3U), kCLK_1M_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 5U), kNONE_to_ADC0 = CLK_ATTACH_MUX(kCLOCK_SelADC0, 7U), kFRO12M_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 0U), kFRO_HF_DIV_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 2U), kCLK_IN_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 3U), kCLK_1M_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 5U), kNONE_to_CMP0 = CLK_ATTACH_MUX(kCLOCK_SelCMP0_RR, 7U), kFRO12M_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 0U), kFRO_HF_DIV_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 2U), kCLK_IN_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 3U), kCLK_1M_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 5U), kNONE_to_CMP1 = CLK_ATTACH_MUX(kCLOCK_SelCMP1_RR, 7U), kCPU_CLK_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 0U), kCLK_1M_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 1U), kCLK_16K_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 2U), kNONE_to_TRACE = CLK_ATTACH_MUX(kCLOCK_SelTRACE, 3U), kFRO12M_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 0U), kFRO_HF_DIV_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 1U), kCLK_IN_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 2U), kCLK_16K_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 3U), kSLOW_CLK_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 6U), kNONE_to_CLKOUT = CLK_ATTACH_MUX(kCLOCK_SelCLKOUT, 7U), kCPU_CLK_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 0U), kCLK_1M_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 1U), kCLK_16K_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 2U), kNONE_to_SYSTICK = CLK_ATTACH_MUX(kCLOCK_SelSYSTICK, 3U), kNONE_to_NONE = (0xFFFFFFFFU) } |
| The enumerator of clock attach Id. More... | |
| enum | clock_div_name_t { kCLOCK_DivI3C0_FCLK = (0x0A4U), kCLOCK_DivCTIMER0 = (0x0ACU), kCLOCK_DivCTIMER1 = (0x0B4U), kCLOCK_DivCTIMER2 = (0x0BCU), kCLOCK_DivWWDT0 = (0x0C4U), kCLOCK_DivLPI2C0 = (0x0CCU), kCLOCK_DivLPSPI0 = (0x0D4U), kCLOCK_DivLPSPI1 = (0x0DCU), kCLOCK_DivLPUART0 = (0x0E4U), kCLOCK_DivLPUART1 = (0x0ECU), kCLOCK_DivLPUART2 = (0x0F4U), kCLOCK_DivLPTMR0 = (0x104U), kCLOCK_DivADC0 = (0x114U), kCLOCK_DivCMP0_FUNC = (0x11CU), kCLOCK_DivCMP0_RR = (0x124U), kCLOCK_DivCMP1_FUNC = (0x12CU), kCLOCK_DivCMP1_RR = (0x134U), kCLOCK_DivTRACE = (0x13CU), kCLOCK_DivCLKOUT = (0x144U), kCLOCK_DivSYSTICK = (0x14CU), kCLOCK_DivFRO_HF_DIV = (0x154U), kCLOCK_DivSLOWCLK = (0x378U), kCLOCK_DivAHBCLK = (0x380U), kCLOCK_DivMax = (0x380U) } |
| Clock dividers. More... | |
| enum | firc_trim_mode_t { kSCG_FircTrimNonUpdate = SCG_FIRCCSR_FIRCTREN_MASK, kSCG_FircTrimUpdate = SCG_FIRCCSR_FIRCTREN_MASK | SCG_FIRCCSR_FIRCTRUP_MASK } |
| firc trim mode. More... | |
| enum | firc_trim_src_t { kSCG_FircTrimSrcUsb0 = 0U, kSCG_FircTrimSrcSysOsc = 2U } |
| firc trim source. More... | |
| enum | sirc_trim_mode_t { kSCG_SircTrimNonUpdate = SCG_SIRCCSR_SIRCTREN_MASK, kSCG_SircTrimUpdate = SCG_SIRCCSR_SIRCTREN_MASK | SCG_SIRCCSR_SIRCTRUP_MASK } |
| sirc trim mode. More... | |
| enum | sirc_trim_src_t { kNoTrimSrc = 0, kSCG_SircTrimSrcSysOsc = 2U } |
| sirc trim source. More... | |
| enum | scg_sosc_monitor_mode_t { kSCG_SysOscMonitorDisable = 0U, kSCG_SysOscMonitorInt = SCG_SOSCCSR_SOSCCM_MASK, kSCG_SysOscMonitorReset } |
| SCG system OSC monitor mode. More... | |
| enum | clke_16k_t { kCLKE_16K_SYSTEM = VBAT_FROCLKE_CLKE(1U), kCLKE_16K_COREMAIN = VBAT_FROCLKE_CLKE(2U) } |
| firc trim source. More... | |
Functions | |
| static void | CLOCK_EnableClock (clock_ip_name_t clk) |
| Enable the clock for specific IP. More... | |
| static void | CLOCK_DisableClock (clock_ip_name_t clk) |
| Disable the clock for specific IP. More... | |
| void | CLOCK_AttachClk (clock_attach_id_t connection) |
| Configure the clock selection muxes. More... | |
| clock_attach_id_t | CLOCK_GetClockAttachId (clock_attach_id_t connection) |
| Get the actual clock attach id. This fuction uses the offset in input attach id, then it reads the actual source value in the register and combine the offset to obtain an actual attach id. More... | |
| void | CLOCK_SetClockSelect (clock_select_name_t sel_name, uint32_t value) |
| Set the clock select value. This fuction set the peripheral clock select value. More... | |
| uint32_t | CLOCK_GetClockSelect (clock_select_name_t sel_name) |
| Get the clock select value. This fuction get the peripheral clock select value. More... | |
| void | CLOCK_SetClockDiv (clock_div_name_t div_name, uint32_t value) |
| Setup peripheral clock dividers. More... | |
| uint32_t | CLOCK_GetClockDiv (clock_div_name_t div_name) |
| Get peripheral clock dividers. More... | |
| void | CLOCK_HaltClockDiv (clock_div_name_t div_name) |
| Halt peripheral clock dividers. More... | |
| status_t | CLOCK_SetupFROHFClocking (uint32_t iFreq) |
| Initialize the FROHF to given frequency (48,64,96,192). This function turns on FIRC and select the given frequency as the source of fro_hf. More... | |
| status_t | CLOCK_SetupFRO12MClocking (void) |
| Initialize the FRO12M. This function turns on FRO12M. More... | |
| status_t | CLOCK_SetupFRO16KClocking (uint8_t clk_16k_enable_mask) |
| Initialize the FRO16K. This function turns on FRO16K. More... | |
| status_t | CLOCK_SetupExtClocking (uint32_t iFreq) |
| Initialize the external osc clock to given frequency. More... | |
| status_t | CLOCK_SetupExtRefClocking (uint32_t iFreq) |
| Initialize the external reference clock to given frequency. More... | |
| uint32_t | CLOCK_GetFreq (clock_name_t clockName) |
| Return Frequency of selected clock. More... | |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| Return Frequency of core. More... | |
| uint32_t | CLOCK_GetI3CFClkFreq (void) |
| Return Frequency of I3C FCLK. More... | |
| uint32_t | CLOCK_GetCTimerClkFreq (uint32_t id) |
| Return Frequency of CTimer functional Clock. More... | |
| uint32_t | CLOCK_GetLpi2cClkFreq (void) |
| Return Frequency of LPI2C0 functional Clock. More... | |
| uint32_t | CLOCK_GetLpspiClkFreq (uint32_t id) |
| Return Frequency of LPSPI functional Clock. More... | |
| uint32_t | CLOCK_GetLpuartClkFreq (uint32_t id) |
| Return Frequency of LPUART functional Clock. More... | |
| uint32_t | CLOCK_GetLptmrClkFreq (void) |
| Return Frequency of LPTMR functional Clock. More... | |
| uint32_t | CLOCK_GetOstimerClkFreq (void) |
| Return Frequency of OSTIMER. More... | |
| uint32_t | CLOCK_GetAdcClkFreq (void) |
| Return Frequency of Adc Clock. More... | |
| uint32_t | CLOCK_GetCmpFClkFreq (uint32_t id) |
| Return Frequency of CMP Function Clock. More... | |
| uint32_t | CLOCK_GetCmpRRClkFreq (uint32_t id) |
| Return Frequency of CMP Round Robin Clock. More... | |
| uint32_t | CLOCK_GetTraceClkFreq (void) |
| Return Frequency of Trace Clock. More... | |
| uint32_t | CLOCK_GetClkoutClkFreq (void) |
| Return Frequency of CLKOUT Clock. More... | |
| uint32_t | CLOCK_GetSystickClkFreq (void) |
| Return Frequency of Systick Clock. More... | |
| uint32_t | CLOCK_GetWwdtClkFreq (void) |
| brief Return Frequency of Systick Clock return Frequency of Systick. | |
| status_t | CLOCK_FROHFTrimConfig (firc_trim_config_t config) |
| Setup FROHF trim. More... | |
| status_t | CLOCK_FRO12MTrimConfig (sirc_trim_config_t config) |
| Setup FRO 12M trim. More... | |
| void | CLOCK_SetSysOscMonitorMode (scg_sosc_monitor_mode_t mode) |
| Sets the system OSC monitor mode. More... | |
| bool | CLOCK_EnableUsbfsClock (void) |
| brief Enable USB FS clock. More... | |
Driver version | |
| #define | FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) |
| CLOCK driver version 1.0.0. More... | |
| struct firc_trim_config_t |
Data Fields | |
| firc_trim_mode_t | trimMode |
| Trim mode. More... | |
| firc_trim_src_t | trimSrc |
| Trim source. More... | |
| uint16_t | trimDiv |
| Divider of SOSC. More... | |
| uint8_t | trimCoar |
| Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| uint8_t | trimFine |
| Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| firc_trim_mode_t firc_trim_config_t::trimMode |
| firc_trim_src_t firc_trim_config_t::trimSrc |
| uint16_t firc_trim_config_t::trimDiv |
| uint8_t firc_trim_config_t::trimCoar |
| uint8_t firc_trim_config_t::trimFine |
| struct sirc_trim_config_t |
Data Fields | |
| sirc_trim_mode_t | trimMode |
| Trim mode. More... | |
| sirc_trim_src_t | trimSrc |
| Trim source. More... | |
| uint16_t | trimDiv |
| Divider of SOSC. More... | |
| uint8_t | cltrim |
| Trim coarse value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| uint8_t | ccotrim |
| Trim fine value; Irrelevant if trimMode is kSCG_TrimUpdate. More... | |
| sirc_trim_mode_t sirc_trim_config_t::trimMode |
| sirc_trim_src_t sirc_trim_config_t::trimSrc |
| uint16_t sirc_trim_config_t::trimDiv |
| uint8_t sirc_trim_config_t::cltrim |
| uint8_t sirc_trim_config_t::ccotrim |
| #define FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) |
| #define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0U |
When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.
| #define CLK_GATE_REG_OFFSET | ( | value | ) | (((uint32_t)(value)) >> 16U) |
| #define AOI_CLOCKS |
| #define CRC_CLOCKS |
| #define CTIMER_CLOCKS |
| #define DMA_CLOCKS |
| #define EDMA_CLOCKS |
| #define ERM_CLOCKS |
| #define EIM_CLOCKS |
| #define FREQME_CLOCKS |
| #define GPIO_CLOCKS |
| #define INPUTMUX_CLOCKS |
| #define LPCMP_CLOCKS |
| #define LPADC_CLOCKS |
| #define LPUART_CLOCKS |
| #define LPI2C_CLOCKS |
| #define LPSPI_CLOCKS |
| #define MTR_CLOCKS |
| #define OSTIMER_CLOCKS |
| #define PWM_CLOCKS |
| #define QDC_CLOCKS |
| #define UTICK_CLOCKS |
| #define WWDT_CLOCKS |
| #define BUS_CLK kCLOCK_BusClk |
| #define CLK_ATTACH_REG_OFFSET | ( | value | ) | (((uint32_t)(value)) >> 16U) |
[4 bits for choice, 0 means invalid choice] [8 bits mux ID]*
| enum clock_ip_name_t |
| enum clock_name_t |
| enum clock_select_name_t |
| enum clock_attach_id_t |
| enum clock_div_name_t |
| enum firc_trim_mode_t |
| Enumerator | |
|---|---|
| kSCG_FircTrimNonUpdate |
Trim enable but not enable trim value update. In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure firc_trim_config_t. |
| kSCG_FircTrimUpdate |
Trim enable and trim value update enable. In this mode, the trim value is auto update. |
| enum firc_trim_src_t |
| enum sirc_trim_mode_t |
| Enumerator | |
|---|---|
| kSCG_SircTrimNonUpdate |
Trim enable but not enable trim value update. In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure sirc_trim_config_t. |
| kSCG_SircTrimUpdate |
Trim enable and trim value update enable. In this mode, the trim value is auto update. |
| enum sirc_trim_src_t |
| enum clke_16k_t |
|
inlinestatic |
| clk | : Clock to be enabled. |
|
inlinestatic |
| clk | : Clock to be Disabled. |
| void CLOCK_AttachClk | ( | clock_attach_id_t | connection | ) |
| connection | : Clock to be configured. |
| clock_attach_id_t CLOCK_GetClockAttachId | ( | clock_attach_id_t | connection | ) |
| connection | : Clock attach id to get. |
| void CLOCK_SetClockSelect | ( | clock_select_name_t | sel_name, |
| uint32_t | value | ||
| ) |
| sel_name | : Clock select. |
| value | : value to be set. |
| uint32_t CLOCK_GetClockSelect | ( | clock_select_name_t | sel_name | ) |
| sel_name | : Clock select. |
| void CLOCK_SetClockDiv | ( | clock_div_name_t | div_name, |
| uint32_t | value | ||
| ) |
| div_name | : Clock divider name |
| value | : Value to be divided |
| uint32_t CLOCK_GetClockDiv | ( | clock_div_name_t | div_name | ) |
| div_name | : Clock divider name |
| void CLOCK_HaltClockDiv | ( | clock_div_name_t | div_name | ) |
| div_name | : Clock divider name |
| status_t CLOCK_SetupFROHFClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency. |
| status_t CLOCK_SetupFRO12MClocking | ( | void | ) |
| status_t CLOCK_SetupFRO16KClocking | ( | uint8_t | clk_16k_enable_mask | ) |
| clk_16k_enable_mask,: | 0-3 0b00: disable both clk_16k0 and clk_16k1 0b01: only enable clk_16k0 0b10: only enable clk_16k1 0b11: enable both clk_16k0 and clk_16k1 |
| status_t CLOCK_SetupExtClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be equal to exact rate in Hz) |
| status_t CLOCK_SetupExtRefClocking | ( | uint32_t | iFreq | ) |
| iFreq | : Desired frequency (must be equal to exact rate in Hz) |
| uint32_t CLOCK_GetFreq | ( | clock_name_t | clockName | ) |
| uint32_t CLOCK_GetCoreSysClkFreq | ( | void | ) |
| uint32_t CLOCK_GetI3CFClkFreq | ( | void | ) |
| uint32_t CLOCK_GetCTimerClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetLpi2cClkFreq | ( | void | ) |
| uint32_t CLOCK_GetLpspiClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetLpuartClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetLptmrClkFreq | ( | void | ) |
| uint32_t CLOCK_GetOstimerClkFreq | ( | void | ) |
| uint32_t CLOCK_GetAdcClkFreq | ( | void | ) |
| uint32_t CLOCK_GetCmpFClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetCmpRRClkFreq | ( | uint32_t | id | ) |
| uint32_t CLOCK_GetTraceClkFreq | ( | void | ) |
| uint32_t CLOCK_GetClkoutClkFreq | ( | void | ) |
| uint32_t CLOCK_GetSystickClkFreq | ( | void | ) |
| status_t CLOCK_FROHFTrimConfig | ( | firc_trim_config_t | config | ) |
| config | : FROHF trim value |
| status_t CLOCK_FRO12MTrimConfig | ( | sirc_trim_config_t | config | ) |
| config | : FRO 12M trim value |
| void CLOCK_SetSysOscMonitorMode | ( | scg_sosc_monitor_mode_t | mode | ) |
This function sets the system OSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
| bool CLOCK_EnableUsbfsClock | ( | void | ) |
Enable USB Full Speed clock.