![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| union | freqme_mode_attribute_t |
| The union of operate mode attribute. More... | |
| struct | freq_measure_config_t |
| The structure of freqme module basic configuration, including operate mode, operate mode attribute and so on. More... | |
Enumerations | |
| enum | _freqme_interrupt_status_flags { kFREQME_UnderflowInterruptStatusFlag = FREQME_CTRLSTAT_LT_MIN_STAT_MASK, kFREQME_OverflowInterruptStatusFlag = FREQME_CTRLSTAT_GT_MAX_STAT_MASK, kFREQME_ReadyInterruptStatusFlag = FREQME_CTRLSTAT_RESULT_READY_STAT_MASK, kFREQME_AllInterruptStatusFlags } |
| The enumeration of interrupt status flags. More... | |
| enum | _freqme_interrupt_enable { kFREQME_UnderflowInterruptEnable = FREQME_CTRL_W_LT_MIN_INT_EN_MASK, kFREQME_OverflowInterruptEnable = FREQME_CTRL_W_GT_MAX_INT_EN_MASK, kFREQME_ReadyInterruptEnable = FREQME_CTRL_W_RESULT_READY_INT_EN_MASK } |
| The enumeration of interrupts, including underflow interrupt, overflow interrupt, and result ready interrupt. More... | |
| enum | freqme_operate_mode_t { kFREQME_FreqMeasurementMode = 0U, kFREOME_PulseWidthMeasurementMode } |
| FREQME module operate mode enumeration, including frequency measurement mode and pulse width measurement mode. More... | |
| enum | freqme_pulse_polarity_t { kFREQME_PulseHighPeriod = 0U, kFREQME_PulseLowPeriod } |
| The enumeration of pulse polarity. More... | |
Driver version | |
| #define | FSL_FREQME_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
| FREQME driver version 2.1.2. More... | |
Basic Control APIs | |
| void | FREQME_Init (FREQME_Type *base, const freq_measure_config_t *config) |
| Initialize freqme module, set operate mode, operate mode attribute and initialize measurement cycle. More... | |
| void | FREQME_GetDefaultConfig (freq_measure_config_t *config) |
| Get default configuration. More... | |
| static void | FREQME_StartMeasurementCycle (FREQME_Type *base) |
| Start frequency or pulse width measurement process. More... | |
| static void | FREQME_TerminateMeasurementCycle (FREQME_Type *base) |
| Force the termination of any measurement cycle currently in progress and resets RESULT or just reset RESULT if the module in idle state. More... | |
| static void | FREQME_EnableContinuousMode (FREQME_Type *base, bool enable) |
| Enable/disable Continuous mode. More... | |
| static bool | FREQME_CheckContinuousMode (FREQME_Type *base) |
| Check whether continuous mode is enabled. More... | |
| static void | FREQME_SetOperateMode (FREQME_Type *base, freqme_operate_mode_t operateMode) |
| Set operate mode of freqme module. More... | |
| static bool | FREQME_CheckOperateMode (FREQME_Type *base) |
| Check module's operate mode. More... | |
| static void | FREQME_SetMinExpectedValue (FREQME_Type *base, uint32_t minValue) |
| Set the minimum expected value for the measurement result. More... | |
| static void | FREQME_SetMaxExpectedValue (FREQME_Type *base, uint32_t maxValue) |
| Set the maximum expected value for the measurement result. More... | |
Frequency Measurement Mode Control APIs | |
| uint32_t | FREQME_CalculateTargetClkFreq (FREQME_Type *base, uint32_t refClkFrequency) |
| Calculate the frequency of selected target clock。 More... | |
| static uint8_t | FREQME_GetReferenceClkScaleValue (FREQME_Type *base) |
| Get reference clock scaling factor. More... | |
Pulse Width Measurement Mode Control APIs | |
| static void | FREQME_SetPulsePolarity (FREQME_Type *base, freqme_pulse_polarity_t pulsePolarity) |
| Set pulse polarity when operate mode is selected as Pulse Width Measurement mode. More... | |
| static bool | FREQME_CheckPulsePolarity (FREQME_Type *base) |
| Check pulse polarity when the operate mode is selected as pulse width measurement mode. More... | |
| static uint32_t | FREQME_GetMeasurementResult (FREQME_Type *base) |
| Get measurement result, if operate mode is selected as pulse width measurement mode this function can be used to calculate pulse width. More... | |
Status Control APIs | |
| static uint32_t | FREQME_GetInterruptStatusFlags (FREQME_Type *base) |
| Get interrupt status flags, such as overflow interrupt status flag, underflow interrupt status flag, and so on. More... | |
| static void | FREQME_ClearInterruptStatusFlags (FREQME_Type *base, uint32_t statusFlags) |
| Clear interrupt status flags. More... | |
Interrupt Control APIs | |
| static void | FREQME_EnableInterrupts (FREQME_Type *base, uint32_t masks) |
| Enable interrupts, such as result ready interrupt, overflow interrupt and so on. More... | |
| static void | FREQME_DisableInterrupts (FREQME_Type *base, uint32_t masks) |
| Disable interrupts, such as result ready interrupt, overflow interrupt and so on. More... | |
| union freqme_mode_attribute_t |
Data Fields | |
| uint8_t | refClkScaleFactor |
| Only useful in frequency measurement operate mode, used to set the reference clock counter scaling factor. More... | |
| freqme_pulse_polarity_t | pulsePolarity |
| Only Useful in pulse width measurement operate mode, used to set period polarity. More... | |
| uint8_t freqme_mode_attribute_t::refClkScaleFactor |
| freqme_pulse_polarity_t freqme_mode_attribute_t::pulsePolarity |
| struct freq_measure_config_t |
Data Fields | |
| freqme_operate_mode_t | operateMode |
| Select operate mode, please refer to freqme_operate_mode_t. More... | |
| freqme_mode_attribute_t | operateModeAttribute |
Used to set the attribute of the selected operate mode, if the operate mode is selected as kFREQME_FreqMeasurementMode set freqme_mode_attribute_t::refClkScaleFactor, if operate mode is selected as kFREOME_PulseWidthMeasurementMode, please set freqme_mode_attribute_t::pulsePolarity. More... | |
| bool | enableContinuousMode |
| Enable/disable continuous mode, if continuous mode is enable, the measurement is performed continuously and the result for the last completed measurement is available in the result register. More... | |
| freqme_operate_mode_t freq_measure_config_t::operateMode |
| freqme_mode_attribute_t freq_measure_config_t::operateModeAttribute |
| bool freq_measure_config_t::enableContinuousMode |
| #define FSL_FREQME_DRIVER_VERSION (MAKE_VERSION(2, 1, 2)) |
| void FREQME_Init | ( | FREQME_Type * | base, |
| const freq_measure_config_t * | config | ||
| ) |
| base | FREQME peripheral base address. |
| config | The pointer to module basic configuration, please refer to freq_measure_config_t. |
| void FREQME_GetDefaultConfig | ( | freq_measure_config_t * | config | ) |
| config | The pointer to module basic configuration, please refer to freq_measure_config_t. |
|
inlinestatic |
| base | FREQME peripheral base address. |
|
inlinestatic |
| base | FREQME peripheral base address. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| enable | Used to enable/disable continuous mode,
|
|
inlinestatic |
| base | FREQME peripheral base address. |
| True | Continuous mode is enabled, the measurement is performed continuously. |
| False | Continuous mode is disabled. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| operateMode | The operate mode to be set, please refer to freqme_operate_mode_t. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| True | Pulse width measurement mode. |
| False | Frequency measurement mode. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| minValue | The minimum value to set, please note that this value is 31 bits width. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| maxValue | The maximum value to set, please note that this value is 31 bits width. |
| uint32_t FREQME_CalculateTargetClkFreq | ( | FREQME_Type * | base, |
| uint32_t | refClkFrequency | ||
| ) |
| base | FREQME peripheral base address. |
| refClkFrequency | The frequency of reference clock. |
|
inlinestatic |
| base | FREQME peripheral base address. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| pulsePolarity | The pulse polarity to be set, please refer to freqme_pulse_polarity_t. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| True | Low period. |
| False | High period. |
|
inlinestatic |
| base | FREQME peripheral base address. |
|
inlinestatic |
| base | FREQME peripheral base address. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| statusFlags | The combination of interrupt status flags to clear, should be the OR'ed value of _freqme_interrupt_status_flags. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| masks | The mask of interrupts to enable, should be the OR'ed value of _freqme_interrupt_enable. |
|
inlinestatic |
| base | FREQME peripheral base address. |
| masks | The mask of interrupts to disable, should be the OR'ed value of _freqme_interrupt_enable. |