![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
Data Structures | |
| struct | i3c_master_dma_callback_t |
| i3c master callback functions. More... | |
| struct | i3c_master_dma_handle_t |
| Driver handle for master DMA APIs. More... | |
Master DMA | |
| void | I3C_MasterTransferCreateHandleDMA (I3C_Type *base, i3c_master_dma_handle_t *handle, const i3c_master_dma_callback_t *callback, void *userData, dma_handle_t *rxDmaHandle, dma_handle_t *txDmaHandle) |
| Create a new handle for the I3C master DMA APIs. More... | |
| status_t | I3C_MasterTransferDMA (I3C_Type *base, i3c_master_dma_handle_t *handle, i3c_master_transfer_t *transfer) |
| Performs a non-blocking DMA-based transaction on the I3C bus. More... | |
| status_t | I3C_MasterTransferGetCountDMA (I3C_Type *base, i3c_master_dma_handle_t *handle, size_t *count) |
| Returns number of bytes transferred so far. More... | |
| void | I3C_MasterTransferAbortDMA (I3C_Type *base, i3c_master_dma_handle_t *handle) |
| Terminates a non-blocking I3C master transmission early. More... | |
| void | I3C_MasterTransferDMAHandleIRQ (I3C_Type *base, void *i3cHandle) |
| Reusable routine to handle master interrupts. More... | |
| struct i3c_master_dma_callback_t |
Data Fields | |
| void(* | slave2Master )(I3C_Type *base, void *userData) |
| Transfer complete callback. | |
| void(* | ibiCallback )(I3C_Type *base, i3c_master_dma_handle_t *handle, i3c_ibi_type_t ibiType, i3c_ibi_state_t ibiState) |
| IBI event callback. | |
| void(* | transferComplete )(I3C_Type *base, i3c_master_dma_handle_t *handle, status_t status, void *userData) |
| Transfer complete callback. | |
| struct _i3c_master_dma_handle |
Data Fields | |
| I3C_Type * | base |
| I3C base pointer. More... | |
| uint8_t | state |
| Transfer state machine current state. More... | |
| uint32_t | transferCount |
| Indicates progress of the transfer. | |
| uint8_t | subaddressBuffer [4] |
| Saving subaddress command. More... | |
| uint8_t | subaddressCount |
| Saving command count. More... | |
| i3c_master_transfer_t | transfer |
| Copy of the current transfer info. More... | |
| i3c_master_dma_callback_t | callback |
| Callback function pointer. More... | |
| void * | userData |
| Application data passed to callback. More... | |
| dma_handle_t * | rxDmaHandle |
| Handle for receive DMA channel. More... | |
| dma_handle_t * | txDmaHandle |
| Handle for transmit DMA channel. More... | |
| uint8_t | ibiAddress |
| Slave address which request IBI. More... | |
| uint8_t * | ibiBuff |
| Pointer to IBI buffer to keep ibi bytes. More... | |
| size_t | ibiPayloadSize |
| IBI payload size. More... | |
| i3c_ibi_type_t | ibiType |
| IBI type. More... | |
| I3C_Type* i3c_master_dma_handle_t::base |
| uint8_t i3c_master_dma_handle_t::state |
| uint8_t i3c_master_dma_handle_t::subaddressBuffer[4] |
| uint8_t i3c_master_dma_handle_t::subaddressCount |
| i3c_master_transfer_t i3c_master_dma_handle_t::transfer |
| i3c_master_dma_callback_t i3c_master_dma_handle_t::callback |
| void* i3c_master_dma_handle_t::userData |
| dma_handle_t* i3c_master_dma_handle_t::rxDmaHandle |
| dma_handle_t* i3c_master_dma_handle_t::txDmaHandle |
| uint8_t i3c_master_dma_handle_t::ibiAddress |
| uint8_t* i3c_master_dma_handle_t::ibiBuff |
| size_t i3c_master_dma_handle_t::ibiPayloadSize |
| i3c_ibi_type_t i3c_master_dma_handle_t::ibiType |
| void I3C_MasterTransferCreateHandleDMA | ( | I3C_Type * | base, |
| i3c_master_dma_handle_t * | handle, | ||
| const i3c_master_dma_callback_t * | callback, | ||
| void * | userData, | ||
| dma_handle_t * | rxDmaHandle, | ||
| dma_handle_t * | txDmaHandle | ||
| ) |
The creation of a handle is for use with the DMA APIs. Once a handle is created, there is not a corresponding destroy handle. If the user wants to terminate a transfer, the I3C_MasterTransferAbortDMA() API shall be called.
For devices where the I3C send and receive DMA requests are OR'd together, the txDmaHandle parameter is ignored and may be set to NULL.
| base | The I3C peripheral base address. |
| handle | Pointer to the I3C master driver handle. |
| callback | User provided pointer to the asynchronous callback function. |
| userData | User provided pointer to the application callback data. |
| rxDmaHandle | Handle for the DMA receive channel. Created by the user prior to calling this function. |
| txDmaHandle | Handle for the DMA transmit channel. Created by the user prior to calling this function. |
| status_t I3C_MasterTransferDMA | ( | I3C_Type * | base, |
| i3c_master_dma_handle_t * | handle, | ||
| i3c_master_transfer_t * | transfer | ||
| ) |
The callback specified when the handle was created is invoked when the transaction has completed.
| base | The I3C peripheral base address. |
| handle | Pointer to the I3C master driver handle. |
| transfer | The pointer to the transfer descriptor. |
| kStatus_Success | The transaction was started successfully. |
| kStatus_I3C_Busy | Either another master is currently utilizing the bus, or another DMA transaction is already in progress. |
| status_t I3C_MasterTransferGetCountDMA | ( | I3C_Type * | base, |
| i3c_master_dma_handle_t * | handle, | ||
| size_t * | count | ||
| ) |
| base | The I3C peripheral base address. | |
| handle | Pointer to the I3C master driver handle. | |
| [out] | count | Number of bytes transferred so far by the non-blocking transaction. |
| kStatus_Success | |
| kStatus_NoTransferInProgress | There is not a DMA transaction currently in progress. |
| void I3C_MasterTransferAbortDMA | ( | I3C_Type * | base, |
| i3c_master_dma_handle_t * | handle | ||
| ) |
| base | The I3C peripheral base address. |
| handle | Pointer to the I3C master driver handle. |
| void I3C_MasterTransferDMAHandleIRQ | ( | I3C_Type * | base, |
| void * | i3cHandle | ||
| ) |
| base | The I3C peripheral base address. |
| handle | Pointer to the I3C master DMA driver handle. |