![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.000
NXP Semiconductors
|
The MCUXpresso SDK provides a driver for the EIM module of MCUXpresso SDK devices.
The Error Injection Module (EIM) is mainly used for diagnostic purposes and enables you to induce artificial errors on error-checking mechanisms of a system. It provides a method for diagnostic coverage of internal memories (for example, system RAM, cache RAMs, and peripheral memories).
This example code shows how to show error injection using the EIM driver.
Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/eim
Functions | |
| void | EIM_Init (EIM_Type *base) |
| EIM module initialization function. More... | |
| void | EIM_Deinit (EIM_Type *base) |
| De-initializes the EIM. | |
Driver version | |
| #define | FSL_ERM_DRIVER_VERSION (MAKE_VERSION(2U, 0U, 1U)) |
| Driver version. More... | |
| #define FSL_ERM_DRIVER_VERSION (MAKE_VERSION(2U, 0U, 1U)) |
| void EIM_Init | ( | EIM_Type * | base | ) |
| base | EIM base address. |