MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
DAC: 10-bit Digital To Analog Converter Driver

Overview

The MCUXpresso SDK provides a peripheral driver for the 10-bit digital to analog converter (DAC) module of MCUXpresso SDK devices.

Typical use case

Polling Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dac

Interrupt Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/dac

Files

file  fsl_dac.h
 

Data Structures

struct  _dac_config
 The configuration of DAC. More...
 

Typedefs

typedef enum _dac_settling_time dac_settling_time_t
 The DAC settling time.
 
typedef struct _dac_config dac_config_t
 The configuration of DAC.
 

Enumerations

enum  _dac_settling_time {
  kDAC_SettlingTimeIs1us = 0U,
  kDAC_SettlingTimeIs25us = 1U
}
 The DAC settling time. More...
 

Functions

void DAC_Init (DAC_Type *base, const dac_config_t *config)
 Initialize the DAC module. More...
 
void DAC_Deinit (DAC_Type *base)
 De-Initialize the DAC module. More...
 
void DAC_GetDefaultConfig (dac_config_t *config)
 Initializes the DAC user configuration structure. More...
 
void DAC_EnableDoubleBuffering (DAC_Type *base, bool enable)
 Enable/Diable double-buffering feature. More...
 
void DAC_SetBufferValue (DAC_Type *base, uint32_t value)
 Write DAC output value into CR register or pre-buffer. More...
 
void DAC_SetCounterValue (DAC_Type *base, uint32_t value)
 Write DAC counter value into CNTVAL register. More...
 
static void DAC_EnableDMA (DAC_Type *base, bool enable)
 Enable/Disable the DMA access. More...
 
static void DAC_EnableCounter (DAC_Type *base, bool enable)
 Enable/Disable the counter operation. More...
 
static bool DAC_GetDMAInterruptRequestFlag (DAC_Type *base)
 Get the status flag of DMA or interrupt request. More...
 

Driver version

#define LPC_DAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))
 DAC driver version 2.0.2. More...
 

Data Structure Documentation

struct _dac_config

Data Fields

dac_settling_time_t settlingTime
 The settling times are valid for a capacitance load on the DAC_OUT pin not exceeding 100 pF. More...
 

Field Documentation

dac_settling_time_t _dac_config::settlingTime

A load impedance value greater than that value will cause settling time longer than the specified time. One or more graphs of load impedance vs. settling time will be included in the final data sheet.

Macro Definition Documentation

#define LPC_DAC_DRIVER_VERSION   (MAKE_VERSION(2, 0, 2))

Enumeration Type Documentation

Enumerator
kDAC_SettlingTimeIs1us 

The settling time of the DAC is 1us max, and the maximum current is 700 mA.

This allows a maximum update rate of 1 MHz.

kDAC_SettlingTimeIs25us 

The settling time of the DAC is 2.5us and the maximum current is 350uA.

This allows a maximum update rate of 400 kHz.

Function Documentation

void DAC_Init ( DAC_Type *  base,
const dac_config_t *  config 
)
Parameters
baseDAC peripheral base address.
configThe pointer to configuration structure. Please refer to "dac_config_t" structure.
void DAC_Deinit ( DAC_Type *  base)
Parameters
baseDAC peripheral base address.
void DAC_GetDefaultConfig ( dac_config_t *  config)

This function initializes the user configuration structure to a default value. The default values are as follows.

* config->settlingTime = kDAC_SettlingTimeIs1us;
*
Parameters
configPointer to the configuration structure. See "dac_config_t".
void DAC_EnableDoubleBuffering ( DAC_Type *  base,
bool  enable 
)

Notice: Disabling the double-buffering feature will disable counter opreation. If double-buffering feature is disabled, any writes to the CR address will go directly to the CR register. If double-buffering feature is enabled, any write to the CR register will only load the pre-buffer, which shares its register address with the CR register. The CR itself will be loaded from the pre-buffer whenever the counter reaches zero and the DMA request is set.

Parameters
baseDAC peripheral base address.
enableEnable or disable the feature.
void DAC_SetBufferValue ( DAC_Type *  base,
uint32_t  value 
)

The DAC output voltage is VALUE*((VREFP)/1024).

Parameters
baseDAC peripheral base address.
valueSetting the value for items in the buffer. 10-bits are available.
void DAC_SetCounterValue ( DAC_Type *  base,
uint32_t  value 
)
   When the counter is enabled bit, the 16-bit counter will begin counting down, at the rate selected by PCLK,
   from the value programmed into the DACCNTVAL register. The counter is decremented Each time the counter

reaches zero, the counter will be reloaded by the value of DACCNTVAL and the DMA request bit INT_DMA_REQ will be set in hardware.

Parameters
baseDAC peripheral basic address.
valueSetting the value for items in the counter. 16-bits are available.
static void DAC_EnableDMA ( DAC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseDAC peripheral base address.
enableEnable or disable the feature.
static void DAC_EnableCounter ( DAC_Type *  base,
bool  enable 
)
inlinestatic
Parameters
baseDAC peripheral base address.
enableEnable or disable the feature.
static bool DAC_GetDMAInterruptRequestFlag ( DAC_Type *  base)
inlinestatic
Parameters
baseDAC peripheral base address.
Returns
If return 'true', it means DMA request or interrupt occurs. If return 'false', it means DMA request or interrupt doesn't occur.