![]()  | 
  
    MCUXpresso SDK API Reference Manual
    Rev 2.16.000
    
   NXP Semiconductors 
   | 
 
Data Structures | |
| union | pflash_prot_status_t | 
| PFlash protection status.  More... | |
| struct | flash_config_t | 
| Flash driver state information.  More... | |
Flash version | |
| #define | FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(3U, 0U, 0U)) | 
| Flash driver version for SDK.  More... | |
Initialization | |
| status_t | FLASH_Init (flash_config_t *config) | 
| Initializes the global flash properties structure members.  More... | |
Erasing | |
| status_t | FLASH_Erase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key) | 
| Erases the Dflash sectors encompassed by parameters passed into function.  More... | |
| status_t | FLASH_EraseAll (flash_config_t *config, uint32_t key) | 
| Erases entire flexnvm.  More... | |
Programming | |
| status_t | FLASH_Program (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes) | 
| Programs flash with data at locations passed in through parameters.  More... | |
| status_t | FLASH_ProgramOnce (flash_config_t *config, uint8_t index, uint8_t *src, uint32_t lengthInBytes) | 
| Program the Program-Once-Field through parameters.  More... | |
Reading | |
| status_t | FLASH_ReadOnce (flash_config_t *config, uint8_t index, uint8_t *dst, uint32_t lengthInBytes) | 
| Reads the Program Once Field through parameters.  More... | |
Verification | |
| status_t | FLASH_VerifyErase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint8_t margin) | 
| Verifies an erasure of the desired flash area at a specified margin level.  More... | |
| status_t | FLASH_VerifyEraseAll (flash_config_t *config, uint8_t margin) | 
| Verifies erasure of the entire flash at a specified margin level.  More... | |
| status_t | FLASH_VerifyProgram (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, const uint8_t *expectedData, uint8_t margin, uint32_t *failedAddress, uint32_t *failedData) | 
| Verifies programming of the desired flash area at a specified margin level.  More... | |
Security | |
| status_t | FLASH_GetSecurityState (flash_config_t *config, ftfx_security_state_t *state) | 
| Returns the security state via the pointer passed into the function.  More... | |
Properties | |
| status_t | FLASH_GetProperty (flash_config_t *config, flash_property_tag_t whichProperty, uint32_t *value) | 
| Returns the desired flash property.  More... | |
| union pflash_prot_status_t | 
Data Fields | |
| uint32_t | protl | 
| PROT[31:0] .  More... | |
| uint32_t | proth | 
| PROT[63:32].  More... | |
| uint8_t | protsl | 
| PROTS[7:0] .  More... | |
| uint8_t | protsh | 
| PROTS[15:8] .  More... | |
| uint32_t pflash_prot_status_t::protl | 
| uint32_t pflash_prot_status_t::proth | 
| uint8_t pflash_prot_status_t::protsl | 
| uint8_t pflash_prot_status_t::protsh | 
| struct flash_config_t | 
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
| #define FSL_FLASH_DRIVER_VERSION (MAKE_VERSION(3U, 0U, 0U)) | 
Version 3.0.0.
| enum flash_prot_state_t | 
| enum flash_property_tag_t | 
| status_t FLASH_Init | ( | flash_config_t * | config | ) | 
This function checks and initializes the Flash module for the other Flash APIs.
| config | Pointer to the storage for the driver runtime state. | 
| kStatus_FTFx_Success | API was executed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_PartitionStatusUpdateFailure | Failed to update the partition status. | 
| status_t FLASH_Erase | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint32_t | key | ||
| ) | 
This function erases the appropriate number of flash sectors based on the desired start address and length.
| config | The pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be erased. The start address does not need to be sector-aligned but must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words) to be erased. Must be word-aligned. | 
| key | The value used to validate all flash erase APIs. | 
| kStatus_FTFx_Success | API was executed successfully; the appropriate number of flash sectors based on the desired start address and length were erased successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | The parameter is not aligned with the specified baseline. | 
| kStatus_FTFx_AddressError | The address is out of range. | 
| kStatus_FTFx_EraseKeyError | The API erase key is invalid. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_EraseAll | ( | flash_config_t * | config, | 
| uint32_t | key | ||
| ) | 
| config | Pointer to the storage for the driver runtime state. | 
| key | A value used to validate all flash erase APIs. | 
| kStatus_FTFx_Success | API was executed successfully; the all pflash and flexnvm were erased successfully, the swap and eeprom have been reset to unconfigured state. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_EraseKeyError | API erase key is invalid. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during command execution. | 
| kStatus_FTFx_PartitionStatusUpdateFailure | Failed to update the partition status. | 
| status_t FLASH_Program | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be programmed. Must be word-aligned. | 
| src | A pointer to the source buffer of data that is to be programmed into the flash. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully; the desired data were programed successfully into flash based on desired start address and length. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with the specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_ProgramOnce | ( | flash_config_t * | config, | 
| uint8_t | index, | ||
| uint8_t * | src, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function Program the Program-once-feild with given index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating the area of program once field to be read. | 
| src | A pointer to the source buffer of data that is used to store data to be write. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully; The index indicating the area of program once field was programed successfully. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_ReadOnce | ( | flash_config_t * | config, | 
| uint8_t | index, | ||
| uint8_t * | dst, | ||
| uint32_t | lengthInBytes | ||
| ) | 
This function reads the read once feild with given index and length.
| config | A pointer to the storage for the driver runtime state. | 
| index | The index indicating the area of program once field to be read. | 
| dst | A pointer to the destination buffer of data that is used to store data to be read. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. | 
| kStatus_FTFx_Success | API was executed successfully; the data have been successfuly read form Program flash0 IFR map and Program Once field based on index and length. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_VerifyErase | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| uint8_t | margin | ||
| ) | 
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. | 
| margin | Read margin choice. | 
| kStatus_FTFx_Success | API was executed successfully; the specified FLASH region has been erased. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_VerifyEraseAll | ( | flash_config_t * | config, | 
| uint8_t | margin | ||
| ) | 
This function checks whether the flash is erased to the specified read margin level.
| config | A pointer to the storage for the driver runtime state. | 
| margin | Read margin choice. | 
| kStatus_FTFx_Success | API was executed successfully; all program flash and flexnvm were in erased state. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_VerifyProgram | ( | flash_config_t * | config, | 
| uint32_t | start, | ||
| uint32_t | lengthInBytes, | ||
| const uint8_t * | expectedData, | ||
| uint8_t | margin, | ||
| uint32_t * | failedAddress, | ||
| uint32_t * | failedData | ||
| ) | 
This function verifies the data programmed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. | 
| start | The start address of the desired flash memory to be verified. Must be word-aligned. | 
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. | 
| expectedData | A pointer to the expected data that is to be verified against. | 
| margin | Read margin choice. | 
| failedAddress | A pointer to the returned failing address. | 
| failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. | 
| kStatus_FTFx_Success | API was executed successfully; the desired data have been successfully programed into specified FLASH region. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_AlignmentError | Parameter is not aligned with specified baseline. | 
| kStatus_FTFx_AddressError | Address is out of range. | 
| kStatus_FTFx_ExecuteInRamFunctionNotReady | Execute-in-RAM function is not available. | 
| kStatus_FTFx_AccessError | Invalid instruction codes and out-of bounds addresses. | 
| kStatus_FTFx_ProtectionViolation | The program/erase operation is requested to execute on protected areas. | 
| kStatus_FTFx_CommandFailure | Run-time error during the command execution. | 
| status_t FLASH_GetSecurityState | ( | flash_config_t * | config, | 
| ftfx_security_state_t * | state | ||
| ) | 
This function retrieves the current flash security status, including the security enabling state and the backdoor key enabling state.
| config | A pointer to storage for the driver runtime state. | 
| state | A pointer to the value returned for the current security status code: | 
| kStatus_FTFx_Success | API was executed successfully; the security state of flash was stored to state. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| status_t FLASH_GetProperty | ( | flash_config_t * | config, | 
| flash_property_tag_t | whichProperty, | ||
| uint32_t * | value | ||
| ) | 
| config | A pointer to the storage for the driver runtime state. | 
| whichProperty | The desired property from the list of properties in enum flash_property_tag_t | 
| value | A pointer to the value returned for the desired flash property. | 
| kStatus_FTFx_Success | API was executed successfully; the flash property was stored to value. | 
| kStatus_FTFx_InvalidArgument | An invalid argument is provided. | 
| kStatus_FTFx_UnknownProperty | An unknown property tag. |