MCUXpresso SDK API Reference Manual  Rev 2.16.000
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Panic

Overview

Data Structures

struct  panic_data_t
 panic data structure. More...
 

Macros

#define PANIC_ENABLE_LOG   (0)
 
More...
 

Typedefs

typedef uint32_t panic_id_t
 
More...
 

Functions

void panic (panic_id_t id, uint32_t location, uint32_t extra1, uint32_t extra2)
 
More...
 

Data Structure Documentation

struct panic_data_t

Macro Definition Documentation

#define PANIC_ENABLE_LOG   (0)

Public macros

Typedef Documentation

typedef uint32_t panic_id_t

Include


Public type definitionspanic id.

Function Documentation

void panic ( panic_id_t  id,
uint32_t  location,
uint32_t  extra1,
uint32_t  extra2 
)

Public prototypes

Panic function.

Parameters
idPanic ID
locationlocation address where the Panic occurred
extra1extra1 parameter to be stored in Panic structure.
extra2extra2 parameter to be stored in Panic structure
Return values
Noreturn vaule.