MCUXpresso SDK API Reference Manual  Rev 2.16.001
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Common Driver

Overview

The MCUXpresso SDK provides a driver for the common module of MCUXpresso SDK devices.

Macros

#define FSL_DRIVER_TRANSFER_DOUBLE_WEAK_IRQ   1
 Macro to use the default weak IRQ handler in drivers. More...
 
#define MAKE_STATUS(group, code)   ((((group)*100L) + (code)))
 Construct a status code value from a group and code number. More...
 
#define MAKE_VERSION(major, minor, bugfix)   (((major)*65536L) + ((minor)*256L) + (bugfix))
 Construct the version number for drivers. More...
 
#define ARRAY_SIZE(x)   (sizeof(x) / sizeof((x)[0]))
 Computes the number of elements in an array. More...
 
#define UINT64_H(X)   ((uint32_t)((((uint64_t) (X)) >> 32U) & 0x0FFFFFFFFULL))
 Macro to get upper 32 bits of a 64-bit value.
 
#define UINT64_L(X)   ((uint32_t)(((uint64_t) (X)) & 0x0FFFFFFFFULL))
 Macro to get lower 32 bits of a 64-bit value.
 
#define SUPPRESS_FALL_THROUGH_WARNING()
 For switch case code block, if case section ends without "break;" statement, there wil be fallthrough warning with compiler flag -Wextra or -Wimplicit-fallthrough=n when using armgcc. More...
 

Typedefs

typedef int32_t status_t
 Type used for all status and error return values. More...
 

Enumerations

enum  _status_groups {
  kStatusGroup_Generic = 0,
  kStatusGroup_FLASH = 1,
  kStatusGroup_LPSPI = 4,
  kStatusGroup_FLEXIO_SPI = 5,
  kStatusGroup_DSPI = 6,
  kStatusGroup_FLEXIO_UART = 7,
  kStatusGroup_FLEXIO_I2C = 8,
  kStatusGroup_LPI2C = 9,
  kStatusGroup_UART = 10,
  kStatusGroup_I2C = 11,
  kStatusGroup_LPSCI = 12,
  kStatusGroup_LPUART = 13,
  kStatusGroup_SPI = 14,
  kStatusGroup_XRDC = 15,
  kStatusGroup_SEMA42 = 16,
  kStatusGroup_SDHC = 17,
  kStatusGroup_SDMMC = 18,
  kStatusGroup_SAI = 19,
  kStatusGroup_MCG = 20,
  kStatusGroup_SCG = 21,
  kStatusGroup_SDSPI = 22,
  kStatusGroup_FLEXIO_I2S = 23,
  kStatusGroup_FLEXIO_MCULCD = 24,
  kStatusGroup_FLASHIAP = 25,
  kStatusGroup_FLEXCOMM_I2C = 26,
  kStatusGroup_I2S = 27,
  kStatusGroup_IUART = 28,
  kStatusGroup_CSI = 29,
  kStatusGroup_MIPI_DSI = 30,
  kStatusGroup_SDRAMC = 35,
  kStatusGroup_POWER = 39,
  kStatusGroup_ENET = 40,
  kStatusGroup_PHY = 41,
  kStatusGroup_TRGMUX = 42,
  kStatusGroup_SMARTCARD = 43,
  kStatusGroup_LMEM = 44,
  kStatusGroup_QSPI = 45,
  kStatusGroup_DMA = 50,
  kStatusGroup_EDMA = 51,
  kStatusGroup_DMAMGR = 52,
  kStatusGroup_FLEXCAN = 53,
  kStatusGroup_LTC = 54,
  kStatusGroup_FLEXIO_CAMERA = 55,
  kStatusGroup_LPC_SPI = 56,
  kStatusGroup_LPC_USART = 57,
  kStatusGroup_DMIC = 58,
  kStatusGroup_SDIF = 59,
  kStatusGroup_SPIFI = 60,
  kStatusGroup_OTP = 61,
  kStatusGroup_MCAN = 62,
  kStatusGroup_CAAM = 63,
  kStatusGroup_ECSPI = 64,
  kStatusGroup_USDHC = 65,
  kStatusGroup_LPC_I2C = 66,
  kStatusGroup_DCP = 67,
  kStatusGroup_MSCAN = 68,
  kStatusGroup_ESAI = 69,
  kStatusGroup_FLEXSPI = 70,
  kStatusGroup_MMDC = 71,
  kStatusGroup_PDM = 72,
  kStatusGroup_SDMA = 73,
  kStatusGroup_ICS = 74,
  kStatusGroup_SPDIF = 75,
  kStatusGroup_LPC_MINISPI = 76,
  kStatusGroup_HASHCRYPT = 77,
  kStatusGroup_LPC_SPI_SSP = 78,
  kStatusGroup_I3C = 79,
  kStatusGroup_LPC_I2C_1 = 97,
  kStatusGroup_NOTIFIER = 98,
  kStatusGroup_DebugConsole = 99,
  kStatusGroup_SEMC = 100,
  kStatusGroup_ApplicationRangeStart = 101,
  kStatusGroup_IAP = 102,
  kStatusGroup_SFA = 103,
  kStatusGroup_SPC = 104,
  kStatusGroup_PUF = 105,
  kStatusGroup_TOUCH_PANEL = 106,
  kStatusGroup_VBAT = 107,
  kStatusGroup_XSPI = 108,
  kStatusGroup_PNGDEC = 109,
  kStatusGroup_JPEGDEC = 110,
  kStatusGroup_HAL_GPIO = 121,
  kStatusGroup_HAL_UART = 122,
  kStatusGroup_HAL_TIMER = 123,
  kStatusGroup_HAL_SPI = 124,
  kStatusGroup_HAL_I2C = 125,
  kStatusGroup_HAL_FLASH = 126,
  kStatusGroup_HAL_PWM = 127,
  kStatusGroup_HAL_RNG = 128,
  kStatusGroup_HAL_I2S = 129,
  kStatusGroup_HAL_ADC_SENSOR = 130,
  kStatusGroup_TIMERMANAGER = 135,
  kStatusGroup_SERIALMANAGER = 136,
  kStatusGroup_LED = 137,
  kStatusGroup_BUTTON = 138,
  kStatusGroup_EXTERN_EEPROM = 139,
  kStatusGroup_SHELL = 140,
  kStatusGroup_MEM_MANAGER = 141,
  kStatusGroup_LIST = 142,
  kStatusGroup_OSA = 143,
  kStatusGroup_COMMON_TASK = 144,
  kStatusGroup_MSG = 145,
  kStatusGroup_SDK_OCOTP = 146,
  kStatusGroup_SDK_FLEXSPINOR = 147,
  kStatusGroup_CODEC = 148,
  kStatusGroup_ASRC = 149,
  kStatusGroup_OTFAD = 150,
  kStatusGroup_SDIOSLV = 151,
  kStatusGroup_MECC = 152,
  kStatusGroup_ENET_QOS = 153,
  kStatusGroup_LOG = 154,
  kStatusGroup_I3CBUS = 155,
  kStatusGroup_QSCI = 156,
  kStatusGroup_ELEMU = 157,
  kStatusGroup_QUEUEDSPI = 158,
  kStatusGroup_POWER_MANAGER = 159,
  kStatusGroup_IPED = 160,
  kStatusGroup_ELS_PKC = 161,
  kStatusGroup_CSS_PKC = 162,
  kStatusGroup_HOSTIF = 163,
  kStatusGroup_CLIF = 164,
  kStatusGroup_BMA = 165,
  kStatusGroup_NETC = 166,
  kStatusGroup_ELE = 167,
  kStatusGroup_GLIKEY = 168
}
 Status group numbers. More...
 
enum  {
  kStatus_Success = MAKE_STATUS(kStatusGroup_Generic, 0),
  kStatus_Fail = MAKE_STATUS(kStatusGroup_Generic, 1),
  kStatus_ReadOnly = MAKE_STATUS(kStatusGroup_Generic, 2),
  kStatus_OutOfRange = MAKE_STATUS(kStatusGroup_Generic, 3),
  kStatus_InvalidArgument = MAKE_STATUS(kStatusGroup_Generic, 4),
  kStatus_Timeout = MAKE_STATUS(kStatusGroup_Generic, 5),
  kStatus_NoTransferInProgress,
  kStatus_Busy = MAKE_STATUS(kStatusGroup_Generic, 7),
  kStatus_NoData
}
 Generic status return codes. More...
 

Functions

void * SDK_Malloc (size_t size, size_t alignbytes)
 Allocate memory with given alignment and aligned size. More...
 
void SDK_Free (void *ptr)
 Free memory. More...
 
void SDK_DelayAtLeastUs (uint32_t delayTime_us, uint32_t coreClock_Hz)
 Delay at least for some time. More...
 
static status_t EnableIRQ (IRQn_Type interrupt)
 Enable specific interrupt. More...
 
static status_t DisableIRQ (IRQn_Type interrupt)
 Disable specific interrupt. More...
 
static status_t EnableIRQWithPriority (IRQn_Type interrupt, uint8_t priNum)
 Enable the IRQ, and also set the interrupt priority. More...
 
static status_t IRQ_SetPriority (IRQn_Type interrupt, uint8_t priNum)
 Set the IRQ priority. More...
 
static status_t IRQ_ClearPendingIRQ (IRQn_Type interrupt)
 Clear the pending IRQ flag. More...
 
static uint32_t DisableGlobalIRQ (void)
 Disable the global IRQ. More...
 
static void EnableGlobalIRQ (uint32_t primask)
 Enable the global IRQ. More...
 

Driver version

#define FSL_COMMON_DRIVER_VERSION   (MAKE_VERSION(2, 4, 1))
 common driver version. More...
 

Debug console type definition.

#define DEBUG_CONSOLE_DEVICE_TYPE_NONE   0U
 No debug console. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_UART   1U
 Debug console based on UART. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_LPUART   2U
 Debug console based on LPUART. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_LPSCI   3U
 Debug console based on LPSCI. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_USBCDC   4U
 Debug console based on USBCDC. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_FLEXCOMM   5U
 Debug console based on FLEXCOMM. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_IUART   6U
 Debug console based on i.MX UART. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_VUSART   7U
 Debug console based on LPC_VUSART. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_MINI_USART   8U
 Debug console based on LPC_USART. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_SWO   9U
 Debug console based on SWO. More...
 
#define DEBUG_CONSOLE_DEVICE_TYPE_QSCI   10U
 Debug console based on QSCI. More...
 

Min/max macros

#define MIN(a, b)   (((a) < (b)) ? (a) : (b))
 Computes the minimum of a and b. More...
 
#define MAX(a, b)   (((a) > (b)) ? (a) : (b))
 Computes the maximum of a and b. More...
 

UINT16_MAX/UINT32_MAX value

#define UINT16_MAX   ((uint16_t)-1)
 Max value of uint16_t type. More...
 
#define UINT32_MAX   ((uint32_t)-1)
 Max value of uint32_t type. More...
 

Atomic modification

These macros are used for atomic access, such as read-modify-write to the peripheral registers.

Take SDK_ATOMIC_LOCAL_CLEAR_AND_SET as an example: the parameter addr means the address of the peripheral register or variable you want to modify atomically, the parameter clearBits is the bits to clear, the parameter setBits it the bits to set. For example, to set a 32-bit register bit1:bit0 to 0b10, use like this:

volatile uint32_t * reg = (volatile uint32_t *)REG_ADDR;

In this example, the register bit1:bit0 are cleared and bit1 is set, as a result, register bit1:bit0 = 0b10.

Note
For the platforms don't support exclusive load and store, these macros disable the global interrupt to pretect the modification.
These macros only guarantee the local processor atomic operations. For the multi-processor devices, use hardware semaphore such as SEMA42 to guarantee exclusive access if necessary.
#define SDK_ATOMIC_LOCAL_ADD(addr, val)
 Add value val from the variable at address address.
 
#define SDK_ATOMIC_LOCAL_SUB(addr, val)
 Subtract value val to the variable at address address.
 
#define SDK_ATOMIC_LOCAL_SET(addr, bits)
 Set the bits specifiled by bits to the variable at address address.
 
#define SDK_ATOMIC_LOCAL_CLEAR(addr, bits)
 Clear the bits specifiled by bits to the variable at address address.
 
#define SDK_ATOMIC_LOCAL_TOGGLE(addr, bits)
 Toggle the bits specifiled by bits to the variable at address address.
 
#define SDK_ATOMIC_LOCAL_CLEAR_AND_SET(addr, clearBits, setBits)
 For the variable at address address, clear the bits specifiled by clearBits and set the bits specifiled by setBits.
 

Timer utilities

#define USEC_TO_COUNT(us, clockFreqInHz)   (uint64_t)(((uint64_t)(us) * (clockFreqInHz)) / 1000000U)
 Macro to convert a microsecond period to raw count value.
 
#define COUNT_TO_USEC(count, clockFreqInHz)   (uint64_t)((uint64_t)(count)*1000000U / (clockFreqInHz))
 Macro to convert a raw count value to microsecond.
 
#define MSEC_TO_COUNT(ms, clockFreqInHz)   (uint64_t)((uint64_t)(ms) * (clockFreqInHz) / 1000U)
 Macro to convert a millisecond period to raw count value.
 
#define COUNT_TO_MSEC(count, clockFreqInHz)   (uint64_t)((uint64_t)(count)*1000U / (clockFreqInHz))
 Macro to convert a raw count value to millisecond.
 

Alignment variable definition macros

#define SDK_ALIGN(var, alignbytes)   var __attribute__((aligned(alignbytes)))
 Macro to define a variable with alignbytes alignment.
 
#define SDK_L1DCACHE_ALIGN(var)   SDK_ALIGN(var, FSL_FEATURE_L1DCACHE_LINESIZE_BYTE)
 Macro to define a variable with L1 d-cache line size alignment.
 
#define SDK_SIZEALIGN(var, alignbytes)   ((unsigned int)((var) + ((alignbytes)-1U)) & (unsigned int)(~(unsigned int)((alignbytes)-1U)))
 Macro to define a variable with L2 cache line size alignment. More...
 

Non-cacheable region definition macros

For initialized non-zero non-cacheable variables, please use "AT_NONCACHEABLE_SECTION_INIT(var) ={xx};" or "AT_NONCACHEABLE_SECTION_ALIGN_INIT(var) ={xx};" in your projects to define them.

For zero-inited non-cacheable variables, please use "AT_NONCACHEABLE_SECTION(var);" or "AT_NONCACHEABLE_SECTION_ALIGN(var);" to define them, these zero-inited variables will be initialized to zero in system startup.

Note
For GCC, when the non-cacheable section is required, please define "__STARTUP_INITIALIZE_NONCACHEDATA" in your projects to make sure the non-cacheable section variables will be initialized in system startup.
#define AT_NONCACHEABLE_SECTION(var)   __attribute__((section("NonCacheable,\"aw\",%nobits @"))) var
 Define a variable var, and place it in non-cacheable section.
 
#define AT_NONCACHEABLE_SECTION_ALIGN(var, alignbytes)   __attribute__((section("NonCacheable,\"aw\",%nobits @"))) var __attribute__((aligned(alignbytes)))
 Define a variable var, and place it in non-cacheable section, the start address of the variable is aligned to alignbytes.
 
#define AT_NONCACHEABLE_SECTION_INIT(var)   __attribute__((section("NonCacheable.init"))) var
 Define a variable var with initial value, and place it in non-cacheable section.
 
#define AT_NONCACHEABLE_SECTION_ALIGN_INIT(var, alignbytes)   __attribute__((section("NonCacheable.init"))) var __attribute__((aligned(alignbytes)))
 Define a variable var with initial value, and place it in non-cacheable section, the start address of the variable is aligned to alignbytes.
 

Time sensitive region

#define AT_QUICKACCESS_SECTION_CODE(func)   __attribute__((section("CodeQuickAccess"), __noinline__)) func
 Place function in a section which can be accessed quickly by core.
 
#define AT_QUICKACCESS_SECTION_DATA(var)   __attribute__((section("DataQuickAccess"))) var
 Place data in a section which can be accessed quickly by core.
 
#define AT_QUICKACCESS_SECTION_DATA_ALIGN(var, alignbytes)   __attribute__((section("DataQuickAccess"))) var __attribute__((aligned(alignbytes)))
 Place data in a section which can be accessed quickly by core, and the variable address is set to align with alignbytes.
 

Ram Function

#define RAMFUNCTION_SECTION_CODE(func)   __attribute__((section("RamFunction"))) func
 Place function in ram.
 

Macro Definition Documentation

#define FSL_DRIVER_TRANSFER_DOUBLE_WEAK_IRQ   1
#define MAKE_STATUS (   group,
  code 
)    ((((group)*100L) + (code)))
#define MAKE_VERSION (   major,
  minor,
  bugfix 
)    (((major)*65536L) + ((minor)*256L) + (bugfix))

The driver version is a 32-bit number, for both 32-bit platforms(such as Cortex M) and 16-bit platforms(such as DSC).

| Unused    || Major Version || Minor Version ||  Bug Fix    |
31        25  24           17  16            9  8            0
#define FSL_COMMON_DRIVER_VERSION   (MAKE_VERSION(2, 4, 1))
#define DEBUG_CONSOLE_DEVICE_TYPE_NONE   0U
#define DEBUG_CONSOLE_DEVICE_TYPE_UART   1U
#define DEBUG_CONSOLE_DEVICE_TYPE_LPUART   2U
#define DEBUG_CONSOLE_DEVICE_TYPE_LPSCI   3U
#define DEBUG_CONSOLE_DEVICE_TYPE_USBCDC   4U
#define DEBUG_CONSOLE_DEVICE_TYPE_FLEXCOMM   5U
#define DEBUG_CONSOLE_DEVICE_TYPE_IUART   6U
#define DEBUG_CONSOLE_DEVICE_TYPE_VUSART   7U
#define DEBUG_CONSOLE_DEVICE_TYPE_MINI_USART   8U
#define DEBUG_CONSOLE_DEVICE_TYPE_SWO   9U
#define DEBUG_CONSOLE_DEVICE_TYPE_QSCI   10U
#define MIN (   a,
 
)    (((a) < (b)) ? (a) : (b))
#define MAX (   a,
 
)    (((a) > (b)) ? (a) : (b))
#define ARRAY_SIZE (   x)    (sizeof(x) / sizeof((x)[0]))
#define UINT16_MAX   ((uint16_t)-1)
#define UINT32_MAX   ((uint32_t)-1)
#define SUPPRESS_FALL_THROUGH_WARNING ( )

To suppress this warning, "SUPPRESS_FALL_THROUGH_WARNING();" need to be added at the end of each case section which misses "break;"statement.

#define SDK_SIZEALIGN (   var,
  alignbytes 
)    ((unsigned int)((var) + ((alignbytes)-1U)) & (unsigned int)(~(unsigned int)((alignbytes)-1U)))

Macro to change a value to a given size aligned value

Typedef Documentation

typedef int32_t status_t

Enumeration Type Documentation

Enumerator
kStatusGroup_Generic 

Group number for generic status codes.

kStatusGroup_FLASH 

Group number for FLASH status codes.

kStatusGroup_LPSPI 

Group number for LPSPI status codes.

kStatusGroup_FLEXIO_SPI 

Group number for FLEXIO SPI status codes.

kStatusGroup_DSPI 

Group number for DSPI status codes.

kStatusGroup_FLEXIO_UART 

Group number for FLEXIO UART status codes.

kStatusGroup_FLEXIO_I2C 

Group number for FLEXIO I2C status codes.

kStatusGroup_LPI2C 

Group number for LPI2C status codes.

kStatusGroup_UART 

Group number for UART status codes.

kStatusGroup_I2C 

Group number for UART status codes.

kStatusGroup_LPSCI 

Group number for LPSCI status codes.

kStatusGroup_LPUART 

Group number for LPUART status codes.

kStatusGroup_SPI 

Group number for SPI status code.

kStatusGroup_XRDC 

Group number for XRDC status code.

kStatusGroup_SEMA42 

Group number for SEMA42 status code.

kStatusGroup_SDHC 

Group number for SDHC status code.

kStatusGroup_SDMMC 

Group number for SDMMC status code.

kStatusGroup_SAI 

Group number for SAI status code.

kStatusGroup_MCG 

Group number for MCG status codes.

kStatusGroup_SCG 

Group number for SCG status codes.

kStatusGroup_SDSPI 

Group number for SDSPI status codes.

kStatusGroup_FLEXIO_I2S 

Group number for FLEXIO I2S status codes.

kStatusGroup_FLEXIO_MCULCD 

Group number for FLEXIO LCD status codes.

kStatusGroup_FLASHIAP 

Group number for FLASHIAP status codes.

kStatusGroup_FLEXCOMM_I2C 

Group number for FLEXCOMM I2C status codes.

kStatusGroup_I2S 

Group number for I2S status codes.

kStatusGroup_IUART 

Group number for IUART status codes.

kStatusGroup_CSI 

Group number for CSI status codes.

kStatusGroup_MIPI_DSI 

Group number for MIPI DSI status codes.

kStatusGroup_SDRAMC 

Group number for SDRAMC status codes.

kStatusGroup_POWER 

Group number for POWER status codes.

kStatusGroup_ENET 

Group number for ENET status codes.

kStatusGroup_PHY 

Group number for PHY status codes.

kStatusGroup_TRGMUX 

Group number for TRGMUX status codes.

kStatusGroup_SMARTCARD 

Group number for SMARTCARD status codes.

kStatusGroup_LMEM 

Group number for LMEM status codes.

kStatusGroup_QSPI 

Group number for QSPI status codes.

kStatusGroup_DMA 

Group number for DMA status codes.

kStatusGroup_EDMA 

Group number for EDMA status codes.

kStatusGroup_DMAMGR 

Group number for DMAMGR status codes.

kStatusGroup_FLEXCAN 

Group number for FlexCAN status codes.

kStatusGroup_LTC 

Group number for LTC status codes.

kStatusGroup_FLEXIO_CAMERA 

Group number for FLEXIO CAMERA status codes.

kStatusGroup_LPC_SPI 

Group number for LPC_SPI status codes.

kStatusGroup_LPC_USART 

Group number for LPC_USART status codes.

kStatusGroup_DMIC 

Group number for DMIC status codes.

kStatusGroup_SDIF 

Group number for SDIF status codes.

kStatusGroup_SPIFI 

Group number for SPIFI status codes.

kStatusGroup_OTP 

Group number for OTP status codes.

kStatusGroup_MCAN 

Group number for MCAN status codes.

kStatusGroup_CAAM 

Group number for CAAM status codes.

kStatusGroup_ECSPI 

Group number for ECSPI status codes.

kStatusGroup_USDHC 

Group number for USDHC status codes.

kStatusGroup_LPC_I2C 

Group number for LPC_I2C status codes.

kStatusGroup_DCP 

Group number for DCP status codes.

kStatusGroup_MSCAN 

Group number for MSCAN status codes.

kStatusGroup_ESAI 

Group number for ESAI status codes.

kStatusGroup_FLEXSPI 

Group number for FLEXSPI status codes.

kStatusGroup_MMDC 

Group number for MMDC status codes.

kStatusGroup_PDM 

Group number for MIC status codes.

kStatusGroup_SDMA 

Group number for SDMA status codes.

kStatusGroup_ICS 

Group number for ICS status codes.

kStatusGroup_SPDIF 

Group number for SPDIF status codes.

kStatusGroup_LPC_MINISPI 

Group number for LPC_MINISPI status codes.

kStatusGroup_HASHCRYPT 

Group number for Hashcrypt status codes.

kStatusGroup_LPC_SPI_SSP 

Group number for LPC_SPI_SSP status codes.

kStatusGroup_I3C 

Group number for I3C status codes.

kStatusGroup_LPC_I2C_1 

Group number for LPC_I2C_1 status codes.

kStatusGroup_NOTIFIER 

Group number for NOTIFIER status codes.

kStatusGroup_DebugConsole 

Group number for debug console status codes.

kStatusGroup_SEMC 

Group number for SEMC status codes.

kStatusGroup_ApplicationRangeStart 

Starting number for application groups.

kStatusGroup_IAP 

Group number for IAP status codes.

kStatusGroup_SFA 

Group number for SFA status codes.

kStatusGroup_SPC 

Group number for SPC status codes.

kStatusGroup_PUF 

Group number for PUF status codes.

kStatusGroup_TOUCH_PANEL 

Group number for touch panel status codes.

kStatusGroup_VBAT 

Group number for VBAT status codes.

kStatusGroup_XSPI 

Group number for XSPI status codes.

kStatusGroup_PNGDEC 

Group number for PNGDEC status codes.

kStatusGroup_JPEGDEC 

Group number for JPEGDEC status codes.

kStatusGroup_HAL_GPIO 

Group number for HAL GPIO status codes.

kStatusGroup_HAL_UART 

Group number for HAL UART status codes.

kStatusGroup_HAL_TIMER 

Group number for HAL TIMER status codes.

kStatusGroup_HAL_SPI 

Group number for HAL SPI status codes.

kStatusGroup_HAL_I2C 

Group number for HAL I2C status codes.

kStatusGroup_HAL_FLASH 

Group number for HAL FLASH status codes.

kStatusGroup_HAL_PWM 

Group number for HAL PWM status codes.

kStatusGroup_HAL_RNG 

Group number for HAL RNG status codes.

kStatusGroup_HAL_I2S 

Group number for HAL I2S status codes.

kStatusGroup_HAL_ADC_SENSOR 

Group number for HAL ADC SENSOR status codes.

kStatusGroup_TIMERMANAGER 

Group number for TiMER MANAGER status codes.

kStatusGroup_SERIALMANAGER 

Group number for SERIAL MANAGER status codes.

kStatusGroup_LED 

Group number for LED status codes.

kStatusGroup_BUTTON 

Group number for BUTTON status codes.

kStatusGroup_EXTERN_EEPROM 

Group number for EXTERN EEPROM status codes.

kStatusGroup_SHELL 

Group number for SHELL status codes.

kStatusGroup_MEM_MANAGER 

Group number for MEM MANAGER status codes.

kStatusGroup_LIST 

Group number for List status codes.

kStatusGroup_OSA 

Group number for OSA status codes.

kStatusGroup_COMMON_TASK 

Group number for Common task status codes.

kStatusGroup_MSG 

Group number for messaging status codes.

kStatusGroup_SDK_OCOTP 

Group number for OCOTP status codes.

kStatusGroup_SDK_FLEXSPINOR 

Group number for FLEXSPINOR status codes.

kStatusGroup_CODEC 

Group number for codec status codes.

kStatusGroup_ASRC 

Group number for codec status ASRC.

kStatusGroup_OTFAD 

Group number for codec status codes.

kStatusGroup_SDIOSLV 

Group number for SDIOSLV status codes.

kStatusGroup_MECC 

Group number for MECC status codes.

kStatusGroup_ENET_QOS 

Group number for ENET_QOS status codes.

kStatusGroup_LOG 

Group number for LOG status codes.

kStatusGroup_I3CBUS 

Group number for I3CBUS status codes.

kStatusGroup_QSCI 

Group number for QSCI status codes.

kStatusGroup_ELEMU 

Group number for ELEMU status codes.

kStatusGroup_QUEUEDSPI 

Group number for QSPI status codes.

kStatusGroup_POWER_MANAGER 

Group number for POWER_MANAGER status codes.

kStatusGroup_IPED 

Group number for IPED status codes.

kStatusGroup_ELS_PKC 

Group number for ELS PKC status codes.

kStatusGroup_CSS_PKC 

Group number for CSS PKC status codes.

kStatusGroup_HOSTIF 

Group number for HOSTIF status codes.

kStatusGroup_CLIF 

Group number for CLIF status codes.

kStatusGroup_BMA 

Group number for BMA status codes.

kStatusGroup_NETC 

Group number for NETC status codes.

kStatusGroup_ELE 

Group number for ELE status codes.

kStatusGroup_GLIKEY 

Group number for GLIKEY status codes.

anonymous enum
Enumerator
kStatus_Success 

Generic status for Success.

kStatus_Fail 

Generic status for Fail.

kStatus_ReadOnly 

Generic status for read only failure.

kStatus_OutOfRange 

Generic status for out of range access.

kStatus_InvalidArgument 

Generic status for invalid argument check.

kStatus_Timeout 

Generic status for timeout.

kStatus_NoTransferInProgress 

Generic status for no transfer in progress.

kStatus_Busy 

Generic status for module is busy.

kStatus_NoData 

Generic status for no data is found for the operation.

Function Documentation

void* SDK_Malloc ( size_t  size,
size_t  alignbytes 
)

This is provided to support the dynamically allocated memory used in cache-able region.

Parameters
sizeThe length required to malloc.
alignbytesThe alignment size.
Return values
Theallocated memory.
void SDK_Free ( void *  ptr)
Parameters
ptrThe memory to be release.
void SDK_DelayAtLeastUs ( uint32_t  delayTime_us,
uint32_t  coreClock_Hz 
)

Please note that, this API uses while loop for delay, different run-time environments make the time not precise, if precise delay count was needed, please implement a new delay function with hardware timer.

Parameters
delayTime_usDelay time in unit of microsecond.
coreClock_HzCore clock frequency with Hz.
static status_t EnableIRQ ( IRQn_Type  interrupt)
inlinestatic

Enable LEVEL1 interrupt. For some devices, there might be multiple interrupt levels. For example, there are NVIC and intmux. Here the interrupts connected to NVIC are the LEVEL1 interrupts, because they are routed to the core directly. The interrupts connected to intmux are the LEVEL2 interrupts, they are routed to NVIC first then routed to core.

This function only enables the LEVEL1 interrupts. The number of LEVEL1 interrupts is indicated by the feature macro FSL_FEATURE_NUMBER_OF_LEVEL1_INT_VECTORS.

Parameters
interruptThe IRQ number.
Return values
kStatus_SuccessInterrupt enabled successfully
kStatus_FailFailed to enable the interrupt
static status_t DisableIRQ ( IRQn_Type  interrupt)
inlinestatic

Disable LEVEL1 interrupt. For some devices, there might be multiple interrupt levels. For example, there are NVIC and intmux. Here the interrupts connected to NVIC are the LEVEL1 interrupts, because they are routed to the core directly. The interrupts connected to intmux are the LEVEL2 interrupts, they are routed to NVIC first then routed to core.

This function only disables the LEVEL1 interrupts. The number of LEVEL1 interrupts is indicated by the feature macro FSL_FEATURE_NUMBER_OF_LEVEL1_INT_VECTORS.

Parameters
interruptThe IRQ number.
Return values
kStatus_SuccessInterrupt disabled successfully
kStatus_FailFailed to disable the interrupt
static status_t EnableIRQWithPriority ( IRQn_Type  interrupt,
uint8_t  priNum 
)
inlinestatic

Only handle LEVEL1 interrupt. For some devices, there might be multiple interrupt levels. For example, there are NVIC and intmux. Here the interrupts connected to NVIC are the LEVEL1 interrupts, because they are routed to the core directly. The interrupts connected to intmux are the LEVEL2 interrupts, they are routed to NVIC first then routed to core.

This function only handles the LEVEL1 interrupts. The number of LEVEL1 interrupts is indicated by the feature macro FSL_FEATURE_NUMBER_OF_LEVEL1_INT_VECTORS.

Parameters
interruptThe IRQ to Enable.
priNumPriority number set to interrupt controller register.
Return values
kStatus_SuccessInterrupt priority set successfully
kStatus_FailFailed to set the interrupt priority.
static status_t IRQ_SetPriority ( IRQn_Type  interrupt,
uint8_t  priNum 
)
inlinestatic

Only handle LEVEL1 interrupt. For some devices, there might be multiple interrupt levels. For example, there are NVIC and intmux. Here the interrupts connected to NVIC are the LEVEL1 interrupts, because they are routed to the core directly. The interrupts connected to intmux are the LEVEL2 interrupts, they are routed to NVIC first then routed to core.

This function only handles the LEVEL1 interrupts. The number of LEVEL1 interrupts is indicated by the feature macro FSL_FEATURE_NUMBER_OF_LEVEL1_INT_VECTORS.

Parameters
interruptThe IRQ to set.
priNumPriority number set to interrupt controller register.
Return values
kStatus_SuccessInterrupt priority set successfully
kStatus_FailFailed to set the interrupt priority.
static status_t IRQ_ClearPendingIRQ ( IRQn_Type  interrupt)
inlinestatic

Only handle LEVEL1 interrupt. For some devices, there might be multiple interrupt levels. For example, there are NVIC and intmux. Here the interrupts connected to NVIC are the LEVEL1 interrupts, because they are routed to the core directly. The interrupts connected to intmux are the LEVEL2 interrupts, they are routed to NVIC first then routed to core.

This function only handles the LEVEL1 interrupts. The number of LEVEL1 interrupts is indicated by the feature macro FSL_FEATURE_NUMBER_OF_LEVEL1_INT_VECTORS.

Parameters
interruptThe flag which IRQ to clear.
Return values
kStatus_SuccessInterrupt priority set successfully
kStatus_FailFailed to set the interrupt priority.
static uint32_t DisableGlobalIRQ ( void  )
inlinestatic

Disable the global interrupt and return the current primask register. User is required to provided the primask register for the EnableGlobalIRQ().

Returns
Current primask value.
static void EnableGlobalIRQ ( uint32_t  primask)
inlinestatic

Set the primask register with the provided primask value but not just enable the primask. The idea is for the convenience of integration of RTOS. some RTOS get its own management mechanism of primask. User is required to use the EnableGlobalIRQ() and DisableGlobalIRQ() in pair.

Parameters
primaskvalue of primask register to be restored. The primask value is supposed to be provided by the DisableGlobalIRQ().