MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
EQDC: Enhanced Quadrature Encoder/Decoder

Overview

The MCUXpresso SDK provides a peripheral driver for the Enhanced Quadrature Encoder/Decoder () module of MCUXpresso SDK devices.

This section describes the programming interface of the EQDC Peripheral driver. The EQDC driver configures the EQDC module and provides a functional interface for the user to build the EQDC application.

Function groups

Initialization and De-initialization

This function group initializes default configuration structure for the EQDC counter and initializes EQDC counter with the normal configuration and de-initialize EQDC module. Some APIs are also created to control the features.

Status

This function group get/clear the EQDC status.

Interrupts

This function group enable/disable the EQDC interrupts.

Value Operation

This function group get the counter/hold value of positions.

Typical use case

Polling Configuration

Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/eqdc

Data Structures

struct  eqdc_config_t
 Define user configuration structure for EQDC module. More...
 

Macros

#define EQDC_CTRL_W1C_FLAGS   (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK)
 W1C bits in EQDC CTRL registers. More...
 
#define EQDC_INTCTRL_W1C_FLAGS
 W1C bits in EQDC INTCTRL registers. More...
 
#define EQDC_CTRL_INT_EN   (EQDC_CTRL_HIE_MASK | EQDC_CTRL_XIE_MASK | EQDC_CTRL_WDIE_MASK)
 Interrupt enable bits in EQDC CTRL registers. More...
 
#define EQDC_INTCTRL_INT_EN
 Interrupt enable bits in EQDC INTCTRL registers. More...
 
#define EQDC_CTRL_INT_FLAGS   (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK)
 Interrupt flag bits in EQDC CTRL registers. More...
 
#define EQDC_INTCTRL_INT_FLAGS
 Interrupt flag bits in EQDC INTCTRL registers. More...
 

Enumerations

enum  _eqdc_status_flags {
  kEQDC_HomeEnableTransitionFlag = EQDC_CTRL_HIRQ_MASK,
  kEQDC_IndexPresetPulseFlag = EQDC_CTRL_XIRQ_MASK,
  kEQDC_WatchdogTimeoutFlag = EQDC_CTRL_WDIRQ_MASK,
  kEQDC_SimultPhaseChangeFlag,
  kEQDC_CountDirectionChangeFlag,
  kEQDC_PositionRollOverFlag,
  kEQDC_PositionRollUnderFlag,
  kEQDC_PositionCompare0Flag,
  kEQDC_PositionCompare1Flag,
  kEQDC_PositionCompare2Flag,
  kEQDC_PositionCompare3Flag
}
 EQDC status flags, these flags indicate the counter's events. More...
 
enum  _eqdc_signal_status {
  kEQDC_SignalStatusRawHomeEnable = EQDC_IMR_HOME_ENABLE_MASK,
  kEQDC_SignalStatusRawIndexPreset = EQDC_IMR_INDEX_PRESET_MASK,
  kEQDC_SignalStatusRawPhaseB = EQDC_IMR_PHB_MASK,
  kEQDC_SignalStatusRawPhaseA = EQDC_IMR_PHA_MASK,
  kEQDC_SignalStatusFilteredHomeEnable = EQDC_IMR_FHOM_ENA_MASK,
  kEQDC_SignalStatusFilteredIndexPreset = EQDC_IMR_FIND_PRE_MASK,
  kEQDC_SignalStatusFilteredPhaseB = EQDC_IMR_FPHB_MASK,
  kEQDC_SignalStatusFilteredPhaseA = EQDC_IMR_FPHA_MASK,
  kEQDC_SignalStatusPositionCompare0Flag = EQDC_IMR_CMPF0_MASK,
  kEQDC_SignalStatusPositionCompare1Flag = EQDC_IMR_CMP1F_MASK,
  kEQDC_SignalStatusPositionCompare2Flag = EQDC_IMR_CMP2F_MASK,
  kEQDC_SignalStatusPositionCompare3Flag = EQDC_IMR_CMP3F_MASK,
  kEQDC_SignalStatusCountDirectionFlagHold = EQDC_IMR_DIRH_MASK,
  kEQDC_SignalStatusCountDirectionFlag = EQDC_IMR_DIR_MASK
}
 Signal status, these flags indicate the raw and filtered input signal status. More...
 
enum  _eqdc_interrupt_enable {
  kEQDC_HomeEnableTransitionInterruptEnable,
  kEQDC_IndexPresetPulseInterruptEnable = EQDC_CTRL_XIE_MASK,
  kEQDC_WatchdogTimeoutInterruptEnable = EQDC_CTRL_WDIE_MASK,
  kEQDC_SimultPhaseChangeInterruptEnable,
  kEQDC_CountDirectionChangeInterruptEnable,
  kEQDC_PositionRollOverInterruptEnable = (uint32_t)EQDC_INTCTRL_ROIE_MASK << 16U,
  kEQDC_PositionRollUnderInterruptEnable,
  kEQDC_PositionCompare0InterruptEnable,
  kEQDC_PositionCompare1InterruptEnable,
  kEQDC_PositionCompare2InterruptEnable,
  kEQDC_PositionCompare3InterruptEnable
}
 Interrupt enable/disable mask. More...
 
enum  eqdc_home_enable_init_pos_counter_mode_t {
  kEQDC_HomeInitPosCounterDisabled = 0U,
  kEQDC_HomeInitPosCounterOnRisingEdge = EQDC_CTRL_HIP_MASK,
  kEQDC_HomeInitPosCounterOnFallingEdge = EQDC_CTRL_HIP_MASK | EQDC_CTRL_HNE_MASK
}
 Define HOME/ENABLE signal's trigger mode. More...
 
enum  eqdc_index_preset_init_pos_counter_mode_t {
  kEQDC_IndexInitPosCounterDisabled = 0U,
  kEQDC_IndexInitPosCounterOnRisingEdge = EQDC_CTRL_XIP_MASK,
  kEQDC_IndexInitPosCounterOnFallingEdge = EQDC_CTRL_XIP_MASK | EQDC_CTRL_XNE_MASK
}
 Define INDEX/PRESET signal's trigger mode. More...
 
enum  eqdc_operate_mode_t {
  kEQDC_QuadratureDecodeOperationMode = 0U,
  kEQDC_QuadratureCountOperationMode,
  kEQDC_SinglePhaseDecodeOperationMode,
  kEQDC_SinglePhaseCountOperationMode
}
 Define type for decoder opertion mode. More...
 
enum  eqdc_count_mode_t {
  kEQDC_QuadratureX4 = 0U,
  kEQDC_QuadratureX2 = 1U,
  kEQDC_QuadratureX1 = 2U,
  kEQDC_UpDownPulseCount,
  kEQDC_SignedCountDoubleEdge,
  kEQDC_SignedCountSingleEdge
}
 Define type for decoder count mode. More...
 
enum  eqdc_output_pulse_mode_t {
  kEQDC_OutputPulseOnCounterEqualCompare = 0U,
  kEQDC_OutputPulseOnReadingPositionCounter
}
 Define type for the condition of POSMATCH pulses. More...
 
enum  eqdc_revolution_count_condition_t {
  kEQDC_RevolutionCountOnIndexPulse = 0U,
  kEQDC_RevolutionCountOnRollOverModulus
}
 Define type for determining how the revolution counter (REV) is incremented/decremented. More...
 
enum  eqdc_filter_sample_count_t {
  kEQDC_Filter3Samples = 0U,
  kEQDC_Filter4Samples = 1U,
  kEQDC_Filter5Samples = 2U,
  kEQDC_Filter6Samples = 3U,
  kEQDC_Filter7Samples = 4U,
  kEQDC_Filter8Samples = 5U,
  kEQDC_Filter9Samples = 6U,
  kEQDC_Filter10Samples = 7U
}
 Input Filter Sample Count. More...
 
enum  eqdc_count_direction_flag_t {
  kEQDC_CountDirectionDown = 0U,
  kEQDC_CountDirectionUp
}
 Count direction. More...
 
enum  eqdc_prescaler_t {
  kEQDC_Prescaler1 = 0U,
  kEQDC_Prescaler2 = 1U,
  kEQDC_Prescaler4 = 2U,
  kEQDC_Prescaler8 = 3U,
  kEQDC_Prescaler16 = 4U,
  kEQDC_Prescaler32 = 5U,
  kEQDC_Prescaler64 = 6U,
  kEQDC_Prescaler128 = 7U,
  kEQDC_Prescaler256 = 8U,
  kEQDC_Prescaler512 = 9U,
  kEQDC_Prescaler1024 = 10U,
  kEQDC_Prescaler2048 = 11U,
  kEQDC_Prescaler4096 = 12U,
  kEQDC_Prescaler8192 = 13U,
  kEQDC_Prescaler16384 = 14U,
  kEQDC_Prescaler32768 = 15U
}
 Prescaler used by Last Edge Time (LASTEDGE) and Position Difference Period Counter (POSDPER). More...
 

Initialization and deinitialization Interfaces

void EQDC_Init (EQDC_Type *base, const eqdc_config_t *psConfig)
 Initializes the EQDC module. More...
 
void EQDC_GetDefaultConfig (eqdc_config_t *psConfig)
 Gets an available pre-defined configuration. More...
 
void EQDC_Deinit (EQDC_Type *base)
 De-initializes the EQDC module. More...
 
void EQDC_SetOperateMode (EQDC_Type *base, eqdc_operate_mode_t operateMode)
 Initializes the mode of operation. More...
 
static void EQDC_SetCountMode (EQDC_Type *base, eqdc_count_mode_t countMode)
 Initializes the mode of count. More...
 

Watchdog

static void EQDC_EnableWatchdog (EQDC_Type *base, bool bEnable)
 Enable watchdog for EQDC module. More...
 
static void EQDC_SetWatchdogTimeout (EQDC_Type *base, uint16_t u16Timeout)
 Set watchdog timeout value. More...
 

DMA

static void EQDC_EnableDMA (EQDC_Type *base, bool bEnable)
 Enable DMA for EQDC module. More...
 

Double-set Registers Loading Operation

static void EQDC_SetBufferedRegisterLoadUpdateMode (EQDC_Type *base)
 Set Buffered Register Load (Update) Mode. More...
 
static void EQDC_ClearBufferedRegisterLoadUpdateMode (EQDC_Type *base)
 Clear Buffered Register Load (Update) Mode. More...
 
static void EQDC_SetEqdcLdok (EQDC_Type *base)
 Set load okay. More...
 
static uint8_t EQDC_GetEqdcLdok (EQDC_Type *base)
 Get load okay. More...
 
static void EQDC_ClearEqdcLdok (EQDC_Type *base)
 Clear load okay. More...
 

Status

static uint32_t EQDC_GetStatusFlags (EQDC_Type *base)
 Get the status flags. More...
 
static void EQDC_ClearStatusFlags (EQDC_Type *base, uint32_t u32Flags)
 Clear the status flags. More...
 
static uint16_t EQDC_GetSignalStatusFlags (EQDC_Type *base)
 Get the signals' real-time status. More...
 
static eqdc_count_direction_flag_t EQDC_GetLastCountDirection (EQDC_Type *base)
 Get the direction of the last count. More...
 

Interrupts

static void EQDC_EnableInterrupts (EQDC_Type *base, uint32_t u32Interrupts)
 Enable the interrupts. More...
 
static void EQDC_DisableInterrupts (EQDC_Type *base, uint32_t u32Interrupts)
 Disable the interrupts. More...
 

Counter Operation

static void EQDC_DoSoftwareLoadInitialPositionValue (EQDC_Type *base)
 Load the initial position value to position counter. More...
 
static void EQDC_SetInitialPositionValue (EQDC_Type *base, uint32_t u32PositionInitValue)
 Set initial position value for EQDC module. More...
 
static void EQDC_SetPositionCounterValue (EQDC_Type *base, uint32_t positionCounterValue)
 Set position counter value. More...
 
static void EQDC_SetPositionModulusValue (EQDC_Type *base, uint32_t positionModulusValue)
 Set position counter modulus value. More...
 
static void EQDC_SetPositionCompare0Value (EQDC_Type *base, uint32_t u32PositionComp0Value)
 Set position counter compare 0 value. More...
 
static void EQDC_SetPositionCompare1Value (EQDC_Type *base, uint32_t u32PositionComp1Value)
 Set position counter compare 1 value. More...
 
static void EQDC_SetPositionCompare2Value (EQDC_Type *base, uint32_t u32PositionComp2Value)
 Set position counter compare 2 value. More...
 
static void EQDC_SetPositionCompare3Value (EQDC_Type *base, uint32_t u32PositionComp3Value)
 Set position counter compare 3 value. More...
 
static uint32_t EQDC_GetPosition (EQDC_Type *base)
 Get the current position counter's value. More...
 
static uint32_t EQDC_GetHoldPosition (EQDC_Type *base)
 Get the hold position counter's value. More...
 
static uint32_t EQDC_GetHoldPosition1 (EQDC_Type *base)
 Get the hold position counter1's value. More...
 
static uint32_t EQDC_GetHoldPosition2 (EQDC_Type *base)
 Get the hold position counter2's value. More...
 
static uint32_t EQDC_GetHoldPosition3 (EQDC_Type *base)
 Get the hold position counter3's value. More...
 
static uint16_t EQDC_GetPositionDifference (EQDC_Type *base)
 Get the position difference counter's value. More...
 
static uint16_t EQDC_GetHoldPositionDifference (EQDC_Type *base)
 Get the hold position difference counter's value. More...
 
static uint16_t EQDC_GetRevolution (EQDC_Type *base)
 Get the revolution counter's value. More...
 
static uint16_t EQDC_GetHoldRevolution (EQDC_Type *base)
 Get the hold revolution counter's value. More...
 
static uint16_t EQDC_GetLastEdgeTime (EQDC_Type *base)
 Get the last edge time. More...
 
static uint16_t EQDC_GetHoldLastEdgeTime (EQDC_Type *base)
 Get the hold last edge time. More...
 
static uint16_t EQDC_GetPositionDifferencePeriod (EQDC_Type *base)
 Get the Position Difference Period counter value. More...
 
static uint16_t EQDC_GetBufferedPositionDifferencePeriod (EQDC_Type *base)
 Get buffered Position Difference Period counter value. More...
 
static uint16_t EQDC_GetHoldPositionDifferencePeriod (EQDC_Type *base)
 Get Hold Position Difference Period counter value. More...
 

Data Structure Documentation

struct eqdc_config_t

Data Fields

bool enableReverseDirection
 Enable reverse direction counting. More...
 
bool countOnce
 Selects modulo loop or one shot counting mode. More...
 
bool enableDma
 Enable DMA for new written buffer values of COMPx/INIT/MOD(x range is 0-3)
 
bool bufferedRegisterLoadMode
 selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). More...
 
bool enableTriggerInitPositionCounter
 
Initialize position counter with initial register(UINIT, LINIT) value

on TRIGGER's rising edge. More...

 
bool enableIndexInitPositionCounter
 Enables the feature that the position counter to be initialized by Index Event Edge Mark. More...
 
bool enableTriggerClearPositionRegisters
 Clear position counter(POS), revolution counter(REV), position difference counter (POSD) on TRIGGER's rising edge. More...
 
bool enableTriggerHoldPositionRegisters
 Load position counter(POS), revolution counter(REV), position difference counter (POSD) values to hold registers on TRIGGER's rising edge. More...
 
bool filterPhaseA
 Filter operation on PHASEA input, when write 1, it means filter for PHASEA input is bypassed. More...
 
bool filterPhaseB
 Filter operation on PHASEB input, when write 1, it means filter for PHASEB input is bypassed. More...
 
bool filterIndPre
 Filter operation on INDEX/PRESET input, when write 1, it means filter for INDEX/PRESET input is bypassed. More...
 
bool filterHomEna
 Filter operation on HOME/ENABLE input, when write 1, it means filter for HOME/ENABLE input is bypassed. More...
 
bool enableWatchdog
 Enable the watchdog to detect if the target is moving or not. More...
 
uint16_t watchdogTimeoutValue
 Watchdog timeout count value. More...
 
eqdc_prescaler_t prescaler
 Prescaler. More...
 
bool filterClockSourceselection
 Filter Clock Source selection. More...
 
eqdc_filter_sample_count_t filterSampleCount
 Input Filter Sample Count. More...
 
uint8_t filterSamplePeriod
 Input Filter Sample Period. More...
 
eqdc_operate_mode_t operateMode
 Selects operation mode. More...
 
eqdc_count_mode_t countMode
 Selects count mode. More...
 
eqdc_home_enable_init_pos_counter_mode_t homeEnableInitPosCounterMode
 
            Select how HOME/Enable signal used to

initialize position counters. More...

 
eqdc_index_preset_init_pos_counter_mode_t indexPresetInitPosCounterMode
 
            Select how INDEX/Preset signal used

to initialize position counters. More...

 
eqdc_output_pulse_mode_t outputPulseMode
 The condition of POSMATCH pulses. More...
 
uint32_t positionCompareValue [4]
 Position compare 0 ~ 3 value. More...
 
eqdc_revolution_count_condition_t revolutionCountCondition
 Revolution Counter Modulus Enable. More...
 
uint32_t positionModulusValue
 Position modulus value. More...
 
uint32_t positionInitialValue
 Position initial value. More...
 
uint32_t positionCounterValue
 Position counter value. More...
 
bool enablePeriodMeasurement
 Enable period measurement. More...
 
uint16_t enabledInterruptsMask
 Mask of interrupts to be enabled, should be OR'ed value of _eqdc_interrupt_enable. More...
 

Field Documentation

bool eqdc_config_t::enableReverseDirection
bool eqdc_config_t::countOnce
bool eqdc_config_t::bufferedRegisterLoadMode
bool eqdc_config_t::enableTriggerInitPositionCounter
bool eqdc_config_t::enableIndexInitPositionCounter

This option works together with _eqdc_index_preset_init_pos_counter_mode and enableReverseDirection; If enabled, the behavior is like this:

When PHA leads PHB (Clockwise): If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnRisingEdge, then INDEX rising edge reset position counter. If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnFallingEdge, then INDEX falling edge reset position counter. If enableReverseDirection is false, then Reset position counter to initial value. If enableReverseDirection is true, then reset position counter to modulus value.

When PHA lags PHB (Counter Clockwise): If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnRisingEdge, then INDEX falling edge reset position counter. If _eqdc_index_preset_init_pos_counter_mode is kEQDC_IndexInitPosCounterOnFallingEdge, then INDEX rising edge reset position counter. If enableReverseDirection is false, then Reset position counter to modulus value. If enableReverseDirection is true, then reset position counter to initial value.

bool eqdc_config_t::enableTriggerClearPositionRegisters
bool eqdc_config_t::enableTriggerHoldPositionRegisters
bool eqdc_config_t::filterPhaseA
bool eqdc_config_t::filterPhaseB
bool eqdc_config_t::filterIndPre
bool eqdc_config_t::filterHomEna
bool eqdc_config_t::enableWatchdog
uint16_t eqdc_config_t::watchdogTimeoutValue

It stores the timeout count for the quadrature decoder module watchdog timer.

eqdc_prescaler_t eqdc_config_t::prescaler
bool eqdc_config_t::filterClockSourceselection
eqdc_filter_sample_count_t eqdc_config_t::filterSampleCount

This value should be chosen to reduce the probability of noisy samples causing an incorrect transition to be recognized. The value represent the number of consecutive samples that must agree prior to the input filter accepting an input transition.

uint8_t eqdc_config_t::filterSamplePeriod

This value should be set such that the sampling period is larger than the period of the expected noise. This value represents the sampling period (in IPBus clock cycles) of the decoder input signals. The available range is 0 - 255.

eqdc_operate_mode_t eqdc_config_t::operateMode
eqdc_count_mode_t eqdc_config_t::countMode
eqdc_home_enable_init_pos_counter_mode_t eqdc_config_t::homeEnableInitPosCounterMode
eqdc_index_preset_init_pos_counter_mode_t eqdc_config_t::indexPresetInitPosCounterMode
eqdc_output_pulse_mode_t eqdc_config_t::outputPulseMode
uint32_t eqdc_config_t::positionCompareValue[4]

The available value is a 32-bit number.

eqdc_revolution_count_condition_t eqdc_config_t::revolutionCountCondition
uint32_t eqdc_config_t::positionModulusValue

The available value is a 32-bit number.

uint32_t eqdc_config_t::positionInitialValue

The available value is a 32-bit number.

uint32_t eqdc_config_t::positionCounterValue

When Modulo mode enabled, the positionCounterValue should be in the range of positionInitialValue and positionModulusValue.

bool eqdc_config_t::enablePeriodMeasurement

When enabled, the position difference hold register (POSDH) is only updated when position difference register (POSD) is read.

uint16_t eqdc_config_t::enabledInterruptsMask

Macro Definition Documentation

#define EQDC_CTRL_W1C_FLAGS   (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK)
#define EQDC_INTCTRL_W1C_FLAGS
Value:
(EQDC_INTCTRL_SABIRQ_MASK | EQDC_INTCTRL_DIRIRQ_MASK | EQDC_INTCTRL_RUIRQ_MASK | EQDC_INTCTRL_ROIRQ_MASK | \
EQDC_INTCTRL_CMP0IRQ_MASK | EQDC_INTCTRL_CMP1IRQ_MASK | EQDC_INTCTRL_CMP2IRQ_MASK | EQDC_INTCTRL_CMP3IRQ_MASK)
#define EQDC_CTRL_INT_EN   (EQDC_CTRL_HIE_MASK | EQDC_CTRL_XIE_MASK | EQDC_CTRL_WDIE_MASK)
#define EQDC_INTCTRL_INT_EN
Value:
(EQDC_INTCTRL_SABIE_MASK | EQDC_INTCTRL_DIRIE_MASK | EQDC_INTCTRL_RUIE_MASK | EQDC_INTCTRL_ROIE_MASK | \
EQDC_INTCTRL_CMP0IE_MASK | EQDC_INTCTRL_CMP1IE_MASK | EQDC_INTCTRL_CMP2IE_MASK | EQDC_INTCTRL_CMP3IE_MASK)
#define EQDC_CTRL_INT_FLAGS   (EQDC_CTRL_HIRQ_MASK | EQDC_CTRL_XIRQ_MASK | EQDC_CTRL_WDIRQ_MASK)
#define EQDC_INTCTRL_INT_FLAGS
Value:
(EQDC_INTCTRL_SABIRQ_MASK | EQDC_INTCTRL_DIRIRQ_MASK | EQDC_INTCTRL_RUIRQ_MASK | EQDC_INTCTRL_ROIRQ_MASK | \
EQDC_INTCTRL_CMP0IRQ_MASK | EQDC_INTCTRL_CMP1IRQ_MASK | EQDC_INTCTRL_CMP2IRQ_MASK | EQDC_INTCTRL_CMP3IRQ_MASK)

Enumeration Type Documentation

Enumerator
kEQDC_HomeEnableTransitionFlag 

HOME/ENABLE signal transition occured.

kEQDC_IndexPresetPulseFlag 

INDEX/PRESET pulse occured.

kEQDC_WatchdogTimeoutFlag 

Watchdog timeout occured.

kEQDC_SimultPhaseChangeFlag 

Simultaneous change of PHASEA and PHASEB occured.

kEQDC_CountDirectionChangeFlag 

Count direction change interrupt enable.

kEQDC_PositionRollOverFlag 

Position counter rolls over from 0xFFFFFFFF to 0, or from MOD value to INIT value.

kEQDC_PositionRollUnderFlag 

Position register roll under from 0 to 0xFFFFFFFF, or from INIT value to MOD value.

kEQDC_PositionCompare0Flag 

Position counter match the COMP0 value.

kEQDC_PositionCompare1Flag 

Position counter match the COMP1 value.

kEQDC_PositionCompare2Flag 

Position counter match the COMP2 value.

kEQDC_PositionCompare3Flag 

Position counter match the COMP3 value.

Enumerator
kEQDC_SignalStatusRawHomeEnable 

Raw HOME/ENABLE input.

kEQDC_SignalStatusRawIndexPreset 

Raw INDEX/PRESET input.

kEQDC_SignalStatusRawPhaseB 

Raw PHASEB input.

kEQDC_SignalStatusRawPhaseA 

Raw PHASEA input.

kEQDC_SignalStatusFilteredHomeEnable 

The filtered HOME/ENABLE input.

kEQDC_SignalStatusFilteredIndexPreset 

The filtered INDEX/PRESET input.

kEQDC_SignalStatusFilteredPhaseB 

The filtered PHASEB input.

kEQDC_SignalStatusFilteredPhaseA 

The filtered PHASEA input.

kEQDC_SignalStatusPositionCompare0Flag 

Position Compare 0 Flag Output.

kEQDC_SignalStatusPositionCompare1Flag 

Position Compare 1 Flag Output.

kEQDC_SignalStatusPositionCompare2Flag 

Position Compare 2 Flag Output.

kEQDC_SignalStatusPositionCompare3Flag 

Position Compare 3 Flag Output.

kEQDC_SignalStatusCountDirectionFlagHold 

Count Direction Flag Hold.

kEQDC_SignalStatusCountDirectionFlag 

Count Direction Flag Output.

Enumerator
kEQDC_HomeEnableTransitionInterruptEnable 

HOME/ENABLE signal transition interrupt enable.

kEQDC_IndexPresetPulseInterruptEnable 

INDEX/PRESET pulse interrupt enable.

kEQDC_WatchdogTimeoutInterruptEnable 

Watchdog timeout interrupt enable.

kEQDC_SimultPhaseChangeInterruptEnable 

Simultaneous PHASEA and PHASEB change interrupt enable.

kEQDC_CountDirectionChangeInterruptEnable 

Count direction change interrupt enable.

kEQDC_PositionRollOverInterruptEnable 

Roll-over interrupt enable.

kEQDC_PositionRollUnderInterruptEnable 

Roll-under interrupt enable.

kEQDC_PositionCompare0InterruptEnable 

Position compare 0 interrupt enable.

kEQDC_PositionCompare1InterruptEnable 

Position compare 1 interrupt enable.

kEQDC_PositionCompare2InterruptEnable 

Position compare 2 interrupt enable.

kEQDC_PositionCompare3InterruptEnable 

Position compare 3 interrupt enable.

Enumerator
kEQDC_HomeInitPosCounterDisabled 

Don't use HOME/ENABLE signal to initialize the position counter.

kEQDC_HomeInitPosCounterOnRisingEdge 

Use positive going edge to trigger initialization of position counters.

kEQDC_HomeInitPosCounterOnFallingEdge 

Use negative going edge to trigger initialization of position counters.

Enumerator
kEQDC_IndexInitPosCounterDisabled 

INDEX/PRESET pulse does not initialize the position counter.

kEQDC_IndexInitPosCounterOnRisingEdge 

Use INDEX/PRESET pulse rising edge to initialize position counter.

kEQDC_IndexInitPosCounterOnFallingEdge 

Use INDEX/PRESET pulse falling edge to initialize position counter.

The Quadrature Decoder operates in following 4 operation modes: 1.Quadrature Decode(QDC) Operation Mode (CTRL[PH1] = 0,CTRL2[OPMODE] = 0) In QDC operation mode, Module uses PHASEA, PHASEB, INDEX, HOME, TRIGGER and ICAP[3:1] to decode the PHASEA and PHASEB signals from Speed/Position sensor. 2.Quadrature Count(QCT) Operation Mode (CTRL[PH1] = 0,CTRL2[OPMODE] = 1) In QCT operation mode, Module uses PHASEA, PHASEB, PRESET, ENABLE, TRIGGER and ICAP[3:1] to count the PHASEA and PHASEB signals from Speed/Position sensor. 3.Single Phase Decode(PH1DC) Operation Mode (CTRL[PH1] = 1,CTRL2[OPMODE] = 0) In PH1DC operation mode, the module uses PHASEA, PHASEB, INDEX, HOME, TRIGGER and ICAP[3:1] to decode the PHASEA and PHASEB signals from Speed/Position sensor. 4.Single Phase Count(PH1CT) Operation Mode (CTRL[PH1] = 1,CTRL2[OPMODE] = 1) In PH1CT operation mode, the module uses PHASEA, PHASEB, PRESET, ENABLE, TRIGGER and ICAP[3:1] to count the PHASEA and PHASEB signals from Speed/Position sensor.

Enumerator
kEQDC_QuadratureDecodeOperationMode 

Use standard quadrature decoder with PHASEA/PHASEB, INDEX/HOME.

kEQDC_QuadratureCountOperationMode 

Use quadrature count operation mode with PHASEA/PHASEB, PRESET/ENABLE.

kEQDC_SinglePhaseDecodeOperationMode 

Use single phase quadrature decoder with PHASEA/PHASEB, INDEX/HOME.

kEQDC_SinglePhaseCountOperationMode 

Use single phase count decoder with PHASEA/PHASEB, PRESET/ENABLE.

In decode mode, it uses the standard quadrature decoder with PHASEA and PHASEB, PHASEA = 0 and PHASEB = 0 mean reverse direction.

  • If PHASEA leads PHASEB, then motion is in the positive direction.
  • If PHASEA trails PHASEB,then motion is in the negative direction. In single phase mode, there are three count modes:
  • In Signed Count mode (Single Edge). Both position counter (POS) and position difference counter (POSD) count on the input PHASEA rising edge while the input PHASEB provides the selected position counter direction (up/down). If CTRL[REV] is 1, then the position counter will count in the opposite direction.
  • In Signed Count mode (double edge), both position counter (POS) and position difference counter (POSD) count the input PHASEA on both rising edge and falling edge while the input PHASEB provides the selected position counter direction (up/down).
  • In UP/DOWN Pulse Count mode. Both position counter (POS) and position difference counter (POSD) count in the up direction when input PHASEA rising edge occurs. Both counters count in the down direction when input PHASEB rising edge occurs. If CTRL[REV] is 1, then the position counter will count in the opposite direction.
Enumerator
kEQDC_QuadratureX4 

Active on kEQDC_QuadratureDecodeOperationMode/kEQDC_QuadratureCountOperationMode.

kEQDC_QuadratureX2 

Active on kEQDC_QuadratureDecodeOperationMode/kEQDC_QuadratureCountOperationMode.

kEQDC_QuadratureX1 

Active on kEQDC_QuadratureDecodeOperationMode/kEQDC_QuadratureCountOperationMode.

kEQDC_UpDownPulseCount 

Active on kEQDC_SinglePhaseDecodeOperationMode/kEQDC_SinglePhaseCountOperationMode.

kEQDC_SignedCountDoubleEdge 

Active on kEQDC_SinglePhaseDecodeOperationMode/kEQDC_SinglePhaseCountOperationMode.

kEQDC_SignedCountSingleEdge 

Active on kEQDC_SinglePhaseDecodeOperationMode/kEQDC_SinglePhaseCountOperationMode.

Enumerator
kEQDC_OutputPulseOnCounterEqualCompare 

POSMATCH pulses when a match occurs between the position counters (POS) and the compare value (UCOMPx/LCOMPx)(x range is 0-3).

kEQDC_OutputPulseOnReadingPositionCounter 

POSMATCH pulses when reading position counter(POS and LPOS), revolution counter(REV), position difference counter(POSD).

Enumerator
kEQDC_RevolutionCountOnIndexPulse 

Use INDEX pulse to increment/decrement revolution counter.

kEQDC_RevolutionCountOnRollOverModulus 

Use modulus counting roll-over/under to increment/decrement revolution counter.

The Input Filter Sample Count represents the number of consecutive samples that must agree, before the input filter accepts an input transition

Enumerator
kEQDC_Filter3Samples 

3 samples.

kEQDC_Filter4Samples 

4 samples.

kEQDC_Filter5Samples 

5 samples.

kEQDC_Filter6Samples 

6 samples.

kEQDC_Filter7Samples 

7 samples.

kEQDC_Filter8Samples 

8 samples.

kEQDC_Filter9Samples 

9 samples.

kEQDC_Filter10Samples 

10 samples.

Enumerator
kEQDC_CountDirectionDown 

Last count was in down direction.

kEQDC_CountDirectionUp 

Last count was in up direction.

Enumerator
kEQDC_Prescaler1 

Prescaler value 1.

kEQDC_Prescaler2 

Prescaler value 2.

kEQDC_Prescaler4 

Prescaler value 4.

kEQDC_Prescaler8 

Prescaler value 8.

kEQDC_Prescaler16 

Prescaler value 16.

kEQDC_Prescaler32 

Prescaler value 32.

kEQDC_Prescaler64 

Prescaler value 64.

kEQDC_Prescaler128 

Prescaler value 128.

kEQDC_Prescaler256 

Prescaler value 256.

kEQDC_Prescaler512 

Prescaler value 512.

kEQDC_Prescaler1024 

Prescaler value 1024.

kEQDC_Prescaler2048 

Prescaler value 2048.

kEQDC_Prescaler4096 

Prescaler value 4096.

kEQDC_Prescaler8192 

Prescaler value 8192.

kEQDC_Prescaler16384 

Prescaler value 16384.

kEQDC_Prescaler32768 

Prescaler value 32768.

Function Documentation

void EQDC_Init ( EQDC_Type *  base,
const eqdc_config_t *  psConfig 
)

This function initializes the EQDC by enabling the IP bus clock (optional).

Parameters
baseEQDC peripheral base address.
psConfigPointer to configuration structure.
void EQDC_GetDefaultConfig ( eqdc_config_t *  psConfig)

The default value are:

psConfig->enableReverseDirection = false;
psConfig->countOnce = false;
psConfig->operateMode = kEQDC_QuadratureDecodeOperationMode;
psConfig->countMode = kEQDC_QuadratureX4;
psConfig->homeEnableInitPosCounterMode = kEQDC_HomeInitPosCounterDisabled;
psConfig->indexPresetInitPosCounterMode = kEQDC_IndexInitPosCounterDisabled;
psConfig->enableIndexInitPositionCounter = false;
psConfig->enableDma = false;
psConfig->bufferedRegisterLoadMode = false;
psConfig->enableTriggerInitPositionCounter = false;
psConfig->enableTriggerClearPositionRegisters = false;
psConfig->enableTriggerHoldPositionRegisters = false;
psConfig->enableWatchdog = false;
psConfig->watchdogTimeoutValue = 0xFFFFU;
psConfig->filterPhaseA = 0U;
psConfig->filterPhaseB = 0U;
psConfig->filterIndPre = 0U;
psConfig->filterHomEna = 0U;
psConfig->filterClockSourceselection = false;
psConfig->filterSampleCount = kEQDC_Filter3Samples;
psConfig->filterSamplePeriod = 0U;
psConfig->outputPulseMode = kEQDC_OutputPulseOnCounterEqualCompare;
psConfig->positionCompareValue[0] = 0xFFFFFFFFU;
psConfig->positionCompareValue[1] = 0xFFFFFFFFU;
psConfig->positionCompareValue[2] = 0xFFFFFFFFU;
psConfig->positionCompareValue[3] = 0xFFFFFFFFU;
psConfig->revolutionCountCondition = kEQDC_RevolutionCountOnIndexPulse;
psConfig->positionModulusValue = 0U;
psConfig->positionInitialValue = 0U;
psConfig->positionCounterValue = 0U;
psConfig->enablePeriodMeasurement = false;
psConfig->prescaler = kEQDC_Prescaler1;
psConfig->enabledInterruptsMask = 0U;
Parameters
psConfigPointer to configuration structure.
void EQDC_Deinit ( EQDC_Type *  base)

This function deinitializes the EQDC by disabling the IP bus clock (optional).

Parameters
baseEQDC peripheral base address.
void EQDC_SetOperateMode ( EQDC_Type *  base,
eqdc_operate_mode_t  operateMode 
)

This function initializes mode of operation by enabling the IP bus clock (optional).

Parameters
baseEQDC peripheral base address.
operateModeSelect operation mode.
static void EQDC_SetCountMode ( EQDC_Type *  base,
eqdc_count_mode_t  countMode 
)
inlinestatic

These bits control the basic counting and behavior of Position Counter and Position Difference Counter. Setting CTRL[REV] to 1 can reverse the counting direction. 1.In quadrature Mode (CTRL[PH1] = 0): 00b - CM0: Normal/Reverse Quadrature X4 01b - CM1: Normal/Reverse Quadrature X2 10b - CM2: Normal/Reverse Quadrature X1 11b - CM3: Reserved 2.In Single Phase Mode (CTRL[PH1] = 1): 00b - CM0: UP/DOWN Pulse Count Mode 01b - CM1: Signed Mode, count PHASEA rising/falling edge, position counter counts up when PHASEB is low and counts down when PHASEB is high 10b - CM2: Signed Count Mode,count PHASEA rising edge only, position counter counts up when PHASEB is low and counts down when PHASEB is high 11b - CM3: Reserved

Parameters
baseEQDC peripheral base address.
countModeSelect count mode.
static void EQDC_EnableWatchdog ( EQDC_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseEQDC peripheral base address
bEnableEnables or disables the watchdog
static void EQDC_SetWatchdogTimeout ( EQDC_Type *  base,
uint16_t  u16Timeout 
)
inlinestatic
Parameters
baseEQDC peripheral base address
u16TimeoutNumber of clock cycles, plus one clock cycle that the watchdog timer counts before timing out
static void EQDC_EnableDMA ( EQDC_Type *  base,
bool  bEnable 
)
inlinestatic
Parameters
baseEQDC peripheral base address
bEnableEnables or disables the DMA
static void EQDC_SetBufferedRegisterLoadUpdateMode ( EQDC_Type *  base)
inlinestatic

This bit selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). Buffered registers are loaded and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.

Parameters
baseEQDC peripheral base address
static void EQDC_ClearBufferedRegisterLoadUpdateMode ( EQDC_Type *  base)
inlinestatic

Buffered Register Load (Update) Mode bit selects the loading time point of the buffered compare registers UCOMPx/LCOMPx, x=0~3, initial register (UINIT/LINIT), and modulus register (UMOD/LMOD). Buffered registers are loaded and take effect immediately upon CTRL[LDOK] is set.

Parameters
baseEQDC peripheral base address
static void EQDC_SetEqdcLdok ( EQDC_Type *  base)
inlinestatic

Load okay enables that the outer-set values of buffered compare registers (UCOMPx/LCOMPx, x=0~3), initial register(UINIT/LINIT) and modulus register(UMOD/LMOD) can be loaded into their inner-sets and take effect. When LDOK is set, this loading action occurs at the next position counter roll-over or roll-under if CTRL2[LDMOD] is set, or it occurs immediately if CTRL2[LDMOD] is cleared. LDOK is automatically cleared after the values in outer-set is loaded into the inner-set.

Parameters
baseEQDC peripheral base address.
static uint8_t EQDC_GetEqdcLdok ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
static void EQDC_ClearEqdcLdok ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
static uint32_t EQDC_GetStatusFlags ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
Returns
Logical OR'ed value of the status flags, _eqdc_status_flags.
static void EQDC_ClearStatusFlags ( EQDC_Type *  base,
uint32_t  u32Flags 
)
inlinestatic
Parameters
baseEQDC peripheral base address.
u32FlagsLogical OR'ed value of the flags to clear, _eqdc_status_flags.
static uint16_t EQDC_GetSignalStatusFlags ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
Returns
Logical OR'ed value of the real-time signal status, _eqdc_signal_status.
static eqdc_count_direction_flag_t EQDC_GetLastCountDirection ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
Returns
Direction of the last count.
static void EQDC_EnableInterrupts ( EQDC_Type *  base,
uint32_t  u32Interrupts 
)
inlinestatic
Parameters
baseEQDC peripheral base address.
u32InterruptsLogical OR'ed value of the interrupts, _eqdc_interrupt_enable.
static void EQDC_DisableInterrupts ( EQDC_Type *  base,
uint32_t  u32Interrupts 
)
inlinestatic
Parameters
baseEQDC peripheral base address.
u32InterruptsLogical OR'ed value of the interrupts, _eqdc_interrupt_enable.
static void EQDC_DoSoftwareLoadInitialPositionValue ( EQDC_Type *  base)
inlinestatic

Software trigger to load the initial position value (UINIT and LINIT) contents to position counter (UPOS and LPOS), so that to provide the consistent operation the position counter registers.

Parameters
baseEQDC peripheral base address.
static void EQDC_SetInitialPositionValue ( EQDC_Type *  base,
uint32_t  u32PositionInitValue 
)
inlinestatic

Set the position counter initial value (UINIT, LINIT). After writing values to the UINIT and LINIT registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
u32PositionInitValuePosition initial value
static void EQDC_SetPositionCounterValue ( EQDC_Type *  base,
uint32_t  positionCounterValue 
)
inlinestatic

Set the position counter value (POS or UPOS, LPOS).

Parameters
baseEQDC peripheral base address
positionCounterValuePosition counter value
static void EQDC_SetPositionModulusValue ( EQDC_Type *  base,
uint32_t  positionModulusValue 
)
inlinestatic

Set the position counter modulus value (UMOD, LMOD). After writing values to the UMOD and LMOD registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
positionModulusValuePosition modulus value
static void EQDC_SetPositionCompare0Value ( EQDC_Type *  base,
uint32_t  u32PositionComp0Value 
)
inlinestatic

Set the position counter compare 0 value (UCOMP0, LCOMP0). After writing values to the UCOMP0 and LCOMP0 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
u32PositionComp0ValuePosition modulus value
static void EQDC_SetPositionCompare1Value ( EQDC_Type *  base,
uint32_t  u32PositionComp1Value 
)
inlinestatic

Set the position counter compare 1 value (UCOMP1, LCOMP1). After writing values to the UCOMP1 and LCOMP1 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
u32PositionComp1ValuePosition modulus value
static void EQDC_SetPositionCompare2Value ( EQDC_Type *  base,
uint32_t  u32PositionComp2Value 
)
inlinestatic

Set the position counter compare 2 value (UCOMP2, LCOMP2). After writing values to the UCOMP2 and LCOMP2 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
u32PositionComp2ValuePosition modulus value
static void EQDC_SetPositionCompare3Value ( EQDC_Type *  base,
uint32_t  u32PositionComp3Value 
)
inlinestatic

Set the position counter compare 3 value (UCOMP3, LCOMP3). After writing values to the UCOMP3 and LCOMP3 registers, the values are "buffered" into outer-set registers temporarily. Values will be loaded into inner-set registers and take effect using the following two methods:

  1. If CTRL2[LDMODE] is 1, "buffered" values are loaded into inner-set and take effect at the next roll-over or roll-under if CTRL[LDOK] is set.
  2. If CTRL2[LDMODE] is 0, "buffered" values are loaded into inner-set and take effect immediately when CTRL[LDOK] is set.
Parameters
baseEQDC peripheral base address
u32PositionComp3ValuePosition modulus value
static uint32_t EQDC_GetPosition ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
Returns
Current position counter's value.
static uint32_t EQDC_GetHoldPosition ( EQDC_Type *  base)
inlinestatic

The position counter (POS or UPOS, LPOS) value is loaded to hold position (POSH or UPOSH, LPOSH) when:

  1. Position register (POS or UPOS, LPOS), or position difference register (POSD), or revolution register (REV) is read.
  2. TRIGGER happens and TRIGGER is enabled to update the hold registers.
Parameters
baseEQDC peripheral base address.
Returns
Hold position counter's value.
static uint32_t EQDC_GetHoldPosition1 ( EQDC_Type *  base)
inlinestatic

The Upper Position Counter Hold Register 1(UPOSH1) shares the same address with UCOMP1. When read, this register means the value of UPOSH1, which is the upper 16 bits of POSH1. The Lower Position Counter Hold Register 1(LPOSH1) shares the same address with LCOMP1. When read, this register means the value of LPOSH1, which is the lower 16 bits of POSH1. Position counter is captured into POSH1 on the rising edge of ICAP[1].

Parameters
baseEQDC peripheral base address.
Returns
Hold position counter1's value.
static uint32_t EQDC_GetHoldPosition2 ( EQDC_Type *  base)
inlinestatic

The Upper Position Counter Hold Register 2(UPOSH2) shares the same address with UCOMP2. When read,this register means the value of UPOSH2, which is the upper 16 bits of POSH2. The Lower Position Counter Hold Register 2(LPOSH2) shares the same address with LCOMP2. When read, this register means the value of LPOSH2, which is the lower 16 bits of POSH2. Position counter is captured into POSH2 on the rising edge of ICAP[2].

Parameters
baseEQDC peripheral base address.
Returns
Hold position counter2's value.
static uint32_t EQDC_GetHoldPosition3 ( EQDC_Type *  base)
inlinestatic

The Upper Position Counter Hold Register 3(UPOSH3) shares the same address with UCOMP3. When read,this register means the value of UPOSH3, which is the upper 16 bits of POSH3. The Lower Position Counter Hold Register 3(LPOSH3) shares the same address with LCOMP3. When read, this register means the value of LPOSH3, which is the lower 16 bits of POSH3. Position counter is captured into POSH3 on the rising edge of ICAP[3].

Parameters
baseEQDC peripheral base address.
Returns
Hold position counter3's value.
static uint16_t EQDC_GetPositionDifference ( EQDC_Type *  base)
inlinestatic
Parameters
baseEQDC peripheral base address.
Returns
The position difference counter's value.
static uint16_t EQDC_GetHoldPositionDifference ( EQDC_Type *  base)
inlinestatic

The position difference (POSD) value is loaded to hold position difference (POSDH) when:

  1. Position register (POS or UPOS, LPOS), or position difference register (POSD), or revolution register (REV) is read. When Period Measurement is enabled (CTRL3[PMEN] = 1), POSDH will only be udpated when reading POSD.
  2. TRIGGER happens and TRIGGER is enabled to update the hold registers.
Parameters
baseEQDC peripheral base address.
Returns
Hold position difference counter's value.
static uint16_t EQDC_GetRevolution ( EQDC_Type *  base)
inlinestatic

Get the revolution counter (REV) value.

Parameters
baseEQDC peripheral base address.
Returns
The revolution counter's value.
static uint16_t EQDC_GetHoldRevolution ( EQDC_Type *  base)
inlinestatic

The revolution counter (REV) value is loaded to hold revolution (REVH) when:

  1. Position register (POS or UPOS, LPOS), or position difference register (POSD), or revolution register (REV) is read.
  2. TRIGGER happens and TRIGGER is enabled to update the hold registers.
Parameters
baseEQDC peripheral base address.
Returns
Hold position revolution counter's value.
static uint16_t EQDC_GetLastEdgeTime ( EQDC_Type *  base)
inlinestatic

Last edge time (LASTEDGE) is the time since the last edge occurred on PHASEA or PHASEB. The last edge time register counts up using the peripheral clock after prescaler. Any edge on PHASEA or PHASEB will reset this register to 0 and start counting. If the last edge timer count reaches 0xffff, the counting will stop in order to prevent an overflow.Counting will continue when an edge occurs on PHASEA or PHASEB.

Parameters
baseEQDC peripheral base address.
Returns
The last edge time.
static uint16_t EQDC_GetHoldLastEdgeTime ( EQDC_Type *  base)
inlinestatic

The hold of last edge time(LASTEDGEH) is update to last edge time(LASTEDGE) when the position difference register register (POSD) is read.

Parameters
baseEQDC peripheral base address.
Returns
Hold of last edge time.
static uint16_t EQDC_GetPositionDifferencePeriod ( EQDC_Type *  base)
inlinestatic

The Position Difference Period counter (POSDPER) counts up using the prescaled peripheral clock. When reading the position difference register(POSD), the last edge time (LASTEDGE) will be loaded to position difference period counter(POSDPER). If the POSDPER count reaches 0xffff, the counting will stop in order to prevent an overflow. Counting will continue when an edge occurs on PHASEA or PHASEB.

Parameters
baseEQDC peripheral base address.
Returns
The position difference period counter value.
static uint16_t EQDC_GetBufferedPositionDifferencePeriod ( EQDC_Type *  base)
inlinestatic

The Bufferd Position Difference Period (POSDPERBFR) value is updated with the position difference period counter(POSDPER) when any edge occurs on PHASEA or PHASEB.

Parameters
baseEQDC peripheral base address.
Returns
The buffered position difference period counter value.
static uint16_t EQDC_GetHoldPositionDifferencePeriod ( EQDC_Type *  base)
inlinestatic

The hold position difference period(POSDPERH) is updated with the value of buffered position difference period(POSDPERBFR) when the position difference(POSD) register is read.

Parameters
baseEQDC peripheral base address.
Returns
The hold position difference period counter value.