![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
The clock driver supports:
The MCUXpresso SDK provides APIs for MCUXpresso SDK devices' clock operation.
Modules | |
| System Clock Generator (SCG) | |
Files | |
| file | fsl_clock.h |
Data Structures | |
| struct | scg_sys_clk_config_t |
| SCG system clock configuration. More... | |
| struct | scg_sosc_config_t |
| SCG system OSC configuration. More... | |
| struct | scg_rosc_config_t |
| SCG ROSC configuration. More... | |
| struct | scg_sirc_config_t |
| SCG slow IRC clock configuration. More... | |
| struct | scg_firc_trim_config_t |
| SCG fast IRC clock trim configuration. More... | |
| struct | scg_firc_config_t |
| SCG fast IRC clock configuration. More... | |
| struct | fro192m_rf_clk_config_t |
| FRO192M RF clock configuration. More... | |
Macros | |
| #define | FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
| Configure whether driver controls clock. More... | |
| #define | EDMA_CLOCKS |
| Clock ip name array for EDMA. More... | |
| #define | SYSPM_CLOCKS |
| Clock ip name array for SYSPM. More... | |
| #define | SFA_CLOCKS |
| Clock ip name array for SFA. More... | |
| #define | CRC_CLOCKS |
| Clock ip name array for CRC. More... | |
| #define | TPM_CLOCKS |
| Clock ip name array for TPM. More... | |
| #define | LPI2C_CLOCKS |
| Clock ip name array for LPI2C. More... | |
| #define | I3C_CLOCKS |
| Clock ip name array for I3C. More... | |
| #define | LPSPI_CLOCKS |
| Clock ip name array for LPSPI. More... | |
| #define | LPUART_CLOCKS |
| Clock ip name array for LPUART. More... | |
| #define | PORT_CLOCKS |
| Clock ip name array for PORT. More... | |
| #define | LPADC_CLOCKS |
| Clock ip name array for LPADC. More... | |
| #define | LPCMP_CLOCKS |
| Clock ip name array for LPCMP. More... | |
| #define | VREF_CLOCKS |
| Clock ip name array for VREF. More... | |
| #define | GPIO_CLOCKS |
| Clock ip name array for GPIO. More... | |
| #define | LPIT_CLOCKS |
| Clock ip name array for LPIT. More... | |
| #define | RF_CLOCKS |
| Clock ip name array for RF. More... | |
| #define | WDOG_CLOCKS |
| Clock ip name array for WDOG. More... | |
| #define | FLEXCAN_CLOCKS |
| Clock ip name array for FLEXCAN. More... | |
| #define | FLEXIO_CLOCKS |
| Clock ip name array for FLEXIO. More... | |
| #define | TSTMR_CLOCKS |
| Clock ip name array for TSTMR. More... | |
| #define | EWM_CLOCKS |
| Clock ip name array for EWM. More... | |
| #define | SEMA42_CLOCKS |
| Clock ip name array for SEMA42. More... | |
| #define | MAKE_MRCC_REGADDR(base, offset) ((base) + (offset)) |
| "IP Connector name difinition used for clock gate, clock source and clock divider setting. More... | |
Enumerations | |
| enum | clock_name_t { kCLOCK_CoreSysClk, kCLOCK_SlowClk, kCLOCK_PlatClk, kCLOCK_SysClk, kCLOCK_BusClk, kCLOCK_ScgSysOscClk, kCLOCK_ScgSircClk, kCLOCK_ScgFircClk, kCLOCK_RtcOscClk } |
| Clock name used to get clock frequency. More... | |
| enum | clock_ip_control_t { kCLOCK_IpClkControl_fun0 = 0U, kCLOCK_IpClkControl_fun1 = 1U, kCLOCK_IpClkControl_fun2 = 2U, kCLOCK_IpClkControl_fun3 } |
| Clock source for peripherals that support various clock selections. More... | |
| enum | clock_ip_src_t { kCLOCK_IpSrcFro6M = 2U, kCLOCK_IpSrcFro192M = 3U, kCLOCK_IpSrcSoscClk = 4U, kCLOCK_IpSrc32kClk = 5U } |
| Clock source for peripherals that support various clock selections. More... | |
| enum | clock_ip_name_t { kCLOCK_NOGATE = 0U, kCLOCK_Ewm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x4C), kCLOCK_Syspm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x5C), kCLOCK_Wdog0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x68), kCLOCK_Wdog1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x6C), kCLOCK_Sfa0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x74), kCLOCK_Crc0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x8C), kCLOCK_Secsubsys = MAKE_MRCC_REGADDR(MRCC_BASE, 0x90), kCLOCK_Lpit0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xBC), kCLOCK_Tstmr0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC0), kCLOCK_Tpm0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC4), kCLOCK_Tpm1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xC8), kCLOCK_Lpi2c0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xCC), kCLOCK_Lpi2c1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD0), kCLOCK_I3c0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD4), kCLOCK_Lpspi0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xD8), kCLOCK_Lpspi1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xDC), kCLOCK_Lpuart0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE0), kCLOCK_Lpuart1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE4), kCLOCK_Flexio0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xE8), kCLOCK_Can0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xEC), kCLOCK_Sema0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0xFC), kCLOCK_Data_stream_2p4 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x104), kCLOCK_PortA = MAKE_MRCC_REGADDR(MRCC_BASE, 0x108), kCLOCK_PortB = MAKE_MRCC_REGADDR(MRCC_BASE, 0x10C), kCLOCK_PortC = MAKE_MRCC_REGADDR(MRCC_BASE, 0x110), kCLOCK_Lpadc0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x11C), kCLOCK_Lpcmp0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x120), kCLOCK_Lpcmp1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x124), kCLOCK_Vref0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x128), kCLOCK_Mtr_master = MAKE_MRCC_REGADDR(MRCC_BASE, 0x134), kCLOCK_GpioA = MAKE_MRCC_REGADDR(MRCC_BASE, 0x404), kCLOCK_GpioB = MAKE_MRCC_REGADDR(MRCC_BASE, 0x408), kCLOCK_GpioC = MAKE_MRCC_REGADDR(MRCC_BASE, 0x40C), kCLOCK_Dma0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x410), kCLOCK_Pflexnvm = MAKE_MRCC_REGADDR(MRCC_BASE, 0x414), kCLOCK_Sram0 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x41C), kCLOCK_Sram1 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x420), kCLOCK_Sram2 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x424), kCLOCK_Sram3 = MAKE_MRCC_REGADDR(MRCC_BASE, 0x428), kCLOCK_Rf_2p4ghz_bist = MAKE_MRCC_REGADDR(MRCC_BASE, 0x42C) } |
| Clock IP name. More... | |
| enum | _scg_status { kStatus_SCG_Busy = MAKE_STATUS(kStatusGroup_SCG, 1), kStatus_SCG_InvalidSrc = MAKE_STATUS(kStatusGroup_SCG, 2) } |
| SCG status return codes. More... | |
| enum | scg_sys_clk_t { kSCG_SysClkSlow, kSCG_SysClkBus, kSCG_SysClkPlatform, kSCG_SysClkCore } |
| SCG system clock type. More... | |
| enum | scg_sys_clk_src_t { kSCG_SysClkSrcSysOsc = 1U, kSCG_SysClkSrcSirc = 2U, kSCG_SysClkSrcFirc = 3U, kSCG_SysClkSrcRosc = 4U } |
| SCG system clock source. More... | |
| enum | scg_sys_clk_div_t { kSCG_SysClkDivBy1 = 0U, kSCG_SysClkDivBy2 = 1U, kSCG_SysClkDivBy3 = 2U, kSCG_SysClkDivBy4 = 3U, kSCG_SysClkDivBy5 = 4U, kSCG_SysClkDivBy6 = 5U, kSCG_SysClkDivBy7 = 6U, kSCG_SysClkDivBy8 = 7U, kSCG_SysClkDivBy9 = 8U, kSCG_SysClkDivBy10 = 9U, kSCG_SysClkDivBy11 = 10U, kSCG_SysClkDivBy12 = 11U, kSCG_SysClkDivBy13 = 12U, kSCG_SysClkDivBy14 = 13U, kSCG_SysClkDivBy15 = 14U, kSCG_SysClkDivBy16 = 15U } |
| SCG system clock divider value. More... | |
| enum | clock_clkout_src_t { kClockClkoutSelScgSlow = 0U, kClockClkoutSelSosc = 1U, kClockClkoutSelSirc = 2U, kClockClkoutSelFirc = 3U, kClockClkoutSelScgRtcOsc = 4U } |
| SCG clock out configuration (CLKOUTSEL). More... | |
| enum | scg_sosc_monitor_mode_t { kSCG_SysOscMonitorDisable = 0U, kSCG_SysOscMonitorInt = SCG_SOSCCSR_SOSCCM_MASK, kSCG_SysOscMonitorReset } |
| SCG system OSC monitor mode. More... | |
| enum | { kSCG_SoscDisable = 0, kSCG_SoscEnable = SCG_SOSCCSR_SOSCEN_MASK, kSCG_SoscEnableInSleep = SCG_SOSCCSR_SOSCSTEN_MASK } |
| SOSC enable mode. More... | |
| enum | scg_rosc_monitor_mode_t { kSCG_RoscMonitorDisable = 0U, kSCG_RoscMonitorInt = SCG_ROSCCSR_ROSCCM_MASK, kSCG_RoscMonitorReset } |
| SCG ROSC monitor mode. More... | |
| enum | scg_sirc_enable_mode_t { kSCG_SircDisableInSleep = 0, kSCG_SircEnableInSleep = SCG_SIRCCSR_SIRCSTEN_MASK } |
| SIRC enable mode. More... | |
| enum | scg_firc_trim_mode_t { kSCG_FircTrimNonUpdate = SCG_FIRCCSR_FIRCTREN_MASK, kSCG_FircTrimUpdate = SCG_FIRCCSR_FIRCTREN_MASK | SCG_FIRCCSR_FIRCTRUP_MASK } |
| SCG fast IRC trim mode. More... | |
| enum | scg_firc_trim_src_t { kSCG_FircTrimSrcSysOsc = 2U, kSCG_FircTrimSrcRtcOsc = 3U } |
| SCG fast IRC trim source. More... | |
| enum | { kSCG_FircDisable = 0, kSCG_FircEnable = SCG_FIRCCSR_FIRCEN_MASK, kSCG_FircEnableInSleep = SCG_FIRCCSR_FIRCSTEN_MASK } |
| FIRC enable mode. More... | |
| enum | scg_firc_range_t { kSCG_FircRange48M, kSCG_FircRange64M, kSCG_FircRange96M, kSCG_FircRange192M } |
| SCG fast IRC clock frequency range. More... | |
| enum | fro192m_rf_range_t { kFro192M_Range16M, kFro192M_Range24M, kFro192M_Range32M, kFro192M_Range48M, kFro192M_Range64M } |
| FRO192M RF clock frequency range. More... | |
| enum | fro192m_rf_clk_div_t { kFro192M_ClkDivBy1 = 0U, kFro192M_ClkDivBy2 = 1U, kFro192M_ClkDivBy4 = 2U, kFro192M_ClkDivBy8 = 3U } |
| RF Flash APB and RF_CMC clock divide. More... | |
Functions | |
| static void | CLOCK_EnableClock (clock_ip_name_t name) |
| Enable the clock for specific IP. More... | |
| static void | CLOCK_EnableClockLPMode (clock_ip_name_t name, clock_ip_control_t control) |
| Enable the clock for specific IP in low power mode. More... | |
| static void | CLOCK_DisableClock (clock_ip_name_t name) |
| Disable the clock for specific IP. More... | |
| static void | CLOCK_SetIpSrc (clock_ip_name_t name, clock_ip_src_t src) |
| Set the clock source for specific IP module. More... | |
| static void | CLOCK_SetIpSrcDiv (clock_ip_name_t name, uint8_t divValue) |
| Set the clock source and divider for specific IP module. More... | |
| uint32_t | CLOCK_GetFreq (clock_name_t clockName) |
| Gets the clock frequency for a specific clock name. More... | |
| uint32_t | CLOCK_GetCoreSysClkFreq (void) |
| Get the core clock or system clock frequency. More... | |
| uint32_t | CLOCK_GetPlatClkFreq (void) |
| Get the platform clock frequency. More... | |
| uint32_t | CLOCK_GetBusClkFreq (void) |
| Get the bus clock frequency. More... | |
| uint32_t | CLOCK_GetFlashClkFreq (void) |
| Get the flash clock frequency. More... | |
| uint32_t | CLOCK_GetIpFreq (clock_ip_name_t name) |
| Gets the functional clock frequency for a specific IP module. More... | |
Variables | |
| volatile uint32_t | g_xtal0Freq |
| External XTAL0 (OSC0/SYSOSC) clock frequency. More... | |
| volatile uint32_t | g_xtal32Freq |
| External XTAL32/EXTAL32 clock frequency. More... | |
Driver version | |
| #define | FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) |
| CLOCK driver version 1.0.0. More... | |
MCU System Clock. | |
| uint32_t | CLOCK_GetSysClkFreq (scg_sys_clk_t type) |
| Gets the SCG system clock frequency. More... | |
| static void | CLOCK_SetRunModeSysClkConfig (const scg_sys_clk_config_t *config) |
| Sets the system clock configuration for RUN mode. More... | |
| static void | CLOCK_GetCurSysClkConfig (scg_sys_clk_config_t *config) |
| Gets the system clock configuration in the current power mode. More... | |
| static void | CLOCK_SetClkOutSel (clock_clkout_src_t setting) |
| Sets the clock out selection. More... | |
SCG System OSC Clock. | |
| status_t | CLOCK_InitSysOsc (const scg_sosc_config_t *config) |
| Initializes the SCG system OSC. More... | |
| status_t | CLOCK_DeinitSysOsc (void) |
| De-initializes the SCG system OSC. More... | |
| uint32_t | CLOCK_GetSysOscFreq (void) |
| Gets the SCG system OSC clock frequency (SYSOSC). More... | |
| static bool | CLOCK_IsSysOscErr (void) |
| Checks whether the system OSC clock error occurs. More... | |
| static void | CLOCK_ClearSysOscErr (void) |
| Clears the system OSC clock error. | |
| static void | CLOCK_SetSysOscMonitorMode (scg_sosc_monitor_mode_t mode) |
| Sets the system OSC monitor mode. More... | |
| static bool | CLOCK_IsSysOscValid (void) |
| Checks whether the system OSC clock is valid. More... | |
| static void | CLOCK_UnlockSysOscControlStatusReg (void) |
| Unlock the SOSCCSR control status register. | |
| static void | CLOCK_LockSysOscControlStatusReg (void) |
| Lock the SOSCCSR control status register. | |
SCG Slow IRC Clock. | |
| status_t | CLOCK_InitSirc (const scg_sirc_config_t *config) |
| Initializes the SCG slow IRC clock. More... | |
| status_t | CLOCK_DeinitSirc (void) |
| De-initializes the SCG slow IRC. More... | |
| uint32_t | CLOCK_GetSircFreq (void) |
| Gets the SCG SIRC clock frequency. More... | |
| static bool | CLOCK_IsSircValid (void) |
| Checks whether the SIRC clock is valid. More... | |
| static void | CLOCK_UnlockSircControlStatusReg (void) |
| Unlock the SIRCCSR control status register. | |
| static void | CLOCK_LockSircControlStatusReg (void) |
| Lock the SIRCCSR control status register. | |
SCG Fast IRC Clock. | |
| status_t | CLOCK_InitFirc (const scg_firc_config_t *config) |
| Initializes the SCG fast IRC clock. More... | |
| status_t | CLOCK_DeinitFirc (void) |
| De-initializes the SCG fast IRC. More... | |
| uint32_t | CLOCK_GetFircFreq (void) |
| Gets the SCG FIRC clock frequency. More... | |
| static bool | CLOCK_IsFircErr (void) |
| Checks whether the FIRC clock error occurs. More... | |
| static void | CLOCK_ClearFircErr (void) |
| Clears the FIRC clock error. | |
| static bool | CLOCK_IsFircValid (void) |
| Checks whether the FIRC clock is valid. More... | |
| static void | CLOCK_UnlockFircControlStatusReg (void) |
| Unlock the FIRCCSR control status register. | |
| static void | CLOCK_LockFircControlStatusReg (void) |
| Lock the FIRCCSR control status register. | |
| status_t | CLOCK_InitRosc (const scg_rosc_config_t *config) |
| brief Initializes the SCG ROSC. More... | |
| status_t | CLOCK_DeinitRosc (void) |
| brief De-initializes the SCG ROSC. More... | |
| uint32_t | CLOCK_GetRtcOscFreq (void) |
| Gets the SCG RTC OSC clock frequency. More... | |
| status_t | CLOCK_InitRfFro192M (const fro192m_rf_clk_config_t *config) |
| Initializes the FRO192M clock for the Radio Mode Controller. More... | |
| uint32_t | CLOCK_GetRfFro192MFreq (void) |
| Gets the FRO192M clock frequency. More... | |
| static bool | CLOCK_IsRoscErr (void) |
| Checks whether the ROSC clock error occurs. More... | |
| static void | CLOCK_ClearRoscErr (void) |
| Clears the ROSC clock error. | |
| static void | CLOCK_SetRoscMonitorMode (scg_rosc_monitor_mode_t mode) |
| Sets the ROSC monitor mode. More... | |
| static bool | CLOCK_IsRoscValid (void) |
| Checks whether the ROSC clock is valid. More... | |
| static void | CLOCK_UnlockRoscControlStatusReg (void) |
| Unlock the ROSCCSR control status register. | |
| static void | CLOCK_LockRoscControlStatusReg (void) |
| Lock the ROSCCSR control status register. | |
External clock frequency | |
| static void | CLOCK_SetXtal0Freq (uint32_t freq) |
| Sets the XTAL0 frequency based on board settings. More... | |
| static void | CLOCK_SetXtal32Freq (uint32_t freq) |
| Sets the XTAL32 frequency based on board settings. More... | |
| struct scg_sys_clk_config_t |
Data Fields | |
| uint32_t | divSlow: 4 |
| Slow clock divider, see scg_sys_clk_div_t. More... | |
| uint32_t | divBus: 4 |
| Bus clock divider, see scg_sys_clk_div_t. More... | |
| uint32_t | __pad0__: 8 |
| Reserved. More... | |
| uint32_t | divCore: 4 |
| Core clock divider, see scg_sys_clk_div_t. More... | |
| uint32_t | __pad1__: 4 |
| Reserved. More... | |
| uint32_t | src: 3 |
| System clock source, see scg_sys_clk_src_t. More... | |
| uint32_t | __pad2__: 5 |
| reserved. More... | |
| uint32_t scg_sys_clk_config_t::divSlow |
| uint32_t scg_sys_clk_config_t::divBus |
| uint32_t scg_sys_clk_config_t::__pad0__ |
| uint32_t scg_sys_clk_config_t::divCore |
| uint32_t scg_sys_clk_config_t::__pad1__ |
| uint32_t scg_sys_clk_config_t::src |
| uint32_t scg_sys_clk_config_t::__pad2__ |
| struct scg_sosc_config_t |
Data Fields | |
| uint32_t | freq |
| System OSC frequency. More... | |
| uint32_t | enableMode |
| Enable mode, OR'ed value of _scg_sosc_enable_mode. More... | |
| scg_sosc_monitor_mode_t | monitorMode |
| Clock monitor mode selected. More... | |
| uint32_t scg_sosc_config_t::freq |
| uint32_t scg_sosc_config_t::enableMode |
| scg_sosc_monitor_mode_t scg_sosc_config_t::monitorMode |
| struct scg_rosc_config_t |
Data Fields | |
| scg_rosc_monitor_mode_t | monitorMode |
| Clock monitor mode selected. More... | |
| scg_rosc_monitor_mode_t scg_rosc_config_t::monitorMode |
| struct scg_sirc_config_t |
Data Fields | |
| scg_sirc_enable_mode_t | enableMode |
| Enable mode, OR'ed value of _scg_sirc_enable_mode. More... | |
| scg_sirc_enable_mode_t scg_sirc_config_t::enableMode |
| struct scg_firc_trim_config_t |
Data Fields | |
| scg_firc_trim_mode_t | trimMode |
| FIRC trim mode. More... | |
| scg_firc_trim_src_t | trimSrc |
| Trim source. More... | |
| uint16_t | trimDiv |
| Divider of SOSC for FIRC. More... | |
| uint8_t | trimCoar |
| Trim coarse value; Irrelevant if trimMode is kSCG_FircTrimUpdate. More... | |
| uint8_t | trimFine |
| Trim fine value; Irrelevant if trimMode is kSCG_FircTrimUpdate. More... | |
| scg_firc_trim_mode_t scg_firc_trim_config_t::trimMode |
| scg_firc_trim_src_t scg_firc_trim_config_t::trimSrc |
| uint16_t scg_firc_trim_config_t::trimDiv |
| uint8_t scg_firc_trim_config_t::trimCoar |
| uint8_t scg_firc_trim_config_t::trimFine |
| struct scg_firc_config_t |
Data Fields | |
| uint32_t | enableMode |
| Enable mode. More... | |
| scg_firc_range_t | range |
| Fast IRC frequency range. More... | |
| const scg_firc_trim_config_t * | trimConfig |
| Pointer to the FIRC trim configuration; set NULL to disable trim. More... | |
| uint32_t scg_firc_config_t::enableMode |
| scg_firc_range_t scg_firc_config_t::range |
| const scg_firc_trim_config_t* scg_firc_config_t::trimConfig |
| struct fro192m_rf_clk_config_t |
Data Fields | |
| fro192m_rf_range_t | range |
| FRO192M RF clock frequency range. More... | |
| fro192m_rf_clk_div_t | apb_rfcmc_div |
| RF Flash APB and RF_CMC clock divide. More... | |
| fro192m_rf_range_t fro192m_rf_clk_config_t::range |
| fro192m_rf_clk_div_t fro192m_rf_clk_config_t::apb_rfcmc_div |
| #define FSL_SDK_DISABLE_DRIVER_CLOCK_CONTROL 0 |
When set to 0, peripheral drivers will enable clock in initialize function and disable clock in de-initialize function. When set to 1, peripheral driver will not control the clock, application could control the clock out of the driver.
| #define FSL_CLOCK_DRIVER_VERSION (MAKE_VERSION(1, 0, 0)) |
| #define EDMA_CLOCKS |
| #define SYSPM_CLOCKS |
| #define SFA_CLOCKS |
| #define CRC_CLOCKS |
| #define TPM_CLOCKS |
| #define LPI2C_CLOCKS |
| #define I3C_CLOCKS |
| #define LPSPI_CLOCKS |
| #define LPUART_CLOCKS |
| #define PORT_CLOCKS |
| #define LPADC_CLOCKS |
| #define LPCMP_CLOCKS |
| #define VREF_CLOCKS |
| #define GPIO_CLOCKS |
| #define LPIT_CLOCKS |
| #define RF_CLOCKS |
| #define WDOG_CLOCKS |
| #define FLEXCAN_CLOCKS |
| #define FLEXIO_CLOCKS |
| #define TSTMR_CLOCKS |
| #define EWM_CLOCKS |
| #define SEMA42_CLOCKS |
| #define MAKE_MRCC_REGADDR | ( | base, | |
| offset | |||
| ) | ((base) + (offset)) |
It is defined as the corresponding register address.
| enum clock_name_t |
These clocks source would be generated from SCG module.
| enum clock_ip_control_t |
These options are for MRCC->XX[CC]
| enum clock_ip_src_t |
| enum clock_ip_name_t |
| enum _scg_status |
| enum scg_sys_clk_t |
| enum scg_sys_clk_src_t |
| enum scg_sys_clk_div_t |
| enum clock_clkout_src_t |
| anonymous enum |
| enum scg_firc_trim_mode_t |
| Enumerator | |
|---|---|
| kSCG_FircTrimNonUpdate |
FIRC trim enable but not enable trim value update. In this mode, the trim value is fixed to the initialized value which is defined by trimCoar and trimFine in configure structure scg_firc_trim_config_t. |
| kSCG_FircTrimUpdate |
FIRC trim enable and trim value update enable. In this mode, the trim value is auto update. |
| enum scg_firc_trim_src_t |
| anonymous enum |
| enum scg_firc_range_t |
| enum fro192m_rf_range_t |
| enum fro192m_rf_clk_div_t |
|
inlinestatic |
| name | Which clock to enable, see clock_ip_name_t. |
|
inlinestatic |
| name | Which clock to enable, see clock_ip_name_t. |
| control | Clock Config, see clock_ip_control_t. |
|
inlinestatic |
| name | Which clock to disable, see clock_ip_name_t. |
|
inlinestatic |
Set the clock source for specific IP, not all modules need to set the clock source, should only use this function for the modules need source setting.
| name | Which peripheral to check, see clock_ip_name_t. |
| src | Clock source to set. |
|
inlinestatic |
Set the clock source and divider for specific IP, not all modules need to set the clock source and divider, should only use this function for the modules need source and divider setting.
Divider output clock = Divider input clock / (divValue+1)]).
| name | Which peripheral to check, see clock_ip_name_t. |
| divValue | The divider value. |
| uint32_t CLOCK_GetFreq | ( | clock_name_t | clockName | ) |
This function checks the current clock configurations and then calculates the clock frequency for a specific clock name defined in clock_name_t.
| clockName | Clock names defined in clock_name_t |
| uint32_t CLOCK_GetCoreSysClkFreq | ( | void | ) |
| uint32_t CLOCK_GetPlatClkFreq | ( | void | ) |
| uint32_t CLOCK_GetBusClkFreq | ( | void | ) |
| uint32_t CLOCK_GetFlashClkFreq | ( | void | ) |
| uint32_t CLOCK_GetIpFreq | ( | clock_ip_name_t | name | ) |
This function gets the IP module's functional clock frequency based on MRCC registers. It is only used for the IP modules which could select clock source by MRCC[PCS].
| name | Which peripheral to get, see clock_ip_name_t. |
| uint32_t CLOCK_GetSysClkFreq | ( | scg_sys_clk_t | type | ) |
This function gets the SCG system clock frequency. These clocks are used for core, platform, external, and bus clock domains.
| type | Which type of clock to get, core clock or slow clock. |
|
inlinestatic |
This function sets the system clock configuration for RUN mode.
| config | Pointer to the configuration. |
|
inlinestatic |
This function gets the system configuration in the current power mode.
| config | Pointer to the configuration. |
|
inlinestatic |
This function sets the clock out selection (CLKOUTSEL).
| setting | The selection to set. |
| status_t CLOCK_InitSysOsc | ( | const scg_sosc_config_t * | config | ) |
This function enables the SCG system OSC clock according to the configuration.
| config | Pointer to the configuration structure. |
| kStatus_Success | System OSC is initialized. |
| kStatus_SCG_Busy | System OSC has been enabled and is used by the system clock. |
| kStatus_ReadOnly | System OSC control register is locked. |
| status_t CLOCK_DeinitSysOsc | ( | void | ) |
This function disables the SCG system OSC clock.
| kStatus_Success | System OSC is deinitialized. |
| kStatus_SCG_Busy | System OSC is used by the system clock. |
| kStatus_ReadOnly | System OSC control register is locked. |
| uint32_t CLOCK_GetSysOscFreq | ( | void | ) |
|
inlinestatic |
|
inlinestatic |
This function sets the system OSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
|
inlinestatic |
| status_t CLOCK_InitSirc | ( | const scg_sirc_config_t * | config | ) |
This function enables the SCG slow IRC clock according to the configuration.
| config | Pointer to the configuration structure. |
| kStatus_Success | SIRC is initialized. |
| kStatus_SCG_Busy | SIRC has been enabled and is used by system clock. |
| kStatus_ReadOnly | SIRC control register is locked. |
| status_t CLOCK_DeinitSirc | ( | void | ) |
This function disables the SCG slow IRC.
| kStatus_Success | SIRC is deinitialized. |
| kStatus_SCG_Busy | SIRC is used by system clock. |
| kStatus_ReadOnly | SIRC control register is locked. |
| uint32_t CLOCK_GetSircFreq | ( | void | ) |
|
inlinestatic |
| status_t CLOCK_InitFirc | ( | const scg_firc_config_t * | config | ) |
This function enables the SCG fast IRC clock according to the configuration.
| config | Pointer to the configuration structure. |
| kStatus_Success | FIRC is initialized. |
| kStatus_SCG_Busy | FIRC has been enabled and is used by the system clock. |
| kStatus_ReadOnly | FIRC control register is locked. |
| status_t CLOCK_DeinitFirc | ( | void | ) |
This function disables the SCG fast IRC.
| kStatus_Success | FIRC is deinitialized. |
| kStatus_SCG_Busy | FIRC is used by the system clock. |
| kStatus_ReadOnly | FIRC control register is locked. |
| uint32_t CLOCK_GetFircFreq | ( | void | ) |
|
inlinestatic |
|
inlinestatic |
| status_t CLOCK_InitRosc | ( | const scg_rosc_config_t * | config | ) |
This function enables the SCG ROSC clock according to the configuration.
param config Pointer to the configuration structure. retval kStatus_Success ROSC is initialized. retval kStatus_SCG_Busy ROSC has been enabled and is used by the system clock. retval kStatus_ReadOnly ROSC control register is locked.
note This function can't detect whether the system OSC has been enabled and used by an IP.
| status_t CLOCK_DeinitRosc | ( | void | ) |
This function disables the SCG ROSC clock.
retval kStatus_Success System OSC is deinitialized. retval kStatus_SCG_Busy System OSC is used by the system clock. retval kStatus_ReadOnly System OSC control register is locked.
note This function can't detect whether the ROSC is used by an IP.
| uint32_t CLOCK_GetRtcOscFreq | ( | void | ) |
| status_t CLOCK_InitRfFro192M | ( | const fro192m_rf_clk_config_t * | config | ) |
This function configure the RF FRO192M clock according to the configuration.
| config | Pointer to the configuration structure. |
| kStatus_Success | RF FRO192M is configured. |
| uint32_t CLOCK_GetRfFro192MFreq | ( | void | ) |
|
inlinestatic |
|
inlinestatic |
This function sets the ROSC monitor mode. The mode can be disabled, it can generate an interrupt when the error is disabled, or reset when the error is detected.
| mode | Monitor mode to set. |
|
inlinestatic |
|
inlinestatic |
| freq | The XTAL0/EXTAL0 input clock frequency in Hz. |
|
inlinestatic |
| freq | The XTAL32/EXTAL32 input clock frequency in Hz. |
| volatile uint32_t g_xtal0Freq |
The XTAL0/EXTAL0 (OSC0/SYSOSC) clock frequency in Hz. When the clock is set up, use the function CLOCK_SetXtal0Freq to set the value in the clock driver. For example, if XTAL0 is 8 MHz:
This is important for the multicore platforms where only one core needs to set up the OSC0/SYSOSC using CLOCK_InitSysOsc. All other cores need to call the CLOCK_SetXtal0Freq to get a valid clock frequency.
| volatile uint32_t g_xtal32Freq |
The XTAL32/EXTAL32 clock frequency in Hz. When the clock is set up, use the function CLOCK_SetXtal32Freq to set the value in the clock driver.
This is important for the multicore platforms where only one core needs to set up the clock. All other cores need to call the CLOCK_SetXtal32Freq to get a valid clock frequency.