MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
Serial_port_virtual

Overview

Data Structures

struct  serial_port_virtual_config_t
 serial port usb config struct More...
 

Macros

#define SERIAL_PORT_BLE_WU_HANDLE_SIZE   (24U)
 serial port USB handle size
 
#define SERIAL_PORT_VIRTUAL_HANDLE_SIZE   (40U)
 serial port USB handle size
 

Enumerations

enum  serial_port_virtual_controller_index_t {
  kSerialManager_UsbVirtualControllerKhci0 = 0U,
  kSerialManager_UsbVirtualControllerKhci1 = 1U,
  kSerialManager_UsbVirtualControllerEhci0 = 2U,
  kSerialManager_UsbVirtualControllerEhci1 = 3U,
  kSerialManager_UsbVirtualControllerLpcIp3511Fs0 = 4U,
  kSerialManager_UsbVirtualControllerLpcIp3511Fs1,
  kSerialManager_UsbVirtualControllerLpcIp3511Hs0 = 6U,
  kSerialManager_UsbVirtualControllerLpcIp3511Hs1,
  kSerialManager_UsbVirtualControllerOhci0 = 8U,
  kSerialManager_UsbVirtualControllerOhci1 = 9U,
  kSerialManager_UsbVirtualControllerIp3516Hs0 = 10U,
  kSerialManager_UsbVirtualControllerIp3516Hs1 = 11U
}
 USB controller ID. More...
 

Data Structure Documentation

struct serial_port_virtual_config_t

Data Fields

serial_port_virtual_controller_index_t controllerIndex
 controller index
 

Enumeration Type Documentation

Enumerator
kSerialManager_UsbVirtualControllerKhci0 

KHCI 0U.

kSerialManager_UsbVirtualControllerKhci1 

KHCI 1U, Currently, there are no platforms which have two KHCI IPs, this is reserved to be used in the future.

kSerialManager_UsbVirtualControllerEhci0 

EHCI 0U.

kSerialManager_UsbVirtualControllerEhci1 

EHCI 1U, Currently, there are no platforms which have two EHCI IPs, this is reserved to be used in the future.

kSerialManager_UsbVirtualControllerLpcIp3511Fs0 

LPC USB IP3511 FS controller 0.

kSerialManager_UsbVirtualControllerLpcIp3511Fs1 

LPC USB IP3511 FS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.

kSerialManager_UsbVirtualControllerLpcIp3511Hs0 

LPC USB IP3511 HS controller 0.

kSerialManager_UsbVirtualControllerLpcIp3511Hs1 

LPC USB IP3511 HS controller 1, there are no platforms which have two IP3511 IPs, this is reserved to be used in the future.

kSerialManager_UsbVirtualControllerOhci0 

OHCI 0U.

kSerialManager_UsbVirtualControllerOhci1 

OHCI 1U, Currently, there are no platforms which have two OHCI IPs, this is reserved to be used in the future.

kSerialManager_UsbVirtualControllerIp3516Hs0 

IP3516HS 0U.

kSerialManager_UsbVirtualControllerIp3516Hs1 

IP3516HS 1U, Currently, there are no platforms which have two IP3516HS IPs, this is reserved to be used in the future.