![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
The ROMAPI driver provides the functionalities to operate the external NOR Flash connected to the FLEXSPI controller.
The ROMAPI driver supports:
Data Structures | |
| struct | serial_nor_config_option_t |
| Serial NOR Configuration Option. More... | |
| struct | flexspi_lut_seq_t |
| FLEXSPI LUT Sequence structure. More... | |
| struct | flexspi_dll_time_t |
| FLEXSPI DLL time. More... | |
| struct | flexspi_mem_config_t |
| FLEXSPI Memory Configuration Block. More... | |
| struct | flexspi_nor_config_t |
| Serial NOR configuration block. More... | |
| struct | flexspi_xfer_t |
| FLEXSPI Transfer Context. More... | |
Macros | |
| #define | FSL_ROM_ROMAPI_VERSION (MAKE_VERSION(1U, 1U, 2U)) |
| ROM API version 1.1.2. More... | |
| #define | FSL_ROM_FLEXSPINOR_DRIVER_VERSION (MAKE_VERSION(1U, 7U, 0U)) |
| ROM FLEXSPI NOR driver version 1.7.0. More... | |
| #define | kROM_StatusGroup_FLEXSPINOR 201U |
| ROM FLEXSPI NOR status group number. More... | |
| #define | FSL_ROM_FLEXSPI_BITMASK(bit_offset) (1U << (bit_offset)) |
| Generate bit mask. | |
| #define | FLEXSPI_CFG_BLK_TAG (0x42464346UL) |
| FLEXSPI memory config block related definitions. More... | |
| #define | FLEXSPI_CFG_BLK_VERSION (0x56010400UL) |
| V1.4.0. | |
| #define | NOR_CMD_LUT_SEQ_IDX_READ 0U |
| NOR LUT sequence index used for default LUT assignment. More... | |
| #define | NOR_CMD_LUT_SEQ_IDX_READSTATUS 1U |
| Read Status LUT sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_READSTATUS_XPI 2U |
| Read status DPI/QPI/OPI sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_WRITEENABLE 3U |
| Write Enable sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_WRITEENABLE_XPI 4U |
| Write Enable DPI/QPI/OPI sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_ERASESECTOR 5U |
| Erase Sector sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_ERASEBLOCK 8U |
| Erase Block sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM 9U |
| Program sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_CHIPERASE 11U |
| Chip Erase sequence in lookupTable id stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_READ_SFDP 13U |
| Read SFDP sequence in lookupTable id stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_RESTORE_NOCMD 14U |
| Restore 0-4-4/0-8-8 mode sequence id in lookupTable stored in config block. | |
| #define | NOR_CMD_LUT_SEQ_IDX_EXIT_NOCMD 15U |
| Exit 0-4-4/0-8-8 mode sequence id in lookupTable stored in config block. | |
| #define | MISRA_CAST(to_type, to_var, from_type, from_var) |
| convert the type for MISRA | |
Enumerations | |
| enum | { kSerialFlash_ISSI_ManufacturerID = 0x9DU, kSerialFlash_Adesto_ManufacturerID = 0x1F, kSerialFlash_Winbond_ManufacturerID = 0xEFU, kSerialFlash_Cypress_ManufacturerID = 0x01U } |
| Manufacturer ID. More... | |
| enum | _flexspi_nor_status { kStatus_ROM_FLEXSPI_SequenceExecutionTimeout, kStatus_ROM_FLEXSPI_InvalidSequence = MAKE_STATUS(kStatusGroup_FLEXSPI, 1), kStatus_ROM_FLEXSPI_DeviceTimeout = MAKE_STATUS(kStatusGroup_FLEXSPI, 2), kStatus_ROM_FLEXSPINOR_SFDP_NotFound, kStatus_ROM_FLEXSPINOR_Flash_NotFound, kStatus_FLEXSPINOR_DTRRead_DummyProbeFailed } |
| ROM FLEXSPI NOR flash status. More... | |
| enum | flexspi_operation_t { kFLEXSPIOperation_Command, kFLEXSPIOperation_Config, kFLEXSPIOperation_Write, kFLEXSPIOperation_Read } |
| FLEXSPI Operation Context. More... | |
Functions | |
| void | ROM_API_Init (void) |
| ROM API init. More... | |
Common ROMAPI features info defines | |
| #define | FSL_ROM_HAS_FLEXSPINOR_API (1) |
| ROM has FLEXSPI NOR API. More... | |
| #define | FSL_ROM_HAS_RUNBOOTLOADER_API (1) |
| ROM has run bootloader API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_GET_CONFIG (1) |
| ROM has FLEXSPI NOR get config API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_FLASH_INIT (1) |
| ROM has flash init API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE (1) |
| ROM has erase API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_SECTOR (1) |
| ROM has erase sector API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_BLOCK (1) |
| ROM has erase block API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_ALL (1) |
| ROM has erase all API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_READ (1) |
| ROM has read API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_UPDATE_LUT (1) |
| ROM has update lut API. More... | |
| #define | FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_CMD_XFER (1) |
| ROM has FLEXSPI command API. More... | |
Enter Bootloader | |
| void | ROM_RunBootloader (void *arg) |
| Enter Bootloader. More... | |
GetConfig | |
| status_t | ROM_FLEXSPI_NorFlash_GetConfig (uint32_t instance, flexspi_nor_config_t *config, serial_nor_config_option_t *option) |
| Get FLEXSPI NOR Configuration Block based on specified option. More... | |
Initialization | |
| status_t | ROM_FLEXSPI_NorFlash_Init (uint32_t instance, flexspi_nor_config_t *config) |
| Initialize Serial NOR devices via FLEXSPI. More... | |
Programming | |
| status_t | ROM_FLEXSPI_NorFlash_ProgramPage (uint32_t instance, flexspi_nor_config_t *config, uint32_t dst_addr, const uint32_t *src) |
| Program data to Serial NOR via FLEXSPI. More... | |
Reading | |
| status_t | ROM_FLEXSPI_NorFlash_Read (uint32_t instance, flexspi_nor_config_t *config, uint32_t *dst, uint32_t start, uint32_t lengthInBytes) |
| Read data from Serial NOR via FLEXSPI. More... | |
Erasing | |
| status_t | ROM_FLEXSPI_NorFlash_Erase (uint32_t instance, flexspi_nor_config_t *config, uint32_t start, uint32_t length) |
| Erase Flash Region specified by address and length. More... | |
| status_t | ROM_FLEXSPI_NorFlash_EraseSector (uint32_t instance, flexspi_nor_config_t *config, uint32_t start) |
| Erase one sector specified by address. More... | |
| status_t | ROM_FLEXSPI_NorFlash_EraseBlock (uint32_t instance, flexspi_nor_config_t *config, uint32_t start) |
| Erase one block specified by address. More... | |
| status_t | ROM_FLEXSPI_NorFlash_EraseAll (uint32_t instance, flexspi_nor_config_t *config) |
| Erase all the Serial NOR devices connected on FLEXSPI. More... | |
Command | |
| status_t | ROM_FLEXSPI_NorFlash_CommandXfer (uint32_t instance, flexspi_xfer_t *xfer) |
| FLEXSPI command. More... | |
UpdateLut | |
| status_t | ROM_FLEXSPI_NorFlash_UpdateLut (uint32_t instance, uint32_t seqIndex, const uint32_t *lutBase, uint32_t seqNumber) |
| Configure FLEXSPI Lookup table. More... | |
Device status | |
| status_t | ROM_FLEXSPI_NorFlash_WaitBusy (uint32_t instance, flexspi_nor_config_t *config, bool isParallelMode, uint32_t address) |
| Wait until device is idle. More... | |
ClearCache | |
| void | ROM_FLEXSPI_NorFlash_ClearCache (uint32_t instance) |
| Software reset for the FLEXSPI logic. More... | |
| struct serial_nor_config_option_t |
| struct flexspi_lut_seq_t |
| struct flexspi_dll_time_t |
Data Fields | |
| uint8_t | time_100ps |
| Data valid time, in terms of 100ps. | |
| uint8_t | delay_cells |
| Data valid time, in terms of delay cells. | |
| struct flexspi_mem_config_t |
Data Fields | |
| uint32_t | tag |
| [0x000-0x003] Tag, fixed value 0x42464346UL | |
| uint32_t | version |
| [0x004-0x007] Version,[31:24] -'V', [23:16] - Major, [15:8] - Minor, [7:0] - bugfix | |
| uint32_t | reserved0 |
| [0x008-0x00b] Reserved for future use | |
| uint8_t | readSampleClkSrc |
| [0x00c-0x00c] Read Sample Clock Source, valid value: 0/1/3 | |
| uint8_t | csHoldTime |
| [0x00d-0x00d] Data hold time, default value: 3 | |
| uint8_t | csSetupTime |
| [0x00e-0x00e] Date setup time, default value: 3 | |
| uint8_t | columnAddressWidth |
| [0x00f-0x00f] Column Address with, for HyperBus protocol, it is fixed to 3, For Serial NAND, need to refer to datasheet | |
| uint8_t | deviceModeCfgEnable |
| [0x010-0x010] Device Mode Configure enable flag, 1 - Enable, 0 - Disable | |
| uint8_t | deviceModeType |
| [0x011-0x011] Specify the configuration command type:Quad Enable, DPI/QPI/OPI switch, Generic configuration, etc. More... | |
| uint16_t | waitTimeCfgCommands |
| [0x012-0x013] Wait time for all configuration commands, unit: 100us, Used for DPI/QPI/OPI switch or reset command | |
| flexspi_lut_seq_t | deviceModeSeq |
| [0x014-0x017] Device mode sequence info, [7:0] - LUT sequence id, [15:8] - LUt sequence number, [31:16] Reserved | |
| uint32_t | deviceModeArg |
| [0x018-0x01b] Argument/Parameter for device configuration | |
| uint8_t | configCmdEnable |
| [0x01c-0x01c] Configure command Enable Flag, 1 - Enable, 0 - Disable | |
| uint8_t | configModeType [3] |
| [0x01d-0x01f] Configure Mode Type, similar as deviceModeTpe | |
| flexspi_lut_seq_t | configCmdSeqs [3] |
| [0x020-0x02b] Sequence info for Device Configuration command, similar as deviceModeSeq | |
| uint32_t | reserved1 |
| [0x02c-0x02f] Reserved for future use | |
| uint32_t | configCmdArgs [3] |
| [0x030-0x03b] Arguments/Parameters for device Configuration commands | |
| uint32_t | reserved2 |
| [0x03c-0x03f] Reserved for future use | |
| uint32_t | controllerMiscOption |
| [0x040-0x043] Controller Misc Options, see Misc feature bit definitions for more details | |
| uint8_t | deviceType |
| [0x044-0x044] Device Type: See Flash Type Definition for more details | |
| uint8_t | sflashPadType |
| [0x045-0x045] Serial Flash Pad Type: 1 - Single, 2 - Dual, 4 - Quad, 8 - Octal | |
| uint8_t | serialClkFreq |
| [0x046-0x046] Serial Flash Frequency, device specific definitions. More... | |
| uint8_t | lutCustomSeqEnable |
| [0x047-0x047] LUT customization Enable, it is required if the program/erase cannot be done using 1 LUT sequence, currently, only applicable to HyperFLASH | |
| uint32_t | reserved3 [2] |
| [0x048-0x04f] Reserved for future use | |
| uint32_t | sflashA1Size |
| [0x050-0x053] Size of Flash connected to A1 | |
| uint32_t | sflashA2Size |
| [0x054-0x057] Size of Flash connected to A2 | |
| uint32_t | sflashB1Size |
| [0x058-0x05b] Size of Flash connected to B1 | |
| uint32_t | sflashB2Size |
| [0x05c-0x05f] Size of Flash connected to B2 | |
| uint32_t | csPadSettingOverride |
| [0x060-0x063] CS pad setting override value | |
| uint32_t | sclkPadSettingOverride |
| [0x064-0x067] SCK pad setting override value | |
| uint32_t | dataPadSettingOverride |
| [0x068-0x06b] data pad setting override value | |
| uint32_t | dqsPadSettingOverride |
| [0x06c-0x06f] DQS pad setting override value | |
| uint32_t | timeoutInMs |
| [0x070-0x073] Timeout threshold for read status command | |
| uint32_t | commandInterval |
| [0x074-0x077] CS deselect interval between two commands | |
| flexspi_dll_time_t | dataValidTime [2] |
| [0x078-0x07b] CLK edge to data valid time for PORT A and PORT B | |
| uint16_t | busyOffset |
| [0x07c-0x07d] Busy offset, valid value: 0-31 | |
| uint16_t | busyBitPolarity |
| [0x07e-0x07f] Busy flag polarity, 0 - busy flag is 1 when flash device is busy, 1 - busy flag is 0 when flash device is busy | |
| uint32_t | lookupTable [64] |
| [0x080-0x17f] Lookup table holds Flash command sequences | |
| flexspi_lut_seq_t | lutCustomSeq [12] |
| [0x180-0x1af] Customizable LUT Sequences | |
| uint32_t | reserved4 [4] |
| [0x1b0-0x1bf] Reserved for future use | |
| uint8_t flexspi_mem_config_t::deviceModeType |
| uint8_t flexspi_mem_config_t::serialClkFreq |
See System Boot Chapter for more details
| struct flexspi_nor_config_t |
Data Fields | |
| flexspi_mem_config_t | memConfig |
| Common memory configuration info via FLEXSPI. | |
| uint32_t | pageSize |
| Page size of Serial NOR. | |
| uint32_t | sectorSize |
| Sector size of Serial NOR. | |
| uint8_t | ipcmdSerialClkFreq |
| Clock frequency for IP command. | |
| uint8_t | isUniformBlockSize |
| Sector/Block size is the same. | |
| uint8_t | isDataOrderSwapped |
| Data order (D0, D1, D2, D3) is swapped (D1,D0, D3, D2) | |
| uint8_t | reserved0 [1] |
| Reserved for future use. | |
| uint8_t | serialNorType |
| Serial NOR Flash type: 0/1/2/3. | |
| uint8_t | needExitNoCmdMode |
| Need to exit NoCmd mode before other IP command. | |
| uint8_t | halfClkForNonReadCmd |
| Half the Serial Clock for non-read command: true/false. | |
| uint8_t | needRestoreNoCmdMode |
| Need to Restore NoCmd mode after IP command execution. | |
| uint32_t | blockSize |
| Block size. | |
| uint32_t | reserve2 [11] |
| Reserved for future use. | |
| struct flexspi_xfer_t |
Data Fields | |
| flexspi_operation_t | operation |
| FLEXSPI operation. | |
| uint32_t | baseAddress |
| FLEXSPI operation base address. | |
| uint32_t | seqId |
| Sequence Id. | |
| uint32_t | seqNum |
| Sequence Number. | |
| bool | isParallelModeEnable |
| Is a parallel transfer. | |
| uint32_t * | txBuffer |
| Tx buffer. | |
| uint32_t | txSize |
| Tx size in bytes. | |
| uint32_t * | rxBuffer |
| Rx buffer. | |
| uint32_t | rxSize |
| Rx size in bytes. | |
| #define FSL_ROM_ROMAPI_VERSION (MAKE_VERSION(1U, 1U, 2U)) |
| #define FSL_ROM_FLEXSPINOR_DRIVER_VERSION (MAKE_VERSION(1U, 7U, 0U)) |
| #define FSL_ROM_HAS_FLEXSPINOR_API (1) |
| #define FSL_ROM_HAS_RUNBOOTLOADER_API (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_GET_CONFIG (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_FLASH_INIT (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_SECTOR (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_BLOCK (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_ERASE_ALL (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_READ (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_UPDATE_LUT (1) |
| #define FSL_ROM_FLEXSPINOR_API_HAS_FEATURE_CMD_XFER (1) |
| #define kROM_StatusGroup_FLEXSPINOR 201U |
| #define FLEXSPI_CFG_BLK_TAG (0x42464346UL) |
ascii "FCFB" Big Endian
| #define NOR_CMD_LUT_SEQ_IDX_READ 0U |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| anonymous enum |
| enum _flexspi_nor_status |
| enum flexspi_operation_t |
| void ROM_API_Init | ( | void | ) |
Get the bootloader api entry address.
| void ROM_RunBootloader | ( | void * | arg | ) |
| arg | A pointer to the storage for the bootloader param. refer to System Boot Chapter in device reference manual for details. |
| status_t ROM_FLEXSPI_NorFlash_GetConfig | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| serial_nor_config_option_t * | option | ||
| ) |
| instance | storage the instance of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| option | A pointer to the storage Serial NOR Configuration Option Context. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_Init | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config | ||
| ) |
This function checks and initializes the FLEXSPI module for the other FLEXSPI APIs.
| instance | storage the instance of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_ProgramPage | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| uint32_t | dst_addr, | ||
| const uint32_t * | src | ||
| ) |
This function programs the NOR flash memory with the dest address for a given flash area as determined by the dst address and the length.
| instance | storage the instance of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| dst_addr | A pointer to the desired flash memory to be programmed. |
| src | A pointer to the source buffer of data that is to be programmed into the NOR flash. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_Read | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| uint32_t * | dst, | ||
| uint32_t | start, | ||
| uint32_t | lengthInBytes | ||
| ) |
This function read the NOR flash memory with the start address for a given flash area as determined by the dst address and the length.
| instance | storage the instance of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| dst | A pointer to the dest buffer of data that is to be read from the NOR flash. |
| start | The start address of the desired NOR flash memory to be read. |
| lengthInBytes | The length, given in bytes to be read. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_Erase | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| uint32_t | start, | ||
| uint32_t | length | ||
| ) |
This function erases the appropriate number of flash sectors based on the desired start address and length.
| instance | storage the index of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired NOR flash memory to be erased. |
| length | The length, given in bytes to be erased. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_EraseSector | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| uint32_t | start | ||
| ) |
This function erases one of NOR flash sectors based on the desired address.
| instance | storage the index of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired NOR flash memory to be erased. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_EraseBlock | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| uint32_t | start | ||
| ) |
This function erases one block of NOR flash based on the desired address.
| instance | storage the index of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired NOR flash memory to be erased. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_EraseAll | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config | ||
| ) |
| instance | storage the instance of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | the device timeout |
| status_t ROM_FLEXSPI_NorFlash_CommandXfer | ( | uint32_t | instance, |
| flexspi_xfer_t * | xfer | ||
| ) |
This function is used to perform the command write sequence to the NOR device.
| instance | storage the index of FLEXSPI. |
| xfer | A pointer to the storage FLEXSPI Transfer Context. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| status_t ROM_FLEXSPI_NorFlash_UpdateLut | ( | uint32_t | instance, |
| uint32_t | seqIndex, | ||
| const uint32_t * | lutBase, | ||
| uint32_t | seqNumber | ||
| ) |
| instance | storage the index of FLEXSPI. |
| seqIndex | storage the sequence Id. |
| lutBase | A pointer to the look-up-table for command sequences. |
| seqNumber | storage sequence number. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| status_t ROM_FLEXSPI_NorFlash_WaitBusy | ( | uint32_t | instance, |
| flexspi_nor_config_t * | config, | ||
| bool | isParallelMode, | ||
| uint32_t | address | ||
| ) |
| instance | Indicates the index of FLEXSPI. |
| config | A pointer to the storage for the driver runtime state |
| isParallelMode | Indicates whether NOR flash is in parallel mode. |
| address | Indicates the operation(erase/program/read) address for serial NOR flash. |
| kStatus_Success | Api was executed successfully. |
| kStatus_InvalidArgument | A invalid argument is provided. |
| kStatus_ROM_FLEXSPI_SequenceExecutionTimeout | Sequence Execution timeout. |
| kStatus_ROM_FLEXSPI_InvalidSequence | A invalid Sequence is provided. |
| kStatus_ROM_FLEXSPI_DeviceTimeout | Device timeout. |
| void ROM_FLEXSPI_NorFlash_ClearCache | ( | uint32_t | instance | ) |
This function sets the software reset flags for both AHB and buffer domain and resets both AHB buffer and also IP FIFOs.
| instance | storage the index of FLEXSPI. |