![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
Modules | |
ftfx adapter | |
Macros | |
#define | FTFx_DRIVER_HAS_FLASH1_SUPPORT (0U) |
Indicates whether the secondary flash is supported in the Flash driver. | |
FTFx configuration | |
#define | FTFx_DRIVER_IS_FLASH_RESIDENT 1U |
Flash driver location. More... | |
#define | FTFx_DRIVER_IS_EXPORTED 0U |
Flash Driver Export option. More... | |
Secondary flash configuration | |
#define | FTFx_FLASH1_HAS_PROT_CONTROL (0U) |
Indicates whether the secondary flash has its own protection register in flash module. More... | |
#define | FTFx_FLASH1_HAS_XACC_CONTROL (0U) |
Indicates whether the secondary flash has its own Execute-Only access register in flash module. More... | |
#define FTFx_DRIVER_IS_FLASH_RESIDENT 1U |
Used for the flash resident application.
#define FTFx_DRIVER_IS_EXPORTED 0U |
Used for the MCUXpresso SDK application.
#define FTFx_FLASH1_HAS_PROT_CONTROL (0U) |
#define FTFx_FLASH1_HAS_XACC_CONTROL (0U) |