MCUXpresso SDK API Reference Manual  Rev 2.16.100
NXP Semiconductors
 All Data Structures Functions Variables Typedefs Enumerations Enumerator Groups Pages
PLU: Programmable Logic Unit

Overview

The MCUXpresso SDK provides a peripheral driver for the Programmable Logic Unit module of MCUXpresso SDK devices.

Function groups

The PLU driver supports the creation of small combinatorial and/or sequential logic networks including simple state machines.

Initialization and de-initialization

The function PLU_Init() enables the PLU clock and reset the module.

The function PIT_Deinit() gates the PLU clock.

Set input/output source and Truth Table

The function PLU_SetLutInputSource() sets the input source for the LUT element.

The function PLU_SetOutputSource() sets output source of the PLU module.

The function PLU_SetLutTruthTable() sets the truth table for the LUT element.

Read current Output State

The function PLU_ReadOutputState() reads the current state of the 8 designated PLU Outputs.

Wake-up/Interrupt Control

The function PLU_EnableWakeIntRequest() enables the wake-up/interrupt request on a PLU output pin with a optional configuration to eliminate the glitches. The function PLU_GetDefaultWakeIntConfig() gets the default configuration which can be used in a case with a given PLU_CLKIN.

The function PLU_LatchInterrupt() latches the interrupt and it can be cleared by function PLU_ClearLatchedInterrupt().

Typical use case

PLU combination example

Create a simple combinatorial logic network to control the LED. Refer to the driver examples codes located at <SDK_ROOT>/boards/<BOARD>/driver_examples/plu/combination

Data Structures

struct  plu_wakeint_config_t
 Wake configuration. More...
 

Enumerations

enum  plu_lut_index_t {
  kPLU_LUT_0 = 0U,
  kPLU_LUT_1 = 1U,
  kPLU_LUT_2 = 2U,
  kPLU_LUT_3 = 3U,
  kPLU_LUT_4 = 4U,
  kPLU_LUT_5 = 5U,
  kPLU_LUT_6 = 6U,
  kPLU_LUT_7 = 7U,
  kPLU_LUT_8 = 8U,
  kPLU_LUT_9 = 9U,
  kPLU_LUT_10 = 10U,
  kPLU_LUT_11 = 11U,
  kPLU_LUT_12 = 12U,
  kPLU_LUT_13 = 13U,
  kPLU_LUT_14 = 14U,
  kPLU_LUT_15 = 15U,
  kPLU_LUT_16 = 16U,
  kPLU_LUT_17 = 17U,
  kPLU_LUT_18 = 18U,
  kPLU_LUT_19 = 19U,
  kPLU_LUT_20 = 20U,
  kPLU_LUT_21 = 21U,
  kPLU_LUT_22 = 22U,
  kPLU_LUT_23 = 23U,
  kPLU_LUT_24 = 24U,
  kPLU_LUT_25 = 25U
}
 Index of LUT. More...
 
enum  plu_lut_in_index_t {
  kPLU_LUT_IN_0 = 0U,
  kPLU_LUT_IN_1 = 1U,
  kPLU_LUT_IN_2 = 2U,
  kPLU_LUT_IN_3 = 3U,
  kPLU_LUT_IN_4 = 4U
}
 Inputs of LUT. More...
 
enum  plu_lut_input_source_t {
  kPLU_LUT_IN_SRC_PLU_IN_0 = 0U,
  kPLU_LUT_IN_SRC_PLU_IN_1 = 1U,
  kPLU_LUT_IN_SRC_PLU_IN_2 = 2U,
  kPLU_LUT_IN_SRC_PLU_IN_3 = 3U,
  kPLU_LUT_IN_SRC_PLU_IN_4 = 4U,
  kPLU_LUT_IN_SRC_PLU_IN_5 = 5U,
  kPLU_LUT_IN_SRC_LUT_OUT_0 = 6U,
  kPLU_LUT_IN_SRC_LUT_OUT_1 = 7U,
  kPLU_LUT_IN_SRC_LUT_OUT_2 = 8U,
  kPLU_LUT_IN_SRC_LUT_OUT_3 = 9U,
  kPLU_LUT_IN_SRC_LUT_OUT_4 = 10U,
  kPLU_LUT_IN_SRC_LUT_OUT_5 = 11U,
  kPLU_LUT_IN_SRC_LUT_OUT_6 = 12U,
  kPLU_LUT_IN_SRC_LUT_OUT_7 = 13U,
  kPLU_LUT_IN_SRC_LUT_OUT_8 = 14U,
  kPLU_LUT_IN_SRC_LUT_OUT_9 = 15U,
  kPLU_LUT_IN_SRC_LUT_OUT_10 = 16U,
  kPLU_LUT_IN_SRC_LUT_OUT_11 = 17U,
  kPLU_LUT_IN_SRC_LUT_OUT_12 = 18U,
  kPLU_LUT_IN_SRC_LUT_OUT_13 = 19U,
  kPLU_LUT_IN_SRC_LUT_OUT_14 = 20U,
  kPLU_LUT_IN_SRC_LUT_OUT_15 = 21U,
  kPLU_LUT_IN_SRC_LUT_OUT_16 = 22U,
  kPLU_LUT_IN_SRC_LUT_OUT_17 = 23U,
  kPLU_LUT_IN_SRC_LUT_OUT_18 = 24U,
  kPLU_LUT_IN_SRC_LUT_OUT_19 = 25U,
  kPLU_LUT_IN_SRC_LUT_OUT_20 = 26U,
  kPLU_LUT_IN_SRC_LUT_OUT_21 = 27U,
  kPLU_LUT_IN_SRC_LUT_OUT_22 = 28U,
  kPLU_LUT_IN_SRC_LUT_OUT_23 = 29U,
  kPLU_LUT_IN_SRC_LUT_OUT_24 = 30U,
  kPLU_LUT_IN_SRC_LUT_OUT_25 = 31U,
  kPLU_LUT_IN_SRC_FLIPFLOP_0 = 32U,
  kPLU_LUT_IN_SRC_FLIPFLOP_1 = 33U,
  kPLU_LUT_IN_SRC_FLIPFLOP_2 = 34U,
  kPLU_LUT_IN_SRC_FLIPFLOP_3 = 35U
}
 Available sources of LUT input. More...
 
enum  plu_output_index_t {
  kPLU_OUTPUT_0 = 0U,
  kPLU_OUTPUT_1 = 1U,
  kPLU_OUTPUT_2 = 2U,
  kPLU_OUTPUT_3 = 3U,
  kPLU_OUTPUT_4 = 4U,
  kPLU_OUTPUT_5 = 5U,
  kPLU_OUTPUT_6 = 6U,
  kPLU_OUTPUT_7 = 7U
}
 PLU output multiplexer registers. More...
 
enum  plu_output_source_t {
  kPLU_OUT_SRC_LUT_0 = 0U,
  kPLU_OUT_SRC_LUT_1 = 1U,
  kPLU_OUT_SRC_LUT_2 = 2U,
  kPLU_OUT_SRC_LUT_3 = 3U,
  kPLU_OUT_SRC_LUT_4 = 4U,
  kPLU_OUT_SRC_LUT_5 = 5U,
  kPLU_OUT_SRC_LUT_6 = 6U,
  kPLU_OUT_SRC_LUT_7 = 7U,
  kPLU_OUT_SRC_LUT_8 = 8U,
  kPLU_OUT_SRC_LUT_9 = 9U,
  kPLU_OUT_SRC_LUT_10 = 10U,
  kPLU_OUT_SRC_LUT_11 = 11U,
  kPLU_OUT_SRC_LUT_12 = 12U,
  kPLU_OUT_SRC_LUT_13 = 13U,
  kPLU_OUT_SRC_LUT_14 = 14U,
  kPLU_OUT_SRC_LUT_15 = 15U,
  kPLU_OUT_SRC_LUT_16 = 16U,
  kPLU_OUT_SRC_LUT_17 = 17U,
  kPLU_OUT_SRC_LUT_18 = 18U,
  kPLU_OUT_SRC_LUT_19 = 19U,
  kPLU_OUT_SRC_LUT_20 = 20U,
  kPLU_OUT_SRC_LUT_21 = 21U,
  kPLU_OUT_SRC_LUT_22 = 22U,
  kPLU_OUT_SRC_LUT_23 = 23U,
  kPLU_OUT_SRC_LUT_24 = 24U,
  kPLU_OUT_SRC_LUT_25 = 25U,
  kPLU_OUT_SRC_FLIPFLOP_0 = 26U,
  kPLU_OUT_SRC_FLIPFLOP_1 = 27U,
  kPLU_OUT_SRC_FLIPFLOP_2 = 28U,
  kPLU_OUT_SRC_FLIPFLOP_3 = 29U
}
 Available sources of PLU output. More...
 
enum  _plu_interrupt_mask {
  kPLU_OUTPUT_0_INTERRUPT_MASK = 1 << 0,
  kPLU_OUTPUT_1_INTERRUPT_MASK = 1 << 1,
  kPLU_OUTPUT_2_INTERRUPT_MASK = 1 << 2,
  kPLU_OUTPUT_3_INTERRUPT_MASK = 1 << 3,
  kPLU_OUTPUT_4_INTERRUPT_MASK = 1 << 4,
  kPLU_OUTPUT_5_INTERRUPT_MASK = 1 << 5,
  kPLU_OUTPUT_6_INTERRUPT_MASK = 1 << 6,
  kPLU_OUTPUT_7_INTERRUPT_MASK = 1 << 7
}
 The enumerator of PLU Interrupt. More...
 
enum  plu_wakeint_filter_mode_t {
  kPLU_WAKEINT_FILTER_MODE_BYPASS = 0U,
  kPLU_WAKEINT_FILTER_MODE_1_CLK_PERIOD = 1U,
  kPLU_WAKEINT_FILTER_MODE_2_CLK_PERIOD = 2U,
  kPLU_WAKEINT_FILTER_MODE_3_CLK_PERIOD = 3U
}
 Control input of the PLU, add filtering for glitch. More...
 
enum  plu_wakeint_filter_clock_source_t {
  kPLU_WAKEINT_FILTER_CLK_SRC_1MHZ_LPOSC = 0U,
  kPLU_WAKEINT_FILTER_CLK_SRC_12MHZ_FRO = 1U,
  kPLU_WAKEINT_FILTER_CLK_SRC_ALT = 2U
}
 Clock source for filter mode. More...
 

Driver version

#define FSL_PLU_DRIVER_VERSION   (MAKE_VERSION(2, 2, 1))
 Version 2.2.1.
 

Initialization and deinitialization

void PLU_Init (PLU_Type *base)
 Enable the PLU clock and reset the module. More...
 
void PLU_Deinit (PLU_Type *base)
 Gate the PLU clock. More...
 

Set input/output source and Truth Table

static void PLU_SetLutInputSource (PLU_Type *base, plu_lut_index_t lutIndex, plu_lut_in_index_t lutInIndex, plu_lut_input_source_t inputSrc)
 Set Input source of LUT. More...
 
static void PLU_SetOutputSource (PLU_Type *base, plu_output_index_t outputIndex, plu_output_source_t outputSrc)
 Set Output source of PLU. More...
 
static void PLU_SetLutTruthTable (PLU_Type *base, plu_lut_index_t lutIndex, uint32_t truthTable)
 Set Truth Table of LUT. More...
 

Read current Output State

static uint32_t PLU_ReadOutputState (PLU_Type *base)
 Read the current state of the 8 designated PLU Outputs. More...
 

Wake-up/Interrupt Control

void PLU_GetDefaultWakeIntConfig (plu_wakeint_config_t *config)
 Gets an available pre-defined settings for wakeup/interrupt control. More...
 
void PLU_EnableWakeIntRequest (PLU_Type *base, uint32_t interruptMask, const plu_wakeint_config_t *config)
 Enable PLU outputs wakeup/interrupt request. More...
 
static void PLU_LatchInterrupt (PLU_Type *base)
 Latch an interrupt. More...
 
void PLU_ClearLatchedInterrupt (PLU_Type *base)
 Clear the latched interrupt. More...
 

Data Structure Documentation

struct plu_wakeint_config_t

Data Fields

plu_wakeint_filter_mode_t filterMode
 Filter Mode. More...
 
plu_wakeint_filter_clock_source_t clockSource
 The clock source for filter mode. More...
 

Field Documentation

plu_wakeint_filter_mode_t plu_wakeint_config_t::filterMode
plu_wakeint_filter_clock_source_t plu_wakeint_config_t::clockSource

Enumeration Type Documentation

Enumerator
kPLU_LUT_0 

5-input Look-up Table 0

kPLU_LUT_1 

5-input Look-up Table 1

kPLU_LUT_2 

5-input Look-up Table 2

kPLU_LUT_3 

5-input Look-up Table 3

kPLU_LUT_4 

5-input Look-up Table 4

kPLU_LUT_5 

5-input Look-up Table 5

kPLU_LUT_6 

5-input Look-up Table 6

kPLU_LUT_7 

5-input Look-up Table 7

kPLU_LUT_8 

5-input Look-up Table 8

kPLU_LUT_9 

5-input Look-up Table 9

kPLU_LUT_10 

5-input Look-up Table 10

kPLU_LUT_11 

5-input Look-up Table 11

kPLU_LUT_12 

5-input Look-up Table 12

kPLU_LUT_13 

5-input Look-up Table 13

kPLU_LUT_14 

5-input Look-up Table 14

kPLU_LUT_15 

5-input Look-up Table 15

kPLU_LUT_16 

5-input Look-up Table 16

kPLU_LUT_17 

5-input Look-up Table 17

kPLU_LUT_18 

5-input Look-up Table 18

kPLU_LUT_19 

5-input Look-up Table 19

kPLU_LUT_20 

5-input Look-up Table 20

kPLU_LUT_21 

5-input Look-up Table 21

kPLU_LUT_22 

5-input Look-up Table 22

kPLU_LUT_23 

5-input Look-up Table 23

kPLU_LUT_24 

5-input Look-up Table 24

kPLU_LUT_25 

5-input Look-up Table 25

5 input present for each LUT.

Enumerator
kPLU_LUT_IN_0 

LUT input 0.

kPLU_LUT_IN_1 

LUT input 1.

kPLU_LUT_IN_2 

LUT input 2.

kPLU_LUT_IN_3 

LUT input 3.

kPLU_LUT_IN_4 

LUT input 4.

Enumerator
kPLU_LUT_IN_SRC_PLU_IN_0 

Select PLU input 0 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_PLU_IN_1 

Select PLU input 1 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_PLU_IN_2 

Select PLU input 2 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_PLU_IN_3 

Select PLU input 3 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_PLU_IN_4 

Select PLU input 4 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_PLU_IN_5 

Select PLU input 5 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_0 

Select LUT output 0 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_1 

Select LUT output 1 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_2 

Select LUT output 2 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_3 

Select LUT output 3 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_4 

Select LUT output 4 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_5 

Select LUT output 5 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_6 

Select LUT output 6 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_7 

Select LUT output 7 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_8 

Select LUT output 8 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_9 

Select LUT output 9 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_10 

Select LUT output 10 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_11 

Select LUT output 11 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_12 

Select LUT output 12 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_13 

Select LUT output 13 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_14 

Select LUT output 14 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_15 

Select LUT output 15 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_16 

Select LUT output 16 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_17 

Select LUT output 17 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_18 

Select LUT output 18 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_19 

Select LUT output 19 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_20 

Select LUT output 20 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_21 

Select LUT output 21 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_22 

Select LUT output 22 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_23 

Select LUT output 23 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_24 

Select LUT output 24 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_LUT_OUT_25 

Select LUT output 25 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_FLIPFLOP_0 

Select Flip-Flops state 0 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_FLIPFLOP_1 

Select Flip-Flops state 1 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_FLIPFLOP_2 

Select Flip-Flops state 2 to be connected to LUTn Input x.

kPLU_LUT_IN_SRC_FLIPFLOP_3 

Select Flip-Flops state 3 to be connected to LUTn Input x.

Enumerator
kPLU_OUTPUT_0 

PLU OUTPUT 0.

kPLU_OUTPUT_1 

PLU OUTPUT 1.

kPLU_OUTPUT_2 

PLU OUTPUT 2.

kPLU_OUTPUT_3 

PLU OUTPUT 3.

kPLU_OUTPUT_4 

PLU OUTPUT 4.

kPLU_OUTPUT_5 

PLU OUTPUT 5.

kPLU_OUTPUT_6 

PLU OUTPUT 6.

kPLU_OUTPUT_7 

PLU OUTPUT 7.

Enumerator
kPLU_OUT_SRC_LUT_0 

Select LUT0 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_1 

Select LUT1 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_2 

Select LUT2 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_3 

Select LUT3 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_4 

Select LUT4 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_5 

Select LUT5 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_6 

Select LUT6 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_7 

Select LUT7 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_8 

Select LUT8 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_9 

Select LUT9 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_10 

Select LUT10 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_11 

Select LUT11 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_12 

Select LUT12 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_13 

Select LUT13 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_14 

Select LUT14 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_15 

Select LUT15 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_16 

Select LUT16 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_17 

Select LUT17 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_18 

Select LUT18 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_19 

Select LUT19 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_20 

Select LUT20 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_21 

Select LUT21 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_22 

Select LUT22 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_23 

Select LUT23 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_24 

Select LUT24 output to be connected to PLU output.

kPLU_OUT_SRC_LUT_25 

Select LUT25 output to be connected to PLU output.

kPLU_OUT_SRC_FLIPFLOP_0 

Select Flip-Flops state(0) to be connected to PLU output.

kPLU_OUT_SRC_FLIPFLOP_1 

Select Flip-Flops state(1) to be connected to PLU output.

kPLU_OUT_SRC_FLIPFLOP_2 

Select Flip-Flops state(2) to be connected to PLU output.

kPLU_OUT_SRC_FLIPFLOP_3 

Select Flip-Flops state(3) to be connected to PLU output.

Enumerator
kPLU_OUTPUT_0_INTERRUPT_MASK 

Select PLU output 0 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_1_INTERRUPT_MASK 

Select PLU output 1 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_2_INTERRUPT_MASK 

Select PLU output 2 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_3_INTERRUPT_MASK 

Select PLU output 3 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_4_INTERRUPT_MASK 

Select PLU output 4 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_5_INTERRUPT_MASK 

Select PLU output 5 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_6_INTERRUPT_MASK 

Select PLU output 6 contribute to interrupt/wake-up generation.

kPLU_OUTPUT_7_INTERRUPT_MASK 

Select PLU output 7 contribute to interrupt/wake-up generation.

Enumerator
kPLU_WAKEINT_FILTER_MODE_BYPASS 

Select Bypass mode.

kPLU_WAKEINT_FILTER_MODE_1_CLK_PERIOD 

Filter 1 clock period.

kPLU_WAKEINT_FILTER_MODE_2_CLK_PERIOD 

Filter 2 clock period.

kPLU_WAKEINT_FILTER_MODE_3_CLK_PERIOD 

Filter 3 clock period.

Enumerator
kPLU_WAKEINT_FILTER_CLK_SRC_1MHZ_LPOSC 

Select the 1MHz low-power oscillator as the filter clock.

kPLU_WAKEINT_FILTER_CLK_SRC_12MHZ_FRO 

Select the 12MHz FRO as the filer clock.

kPLU_WAKEINT_FILTER_CLK_SRC_ALT 

Select a third clock source.

Function Documentation

void PLU_Init ( PLU_Type *  base)
Note
This API should be called at the beginning of the application using the PLU driver.
Parameters
basePLU peripheral base address
void PLU_Deinit ( PLU_Type *  base)
Parameters
basePLU peripheral base address
static void PLU_SetLutInputSource ( PLU_Type *  base,
plu_lut_index_t  lutIndex,
plu_lut_in_index_t  lutInIndex,
plu_lut_input_source_t  inputSrc 
)
inlinestatic

Note: An external clock must be applied to the PLU_CLKIN input when using FFs. For each LUT, the slot associated with the output from LUTn itself is tied low.

Parameters
basePLU peripheral base address.
lutIndexLUT index (see plu_lut_index_t typedef enumeration).
lutInIndexLUT input index (see plu_lut_in_index_t typedef enumeration).
inputSrcLUT input source (see plu_lut_input_source_t typedef enumeration).
static void PLU_SetOutputSource ( PLU_Type *  base,
plu_output_index_t  outputIndex,
plu_output_source_t  outputSrc 
)
inlinestatic

Note: An external clock must be applied to the PLU_CLKIN input when using FFs.

Parameters
basePLU peripheral base address.
outputIndexPLU output index (see plu_output_index_t typedef enumeration).
outputSrcPLU output source (see plu_output_source_t typedef enumeration).
static void PLU_SetLutTruthTable ( PLU_Type *  base,
plu_lut_index_t  lutIndex,
uint32_t  truthTable 
)
inlinestatic
Parameters
basePLU peripheral base address.
lutIndexLUT index (see plu_lut_index_t typedef enumeration).
truthTableTruth Table value.
static uint32_t PLU_ReadOutputState ( PLU_Type *  base)
inlinestatic

Note: The PLU bus clock must be re-enabled prior to reading the Outpus Register if PLU bus clock is shut-off.

Parameters
basePLU peripheral base address.
Returns
Current PLU output state value.
void PLU_GetDefaultWakeIntConfig ( plu_wakeint_config_t *  config)

This function initializes the initial configuration structure with an available settings. The default values are:

* config->filterMode = kPLU_WAKEINT_FILTER_MODE_BYPASS;
*
Parameters
configPointer to configuration structure.
void PLU_EnableWakeIntRequest ( PLU_Type *  base,
uint32_t  interruptMask,
const plu_wakeint_config_t *  config 
)

This function enables Any of the eight selected PLU outputs to contribute to an asynchronous wake-up or an interrupt request.

Note: If a PLU_CLKIN is provided, the raw wake-up/interrupt request will be set on the rising-edge of the PLU_CLKIN whenever the raw request signal is high. This registered signal will be glitch-free and just use the default wakeint config by PLU_GetDefaultWakeIntConfig(). If not, have to specify the filter mode and clock source to eliminate the glitches caused by long and widely disparate delays through the network of LUTs making up the PLU. This way may increase power consumption in low-power operating modes and inject delay before the wake-up/interrupt request is generated.

Parameters
basePLU peripheral base address.
interruptMaskPLU interrupt mask (see _plu_interrupt_mask enumeration).
configPointer to configuration structure (see plu_wakeint_config_t typedef enumeration)
static void PLU_LatchInterrupt ( PLU_Type *  base)
inlinestatic

This function latches the interrupt and then it can be cleared with PLU_ClearLatchedInterrupt().

Note: This mode is not compatible with use of the glitch filter. If this bit is set, the FILTER MODE should be set to kPLU_WAKEINT_FILTER_MODE_BYPASS (Bypass Mode) and PLU_CLKIN should be provided. If this bit is set, the wake-up/interrupt request will be set on the rising-edge of PLU_CLKIN whenever the raw wake-up/interrupt signal is high. The request must be cleared by software.

Parameters
basePLU peripheral base address.
void PLU_ClearLatchedInterrupt ( PLU_Type *  base)

This function clears the wake-up/interrupt request flag latched by PLU_LatchInterrupt()

Note: It is not necessary for the PLU bus clock to be enabled in order to write-to or read-back this bit.

Parameters
basePLU peripheral base address.