![]() |
MCUXpresso SDK API Reference Manual
Rev 2.16.100
NXP Semiconductors
|
The ROMAPI driver provides the functionalities to operate the internal Flash.
The ROMAPI driver provides the functionalities to operate the Flash and ROM.
Data Structures | |
| struct | flash_ffr_config_t |
| Flash controller paramter config. More... | |
| struct | flash_config_t |
| Flash driver state information. More... | |
| struct | flash_driver_interface_t |
| Interface for the flash driver. More... | |
| struct | bootloader_tree_t |
| Root of the bootloader API tree. More... | |
Macros | |
| #define | FOUR_CHAR_CODE(a, b, c, d) (((d) << 24) | ((c) << 16) | ((b) << 8) | ((a))) |
| Constructs the four character code for the Flash driver API key. More... | |
| #define | ROM_API_BASE (0x03003fe0u) |
| #define | ROM_API ((bootloader_tree_t *)ROM_API_BASE) |
| #define | FLASH_API (ROM_API->flash_driver) |
Enumerations | |
| enum | flash_property_tag_t { kFLASH_PropertyPflashSectorSize = 0x00U, kFLASH_PropertyPflashTotalSize = 0x01U, kFLASH_PropertyPflashBlockSize = 0x02U, kFLASH_PropertyPflashBlockCount = 0x03U, kFLASH_PropertyPflashBlockBaseAddr = 0x04U, kFLASH_PropertyPflashPageSize = 0x30U, kFLASH_PropertyPflashSystemFreq = 0x31U, kFLASH_PropertyFfrSectorSize = 0x40U, kFLASH_PropertyFfrTotalSize = 0x41U, kFLASH_PropertyFfrBlockBaseAddr = 0x42U, kFLASH_PropertyFfrPageSize = 0x43U } |
| Enumeration for various flash properties. More... | |
| enum | _flash_driver_api_keys { kFLASH_ApiEraseKey = FOUR_CHAR_CODE('l', 'f', 'e', 'k') } |
| Enumeration for Flash driver API keys. More... | |
Driver version | |
| #define | FSL_ROMAPI_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| romapi driver version 2.0.0. More... | |
Flash status | |
| enum | { kStatus_FLASH_Success = MAKE_STATUS(kStatusGroupGeneric, 0), kStatus_FLASH_InvalidArgument = MAKE_STATUS(kStatusGroupGeneric, 4), kStatus_FLASH_SizeError = MAKE_STATUS(kStatusGroupFlashDriver, 0), kStatus_FLASH_AlignmentError, kStatus_FLASH_AddressError = MAKE_STATUS(kStatusGroupFlashDriver, 2), kStatus_FLASH_AccessError, kStatus_FLASH_ProtectionViolation, kStatus_FLASH_CommandFailure, kStatus_FLASH_UnknownProperty = MAKE_STATUS(kStatusGroupFlashDriver, 6), kStatus_FLASH_EraseKeyError = MAKE_STATUS(kStatusGroupFlashDriver, 7) } |
| Flash driver status codes. More... | |
| #define | kStatusGroupGeneric 0 |
| Flash driver status group. More... | |
| #define | kStatusGroupFlashDriver 1 |
| #define | MAKE_STATUS(group, code) ((((group) * 100) + (code))) |
| Constructs a status code value from a group and a code number. More... | |
Flash API | |
| static status_t | FLASH_Init (flash_config_t *config) |
| Initializes the global flash properties structure members. More... | |
| static status_t | FLASH_EraseSector (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, uint32_t key) |
| Erases the flash sectors encompassed by parameters passed into function. More... | |
| static status_t | FLASH_ProgramPhrase (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes) |
| Programs flash phrases with data at locations passed in through parameters. More... | |
| static status_t | FLASH_ProgramPage (flash_config_t *config, uint32_t start, uint8_t *src, uint32_t lengthInBytes) |
| Programs flash page with data at locations passed in through parameters. More... | |
| static status_t | FLASH_VerifyProgram (flash_config_t *config, uint32_t start, uint32_t lengthInBytes, const uint8_t *expectedData, uint32_t *failedAddress, uint32_t *failedData) |
| Verifies programming of the desired flash area. More... | |
| static status_t | FLASH_VerifyErasePhrase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the flash phrases are erased. More... | |
| static status_t | FLASH_VerifyErasePage (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the flash pages are erased. More... | |
| static status_t | FLASH_VerifyEraseSector (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the flash sectors are erased. More... | |
| static status_t | FLASH_GetProperty (flash_config_t *config, flash_property_tag_t whichProperty, uint32_t *value) |
| Returns the desired flash property. More... | |
| static status_t | IFR_VerifyErasePhrase (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the IFR0 phrases are erased. More... | |
| static status_t | IFR_VerifyErasePage (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the IFR0 pages are erased. More... | |
| static status_t | IFR_VerifyEraseSector (flash_config_t *config, uint32_t start, uint32_t lengthInBytes) |
| Verify that the IFR0 sectors are erased. More... | |
| static status_t | FLASH_Read (flash_config_t *config, uint32_t start, uint8_t *dest, uint32_t lengthInBytes) |
| Reads flash at locations passed in through parameters. More... | |
| static uint32_t | ROMAPI_GetVersion (void) |
| Get ROM API version. More... | |
| static void | ROMAPI_RunBootloader (void *arg) |
| Run the Bootloader API to force into the ISP mode base on the user arg. More... | |
| static void | ROMAPI_GetUUID (uint8_t *uuid) |
| Get the UUID. More... | |
| struct flash_ffr_config_t |
| struct flash_config_t |
An instance of this structure is allocated by the user of the flash driver and passed into each of the driver APIs.
Data Fields | |
| uint32_t | PFlashBlockBase |
| A base address of the first PFlash block. | |
| uint32_t | PFlashTotalSize |
| The size of the combined PFlash block. More... | |
| uint32_t | PFlashBlockCount |
| A number of PFlash blocks. More... | |
| uint32_t | PFlashPageSize |
| The size in bytes of a page of PFlash. More... | |
| uint32_t | PFlashSectorSize |
| The size in bytes of a sector of PFlash. More... | |
| uint32_t flash_config_t::PFlashTotalSize |
| uint32_t flash_config_t::PFlashBlockCount |
| uint32_t flash_config_t::PFlashPageSize |
| uint32_t flash_config_t::PFlashSectorSize |
| struct flash_driver_interface_t |
| struct bootloader_tree_t |
An instance of this struct resides in read-only memory in the bootloader. It provides a user application access to APIs exported by the bootloader.
Data Fields | |
| void(* | run_bootloader )(void *arg) |
| Function to start the bootloader executing. More... | |
| const flash_driver_interface_t * | flash_driver |
| Internal Flash driver API. More... | |
| void(* bootloader_tree_t::run_bootloader)(void *arg) |
| const flash_driver_interface_t* bootloader_tree_t::flash_driver |
| #define FSL_ROMAPI_DRIVER_VERSION (MAKE_VERSION(2, 0, 0)) |
| #define kStatusGroupGeneric 0 |
| #define MAKE_STATUS | ( | group, | |
| code | |||
| ) | ((((group) * 100) + (code))) |
| #define FOUR_CHAR_CODE | ( | a, | |
| b, | |||
| c, | |||
| d | |||
| ) | (((d) << 24) | ((c) << 16) | ((b) << 8) | ((a))) |
| #define ROM_API_BASE (0x03003fe0u) |
ROM API base address
| #define ROM_API ((bootloader_tree_t *)ROM_API_BASE) |
ROM API base pointer
| #define FLASH_API (ROM_API->flash_driver) |
FLASH API base pointer
| anonymous enum |
| enum flash_property_tag_t |
|
inlinestatic |
This function checks and initializes the Flash module for the other Flash APIs.
| config | Pointer to the storage for the driver runtime state. |
|
inlinestatic |
This function erases the appropriate number of flash sectors based on the desired start address and length.
| config | The pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be erased. NOTE: The start address need to be 4 Bytes-aligned. |
| lengthInBytes | The length, given in bytes need be 4 Bytes-aligned. |
| key | The value used to validate all flash erase APIs. |
|
inlinestatic |
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be programmed. Must be word-aligned. |
| src | A pointer to the source buffer of data that is to be programmed into the flash. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. |
|
inlinestatic |
This function programs the flash memory with the desired data for a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be programmed. Must be word-aligned. |
| src | A pointer to the source buffer of data that is to be programmed into the flash. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be programmed. Must be word-aligned. |
|
inlinestatic |
This function verifies the data programed in the flash memory using the Flash Program Check Command and compares it to the expected data for a given flash area as determined by the start address and length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. Must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
| expectedData | A pointer to the expected data that is to be verified against. |
| failedAddress | A pointer to the returned failing address. |
| failedData | A pointer to the returned failing data. Some derivatives do not include failed data as part of the FCCOBx registers. In this case, zeros are returned upon failure. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
| config | A pointer to the storage for the driver runtime state. |
| whichProperty | The desired property from the list of properties in enum flash_property_tag_t |
| value | A pointer to the value returned for the desired flash property. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
This function checks the appropriate number of flash sectors based on the desired start address and length to check whether the flash is erased
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be verified. The start address does not need to be sector-aligned but must be word-aligned. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be verified. Must be word-aligned. |
|
inlinestatic |
This function read the flash memory from a given flash area as determined by the start address and the length.
| config | A pointer to the storage for the driver runtime state. |
| start | The start address of the desired flash memory to be read. |
| dest | A pointer to the dest buffer of data that is to be read from the flash. |
| lengthInBytes | The length, given in bytes (not words or long-words), to be read. |
|
inlinestatic |
This function read the ROM API version.
|
inlinestatic |
| arg | Indicates API prototype fields definition. Refer to the above #user_app_boot_invoke_option_t structure |
|
inlinestatic |
| uuid | UUID data array |